Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
there has no FreeMaster plug-in module I installed freemaster version 3.2.7, and tried many methods, but there's nothing under the plug-in module。I'm in a hurry. This is a necessary tool for my work. Can someone help me? Thank you very much. 1.install FreeMASTER "as administrator" or run the "c:\NXP\FreeMASTER 3.2\FreeMASTER\register.bat----no effect!!! PixPin_2026-07-20_20-46-19.png 2. PixPin_2026-07-20_20-36-29.png PixPin_2026-07-20_20-40-48.png Re: there has no FreeMaster plug-in module Hello, as far as I know, the latest Windows update does not change the way the COM+ and ActiveX objects work. This shall not be related. The issue you are facing is strange indeed.  Let's pick up one plug-in (CAN communication) and see its registration details. Run the "command prompt" as administrator again, then cd to "c:\NXP\FreeMASTER 3.2\FreeMASTER" and use the regsvr32 command without the /s (silent) option: regsvr32 plugins/can/focpgi.dll The confirmation shall appear: MichalH_1-1784615468404.png Then in the same Command Prompt console, start the Registry Editor by command: regedit It will take some time (can be few minutes) then the editor will appear. Navigate to  Computer\HKEY_CLASSES_ROOT\WOW6432Node\CLSID\{C10A92C3-7D47-4FDC-94B6-64B8E5C85E01} This entry represents the FreeMASTER-over-CAN plugin (focpgi.dll). It shall be present in the registry. MichalH_0-1784615359152.png You can check the InprocServer32 entry points to the correct focpgi.dll file.  MichalH_2-1784615691533.png The "Implemented Categories" ID is the one FreeMASTER uses to locate all plug ins using Windows COM Category API. Just to be sure the plug-in category exist, please check the Computer\HKEY_CLASSES_ROOT\Component Categories\{48A185C0-FFDB-11D3-80E3-00C04F176153} key in the Registry editor, you shall see the "MCB Communication Plugins" text value: MichalH_3-1784615997310.png Another experiment would be to remove the /s switch from register.bat script and run it. You shall see a registration confirmation box for each DLL.  Please share the respective screenshots or errors. Thank you for your cooperation. Regards, Michal Re: there has no FreeMaster plug-in module If someone can help me solve this problem, I will treat him to coffee. Re: there has no FreeMaster plug-in module I have tried installing your method, but the module still hasn't appeared. Is this related to my Windows system being updated to the latest version? ScreenShot_2026-07-21_095319_274.png PixPin_2026-07-21_10-13-18.png Re: there has no FreeMaster plug-in module Hello,  both the installer and the register.bat use the "regsvr32.exe" system utility, which shall be installed by default in any Windows operating system.  First, make sure the regsvr32 utility exists on your system. Just press Win+R and Run the command "regsvr32". MichalH_3-1784558060323.png You should see the a help box like this one: MichalH_0-1784557473602.png If this utility does not work, your computer might have a system restriction applied by your administrator. You will need to get it fixed. If the regsvr32 works normally, let's see what errors the register.bat prints: Open the start menu. Locate the "Command Prompt" application Right-click and select "Run as administrator" (see picture below) In the console, type cd "c:\NXP\FreeMASTER 3.2\FreeMASTER" Run register.bat You should see no errors (like in the picture at the end). If no errors, the plug-ins shall appear in FreeMASTER. If there are any errors, please share it here. MichalH_1-1784557809666.png MichalH_2-1784557992554.png Regards, Michal Re: there has no FreeMaster plug-in module Hello, I've tested again. Currently, that module is still not available. I've removed all the lines containing "/s" in the register.bat file. Are there any other solutions available now? 1.png 2.png 3.png 4.png 5.png Re: there has no FreeMaster plug-in module Hello, to summarize - all plugin registrations finish successfully, but the plugin list in FreeMASTER Options dialog is still empty.  Is there any chance you could test on a different computer?  Also, there are two other utilities which access the plugin list. Please try to run the Remote Server tool ("c:\NXP\FreeMASTER 3.2\FreeMASTER\mcbsvr.exe"). Then press the "Add" button and see if the plug-in list will also be empty: MichalH_0-1784702997668.png A similar can be tried in "Named Connection" manager (c:\NXP\FreeMASTER 3.2\FreeMASTER\pgimgr.exe", then press the "New" button: MichalH_1-1784703133393.png Let me know if any of the two tools would display the plugin list not empty. Thank you, Michal Re: there has no FreeMaster plug-in module I've tried, but it still doesn't work. I have a lot of data on my computer and I don't want to reinstall the system. This is really troublesome.I was functioning normally before, but one day it suddenly stopped being able to connect. 1.png 2.png Re: there has no FreeMaster plug-in module Hello,  I have prepared a small test utility which shall help us detect what is wrong on your machine. Please see "plugin_test.exe" attached below.  Run it on cmd Command Prompt console (no need to run as administrator). Usage: plugin_test [ProgID|CLSID] test# 0 - create and release the component test# 1 - create and call Configure() test# 2 - enumerate all registered McbCommPlugin components (ProgID|CLSID argument is optional for test 2) The test of selected plugin instantiation could pass. Try this: plugin_test.exe 0 MCBPGI.TCPSERIAL.1 Component : MCBPGI.TCPSERIAL.1 CLSID : {ED244618-9103-41BE-B382-E92036BD04FC} Test : 0 [test 0] CoCreateInstance ... [test 0] OK - component created successfully. [test 0] Releasing ... [test 0] Released. Result: PASS The tool can even try to display the plugin configuration dialog: plugin_test.exe 1 MCBPGI.TCPSERIAL.1 And it shall appear: MichalH_0-1784793243679.png Finally, the test 2 does plug-in enumeration similarly to FreeMASTER. It will most likely fail at your side: plugin_test.exe 2 Test : 2 [test 2] Creating StdComponentCategoriesMgr ... [test 2] OK - ICatInformation obtained. [test 2] Enumerating McbCommPlugin classes: [1] {1BB3C904-F1F4-4652-92EE-368716FE1D10} (BDMPGI.DAPCOM.1) [2] {2080BBA8-0641-4306-A956-6BEBB7C75249} (JTAGPGI.CCSCOM.1) [3] {225E034C-1AA6-4EC5-9A6C-A9FA9E890373} (BDMPGI.HCSCOM.1) [4] {30AB7AA1-493A-4DD7-9509-C9C91EFFF0FD} (BDMPGI.PDBDMCOM.1) [5] {5A129680-897E-4014-916D-9B1FE13DE156} (BDMPGI.EONCECOM.1) [6] {6D13CD9D-9F2D-4066-B655-45B54CA7494B} (MCBPGI.NETCOM.1) [7] {7AC03FB7-4792-4F26-8152-92E466276068} (DEMOPGI.DummyCom.1) [8] {80F17965-EDBD-41F1-9182-3C44E04E5794} (BDMPGI.ISYSCOM.1) [9] {8C575DB3-9769-4B66-AB60-C83CEA683E01} (BDMPGI.JLINKCOM.1) [10] {C10A92C3-7D47-4FDC-94B6-64B8E5C85E01} (FOCPGI.FocCom.1) [11] {C10A92C4-7D47-4FDC-94B6-64B8E5C85E01} (FOLPGI.FolCom.1) [12] {ED244616-9103-41BE-B382-E92036BD04FC} (MCBPGI.STDCOM.1) [13] {ED244617-9103-41BE-B382-E92036BD04FC} (MCBPGI.HTTPCOM.1) [14] {ED244618-9103-41BE-B382-E92036BD04FC} (MCBPGI.TCPSERIAL.1) [test 2] Total: 14 plug-in(s) found. Result: PASS Thank you for your cooperation, Michal Re: there has no FreeMaster plug-in module Hello thanks for keeping trying. Let me summarize the facts - translated a bit to Windows programming API as used in FreeMASTER: The API EnumClassesOfCategories() returns empty list even if components are registered properly with all registry entries and even if executed with administrator rights. The EnumClassesOfCategories() return S_OK but the Next() called on the returned iterator does not enumerate anything. Both the component DLLs and the app which enumerates them are compiled as 32bit code. This issue is only observed on a single computer, many other computers work fine. The CoCreateInstance on the target CLSID work well even on this problematic computer. I have to admit I do not know what could be the reason. Some internet sources recommend to try un-registering and then registering the Windows component manager. So please try this in cmd under administrator and then restart the system: regsvr32 /u comcat.dll regsvr32 comcat.dll regsvr32 /u c:\Windows\SysWOW64\comcat.dll regsvr32 c:\Windows\SysWOW64\comcat.dll You should get a confirmation box for each command. If this does not help, I will continue investigation. Thanks, Michal Re: there has no FreeMaster plug-in module Thanks for making the experiment. Did any dialog appear in the "test 1" started like this:  plugin_test.exe 1 MCBPGI.TCPSERIAL.1 Also, can you please run the test 2 in a command prompt which was started "As administrator" ? plugin_test.exe 2 Thank you, Michal Re: there has no FreeMaster plug-in module I tested it, but it didn't work. 1.png 2.png 3.png Re: there has no FreeMaster plug-in module 1. The plugin_test.exe 1 MCBPGI.TCPSERIAL.1 has a dialog box. 2. The plugin_test.exe 2 has been run with administrator privileges. 1.png 2.png Re: there has no FreeMaster plug-in module Thank you very much for your assistance during this period, but it didn't work this time either.
查看全文
Flash 配置混乱 RT1176 八路 DDR 您好,恩智浦 我在配置Macronix Octal DDR模式的闪存时遇到了一些问题。 我正在基于 NXP FMU-6XRT 参考设计的定制板上使用 PX4 代码栈。我使用的是 MX25UM51245G 而不是 MX25UM51345G,但这两个部件之间的差异很小。 我尝试在 Macronix 八进制 DDR 模式下运行它,并启用 DQS 外部采样,采样频率至少为 100MHz。参考设计运行频率为 200MHz。启动内存配置即使在 166MHz 的频率下也能成功测试所需配置的内存。 我尝试的配置是以下默认配置。第一个程序“g_flash_config”可以成功启动、写入、读取等,但对于软件来说并不理想。"g_flash_fast_config" 失败。 我尝试在“fast_config”的DTR模式下将频率降低到166MHz、133MHz、50MHz和30MHz,但都没有效果。 我尝试使用从启动内存配置生成的 FCB,但由于结构布局存在一些差异,因此很难将其应用于 PX4 代码。 我也尝试过 csHoldTime、csSetupTime 和 dataValidTime 的不同组合,但都没有结果。 我尝试在低频 DTR 八进制中使用 DQS 内部模式,但也没有成功。 接下来我还可以尝试什么? #include /**************************************************************************** * Public Data ****************************************************************************/ locate_data(".boot_hdr.conf") const struct flexspi_nor_config_s g_flash_config = { .memConfig = { #if !defined(CONFIG_BOARD_BOOTLOADER_INVALID_FCB) .tag = FLEXSPI_CFG_BLK_TAG, #else .tag = 0xffffffffL, #endif .version = FLEXSPI_CFG_BLK_VERSION, .readSampleClksrc=kFlexSPIReadSampleClk_LoopbackInternally, .csHoldTime = 1, .csSetupTime = 1, .deviceModeCfgEnable = 1, .deviceModeType = kDeviceConfigCmdType_Generic, .waitTimeCfgCommands = 1, .controllerMiscOption = (1u << kFlexSpiMiscOffset_SafeConfigFreqEnable), .deviceType = kFlexSpiDeviceType_SerialNOR, .sflashPadType = kSerialFlash_1Pad, .serialClkFreq = kFlexSpiSerialClk_100MHz, .sflashA1Size = 64ul * 1024u * 1024u, .dataValidTime = { [0] = {.time_100ps = 0}, }, .busyOffset = 0u, .busyBitPolarity = 0u, .lookupTable = { /* Read Dedicated 3Byte Address Read(0x03), 24bit address */ [0 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x03, RADDR_SDR, FLEXSPI_1PAD, 0x18), //0x871187ee, [0 + 1] = FLEXSPI_LUT_SEQ(READ_SDR, FLEXSPI_1PAD, 0x04, STOP_EXE, FLEXSPI_1PAD, 0),//0xb3048b20 }, }, .pageSize = 256u, .sectorSize = 4u * 1024u, .blockSize = 64u * 1024u, .isUniformBlockSize = false, .ipcmdSerialClkFreq = 1, .serialNorType = 2, .reserve2[0] = 0x7008200, }; const struct flexspi_nor_config_s g_flash_fast_config = { .memConfig = { .tag = FLEXSPI_CFG_BLK_TAG, .version = FLEXSPI_CFG_BLK_VERSION, .readSampleClksrc=kFlexSPIReadSampleClk_LoopbackInternally, .csHoldTime = 3, .csSetupTime = 3, .deviceModeCfgEnable = 1, .deviceModeType = kDeviceConfigCmdType_Spi2Xpi, .waitTimeCfgCommands = 1, .deviceModeSeq = { .seqNum = 1, .seqId = 6, /* See Lookup table for more details */ .reserved = 0, }, .deviceModeArg = 2, /* Enable OPI DDR mode */ .controllerMiscOption = (1u << kFlexSpiMiscOffset_SafeConfigFreqEnable) | (1u << kFlexSpiMiscOffset_DdrModeEnable), .deviceType = kFlexSpiDeviceType_SerialNOR, .sflashPadType = kSerialFlash_8Pads, .serialClkFreq = kFlexSpiSerialClk_133MHz, .sflashA1Size = 64ul * 1024u * 1024u, .dataValidTime = { [0] = {.time_100ps = 10}, }, .busyOffset = 0u, .busyBitPolarity = 0u, .lookupTable = { /* Read */// EEH+11H+32bit addr+20dummy cycles+ 4Bytes read data /* Macronix manual says 20 dummy cycles @ 200Mhz, FlexSPI peripheral Operand value needs to be 2N in DDR mode hence 0x28 */ [0 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0xEE, CMD_DDR, FLEXSPI_8PAD, 0x11), //0x871187ee, [0 + 1] = FLEXSPI_LUT_SEQ(RADDR_DDR, FLEXSPI_8PAD, 0x20, DUMMY_DDR, FLEXSPI_8PAD, 0x28),//0xb3288b20, [0 + 2] = FLEXSPI_LUT_SEQ(READ_DDR, FLEXSPI_8PAD, 0x04, STOP_EXE, FLEXSPI_1PAD, 0x00), //0xa704, /* Read status */ [4 * 2 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x05, CMD_DDR, FLEXSPI_8PAD, 0xfa), [4 * 2 + 1] = FLEXSPI_LUT_SEQ(RADDR_DDR, FLEXSPI_8PAD, 0x20, DUMMY_DDR, FLEXSPI_8PAD, 0x04), [4 * 2 + 2] = FLEXSPI_LUT_SEQ(READ_DDR, FLEXSPI_8PAD, 0x04, STOP_EXE, FLEXSPI_1PAD, 0x00), /* Write enable SPI *///06h [4 * 3 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06, STOP_EXE, FLEXSPI_1PAD, 0x00),//0x00000406, /* Write enable OPI SPI *///06h [4 * 4 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x06, CMD_DDR, FLEXSPI_8PAD, 0xF9), /* Erase sector */ [4 * 5 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x21, CMD_DDR, FLEXSPI_8PAD, 0xDE), [4 * 5 + 1] = FLEXSPI_LUT_SEQ(RADDR_DDR, FLEXSPI_8PAD, 0x20, STOP_EXE, FLEXSPI_1PAD, 0x00), /*Write Configuration Register 2 =01, Enable OPI DDR mode*/ //72H +32bit address + CR20x00000000 = 0x01 [4 * 6 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x72, CMD_SDR, FLEXSPI_1PAD, 0x00),//0x04000472, [4 * 6 + 1] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x00, CMD_SDR, FLEXSPI_1PAD, 0x00),//0x04000400, [4 * 6 + 2] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x00, WRITE_SDR, FLEXSPI_1PAD, 0x01),//0x20010400, /*Page program*/ [4 * 9 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x12, CMD_DDR, FLEXSPI_8PAD, 0xED),//0x87ed8712, [4 * 9 + 1] = FLEXSPI_LUT_SEQ(RADDR_DDR, FLEXSPI_8PAD, 0x20, WRITE_DDR, FLEXSPI_8PAD, 0x04),//0xa3048b20, }, }, .pageSize = 256u, .sectorSize = 4u * 1024u, .blockSize = 64u * 1024u, .isUniformBlockSize = false, .ipcmdSerialClkFreq = 1, .serialNorType = 2, .reserve2[0] = 0x7008200, }; Re: Flash configuration confusion RT1176 Octal DDR 你好@SimonHugr , 如果您计划使用 DDR 模式,请记住还必须考虑字节交换配置。本文提供了一些有用的信息,说明在使用 DDR 模式时,MX25UM51245GXDI00 的字节交换为何如此重要。 我强烈建议使用启动内存配置来生成 FCB,安全配置工具v26.6 提供了 MX25UM51245G 的模板,可以作为您配置的良好起点。另外,您可能也知道,这个工具可以帮助您测试配置。 此外,我建议查看这篇社区帖子,特别是从第 15 点开始的步骤。该部分更详细地解释了安全配置工具如何生成启动内存配置,并有助于阐明该工具生成的参数和输出。 最后,您可以使用 flexspi_nor_polling_transfer_cm7 示例来验证生成的 FCB,并在继续进行启动配置之前验证读取和写入操作是否正常工作。 BR 哈比卜 Re: Flash configuration confusion RT1176 Octal DDR 很遗憾,目前还没有结果。我仍然认为这与数据顺序互换有关,我可能漏掉了一些配置字节…… Re: Flash configuration confusion RT1176 Octal DDR 谢谢你,马斯米塞姆 事实上,我注意到例如数据应该互换一下。我将再次检查我的查找表。 Re: Flash configuration confusion RT1176 Octal DDR 参考此帖: https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Internal-Boot-from-Flash-memory-not-starting-on-imxRT1176-custom/mp/1830699 我应该通过编辑 misc 选项来交换数据顺序,根据 Zephyr RTOS 的说明(https://github.com/zephyrproject-rtos/hal_nxp/blob/3a36ee1f8b9fc2168fc0bf80377ace8298292993/mcux/mcux-sdk-ng/devices/RT/RT1170/MIMXRT1176/drivers/romapi/fsl_romapi.h#L340-L355 ) 数据交换字节已经插入,但我感觉好像漏掉了什么。 .pageSize = 256u, .sectorSize = 4u * 1024u, .blockSize = 64u * 1024u, .isUniformBlockSize = false, .ipcmdSerialClkFreq = 1, .isDataOrderSwapped = true .serialNorType = 2, .reserve2[0] = 0x7008200, Re: Flash configuration confusion RT1176 Octal DDR 嘿@SimonHugr , 我首先要确认的是 MX25UM51245G 和 MX25UM51345G 之间的实际区别。虽然零件编号非常相似,但它们并不是完全相同的设备。根据 Macronix 的数据手册,MX25UM51345G 明确支持 DOPI(双倍传输速率 OPI)字节模式数据序列,而 MX25UM51245G 属于不同的产品型号。这会影响 FlexSPI 控制器使用的命令格式、字节顺序和 LUT 配置。 您还可以对比一下我的配置,我的配置适用于 MX25UM513 和 MX25UW6345G: https://github.com/Masmiseim36/Coremark_iMXRT/blob/master/XiP/flexspi_flash_OSPI_Macronix.c 雷加尔斯 Re: Flash configuration confusion RT1176 Octal DDR 你好,哈比卜 对于我们的固件,我无法使用安全配置工具生成 FCB,而是需要在固件启动时加载 FCB,因此我需要创建 mem_config 和 flash_config 结构并自行配置。 我发现 Zephyr 项目在 flash_nor_config 中引用了一个 isDataOrderSwapped 字节。 https://github.com/zephyrproject-rtos/hal_nxp/blob/3a36ee1f8b9fc2168fc0bf80377ace8298292993/mcux/mcux-sdk-ng/devices/RT/RT1170/MIMXRT1176/drivers/romapi/fsl_romapi.h#L347-L348 Claude 提到 controllerMiscOption 的第 5 位有一个 padSettingOverride 位,第 7 位有一个 dataSwap 位,但我不太确定 LLM 是否严重地臆造了这些信息。 使用安全配置工具生成 FCB 并使用此工具将其转换为 C 结构体时 https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/i-MX-RT-FLEXSPI-booting-guide/ta-p/1669262 我没有设置第 5 位或第 7 位,所以我认为 LLM 有问题,但是 isDataSwapped 已设置,并且在 FCB 中通常被引用为 reserved0[0]。 我在安全配置工具中找不到 MX25UM51245G 的模板,只有 MX25U51245G(四闪存)、MX25UM51345G 和 MX25UMxxx45G 的模板。 但我尝试过的所有八进制DDR配置都无法启动。 有趣的是,尽管 BT_FUSE_SEL = 1 且引脚 BOOTMODE0/1 = 0,MCU 在某些配置后通常会自动进入 ISP 模式。这种情况并不稳定,我不确定是什么配置导致了这个问题。 MCU在读取闪存失败后是否会进入ISP模式? 谢谢 BR Re: Flash configuration confusion RT1176 Octal DDR 你好@SimonHugr , 很抱歉,MX25UM51245G 没有模板,只有 MX25U51245G 和 MX25UM51345G 可用。 根据您的描述,使用您当前的启动内存配置设置,与闪存设备的通信似乎工作正常。单击“转换为完整 FCB”后,该工具会将配置编程到闪存中,然后使用您指定的参数将其读取回来,如下所述: Habib_MS_0-1784753481563.png 如果所选设置中有任何一项不被闪存设备支持,该工具应报告类似于以下内容的错误: Habib_MS_1-1784753506390.png 为了进一步验证社区帖子中提到的使用 FCB 变流器生成的 LUT 是否正常工作,请您在从内部 RAM 运行应用程序时,使用 flexspi_nor_polling_transfer_cm7 SDK 示例进行测试。如果您对示例有任何疑问,请随时联系我。 此外,您能否提供一些关于您尝试启动的应用程序的更多详细信息? -这是 SDK 示例还是您自己的应用程序? 你使用的是哪个集成开发环境(IDE)? -您的应用程序是执行 XIP 还是非 XIP? -除了启动过程之外,您是否在任何其他阶段访问过闪存? 关于进入 ISP 模式,请确保您的定制板上的启动引脚符合MIMXRT1160/1170 硬件开发指南第 5 章“启动、复位和其他”中提到的建议?这样做是为了避免与启动引脚相关的任何硬件问题。 回答您的问题,如果没有有效的镜像文件,您可以进入ISP模式,如图10-1所示的RM“启动流程”: Habib_MS_2-1784754516601.png BR 哈比卜 Re: Flash configuration confusion RT1176 Octal DDR 你好,哈比卜。 我现在至少已经让八进制 SPI STR 模式在 200MHz 下工作了。问题出在一些未描述的神秘的“reserve2”字节上。我还选择在设备模式序列之上设置一个配置命令序列,并添加一个额外的字节。 设置字节交换并没有起到任何作用,但我对在 200MHz STR 八进制下能够达到的速度感到满意。 顺祝商祺!
查看全文
i.MX6UL 是否提供任何机制(定时器/寄存器)来延迟或控制篡改后的 ZMK 清零? i.MX6UL是否提供任何硬件机制(寄存器、定时器、计数器或配置)来防止或推迟在有效的外部篡改事件后自动ZMK 清零?如果存在这样的机制,请您指出安全参考手册中描述的相关寄存器、定时器或配置。 平台: i.MX6UL 引导加载程序: U-Boot 2016.03 操作系统: Linux + OP-TEE 参考资料: 《i.MX 6UltraLite 应用处理器网络安全参考手册》,修订版 0,2016 年 4 月 @nxp
查看全文
meter 我想在组件里面找到meter控件,怎么没有啊
查看全文
MEXの設定はWindowsやLinuxとは異なるコードを生成します 同じXEMファイルでも、システムによって生成されるコードが異なる。 Windowsファイルはコード正常生成ですが、Linuxシステムは異常な生成をします 前提条件:RTDおよびSDKバージョンインストールと同じです 5.jpg Re: mex config generate code different from windows and linux こんにちは、 @Littenさん 現在、RTDはWindowsプラットフォームでのみサポートされており、Linuxでは公式にはサポートされていません。たとえLinuxにインストールできても、開発や統合の過程で追加の問題に直面する可能性があります。 主な理由の一つは、Linuxが大文字大文字を区別するオペレーティングシステムであることです。この状況の詳細は スレッド「S32DSのLpi2c_Ip_MasterConfigとLpi2c_Ip_SlaveState構造体生成の問題」で議論されています。S32K344。 BR、VaneB
查看全文
关于“智能能源”太阳能的观点 编辑:谢谢大家。感谢您的建议!我会让他们滚蛋,反正我还没准备好做任何决定。 今天有几个来自 Smart Energy 的推销员上门推销太阳能电池板。我对太阳能很感兴趣,但没有足够的资金进行前期投资,他们提到有一个政府资助的计划,无需预付任何费用。 我自然非常怀疑。很想听听和他们打过交道的人的意见。
查看全文
KinetisとLPC用のデバッグインターフェースのおすすめはありますか? 私は主にKinetisシリーズで開発をしており、近い将来LPCのパーツもいくつか手がけるかもしれません。P&E Microのデバッグインターフェースが引き出しいっぱいにあり、よく使っているCyclone ACPも含まれています。 時々、600ドルのCycloneから20ドルのLPC-Link2に切り替えることがあります。なぜなら、CycloneはMCUXpressoに多くの奇妙な問題があるからです。正直なところ、LPC-Link2は私の必要な機能のほとんどを満たしてくれるのですが、少し動作が遅いのが難点です。 Seggerインターフェースを検討しるべきでしょうか?MCUXpresso(そしてできればCodeWarrior 11でも)で十分にサポートされ、クラッシュや走行中のターゲットを止められない信頼性が高く、そこそこ高速なインターフェースを誰かおすすめできませんか?トレースサポートがあれば助かります。 よろしくお願いします! Re: Debug interface recommendations for Kinetis and LPC? こんにちは、 @zeref さん。 これは繰り返し投稿です。KinetisとLPCのデバッグインターフェース推奨に関する私の返信を参照してください。 BR セレステ
查看全文
「スマートエネルギー」太陽光発電に関する意見 追記:皆さん、ありがとうございます。ご意見ありがとうございます!彼らには「とっとと失せろ」と言ってやるよ。どうせ私は何も約束する準備ができていないんだから。 今日はスマートエナジーという会社の訪問販売員が何人か来て、太陽光パネルについて話したがっていました。太陽光発電に興味はあるのですが、初期投資をする資金がありません。そこで、初期費用ゼロで利用できる政府資金による制度があると聞きました。 もちろん、私は非常に懐疑的です。彼らと取引したことのある方からのご意見をぜひお聞かせください。
查看全文
Does i.MX6UL provide any mechanism (timer/register) to delay or control ZMK zeroization after tamper Does the i.MX6UL provide any hardware mechanism (register, timer, counter, or configuration) to prevent or postpone automatic ZMK zeroization after a valid external tamper event? If such a mechanism exists, could you please point me to the relevant register(s), timer, or configuration described in the Security Reference Manual? Platform: i.MX6UL  Bootloader: U-Boot 2016.03 OS: Linux + OP-TEE Reference used: Security Reference Manual for the i.MX 6UltraLite Applications Processor, Rev. 0, 04/2016 @nxp 
查看全文
FreeMasterプラグインモジュールはありません 私はフリーマスターバージョン3.2.7をインストールしました。いろいろな方法を試しましたが、プラグインモジュールの下には何もありません。急いでるんだ。これは私の仕事に欠かせない道具です。どなたか助けていただけますか?どうもありがとうございます。 1. FreeMASTERを「管理者として」インストールするか、「c:\NXP\FreeMASTER 3.2\FreeMASTER\register.bat」を実行してください。効果はありません!!! PixPin_2026-07-20_20-46-19.png 2. PixPin_2026-07-20_20-36-29.png PixPin_2026-07-20_20-40-48.png Re: there has no FreeMaster plug-in module こんにちは、 私の知る限り、最新のWindowsアップデートではCOM+およびActiveXオブジェクトの動作方法は変更されません。これは関係ない。あなたが直面している問題は、実に奇妙です。 一つのプラグイン(CAN通信)を選んで登録情報を確認しましょう。 再度「コマンドプロンプト」を管理者として実行し、「c:\NXP\FreeMASTER 3.2\FreeMASTER」に移動して、/s (サイレント) オプションなしで regsvr32 コマンドを実行します。 regsvr32 プラグイン/CAN/focpgi.dll 確認メッセージは以下に表示されます。 MichalH_1-1784615468404.png 次に、同じコマンドプロンプトコンソールで、以下のコマンドを使用してレジストリエディターを起動します。 レジストリエディタ 数分かかることもありますが、その後エディターが表示されます。ナビゲート先 Computer\HKEY_CLASSES_ROOT\WOW6432Node\CLSID\{C10A92C3-7D47-4FDC-94B6-64B8E5C85E01} この項目はFreeMASTER-over-CANプラグイン(focpgi.dll)を表しています。それは登記簿に記載されなければならない。 MichalH_0-1784615359152.png InprocServer32のエントリポイントを正しいfocpgi.dllファイルに確認できます。 MichalH_2-1784615691533.png 「実装済みカテゴリ」IDは、FreeMASTERがWindows COMカテゴリAPIを使用してすべてのプラグインを特定するために使用するIDです。プラグインカテゴリが存在することを確認するために、レジストリエディタでComputer\HKEY_CLASSES_ROOT\Component Categories\{48A185C0-FFDB-11D3-80E3-00C04F176153}キーを確認してください。「MCB Communication Plugins」というテキスト値が表示されます。 MichalH_3-1784615997310.png もう一つの実験は、スクリプトから/sスイッチを外して実行register.batことです。各DLLごとに登録確認ボックスが表示されます。 該当するスクリーンショットまたはエラーメッセージを共有してください。ご協力ありがとうございました。 よろしくお願いいたします。 ミハル Re: there has no FreeMaster plug-in module もし誰かがこの問題を解決する手助けをしてくれたら、コーヒーをご馳走します。 Re: there has no FreeMaster plug-in module あなたの方法を試しましたが、モジュールはまだ表示されていません。 これは、Windowsシステムが最新バージョンにアップデートされたことと関係がありますか? ScreenShot_2026-07-21_095319_274.png PixPin_2026-07-21_10-13-18.png Re: there has no FreeMaster plug-in module こんにちは、 インストーラーとregister.batの両方が「 regsvr32.exe 」を使用します。システムユーティリティであり、すべてのWindowsオペレーティングシステムにデフォルトでインストールされる。 まず、システムにregsvr32ユーティリティが存在することを確認してください。Win+Rキーを押して、「regsvr32」コマンドを実行してください。 MichalH_3-1784558060323.png 次のようなヘルプボックスが表示されるはずです。 MichalH_0-1784557473602.png このユーティリティが動作しない場合は、お使いのコンピュータに管理者によるシステム制限が適用されている可能性があります。修理してもらう必要があります。 regsvr32が正常に動作している場合、register.batが出力するエラーを確認してみましょう。 スタートメニューを開きます。 「コマンドプロンプト」アプリケーションを探してください 右クリックして「管理者として実行」を選択してください(下の画像を参照)。 コンソールで「cd "c:\NXP\FreeMASTER 3.2\FreeMASTER"」と入力します。 register.batを実行します。 エラーは表示されないはずです(最後の画像のように)。 エラーがなければ、プラグインはFreeMASTERに表示されます。誤りがあれば、こちらでお知らせください。 MichalH_1-1784557809666.png MichalH_2-1784557992554.png よろしくお願いいたします。 ミハル Re: there has no FreeMaster plug-in module こんにちは、再度テストしてみました。現在、そのモジュールはまだ利用できません。register.bat ファイル内の「/s」を含む行をすべて削除しました。他に現在利用可能な解決策はありますか? 1.png 2.png 3.png 4.png 5.png Re: there has no FreeMaster plug-in module こんにちは、 要約すると、すべてのプラグイン登録は正常に完了しますが、FreeMASTERのオプションダイアログのプラグインリストは空のままです。 別のパソコンでテストすることは可能でしょうか? また、プラグインリストにアクセスする他の2つのユーティリティもあります。リモートサーバーツール("c:\NXP\FreeMASTER 3.2\FreeMASTER\mcbsvr.exe"))を実行してみてください。次に「追加」ボタンを押して、プラグインリストも空になっているかどうかを確認してください。 MichalH_0-1784702997668.png 「Named Connection」マネージャー(c:\NXP\FreeMASTER 3.2\FreeMASTER\pgimgr.exe」で同様の方法を試し、「New」ボタンを押すことができます: MichalH_1-1784703133393.png どちらかのツールでプラグインリストが空でない状態で表示されるかどうか教えてください。 ありがとう、 ミハル Re: there has no FreeMaster plug-in module 試してみましたが、それでもうまくいきません。私のパソコンには大量のデータが入っているので、システムを再インストールしたくありません。これは本当に困ったものです。以前は正常に動作していたのですが、ある日突然接続できなくなってしまいました。 1.png 2.png Re: there has no FreeMaster plug-in module こんにちは、 お使いのコンピューターの不具合箇所を特定するのに役立つ、簡単なテストユーティリティを用意しました。下記に添付されている「plugin_test.exe」をご覧ください。 コマンドプロンプト(cmd)コンソールで実行してください(管理者として実行する必要はありません)。 Usage: plugin_test [ProgID|CLSID] test# 0 - create and release the component test# 1 - create and call Configure() test# 2 - enumerate all registered McbCommPlugin components (ProgID|CLSID argument is optional for test 2) 選択されたプラグインインスタンス化のテストは合格する可能性があります。これを試してみてください: plugin_test.exe 0 MCBPGI.TCPSERIAL.1 Component : MCBPGI.TCPSERIAL.1 CLSID : {ED244618-9103-41BE-B382-E92036BD04FC} Test : 0 [test 0] CoCreateInstance ... [test 0] OK - component created successfully. [test 0] Releasing ... [test 0] Released. Result: PASS ツールはプラグイン設定ダイアログの表示も試みることができます: plugin_test.exe 1 MCBPGI.TCPSERIAL.1 そして、それは明らかになるだろう。 MichalH_0-1784793243679.png 最後に、テスト2ではFreeMASTERと同様の方法でプラグインの列挙を行います。それはおそらくあなたの側で失敗するでしょう。 plugin_test.exe 2 Test : 2 [test 2] Creating StdComponentCategoriesMgr ... [test 2] OK - ICatInformation obtained. [test 2] Enumerating McbCommPlugin classes: [1] {1BB3C904-F1F4-4652-92EE-368716FE1D10} (BDMPGI.DAPCOM.1) [2] {2080BBA8-0641-4306-A956-6BEBB7C75249} (JTAGPGI.CCSCOM.1) [3] {225E034C-1AA6-4EC5-9A6C-A9FA9E890373} (BDMPGI.HCSCOM.1) [4] {30AB7AA1-493A-4DD7-9509-C9C91EFFF0FD} (BDMPGI.PDBDMCOM.1) [5] {5A129680-897E-4014-916D-9B1FE13DE156} (BDMPGI.EONCECOM.1) [6] {6D13CD9D-9F2D-4066-B655-45B54CA7494B} (MCBPGI.NETCOM.1) [7] {7AC03FB7-4792-4F26-8152-92E466276068} (DEMOPGI.DummyCom.1) [8] {80F17965-EDBD-41F1-9182-3C44E04E5794} (BDMPGI.ISYSCOM.1) [9] {8C575DB3-9769-4B66-AB60-C83CEA683E01} (BDMPGI.JLINKCOM.1) [10] {C10A92C3-7D47-4FDC-94B6-64B8E5C85E01} (FOCPGI.FocCom.1) [11] {C10A92C4-7D47-4FDC-94B6-64B8E5C85E01} (FOLPGI.FolCom.1) [12] {ED244616-9103-41BE-B382-E92036BD04FC} (MCBPGI.STDCOM.1) [13] {ED244617-9103-41BE-B382-E92036BD04FC} (MCBPGI.HTTPCOM.1) [14] {ED244618-9103-41BE-B382-E92036BD04FC} (MCBPGI.TCPSERIAL.1) [test 2] Total: 14 plug-in(s) found. Result: PASS ご協力ありがとうございます。 ミハル Re: there has no FreeMaster plug-in module 1.plugin_test.exe 1 MCBPGI.TCPSERIAL.1 にはダイアログボックスがあります。 2. plugin_test.exe 2 は管理者権限で実行されました。 1.png 2.png Re: there has no FreeMaster plug-in module 試してみましたが、うまくいきませんでした。 1.png 2.png 3.png Re: there has no FreeMaster plug-in module 実験にご協力いただき、ありがとうございました。 「テスト1」で次のようなダイアログが表示されましたか? plugin_test.exe 1 MCBPGI.TCPSERIAL.1 また、「管理者として」起動したコマンドプロンプトでテスト2を実行してもらえますか? plugin_test.exe 2 ありがとう、 ミハル Re: there has no FreeMaster plug-in module こんにちは、諦めずに続けてくださってありがとうございます。 事実関係を要約してみましょう。FreeMASTERで使用されているWindowsプログラミングAPIに少し置き換えて説明します。 API EnumClassesOfCategories() は、コンポーネントがすべてのレジストリエントリに正しく登録されている場合や、管理者権限で実行された場合でも、空のリストを返します。 EnumClassesOfCategories() は S_OK を返しますが、返されたイテレータに対して Next() を呼び出すと何も列挙されません。 コンポーネントDLLと、それらを列挙するアプリケーションはどちらも32ビットコードとしてコンパイルされます。 この問題は特定の1台のコンピューターでのみ発生しており、他の多くのコンピューターでは正常に動作しています。 ターゲットCLSID上のCoCreateInstanceは、この問題のあるコンピュータでも正常に動作します。 正直なところ、その理由が何なのか分かりません。インターネットの中には、登録解除してからWindowsコンポーネントマネージャーを登録することを勧めるところもあります。ですので、 管理者のコマンドでこれを試してからシステムを再起動してください: regsvr32 /u comcat.dll regsvr32 comcat.dll regsvr32 /u c:\Windows\SysWOW64\comcat.dll regsvr32 c:\Windows\SysWOW64\comcat.dll 各コマンドを実行するたびに確認ボックスが表示されます。 これで解決しない場合は、調査を継続します。 ありがとう、 ミハル Re: there has no FreeMaster plug-in module この間、ご協力いただき大変感謝しておりますが、今回もうまくいきませんでした。
查看全文
メートル 部品の中からメーター制御装置を探しているのですが、見つかりません。
查看全文
Flash configuration confusion RT1176 Octal DDR Hello NXP I got some issues configuring the flash memory for Macronix Octal DDR mode. I am using the PX4 code stack on a custom board based on the NXP FMU-6XRT reference design. I am using the MX25UM51245G instead of the MX25UM51345G, but the part differences are minimal. I am trying to run it in Macronix Octal DDR mode with DQS external sampling at atleast 100MHz. Reference design is running it at 200MHz. The Boot Memory Configuration succesfully tests the memory with the desired configuration even at 166MHz. The configuration I have tried is the following default config. The first one, "g_flash_config" succesfully boots, writes, read, etc, but is not ideal for the software. "g_flash_fast_config" fails. I have tried reducing the frequency to 166MHZ, 133MHz, 50 MHz, and 30MHz without results in the DTR mode in the "fast_config". I have tried using the FCB generated from the Boot Memory Configuration, but there is some struct layout differences which have made it hard to apply to the PX4 code.  I am tried different combinations of csHoldTime, csSetupTime and dataValidTime without results aswell. I tried DQS interal in low freq DTR Octal, but it did not work either. What could I try next? #include /**************************************************************************** * Public Data ****************************************************************************/ locate_data(".boot_hdr.conf") const struct flexspi_nor_config_s g_flash_config = { .memConfig = { #if !defined(CONFIG_BOARD_BOOTLOADER_INVALID_FCB) .tag = FLEXSPI_CFG_BLK_TAG, #else .tag = 0xffffffffL, #endif .version = FLEXSPI_CFG_BLK_VERSION, .readSampleClksrc=kFlexSPIReadSampleClk_LoopbackInternally, .csHoldTime = 1, .csSetupTime = 1, .deviceModeCfgEnable = 1, .deviceModeType = kDeviceConfigCmdType_Generic, .waitTimeCfgCommands = 1, .controllerMiscOption = (1u << kFlexSpiMiscOffset_SafeConfigFreqEnable), .deviceType = kFlexSpiDeviceType_SerialNOR, .sflashPadType = kSerialFlash_1Pad, .serialClkFreq = kFlexSpiSerialClk_100MHz, .sflashA1Size = 64ul * 1024u * 1024u, .dataValidTime = { [0] = {.time_100ps = 0}, }, .busyOffset = 0u, .busyBitPolarity = 0u, .lookupTable = { /* Read Dedicated 3Byte Address Read(0x03), 24bit address */ [0 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x03, RADDR_SDR, FLEXSPI_1PAD, 0x18), //0x871187ee, [0 + 1] = FLEXSPI_LUT_SEQ(READ_SDR, FLEXSPI_1PAD, 0x04, STOP_EXE, FLEXSPI_1PAD, 0),//0xb3048b20 }, }, .pageSize = 256u, .sectorSize = 4u * 1024u, .blockSize = 64u * 1024u, .isUniformBlockSize = false, .ipcmdSerialClkFreq = 1, .serialNorType = 2, .reserve2[0] = 0x7008200, }; const struct flexspi_nor_config_s g_flash_fast_config = { .memConfig = { .tag = FLEXSPI_CFG_BLK_TAG, .version = FLEXSPI_CFG_BLK_VERSION, .readSampleClksrc=kFlexSPIReadSampleClk_LoopbackInternally, .csHoldTime = 3, .csSetupTime = 3, .deviceModeCfgEnable = 1, .deviceModeType = kDeviceConfigCmdType_Spi2Xpi, .waitTimeCfgCommands = 1, .deviceModeSeq = { .seqNum = 1, .seqId = 6, /* See Lookup table for more details */ .reserved = 0, }, .deviceModeArg = 2, /* Enable OPI DDR mode */ .controllerMiscOption = (1u << kFlexSpiMiscOffset_SafeConfigFreqEnable) | (1u << kFlexSpiMiscOffset_DdrModeEnable), .deviceType = kFlexSpiDeviceType_SerialNOR, .sflashPadType = kSerialFlash_8Pads, .serialClkFreq = kFlexSpiSerialClk_133MHz, .sflashA1Size = 64ul * 1024u * 1024u, .dataValidTime = { [0] = {.time_100ps = 10}, }, .busyOffset = 0u, .busyBitPolarity = 0u, .lookupTable = { /* Read */// EEH+11H+32bit addr+20dummy cycles+ 4Bytes read data /* Macronix manual says 20 dummy cycles @ 200Mhz, FlexSPI peripheral Operand value needs to be 2N in DDR mode hence 0x28 */ [0 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0xEE, CMD_DDR, FLEXSPI_8PAD, 0x11), //0x871187ee, [0 + 1] = FLEXSPI_LUT_SEQ(RADDR_DDR, FLEXSPI_8PAD, 0x20, DUMMY_DDR, FLEXSPI_8PAD, 0x28),//0xb3288b20, [0 + 2] = FLEXSPI_LUT_SEQ(READ_DDR, FLEXSPI_8PAD, 0x04, STOP_EXE, FLEXSPI_1PAD, 0x00), //0xa704, /* Read status */ [4 * 2 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x05, CMD_DDR, FLEXSPI_8PAD, 0xfa), [4 * 2 + 1] = FLEXSPI_LUT_SEQ(RADDR_DDR, FLEXSPI_8PAD, 0x20, DUMMY_DDR, FLEXSPI_8PAD, 0x04), [4 * 2 + 2] = FLEXSPI_LUT_SEQ(READ_DDR, FLEXSPI_8PAD, 0x04, STOP_EXE, FLEXSPI_1PAD, 0x00), /* Write enable SPI *///06h [4 * 3 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x06, STOP_EXE, FLEXSPI_1PAD, 0x00),//0x00000406, /* Write enable OPI SPI *///06h [4 * 4 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x06, CMD_DDR, FLEXSPI_8PAD, 0xF9), /* Erase sector */ [4 * 5 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x21, CMD_DDR, FLEXSPI_8PAD, 0xDE), [4 * 5 + 1] = FLEXSPI_LUT_SEQ(RADDR_DDR, FLEXSPI_8PAD, 0x20, STOP_EXE, FLEXSPI_1PAD, 0x00), /*Write Configuration Register 2 =01, Enable OPI DDR mode*/ //72H +32bit address + CR20x00000000 = 0x01 [4 * 6 + 0] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x72, CMD_SDR, FLEXSPI_1PAD, 0x00),//0x04000472, [4 * 6 + 1] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x00, CMD_SDR, FLEXSPI_1PAD, 0x00),//0x04000400, [4 * 6 + 2] = FLEXSPI_LUT_SEQ(CMD_SDR, FLEXSPI_1PAD, 0x00, WRITE_SDR, FLEXSPI_1PAD, 0x01),//0x20010400, /*Page program*/ [4 * 9 + 0] = FLEXSPI_LUT_SEQ(CMD_DDR, FLEXSPI_8PAD, 0x12, CMD_DDR, FLEXSPI_8PAD, 0xED),//0x87ed8712, [4 * 9 + 1] = FLEXSPI_LUT_SEQ(RADDR_DDR, FLEXSPI_8PAD, 0x20, WRITE_DDR, FLEXSPI_8PAD, 0x04),//0xa3048b20, }, }, .pageSize = 256u, .sectorSize = 4u * 1024u, .blockSize = 64u * 1024u, .isUniformBlockSize = false, .ipcmdSerialClkFreq = 1, .serialNorType = 2, .reserve2[0] = 0x7008200, }; Re: Flash configuration confusion RT1176 Octal DDR Hello @SimonHugr, If you plan to use DDR mode, please keep in mind that the byte swapping configuration must also be considered. this post provides useful information about why important take in mind the byte swapping on the MX25UM51245GXDI00 when you are using DDR mode.  I highly recommend use the Boot Memory Configuration to generate the FCB, the Secure provisioning tool v26.6 offers a template of the MX25UM51245G, which can serve as a good starting point for your configuration. Also, as you may know, this tool allows you to test your configurations. Additionally, I recommend see this community post, particularly the steps starting from point 15. That section provides a more detailed explanation of how the Secure Provisioning Tool generates the boot memory configuration and may help clarify the parameters and output produced by the tool. Finally, you can use the flexspi_nor_polling_transfer_cm7 example to validate the generated FCB and verify that read and write operations are functioning correctly before proceeding with the boot configuration. BR Habib Re: Flash configuration confusion RT1176 Octal DDR No results yet sadly, I still think it has something to do with some data order swap is done and I am missing some configuration byte somewhere... Re: Flash configuration confusion RT1176 Octal DDR Thank you Masmiseim Indeed, I noticed that the data should be swapped for example. I will go through my LUT once more. Re: Flash configuration confusion RT1176 Octal DDR Refering to this thread: https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/Internal-Boot-from-Flash-memory-not-starting-on-imxRT1176-custom/m-p/1830699 I should swap the data order by editing the misc option and according to zephyr RTOS https://github.com/zephyrproject-rtos/hal_nxp/blob/3a36ee1f8b9fc2168fc0bf80377ace8298292993/mcux/mcux-sdk-ng/devices/RT/RT1170/MIMXRT1176/drivers/romapi/fsl_romapi.h#L340-L355 the dataswap byte goes in, but I think I am missing something. .pageSize = 256u, .sectorSize = 4u * 1024u, .blockSize = 64u * 1024u, .isUniformBlockSize = false, .ipcmdSerialClkFreq = 1, .isDataOrderSwapped = true .serialNorType = 2, .reserve2[0] = 0x7008200, Re: Flash configuration confusion RT1176 Octal DDR Hey @SimonHugr, One thing I would verify first is the actual difference between the MX25UM51245G and MX25UM51345G. Although the part numbers are very similar, they are not identical devices. According to the Macronix datasheets, the MX25UM51345G explicitly supports DOPI (Double Transfer Rate OPI) Byte Mode data sequence, while the MX25UM51245G belongs to a different product variant. This can affect the command format, byte ordering and LUT configuration used by the FlexSPI controller. You can also compare my configuration which works with MX25UM513 and MX25UW6345G: https://github.com/Masmiseim36/Coremark_iMXRT/blob/master/XiP/flexspi_flash_OSPI_Macronix.c Regars Re: Flash configuration confusion RT1176 Octal DDR Hello Habib For our firmware I am not able to use the secure provisioning tool to generate the FCB, and instead the FCB needs to be loaded on boot in firmware and therefor I need to create the mem_config and flash_config struct and configure it myself. I found the zephyr project referenced a isDataOrderSwapped byte in the flash_nor_config https://github.com/zephyrproject-rtos/hal_nxp/blob/3a36ee1f8b9fc2168fc0bf80377ace8298292993/mcux/mcux-sdk-ng/devices/RT/RT1170/MIMXRT1176/drivers/romapi/fsl_romapi.h#L347-L348 and Claude reference a padSettingOverride bit on bit 5 and a dataSwap bit on bit 7 in the controllerMiscOption, but I am not sure if the LLM is heavily hallucinating this information. When generating the FCB using the Secure Provisioning tool and converting it into a C-struct using this tool https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/i-MX-RT-FLEXSPI-booting-guide/ta-p/1669262 I do not get bit 5 or 7 set so I think the LLM is wrong, but the isDataSwapped is set and is referenced as reserved0[0] in the FCB normally. I can not find a template for the MX25UM51245G in the secure provisioning tool, only the MX25U51245G (which is a Quad flash), the MX25UM51345G and the MX25UMxxx45G. But any config Octal DDR config that I have tried have not worked to boot. Interestingly often the MCU goes automatically into ISP mode after certain configuration despite BT_FUSE_SEL = 1 and having pins BOOTMODE0/1 = 0. This has not been consistent and I am not sure what configuration causes this. Does the MCU go into ISP mode after failing to read the flash or something? Thank you BR Re: Flash configuration confusion RT1176 Octal DDR Hello @SimonHugr, I apologies there is not a template to MX25UM51245G, only are available the MX25U51245G and MX25UM51345G. Based on your description, it seems that communication with the flash device is working correctly using your current Boot Memory Configuration settings. When you click "Convert to Complete FCB", the tool programs the configuration into the flash and then reads it back using the parameters you specified, as described below: Habib_MS_0-1784753481563.png If any of the selected settings are not supported by the flash device, the tool should report an error similar to the following: Habib_MS_1-1784753506390.png To further verify that the LUT generated using the FCB converter from the community post is functioning correctly, could you please test it with the flexspi_nor_polling_transfer_cm7 SDK example while running the application from internal RAM? Please let me know if you have questions about the example. In addition, could you provide me a few more details about the application you are trying to boot? -Is an SDK example or if your own application? -Which IDE you are using? -Is your application performing XIP or NON-XIP? -Are you accessing the flash at any point other than during the boot process? Regarding to entering in ISP mode, could you please make sure that the boot pins on your custom board followed the recommendations mentioned in the chapter 5 "Boot, reset, and miscellaneous" of the Hardware Development Guide for the MIMXRT1160/1170? This to avoid any hardware issue regarding the boot pins.   Answering your question, you can enter in ISP mode if is not available a valid image, as shown the figure 10-1 "boot flow" of the RM: Habib_MS_2-1784754516601.png BR Habib  Re: Flash configuration confusion RT1176 Octal DDR Hello Habib. I got octal SPI STR mode working at 200MHz now atleast. The problem was some magic non-described "reserve2" bytes that was being set. I also opted to set a config cmd sequence ontop of the device mode sequence setting an additional byte. Setting the byte swap did not accomplish anything, but I am happy with the speed I am able to achieve at 200MHz STR Octal Best regards
查看全文
i.MX6ULは、改ざん後のZMKのゼロ化を遅延または制御するためのメカニズム(タイマー/レジスタ)を提供しますか? i.MX6ULは、有効な外部改ざんイベント後に自動ZMKゼロ化を防止または延期するためのハードウェア機構(レジスタ、タイマー、カウンター、または設定)を提供していますか?もしそのような仕組みが存在するなら、セキュリティリファレンスマニュアルに記載されている該当レジスタ、タイマー、または設定をご紹介いただけますか? プラットフォーム: i.MX6UL  ブートローダー: U-Boot 2016.03 OS: Linux + OP-TEE 参考文献: i.MX 6UltraLiteアプリケーションプロセッサのセキュリティリファレンスマニュアル、Rev. 0、2016年4月 @nxp 
查看全文
Kinetis 和 LPC 的调试接口有什么建议? 我目前主要从事 Kinetis 系列芯片的开发工作,未来可能还会开发一些 LPC 芯片。我抽屉里装满了 P&E Micro 的调试接口,其中最常用的是 Cyclone ACP。 我有时会发现自己从 600 美元的 Cyclone 换成了 20 美元的 LPC-Link2,因为 Cyclone 与 MCUXpresso 存在很多奇怪的问题。说实话,LPC-Link2 基本能满足我的需求,只是速度有点慢。 我应该考虑使用Segger接口吗?请问有人可以推荐一款可靠、速度适中、在 MCUXpresso(最好也能在 CodeWarrior 11)中支持良好的接口吗?这款接口不会经常导致程序崩溃,也不会无法停止正在运行的目标。如果能支持追踪功能就更好了。 谢谢您! Re: Debug interface recommendations for Kinetis and LPC? 你好@zeref , 这是重复发帖,请参考我在“Kinetis 和 LPC 的调试接口建议?”中的回复。 BR 塞莱斯特
查看全文
没有 FreeMaster 插件模块 我安装了freemaster 3.2.7版本,我尝试了很多方法,但插件模块里什么都没有。我很着急。这是我工作中必不可少的工具。有人能帮帮我吗?非常感谢。 1.我以管理员身份安装FreeMASTER,或者运行“c:\NXP\FreeMASTER 3.2\FreeMASTER\register.bat”——均无效!!! PixPin_2026-07-20_20-46-19.png 2. PixPin_2026-07-20_20-36-29.png PixPin_2026-07-20_20-40-48.png Re: there has no FreeMaster plug-in module 你好, 据我所知,最新的 Windows 更新并没有改变 COM+ 和 ActiveX 对象的工作方式。这两件事无关。你遇到的问题确实很奇怪。 我们选取一个插件(CAN 通信)并查看其注册详情。 再次以管理员身份运行“命令提示符”,然后切换到“c:\NXP\FreeMASTER 3.2\FreeMASTER”目录,并使用不带 /s(静默)选项的 regsvr32 命令: regsvr32 插件/can/focpgi.dll 确认信息将显示: MichalH_1-1784615468404.png 然后在同一命令提示符控制台中,使用以下命令启动注册表编辑器: 注册表 需要一些时间(可能需要几分钟),然后编辑器就会出现。导航至 计算机\HKEY_CLASSES_ROOT\WOW6432Node\CLSID\{C10A92C3-7D47-4FDC-94B6-64B8E5C85E01} 此条目代表 FreeMASTER-over-CAN 插件 (focpgi.dll)。它必须登记在册。 MichalH_0-1784615359152.png 您可以检查 InprocServer32 入口点是否指向正确的 focpgi.dll 文件。 MichalH_2-1784615691533.png “已实现类别”ID 是 FreeMASTER 使用 Windows COM 类别 API来查找所有插件的 ID。为了确保插件类别存在,请在注册表编辑器中检查Computer\HKEY_CLASSES_ROOT\Component Categories\{48A185C0-FFDB-11D3-80E3-00C04F176153}项,您应该会看到“MCB Communication Plugins”文本值: MichalH_3-1784615997310.png 另一个实验方法是从 register.bat 脚本中删除 /s 开关并运行它。每个 DLL 文件都会显示一个注册确认框。 请分享相关的屏幕截图或错误信息。感谢您的合作。 问候, 米哈尔 Re: there has no FreeMaster plug-in module 如果有人能帮我解决这个问题,我请他喝咖啡。 Re: there has no FreeMaster plug-in module 我尝试了你的方法,但模块仍然没有出现。 这是否与我的Windows系统更新到最新版本有关? ScreenShot_2026-07-21_095319_274.png PixPin_2026-07-21_10-13-18.png Re: there has no FreeMaster plug-in module 你好, 安装程序和 register.bat 都使用了“ regsvr32.exe ”。系统实用程序,应默认安装在任何 Windows 操作系统中。 首先,请确保您的系统上存在 regsvr32 工具。只需按下 Win+R 键,然后运行命令“regsvr32”。 MichalH_3-1784558060323.png 你应该会看到类似这样的帮助框: MichalH_0-1784557473602.png 如果此工具无法正常工作,则可能是您的计算机受到了管理员的系统限制。你需要把它修好。 如果 regsvr32 运行正常,我们来看看 register.bat 会输出什么错误信息: 打开开始菜单。 找到“命令提示符”应用程序 右键单击并选择“以管理员身份运行”(见下图) 在控制台中,输入cd "c:\NXP\FreeMASTER 3.2\FreeMASTER" 运行register.bat 您应该看不到任何错误(就像最后图片中显示的那样)。 如果没有错误,插件将出现在 FreeMASTER 中。如有任何错误,请在此处告知。 MichalH_1-1784557809666.png MichalH_2-1784557992554.png 问候, 米哈尔 Re: there has no FreeMaster plug-in module 你好, 总结一下——所有插件注册都成功完成,但 FreeMASTER 选项对话框中的插件列表仍然为空。 您能否尝试在另一台电脑上进行测试? 此外,还有两个其他实用程序可以访问插件列表。请尝试运行远程服务器工具(“c:\NXP\FreeMASTER 3.2\FreeMASTER\mcbsvr.exe”)。然后按下“添加”按钮,看看插件列表是否也为空: MichalH_0-1784702997668.png 在“命名连接”管理器(c:\NXP\FreeMASTER 3.2\FreeMASTER\pgimgr.exe)中也可以尝试类似的操作,然后按“新建”按钮: MichalH_1-1784703133393.png 如果这两个工具中任何一个能够显示不为空的插件列表,请告诉我。 谢谢你, 米哈尔 Re: there has no FreeMaster plug-in module 你好,我又测试了一遍。目前该模块仍不可用。我已经删除了 register.bat 文件中所有包含“/s”的行。目前还有其他解决方案吗? 1.png 2.png 3.png 4.png 5.png Re: there has no FreeMaster plug-in module 我试过了,但还是不行。我的电脑里有很多数据,我不想重装系统。这真是太麻烦了。之前一直都正常,但有一天突然就连不上了。 1.png 2.png Re: there has no FreeMaster plug-in module 你好, 我准备了一个小型测试工具,它可以帮助我们发现您机器上的问题所在。请查看下方附件“plugin_test.exe”。 在命令提示符控制台中运行(无需以管理员身份运行)。 Usage: plugin_test [ProgID|CLSID] test# 0 - create and release the component test# 1 - create and call Configure() test# 2 - enumerate all registered McbCommPlugin components (ProgID|CLSID argument is optional for test 2) 所选插件实例化的测试可能通过。试试这个: plugin_test.exe 0 MCBPGI.TCPSERIAL.1 Component : MCBPGI.TCPSERIAL.1 CLSID : {ED244618-9103-41BE-B382-E92036BD04FC} Test : 0 [test 0] CoCreateInstance ... [test 0] OK - component created successfully. [test 0] Releasing ... [test 0] Released. Result: PASS 该工具甚至可以尝试显示插件配置对话框: plugin_test.exe 1 MCBPGI.TCPSERIAL.1 而它终将显现: MichalH_0-1784793243679.png 最后,测试 2 以类似于 FreeMASTER 的方式进行插件枚举。它很可能在你这边失败: plugin_test.exe 2 Test : 2 [test 2] Creating StdComponentCategoriesMgr ... [test 2] OK - ICatInformation obtained. [test 2] Enumerating McbCommPlugin classes: [1] {1BB3C904-F1F4-4652-92EE-368716FE1D10} (BDMPGI.DAPCOM.1) [2] {2080BBA8-0641-4306-A956-6BEBB7C75249} (JTAGPGI.CCSCOM.1) [3] {225E034C-1AA6-4EC5-9A6C-A9FA9E890373} (BDMPGI.HCSCOM.1) [4] {30AB7AA1-493A-4DD7-9509-C9C91EFFF0FD} (BDMPGI.PDBDMCOM.1) [5] {5A129680-897E-4014-916D-9B1FE13DE156} (BDMPGI.EONCECOM.1) [6] {6D13CD9D-9F2D-4066-B655-45B54CA7494B} (MCBPGI.NETCOM.1) [7] {7AC03FB7-4792-4F26-8152-92E466276068} (DEMOPGI.DummyCom.1) [8] {80F17965-EDBD-41F1-9182-3C44E04E5794} (BDMPGI.ISYSCOM.1) [9] {8C575DB3-9769-4B66-AB60-C83CEA683E01} (BDMPGI.JLINKCOM.1) [10] {C10A92C3-7D47-4FDC-94B6-64B8E5C85E01} (FOCPGI.FocCom.1) [11] {C10A92C4-7D47-4FDC-94B6-64B8E5C85E01} (FOLPGI.FolCom.1) [12] {ED244616-9103-41BE-B382-E92036BD04FC} (MCBPGI.STDCOM.1) [13] {ED244617-9103-41BE-B382-E92036BD04FC} (MCBPGI.HTTPCOM.1) [14] {ED244618-9103-41BE-B382-E92036BD04FC} (MCBPGI.TCPSERIAL.1) [test 2] Total: 14 plug-in(s) found. Result: PASS 谢谢您的合作。 Michal Re: there has no FreeMaster plug-in module 1.plugin_test.exe 1 MCBPGI.TCPSERIAL.1 有一个对话框。 2. plugin_test.exe 2 已以管理员权限运行。 1.png 2.png Re: there has no FreeMaster plug-in module 我测试过了,但是没成功。 1.png 2.png 3.png Re: there has no FreeMaster plug-in module 你好,感谢你的持续尝试。 让我总结一下事实——以下内容稍作翻译,使其更符合 FreeMASTER 中使用的 Windows 编程 API: 即使元器件已正确注册到所有注册表项,并且即使以管理员权限执行,API EnumClassesOfCategories() 仍返回空列表。 EnumClassesOfCategories() 返回 S_OK,但对返回的迭代器调用 Next() 却无法枚举任何内容。 组件 DLL 和枚举它们的应用程序均编译为 32 位代码。 这个问题只出现在一台电脑上,其他很多电脑运行正常。 即使在这台有问题的计算机上,目标 CLSID 上的 CoCreateInstance 也能正常工作。 我必须承认,我不知道原因可能是什么。一些网络资源建议尝试注销并重新注册 Windows 组件管理器。所以请以管理员身份在命令提示符中尝试以下命令,然后重启系统: regsvr32 /u comcat.dll regsvr32 comcat.dll regsvr32 /u c:\Windows\SysWOW64\comcat.dll regsvr32 c:\Windows\SysWOW64\comcat.dll 每条命令都应该弹出确认框。 如果这样还是不行,我会继续调查。 谢谢, 米哈尔 Re: there has no FreeMaster plug-in module 感谢你进行这项实验。 “测试 1”开始时是否出现任何对话框: plugin_test.exe 1 MCBPGI.TCPSERIAL.1 另外,请您在以“管理员身份”启动的命令提示符中运行测试 2好吗? plugin_test.exe 2 谢谢你, 米哈尔 Re: there has no FreeMaster plug-in module 非常感谢您在此期间的帮助,但这次仍然没有成功。
查看全文
IMX95 { 15 x 15 }はLPDDR4/4X 16 GB RAMをサポートしていますか? こんにちは、NXPチームの皆さん、 IMX95{ 15 x 15 }について一般的な情報が欲しいです。MIMX9556CVTXN"は16GBのRAMをサポートします{ LPDDR4/4X } "MT53E4G32D8GS-046 WT:C ?" 16GB RAMをIMX 95に接続するための回路図の参照が見つかりませんでした { 15x 15} 16GB RAMのIMX95 { 19 x 19 }の回路図しか見つけられませんでした。 もし対応しているなら、16GB RAM{ LPDDR4/4x }とimx95{ 15 x 15 }の接続について教えていただけませんか? そしてBSPファイルはどうですか?16GBのRAMに対してDTSファイルが存在するのか、それとも手動で生成する必要があるのか。 Yocto Project Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM こんにちは、 @Asadeds さん。 NXPサポートまでご連絡いただきありがとうございます。 当社の メモリ互換性ガイドによると、メモリ部品番号MT53E4G32D8GS-046はi.MX95と完全に互換性があり、このプラットフォーム上で徹底的に検証・テストされています。 したがって、このデバイスは推奨される構成および 設計ガイドラインに従い、i.MX95と併用可能です。 よろしくお願いします、 アレハンドロ・ガルシア Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM こんにちは、 @Asadeds さん。 MT53E4G32D8GSはサポートされているメモリデバイスであり、i.MX95との社内検証済みです。しかし、このデバイスは特別なバイトモード構成を使用しており、設定ツールとソフトウェアスタックの両方で追加のサポートが必要です。 現時点では内部サポートはありますが、現在のConfig Toolsの公開リリースには、この特定のメモリデバイスを設定するための必要なオプションはまだ含まれていません。このメモリのサポートはFUTUREツールリリースで予定されています。 よろしくお願いします、 チャビラ Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM こんにちは @Chavira  迅速な返信ありがとうございます。 DDRの設定を試みると「Imx 26.06のConfig tool」アプリケーションが表示され、対応可能な LPDDR4/4xは最大8GBまでしかなく、対応するパッケージは LPDDR5 を選択します 最大16GBです。 参考のためにスクリーンショットを添付しました。もし何か見落としている点があれば教えてください。 Asadeds_0-1784697908014.png Asadeds_1-1784698046354.png これについて助けていただけませんか?それと、プロジェクトにLPDDR4/4xを使いたいと思っています。部品番号は「MT53E4G32D8GS-046 WT:C」です。 Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM こんにちは、 @Chavira さん。 迅速なご返信ありがとうございます。 まだ混乱しているので、質問を簡単にしたいと思います。 今のところ、特定のRAMベンダーと部品番号は無視しましょう。 config Toolsが i.MX95 の 15× 15または 19×19 パッケージで 16GB LPDDR4/LPDDR4X メモリ をサポートしているか確認していただけます か? もし答えがノーなら、どうやって16GBのサポートを得るのでしょうか?社内サポートが利用可能だとおっしゃっていましたので、そのサポートにアクセスする手続きについて説明していただけると助かります。 現在、PCB設計を最終調整中で、RAMの選択肢のせいでプロジェクトは保留中です。これが前進を妨げる唯一の残された問題なので、できるだけ早く明確な答えが必要です。 ご回答をいただければ幸いです。 よろしくお願いします。 Re: Is IMX95 { 15 x 15 } supported LPDDR4/4X 16 GB RAM こんにちは、 @Asadeds さん。 社内チームと協議した結果、以下のとおり最新情報をお伝えいたします。 NXPは通常、四半期ごとに新しいバージョンのConfig Toolsをリリースするため、次のリリースはバージョン26.09が予定されています。 i.MX95自体はこの16GBメモリデバイスをサポートしていますが、現在の公開版DDR設定ツールはまだこの特定のメモリの設定をサポートしていません。良いニュースは、すでにツールの内部バージョンでサポートが存在しているものの、まだ公開リリースには組み込まれていないことです。 内部ツールへのアクセスが可能かどうかは確信が持てません。ただし、会社のメールアドレスを使って当 サイト からサポートケースを開くことをお勧めします。これにより、適切なチームがあなたの要望を確認し、追加のサポートや早期サポートの選択肢があるかどうかを判断できます。 ご不便をおかけし申し訳ありません。今後の公開リリースにこのサポートが統合されるまでのご理解に感謝いたします。 よろしくお願いします、 チャビラ
查看全文
Opinions on "Smart Energy" solar Edit: thanks everyone. Appreciate the input! I'll tell them to bugger off, I'm not ready to commit to anything anyway. I had some door knocker salesmen around today from Smart Energy wanting to talk about solar panels. I'm interested in solar but don't have the funds to invest up front and they said something about a govt funded scheme with $0 upfront. Naturally I'm very sceptical. Would love to hear from anyone who has dealt with them.
查看全文
mex config generate code different from windows and linux The same XEM file generates different code on different systems. Windows  file generate code normal but linux system generate abnormal precondition:the same as RTD and SDK version install 5.jpg Re: mex config generate code different from windows and linux Hi @Litten  Currently, RTDs are supported only on the Windows platform and are not officially supported on Linux. Even if you are able to install them on Linux, you may encounter additional issues during development and integration. One of the main reasons is that Linux is a case-sensitive operating system,  details about this situation have been discussed in the thread Problems with Lpi2c_Ip_MasterConfig and Lpi2c_Ip_SlaveState struct generation on S32DS for S32K344. BR, VaneB
查看全文
mex 配置生成的代码与 Windows 和 Linux 不同 同一个XEM文件在不同的系统中会生成不同的代码。 Windows系统生成的文件代码正常,但Linux系统生成的文件代码异常。 前提条件:与 RTD 和 SDK 版本安装相同 5.jpg Re: mex config generate code different from windows and linux 嗨@Litten 目前,RTD 仅在 Windows 平台上受支持,Linux 平台尚未获得官方支持。即使您能够在 Linux 上安装它们,在开发和集成过程中也可能会遇到其他问题。 主要原因之一是 Linux 是一个区分大小写的操作系统,有关此情况的详细信息已在 S32DS 上针对 S32K344 的 Lpi2c_Ip_MasterConfig 和 Lpi2c_Ip_SlaveState 结构体生成问题线程中进行了讨论。 BR,VaneB
查看全文
meter I'm trying to find the meter control within the components, but I can't find it.
查看全文