Camera sensor os02g10 MIPI CSI for IMX8MM Hi all. I got the driver for os02g10 from: https://github.com/Shaggy013/kernel-5.10 I added driver as a patch. My DeviceTree looks that: csi1_bridge: csi1_bridge@32e20000 {
compatible = "fsl,imx8mm-csi", "fsl,imx8mq-csi", "fsl,imx6s-csi";
reg = <0x32e20000 0x1000>;
interrupts = ;
clocks = <&clk IMX8MM_CLK_DISP_AXI_ROOT>,
<&clk IMX8MM_CLK_CSI1_ROOT>,
<&clk IMX8MM_CLK_DISP_APB_ROOT>;
clock-names = "disp-axi", "csi_mclk", "disp_dcic";
power-domains = <&dispmix_pd>;
status = "disabled";
};
mipi_csi_1: mipi_csi@32e30000 {
compatible = "fsl,imx8mm-mipi-csi";
reg = <0x32e30000 0x1000>;
interrupts = ;
clock-frequency = <360000000>;
clocks = <&clk IMX8MM_CLK_CSI1_CORE>,
<&clk IMX8MM_CLK_CSI1_PHY_REF>,
<&clk IMX8MM_CLK_DISP_AXI_ROOT>,
<&clk IMX8MM_CLK_DISP_APB_ROOT>;
clock-names = "mipi_clk", "phy_clk", "disp_axi", "disp_apb";
bus-width = <2>;
resets = <&mipi_csi_resets>;
power-domains = <&mipi_pd>;
status = "disabled";
};
os02g10: os02g10@3c {
compatible = "ovti,os02g10";
reg = <0x3c>; // spec (manual) says that I2c addres is 0x3d
status = "okay";
pinctrl-names = "rockchip,camera_default", "rockchip,camera_sleep";
pinctrl-0 = <&pinctrl_csi_pwdn>, <&pinctrl_csi_rst>, <&pinctrl_mux_oe>;
pinctrl-1 = <&pinctrl_csi_pwdn>, <&pinctrl_csi_rst>, <&pinctrl_mux_oe>;
csi_id = <0>;
pwdn-gpios = <&gpio2 16 GPIO_ACTIVE_HIGH>;
reset-gpios = <&gpio2 13 GPIO_ACTIVE_HIGH>;
mux-gpios = <&gpio2 14 GPIO_ACTIVE_HIGH>;
mclk = <24000000>;
mclk_source = <0>;
rockchip,camera-module-index = <1>;
rockchip,camera-module-facing = "back";
rockchip,camera-module-name = "OS02G10 camera";
rockchip,camera-module-lens-name = "1//2.9 inch 15*";
rockchip,camera-hdr-mode = <0>; // kernel-5.10\include\uapi\linux\rk-camera-module.h:307 (enum rkmodule_hdr_mode)
mipi_csi;
port {
os02g10_ep: endpoint {
remote-endpoint = <&mipi1_sensor_ep>;
};
};
};
};
&csi1_bridge {
fsl,mipi-mode;
status = "okay";
port {
csi1_ep: endpoint {
remote-endpoint = <&csi1_mipi_ep>;
};
};
};
&mipi_csi_1 {
status = "okay";
port {
#address-cells = <1>;
#size-cells = <0>;
mipi1_sensor_ep: endpoint@1 {
reg = <1>;
remote-endpoint = <&os02g10_ep>;
data-lanes = <2>;
csis-hs-settle = <13>;
csis-clk-settle = <2>;
csis-wclk;
};
csi1_mipi_ep: endpoint@2 {
reg = <2>;
remote-endpoint = <&csi1_ep>;
};
};
};
&clk {
init-on-array = ;
}; I modified probe function for camera driver and for mxc_mipi-csi.c, mx6s-csi.c Before I had 2 times format match error but I added to the mx6s-csi {
.name = "RAWRGB10 (SBGGR10)",
.fourcc = V4L2_PIX_FMT_SBGGR10,
.pixelformat = V4L2_PIX_FMT_SBGGR10,
.mbus_code = MEDIA_BUS_FMT_SBGGR10_1X10,
.bpp = 1,
} and added to mxc_mipi-csi.c {
.code = MEDIA_BUS_FMT_SBGGR10_1X10,
.fmt_reg = MIPI_CSIS_ISPCFG_FMT_RAW10,
.data_alignment = 8,
} and v4l2 API works, there is no error. Below my command to get picture v4l2-ctl -d /dev/video0 --verbose --set-fmt-video=width=1920,height=1080,pixelformat=BG10 --stream-mmap --stream-count=1 --stream-to=bb001.raw and the result with my debug messages mxc_mipi-csi 32e30000.mipi_csi: in function: mipi_csis_s_power
os02g10 3-003c: in function: os02g10_s_power
os02g10 3-003c: in function: os02g10_runtime_resume
os02g10 3-003c: in function: __os02g10_power_on
os02g10 3-003c: OS02G10_REG_SOFTWARE_RESET
mxc_mipi-csi 32e30000.mipi_csi: in function: mipi_csis_clk_enable
mxc_mipi-csi 32e30000.mipi_csi: enable mipi_clk returns: 0
mxc_mipi-csi 32e30000.mipi_csi: enable phy_clk returns: 0
mxc_mipi-csi 32e30000.mipi_csi: enable disp_axi returns: 0
mxc_mipi-csi 32e30000.mipi_csi: enable disp_apb returns: 0
VIDIOC_QUERYCAP: ok
VIDIOC_G_FMT: ok
mxc_mipi-csi 32e30000.mipi_csi: in function: mipi_csis_enum_mbus_code
os02g10 3-003c: in function: os02g10_enum_mbus_code
mxc_mipi-csi 32e30000.mipi_csi: camera sensor format (media-bus-format.h): 0x3007
mxc_mipi-csi 32e30000.mipi_csi: supported format0 by mipi-csi driver: 0x2008
mxc_mipi-csi 32e30000.mipi_csi: supported format1 by mipi-csi driver: 0x2007
mxc_mipi-csi 32e30000.mipi_csi: supported format2 by mipi-csi driver: 0x3001
mxc_mipi-csi 32e30000.mipi_csi: supported format3 by mipi-csi driver: 0x3007
mx6s-csi 32e20000.csi1_bridge: in function: mx6s_vidioc_enum_fmt_vid_cap - format RAWRGB10 (SBGGR10)
mxc_mipi-csi 32e30000.mipi_csi: in function: mipi_csis_set_fmt
VIDIOC_S_FMT: ok
Format Video Capture:
Width/Height : 1920/1080
mxc_mipi-csi 32e30000.mipi_csi: in function: mipi_csis_enum_mbus_code
os02g10 3-003c: in function: os02g10_enum_mbus_code
mxc_mipi-csi 32e30000.mipi_csi: camera sensor format (media-bus-format.h): 0x3007
mxc_mipi-csi 32e30000.mipi_csi: supported format0 by mipi-csi driver: 0x2008
mxc_mipi-csi 32e30000.mipi_csi: supported format1 by mipi-csi driver: 0x2007
mxc_mipi-csi 32e30000.mipi_csi: supported format2 by mipi-csi driver: 0x3001
mxc_mipi-csi 32e30000.mipi_csi: supported format3 by mipi-csi driver: 0x3007
mx6s-csi 32e20000.csi1_bridge: in function: mx6s_vidioc_enum_fmt_vid_cap - format RAWRGB10 (SBGGR10)
Pixel Format : 'BG10' (10-bit Bayer BGBG/GRGR)
Field : None
Bytes per Line : 1920
Size Image : 2073600
Colorspace : sRGB
Transfer Function : Default (maps to sRGB)
YCbCr/HSV Encoding: ITU-R 601
Quantization : Full Range
Flags:
mxc_mipi-csi 32e30000.mipi_csi: in function: mipi_csis_s_stream
mxc_mipi-csi 32e30000.mipi_csi: in function: mipi_csis_clear_counters
mxc_mipi-csi 32e30000.mipi_csi: in function: mipi_csis_start_stream
mxc_mipi-csi 32e30000.mipi_csi: in function: mipi_csis_sw_reset: REG CMN_CTRL 0x32E30004 = 0x00004000
mxc_mipi-csi 32e30000.mipi_csi: in function: mipi_csis_set_params
mxc_mipi-csi 32e30000.mipi_csi: in function: __mipi_csis_set_format
mxc_mipi-csi.0: fmt: 0x3007, 1920 x 1080
mxc_mipi-csi 32e30000.mipi_csi: in function: __mipi_csis_set_format: REG ISPRESOL_CH0 0x32E30044 = 0x04380780
mxc_mipi-csi 32e30000.mipi_csi: in function: mipi_csis_set_hsync_settle: REG DPHYCTRL 0x32E30024=0x0d800000
mxc_mipi-csi 32e30000.mipi_csi: in function: mipi_csis_set_params: REG CMN_CTRL 0x32E30004 = 0x00004104
mxc_mipi-csi 32e30000.mipi_csi: in function: mipi_csis_system_enable: REG CMN_CTRL 0x32E30004=0x00004105
VIDIOC_REQBUFS returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_QUERYBUF returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
VIDIOC_QBUF returned 0 (Success)
mxc_mipi-csi 32e30000.mipi_csi: in function: mipi_csis_system_enable: REG DPHYCTRL 0x32E30024=0x0d800007
mxc_mipi-csi 32e30000.mipi_csi: in function: mipi_csis_enable_interrupts: REG CSIS_INTMSK 0x32E30010 = 0xf00fffff
mxc_mipi-csi.0: --- mipi_csis_start_stream ---
mxc_mipi-csi.0: 0x04 CMM CTRL : 0x00004105
mxc_mipi-csi.0: 0x08 CLK CTRL : 0x000f0000
mxc_mipi-csi.0: 0x10 INT MASK0: 0xf00fffff
mxc_mipi-csi.0: 0x14 INT SRC0 : 0x00000000
mxc_mipi-csi.0: 0x18 INT MASK1: 0x00000000
mxc_mipi-csi.0: 0x1c INT SRC1 : 0x00000000
mxc_mipi-csi.0: 0x20 PHY STAT : 0x000000f1
mxc_mipi-csi.0: 0x24 PHY CTRL : 0x0d800007
mxc_mipi-csi.0: 0x30 PHY M/S-L: 0x000001f4
mxc_mipi-csi.0: 0x34 PHY M/S-H: 0x00000000
mxc_mipi-csi.0: 0x38 PHY S-CTL: 0x00000000
mxc_mipi-csi.0: 0x3C PHY S-CTH: 0x00000000
mxc_mipi-csi.0: 0x40 ISP CONF : 0x000000ac
mxc_mipi-csi.0: 0x44 ISP RESOL: 0x04380780
mxc_mipi-csi.0: 0x48 ISP SYNC : 0x04380780
os02g10 3-003c: in function: os02g10_s_stream
os02g10 3-003c: in function: __os02g10_start_stream
os02g10 3-003c: in function: __os02g10_start_stream __v4l2_ctrl_handler_setup returns: 0
os02g10 3-003c: in function: os02g10_s_stream: unlock_and_return
VIDIOC_STREAMON returned 0 (Success) After that nothing is going to happen, just waiting and waiting and nothing. I can not observe any traffic on MIPI DATA and MIPI CLK lines by 20MHz oscilloscope. (I know the bandwidth is low but for data lines there should be anything seen - any change but there is completely silence) Im not sure if clk node is correct and maybe there is no match &clk node with mipi_csi clocks by clock names. Has anyone experience with it? What can I do ? i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: Camera sensor os02g10 MIPI CSI for IMX8MM Hi, you can use our linux upstreamed driver, we have tested this on i.mx8mp based debix platform. Here is our driver https://web.git.kernel.org/pub/scm/linux/kernel/git/next/linux-next.git/commit/?id=263d0fa1d46ac1ae2eebc5a5490fec58233c69ad Here is our DT https://web.git.kernel.org/pub/scm/linux/kernel/git/next/linux-next.git/commit/?id=a4d0f0c88ae8185315afbc1eb68c978ed710f759 -- Rutvij SiliconSignals Re: Camera sensor os02g10 MIPI CSI for IMX8MM I got it to work. .bpp has to be = 2 but main issue was with hardware
View full article