2394848_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2394848_en-US

2394848_en-US

What is the min to max sleep current mA for the iMX 937 processor
 
In my project I am using I.MX937 processor, what is the typical sleep current (mA) for the i.MX 937 processor? 
 
Re: What is the min to max sleep current mA for the iMX 937 processor

With those resources required to stay functional, 150 µA sleep current is not realistic for the i.MX 937 / i.MX 93 processor itself .

Why:

Mode Current/power implication Fits 150 µA? Functional fit
BBSM / RTC mode Datasheet lists 0.14 mW at 1.8 V , and the power-measurement app note shows about 97.978 µW total , with only NVCC_BBSM_1P8 active. Power-wise, yes No — only BBSM/RTC logic remains powered; GPIO wakeup is OFF, and timer/PWM/ADC are not available.
Suspend Datasheet lists 15.1 mW typical at 25 °C. No — far above 150 µA equivalent No / limited — suspend turns off clocks, powers down the Cortex-A55, and powers down internal logic/analog blocks that can be shut off.
Linux Suspend + M33 in WFI App note lists 122.4 mW total for this use case. No Closer architecturally, but still far above your current target.
Low-power run / AONMIX using Cortex-M33 AONMIX can run while other domains are powered down, and includes timer/PWM and timer resources. Not documented as meeting 150 µA This is the relevant i.MX 93 mode class if peripherals must remain active, but it is not a 150 µA-class mode.
 

A 150 µA budget corresponds to only 0.27 mW at 1.8 V or 0.495 mW at 3.3 V . That is in the range of the i.MX 93 BBSM/RTC-only state, not a state with active timer output, ADC, PWM, RTC, and GPIOs.

Recommended architecture: keep the i.MX 937 in BBSM/RTC or fully power-gated sleep , and move the always-on functions — timer output, ADC monitoring, PWM, and GPIO supervision — to a very-low-power companion MCU or analog/RTC circuit. The companion device can wake the i.MX 937 when the condition is met.

The i.MX 937 can meet ~150 µA only in a very limited RTC/BBSM-style state; it cannot keep timer/PWM/ADC/GPIO functionality active within that current budget.

Re: What is the min to max sleep current mA for the iMX 937 processor

In our application, the following resources are required to remain functional during the low-power/sleep mode:

  • 1 Timer output pin
  • 1 ADC input
  • 1 PWM
  • RTC
  • 2–3 GPIOs

Our requirement of sleep current is 150 µA.

Re: What is the min to max sleep current mA for the iMX 937 processor

For the i.MX 937 / i.MX 93 processor itself, the datasheet does not give a single “sleep current” in mA. It specifies SUSPEND mode total power = 15.1 mW at 25 °C , and notes that the number is use-case dependent . SUSPEND is the lowest-power mode where clocks are off, unnecessary supplies are off, power-gateable SoC portions are gated, Cortex-A55 is fully power-gated, and DRAM is in self-refresh/retention.

If you need an equivalent current for budgeting, use:

yipingwang_0-1784086916714.pngyipingwang_0-1784086916714.png




So 15.1 mW corresponds approximately to:

Assumed supply basis

Equivalent current

5.0 V input

3.0 mA

3.3 V input

4.6 mA


That is an equivalent input current , not a single SoC rail current; the actual processor current is distributed across multiple power rails.

If you mean board/SOM deep-sleep current , measured values can be higher and configuration-dependent. One i.MX93 SOM DSM measurement reported 4.04 mA at 5 V , with other optimized/configuration-dependent reports around 1.5 mA to 9.3 mA at 5 V .

Use 15.1 mW typical SUSPEND power for the processor spec; convert to mA only against your actual input rail, e.g. about 3.0 mA at 5 V .

Tags (1)
No ratings
Version history
Last update:
‎07-15-2026 02:27 AM
Updated by: