This article walks through the complete process of setting up the NXP Model-Based Design Toolbox (MBDT) and running a first application on NXP hardware. Before starting the installation, make sure that the prerequisite toolboxes are available in MATLAB. By the end of this guide, the reader will have a fully functional MBDT environment and will have successfully generated, compiled, and deployed embedded C code from a Simulink model to NXP hardware.
This guide begins with the installation prerequisites and required toolboxes, then continues with the MATLAB Add-On Explorer flow for installing NXP_Support_Package_S32K3. After the support package is installed, the guide explains how to launch the multistep installer, verify the required toolboxes and installation path, download the toolbox package from NXP, and complete the toolbox installation before running the first application.
This article focuses on practical installation flow required to start working with the NXP Model-Based Design Toolbox and run a first example application. It covers the software prerequisites, the toolbox setup sequence, and the validation steps needed before opening and deploying a model on the target board. The installation content in this guide should use the current multistep installer flow.
This article is intended for engineers and technical professionals who want to begin developing embedded applications for NXP hardware using a Model-Based Design workflow. The main target audience includes:
Before starting the installation, verify that the following prerequisite toolboxes and setup conditions are met:
Figure 1 - MATLAB Add-On Manager confirming requirement are installed
NXP's Model-Based Design Toolbox is delivered as a MATLAB Toolbox Package that can be installed offline or online from MathWorks Add-ons. The recommended installation path uses the NXP Support Package, a graphical wizard that guides through download, installation, and license activation in a single workflow.
{platform} refers to the NXP MCU family targeted by the toolbox (for example S32K3, S32K1, S32M2, MPC57XX, etc.). Each family has its own dedicated Support Package and Toolbox in the MATLAB Add-On Explorer. When following the steps below, replace {platform} with the identifier matching the hardware family in use, for instance, for the S32K3 evaluation boards, the script name becomes NXP_Support_Package_s32k3.m and the path command becomes mbd_s32k3_path.Install the current NXP support package directly from the MATLAB Add-On Explorer. This package provides the multistep installer flow used to verify prerequisites, download the toolbox, and guide the installation for S32K3.
In MATLAB, navigate to Home → Add-Ons → Get Add-Ons.
image2.png
Figure 2 - Open the Add-On Explorer from the MATLAB Home tab
Search for NXP_Support_Package_S32K3 in the Add-On Explorer.
image3.png
Figure 3 - Search results for NXP_Support_Package_S32K3 in the Add-On Explorer
Open the package page and click Add to start the installation.
image4.png
Figure 4 - Open the NXP_Support_Package_S32K3 page and click Add
Review the license agreement for NXP_Support_Package_S32K3 and click I Accept.
image5.png
Figure 5 - License agreement shown during installation of NXP_Support_Package_S32K3
Wait for the installation to complete. When finished, the Getting Started Guide opens automatically.
image6.png
Figure 6 - Support package installation completed successfully
In the MATLAB Command Window, run sp_s32k3.nxp.setup(); to launch the multistep installer.
sp_s32k3.nxp.setup();
image7.png
Figure 7 - Run sp_s32k3.nxp.setup(); from the MATLAB Command Window
The multistep installer guides you through prerequisite verification, toolbox download, installation, activation, and access to the documentation for S32K3.
image8.png
Figure 8 - Welcome page of the S32K3 multistep installer
In the installer, continue to the download step. On the NXP website, review the software terms and conditions and click I Agree before downloading the toolbox package. If the product download page does not open automatically, sign in to your NXP account and open the Product Download page for the required S32K3 toolbox release or click the link from Download page of the S32K3 multistep installer.
image9.png
Figure 9 - Download page of the S32K3 multistep installer
image10.png
Figure 10 - Accept the NXP software terms and conditions before downloading
Download the toolbox package from the Product Download page. The installer accepts both .zip and .mltbx files.
image11.png
Figure 11 - Product Download page for the S32K3 MBDT package
The setup verification step checks whether all required toolboxes are installed in MATLAB and whether the installation path is valid for the S32K3 toolbox setup. If any dependency is missing or an unsupported version is detected, resolve the issue before continuing to the download and installation steps.
image12.png
Figure 12 - Setup verification page showing required toolboxes and installation path checks
After downloading the package, return to the installer and continue with the local file selection step. Browse to the downloaded archive or toolbox package and click Install to continue. The installer accepts both .zip and .mltbx files.
image13.png
Figure 13 - Browse to and download the S32K3 MBDT package from the Product Download page
image14.png
Figure 14 - Accept the license agreement for NXP_MBDToolbox_S32K3
Accept the toolbox license agreement to allow MATLAB to complete the MBDT installation.
image15.png
Figure 15 - Toolbox installation in progress
After the installation is complete, use the Add-On Manager context menu to open the installed toolbox folder if you need to inspect the package contents or access installed files directly.
Wait until the installation finishes. The process may take several minutes depending on the system configuration and package size.
image16.png
Figure 16 - Open the installed toolbox location from MATLAB Add-On Manager
The MBDT uses Simulink's toolchain mechanism to enable automatic code generation with Embedded Coder. When installed as a MATLAB add-on, the toolbox path is configured automatically. If manual configuration is still required in your environment, run the platform path script from the installation directory.
If manual setup is required, in MATLAB change the Current Directory to the toolbox installation folder:
..\MATLAB\Add-Ons\Toolboxes\NXP_MBDToolbox_{platform}\
Then run the configuration script:
mbd_{platform}_path
image17.png
Figure 17 - Output of the mbd_{platform}_path script in the MATLAB Command Window
With the toolbox installed and the compiler configured, the following steps demonstrate how to open, build, and deploy the LED blinky example - the embedded equivalent of Hello World to an NXP evaluation board.
Open MATLAB and start Simulink by typing simulink in the Command Window (or by clicking the Simulink button on the Home tab).
In the Simulink Start Page, open the Simulink Library Browser (View → Library Browser, or press Ctrl+Shift+L).
In the Library Browser tree, expand NXP Model-Based Design Toolbox for {platform} to confirm that the NXP blocks are available. This validates that the toolbox is properly registered with Simulink.
Open the Example Projects tab from the Simulink Start Page, it lists every example shipped with the MBDT, grouped by peripheral (ADC, CAN, DIO, PWM, UART, etc.). Browse the list, select the example matching your hardware (for instance s32k3xx_dio_s32ct for the LED blinky on FRDM-A-S32K312 / FRDM-A-S32K344), and click Open to load the model.
image18.png
Figure 18 - MBDT Examples Library available from the Simulink Library Browser
Open the example model (.slx/.mdl file).
image19.pngFigure 19 - Model Settings
image20.png
Figure 20 - Code Generation
This article described the complete setup of the NXP Model-Based Design Toolbox: from installation and compiler configuration to building and deploying a first application to NXP hardware.
The next article in the series focuses on the Toolbox Workflow, presenting in detail the end-to-end development flow with the MBDT, from configuring a Simulink model with NXP blocks, through code generation with Embedded Coder, to building, deploying and validating the resulting application on NXP hardware.