2394729_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2394729_en-US

2394729_en-US

KW47 extended advertising

Hi,

The sdk version I'm using is 26.06 .

The routine is kw47loc_loc_reader_freertos .

#define gAppIsPeripheral_d                   1U
 
It was found that the return value of calling BluetoothLEHost_StartExtAdvertising is 4(gBleFeatureNotSupported_c) 
I'd like to use extended advertising. Please give me your support.
 
Thanks!
 
Re: KW47 extended advertising

Hello,
Hope you are doing well.


What modifications have you made in the example? In order to configure Extended Advertising in an application, the first steps are to set the extended advertising parameters with Gap_SetExtAdvertisingParameters and setting the advertising data by calling Gap_SetExtAdvertisingData.

For the full setup sequence and parameter details, please check this guide: Extended advertising — MCUXpresso SDK Documentation

 

Hope this helps!

Best regards,
Ana Sofia.

Re: KW47 extended advertising

Hi,

The sdk version I'm using is 26.06. The imported routine is kw47loc_loc_reader_freertos.  Modify the macro definition of gAppIsPeripheral_d in the routine to 1, and at the same time add BleApp_Start() in the BluetoothLEHost_AppInit function;  Nothing else has been modified.

It was found that the return value of calling BluetoothLEHost_StartExtAdvertising is 4(gBleFeatureNotSupported_c) 
wjw2026_1-1784164794603.pngwjw2026_1-1784164794603.png
wjw2026_0-1784164779249.pngwjw2026_0-1784164779249.png
 
Thanks!
Re: KW47 extended advertising

Hi @wjw2026 ,

Could you please confirm if you were able to follow the steps from the Extended Advertising Guide ? There are several required steps involved in the Peripheral configuration for extended advertising, verifying those settings may be helpful in troubleshooting the behavior you're observing.


Best regards,
Ana Sofia.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-21-2026 02:37 AM
更新者: