Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Security software consultation for s32k388 I'd like to know if there's a security development kit (SDK) for the S32K388 similar to Example_S32K344_BIST_eMCEM_SPD106_v2_0_S32DS365_RTD700. I'm currently developing security-related code for the S32K388, and I'm using the manual and the example code 344 as a reference. However, the development process isn't going very smoothly. Having the source code for a software security kit for the S32K388 would be extremely helpful, and I need NXP's support for this. 1. If you have a free s32k388 security resource package, please provide the path to it. 2. If it's not free, then we can arrange for procurement or purchase to facilitate development. Please provide the procurement channels. Thanks! Re: s32k388的安全软件咨询 Hello @xlele, I've used translator for this question, so please let me know if there are any misunderstandings. Example_S32K344_BIST_eMCEM_SPD106_v2_0_S32DS365_RTD700 is provided as a reference example on how to implement BIST & eMCEM modules, which are provided for all S32K3 derivatives. 1. Yes, SPD (BIST & eMCEM modules) are available as Standard SW (included in silicon price) for S32K388 and all other S32K3 derivatives. You can see in the latest release for S32K3 Safety Peripheral Drivers v1.0.6, S32K388 is included in the supported derivatives: Julin_AragnM_1-1788551806085.pngJulin_AragnM_1-1788551806085.pngJulin_AragnM_1-1788551806085.png Julin_AragnM_2-1788551809724.pngJulin_AragnM_2-1788551809724.pngJulin_AragnM_2-1788551809724.png You can access the SW package through: "Automotive SW - S32K3 Standard Software > Automotive SW - S32K3 - Safety Peripheral Drivers (SPD)" 2. Added to SPD, we also provide SAF package which includes: BIST (same as SPD) eMCEM (same as SPD) Mode Selector SW Recovery sBoot SquareCheck Julin_AragnM_3-1788551884442.pngJulin_AragnM_3-1788551884442.pngJulin_AragnM_3-1788551884442.png SAF is provided as premium/licensed software, for availability and pricing information, please help me by contacting your NXP representative, or assigned salesperson.  Best regards, Julián Re: s32k388的安全软件咨询 We appreciate your help and your patien.
View full article
S32DSライセンスの延長申請 こんにちは、NXPサポートの皆さん、 S32 Design Studioのライセンス延長を手伝ってください アクティベーションID: 4C09-7241-70F8-E2D3 ご協力の程、よろしくお願い申し上げます。 Re: Request to extend S32DS license こんにちは、 お客様のS32DSライセンスが延長されました。以前使用していたコードを使って、S32DSを再度有効化してください。 Re: Request to extend S32DS license アクティベートIDを削除し、返品番号をリセットするのを手伝ってください。 ありがとうございます。 Re: Request to extend S32DS license 私が言っているのは、投稿の中に隠されている情報のことです。 よろしくお願いします。
View full article
LCD and MIPI Camera Proven on i.MX6ULL Hello,   Could you please recommend an LCD panel and a MIPI camera that have been successfully used with the i.MX6ULL?   I would like to connect them to the following evaluation board:   MCIMX6ULL-EVK https://www.nxp.jp/part/MCIMX6ULL-EVK   If possible, please provide the model numbers and any available software/BSP information.   Thank you. Re: LCD and MIPI Camera Proven on i.MX6ULL Hello, On this board, validated Parallel-LCD Display are: SEIKO WVGA panel. Embest LCD8000-43T LCD panel. Regarding MIPI CSI camera, please take a look into a OV5640 camera sensor. Best regards. Re: LCD and MIPI Camera Proven on i.MX6ULL Thank you for your response. I have given up on using the OV5640 camera sensor because I could not find a product that can be connected to the i.MX6ULL. For the LCD, I plan to use the LCD8000-43T.
View full article
i.MX6ULL 已验证 LCD 和 MIPI 摄像头功能 你好,   请问您能否推荐一款已成功与 i.MX6ULL 配合使用的液晶面板和 MIPI 摄像头?   我想将他们与以下评估板联系起来:   MCIMX6ULL-EVK https://www.nxp.jp/part/MCIMX6ULL-EVK   如果可以,请提供型号以及任何可用的软件/BSP信息。   谢谢! Re: LCD and MIPI Camera Proven on i.MX6ULL 你好, 该电路板上经过验证的并行液晶显示器有: 精工WVGA面板。 Embest LCD8000-43T液晶面板。 关于 MIPI CSI 摄像头,请参考 OV5640 摄像头传感器。 顺祝商祺! Re: LCD and MIPI Camera Proven on i.MX6ULL 感谢您的反馈, 我已经放弃使用 OV5640 相机传感器,因为我找不到可以连接到 i.MX6ULL 的产品。 LCD方面,我计划使用LCD8000-43T。
View full article
i.MX6ULLでLCDとMIPIカメラの性能が実証されました こんにちは、   i.MX6ULLで成功裏に使われたLCDパネルとMIPIカメラをおすすめしていただけますか?   以下の評価ボードに彼らをつなげたいと思います。   MCIMX6ULL-EVK https://www.nxp.jp/part/MCIMX6ULL-EVK   可能であれば、モデル番号および利用可能なソフトウェア/BSP情報をご提供ください。   よろしくお願いします。 Re: LCD and MIPI Camera Proven on i.MX6ULL こんにちは、 このボード上で検証済みのパラレルLCDディスプレイは以下のとおりです。 セイコー製WVGAパネル。 Embest LCD8000-43T LCDパネル。 MIPI CSIカメラについては、OV5640カメラセンサーを検討してみてください。 よろしくお願いいたします。 Re: LCD and MIPI Camera Proven on i.MX6ULL ご返信ありがとうございます。 i.MX6ULLに接続できる製品が見つからなかったため、OV5640カメラセンサーの使用を諦めました。 液晶ディスプレイには、LCD8000-43Tを使用する予定です。
View full article
i.MX95 Triple display Linux Patch i.MX95 Triple Display Patches for LF-6.6.52-2.2.0 BSP. iMX95 19x19 EVK. qiang_limpu_se_0-1739859470230.pngqiang_limpu_se_0-1739859470230.png   Patches files: 0001-iMX95-EVK-IT6263-LVDS-to-HDMI-bridge-chip-combine-it.patch Combine IT6263 with simple panel driver, no EDID is needed, 720P and 1080P display mode had been added as two examples.   0002-IT6263-Always-reported-connected-for-force-output.patch Let IT6263 always report cable connected to force output HDMI signals.   0003-iMX95-EVK-add-LVDS-clone-mode-based-on-IT6263.patch LVDS clone mode is supported on two LVDS ports, they output same content and same timing from one DPU display engine (1920*1080@60fps).   0004-iMX95-EVK-add-dual-LVDS-interleaver-mode-based-on-IT.patch LVDS interleave mode is supported on two LVDS ports, they output different content and same timing from one DPU display engine (3840*1080@60fps).   0005-iMX95-EVK-add-triple-display-support.patch Triple display is supported, 1 MIPI DSI + 2 LVDS.  imx95-19x19-evk-triple-display-lvds-clone.dtb: the two LVDS is in clone mode. imx95-19x19-evk-triple-display-lvds-interleaver.dtb: the two LVDS is in interleave mode.   For 1 MIPI DSI + 2 LVDS display clone mode: qiang_limpu_se_0-1739858854733.pngqiang_limpu_se_0-1739858854733.png For 1 MIPI DSI + 2 LVDS Interleave mode: qiang_limpu_se_2-1739859096402.pngqiang_limpu_se_2-1739859096402.png Know issues:  Due to bridge numbers (3) and DPU engine/Pixel link/Pixel Interleaver number (2) is not aligned, during kernel boot up, there will be followed link error log, but there is no real function impact.   [    3.178741] imx95-ldb 4b0c0000.syscon:ldb@4: Failed to create device link (0x180) with 4b010000.syscon:bridge@8 ... [    4.209299] imx95-pixel-interleaver 4b0d0000.bridge: Failed to create device link (0x180) with 4b400000.display-controller [    4.220355] imx95-pixel-interleaver 4b0d0000.bridge: Failed to create device link (0x180) with 4b400000.display-controller ...     2025-8-19 update: Add the patch for L6.12.20_2.0.0 BSP. lf-6.12.20-2.0.0_triple_display_patches.zip   2026-9-7 update: Add patch for L6.18.37_2.1.0 BSP based on FRDM-IMX95.   BL: Auto BL: non-Auto
View full article
Request for Old Version of Code Signing Tool (CST) for i.MX6Q HAB Development Dear NXP Technical Support Team, I am currently developing a High Assurance Boot (HAB) secure boot solution based on the ‌i.MX6Q SabreSD platform‌, using the official NXP BSP release L3.14.52_1.1.0 GA which is fully validated for our product. The latest CST v3.1.0 downloaded from the official portal is not fully compatible with this legacy BSP version, and it cannot generate valid signature data that matches the HABv4 protocol of i.MX6Q. This blocks our subsequent secure boot verification work. I have already read and accepted the NXP Software License Agreement for the Code Signing Tool, and I confirm that this tool will only be used for internal product development on our NXP i.MX series chips. Could you please provide the download link for ‌CST v2.3.2 (for HABv4)‌? This version is the officially recommended matching tool for the i.MX6Q BSP we are using. If you need any additional information about our project or chip part number, please feel free to contact me. Thank you for your support. Best regards, lixuehui i.MX6Quad Re: Request for Old Version of Code Signing Tool (CST) for i.MX6Q HAB Development Hello, Hope you're doing well, I can share an old version but I cannot share it here on the community, please help me creating a support ticket and ask for me on it so I can track it. https://support.nxp.com/s/?language=en_US Best regards/Saludos, Aldo. Re: Request for Old Version of Code Signing Tool (CST) for i.MX6Q HAB Development Hello, I’m working with an i.MX6Q SabreSD and the legacy L3.14.52_1.1.0 BSP, but CST v3.1.0 isn’t fully compatible. Any official download link or guidance would be greatly appreciated.  Re: Request for Old Version of Code Signing Tool (CST) for i.MX6Q HAB Development NXP’s current i.MX6Q software page lists CST 3.1.0 as the downloadable “i.MX High Assurance Boot Reference Code Signing Tool,” revision 3.1.0. fmc4me
View full article
VSC拡張機能にボード番号やデバイス番号が記載されていないプロジェクトを作成する方法 VS CodeのMCUXpresso拡張機能で、デバイス/ボードがライブラリに表示されていない場合、新しいプロジェクトを作成するにはどうすればよいですか? VS Codeのバージョンは1.135.0、MCUXpresso拡張機能のバージョンは26.06.123です。MCUXpresso SDKの開発はバージョン26.06に、Arm GNU Toolchainは14.2.1にインストールされています。 LPC1768向けにコードリポジトリを再構築しました。部品番号がリストになければ、プロジェクトを作成できないようです......(添付のスナップショットでは「プロジェクト作成」ボタンがグレーアウトしています。) お知らせ下さい。 # VSCode #MCUXpress LPC1768FBD100 回复: How to create a project without a board or device number listed in the VSC extension こんにちは、 @Microsystemca 新しいプロジェクトウィザードは、インポートされたMCUXpresso SDKリポジトリ(またはSDK Builderパッケージ)に含まれるデバイスやボード用プロジェクトのみを作成できます。ターゲットデバイスがSDKパッケージに含まれていない場合、ウィザードは必要なデバイスやボードの定義を見つけられず、新しいプロジェクトを直接作成できません。 新しいプロジェクトウィザード — MCUXpresso for VS Code 26.08 ドキュメント 回避策として、MCUXpresso IDEを使って対応するデバイスサポートパッケージをインストールし、そこでターゲットデバイス用のプロジェクトを作成することができます。プロジェクトがMCUXpresso IDEで正常に作成・構築されたら、MCUXpresso for VS Codeの「プロジェクトインポート」機能を使って既存のプロジェクトをインポートし、VS Code環境内での開発を継続できます。 BR ハリー 回复: How to create a project without a board or device number listed in the VSC extension 回避策を教えていただきありがとうございます。私たちはそれを実行しましたが、うまくいっているようです。ちなみに、MCUXpresso IDEは一部の企業が採用しているセキュリティ標準と完全に互換性がなく、インストール後にコンピュータのフルスキャンがトリガーされました。SHA/MCXハッシュは発行元不明です。VSCode MCUXpressoは、Microsoftの認証を受けているため、直接インストールできます。だからユーザーはすべてのパーツをVSCode MCUXpressoリポジトリにまとめておきたいのです。
View full article
S32K142 PWM Signal input reading Hello Team, Is there any example available for PWM reading in S32K142 using FTM input capture? If yes, please share the example. Re: S32K142 PWM Signal input reading Hello @Julián_AragónM , Thank you so much for quick reply. One small doubt, can i use single CH to measure both duty cycle and period?  If i set input capture mode as DETECT BOTH EDGE. What measurement value i will get from IC_GetMeasurement? Re: S32K142 PWM Signal input reading Hello @nirmal_masilamani, You can refer to: Example 4. from AN5303: Features and Operation Modes of FlexTimer Module on S32K – Application Note. Example 2.5 Timed I/O (FTM) from AN5413: S32K1xx Series Cookbook – Application Note Ftm_Icu_Ip_BlinkLed_S32K144 example from RTD package (uses Ftm_Icu_Ip_EnableEdgeDetection API) ic_pal & ftm_signal_measurement examlpes from SDK You can also refer to some community posts: s32k1:How to measure PWM frequency and duty cycle on the same FTM channel S32K Input Capture S32K1-Calculate the motor speed based on the FTM Hope this helps. Best regards, Julián   Re: S32K142 PWM Signal input reading Hello @nirmal_masilamani, Input capture supports 3 modes: Capture on Rising Edge Only -> period only Capture on Falling Edge Only -> period only Capture on Rising or Falling Edge -> Need to read the level status through GPIO or CnSC [CHIS] bit to know the high-level pulse width or the low-level pulse width. NOTE: The CHIS bit should be ignored when the channel (n) is not in an input mode. NOTE: When the pair channels is on dual edge mode, the channel (n+1) CHIS bit is the channel (n+1) input value and not the channel (n) input value (this signal is the input signal used by the dual edge mode). For PWM duty cycle capture, you should use dual edge capture. Otherwise, you will only get the period of high level or low level. In the dual edge capture mode, only channel (n) input is used and channel (n+1) input is ignored. Julin_AragnM_0-1788457862022.pngJulin_AragnM_0-1788457862022.pngJulin_AragnM_0-1788457862022.png IC_GetMeasurement will return the pulse width in ticks, which you can then use to calculate signal frequency:  /* Get the latest value */ inputCaptureMeas = IC_GetMeasurement(&ic_pal_1_instanceConfig, channel); /* Calculate the signal frequency using recorded data*/ inputCaptureMeas = frequency / (inputCaptureMeas); Best regards, Julián Re: S32K142 PWM Signal input reading Hello @Julián_AragónM , Thank you for reply. I am still little confused. To measure PWM signal, how many pins i need?  I am using IC_PAL for measuring. But i am unable to measure PWM using signal pin and single ch. RTD used V4.0.0
View full article
I want to know the CCO of MC34PF3000A7E The factory label only shows it was assemblied in PH, but I don't the Chip Country of Original. Could you tell me how I can find out it through label information? Thanks a lot
View full article
如何在 VSC 扩展中未列出板或设备编号的情况下创建项目 如果设备/板未列在库中,我们如何在 VSCode MCUXpresso 扩展中创建新项目? VSCode 版本为 1.135.0,MCUXpresso 扩展版本为 26.06.123。MCUXpresso SDK 开发版已安装至 26.06 版本,Arm GNU 工具链已安装至 14.2.1 版本。 我们重新构建了 LPC1768 的代码仓库。如果零件编号不在列表中,我们就无法创建项目……(附图中,“创建项目”按钮呈灰色。) 请指教。 # VSCode #MCUXpress LPC1768FBD100 回复: How to create a project without a board or device number listed in the VSC extension 您好@Microsystemca 新建项目向导只能为导入的 MCUXpresso SDK 存储库(或 SDK 构建器包)中包含的设备或板创建项目。如果目标设备在 SDK 包中不可用,向导将无法找到所需的设备或板定义,因此无法直接创建新项目。 新建项目向导 — MCUXpresso for VS Code 26.08 文档 作为一种变通方法,您可以使用 MCUXpresso IDE 安装相应的设备支持包,并在其中为目标设备创建一个项目。项目在 MCUXpresso IDE 中成功创建和构建后,您可以使用 MCUXpresso for VS Code 中的“导入项目”功能导入现有项目,并在 VS Code 环境中继续开发。 BR 哈里 回复: How to create a project without a board or device number listed in the VSC extension 谢谢你提供的解决方法。我们照做了,而且似乎效果不错。需要注意的是,MCUXpresso IDE 与某些公司采用的**网络安全**标准并不完全兼容,安装后会触发对计算机的全面扫描。安全散列算法(SHA)/MCX 哈希值来自未知发布者。由于获得了微软认证,VSCode MCUXpresso 可以直接安装。这就是为什么用户更希望 VSCode MCUXpresso 仓库中列出所有部件的原因。
View full article
S32K142 PWM信号输入读取 各位团队成员,大家好! 是否有使用 FTM 输入捕获在 S32K142 中读取 PWM 的示例? 如果可以,请分享一下例子。 Re: S32K142 PWM Signal input reading 你好@Julián_AragónM , 非常感谢您的快速回复。 还有一个小疑问,我可以用单个通道同时测量占空比和周期吗? 如果我将输入捕获模式设置为检测两侧边缘。我从IC_GetMeasurement 函数会得到什么测量值? Re: S32K142 PWM Signal input reading 你好@nirmal_masilamani , 您可以参考: 示例 4.来自AN5303:S32K 上 FlexTimer 模块的特性和操作模式 – 应用笔记。 示例 2.5 定时 I/O (FTM) (摘自AN5413:S32K1xx 系列应用笔记) 来自 RTD 包的 Ftm_Icu_Ip_BlinkLed_S32K144 示例(使用Ftm_Icu_Ip_EnableEdgeDetection API) SDK 中的 ic_pal 和 ftm_signal_measurement 示例 您还可以参考一些社区帖子: s32k1:如何在同一FTM通道上测量PWM频率和占空比 S32K 输入捕获 S32K1 - 基于 FTM 的电机速度计算 希望这能帮到您。 此致, 朱利安   Re: S32K142 PWM Signal input reading 你好@nirmal_masilamani , 输入捕获支持 3 种模式: 仅限 上升沿 捕获 -> 句号 仅捕捉下落边缘 -> 句号 上升沿或下降沿捕获 -> 需要通过 GPIO 或 CnSC [CHIS] 位读取电平状态,以了解高电平脉冲宽度或低电平脉冲宽度。 注意:当通道 (n) 不在输入模式下时,应忽略 CHIS 位。 注意:当通道对处于双边沿模式时,通道 (n+1) CHIS 位是通道 (n+1) 输入值,而不是通道 (n) 输入值(此信号是双边沿模式使用的输入信号)。 对于PWM占空比捕获,应使用双边沿捕获。否则,你只会经历高水平或低水平的时期。在双边沿捕获模式下,仅使用通道(n)输入,而忽略通道(n+1)输入。 Julin_AragnM_0-1788457862022.pngJulin_AragnM_0-1788457862022.pngJulin_AragnM_0-1788457862022.png IC_GetMeasurement 函数会返回以时钟周期为单位的脉冲宽度,然后你可以用它来计算信号频率: /* Get the latest value */ inputCaptureMeas = IC_GetMeasurement(&ic_pal_1_instanceConfig, channel); /* Calculate the signal frequency using recorded data*/ inputCaptureMeas = frequency / (inputCaptureMeas); 此致, 朱利安 Re: S32K142 PWM Signal input reading 你好@Julián_AragónM , 感谢您的回复。 我还是有点困惑。 要测量PWM信号,需要多少个引脚? 我使用IC_PAL进行测量。但我无法使用信号引脚和单个通道测量 PWM。 RTD 使用的是 V4.0.0 版本
View full article
i.MX6Q HAB開発用の旧バージョンのコード署名ツール(CST)の提供依頼 NXP技術サポートチームへ、 現在、i.MX6Q SabreSDプラットフォームをベースにしたHigh Assurance Boot(HAB)セキュアブートソリューションを開発しており、公式のNXP BSPリリースL3.14.52_1.1.0を使用していますGAは当社の製品に対して完全に検証されています。 最新のCST v3.1.0公式ポータルからダウンロードしたものは、このレガシーBSPバージョンと完全に互換性がなく、i.MX6QのHABv4プロトコルに一致する有効な署名データを生成できません。これにより、その後のセキュアブート検証作業が妨げられます。 私はすでにNXPのコード署名ツールに関するソフトウェアライセンス契約を読み、受け入れており、このツールはNXP i.MX シリーズチップの社内製品開発にのみ使用されることを確認しています。 CST v2.3.2(HABv4用)のダウンロードリンクを教えていただけますか?このバージョンは、私たちが使用しているi.MX6Q BSPに対して公式に推奨されているマッチングツールです。 プロジェクトやチップの部品番号について追加情報が必要な場合は、どうぞお気軽にご連絡ください。 再開まで今しばらくお待ちください。 よろしくお願いいたします。 リクエフイ i.MX6Quad Re: Request for Old Version of Code Signing Tool (CST) for i.MX6Q HAB Development こんにちは、 お元気でいらっしゃいますか?古いバージョンは共有できますが、コミュニティでは共有できません。サポートチケットの作成を手伝って、私に連絡して追跡できるようにしてください。 https://support.nxp.com/s/?language=en_US よろしくお願いいたします。 アルド。 Re: Request for Old Version of Code Signing Tool (CST) for i.MX6Q HAB Development こんにちは、 私はi.MX6Q SabreSDと旧バージョンのL3.14.52_1.1.0を使用しています。BSP、ただしCST v3.1.0完全な互換性はありません。公式のダウンロードリンクやダウンロード方法に関する情報があれば大変ありがたいです。 Re: Request for Old Version of Code Signing Tool (CST) for i.MX6Q HAB Development NXPの現在のi.MX6QソフトウェアページにはCST 3.1.0が記載されていますダウンロード可能な「i.MX High Assurance Boot Reference Code Signing Tool」、リビジョン3.1.0として提供されます。fc4me
View full article
How to create a project without a board or device number listed in the VSC extension How do we create a new project in the VSCode MCUXpresso extension if the device/board is not listed in the library? The VSCode version is 1.135.0 and the MCUXpresso extension is 26.06.123. The MCUXpresso SDK dev is installed to version 26.06 and Arm GNU Toolchain is installed to 14.2.1.  We re-spin the code repo for LPC1768. It seems like if the part number is not in the list, we can't create the project...... (The create project button is greyed out in the attached snapshot.) Please advise. #VSCode #MCUXpress LPC1768FBD100  回复: How to create a project without a board or device number listed in the VSC extension Hi @Microsystemca  The New Project Wizard can only create projects for devices or boards that are included in an imported MCUXpresso SDK repository (or SDK Builder package). If the target device is not available in the SDK package, the wizard cannot find the required device or board definitions and therefore cannot create a new project directly. New Project Wizard — MCUXpresso for VS Code 26.08 documentation As a workaround, you can use MCUXpresso IDE to install the corresponding device support package and create a project for the target device there. Once the project has been successfully created and built in MCUXpresso IDE, you can then use the Import Project feature in MCUXpresso for VS Code to import the existing project and continue development within the VS Code environment. BR Harry 回复: How to create a project without a board or device number listed in the VSC extension Thank you for the workaround. We did that and it seems to be working. Quick note, MCUXpresso IDE is not fully compatible with the security standards adopted by some companies and it triggered a full scan of the computer after installation. The SHA/MCX hash is from unknown publisher. VSCode MCUXpresso is a direct installation because of the Microsoft certification. That's why users would prefer to have all the parts listed in the VSCode MCUXpresso repo.
View full article
请求提供 i.MX6Q HAB 开发用旧版代码签名工具 (CST) 尊敬的恩智浦技术支持团队: 我目前正在基于 i.MX6Q SabreSD 平台开发高度保证启动 (HAB) 安全启动解决方案,使用的是 NXP 官方 BSP (电路板支持包) 版本 L3.14.52_1.1.0。GA 已针对我们的产品进行了全面验证。 最新版 CST v3.1.0从官方门户网站下载的版本与此旧版 电路板支持包。 不完全兼容,无法生成与 i.MX6Q 的 HABv4 协议匹配的有效签名数据。这会阻碍我们后续的安全启动验证工作。 我已经阅读并接受了 NXP 代码签名工具的软件许可协议,并且我确认该工具将仅用于我们 NXP i.MX 系列芯片的内部产品开发。 请问能否提供CST v2.3.2 (适用于 HABv4)的下载链接?这是我们使用的 i.MX6Q 电路板支持包。的官方推荐匹配工具。 如果您需要有关我们项目或芯片零件编号的任何其他信息,请随时与我联系。 感谢您的支持。 顺祝商祺! 立学会 i.MX6 四核 Re: Request for Old Version of Code Signing Tool (CST) for i.MX6Q HAB Development 你好, 我正在使用 i.MX6Q SabreSD 和旧版 L3.14.52_1.1.0。电路板支持包,但 CST v3.1.0不完全兼容。任何官方下载链接或指导都将不胜感激。 Re: Request for Old Version of Code Signing Tool (CST) for i.MX6Q HAB Development 你好, 希望你一切都好。我可以分享一个旧版本,但我不能在这里的社区分享,请帮我创建一个支持工单,并在工单中向我咨询,以便我跟踪问题。 https://support.nxp.com/s/?language=en_US 此致敬礼/Saludos, 阿尔多。 Re: Request for Old Version of Code Signing Tool (CST) for i.MX6Q HAB Development NXP 当前的 i.MX6Q 软件页面列出了 CST 3.1.0 版本。可下载的“i.MX 高度保证启动参考代码签名工具”,版本 3.1.0。fmc4me
View full article
我想知道MC34PF3000A7E的CCO值。 工厂标签只显示它是在菲律宾组装的,但我不知道芯片的原始产地。 请问如何通过标签信息找到它?多谢
View full article
MC34PF3000A7EのCCOを知りたいです 工場出荷時のラベルにはPHで組み立てられたと記載されていますが、チップの国名は知りません。 ラベル情報から調べる方法を教えてもらえますか?どうもありがとう
View full article
S32K142 PWM信号入力読み取り こんにちは、チームの皆さん、 S32K142でFTM入力キャプチャを使用してPWMを読み取るためのサンプルコードはありますか? はいの場合、例を共有してください。 Re: S32K142 PWM Signal input reading こんにちは、 @Julián_AragónM さん、 迅速なご返信、本当にありがとうございます。 一つ小さな疑問ですが、単一のCHを使ってデューティサイクルと周期の両方を測定できますか? 入力キャプチャモードを「両エッジを検出」に設定した場合。IC_GetMeasurementからどのような測定値が得られますか? Re: S32K142 PWM Signal input reading こんにちは、 @nirmal_masilamani さん、 参照できるのは: 例4。AN5303より:S32K上のFlexTimerモジュールの特徴と動作モード – アプリケーションノート。 AN5413の例2.5 時限I/O(FTM):S32K1xxシリーズクックブック – アプリケーションノート Ftm_Icu_Ip_BlinkLed_S32K144 RTDパッケージの例(Ftm_Icu_Ip_EnableEdgeDetection API使用) SDK からの ic_pal & ftm_signal_measurement examlpes また、いくつかのコミュニティ投稿も参照できます: s32k1:同じFTMチャネルでのPWM周波数とデューティサイクルの測定方法 S32K入力キャプチャ S32K1-FTMに基づいてモーターの速度を計算する これがお役に立てば幸いです。 よろしくお願いします、 ジュリアン   Re: S32K142 PWM Signal input reading こんにちは、 @nirmal_masilamani さん、 入力キャプチャは3つのモードをサポートしています: 立ち上がりエッジのみキャプチャ -> 期間のみ 立ち下がりエッジのみキャプチャ -> ピリオドのみ 立ち上がりエッジまたは立ち下がりエッジでのキャプチャ -> 高レベルパルス幅または低レベルパルス幅を知るには、GPIO または CnSC [CHIS] ビットを介してレベル状態を読み取る必要があります。 注意: チャネル(n)が入力モードでない場合はCHISビットは無視すべきです。 注意: ペアチャネルがデュアルエッジモードの場合、チャネル(n+1)のCHISビットはチャネル(n+1)の入力値であり、チャネル(n)入力値ではありません(この信号はデュアルエッジモードで使用される入力信号です)。 PWMデューティサイクルのキャプチャには、デュアルエッジキャプチャを使用する必要があります。そうしないと、高水準の期間か低水準の期間しか得られません。デュアルエッジキャプチャモードでは、チャネル(n)入力のみを使用し、チャネル(n+1)入力は無視されます。 Julin_AragnM_0-1788457862022.pngJulin_AragnM_0-1788457862022.pngJulin_AragnM_0-1788457862022.png IC_GetMeasurementはティック単位のパルス幅を返し、それを使って信号周波数を計算できます: /* Get the latest value */ inputCaptureMeas = IC_GetMeasurement(&ic_pal_1_instanceConfig, channel); /* Calculate the signal frequency using recorded data*/ inputCaptureMeas = frequency / (inputCaptureMeas); よろしくお願いします、 ジュリアン Re: S32K142 PWM Signal input reading こんにちは、 @Julián_AragónM さん、 ご返信ありがとうございます。 まだ少し混乱しています。 PWM信号を測定するには、何本のピンが必要ですか? 測定にはIC_PALを使用しています。しかし、信号ピンとシングルチャンネルを使用してPWMを測定することはできません。 RTDはV4.0.0を使用しました
View full article
支持 iOS 26 的 Wi-Fi 感知型 NAN(适用于 IW612 和 FRDM-IMX93 的示例代码)以及 88W9098 支持 你好, 我正在开发一款使用 Wi-Fi Aware (NAN) 技术的 iPhone 消费级配件。 作为其数据链路。苹果在 iOS 26 中添加了公共 Wi-Fi 感知框架, 我已经有一个可用的 iPhone 到 iPhone 基准测试应用程序(发布/订阅, 配对设备,TCP 数据路径)。我现在选择NXP一方。 我的计划是在FRDM-IMX93板上评估IW612作为NAN对等器件的性能, 然后转向基于 i.MX 8M Plus 的设计,并采用 NVMe 存储。 我有四个问题: 1.在主题 2170706 中(“iMX 板上 WiFi Aware (NAN) 的示例代码”) IW612 三频模块”),NXP 分享了 Wi-Fi Aware 示例代码 通过安全文件实现iOS互操作性。我可以获得访问权限吗? 同一种材料?如果需要,我可以提交正式的支持案例。 渠道。 2. FRDM-IMX93 Debian/Yocto 电路板支持包 是否附带 IW612 固件? 是否默认启用NAN?我应该使用哪个电路板支持包 版本? 3. 对于相同设计的 2x2 变体,88W9098 固件是否支持 MXM驱动程序支持NAN/Wi-Fi吗? 4. NXP 是否已针对 iOS 26(Wi-Fi 感知)验证了 NAN 配对和数据路径 4.0 / PASN 配对)?任何已知的局限性都将非常有帮助。 目标平台:运行 iOS 26.5 和 Xcode 26 的 iPhone 17 Pro Max 和 iPhone 12 Pro Max。 也欢迎提供 IW612 NAN 数据路径的吞吐量数据。 谢谢你, 优素福 ( https://community.nxp.com/t5/i-MX-Processors/Sample-code-for-WiFi-Aware-NAN-on-iMX-boards-with-the-IW612-tri/td-p/2170706 ) Re: Wi-Fi Aware NAN with iOS 26 on IW612 and FRDM-IMX93 sample code and 88W9098 support 你好, 希望你一切都好。有关我们 Wi-Fi 设备的功能列表,我建议查看NXP 无线 SoC 功能和 Linux 版本说明。 对于受“安全文件”保护的文档:安全访问权限 | NXP 半导体 请您按照以下步骤操作? 另外,我建议您查看恩智浦半导体 (NXP Semiconductors) 的“安全访问权限常见问题解答”。 顺祝商祺! 里卡多
View full article
关于“智能能源”太阳能的观点 今天有几个来自 Smart Energy 的推销员上门推销太阳能电池板。我对太阳能很感兴趣,但没有足够的资金进行前期投资,他们提到有一个政府资助的计划,无需预付任何费用。 我自然非常怀疑。很想听听和他们打过交道的人的意见。
View full article