LCD and MIPI Camera Proven on i.MX6ULLHello,
Could you please recommend an LCD panel and a MIPI camera that have been successfully used with the i.MX6ULL?
I would like to connect them to the following evaluation board:
MCIMX6ULL-EVK
If possible, please provide the model numbers and any available software/BSP information.
Thank you.
Re: LCD and MIPI Camera Proven on i.MX6ULLHello,
On this board, validated Parallel-LCD Display are:
- SEIKO WVGA panel.
- Embest LCD8000-43T LCD panel.
Regarding MIPI CSI camera, please take a look into a OV5640 camera sensor.
Best regards.
Re: LCD and MIPI Camera Proven on i.MX6ULLThank you for your response.
I have given up on using the OV5640 camera sensor because I could not find a product that can be connected to the i.MX6ULL.
For the LCD, I plan to use the LCD8000-43T.