About the Finite-State Machine (FSM) of i.MX8Mplus We use Toradex's Veridin i.MX8Mplus at our company. At that time, the SOM_PW_ON signal is input to control the SoM's power supply. (Directly connected to the ON/OFF signal of the i.mx8MPlusSoC). *Please refer to the waveform on the attached oscilloscope. V1-1B_tool0_OFF.pngV1-1B_tool0_OFF.pngV1-1B_tool0_OFF.pngV1-1B_tool0_OFF.pngV1-1B_tool0_OFF.pngV1-1B_tool0_OFF.png Due to the circuit configuration on the SoM side, the voltage should be High (1.8V), but for about 800 msec after startup, it remains at an intermediate potential of approximately 0.3-0.4V. I'd like to know how this voltage (0.3 to 0.4V) is handled as an ON/OFF signal on the SoC side. This information was not included in the datasheet or reference manual. I think that in cases of very short ON/OFF operations (<5s), the system may proceed to shutdown. Would the operation detection criteria be the transition from High to Low edge state and the duration of the Low state? I would also like to know the exact minimum/maximum times for those times. i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: i.MX8MplusのFinite-State Machine (FSM)について For i.MX8M Plus, ONOFF is handled as a level-held button input with configurable 0/50/100/500 ms qualification and 5/10/15 s forced-off timing, and your observed 0.3–0.4 V on a 1.8 V ONOFF net is most consistently interpreted as logic Low by the available input-threshold documentation. Re: i.MX8MplusのFinite-State Machine (FSM)について Thank you for your reply. The observed V values of 0.3–0.41.8V on the ONOFF network are most consistently interpreted as logically low by the available input threshold documentation. By the way, could you also tell me about the voltage threshold that is interpreted as logically low? Furthermore, if interpreted as logically low, the ON/OFF state will remain logically low for approximately 800 msec after startup before changing to logically high. In that case, would it be considered that a button input occurred? My concern is whether a button press might cause the system to automatically shut down immediately after startup. Re: i.MX8MplusのFinite-State Machine (FSM)について By the way, could you also tell me about the voltage threshold that is interpreted as logically low? I apologize. I would like to know the voltage threshold at which the logic value is interpreted. Re: i.MX8MplusのFinite-State Machine (FSM)について Thank you for your reply. The observed V values of 0.3–0.41.8V on the ONOFF network are most consistently interpreted as logically low by the available input threshold documentation. By the way, could you also tell me about the voltage threshold that is interpreted as the logical high? Furthermore, if interpreted as logically low, the ON/OFF state will remain logically low for approximately 800 msec after startup before changing to logically high. In that case, would it be considered that a button input occurred? My concern is whether a button press might cause the system to automatically shut down immediately after startup. To the NXP TechSupport representative What do you think about this matter? I have one more question: ON/OFF is processed as a level hold button input, with conditions of 0/50/100/500 ms. Regarding that point, I believe the default is 0. In this case, if the level momentarily exceeds the logical high or logical low threshold due to noise or other factors, will the level be held? I am concerned that with this default setting, if noise is received, there is a possibility of malfunction if something that causes a logic judgment opposite to the currently held level logic is introduced, even for a moment. Re: i.MX8MplusのFinite-State Machine (FSM)について @Rita_Wang I have added a few more questions. We apologize for the inconvenience, but please provide your response. Re: i.MX8MplusのFinite-State Machine (FSM)について @Rita_Wang How is the confirmation process going? Please provide an answer. Re: i.MX8MplusのFinite-State Machine (FSM)について Sorry to miss your message, I can help checking it and will give you reply next week.
Wish you have a nice day Re: i.MX8MplusのFinite-State Machine (FSM)について @Rita_Wang Thank you for your assistance. This is Mori from Pal Giken. It's been almost a week now, how is the response going? Thank you for your cooperation. Re: i.MX8MplusのFinite-State Machine (FSM)について @Rita_Wang I apologize for the inconvenience, but could you please answer this question as well? Re: i.MX8MplusのFinite-State Machine (FSM)について @Rita_Wang Please provide an answer to the question I asked. Re: i.MX8MplusのFinite-State Machine (FSM)について @Rita_Wang Thank you for your reply. What I wanted to ask with this question is The question is whether a button input is recognized when the ONOFF pin is in a logically low state during startup. Our verification One observed behavior was that when the ONOFF pin started in a logically high state and then transitioned to a logically low state 10ms to 20ms later, the system would immediately shut down after startup. When the system is started in a logically low state, no cases have been observed where it immediately proceeds to shutdown after startup. Re: i.MX8MplusのFinite-State Machine (FSM)について @ShujiMouri
For i.MX8MP, the ONOFF pin belongs to the NVCC_SNVS power group and is listed as a GPIO-type input with reset state “Input with PU” . The applicable GPIO DC input-low specification is:
VIL(max)=0.3×VDDVIL(max)=0.3×VDD
with the table specifying low-level input voltage as min = -0.3 V, max = 0.3 × VDD .
Therefore, if ONOFF is powered from a 1.8 V SNVS I/O domain , the guaranteed logic-low threshold is:
0.3×1.8 V=0.54 V0.3×1.8 V=0.54 V
So an observed ONOFF voltage of approximately 0.3–0.4 V would be interpreted as logic low .
Regarding whether this would be considered a button input: yes, if the ONOFF pin remains low long enough after the device is in ON mode, it can be treated as a valid ONOFF button event.
An 800 ms low level can be recognized as a normal ONOFF button event , because it exceeds the configured normal button debounce duration.
It should not directly trigger the hardware emergency forced shutdown , because that requires about 5 seconds .
Whether the system shuts down immediately after startup depends on the software/PMIC handling of the normal ONOFF event. In ON mode, a brief connection to GND generates an interrupt intended to initiate a software-controllable power-down. If the boot software or OS power-key handler treats that interrupt as a power-off request, then an unintended shutdown after startup is possible.
Re: i.MX8MplusのFinite-State Machine (FSM)について @Rita_Wang The question is whether a button input is recognized when the ONOFF pin is in a logically low state during startup. What are your thoughts on this question? Re: i.MX8MplusのFinite-State Machine (FSM)について @Rita_Wang What are your thoughts on the answers to these questions? Please check.
View full article