Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
因软件许可到期而申请延期 Mail.png   尊敬的技术支持团队: 如附图所示,我收到一封电子邮件通知我,我的 S32DS 许可证即将到期。 我需要继续使用 S32DS 来进行我的工作。请问您能否延长我的软件使用许可,以便我能继续使用该软件? 感谢您的协助。 顺祝商祺! JINNAMGUNG_0-1784598976302.png Re: Request for Software License Extension Due to Expiration 你好, 我查看了您的账户,您的许可证有效期至2028年。 Re: Request for Software License Extension Due to Expiration 主题:如何将 S32 Design Studio 许可证转移/重新注册到我自己的 NXP 帐户 你好, 我的办公电脑是我从前任经理那里继承来的,S32 Design Studio 仍然是在他的 NXP 账户下激活的,而不是我的。因此,我电脑上安装的许可证似乎已经过期了。 我已经确认我的许可证有效期至 2028 年,因此我想将这台电脑上的 S32DS 切换到我的 NXP 帐户和许可证,而不是前任所有者的帐户和许可证。 请问正确的操作步骤是什么?具体来说: 1. 是否有办法停用或解除与先前帐户关联的现有激活状态? 2. 我能否使用我自己的帐户凭据重新激活 S32DS,还是需要完全卸载并重新安装? 感谢您的帮助。 顺祝商祺! Re: Request for Software License Extension Due to Expiration 你好, 您可以使用您的真实密钥在任何设备上进行任何新安装。S32DS 默认提供 101 个许可证。您可以在电脑上启动安装程序,并使用您之前的激活码进行激活。
View full article
Need help to find Neutron Converter sdk for i.MX95 kernel version (v6.6.52-2.2.0) Hello NXP Team, I am currently using LF_v6.6.52-2.2.2_images_IMX95 and I'm trying to identify the correct version of the Neutron Converter SDK to convert a TensorFlow Lite INT8 quantized model for the NPU. I have tried multiple versions of the Neutron Converter SDK, but every attempt results in the following error: INFO: NeutronDelegate delegate: 1 nodes delegated out of 27 nodes with 1 partitions. INFO: Created TensorFlow Lite XNNPACK delegate for CPU. Warning: microcode version mismatch! 0x359f358d (expected 0xa186aaf2) Warning: microcode version mismatch! 0x359f358d (expected 0xa186aaf2) Inference poll timeout Error: component='Neutron Driver', category='timeout', code=754 Traceback (most recent call last): File "/home/object_detc/main.py", line 80, in interpreter.invoke() File "/usr/lib/python3.12/site-packages/tflite_runtime/interpreter.py", line 941, in invoke self._interpreter.Invoke() RuntimeError: /usr/src/debug/tensorflow-lite-neutron-delegate/2.16.2/neutron_delegate.cc:355 neutronRC != ENONE (193099 != 0)Node number 27 (NeutronD. Could you clarify why support for LF_v6.6.52-2.2.2_images_IMX95 was removed? Is this because the BSP is still considered an alpha release? Could you also please advise on the following: Is it possible to use the Neutron Converter SDK with this kernel/BSP version? If so, which version of the Neutron Converter SDK is compatible with LF_v6.6.52-2.2.2_images_IMX95? If not, is there another version of the eIQ tools or a different workflow that should be used with this BSP? Thank you for your help. I look forward to your guidance. Suspected Software Defect Re: Need help to find Neutron Converter sdk for i.MX95 kernel version (v6.6.52-2.2.0) Hi @boopathi123, Thank you for contacting NXP Support! It appears that you are using a very early silicon revision. In that case, I recommend using the Neutron Converter included with the eIQ Toolkit. However, please note that this BSP version is not officially supported for the i.MX95. The i.MX95 was officially released with the B0 silicon revision and BSP 6.12.34. Earlier silicon revisions were intended for evaluation and pre production purposes, and therefore may not provide the same level of functionality, stability, compatibility, or performance as the currently supported devices. For this reason, I strongly recommend migrating to a supported combination of: i.MX95 B0 silicon BSP 6.12.34 or later Using a supported software and hardware configuration will ensure that you benefit from the latest fixes, optimizations, and NPU software support available for the i.MX95 platform. The behavior you are observing may be related to limitations or known issues present in the early silicon revisions rather than the model itself. Best regards, Chavira Re: Need help to find Neutron Converter sdk for i.MX95 kernel version (v6.6.52-2.2.0) thank you 🙂 ...
View full article
i.MX95 LPI2Cにおける動的I2Cスレーブアドレス構成 こんにちは、専門家の皆様。 私はiについて取り組んでいます。MX95 プラットフォームで、 Linux上でLPI2CコントローラをI2Cスレーブモードで 使用しています。 現在、I2Cスレーブアドレスはデバイスツリー内で静的に定義されています。私の要件は、デバイスツリーにアドレスをハードコーディングするのではなく、外部GPIO入力(例えば、ボードIDやアドレス選択GPIO)に基づいてスレーブアドレスを動的に決定することです。 知りたいのは以下の点です。 i.MX95 LPI2Cハードウェアは、実行時にI2Cスレーブアドレスを動的に変更することをサポートしていますか? NXP BSP/Linux LPI2Cのスレーブドライバーは、起動後にスレーブアドレスを更新できるのでしょうか?それともドライバーの変更が必要でしょうか? SoCまたはBSPの観点から、スレーブ登録前または登録中に外部GPIOに基づいてスレーブアドレスを選択するための推奨されるメカニズムはありますか? 動的なI2Cスレーブアドレス設定を示すリファレンス実装やサンプルはありますか? 何かご助言や推奨される方法があれば、ぜひお聞かせください。 BR、 アルン・クマール Re: Dynamic I2C Slave Address Configuration on i.MX95 LPI2C こんにちは、 1. はい、i.MX95のLPI2Cモジュールで可能です。 2. いいえ、ドライバの改造は不要です。 現在のNXP BSP Linuxドライバはマスターモードとスレーブモードの両方をサポートしていますが、スレーブアドレスはデバイスツリーから一度だけ読み込みます。 3. このモモディットドライバーがプローブ中にGPIOアドレスを読み取り、ラインを変更する最良の方法。 https://github.com/nxp-imx/linux-imx/blob/b096ce610e956cc2596006343df8a2a26ed6e019/drivers/i2c/busses/i2c-imx-lpi2c.c 4. i2c-imx-lpi2c.c を使用するスレーブ DTS のサンプルがあります。ただし、GPIOを使って実行時にアドレスを変更することはできません。次のリンクからご覧いただけます: https://github.com/nxp-imx/linux-imx/blob/74521e3f425001c27a54323ee8de4f7c59ee88dc/arch/arm64/boot/dts/freescale/imx95-15x15-evk-i2c-spi-slave.dts よろしくお願いいたします。
View full article
在 MCUXpresso 安全配置工具 26.06 版中使用 IMX95 我从 github 下载了 imx-oei-master,并使用 make 生成了 oei-m33-ddr.bin 和 oei-m33-tcm.bin。我尝试将图像构建为图片附件。 我有一些问题: 1. 我的设置是否正确? 2. 在“类型”中,我看到了很多项目。我不知道该选哪个? 3. 在“加载地址”和“入口点”中,我的设置是否正确?我只在 oei-m33-ddr.map 中看到了 CM33_TCMU_OFFSET = 0x1ffc0000。我甚至都没听说过lpddr5。 4. 在“图像类型”中,我还看到了很多项目。我不知道该选哪个?顺便问一下,“类型”和“图像类型”有什么区别? 5. 在“容器集”中,我应该选择主图像还是辅助图像? Re: Using IMX95 in MCUXpresso Secure Provisioning Tool Version 26.06 请参考此处的指南来构建 i.MX95 启动映像: https://docs.mcuxpresso.nxp.com/secure/26.06/06_processor_specific_workflow.html#i-mx-95-bootable-image-examples 它详细描述并展示了所需的图像。 另请注意,在添加映像“OEI DDR no QB”时,可以为 i.MX95 B0 设备选择 DDR 快速启动二进制文件,如下所示:   image-2026-07-24-17-41-23-792.png   image-2026-07-24-17-40-38-998.png   Re: Using IMX95 in MCUXpresso Secure Provisioning Tool Version 26.06 感谢您的快速回复。
View full article
Using IMX95 in MCUXpresso Secure Provisioning Tool Version 26.06 I have download imx-oei-master on github and use make to generate oei-m33-ddr.bin and oei-m33-tcm.bin. And I try to build image as picture attach. I have some questions: 1. Is my setting correct? 2. In "Type", I saw many of items. I don't know which one I need to select? 3. In "Load address" and "Entry point", Is my setting is correct or not? I only saw CM33_TCMU_OFFSET = 0x1ffc0000 in oei-m33-ddr.map. I even didn't see about lpddr5 4. In "Image Type", I also saw many of items. I don't know which one I need to select? By the way what is the difference between "Type" and "Image Type" 5. In "Container set", which one I should select Primary or Secondary image? Re: Using IMX95 in MCUXpresso Secure Provisioning Tool Version 26.06 Please refer to the guidance here for building i.MX95 boot images: https://docs.mcuxpresso.nxp.com/secure/26.06/06_processor_specific_workflow.html#i-mx-95-bootable-image-examples It has detailed description and snapshot about what images are needed. Also note that the ddr quick boot binaries can be selected for i.MX95 B0 devices while adding image "OEI DDR no QB" as below:   image-2026-07-24-17-41-23-792.png   image-2026-07-24-17-40-38-998.png   Re: Using IMX95 in MCUXpresso Secure Provisioning Tool Version 26.06 Thanks for your quickly reply.
View full article
ソフトウェアライセンス延長の期限切れ申請 Mail.png   サポートチームの皆様、 添付画像に示すように、S32DSのライセンスの有効期限が近づいていることを通知するメールを受け取りました。 現在進行中の作業では、引き続きS32DSを使用する必要があります。ソフトウェアを使い続けられるようにライセンスを延長してもらえますか? ご協力ありがとうございます。 よろしくお願いいたします。 JINNAMGUNG_0-1784598976302.png Re: Request for Software License Extension Due to Expiration こんにちは、 あなたのアカウントを確認したところ、ライセンスは2028年まで有効です。 Re: Request for Software License Extension Due to Expiration 件名:S32 Design Studioライセンスを自分のNXPアカウントに移管/再登録する方法 こんにちは、 私は元マネージャーから仕事用PCを引き継ぎましたが、S32 Design Studioは私のではなく彼のNXPアカウントでまだ有効化されています。そのため、私のマシンにインストールされているライセンスの有効期限が切れてしまったようです。 自分のライセンスが2028年まで有効であることを確認したので、このPCのS32DSを前の所有者ではなくNXPのアカウントとライセンスに切り替えたいと考えています。 正しい手順を教えてもらえますか?具体的には: 1. 前のアカウントに紐づいた既存のアクティベーションを無効化または解除する方法はありますか? 2. 自分のアカウント認証情報でS32DSを再アクティベートできますか?それとも完全なアンインストールとクリーンインストールが必要ですか? ご協力ありがとうございます。 よろしくお願いいたします。 Re: Request for Software License Extension Due to Expiration こんにちは、 どのデバイスでも新しいインストールには実際のキーを使うことができます。S32DSの場合、デフォルトでは101個のライセンスが利用可能です。PCでインストーラーを起動し、古いコードを使ってアクティベートできます。
View full article
Dynamic I2C Slave Address Configuration on i.MX95 LPI2C Hello Experts, I am working on the i.MX95 platform and using the LPI2C controller in I2C slave mode under Linux. Currently, the I2C slave address is defined statically in the Device Tree. My requirement is to determine the slave address dynamically based on an external GPIO input (for example, a board ID or address-select GPIO) instead of hardcoding it in the Device Tree. I would like to know: Does the i.MX95 LPI2C hardware support changing the I2C slave address dynamically at runtime? Does the NXP BSP/Linux LPI2C slave driver support updating the slave address after boot, or would it require driver modifications? Is there any recommended mechanism from the SoC or BSP perspective to select the slave address based on an external GPIO before or during slave registration? Are there any reference implementations or examples demonstrating dynamic I2C slave address configuration? Any guidance or recommended approach would be appreciated. BR, Arun Kumar Re: Dynamic I2C Slave Address Configuration on i.MX95 LPI2C Hello, 1. Yes, is possible with LPI2C module of i.MX95. 2. No, driver modifications are needed. The current NXP BSP Linux driver supports both master and slave modes but, the slave address is read once from the Device Tree. 3. The best approach for this modify driver to read the GPIO address and change line during probe. https://github.com/nxp-imx/linux-imx/blob/b096ce610e956cc2596006343df8a2a26ed6e019/drivers/i2c/busses/i2c-imx-lpi2c.c 4. We have an slave DTS example that uses i2c-imx-lpi2c.c driver but the address cannot be changed in runtime using GPIOs. You can take a look in the next link: https://github.com/nxp-imx/linux-imx/blob/74521e3f425001c27a54323ee8de4f7c59ee88dc/arch/arm64/boot/dts/freescale/imx95-15x15-evk-i2c-spi-slave.dts Best regards.
View full article
S32DSライセンスの有効期限が切れます こんにちは、 S32DS を開くと次のメッセージが表示されます。   Arm用Design Studio アクティベーションID: 8AEC-51FD-AB5B-6A4D 評価日数: 9 機能バージョン: 2.2 機能のステータス: 評価 (9 日間) ライセンスを延長するには何をする必要がありますか? よろしくお願いいたします。 サンドラ Re: S32DS license expiring こんにちは、 ライセンスを延長するよう管理者に通知しました。 よろしくお願いいたします。 ピーター Re: S32DS license expiring こんにちは、 ライセンスは 2030 年まで延長されました。 よろしくお願いいたします。 ピーター Re: S32DS license expiring こんにちは、 画像の問題でS32DSをアクティベートできませんでした。この問題を解決する方法を教えていただけますか? HelenLi_0-1778831877838.png Re: S32DS license expiring 助けて! 私のS32DS IDEライセンスがもうすぐ期限切れです。使用期間を延長するのを手伝ってもらえますか?ありがとう ! ライセンス番号:1A99 90A8 2F06 339B
View full article
Request for Software License Extension Due to Expiration Mail.png   Dear Support Team, As shown in the attached image, I received an email notifying me that my S32DS license is about to expire. I need to continue using S32DS for my ongoing work. Could you please extend my license so that I can keep using the software? Thank you in advance for your assistance. Best regards, JINNAMGUNG_0-1784598976302.png Re: Request for Software License Extension Due to Expiration Hi,  I checked your account and your license is valid till 2028.  Re: Request for Software License Extension Due to Expiration Subject: How to transfer/re-register an S32 Design Studio license to my own NXP account Hello, I inherited my work PC from my former manager, and S32 Design Studio is still activated under his NXP account, not mine. Because of this, the installed license appears to have expired on my machine. I have confirmed that my own license is valid until 2028, so I would like to switch S32DS on this PC over to my NXP account and license instead of the previous owner's. Could you let me know the correct procedure for this? Specifically: 1. Is there a way to deactivate or release the existing activation tied to the previous account? 2. Can I simply re-activate S32DS with my own account credentials, or is a full uninstall and clean reinstall required? Thank you for your help. Best regards, Re: Request for Software License Extension Due to Expiration Hi,  You can use your actual key for any new installation on any device. For S32DS is by default 101 licenses available. You can start installer on your PC and use your old code for activation. 
View full article
リクエスト: RAppID Init v2.1.0(またはそれ以降)MPC5644Aデバイスサポート — ダウンロードリンクが必要 こんにちは、 私はMPC5644Aを基にしたプロジェクトに取り組んでおり、このデバイスをサポートするRAppID Initツールを入手する必要があります。 私は元々私たちのプラットフォーム用に作成されたRAppID Initプロジェクトファイル(.rsp)を持っています。ファイルヘッダーには以下のように表示されます。 ツールバージョン:2.1.0(ツールバージョンメジャー 2、ツールバージョンマイナー 1、サブバージョン番号 0) 対象デバイス: MPC5644A 作成日:2013年4月 つまり、MPC5644Aサポートは明らかにRAppID Init v2.1.0に存在していました。しかし、現在のNXPのウェブサイトでは一致するダウンロードが見つかりません: 「RAppID Initialization for Power Architecture」ページ(RAPPID)には11件の公開ダウンロードが掲載されていますが、MPC564xA ファミリをカバーしているものはなく(MPC564xL、MPC560xB/xS、MPC563xM、MPC567xR/xK/xF、MPC5748G、MPC577xK/Mのみ)、 アーカイブのセクションでは「Archive: Pin Wizard for MPC564xA」は見つかりましたが、「Init for MPC564xA」パッケージは見つかりませんでした。ピンウィザードはシステムやペリフェラルの初期化をカバーしておらず、私の.rspも開けられませんプロジェクトファイル。 モデレーターの方、RAppID Init v2.1.0のダウンロードリンクを教えていただけますか?あるいはMPC5644Aデバイスサポート付きで、既存の.rspを開いて変更できるようになった後soでもありますプロジェクト? ご協力ありがとうございます。 Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed こんにちは、 はい、おっしゃる通りです。RAPPID-564XASWは既に存在します。 しかし、NXPはそれを公式ウェブページでは提供していない。 入手するための手続きについて、社内で確認してみます。 よろしくお願いいたします。 ピーター Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed Please check the link at RAppID Initialization for Power Architecture | NXP Semiconductors    RAppID Boot Loader Utility   Init for MPC564xL https://www.nxp.com/design/design-center/software/embedded-software/rappid-initialization-for-power-architecture:RAPPID ところで、MPC5644Aはどんなアプリケーションでうまくいっていますか? Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed そのページは既に見ていますが、私のものはMPC5644Aなので少し違います。 また、私のMPC5644Aは車両制御に使われているようです。 Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed いつ返事が来るのでしょうか? Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed https://www.nxp.com/webapp/Download?colCode=ETPUGCT&appType=license&location=null eTPUのグラフィカル設定ツールはいかがでしょうか?それもかなり役に立ちそうだ。製品自体がかなり古いため、サービス遅延が予想されるかもしれません
View full article
需要帮助查找适用于 i.MX95 内核版本 (v6.6.52-2.2.0) 的 Neutron 变流器 SDK。 您好,NXP团队, 我目前正在使用 LF_v6.6.52-2.2.2_images_IMX95 ,并且我正在尝试确定 Neutron Converter SDK 的正确版本,以便将 TensorFlow Lite INT8 量化 模型 转换 为 NPU 格式。 我尝试过多个版本的 Neutron 变流器 SDK,但每次尝试都出现以下错误: 信息:NeutronDelegate 委托:27 个节点中有 1 个节点被委托,共 1 个分区。 信息:已为 CPU 创建 TensorFlow Lite XNNPACK 委托。 警告:微代码版本不匹配!0x359f358d(预期为 0xa186aaf2) 警告:微代码版本不匹配!0x359f358d(预期为 0xa186aaf2) 推理轮询超时 错误:元器件='Neutron Driver',类别='超时',代码=754 回溯(最近一次调用): 文件“/home/object_detc/main.py”,第 80 行,在 中 解释器.调用() 文件“/usr/lib/python3.12/site-packages/tflite_runtime/interpreter.py”,第 941 行,在 invoke 中 self._interpreter.Invoke() RuntimeError: /usr/src/debug/tensorflow-lite-neutron-delegate/2.16.2/neutron_delegate.cc:355 neutronRC != ENONE (193099 != 0)节点编号 27 (NeutronD. 能否解释一下为什么移除了对LF_v6.6.52-2.2.2_images_IMX95的支持?是因为该电路板支持包仍被视为 alpha 版本吗? 请问您能否也就以下问题提供一些建议: 是否可以将 Neutron 变流器 SDK 与此内核/电路板支持包 版本一起使用? 如果是这样,那么哪个版本的 Neutron 变流器 SDK 与 LF_v6.6.52-2.2.2_images_IMX95 兼容 ? 如果没有,是否有其他版本的 eIQ 工具或不同的工作流程可以与此 BSP 一起使用? 感谢您的帮助。期待您的指导。 疑似软件缺陷 Re: Need help to find Neutron Converter sdk for i.MX95 kernel version (v6.6.52-2.2.0) 你好@boopathi123 , 感谢您联系恩智浦技术支持! 看来您使用的是非常早期的芯片版本。在这种情况下,我建议使用 eIQ 工具包中包含的 Neutron 变流器。但是请注意,此 BSP 版本并未得到 i.MX95 的官方支持。 i.MX95 正式发布,采用 B0 硅版本和 BSP 6.12.34。早期的硅片版本旨在用于评估和预生产目的,因此可能无法提供与当前支持的设备相同的功能、稳定性、兼容性或性能。 因此,我强烈建议迁移到以下受支持的组合: i.MX95 B0 硅 BSP 6.12.34 或更高版本 使用受支持的软件和硬件配置将确保您能够享受到 i.MX95 平台的最新修复、优化和 NPU 软件支持。 你观察到的现象可能与早期硅片版本中的局限性或已知问题有关,而不是与模型本身有关。 此致, 查维拉 Re: Need help to find Neutron Converter sdk for i.MX95 kernel version (v6.6.52-2.2.0) 谢谢 🙂 ...
View full article
When GUIGuider-2.0.0 generates C code, the folder under the generated folder is completely empty. When using GUIGuider-2.0.0 on Windows 11 to generate C code, the folders under the "generated" folder are all empty, even though the logs show successful generation. This happens on the same computer as GUI-Guider-1.10.1-GA, which generates the code perfectly. I've tried various methods, including disabling antivirus software and running it as administrator, but the problem persists. Has anyone encountered the same issue? I would appreciate any help. 21:10:08 INFO [gg_event] gg_event_layer_sys.c Generated 21:10:08 INFO [gg_event] gg_event_layer_top.c Generated 21:10:08 INFO [gg_event] gg_event_layer_bottom.c Generated 21:10:08 INFO update-sdk Started 21:10:08 INFO Target Executor initialized 21:10:08 SUCCESS SDK template updated successfully 21:10:08 SUCCESS Operation completed in 0.00s 21:10:08 INFO [gg_event] gg_event_screen.c Generated 21:10:08 INFO [gg_event] gg_event.h Generated 21:10:08 INFO [gg_event] Generation completed 21:10:08 SUCCESS === Code generation completed successfully === Re: GUIGuider-2.0.0生成C代码时generated文件下面的文件夹全是空的 I reinstalled the system but it still didn't work; GUI Guider 1.10 works fine. I added a button to a blank project. Re: GUIGuider-2.0.0生成C代码时generated文件下面的文件夹全是空的 Hello @IFYINT , Sorry to keep you waiting. Could you please share the project where the problem occurred? We'll try to reproduce it. BR Celeste Re: GUIGuider-2.0.0生成C代码时generated文件下面的文件夹全是空的 I tried it on my Windows 11 PC, but I couldn't reproduce your problem: Celeste_Liu_0-1784687143167.png Would it be convenient for you to try a different computer? Re: GUIGuider-2.0.0生成C代码时generated文件下面的文件夹全是空的 It works on a different computer and can generate files normally, but it's not working on this computer. It worked fine on version 1.10 before. 屏幕截图 2026-07-24 202549.png Re: GUIGuider-2.0.0生成C代码时generated文件下面的文件夹全是空的 I tried again, but I still couldn't reproduce your situation. Could you check your project path? Did you generate a "generated" folder? If not, could you create it manually and then regenerate the code? Celeste_Liu_0-1785142973015.png We still suggest you export the project and send it to us for review.
View full article
GUIGuider-2.0.0生成C代码时generated文件下面的文件夹全是空的 GUIGuider-2.0.0,Windows11,生成C代码时generated文件下面的文件夹全是空的,日志显示已经生成成功,实际文件夹全是空的,同意电脑,GUI-Guider-1.10.1-GA可以完美生成。关了杀毒软件,用管理员启动,等等试了各种方法,都一样,有没有遇到相同问题的,请教一下。 21:10:08INFO[gg_event] gg_event_layer_sys.c Generated 21:10:08INFO[gg_event] gg_event_layer_top.c Generated 21:10:08INFO[gg_event] gg_event_layer_bottom.c Generated 21:10:08INFOupdate-sdk Started 21:10:08INFOTarget Executor initialized 21:10:08SUCCESSSDK template updated successfully 21:10:08SUCCESSOperation completed in 0.00s 21:10:08INFO[gg_event] gg_event_screen.c Generated 21:10:08INFO[gg_event] gg_event.h Generated 21:10:08INFO[gg_event] Generation completed 21:10:08SUCCESS=== Code generation completed successfully === Re: GUIGuider-2.0.0生成C代码时generated文件下面的文件夹全是空的 我重装系统都不行,GUI Guider1.10能够正常使用。一个空白工程加了一个按钮。 Re: GUIGuider-2.0.0生成C代码时generated文件下面的文件夹全是空的 Hello @IFYINT , 抱歉让您久等了。您方便共享一下出问题的工程吗,我们这边尝试复现一下。 BR Celeste Re: GUIGuider-2.0.0生成C代码时generated文件下面的文件夹全是空的 我这边试了一下(windows 11 PC),没能复现您的问题: Celeste_Liu_0-1784687143167.png 您那边方便换一台电脑再试一下吗? Re: GUIGuider-2.0.0生成C代码时generated文件下面的文件夹全是空的 换电脑是可以的,能够正常生成文件,就是这台电脑不行,之前运行1.10版本是可以的。 屏幕截图 2026-07-24 202549.png Re: GUIGuider-2.0.0生成C代码时generated文件下面的文件夹全是空的 我这边又试了一下,还是没能复现你的情况,你能检查一下你项目工程的路径吗?有没有生成generated文件夹,如果没有文件夹,你手动创建后重新generate code试试呢? Celeste_Liu_0-1785142973015.png 同时还是建议你导出工程发我们看看。
View full article
Conv2D on i.MX 8M Plus VX delegate produces incorrect output when either spatial kernel dim >= 16 Summary On i.MX 8M Plus EVK, Conv2D ops where either spatial kernel dimension (H or W) is >= 16 produce incorrect output under the VX delegate (libvx_delegate.so). The model loads, the Conv2D is bound to an OPENVX kernel by vsi_nn_kernel_selector, error_during_init/prepare/invoke are all 0, and inference latency is normal, but the int8 output is saturated to a single value (int8 = 127) at every position across diverse inputs. The boundary is sharp between K=15 and K=16 along either spatial axis. This matches the threshold of the documented stride > 15 limit (https://community.nxp.com/t5/i-MX-Processors/Conv2D-not-working-with-stride-16-for-NPU-Kernel-crashes/td-p/1754217). Two questions: Is this kernel-dim ≥ 16 cliff a known limitation, and if so could it be added to the i.MX Machine Learning User's Guide (UG10166) Conv2D constraints section? Should vsi_nn_op_conv2d::op_check (or the VX delegate's partition logic) reject this case at graph-compile time so the op falls back to CPU? The current "accept, run, return constant int8=127, no diagnostic" behaviour is unsafe — a deployed model with a large kernel appears to load and run normally. Environment Component Value Board i.MX 8M Plus EVK BSP NXP i.MX Release Distro 6.18-whinlatter (VERSION_ID=6.18-whinlatter) Kernel Linux 6.18.2-1.0.0-gf49f45233f7b SMP PREEMPT (aarch64) libvx_delegate.so md5 2f88ec0871d18298bfa357ddaaea4d6d libGAL.so md5 af4806f617b23363b3be69c4dad2dc05 libOpenVX.so{,.1,.1.3.0} md5 92f85c32746d4d0b38800e21503d13d0 (all three identical) imx-gpu-viv package 1:6.4.11.p4.4-aarch64-r0 tim-vx package 1.2.2-r0 OVxlib (runtime-reported) OVXLIB_VERSION==1.2.14 TFLite runtime TFLite 2.19.0 (/usr/bin/tensorflow-lite-2.19.0/examples/benchmark_model) Reproducer The attached conv_1x17_broken.tflite (2,136 bytes) is a single-Conv2D artifact: kernel (1, 17), input 1×1×1000×5 int8, output 1×1×1000×8 int8, per-channel int8 weight quantization, padding=SAME, stride=(1,1), no fused activation. # On the i.MX 8M Plus board: python3 reproduce.py conv_1x17_broken.tflite # exits 1: BROKEN, saturated to int8=127 python3 reproduce.py conv_1x15_torch_control.tflite # exits 0: OK (K<16, same pipeline) reproduce.py (attached, depends only on tflite_runtime and numpy) feeds 6 seeded random int8 inputs through plain and VX-delegated interpreters and reports mean|Δ|, max|Δ|, and the count of unique int8 output values from the VX path. Kernel-size sweep Single-Conv2D unit-test models, INT8 PTQ. mean|Δ| board VX vs board CPU on the same int8 input bytes; uniq_VX = unique int8 output values across 6 inputs (out of 256). kernel (H, W) mean |Δ| uniq_VX result (1, 11) 0.03 256 OK (1, 15) 0.02 256 OK (1, 16) 134.9 1 BROKEN (constant int8=127) (1, 17) 136.9 1 BROKEN (constant int8=127) (1, 23) 130.5 1 BROKEN (constant int8=127) (15, 1) 0.11 256 OK (17, 1) 136.9 1 BROKEN (constant int8=127) (23, 1) 129.3 1 BROKEN (constant int8=127) (3, 3), (5, 5), (7, 7) < 0.2 256 OK (15, 15) (area 225) 0.41 256 OK (3, 23) 123.4 1 BROKEN (constant int8=127) (5, 15) 0.24 256 OK The threshold applies independently to H and W. In every broken case the VX output saturates to int8 = 127 at every position — saturation to the positive int8 extreme (rather than to output_zp or 0) suggests either multiplier-shift overflow before the final clamp, or a fixed value being written into the output tile in place of the MAC result. The issue doesn't seem related to kernel area (e.g., 15x15 works fine) The threshold is necessary but not sufficient — some int8 weight value patterns at K ≥ 16 trigger the bug, others don't. We've done byte-level isolation experiments (grafting individual TFLite tensor fields between broken and non-broken artifacts) narrowing the value-pattern trigger to specific tensor fields. Happy to share the isolation results and tooling if useful. Verbose log excerpt (VSI_NN_LOG_LEVEL=5, broken case) INFO: Vx delegate: error_during_init set to 0. INFO: Vx delegate: error_during_prepare set to 0. INFO: Vx delegate: error_during_invoke set to 0. I [vsi_nn_CreateGraph:1327] OVXLIB_VERSION==1.2.14 D [setup_node:535] Setup node id[3] uid[30000] op[DATACONVERT] D [setup_node:535] Setup node id[0] uid[1] op[PERMUTE] D [setup_node:535] Setup node id[1] uid[2] op[CONV2D] D [setup_node:535] Setup node id[2] uid[3] op[PERMUTE] D [setup_node:535] Setup node id[4] uid[30001] op[DATACONVERT] D [vsi_nn_kernel_selector:1286] Instance OPENVX node with kernel "conv2d" Full log attached as vsi_nn_log_level_5_conv_1x17.txt. Attachments Bundled as bug_report_artifacts.tar.gz conv_1x17_broken.tflite — 2,136-byte broken artifact. conv_1x15_torch_control.tflite — 2,056-byte sub-threshold control, same pipeline. reproduce.py — board-side reproducer (tflite_runtime + numpy only). vsi_nn_log_level_5_conv_1x17.txt — full verbose log. Additional artifacts available on request: byte-level isolation tooling, a structurally-identical working (1, 17) artifact for delta analysis, full sufficient-condition graft results. i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Linux Suspected Software Defect Re: Conv2D on i.MX 8M Plus VX delegate produces incorrect output when either spatial kernel dim > Hi @themis_stewart  Thanks for your information, i am checking with internal team about your two questions. Best Regards, Zhiming Re: Conv2D on i.MX 8M Plus VX delegate produces incorrect output when either spatial kernel dim > Hello @themis_stewart  Please try the following patch based on L6.18.2 to fallback the op to the CPU if the kernel size is > 16 Best Regards, Zhiming Re: Conv2D on i.MX 8M Plus VX delegate produces incorrect output when either spatial kernel dim > Thanks very much for the quick turnaround on this — we've applied and tested the guard patch and can confirm it resolves the issue on our side. We built the patched libvx_delegate.so from the lf-6.18.2_1.0.0 delegate source with your op_map.cc change and validated it on our i.MX 8M Plus EVK against the minimal reproducers from the original report. With the patch: The affected INT8 Conv2D (spatial kernel ≥ 16) is now cleanly rejected by the delegate and falls back to TFLite CPU, with the log message making the fallback explicit — no more silent saturation to int8 = 127. Output matches the CPU reference exactly. Our production models (kernels ≤ 15) are unaffected — still fully delegated to the NPU, so the guard doesn't over-trigger. The CPU-fallback path is performing well for us in practice, though the fallback is naturally slower than a model able to run fully on the NPU. We're happy to share detailed before/after benchmarks privately if they'd be useful for your regression coverage. Thanks again — much appreciated.
View full article
Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed Hello, I am working on a project based on the MPC5644A, and I need to obtain the RAppID Init tool that supports this device. I have an existing RAppID Init project file (.rsp) that was originally created for our platform. The file header shows the following: Tool version: 2.1.0 (toolVersionMajor 2, toolVersionMinor 1, subVersionNumber 0) Target device: MPC5644A Created: April 2013 So MPC5644A support clearly existed in RAppID Init v2.1.0. However, I cannot find a matching download on the current NXP website: The "RAppID Initialization for Power Architecture" page (RAPPID) lists 11 public downloads, but none of them cover the MPC564xA family (only MPC564xL, MPC560xB/xS, MPC563xM, MPC567xR/xK/xF, MPC5748G, MPC577xK/M). In the archive section I did find "Archive: Pin Wizard for MPC564xA", but no corresponding "Init for MPC564xA" package. The Pin Wizard does not cover system/peripheral initialization, and it cannot open my .rsp project file. Could a moderator please provide a download link for RAppID Init v2.1.0 or later with MPC5644A device support, so that I can open and modify my existing .rsp project? Thank you in advance for your help. Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed Hello, Yes, you are correct, there is existing RAPPID-564XASW. But NXP is not offering it on public web page. I will ask internally what is the procedure to obtain it. Best regards, Peter Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed Please check the link at RAppID Initialization for Power Architecture | NXP Semiconductors    RAppID Boot Loader Utility   Init for MPC564xL https://www.nxp.com/design/design-center/software/embedded-software/rappid-initialization-for-power-architecture:RAPPID btw, what kind of application does MPC5644A is working for you?  Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed I've already seen that page, but mine is different because it's an MPC5644A. Also, my MPC5644A appears to be used for vehicle control. Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed When can I expect a response? Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed https://www.nxp.com/webapp/Download?colCode=ETPUGCT&appType=license&location=null How about eTPU Graphical Configuration Tool? It seems pretty useful as well. Since the product is pretty old device, some service delay could be expected
View full article
T Embed 使用的是哪种接口? 我有一台标准的 T 型嵌入式开发板,但我不知道它用的是哪种接口(不是 USB-C 接口),因为官方网站说它是 Grove 接口,而 Lilygo Wiki 网站说它是 Qwiic 接口。请问有人可以帮帮我吗? Re: What kind of port does the T Embed have? 你好, 由于该设备并非 NXP 产品,我建议您直接联系 Lilygo 支持部门,提供元器件零件编号,您可以与他们一起查看引脚图或物料清单。 顺祝商祺!
View full article
What kind of port does the T Embed have? I have the standard model T Embed, but i have no Idea what kind of port it has (the other port, not usb c), because the official site says its a grove port, the lilygo Wiki site says its a qwiic port. Can anyone help me please? Re: What kind of port does the T Embed have? Hello, Since the device is not an NXP product, I would recommend you contact directly the Lilygo support to share the component part number, you could check the pin diagram or BOM with the page and them. Best Regards
View full article
i.MX 8M Plus VXデリゲート上のConv2Dは、空間カーネル次元が16以上の場合に誤った出力を生成します。 概要 i.MX 8M Plus EVK では、空間カーネル次元 (H または W) のいずれかが 16 以上である Conv2D 演算で、VX デリゲート (libvx_delegate.so) の下で誤った出力が生成されます。モデルはロードされ、Conv2D は vsi_nn_kernel_selector によって OPENVX カーネルにバインドされ、error_during_init/prepare/invoke はすべて 0 であり、推論レイテンシは正常ですが、int8 出力はさまざまな入力に対してすべての位置で単一の値 (int8 = 127) に飽和します。 空間軸のどちらにおいても、K=15とK=16の境界は明確である。これは、文書化されたストライド > 15 の制限のしきい値と一致します ( https://community.nxp.com/t5/i-MX-Processors/Conv2D-not-working-with-stride-16-for-NPU-Kernel-crashes/td-p/1754217 )。 2つの質問があります。 このカーネル次元が16以上という制限は既知のものですか?もしそうであれば、i.MX機械学習ユーザーガイド(UG10166)のConv2D制約のセクションに追加していただけますか? vsi_nn_op_conv2d::op_check(またはVXデリゲートのパーティションロジック)は、グラフコンパイル時にこのケースを拒否し、演算をCPUにフォールバックさせるべきでしょうか?現在の「受け入れ、実行、定数 int8=127 を返す、診断なし」という動作は安全ではありません。カーネルが大きいデプロイ済みモデルは、正常にロードされ実行されるように見えます。 環境 コンポーネント値 ボード i.MX 8M Plus EVK BSP NXP i.MX リリースディストリビューション 6.18-whinlatter (VERSION_ID=6.18-whinlatter) カーネル Linux 6.18.2-1.0.0-gf49f45233f7bSMPプリエンプト(aarch64) libvx_delegate.so のMD5 2f88ec0871d18298bfa357ddaaea4d6d libGAL.so md5 af4806f617b23363b3be69c4dad2dc05 libOpenVX.so{,.1,.1.3.0}MD5 92f85c32746d4d0b38800e21503d13d0(3つとも同一) imx-gpu-viv パッケージ 1:6.4.11.p4.4-aarch64-r0 tim-vxパッケージ 1.2.2-r0 OVxlib(ランタイム報告) OVXLIB_VERSION==1.2.14 TFLiteランタイム TFLite 2.19.0 (/usr/bin/tensorflow-lite-2.19.0/examples/benchmark_model) 再生装置 添付の conv_1x17_broken.tflite (2,136 バイト) は、単一の Conv2D アーティファクトです。カーネル (1, 17)、入力 1×1×1000×5 int8、出力 1×1×1000×8 int8、チャネルごとの int8 重み量子化、パディング=SAME、ストライド=(1,1)、融合活性化なし。 # On the i.MX 8M Plus board: python3 reproduce.py conv_1x17_broken.tflite # exits 1: BROKEN, saturated to int8=127 python3 reproduce.py conv_1x15_torch_control.tflite # exits 0: OK (K<16, same pipeline) reproduce.py(添付ファイル、tflite_runtimeとnumpyのみに依存)は、6つのシード付きランダムなint8入力をプレーンおよびVX委任インタープリタに通し、平均|Δ|、最大|Δ|、およびVXパスからの一意のint8出力値のカウントを報告します。 カーネルサイズスイープ 単一Conv2Dユニットテストモデル、INT8 PTQ。同じ int8 入力バイトにおける、ボード VX とボード CPU の平均 |Δ|。uniq_VX = 6 つの入力 (256 個中) における一意の int8 出力値。 カーネル(H, W)平均|Δ|uniq_VX結果 (1、11) 0.03 256 OK (1、15) 0.02 256 OK (1、16) 134.9 1 破損しています(定数 int8=127) (1、17) 136.9 1 破損しています(定数 int8=127) (1、23) 130.5 1 破損しています(定数 int8=127) (15、1) 0.11 256 OK (17、1) 136.9 1 破損しています(定数 int8=127) (23、1) 129.3 1 破損しています(定数 int8=127) (3, 3)、(5, 5)、(7, 7) < 0.2 256 OK (15、15)(エリア225) 0.41 256 OK (3、23) 123.4 1 破損しています(定数 int8=127) (5、15) 0.24 256 OK しきい値は H と W にそれぞれ独立して適用されます。すべての不具合ケースにおいて、VX 出力はすべての位置で int8 = 127 に飽和します。正の int8 極値への飽和 (output_zp または 0 ではなく) は、最終クランプ前の乗算器シフトオーバーフロー、または MAC 結果の代わりに固定値が出力タイルに書き込まれていることを示唆しています。この問題はカーネル領域とは関係ないようです(例えば、15x15は正常に動作します)。 このしきい値は必要条件ではあるが十分条件ではない。K ≥ 16 の場合、一部の int8 の重み値のパターンはバグを引き起こすが、他のパターンは引き起こさない。バイトレベルの分離実験(破損したアーティファクトと破損していないアーティファクトの間に個々のTFLiteテンソルフィールドを移植する)を行い、値パターンのトリガーを特定のテンソルフィールドに絞り込みました。もしお役に立てるようでしたら、分離結果と使用したツールを喜んで共有いたします。 詳細ログ抜粋(VSI_NN_LOG_LEVEL=5、大文字小文字を区別しない) INFO: Vx delegate: error_during_init set to 0. INFO: Vx delegate: error_during_prepare set to 0. INFO: Vx delegate: error_during_invoke set to 0. I [vsi_nn_CreateGraph:1327] OVXLIB_VERSION==1.2.14 D [setup_node:535] Setup node id[3] uid[30000] op[DATACONVERT] D [setup_node:535] Setup node id[0] uid[1] op[PERMUTE] D [setup_node:535] Setup node id[1] uid[2] op[CONV2D] D [setup_node:535] Setup node id[2] uid[3] op[PERMUTE] D [setup_node:535] Setup node id[4] uid[30001] op[DATACONVERT] D [vsi_nn_kernel_selector:1286] Instance OPENVX node with kernel "conv2d" 完全なログファイルは vsi_nn_log_level_5_conv_1x17.txt として添付されています。 添付ファイル bug_report_artifacts.tar.gz としてバンドルされています。 conv_1x17_broken.tflite — 2,136バイトの破損したアーティファクト。 conv_1x15_torch_control.tflite — 2,056バイトのサブスレッショルド制御、同じパイプライン。 reproduce.py — ボード側再現ツール(tflite_runtime + numpyのみ)。 vsi_nn_log_level_5_conv_1x17.txt — 完全な詳細ログ。 ご要望に応じて、追加のアーティファクトを提供できます。バイトレベルの分離ツール、デルタ解析用の構造的に同一の動作アーティファクト(1、17)、完全な十分条件グラフト結果。 i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Linux ソフトウェア不具合の疑い Re: Conv2D on i.MX 8M Plus VX delegate produces incorrect output when either spatial kernel dim > こんにちは、 @themis_stewartさん 情報ありがとうございます。いただいた2つの質問について、社内チームに確認中です。 よろしくお願いします、 志明 Re: Conv2D on i.MX 8M Plus VX delegate produces incorrect output when either spatial kernel dim > こんにちは、 @themis_stewartさん カーネルサイズが16より大きい場合に演算をCPUにフォールバックさせるには、 L6.18.2に基づいた以下のパッチをお試しください。 よろしくお願いします、 志明 Re: Conv2D on i.MX 8M Plus VX delegate produces incorrect output when either spatial kernel dim > 迅速な対応をありがとうございます。ガードパッチを適用・テストした結果、こちらの問題は解決したと確認しています。 op_map.ccの変更を含むlf-6.18.2_1.0.0のデリゲートソースからパッチ付きlibvx_delegate.soを作成し、元のレポートの最小限のリプロダクターと比較して i.MX 8M Plus EVKで検証しました。パッチ適用後: 影響を受けるINT8 Conv2D(空間カーネル≥16)は、デリゲートによって適切に拒否され、TFLite CPUにフォールバックするようになりました。ログメッセージにはフォールバックが明示的に表示され、int8 = 127へのサイレント飽和はなくなりました。出力はCPUの参照値と完全に一致する。 本番モデル(カーネル≤15)は影響を受けず、完全にNPUに委譲されているため、ガードが過剰トリガーされないようにしています。 CPUフォールバックパスは実際には良好に機能していますが、フォールバックはNPU上で完全に動作するモデルよりも自然に遅いです。回帰テストのカバレッジ向上に役立つようでしたら、詳細な前後比較ベンチマークを個別にご提供いたします。 改めてありがとうございました。大変感謝しています。
View full article
S32K396 RTD 5.0: eMIOS CH0/CH1 PWM Not Generated and Unexpected LCU Output Behavior Hi NXP Team, I am working on an S32K312 using S32 Design Studio 3.6.7 with RTD 5.0 (AUTOSAR 4.7). I have configured eMIOS to generate six PWM signals through eMIOS → TRGMUX → LCU → Output Pins for motor control. I am facing two issues: eMIOS CH0 and CH1 do not generate PWM, while CH2 to CH5 generate PWM correctly. Clock, Port, eMIOS MCL, eMIOS PWM, Global Time Base, TRGMUX, and LCU are all initialized successfully, and the PWM configuration for CH0 and CH1 is the same as the working channels. I have observed unexpected behavior with the LCU outputs. When I set LCU Output Index 4 to 0, Output 4 continues to generate PWM, but Output 5 becomes permanently OFF. Similarly, when I set LCU Output Index 2 to 0, Output 2 continues to generate PWM, but Output 3 becomes permanently OFF. I expected each LCU output to operate independently, but changing one output appears to affect the adjacent output. Could you please advise: Are there any hardware or RTD restrictions for using eMIOS CH0 and CH1 with the LCU? Is any additional TRGMUX or LCU configuration required for CH0 and CH1? Are LCU outputs internally paired or dependent in complementary mode? Is this behavior expected, or does it indicate an incorrect LCU/TRGMUX configuration or a known issue in RTD 5.0? I have attached my project and configuration files for reference. Thank you for your support. Re: S32K396 RTD 5.0: eMIOS CH0/CH1 PWM Not Generated and Unexpected LCU Output Behavior Hi @Esakki  I made a few tests by modifying the period, duty cycle, and phase shift of the PWM signals generated by eMIOS channels 0 and 1, based on the PMSM Motor Control Sensorless Dual Shunt FOC on FRDM-A-S32K312 demo application. During these tests, the LCU generated output signals as expected, which suggests that the eMIOS channels themselves do not have any inherent limitation in this use case. Based on the results, it appears that the current PWM configuration may be causing the LCU output to remain constantly low, even though both PWM signals are correctly routed to and received by the LCU.  I would recommend reviewing the previously shared demo application, as well as the example provided in the thread S32M27x/S32K3 – eMIOS/TRGMUX/LCU – [RTD600]. These examples demonstrate a working eMIOS → TRGMUX → LCU configuration and may serve as a useful reference. BR, vaneB
View full article
S32K396 RTD 5.0:eMIOS CH0/CH1 PWM 未生成且 LCU 输出行为异常 您好,NXP团队: 我正在使用S32 Design Studio 3.6.7和RTD 5.0 (AUTOSAR 4.7)开发S32K312 。我已经配置 eMIOS 通过eMIOS → TRGMUX → LCU → 输出引脚生成六个 PWM 信号,用于电机控制。 我面临两个问题: eMIOS CH0 和 CH1 不产生 PWM ,而CH2 至 CH5 正确产生 PWM 。时钟、端口、eMIOS MCL、eMIOS PWM、全局时基、TRGMUX 和 LCU 均已成功初始化,CH0 和 CH1 的 PWM 配置与工作通道相同。 我发现 LCU 输出出现了异常行为。当我将LCU 输出索引 4设置为 0 时,输出 4 继续产生 PWM ,但输出 5 永久关闭。同样地,当我将LCU 输出索引 2设置为 0 时,输出 2 继续产生 PWM ,但输出 3 永久关闭。我原以为每个 LCU 输出都会独立运行,但改变一个输出似乎会影响相邻的输出。 请问您能否提供以下建议: 使用 eMIOS CH0 和 CH1 与 LCU 配合使用时,是否存在任何硬件或 RTD 限制? CH0 和 CH1 是否需要额外的 TRGMUX 或 LCU 配置? LCU 输出在内部是成对的还是互补模式下相互依赖的? 这种行为是预期的,还是表明 LCU/TRGMUX 配置不正确,或者 RTD 5.0 中存在已知问题? 我已附上我的项目文件和配置文件供您参考。 感谢您的支持。 Re: S32K396 RTD 5.0: eMIOS CH0/CH1 PWM Not Generated and Unexpected LCU Output Behavior 嗨@Esakki 我根据FRDM-A-S32K312 演示应用程序上的 PMSM 电机控制无传感器双并联 FOC ,通过修改 eMIOS 通道 0 和 1 生成的 PWM 信号的周期、占空比和相移进行了一些测试。在这些测试中,LCU 按预期生成了输出信号,这表明 eMIOS 通道本身在此用例中没有任何固有的限制。 根据结果来看,当前的 PWM 配置可能导致 LCU 输出始终保持低电平,即使两个 PWM 信号都已正确路由到 LCU 并被 LCU 接收。 我建议您查看之前分享的演示应用程序,以及在S32M27x/S32K3 – eMIOS/TRGMUX/LCU – [RTD600]主题中提供的示例。这些示例展示了 eMIOS → TRGMUX → LCU 的可行配置,可作为有用的参考。 BR,叶片B
View full article