Hi NXP Team,
I am working on an S32K312 using S32 Design Studio 3.6.7 with RTD 5.0 (AUTOSAR 4.7). I have configured eMIOS to generate six PWM signals through eMIOS → TRGMUX → LCU → Output Pins for motor control.
I am facing two issues:
eMIOS CH0 and CH1 do not generate PWM, while CH2 to CH5 generate PWM correctly. Clock, Port, eMIOS MCL, eMIOS PWM, Global Time Base, TRGMUX, and LCU are all initialized successfully, and the PWM configuration for CH0 and CH1 is the same as the working channels.
I have observed unexpected behavior with the LCU outputs. When I set LCU Output Index 4 to 0, Output 4 continues to generate PWM, but Output 5 becomes permanently OFF. Similarly, when I set LCU Output Index 2 to 0, Output 2 continues to generate PWM, but Output 3 becomes permanently OFF. I expected each LCU output to operate independently, but changing one output appears to affect the adjacent output.
Could you please advise:
Are there any hardware or RTD restrictions for using eMIOS CH0 and CH1 with the LCU?
Is any additional TRGMUX or LCU configuration required for CH0 and CH1?
Are LCU outputs internally paired or dependent in complementary mode?
Is this behavior expected, or does it indicate an incorrect LCU/TRGMUX configuration or a known issue in RTD 5.0?
I have attached my project and configuration files for reference.
Thank you for your support.
Hi @Esakki
I made a few tests by modifying the period, duty cycle, and phase shift of the PWM signals generated by eMIOS channels 0 and 1, based on the PMSM Motor Control Sensorless Dual Shunt FOC on FRDM-A-S32K312 demo application. During these tests, the LCU generated output signals as expected, which suggests that the eMIOS channels themselves do not have any inherent limitation in this use case.
Based on the results, it appears that the current PWM configuration may be causing the LCU output to remain constantly low, even though both PWM signals are correctly routed to and received by the LCU.
I would recommend reviewing the previously shared demo application, as well as the example provided in the thread S32M27x/S32K3 – eMIOS/TRGMUX/LCU – [RTD600]. These examples demonstrate a working eMIOS → TRGMUX → LCU configuration and may serve as a useful reference.
BR, vaneB