2397486_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2397486_en-US

2397486_en-US

Using IMX95 in MCUXpresso Secure Provisioning Tool Version 26.06

I have download imx-oei-master on github and use make to generate oei-m33-ddr.bin and oei-m33-tcm.bin. And I try to build image as picture attach.

1.jpg

jimmychang_0-1784688980880.png


I have some questions:

1. Is my setting correct?

2. In "Type", I saw many of items. I don't know which one I need to select?

3. In "Load address" and "Entry point", Is my setting is correct or not? I only saw CM33_TCMU_OFFSET = 0x1ffc0000 in oei-m33-ddr.map. I even didn't see about lpddr5

4. In "Image Type", I also saw many of items. I don't know which one I need to select? By the way what is the difference between "Type" and "Image Type"

5. In "Container set", which one I should select Primary or Secondary image?

Re: Using IMX95 in MCUXpresso Secure Provisioning Tool Version 26.06

Please refer to the guidance here for building i.MX95 boot images: https://docs.mcuxpresso.nxp.com/secure/26.06/06_processor_specific_workflow.html#i-mx-95-bootable-im...

It has detailed description and snapshot about what images are needed.

Also note that the ddr quick boot binaries can be selected for i.MX95 B0 devices while adding image "OEI DDR no QB" as below:

 

image-2026-07-24-17-41-23-792.pngimage-2026-07-24-17-41-23-792.png

image-2026-07-24-17-40-38-998.pngimage-2026-07-24-17-40-38-998.png


Re: Using IMX95 in MCUXpresso Secure Provisioning Tool Version 26.06

Thanks for your quickly reply.

タグ(1)
評価なし
バージョン履歴
最終更新日:
1ヶ月前
更新者: