2396704_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2396704_en-US

2396704_en-US

Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed

Hello,
I am working on a project based on the MPC5644A, and I need to obtain the RAppID Init tool that supports this device.
I have an existing RAppID Init project file (.rsp) that was originally created for our platform. The file header shows the following:

Tool version: 2.1.0 (toolVersionMajor 2, toolVersionMinor 1, subVersionNumber 0)
Target device: MPC5644A
Created: April 2013

So MPC5644A support clearly existed in RAppID Init v2.1.0. However, I cannot find a matching download on the current NXP website:

The "RAppID Initialization for Power Architecture" page (RAPPID) lists 11 public downloads, but none of them cover the MPC564xA family (only MPC564xL, MPC560xB/xS, MPC563xM, MPC567xR/xK/xF, MPC5748G, MPC577xK/M).
In the archive section I did find "Archive: Pin Wizard for MPC564xA", but no corresponding "Init for MPC564xA" package. The Pin Wizard does not cover system/peripheral initialization, and it cannot open my .rsp project file.

Could a moderator please provide a download link for RAppID Init v2.1.0 or later with MPC5644A device support, so that I can open and modify my existing .rsp project?
Thank you in advance for your help.

Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed

Hello,

Yes, you are correct, there is existing RAPPID-564XASW.

But NXP is not offering it on public web page.

I will ask internally what is the procedure to obtain it.

Best regards,

Peter






Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed

Please check the link at RAppID Initialization for Power Architecture | NXP Semiconductors   
RAppID Boot Loader Utility   Init for MPC564xL

https://www.nxp.com/design/design-center/software/embedded-software/rappid-initialization-for-power-...

btw, what kind of application does MPC5644A is working for you? 

Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link neededI've already seen that page, but mine is different because it's an MPC5644A.

Also, my MPC5644A appears to be used for vehicle control.
Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link neededWhen can I expect a response?Re: Request: RAppID Init v2.1.0 (or later) with MPC5644A device support — download link needed

https://www.nxp.com/webapp/Download?colCode=ETPUGCT&appType=license&location=null
How about eTPU Graphical Configuration Tool? It seems pretty useful as well. Since the product is pretty old device, some service delay could be expected

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-28-2026 04:30 AM
更新者: