LPC Microcontrollers Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC Microcontrollers Knowledge Base

Discussions

Sort by:
This document was made to explain how to regain control of any LPC EVK on brick mode without using an external debugger. Explore the simple way. In some cases, this method forms well and is the easy way, open your IDE and select your project.   At this point you may have a debugger configuration of your last debug session, so, you have similar icons to the image. Open the tab below and select erase. Depending on your debugger configuration you need to select the same icons below. Note: In some cases will be necessary to put your MCU in ISP. And that’s all, could try if the MCU is out the brick mode.   Introduction First, you need to install these tools on your PC. LPCScrypt [LPCScrypt v2.1.2 | NXP Semiconductors]. J-Link Commander. [J-Link Commander (segger.com)]. To understand this document, we need to know that every EVK [Evaluation Kit] can be divided into 2 parts. The debugger on the board Link2 and the target LPC55sXX. Figure 1. Link2 Green square, LPC55sXX Red square This document will describe two methods that must be done in the order mentioned because we will see how to update the firmware of the debugger to use the same board for a self-recovery, this step is necessary for the tool J-Link Commander to recognize the debugger as a Segger probe, then when the update is done the second step should be to enter ISP mode to do a mass erase of the target to get out of the brick mode. Link2 The Link 2 (LPC4370) debugger on the board probe can be configured to support various development tools and IDEs using a variety of different downloadable firmware images. Available firmware images include: J-Link by Segger. LinkServer. By default, the EVK board has the firmware LinkServer on the LPC4322 (dependent on your board), for this proposal we will see how to change to J-Link On-Board. DFU The EVK needs to be prepared to receive this firmware on the debugger, to do that we need to put the board on DFU [Device Firmware Update]. On the schematic need to find the DFU jumper to put on the board, the image below is an example of different EVKs check Figure 2.   Figure 2. DFU from different boards. Then connect it to the PC. Note: The firmware update is completely reversible. LPCScrypt Once installed on the PC we need to locate these files of the installation. Root example: C:\nxp\LPCScrypt\scripts When you have the board on DFU, connecting the USB Llink2 to the PC and then RUN the Scrypt (program_JLINK) in CMD check Figure 3. Press any key to continue… Figure 3. Flash firmware of J-Link in DFU mode. Successfully done, at this moment the EVK has the firmware of J-Link Segger. Review the Figure 4. Figure 4. The firmware was flashed successfully. Remove the USB cable to remove the DFU jumper with the board unpowered. ISP Brief of ISP (In System Programming) this method is used to recover a part programmed with a corrupted image which is not detectable by ROM. So, to enter this mode the user needs to put a jumper in the ISP header pins, search for this in the schematic, then connect to the PC and check Figure 5.     Figure 5. ISP image examples from different boards. J-LINK Commander Open the software and if the communication is right the message will appear J-Link via USB… OK check Figure 6. Figure 6. The EVK is now communicating to the tool J-Link Commander. Commands To start the communication needs to send the command “connect”. Then the tool shows your last target (if you use it) and use the next command “?” to change the target review Figure 7. Figure 7. Review the target. In the new popup window in the green area, you need to put the name of the target, take care you do not put the debugger check Figure 8. Figure 8. In the green area, you need to put the matricula of the MCU target. Example [LPC55s16 or LPC55s69] depending of your target check Figure 9. Figure 9. If the tool supports the MCU will show below the red square. In the next selections the tool is asking for the interface of communication, the communication of the EVK is SWD, and for that write “S” as SWD. On speed, only click enter without entry. Then this will appear before the connection check Figure 10. Figure 10. The communication is Done. Then use the command “erase” like the Figure 11. Figure 11. The tool indicate the erase is done. Finally disconnect the USB and remove the ISP jumper, then open the IDE and test the blinky led example, or if you wanted you could use the BLHOST. Flashing the MCU using  BLHOST. At this step you could able to use the IDE or use BLHOST. You could install SPSDK if you wanted [Installation Guide — SPSDK documentation]. In ISP mode… blhost -p COMxx  get-property 1 Figure 12. The first command is to check the communication. blhost -p COMxx flash-erase-all Figure 13. Do a mass erase. blhost -p COMxx write-memory 0 C:\root_example\Debug\led_blinky.bin Figure 14. The flashing was done. Remove the ISP jumper and reset your device. Common error LPCScrypt If the message appears “Nothing to boot”, need to be sure the board is connected to the PC with the DFU mode in LINK 2 check Figure 16. Figure 16. The red square is an example of an error communication. J-Link Commander If a similar message appears, “Cannot connect to target”, need to put the target in ISP mode, and return to the first steps with J-Link commander check Figure 18. Figure 18. Show how the communication is not done.
View full article
Introduction Amazon Web Services (AWS) is the world’s most comprehensive and broadly adopted cloud platform, offering over 165 fully-featured services from data centers globally. Millions of customers —including the fastest-growing startups, largest enterprises, and leading government agencies—trust AWS to power their infrastructure, become more agile, and lower costs.This document will take you step-by-step in a simple approach to adding peripherals to your AWS IOT and Alexa skills project. This is in continuation of the demo established in the following link, it is important to have this completed before continuing with this guide: Connecting the LPC55S69 to Amazon Web Services  Prerequisites - LPC55S69-EVK - Mikroe WiFi 10 Click - AWS Account - Alexa Developer Account - MCUXpresso IDE 11.2 - LPC55S69 SDK 2.8.0 Modifying "AWS_REMOTE_CONTROL_WIFI" In this example I will be adding a single-ended ADC peripheral. 1. First, create a separate .c and .h files in my source folder to keep it organized.  2. Initialize your peripheral. This includes your global variables, pins, clocks, interrupt handlers and other necessary peripheral configurations yours may have.  In my new_peripherals.c file, I add the following 2.1 Definitions: 2.2 Global variables: 2.3 Interrupt handler: 2.4 Initialization function: 2.5 Read ADC Function: 3.  Create header file with the two functions that will be used to enable the ADC, make sure to include the "fsl_lpadc"drivers. 4.  Add the ADC pin with pin configuration tool.  4.1 In this example I use PIO0_23 for the ADC0 Channel 0, 5. Add ADC_Init function to the main. 6. Now let's go ahead and modify "remote_control.c". Here we need to build the JSON text that we want updating our Thing's shadow with the ADC value, add the read function, add the variable in the initial shadow document and the keyword for our DeltaJSON. 6.1 First create global variables for the actual state of the ADC interaction and the parsed state. 6.2 Add external function which will read the ADC value. 6.3 Shadows use JSON shadow documents to store and retrieve data. A shadow’s document contains a state property that describes these aspects of the device’s state: desired: Apps specify the desired states of device properties by updating the desired object. reported: Devices report their current state in the reported object. delta: AWS IoT reports differences between the desired and the reported state in the delta object. 6.4 I've added the initial ADC state with a hard-coded 0, so that I can verify my Thing's shadow is initialized with the new information. 6.5 In the "void processShadowDeltaJSON(char *json, uint32_t jsonLength)" function, we need to add the condition for the change in state of the ADC. This will helps us identify when the action to read the ADC is requested. 6.6 Finally in the "prvShadowMainTask" function, we will create the action based on the above request. We can add some PRINTFs so that we know that the action is requested and processed properly through the serial console. As you may see I only want to update the ADC value when it is requested. Meaning the value of the ADC's state or parsed state is important. We will clear it to zero after we read the ADC and only update the value when it is 1. As opposed to the LEDState and parsedLEDState, where the value is important since it points to which color LED will be on/off. That's it you can build and run the project! Now we can add the Alexa Skill and the functionality in the AWS Lambda. MODIFYING AWS LAMBDA Since the lambda will be the connection between our LPCXpresso board and the Alexa Skill, we need to add the handler for  our new ADC requests. 1.  In this example we add the third request type which is the ADC event and the name of the callback function we will use.  2. The callback function "manage_ADC_request" will contain the attributes for reading and updating the shadow, this will consequently cause the change in delta shadow so our LPC55S69 will read the ADC pin. In addition, the utterances sent to the Alexa skill as well as how we want Alexa to respond will also be defined here.  As you may observe our function builds the JSON payload to update the shadow with a "1" when it is called and ignores the led and accelerometer values. We delay for 2.5 seconds to allow the LPC to read and write the ADC value in the necessary field and send the updated shadow. Then the Lambda will read the shadow and create the return message.  With this we construct the answer for Alexa. MODIFYING ALEXA SKILLS 1.  First create a custom 'intent'. Here is the general definition of what the utterances will be to request an action from the AWS Thing.    1.1 The name needs to match the name used for the event in the Lambda. In this example it is ADC_INTENT 2. Before we create the utterances, let's create the slot types. This is the list of all the words possible that may come to mind that a user might say to request a reading from the ADC.  2.1 The name of the slot type is not crucial, however please note it as we will need it later.  2.2 Add slot values. You can add as many as you think are necessary. For recommendations on custom slot values please check, best practices for sample utterances. 2.3 Go back to the general view of the ADC_INTENT, scroll down and we will add how the slot will be included in the utterances. In this example I use adc_name, however the name here is also not crucial. Select the slot type list we created earlier. 2.4 Now scroll back up and lets begin adding the sample utterances. This can be any command that you believe a user can say to invoke this action. You do not need to include the wake word here. In brackets add the name of your intent slot, in this case it is {adc_name}. That's it! You can save and rebuild the model. You are now ready to test it. You can do so through the 'Test' tab on the developer's console. In addition if you have an Alexa device or the SLN-ALEXA-IOT, you can test it by speaking with Alexa directly. In your LPCXpresso55S69 you can connect the 3.3V or the 0V to the ADC pin so you can see how the value is returned every request. 
View full article
To help you get started with the LPC800 Mini-Kit, we've put together a few basic resources for you here. LPC800 Mini-Kit Code Base The LPC800 comes populated with an LPC810 MCU in a DIP8 package. The LPC810 package a lot of peripheral punch into a small, extremely affordable package, but as with any deeply embedded device, it's always a challenge to fit the most code and functionality possible into the smallest device available. The LPC810 with 4KB flash and 1KB SRAM is no exception. To help you get started writing light-weight, but easy to understand code in C, we've put together a basic code base for the LPC810 Mini-Kit based around NXP's free LPCXpresso IDE, which uses the free GNU toolchain beneath the surface. The latest version of the code can be viewed and downloaded online on github (LPC810 Code Base), or you can download the latest version directly. Board Schematic The schematics for the LPC800 Mini-Kit are available for download here. See what the LPCWare community did with it! In 2013, NXP ran the LPC800 Simplicity Challenge, and the LPCWare community showed amazing inventiveness in what they created. Check out what they did on our LPC800 campaign pages. Further LPC800 Resources In addition to the LPC800 Mini-Kit Code Base above, you may find some of the following links useful working with the LPC810: LPC810 Product Page on NXP.com LPC800 Switch Matrix Configuration Tool Introducing the LPC800 Videos on YouTube LPC800 Switch Matrix: Making life easier one pin at a time (LPCNow.com) LPC800 LPCXpresso Board Schematics LPCXpresso Forum (for LPCXpresso related support) Tutorial: Getting Started with the LPC810 (Adafruit.com) Programming the LPC800 Mini-Kit with Flash Magic The LPC800 mini board can be programmed using any SWD debugger and your favorite IDE -- NXP's own LPCXpresso, as well as IAR, Keil uVision, and Crossworks for ARM all support the LPC800 out of the box! -- but you can also use an inexpensive UART/USB adapter and ISP mode to program the flash memory on the LPC810. What You'll Need A USB to UART cable or adapter, such as FTDI's popular 'TTL-232R-3V3' cables or a breakout based on the FT232RL chipset The latest version of the free Flash Magic tool​ Configuring the LPC800 Mini Board The first step you will need to do is connect you UART to USB adapter cable to the 'FTDI' header on the top of the LPC800 Mini Board. The pin layout is setup to match FTDI's popular cables by default, specifically the 'TTL-232R-3V3'. Other adapters can of course be used, but you will need to connect the GND, VCC, TXD and RXD pins in the right location yourself. FTDI's TTL-232R-3V3 cable is shown connected here as a reference: LPC800-mini-board The next step is placing the LPC810 in 'ISP' mode. This is accomplished by pulling PIO0_1 'low' during reset, which causes the bootloader to enter ISP mode. The LPC800 mini board conveniently has an 'ISP' switch – the white button in the bottom left-hand side of the board – which we can hold down to pull the ISP pin low. While continuing to press the ISP button, press and then release the 'RESET' button (the red button on the opposite side of the board). This will cause the board to reset, the internal bootloader will see that the ISP pin is low, and it will enter ISP mode where we can program the flash in Flash Magic using the on-chip UART0 peripheral. Configuring Flash Magic for the LPC810 The next step requires you to download and install the latest version of Flash Magic if you haven't already done so. It's available for free at http://www.flashmagictool.com/. Once installed, open the tool, and the run through the following steps: Setup the 'Communications' options: Select LPC810M021FN8 as your target device Set your COM port to whatever port your USB to UART adapter enumerated as (you can find this in the device manager in Windows) Set the Baud Rate to 115200, or whatever matches your USB to UART adapter Make sure that the 'Interface' is set to 'None (ISP)' Set the Oscillator to '12', which matches the speed of the IRC used by the bootloader You can double-check all of your communications settings and connection by selecting the 'ISP > Read Device Signature …' menu item. If you are in ISP mode and properly connected, with the right 'Communications' settings, you should see something similar to the following screen:FlashMagic Device IDIf you get an error message, double check your connections and your settings in Flash Magic, making sure you are actually in ISP mode on the LPC810, and that you've selected the right COM port. Check the 'Erase blocks used by Hex File' checkbox in the 'Erase' section. Select your hex file in the 'Hex File' section: Use the 'Browse' button to point to the Intel Hex file generated by your toolchain or IDE (for example, LPCXpresso). You can also use one of the sample .hex files available here if you don't have a .hex file ready yet. You should end up with Flash Magic configuration as follows ('Verify after programming' is optional): Flash magic settings: Now click the 'Start' button to program the flash … … and finally, once the device has been programmed, reset your board (via the red 'Reset' button). If at some point you want to change your firmware, simply repeat the process of re-entering ISP mode by holding the ISP pin low, resetting the LPC810, releasing the ISP pin, and the programming the device via Flash Magic again. Known issues There is an issue with some of the LPC810 DIP8 parts that are populated on the mini board that prevents the analog comparator from functioning. To see if the part on your board is affected, locate the date code on the top of the DIP8 package (the last line of text on top of the chip). If this line end with either "2X" or "2A", your part is affected. LPC800 mini board schematics Rev AR2.pdf - Attached
View full article
Hi: Since LPC series ADC has sequence function, so implement multi-channel ADC transfer is easy. But use DMA is also meaning, so there are two demos to show how to use such applications 1.lpc_multi-channels_adc_dma_sw_trg Use SW trigger multi channels ADC transfer, but use DMA to transfer result to result array. use don't need to care the channel result register, but fetch data from global data register; 2.lpc_multi-channels_adc_dma_hw_trg for many cases, user need to trigger ADC multi channels transfer periodly, and collect enough data for processing. so this demo use SCT_OUT7 to trigger ADC Sequence A for 6 channels, then after 1024 rounds, generate DMA interrupt to process all 6*1024 data array. all demos are implemented on SDK2.6.0 
View full article
I already have several customers met SB file loading error Inject command 'receive-sb-file' while working on LPC55S6xx 1B version. There is significant change of Secure Boot in LPC55S6xx 1B version and 0A version. To solve this problem, we need to understand it first.     1  SB2.1  vs. SB2.0 SB2 container is described in elftosb User’s Guide. SB file config file contains configuration commands that will be processed after SB2 file is loaded in the device. The image location is stated in the "sources" .bd file section. SB key in text file is used for encryption with elftosb command line tool.   The 0A version of the LPC55S6xx silicon supports version 2.0 of the SB image format. The 1B version of the LPC55S6xx silicon supports version 2.1 of the SB image format. The main difference between version 2.0 and version 2.1 is in the usage of the digital signature. SB 2.0 is encrypted and SB2.1 is encrypted + signed.     2. SB file Preparation and Usage   Example of use (Encrypted SB2):   elftosb -f lpc55xx -k "sbkek.txt" -c "commandFile.bd" -o "output.sb2" "input.bin"   where -f = family lpc55xx -k = path to KEK file (SBKEK) -c = path to command file to be processed:   options { flags = 0x4; // 0x8 encrypted + signed, 0x4 encrypted buildNumber = 0x1; productVersion = "1.00.00"; componentVersion = "1.00.00"; } sources { inputFile = extern(0); } section (0) {       erase 0x0..0x40000; load inputFile > 0x0; }   -o = path to output file   files... = path to files (usually image files), which will be replacing placeholders defined in command file, paths can be hardcoded in command file and then not inserted as input   Example of use (Encrypted + Signed SB):   1 root key   elftosb.exe -f lpc55xx -k "sbkek.txt" -c "commandFile.bd" -o "output.sb2" -s "selfsign_privatekey_rsa2048.pem" -S "selfsign_v3.der.crt" -R "selfsign_v3.der.crt" -h "RKTH.bin" "input.bin"   4 root keys   elftosb.exe  -f lpc55xx -k "sbkek.txt" -c "commandFile.bd" -o "output.sb2" -s private_key_1_2048.pem -S certificate_1_2048.der.crt -R certificate_1_2048.der.crt -R certificate_2_2048.der.crt -R certificate_3_2048.der.crt -R certificate_4_2048.der.crt -h "RHKT.bin" "input.bin"   where -f = family lpc55xx -k = path to KEK file (SBKEK) c = path to command file to be processed   options { flags = 0x8; // 0x8 encrypted + signed, 0x4 encrypted buildNumber = 0x1; productVersion = "1.00.00"; componentVersion = "1.00.00"; } sources { inputFile = extern(0); } section (0) {       erase 0x0..0x40000; load inputFile > 0x0; }   -o = path to output file -s = path to private key of certificate used for signing -S = path(s) to certificates in certificate chain, each certificate in chain must be specified with new -S switch in order of how was chain created (root certificate first) -R = path(s) to root certificate(s), 1-4 root certificates can be specified, each root certificate must be specified with new -R switch, one of the root certificates must be first certificate specified by -S switch -h = path and name of output binary file generated by elftosb, which contain hash of hashes of all root certificates (RKTH), which must be uploaded to the device register files... = path to files (usually image files), which will be replacing placeholders defined in command file, paths can be hardcoded in command file and then not inserted as input The SB2.0 file created with the updated binary image can be loaded into the device through ISP command handler with command “receive-sb-file“   blhost -p COMxx receive-sb-file <path to the secured binary(.sb2)>   The SB2.1 file created with the updated binary image can be loaded into the device through ISP command handler with command “receive-sb-file“ but keep in mind that before sending SB2.1 file into device has to be there already RKTH in CMPA (see AN12283 chapter 5.5 CMPA preparation) and enabled RoT keys in ROTKH_REVOKE field at CFPA page address 0x9DE18 (see chapter AN12283 5.4 CFPA preparation).   blhost -p COMxx receive-sb-file <path to the secured binary(.sb2)>   After successfully loading the SB2 file it is executed as configured in SB configuration file (.bd file). The above figure shows an example of SB configuration file. When the file is executed, the internal flash address from 0x0 to 0x40000 is erased. After flash erase operation, the image mentioned in the sources parameter is loaded to address 0x0. Reset the device after these operations. The updated image loaded into internal flash starts to execute.    English and Chinese versions of this article are both attached.
View full article
Contents 1. Principle of energy measurement 2. Energy measurement test   2.1 Use in non-Debug state   2.2 Use in Debug state   During the operation of MCU, real-time measurement of board current and voltage is of great significance to the stability of system power consumption. Especially in scenarios that are sensitive to voltage and current fluctuations, it is particularly important to collect and analyze high-frequency samples. MCUXpresso IDE integrates the power measurement function, which can measure the current and voltage of the development board in real time and calculate the real-time power consumption. Based on MCUXpresso IDE v11.5.0, this article mainly explains power measurement function usage. 1.   Principle of energy measurement Currently the MCUXpresso IDE energy measurement function supports the following development boards: -LPCXpresso546x8/540xx/54S0xx -LPCXpresso54102 -LPCXpresso51U68/54114 -QN9090-DK006/ JN5189-DK006/IOTZKB-DK006 -QN9080DK The power measurement actually uses the LPC-Link2/MCU-Link debugger on the development board to collect the conversion value of the A/D conversion chip, and perform software calculation to obtain the power measurement result. Taking LPCXpresso54628 development board as an example, the following is the circuit diagram of the power measurement part: Fig.1 The MAX9634TEUK+T is a precision current amplifier. And ADC122S021 is a 12-bit A/D converter with dual-channel sampling, its rate can reach 200ksps. ADC122S021 collects LPC54xx_CURR and SHLD_CURR voltages, IDE sets Target resistor (Total Rvsense in the figure) and Shield resistor (resistance value corresponding to SHLD_CURR) in advance. The LPC-Link2 debugger can calculate the voltage, current and power consumption information by collecting AD conversion values. 2.   Energy measurement test Taking LPCXpresso54628 development board as an example. Open the menu bar : Analysis->Energy Measurement. The Energy Measurement interface will appear in the lower right corner of the screen, which is divided into Plot drawing and Config configuration interface. It can be used in Debug state or in non-Debug state during measurement. Test the case of LED small light flickering and observe the changes of voltage, current and energy consumption. Note that the LPC-Link2 debugger version should be CMSIS-DAP probe version 5.147 and above. 2.1 Use in non-Debug state Click the button  in energy measurement interface and select the measured in the config interface. You can select the target voltage, target current and shielding current. The sampling rate can be selected as 50ksps, 62.5ksps or 100ksps. First select the model of the development board to be tested, and then continue to select the target resistance and shielding resistance. The target resistance value is selected according to the jumper cap description in Figure 1. The resistance value of the shielding resistance is the fixed resistance value of development board. As shown in the figure below: Fig.2 Select the target voltage to be measured, and click the button to run the Energy Measurement interface. You can see the slight fluctuation of voltage in the plot interface and view the average voltage through the delimited area of horizontal measurement, as follows: Fig.3 Select the target current to be measured. Before measuring the target current, click Read from target on the config interface to calculate the average value of the target voltage within 0.5s for subsequent power consumption calculation. Click the run button to see that the target current fluctuates slightly with the flashing of the small light in the plot interface. At the same time, check the average current, power consumption and energy consumption through the delimited area of horizontal measurement, as follows: Fig.4 2.2 Use in Debug state When used in the debug state, you can use MCUXpresso IDE or KEIL to enter the debugging state. Click the button on the energy measurement interface to read the power consumption in the debug state. The measurement process is the same as the non-Debug state, as follows: Fig.5 This is a general enablement document of how to use energy measurement feature in debug and non-debug mode. For more, please refer  MCUXpresso_IDE_Energy_Measurement. pdf under MCUXpresso IDE install folder.    
View full article
Unboxing of the Mini-Monkey.    This was a demonstration of how you can use a low cost 2-layer PCB process with the LP55S69 in the 0.5mm pitch VFBGA98 package.    We used Macrofab for the prototypes and the results were fabulous. Blog articles on the Mini-Monkey: https://community.nxp.com/community/general-purpose-mcus/lpc/blog/2020/03/13/mini-monkey-part-1-how-to-design-with-the-lpc55s69-in-the-vfbga98-package https://community.nxp.com/community/general-purpose-mcus/lpc/blog/2020/03/29/mini-monkey-part-2-using-mcuxpresso-to-accelerate-the-pcb-design-process https://community.nxp.com/community/general-purpose-mcus/lpc/blog/2020/04/19/lpc55s69-mini-monkey-build-update-off-to-fabrication
View full article
Now that you've downloaded & unzipped your LPCXpresso54608 SDK, let's open KEIL uVision IDE. Note: you must have at least uVision version 5.22.0.0 to use this board Before we start utilizing uVision we must make sure that we have the relevant packs installed to work with the LPCXpresso54608 board. Select the Pack Installer on the toolbar. The Pack installer shows you which parts and boards for which you have support. On the left hand side you see a variety of different manufacturers. The easiest way to search will be to type 'lpc' into the search right below the devices tab. Then select 'LPC54000 Series'. On the right hand side under the packs tab you will see one item listed under 'Device Specific' called 'Keil::LPC54000_DFP' click on install Note: Version 2.1.0 released on 10-18-2016 added LPC5460x support. If you had downloaded this pack before go to Packs>Check for Updates at the top to download the latest version Once installed the diamond will turn green. To double check we are ready, select boards on the left side and search  'lpcxpresso54'. You will notice that our board is green indicating we have support for it in uVision. Now we can close the Pack Installer to return to uVision Select File>Open and navigate to the location you unzipped your SDK download.  By the way, within this folder there are plenty of SDK based demos for you to explore our microcontroller.  We will use one of them to guide you through this tutorial, but definitely take time to try all of them! Navigate to boards>lpcxpresso54608>demo_apps>touch_cursor>mdk, change file type to ''Project Files (*.uvproj, *.uvprojx) and select 'touch_cursor' Once opened, select 'Build' right above the Project window. Once the Build Output window tells you that you have successfully built the program select the 'Start/Stop Debug Session' icon. Note: You may receive a warning if you have a size limitation on the license you are using. If you do get a warning you can resolve licensing issues by going to File>License Management. Once the debug session has been started select 'Run' on the left side Once you have successfully flashed the board with this demo you will see the following, This demo utilizes the touch interface on the screen to read where you are touching and updates the cursor position to the last known location.   Remember that other demos and sample code are provided in the root folder of the SDK download.   Be sure to explore these demos and reach out on the community if you need help!
View full article
1    introduction The doc demonstrates how to use MRT(Multi-rate Timer) module to implement the delay function, the delay time is programmable. The MRT has a One-shot stall mode, with the mode, while the MRT channel counter counts down, the core stalls until the MRT channel counter reaches to zero. After the MRT channel counter reaches to zero, the MRT channel becomes idle, the core continues to work.   2 delay function description Sometimes, it is expected that there is a programmable delay between two instructions, for example Instruction 1 Delay Instruction 2 In general, the delay function can be implemented by forcing the core to execute __asm(“NOP”) instructions This code is like: Void delay(uint32_t interval) {        Uint32_t counter;        Counter=ConvertTimeToCounter(interval);        For(uint32_t i=0; i<counter); i++)        {        __asm(“nop”)        } }   The macro convertTimeToCounter is used to convert a time to a number of loop   1.   MRT feature The MRT module of LPC family provides a unique feature called One-shot stall mode, because the test is based on LPC55S69-EVK board, so I referred to the section 27.5.3 One-shot stall mode in UM11126.pdf. The MRT does not have external pad.   One-shot stall mode: Bus stall mode can be used when a short delay is need between two software controlled events, or when a delay is expected before software can continue. Since in this mode there are no bus transactions while the MRT is counting down, the CPU core stalls, consumes a minimum amount of power during that time until the MRT counter reaches to zero. Therefore the One-shot stall mode of MRT can make core stall during the MRT counting down process, the delay function can be implemented.   3 MRT clock source and delay time For the LPC55S69, the clock source of MRT module is the AHB Bus clock, which is the same as the core clock. For the LPC55S69 example, there is the code to set up the core clock void BOARD_InitBootClocks(void) {     BOARD_BootClockPLL150M(); } So the  MRT clock frequency is 150MHz.       The delay time is a time, but the MRT is a counter, so the delay time must be converted to the counter value. The counter value is dependent on the MRT clock frequency. The MRT clock source is AHB bus clock, or the core clock. The LPC55S69 core clock frequency is 150Mhz, so we can define #define MRT_CLOCK_FREQUENCY 150MHz If the required delay time is delay_time variable in second unit, the required MRT counter value is   MRT counter value=delay_time/(MRT clock cycle time)=delay_time* MRT_CLOCK_FREQUENCY.   For example, assume the required delay_time is 1mS or 1*10**(-3)  Second, the corresponding counter value is 1*(10**-3)*150*(10**6)=150 000   The MRT delay time restriction. The MRT counter register is 24 bits, the maximum counter value is 2**24= 16,777,216, the maximum delay time is 16777216/(150*10**6)=0.111848 S or 111 mS.     3 source code description MRT delay function source code is based on SDK package SDK_2_11_1_LPCXpresso55S69.zip, the tools is MCUXpresso IDE v11.5.0. The example is run on LPC55S69-EVK The example uses MRT to delay 100mS(0.1 Second), after the delay, a LED is toggled The MRT counter value is 0.1S*150*(10**6)=15 000 000   For the mrt_init() api function, it initializes the MRT and set the MRT channel0 in OneShotStall mode. Once the core executes the line MRT_StartTimer(MRT0, kMRT_Channel_0, 15000000); the MRT channel0 counter will count down from 15000000, during the counting process the Cortex-M33 will stall. After the counter reach to ZERO, the core finishes the stalling mode and continues to execute the next line, the MRT channel0 counter will be in idle mode.       /**  * @file    LPC55S69_Project_mrt_stall.c  * @brief   Application entry point.  */ #include <stdio.h> #include "board.h" #include "peripherals.h" #include "pin_mux.h" #include "clock_config.h" #include "LPC55S69_cm33_core0.h" #include "fsl_debug_console.h" #include "fsl_mrt.h" #include "fsl_iocon.h"   /* TODO: insert other include files here. */ #define BOARD_LED_PORT BOARD_LED_BLUE_GPIO_PORT #define BOARD_LED_PIN  BOARD_LED_BLUE_GPIO_PIN /* TODO: insert other definitions and declarations here. */ void mrt_init(void); /*  * @brief   Application entry point.  */ int main(void) {       /* Init board hardware. */     BOARD_InitBootPins();     BOARD_InitBootClocks();     BOARD_InitBootPeripherals(); #ifndef BOARD_INIT_DEBUG_CONSOLE_PERIPHERAL     /* Init FSL debug console. */     BOARD_InitDebugConsole(); #endif     mrt_init();     PRINTF("Hello World\n");     for(;;)     {     MRT_StartTimer(MRT0, kMRT_Channel_0, 15000000);     GPIO_PortToggle(GPIO, BOARD_LED_PORT, 1u << BOARD_LED_PIN);     __asm("nop");       }     /* Force the counter to be placed into memory. */     volatile static int i = 0 ;     /* Enter an infinite loop, just incrementing a counter. */     while(1) {         i++ ;         /* 'Dummy' NOP to allow source level single stepping of             tight while() loop */         __asm volatile ("nop");     }     return 0 ; }   uint32_t mrt_clock; mrt_config_t mrtConfig; void mrt_init(void) {           /* mrtConfig.enableMultiTask = false; */         MRT_GetDefaultConfig(&mrtConfig);           /* Init mrt module */         MRT_Init(MRT0, &mrtConfig);           /* Setup Channel 0 to be repeated */         MRT_SetupChannelMode(MRT0, kMRT_Channel_0, kMRT_OneShotStallMode);           //MRT_StartTimer(MRT0, kMRT_Channel_0,  15000000);   }       }                                                                                                              When the above code is running, user can see the blue LED toggles on the LPC55S69-EVK board. Connecting the PIO1_4 pin signal ( the pin 5 of P18 connector) on LPC55S69-EVK, the PIO1_4 signal toggling frequency is 5Hz, the cycle time is 200mS, so the delay is 100mS.      
View full article
The ADC converter for LPC55Sxx is a new IP, it has a lot of new features. The ADC converter clock frequency must be less than 24MHz, the ADC converter sampling rate can reach up to 1MSPS, the ADC converter supports to sample both the single-end analog signal and differential analog signal. It supports software triggering mode and hardware triggering mode, the triggering source can be from internal Timer, external pins, comparator output signal. The ADC converter supports synchronous sampling for only single-ended analog channel, but the analog channel pair are fixed for example CH0A/CH0B and CH1A/CH1B. The ADC of LPC55S6x consist of 16 Trigger Control (TCTRLa) registers, one trigger control register corresponds one hardware trigger source. For example, the TCTRL[0] corresponds trigger source0 GPIO irq_pint[0], the TCTRL[1] corresponds trigger source1 GPIO irq_pint[1]. When the GPIO IRQ_PIN[0] signal edge is detected, the ADC will be trigger to convert the analog channel. Hardware trigger Mapped to 0 GPIO irq_pint[0] 1 GPIO irq_pint[1] 2 State Configurable Timer (SCT) sct0_outputs[4] 3 State Configurable Timer (SCT) sct0_outputs[5] 4 State Configurable Timer (SCT) sct0_outputs[9] 5 State Counter Timer (CTIMER) ct0_mat3_out 6 State Counter Timer (CTIMER) ct1_mat3_out 7 State Counter Timer (CTIMER) ct2_mat3_out 8 State Counter Timer (CTIMER) ct3_mat3_out 9 State Counter Timer (CTIMER) ct4_mat3_out 10 Comparator 11 ARM tx event 12 GPIO BMATCH   The trigger attributes is defined in the corresponding TCTRLaXX register, when the TCTRLaXX[HTEN]=0, software trigger is enabled, hardware trigger is disabled. Setting the SWTRIG[xx] bit will trigger ADC to start conversion. The TCTRLaXX[TCMD] specifies which command buffer is executed.   There are 15 command buffers (CMDa), each consists of  two 32-bit registers (CMDLa:CMDHa), which specifies the ADC channels, resolution, sampling time.. For all the examples, a hardware triggering mode example is developed, the hardware triggering source 7 “State Counter Timer (CTIMER) ct2_mat3_out” is used to trigger ADC, so TCTRL[7] register is initialized, the TCMD bits in TCTRL[7] register is set up as 1, so the CMDH[1]:CMDL[1] are initialized to configure the analog channel, ADC sample resolution… .  
View full article
A vulnerability (CVE-2022-22819) has been identified on select NXP processors by which a malformed SB2 file header sent to the device as part of an update or recovery boot can be used to create a buffer overflow. The buffer overflow can then be used to launch various exploits. Refer to the attached bulletin for more information.   09/26/2022 - Bulletin updated to include fix datecode information. 11/01/2022 - Bulletin updated with clarification that mixed datecodes are RT600 only.    
View full article
Introducing MCUXpresso SDK v.2 for LPC54xxx Series What's New in MCUXpresso SDK v.2 for LPC54xxx? The Software Development Kit (SDK) 2.0.0 is a collection of software enablement for microcontrollers that includes peripheral drivers, multicore support, and integrated RTOS support for FreeRTOS OS and μC/OS. In addition to the base enablement, the SDK is augmented with demo applications and driver example projects, and API documentation to help the customers quickly leverage the support of the SDK. Development Tools The MCUXpresso SDK v.2 for LPC54xxx 2.0.0 was compiled and tested with these development tools: - LPCXpresso 8.2.0 - IAR Embedded Workbench for ARM® platform version 7.60.2 - MDK-ARM Microcontroller Development Kit (Keil)® 5.20 Supported Development Systems Development boards MCU devices LPCXpresso54114 LPC54114J256BD64, LPC54114J256UK49, LPC54113J128BD64, LPC54113J256BD64, LPC54113J256UK49 LPCXpresso54608 LPC54605J256ET180, LPC54605J512ET180, LPC54606J256ET180, LPC54606J512BD208, LPC54607J256ET180, LPC54607J512ET180, LPC54607J256BD208, LPC54608J512ET180, LPC54608J512BD208   SDK Board Support Folders SDK board support provides example applications for development and evaluation boards. Board support packages are found inside of the top level boards folder, and each supported board has its own folder (a SDK package can support multiple boards). Within each <board_name> folder there are various sub-folders to classify the type of examples they contain.   demo_apps: Full-featured applications intended to highlight key functionality and use cases of the target MCU. These applications typically use multiple MCU peripherals and may leverage stacks and middleware. driver_examples: Simple applications intended to concisely illustrate how to use the SDK’s peripheral drivers for a single use case. These applications typically only use a single peripheral, but there are cases where multiple are used (for example, ADC conversion using DMA). rtos_examples: Basic FreeRTOS examples showcasing the use of various RTOS objects (semaphores, queues, and so on) and interfacing with the SDK’s RTOS drivers usb_examples: Applications that use the USB host/device/OTG stack. multicore_examples: Applications for both cores showing the usage of multicore software components and the interaction between cores. Example Application Structure This section describes how the various types of example applications interact with the other components in the SDK. To get a comprehensive understanding of all SDK components and folder structure, see the SDK v.2.0 API Reference Manual document (SDK20APIRM). Each <board_name> folder in the boards directory contains a comprehensive set of examples that are relevant to that specific piece of hardware. We’ll discuss the hello_world example (part of the demo_apps folder), but the same general rules apply to any type of example in the <board_name> folder. In the hello_world application folder you see this: All files in the application folder are specific to that example, so it’s very easy to copy-paste an existing example to start developing a custom application based on a project provided in the SDK. Related links: For information on how to import and debug the MCUXpresso SDK example projects using LPCXpresso or generate your MCUXpresso SDK package take a look to this document: How to start with SDK v.2.0 for LPC5411x using LPCXpresso IDE Generating a downloadable MCUXpresso SDK v.2 package https://community.nxp.com/docs/DOC-333369  MCUXpresso Config Tools is now available!  
View full article
The OM13043 kit described below is no longer available (the LPC1227 and LPC1100XL devices are still available). This material is provided for reference materials, but KNX software is still available from Weinzierl Engineering. Building automation systems based on KNX communication protocols Communication is becoming essential in complex buildings. For this reason, NXP cooperates with Weinzierl Engineering to offer dedicated components to realize KNX based systems. A professional version of the KNX system B stack is now available on LPC Microcontrollers to allow a jump start with KNX development. System notes LPC1100XL and LPC1200 series microcontrollers: Based on the highly energy-efficient ARM® Cortex™-M0 processor Dramatically lower the cost per KNX node in home and building automation networks Cortex-M0 architecture ideally suited for low-complexity end nodes Include up to 128 KB Flash and 8 KB SRAM, and offer highly configurable peripherals Can be powered directly from the DC-DC converter of the KNX twisted-pair transceivers, making bus-powered devices easy to implement With performance levels up to 45 DMIPS, a single MCU delivers the resources required to run a KNX System B stack (up to 65535 nodes), with enough bandwidth available for the end application Reduced time to market – full professional stack available from partners with flexible license models A certified implementation of the KNX System B is available for the LPC1200 from Weinzierl Engineering  Implementation example (OM13042 demo board): Available with the NXP LPC1227 microcontroller and ON Semiconductor’s NCN5120 transceiver, suitable for use in KNX twisted pair networks (KNX TP1-256) Specifically designed to simplify design process with a ready-to-implement, energy-efficient KNX TP solution for applications such as lighting switches and control, HVAC control, shutters and occupancy detection Improves power efficiency, reduces development costs, accelerates time to market for KNX applications on ARM Cortex-M0 Application Note AN11231 is available here More information on KNX:  www.knx.org KNX TP Stack System B from Weinzierl Engineering - The new dimension of KNX development Each KNX device is based on a device model, that specifies both the management procedure (that is, how the device is configured via the bus) and identifies the resources available to the device (for example, the maximum size of the connection table). System B (mask version 07B0) is a new device model that has been defined specifically for the implementation of complex KNX devices. The main advantage lies in the number of available communication objects. While previous devices models were limited to 255 objects or less, System B theoretically permits up to 65,535 communication objects. To achieve this, the formats of the communication tables (group address, association and group object tables) have been redefined in the KNX specification for System B. System B devices can update their communication objects at system startup. This function is called Read-On-Init and can be activated individually for each object. Once the application is started the system software sends group read-value services independent from the application task. These services are scheduled by the stack to ensure that the bus is not excessively loaded at startup. System B also offers a greatly increased address space. The configuration data (application, parameters and tables) can be loaded into a range of up to 1 MB (20-bit addressing) via the bus (using memory services). To access system parameters, additional properties in the interface objects of the system have been introduced. System B is supported by the ETS manufacturer tool MT4, by ETS3 andETS4. Implementation for optimal performance Weinzierl Engineering as a KNX system supplier offers a new implementation for KNX System B, specifically targeted at complex devices with a 32-bit architecture like the Cortex M0 from NXP. It includes a complete implementation of the specification and is optimized to ensure high performance for all application sizes. A major consideration in the development of System B is the timely (real-time) processing of the large association table, which contains the assignment of group addresses to the communication objects and vice versa. It is loaded by ETS and is not sorted. For a table length of more than a thousand entries, linear search algorithms are not effective and therefore additional look-up tables have been introduced that allow quick access via indices. The processing of the communication objects has also been accelerated and a linear search through all objects is avoided with the use of additional buffers. Although these design features may require additional memory, they facilitate low CPU clock speeds. Higher performance is achieved at the same frequency with than with previous implementations with considerably reduced KNX resources. The System B implementation from Weinzierl Engineering uses a virtual address space that is resolved at the driver level and mapped to the corresponding physical storage areas. This means that applications are easily ported to different platforms. As for all Weinzierl's stack implementations, the focus is to ensure ease of application development. The application interface has been largely maintained and is accessible via comprehensive API functions. It is possible to implement either internal or external applications. An internal application is bundled together with the stack in the device and the ETS simply has to load the parameters and tables, which ensures quick download times. An external application is loaded by the ETS along with the parameters and tables. The stack also supports additional interface objects (user properties). These objects can be used, for example, to set device parameters using point-to-point communication on the bus. ETS parameters can also be realized with Properties. For the creation of the product data base with ETS MT4 (Manufacturer Tool) our bus monitor and KNX development tool Net'n Node has been extended with a new export function. After importing the data of the software project it directly generates an XML file that contains all the storage areas, load controls and binary application data. This XML file can be imported directly into the MT4 solution.
View full article
The documentation discusses how to generate phase-shift PWM signals based on SCTimer/PWM module, the code is developed based on MCUXpresso IDE version 10.3 and LPCXpresso5411x board. The LPC family has SCTimer/PWM module and CTimer modules, both of them can generate PWM signals, but only the SCTimer/PWM module  can generate phase-shift PWM signals. In the code, only the match registers are used to generate events, I/O signals are not used.  The match0 register is set up as (SystemCoreClock/100), which determines the PWM signal frequency. The the match1 register is set up as 0x00, which generate event1. The the match2 register is set up as (SystemCoreClock/100)/2;, which generate event2. The duty cycle is (SystemCoreClock/100)/2-0x00= (SystemCoreClock/100)/2, which is 50% duty cycle, the cycle time is (SystemCoreClock/100). The event1 sets the SCT0_OUT1, event2 clears the SCT0_OUT1, so SCT0_OUT1 has 50% duty cycle. The the match3 register is set up as (SystemCoreClock/100)/4;, which generate even3. The the match4 register is set up as 3*(SystemCoreClock/100)/4, which generate event4. The duty cycle is 3*(SystemCoreClock/100)/4  -  (SystemCoreClock/100)/4= (SystemCoreClock/100)/2, which is 50% duty cycle. The event3 sets the SCT0_OUT2, event4 clears the SCT0_OUT2, so SCT0_OUT2 has 50% duty cycle. The phase shift is (SystemCoreClock/100)/4 - 0x00= (SystemCoreClock/100)/4, which corresponds 90 degree phase shift. PWM initilization code: //The SCT0_OUT1 can output PWM signal with 50 duty cycle from PIO0_8 pin //The SCT_OUT2 can output PWM signal with 50 duty cycle fron PIO0_9 pin //The SCT0_OUT1 and SCT0_OUT2 PWM signal has 90 degree phase shift. void SCT0_PWM(void) {     SYSCON->AHBCLKCTRL[1]|=(1<<2); //SET SCT0 bit     SCT0->CONFIG = (1 << 0) | (1 << 17); // unified 32-bit timer, auto limit     SCT0->SCTMATCHREL[0] = SystemCoreClock/100; // match 0 @ 100 Hz = 10 msec     SCT0->EVENT[0].STATE = 0xFFFFFFFF; // event 0 happens in all states     //set event1     SCT0->SCTMATCHREL[1]=0x00;     SCT0->EVENT[1].STATE = 0xFFFFFFFF; // event 1 happens in all states     SCT0->EVENT[1].CTRL = (1 << 12)|(1<<0); // match 1 condition only     //set event2     SCT0->SCTMATCHREL[2]=(SystemCoreClock/100)/2;     SCT0->EVENT[2].STATE = 0xFFFFFFFF; // event 2 happens in all states     SCT0->EVENT[2].CTRL = (1 << 12)|(2<<0); // match 2 condition only     //set event3     SCT0->SCTMATCHREL[3]=(SystemCoreClock/100)/4;     SCT0->EVENT[3].STATE = 0xFFFFFFFF; // event 3 happens in all states     SCT0->EVENT[3].CTRL = (1 << 12)|(3<<0); // match 3 condition only     //set event4     SCT0->SCTMATCHREL[4]=3*(SystemCoreClock/100)/4;     SCT0->EVENT[4].STATE = 0xFFFFFFFF; // event 4 happens in all states     SCT0->EVENT[4].CTRL = (1 << 12)|(4<<0); // match 4 condition only     //PWM output1 signal     SCT0->OUT[1].SET = (1 << 1); // event 1 will set SCT1_OUT0     SCT0->OUT[1].CLR = (1 << 2); // event 2 will clear SCT1_OUT0     SCT0->RES |= (3 << 2); // output 0 toggles on conflict     //PWM output2 signal     SCT0->OUT[2].SET = (1 << 3); // event 3 will set SCT1_OUT0     SCT0->OUT[2].CLR = (1 << 4); // event 4 will clear SCT1_OUT0     SCT0->RES = (3 << 4); // output 0 toggles on conflict     //PWM start     SCT0->CTRL &= ~(1 << 2); // unhalt by clearing bit 2 of the CTRL } Pin initialization code: //PIO0_8 PIO0_8 FC2_RXD_SDA_MOSI SCT0_OUT1 CTIMER0_MAT3 //PIO0_9 PIO0_9 FC2_TXD_SCL_MISO SCT0_OUT2 CTIMER3_CAP0 - FC3_CTS_SDA_SSEL0 void SCTimerPinInit(void) {     //Enable the     SCTimer clock     SYSCON->AHBCLKCTRL[0]|=(1<<13); //set IOCON bit     //SCTimer pin assignment     IOCON->PIO[0][8]=0x182;     IOCON->PIO[0][9]=0x182;     IOCON->PIO[0][10]=0x182; } Main Code: #include <stdio.h> #include "board.h" #include "peripherals.h" #include "pin_mux.h" #include "clock_config.h" #include "LPC54114_cm4.h" void SCT0_Init(void); void SCTimerPinInit(void); void P1_9_GPIO(void); void SCT0_PWM(void); int main(void) {       /* Init board hardware. */     BOARD_InitBootPins();     BOARD_InitBootClocks();     BOARD_InitBootPeripherals();     printf("Hello World\n");    // SCT0_Init();    // P1_9_GPIO();     SCTimerPinInit();     SCT0_PWM();     /* Force the counter to be placed into memory. */     volatile static int i = 0 ;     /* Enter an infinite loop, just incrementing a counter. */     while(1) {         i++ ;     }     return 0 ; } The Yellow channel is PIO0_8 pin output signal, which is SCT0_OUT1 PWM output signal. The Bule channel is PIO0_9 pin output signal, which is SCT0_OUT2 PWM output signal.
View full article
        In recent years of MCU technology evolving, booting from the external flash seems to become more and more popular, actually, LPC already has employed this technology for many years.         NXP's recently released the LPC540xx family which continues the trend of high-performance flash-less MCU.         The developers may be a bit confused with the external FLASH which is used for storing the program, as they are used to directly using the internal FLASH for programming and debugging the chip. But, don't worry, let me introduce it in the following sections. LPC54018's three ways of loading program        In general, RAM stores data, however, RAM can also store programs. In previous projects, we occasionally move some key functions in RAM in order to improve the execution speed of these programs. The current implementation is to put all the programs in RAM more thoroughly. Based on this idea, you can directly use the debugger to load the executable image into the on-chip RAM and this method is called RAM TARGET.       After downloading the executable program image file to the external flash, when the bootloader loads the complete image to on-chip RAM to run, the method is called the Plain Load Image method.             Actually, both of these above ideas are routine, chip designers have also created a "super-capability" that allows the chip to directly execute external FLASH programs (Execute In Place, XIP). With this 'superpower', no matter whether the program boot from the external FLASH or the internal FLASH, there is no difference in operating performance.       The RAM TARGET method mentioned above is only suitable for debugging the application. Once the chip is powered off or reset, the downloaded program in the RAM will disappear. Meanwhile, the size of the RAM also give some restrictions for debugging.        In the Plain Load and XIP modes, the executable image file is stored in the external flash. After MCU is powered, the bootloader which is resided in ROM copies the first 512 bytes from the image (vector components and image header) into internal SRAMX at location 0x0000 0000 to validate the vector table and image header to confirm the booting mode. And the program will not be lost after power-off or reset. Fig1 illustrates the boot process of LPC54018. Fig1 LPC54018 boot process flow Experiment show         Board: LPCXpresso54018 board (OM40003) Fig1 LPCXpresso54018 board       Demo code: Hello world (From the SDK), modifying the hello world code in below way, which points out the load program way and date time. PRINTF("hello world. XXXXXXXX \r\n");    PRINTF("hello world, %s, %s.\r\n", __DATE__, __TIME__);‍‍‍‍‍‍‍‍‍‍‍‍ Experiment 1: RAM Target         Demo code: Hello world (From the SDK), modifying the hello world code in below way. PRINTF("hello world. RAM Target \r\n"); PRINTF("hello world, %s, %s.\r\n", __DATE__, __TIME__);‍‍‍‍‍‍‍‍‍‍      Note: Setting the Reset: Core when debugging the demo Fig2 Setting the Reset: Core Running testing: As the Fig3 illustrates, it would print the below message when debugging the demo, however, after reset, it would run the plain load image which is programmed before, as the RAM lost the hello world demo. Fig3 RAM Target runing testing Experiment 2: Plain Load Image        Demo code: Hello world (From the SDK), modifying the hello world code in below way. PRINTF("hello world. PLAIN LOAD IMAGE \r\n"); PRINTF("hello world, %s, %s.\r\n", __DATE__, __TIME__);‍‍‍‍‍‍‍‍‍‍‍‍‍      Download image to external flash:        1. Build the demo to generate a bin file.           This plainload example linked the vector table to 0x00000000, but program to external flash 0x10000000.        2. Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):             a. Open SEGGER J-FLASH Lite, select device LPC54018.             b. Click the 'Erase Chip' to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)                 Note: if can not success( press SW4 and reset the board, and try to erase again) Fig4 Erase the external flash              c. Select the bin data file, set the '.bin/Erase Start' address to 0x10000000, then click 'Program Device' Fig5 Program the external flash Running testing: Fig6 illustrates the result of  running the plain load image. Fig6 Plain load image runing testing Experiment 3: XIP Image        Demo code: Hello world qspi_xip (From the SDK), modifying the code in below way. PRINTF("hello world. PLAIN LOAD IMAGE \r\n"); PRINTF("hello world, %s, %s.\r\n", __DATE__, __TIME__);‍‍‍‍‍‍‍‍‍‍‍‍‍‍      Download image to external flash:        1. Build the demo to generate a bin file.        2. Program the bin file to external on board flash via SEGGER J-FLASH Lite(V6.22 or higher):            a. Open SEGGER J-FLASH Lite, select device LPC54018.            b. Click the 'Erase Chip' to erase the extrenal flash.(if can not success, press SW4 button and reset the board, and try to erase again)            Note: if can not success( press SW4 and reset the board, and try to erase again) Fig7 Erase the external flash           c. Select the bin data file, set the '.bin/Erase Start' address to 0x10000000, then click 'Program Device' Fig8 Program the external flash      Running testing:      Fig9 illustrates the result of  running the plain load image. Fig9 XIP image runing testing  
View full article
This document introduces how to debug TrustZone project on MCUXpresso IDE.   Use the latest version of MCUXpresso IDE v10.3.1. Project is from SDK_2.5.0_LPCXpresso55S69. Board is LPCXpresso55s69, use the LinkServer debug probe(on board debugger).   Every TrustZone based application consists of two independent parts - secure part/project and non-secure part/project. The secure project is stored in SDK_2.5.0_LPCXpresso55S69\boards\lpcxpresso55s69\trustzone_examples\<application_name>\ cm33_core0 \<application_name>_s directory. The non-secure project is stored in SDK_2.5.0_LPCXpresso55S69\boards\lpcxpresso55s69\ trustzone_examples\<application_name>\ cm33_core0 \<application_name>_ns directory. The secure projects always contains TrustZone configuration and it is executed after device RESET. The secure project usually ends by jump to non-secure application/project. In this document, we use “hello_world” as example, this project contains both “hello_world_s” and “hello_world_ns” projects. Unlike Keil or IAR IDE, MCUXpresso IDE can’t debug jump directly from secure project to no-secure project, so we need add the no-secure executable file to secure project debug configuration manually(For this version of MCUXpresso IDE v10.3.1, we need do this step, while for  the later new versions, maybe they support jump directly from secure project to no-secure project ). Steps outline: Import “hello_world_s” and “hello_world_ns” project. Build “hello_world_s” and “hello_world_ns”, without any error. Erase flash. Program no-secure project “hello_world_ns ”. Kill active debug. Add the location of file “lpcxpresso55s69_hello_world_ns.axf” to Debugger commands of “hello_world_s” project, and download “hello_world_s” project. After finish download, it stop at “hello_world_s” project, set a breakpoint at “hello_world_ns” project: Debug project Detailed steps please refer to DOC in attachment. Hope it helps, BR Alice
View full article
Continuously reducing the power consumption of integrated circuits is a constant topic in the development of integrated circuits. Reduced power consumption helps save power, extend standby time and reduce product heat, etc. Needless to say, low power consumption has become one of the important factors to measure product performance.   We usually recommend customers to refer MCUXpresso SDK power_mode_switch_lpc demo as low power design reference code. With this demo, customers can use serial terminal to control MCU to enter four low power consumption modes:Sleep mode,Deep Sleep mode,Power Down mode and deep power down mode. Meanwhile, user can also choose a variety of wake-up methods to wake up MCU through UART command.   However, when customers take use of power_mode_switch_lpc demo to measure lower power static characteristics, they find discrepancies with data sheet. Take example with LPCXpresso845MAX board. In power down mode, the demo board current reaches to around 100uA in debug mode. But data sheet states the typical current value is 1.5uA, no more than 10uA (see the Table below). Where is the problem? The purpose of the power_mode_switch_lpc demo is to demonstrate several low power modes and multiple wake-up methods to customers. We can’t get similar low power current value with default demo board as spec shows, but let's walk through a step-by-step demonstration and modify the routine to get the data sheet values.   LAB ENVIRONMENT: Demo Board: LPCXpresso845MAX SDK: SDK_2.11.0_LPCXpresso845MAX Demo Code: power_mode_switch_lpc IDE:MCUXpresso IDE v11.5.0   STEP: 1. Download power_mode_switch_lpc to LPC845 development board and run it. The serial port selects low power mode, press (SW2 button) to wake up. The program runs into power down mode, with debugger connected, the measured Idd is 99.5uA To enter low power mode, the following code is used: POWER_EnterPowerDown(DEMO_ACTIVE_IN_DEEPSLEEP); In order to wake up, parameter DEMO_ACTIVE_IN_DEEPSLEEP is configured with PDSLEEPCFG. BOD and watchdog oscillator power domains are turned on. All these setting results in potential current loss, causing power supply current higher than expectation.   2. In this step, we will remove wakeup initialization code // DEMO_InitWkt(); Replace this line of code //POWER_EnterPowerDown(DEMO_ACTIVE_IN_DEEPSLEEP); //enter power down mode with BOD and watchdog osc with POWER_EnterPowerDown(0); //power down BOD and watchdog osc   The modification is to turn off BOD power domain and watchdog clock in power down mode, compile and download the code again and enter the power down mode. At this time, the measured Idd is 57.3uA   In this way, Idd is significantly reduced. However, 57.3uA is still far from the typical value of 1.5uA stated in the data sheet. This is due to MCU debug power domain is turned on by IDE debugger, which leads to extra current consumption.  3. Thus we disconnect debugger and let the development board work in stand-alone mode (power off and re-power on). After power on, LPC is in power down mode. At this time, the measured Idd is 1.4uA. This is quite similar as the current value in datasheet. Consider GPIO configuration: The spec data shown in datasheet are tested under a dedicated test board with almost no external peripheral devices, and unused pins are basically in a floating state. For custom board or  LPCXpresso804 EVK. Some of its IO pins have external pull-up resistors and LEDs. If the GPIO is configured to output low power, the small light will be lit, resulting in additional power consumption. So we configure all pins as pull-up inputs for low power measurement.   Consider package: The test is based on LPCXpresso845MAX equipped LPC845 64pin package. It also applies to LPC845 48pin package. 33 package doesn't have VDDA pin. Due to VDD and VDDA pin design are not exactly the same as other package, for instance, 33pin low power consumption in power down mode is slightly higher than 64/48pin, but no more than 10uA as our spec in DS. Summary: Low power current parameters of the data sheet are measured with all MCU oscillators and analog domains off. Besides, reasonable configuration of GPIO can further reduce MCU power consumption. Before entering the low power consumption mode, it is recommended to set the unused GPIO as a pull-up input according to the actual situation (It can also be set to output low when the pin is floating). In applications with high requirements for low power consumption, users need to carefully optimize the code design to obtain the best low power consumption design.
View full article
This article introduces how to create a custom board MCUXpresso SDK and how to use it, mainly includes three parts: Part1: Generating a Board Support Configuration (.mex) Part2: Create a Custom Board SDK Using the Board SDK Wizard Part3. Using the Custom SDK to Create a New Project   Requirements: MCUXpresso IDE v11.1.1, MCUXpresso SDK for LPC845, LPC845-BRK board. This method works for all NXP mcu which support by MCUXpresso SDK. About detail steps, please refer to attachment. Thanks!
View full article
The example demos how to use ARM TX Event to trigger ADC based on LPC55S69-EVK board and MCUXPresso IDE and SDK. As the Table 753, the “ARM tx event” is the one of the ADC triggering source, although it is a hardware triggering, but the mechanism is the same as software triggering, after ADC configuration, you execute the instruction asm(“SEV”); the ARM tx event will be generated and trigger ADC to sample. The ADC of LPC55xx support hardware trigger mode, each hardware trigger source corresponds to a trigger register, as the Table 753, the ARM tx event ASC triggering source index is 11, so you have to initialize the ADC trigger control register TCTRL11. In the TCTRL11 register, you can assign the command ID, select the FIFO0 or FIFO1 to save the ADC result, enable hardware triggering.    
View full article
经常有客户在使用LPC55S69的过程中遇到读 Flash进入异常HardFault中断的现象。如果在Flash Mass Erase之后从未对Flash扇区进行过写操作,直接用指针通过AHB读Flash地址会导致程序跳入HardFault 中断而无法继续正常运行。 原因    刚出厂的LPC55Sxx FLASH处于全零的全擦除状态,没有设置ECC。当芯片通过LinkServer 和MCUXpresso IDE建立连接时,先擦除要下载代码用到的扇区,再把代码下载到对应位置,并对相应存储区的ECC值同时进行更新。代码以外的区域仍然是无ECC设置的擦除状态。 当LPC55Sxx 通过AHB总线直接读取Flash内存区域时(例如,mytemp = *(uint32_t*)0x4000)要对Flash ECC进行校验。这一指令对于读有效代码区是没有问题的, 因为这一区域的ECC在下载代码时早已设置好。但是一旦读取没有代码的扇区,由于没有检测到正确的ECC,导致Flash读取失败,并跳转到下图中的HardFault_Handler()异常中断:   我们在Sector Erase后通过AHB读取Flash内存内容,也会遇到同样的HardFault异常跳转,出问题的原因都是一样的。 解决方法 针对这一问题我们有如下两种解决方法: 先执行Flash写操作,再读取Flash 与Flash 擦除操作不同,执行Flash写操作后对应的ECC值也同步更新。这样,ECC校验通过后,通过下面的代码就可以对Flash直接进行AHB读取。 volatile uint32_t mytemp; …… mytemp = *(uint32_t*)0x1000;//read memory content 0x1000 to mytemp 请注意:0x1000必须是一个已经写过的地址。 如果Flash的某个扇区处于被擦除的状态,我们只需要在通过AHB总线读取内存区域之前对该区域执行写操作,这样ECC校验位更新正确后,就可以正常读Flash。 Flash的写操作可以参考MCUXpresso SDK自带的flashiap例程,函数FLASH_Program。   使用Flash控制指令读取Flash区内容 使用Flash控制指令进行读操作不会导致硬件错误(请参阅UM11126 “Command listing (CMD)”章节)。这是用户手册中推荐的读Flash正确打开方式。 请注意:CPU只有在频率低于100MHz时,才能进行Flash操作(读,写,擦除,校验,等等),当CPU频率超过100MHz时是不能实现上述操作的。 目前,官方没有提供上用控制指令读取Flash内容的例程,因此需要您根据下面步骤创建自己的读Flash程序。 开发环境: IDE: MCUXpresso IDE v11.1.0 SDK MCUXpresso SDK v2.7.0 步骤: 在MCUXpresso IDE中导入一个基础例程,如led_blinky 在下图所述选项中添加iap组件   选择iap1,点击OK   点击完OK之后,fsl_iap_ffr.h, fsl_iap.c, fsl_iap.h文件将自动添加到工程中   在source文件夹中添加附件中的memory.h和memory.c文件   4) 使用Flash 控制指令时,需要在源文件中添加memory.h, fsl_iap.h   5) 调用memory初始化和memory读取函数   6)调试,单步执行(step over)到memory_read(),查看结果  
View full article