Kinetisマイクロコントローラ・ナレッジ・ベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Microcontrollers Knowledge Base

ディスカッション

ソート順:
Hello Kinetis friends! The launch of new Kinetis devices and development tools called "Kinetis K2" brought some new K22_120 MHz devices to the K22 family portfolio. :smileyinfo: Please notice the name "Kinetis K2" only refers to the Kinetis generation, but it is not related to part number (e.g. K63/K64 are part of K2 generation). Previously existing Kinetis portfolio already had some K22_120 MHz devices, so this  caused confusion regarding the documentation, header files, features, development boards and others, because the part numbers are very similar. I created the next reference table outlining the existing K22_120 MHz parts with their corresponding files and boards. The last column is an overview of the features or peripherals that are either missing or added in each device. :smileyalert: IMPORTANT NOTES:           - I gathered and put together this information as reference, but it is not official. For the most accurate information please visit our webpage www.nxp.com.           - Header files MK22F12.h and MK22FA12.h apply for legacy K22_120 devices. However TWR-K21F120M(A) board has a K21_120 part, so use MK21F12.h or MK21FA12.h instead.      Colleague Carlos Chavez released an Engineering Bulletin (EB811) with good information related to this document:      http://cache.nxp.com/files/microcontrollers/doc/eng_bulletin/EB811.pdf Regards! Jorge Gonzalez
記事全体を表示
Test environment: FRDM-K64F Rev.D IAR ARM Workbench IDE V8.30.1 MCUXpresso SDK for FRDM-K64F v2.4.2(2018-08-02) Test project is [ftm_output_compare] located with default path: ..\FRDM-K64F\boards\frdmk64f\driver_examples\ftm\output_compare Test reason to verify the CnV register is updated on the next FTM counter change. Three test signals: FTM0_CH0 pin as output compare pin will generate square signal with 1.33KHz . FTM0_CH1 pin generate 24KHz Edge-Aligned PWM signal(High-true pulses (clear Output on match)) with 50% duty cycle as FTM counter monitor. When FTM counter change, the FTM0_CH1 will toggle to output high voltage. Test using a delay() function to emulate modify FTM0_CH0 output compare mode and CnV value periodically. There is a GPIO pin will toggle after each delay() function to detect/verify the CnV value actual load point. FlexTimer module setting: The FTM0 refer clock is 60MHz For the FTM0_CH1 pin generate 24KHz PWM signal, the FTM0 MOD value is fixed to 0x9C3 (60MHz/24KHz = 2500).   Below is the overall signals: Test Process Record: During FTM0 module initialization, set the FTM0_CH0 pin output compare value to 0xA00 (more than MOD register value (0x9C3)) with below code: Set the CnV value more than MOD register is to avoid the output compare be set during at start. After that,  enable FTM0 counter and toggle GPIO pin to set a mark: After delay, toggle GPIO pin and update CnV register to 0x270 (the match point is half of the PWM high voltage). The actual signal is : After the first CH0 output compare set match, before set CH0 pin clear on match. It need to keep the CH0 pin with same output compare mode and set CnV back to 0xA00 (more than MOD) again with below code: Then we set CH0 with clear on match mode and update CnV value to 0x752 (middle of CH1 PWM low voltage): The actual signal is: With the similar code, before next CH0 set on match, it need to keep the CH0 pin with same match compare mode setting and CnV change back to 0xA00 (more than MOD). The actual signal is below: Note: During the output compare signal compare mode set/clear change phase, it need to keep previous output compare mode setting, please don't using kFTM_NoOutputSignal setting at code. Otherwise, the output compare signal will exist decay: Test Result: From FTM0 register value, the FTM0_SYNCONF[SWRSTCNT] bit is clear, which means select Legacy PWM synchronization method. The legacy PWM synchronization method will update Output Compare mode CnV register value at the next FTM counter change. The actual signal also verify it. Below is FTM0 all registers value: For the more detailed info, please check the original thread at here. Please check attachment about test code.
記事全体を表示
The USB OTG module in Kinetis parts uses a Buffer Descriptor Table (BDT) in system memory to manage USB endpoint communications, the BDT is a a 512-byte buffer and there are 3 registers in USB module to contain the base address for it, and it must be 512-byte aligned otherwise there would be issue during transfer. In USB stack ver 4.1.1, some Kinetis old parts like K60N512, K20D72M have the demo project basked on CodeWarrior ARM compiler, and in khci_kinetis.c, bdt is defined as following: #define _BDT_RESERVED_SECTION_ #if(defined _BDT_RESERVED_SECTION_) #ifdef __CWCC__ #pragma define_section usb_bdt ".usb_bdt" RW __declspec(usb_bdt) uint_8_ptr bdt; but since the base address is defined as below: #define BDT_BASE               ((uint_32*)(bdt)) so the bdt definition is not correct , and we have to change it as below: #define _BDT_RESERVED_SECTION_ #if(defined _BDT_RESERVED_SECTION_) #ifdef __CWCC__ #pragma define_section usb_bdt ".usb_bdt" RW __declspec(usb_bdt) uint_8 bdt[512];//uint_8_ptr bdt; and the definition for usb_dbt section can be found in MK20X256_flash.lcf. with above modification, we can make the demo of "msd_mfs_generic" work well as expected. Please kindly refer to the following result got from TWR-K20D72M. FAT demo Waiting for USB mass storage to be attached... Mass Storage Device Attached ****************************************************************************** * FATfs DEMO * * Configuration:  LNF Enabled, Code page =1258 * ****************************************************************************** ****************************************************************************** * DRIVER OPERATION * ****************************************************************************** 1. Demo function: f_mount   Initializing logical drive 0...   Initialization complete ----------------------------------------------------------------------------- 2. Demo functions:f_getfree, f_opendir, f_readdir getting drive 0 attributes............... Logical drive 0 attributes: FAT type = FAT16 Bytes/Cluster = 2048 Number of FATs = 2 Root DIR entries = 512 Sectors/FAT = 250 Number of clusters = 63858 FAT start (lba) = 36 DIR start (lba,clustor) = 536 Data start (lba) = 568 ... 127716 KB total disk space. 127624 KB available. ----------------------------------------------------------------------------- ****************************************************************************** * DRECTORY OPERATION * ****************************************************************************** 1. Demo functions:f_opendir, f_readdir Directory listing...     ----A 2014/04/16 17:25     32253  tek00000.png     ----A 2014/04/16 17:34     31451  tek00001.png     ----A 2014/07/04 14:57     20549  tek00002.png     DR--- 2010/12/25 23:30         0 DIRECT~1     D---- 2010/01/01 00:00         0 DIRECT~2 3    File(s),     84253 bytes total 2    Dir(s) ----------------------------------------------------------------------------- 2. Demo functions:f_mkdir 2.0. Create <Directory_1> 2.1. Create <Directory_2> 2.2. Create <Sub1> as a sub directory of <Directory_1> 2.3. Directory list Directory listing...     ----A 2014/04/16 17:25     32253  tek00000.png     ----A 2014/04/16 17:34     31451  tek00001.png     ----A 2014/07/04 14:57     20549  tek00002.png     DR--- 2010/12/25 23:30         0 DIRECT~1     D---- 2010/01/01 00:00         0 DIRECT~2 3    File(s),     84253 bytes total 2    Dir(s) ----------------------------------------------------------------------------- 3. Demo functions:f_getcwd, f_chdir 3.0. Get the current directory     CWD: 0:/ 3.1. Change current directory to <Directory_1> 3.2. Directory listing Directory listing...     D---- 2010/01/01 00:00         0  .     D---- 2010/01/01 00:00         0  ..     D---- 2010/01/01 00:00         0  sub1 0    File(s),         0 bytes total 3    Dir(s) 3.3. Get the current directory     CWD: 0:/Directory_1 ----------------------------------------------------------------------------- 4. Demo functions:f_stat(File status), f_chmod, f_utime 4.1. Get directory information of <Directory_1>     DR--- 2010/12/25 23:30         0 Directory_1 4.2  Change the timestamp of Directory_1 to 12.25.2010: 23h 30' 20 4.3. Set Read Only Attribute to Directory_1 4.4. Get directory information (Directory_1)     DR--- 2010/12/25 23:30         0 Directory_1 ----------------------------------------------------------------------------- 5. Demo functions:f_rename Rename <sub1> to <sub1_renamed> and move it to <Directory_2> Directory listing...     D---- 2010/01/01 00:00         0  .     D---- 2010/01/01 00:00         0  ..     D---A 2010/01/01 00:00         0 SUB1_R~1 0    File(s),         0 bytes total 3    Dir(s) ----------------------------------------------------------------------------- 6. Demo functions:f_unlink Delete Directory_1/sub1_renamed Directory listing...     D---- 2010/01/01 00:00         0  .     D---- 2010/01/01 00:00         0  .. 0    File(s),         0 bytes total 2    Dir(s) ****************************************************************************** * FILE OPERATION * ****************************************************************************** 1. Demo functions:f_open,f_write, f_printf, f_putc, f_puts, fclose 1.0. Create new file <New_File_1> (f_open)     File size =    0 1.1. Write data to <New_File_1>(f_write) 1.2. Flush cached data     File size =   52 1.3. Write data to <New_File_1> (f_printf) 1.4. Flush cached data     File size =  103 1.5. Write data to <New_File_1> (f_puts) 1.6. Flush cached data     File size =  152 1.7. Write data to <New_File_1> uses f_putc function 1.8. Flush cached data     File size =  199 1.9. Close file <New_File_1> ----------------------------------------------------------------------------- 2. Demo functions:f_open,f_read, f_seek, f_gets, f_close 2.0. Open <New_File_1> to read (f_open) 2.1. Get a string from file (f_gets)     Line 1: Write data to  file uses f_write function 2.2. Get the rest of file content (f_read)     Line 2: Write data to file uses f_printf function Line 3: Write data to file uses f_puts function Line 4: Write data to file uses f_putc functionûöF¬ â•:7Rz}™ yzjw8¸×áÀ—»ÃЭ¹òÍ­ ä‹Hïk¨Wã½c'     ²7këÞÑ%VrC×»Ô¼ÒSÈÑèR+NjD¡¾òû>ú3‰SËþo^ÎI Pë±ñ‰þ/Directory_1[1] 2.3. Close file (f_close) ----------------------------------------------------------------------------- 3. Demo functions:f_stat, f_utime, f_chmod 3.1. Get  information of <New_File_1> file (f_stat)     ----A 2010/01/01 00:00       199  New_File_1.dat 3.2  Change the timestamp of Directory_1 to 12.25.2010: 23h 30' 20 (f_utime) 3.3. Set Read Only Attribute to <New_File_1> (f_chmod) 3.4. Get directory information of <New_File_1> (f_stat)     -R--A 2010/12/25 23:30       199  New_File_1.dat 3.5. Clear Read Only Attribute of <New_File_1> (f_chmod) 3.6. Get directory information of <New_File_1>     ----A 2010/12/25 23:30       199  New_File_1.dat ----------------------------------------------------------------------------- 4. Demo functions:f_ulink Rename <New_File_1.dat> to  <File_Renamed.txt> Directory listing...     D---- 2010/01/01 00:00         0  .     D---- 2010/01/01 00:00         0  ..     ----A 2010/12/25 23:30       199  FILE_R~1.TXT 1    File(s),       199 bytes total 2    Dir(s) ----------------------------------------------------------------------------- 5. Demo functions:f_truncate Truncate file <File_Renamed.txt> 5.0. Open <File_Renamed.txt> to write 5.1. Seek file pointer     Current file pointer:    0     File pointer after seeking:  102 5.2. Truncate file     File size =  102 5.3. Close file ----------------------------------------------------------------------------- 6. Demo functions:f_forward 6.0. Open <File_Renamed.txt> to read 6.1. Forward file to terminal Line 1: Write data to  file uses f_write function Line 2: Write data to file uses f_printf function 6.2. Close file ----------------------------------------------------------------------------- 7. Demo functions:f_ulink Delete <File_Renamed.txt> Directory listing...     D---- 2010/01/01 00:00         0  .     D---- 2010/01/01 00:00         0  .. 0    File(s),         0 bytes total 2    Dir(s) *------------------------------ DEMO COMPLETED    ------------------------ * ******************************************************************************
記事全体を表示
Since the mbed Ethernet library and interface for FRDM-K64 have not yet been fully tested, instead of using mbed we will use one of the latest demo codes from MQX specifically developed for the FRDM-K64 platform. Before starting please make sure you have the following files and software installed in your computer: CodeWarrior 10.6 (professional or evaluation edition) MQX 4.1 for FRDM-K64 (it is not necessary to install full MQX 4.1) JLink_OpenSDA_V2.bin (this is the debugger application) * If you don't have a valid license, you can find a temporary license below, it will only be valid until 7/30/2014 and it will only be available online until 7/05/2014. Building the project The first step to use an MQX project is to compile the target/IDE libraries for the specific platform: 1. Open CodeWarrior and drag the file from the following path C:\Freescale\Freescale_MQX_4_1_FRDMK64F\build\frdmk64f\cw10gcc onto your project area: This will load all the necessary libraries to build the project, once they are loaded build them it is necessary to modify a couple of paths on the BSP: 2. Right click on the BSP project and then click on properties 3. Once the properties are displayed, expand the C/C++ Build option, click on settings, on the right pane expand the ARM Ltd Windows GCC Assembler and select the directories folder, this will display all the libraries paths the compiler is using 4. Double click on the "C\Freescale\CW MCU v10.6\MCU\ProcessorExpert\lib\Kinetis\pdd_100331\inc" path to modify it, once the editor window is open, change the path from "pdd_100331" to "pdd" 5. Repeat steps 2 and 3 for the ARM Ltd Windows GCC Compiler 6. Now you can build the libraries, build them one at a time by right clicking on the library and selecting build project, build them in the following order, it is imperative you do it in that order. BSP PSP MFS RTCS SHELL USBD USBH 7. Once all the libraries are built, import the web hvac demo, do it by dragging the .project file to your project area; the project is located in the following directory:                     C:\Freescale\Freescale_MQX_4_1_FRDMK64F\demo\web_hvac\build\cw10gcc\web_hvac_frdmk64f 8. Once the project is loaded, build it by right clicking on the project folder and select Build project Debugging the project To debug the project it is necessary to update the FRDM-K64 debugging application: Press the reset button on the board and connect the USB cable Once the board enumerates as "BOOTLOADER" copy the JLink_OpenSDA_vs.bin file to the unit Disconnect and reconnect the board On CodeWarrior (having previously compiled the libraries and project) click on debug configurations 5. Select the connection and click on debug 6. Open HVAC.h and change the IP Address to 192.168.1.202 Now the demo code has been downloaded to the platform you will need the following to access all the demo features: Router Ethernet Cable Serial Terminal The code enables a shell access through the serial terminal, it also provides web server access with a series of options to simulate an Heating Air Conditioning Ventilation System, the system was implemented using MQX and a series of tasks, for more details on how the task are created, the information regarding how to modify the code please check the attached document: Freescale MQX RTOS Example guide.
記事全体を表示
In this document we are going to see how to use the attached code which implements the configuration of the FRDM-KL25 board as a USB HOST interfacing with a Numeric Keyboard and a 16x2 LCD. The project is compiled in the CodeWarrior IDE using Processor Expert and the Components to support the USB module of the USB Stack 4.1.1. How to add the Processor Expert USB components. The instructions to install the USB components to use them with Processor Expert are in the documentation of the USB Stack 4.1.1; here you can see the steps as well: Download the USB Stack 4.1.1 from the Freescale’s Website (USB Stack 4.1.1) Run the .exe file and install it in the default location. Open CodeWarrior and select Import Components in the Processor Expert button in menu bar. An Open windows will pop up, there you need to go to the path: <install folder>\Freescale USB Stack v4.1.1\ProcessorExpert\Components. To have the complete components and support for the USB module add each PEupd file repeating this step. Close CodeWarrior and open it again to ensure correct installation of the components. Check that the new components are available in the Components Library. About this Project. This project is based in the example code for Processor Expert in the USB Stack 4.1.1 USB_HID_MOUSE_HOST_MKL25Z128_PEx which implements the use of the FRDM-BOARD KL25 and a HID Mouse Device to interface with. In this project the HID Device is a Numeric Keyboard and the HOST Device (FRDM-KL25) is handling the data and printing them in a 16x2 LCD used in 8 bits mode (The LCDHTA component used here was created by Erich Styger; find the component an all the information about it here: http://mcuoneclipse.com/2012/12/22/hd44780-2x16-character-display-for-kinetis-and-freedom-board/ and say Thank you Erich: “Thank you Erich”). Here you can find a video of the implementation of this application: HID HOST WITH FRDM-KL25 The hardware components are: FRMD-KL25 Rev.E Adafruit Prototype Shield v.5 LCD JHD-162A Numeric USB Keyboard (Product Name: Numpad i110, Model No. GK-100010) USB _host Inside the project you can see there is a folder called USB_Host an it contains two important folders with source files: App_keyboard: Contains the specific function for the Keyboard configuration: in use, attached detached, callbacks and more; contain how to handle the data coming from the device. The function process_kdb_buffer is where the data is transmitted to the LCD and use it for the application. Classes: contain the necessary function to handle a hid as the device. Handle all the functions necessary for the USB protocol. Note: The usb_classes.c and usb_classes.h files are generated by processor expert. I attach these two files as well to have a reference how these files must look like. This is because sometimes during the code generation process Processor Expert erases part of the code. I hope this project is useful for you. Best Regards, Adrian.
記事全体を表示
Using five channels from FTM2 module of the KE02 microcontroller included on the FRDM-KE02Z board for controlling a robotic arm powered by five servomotors. Each servomotor is controlled by a couple of buttons of a matrix keyboard, which is connected to eigth GPIOs. Interrupts are not used in this example. The code was generated and compiled on CodeWarrior for Microcontrollers v10.5.
記事全体を表示
The SPI bus has the capability of addressing multiple slave devices by a single master. The Kinetis L series of devices feature either an 8-bit or 16-bit capable SPI module; however, there is only one dedicated CS/SS signal per instance of the module. Of course this signal is muxed to a few pin locations on the device. Unfortunately, there are not that many pins with the CS/SS muxing and they are most likely they are not near to each other physically. A solution to this issue is to use GPIO as CS/SS lines. This way you can take advantage of the SPI bus protocol and the Kinetis L series IOPORT interface (also known as FGPIO on Kinetis L). The Cortex-M0+ allows accesses to the IOPORT to occur in parallel with any instruction fetches; therefore, these accesses will complete in a single cycle. Core vs. SPI I'm sure many who have tried to use GPIO as CS/SS have written code similar to this pseudo code, I know I have: while(1) {      set_cs_low;      send_byte;      set_cs_high; } Logically this makes sense, but on an oscilloscope you will see the GPIO CS/SS line toggling at irregular intervals and out of sync with the SPI transfers. This is due to the nature of the 'send_byte' function or instruction. Simply transmitting a data packet will not prevent the core from waiting for the transmission to complete. The core will move on from writing data to the SPI data register, and execute the next instruction. If you have a core operating at 48 MHz and you are performing, at most depending on instance, 24 MHz SPI transfers the core will always move onto the next instruction before the data has left the module. The code must either implement a delay or wait for the transmission to complete. Incorporating an accurate delay can be tricky and can be interrupted by any interrupts occurring during the delay process. A more robust solution is to wait for the transmission to complete. However, there appears to be no Transmit Complete Flag (TCF) in the L-Series SPI module. The Solution Fortunately, there is a way to wait for transmit complete. Software must wait for the SPI read buffer full flag (SPRF) to be set in the SPI status register (SPIx_S) after writing data to the SPI data register (SPIx_D) . When the SPRF bit is set, software must read the SPIx_D. This procedure will ensure that the core does not move onto GPIO toggling, or other instructions, until the data has left the SPI module. The following function demonstrates how to write the above procedure in C using SPI0 and PTD0 as the CS/SS line: uint8_t SPI_send(uint8_t spiWrite) {     uint8_t spiRead;                        //Variable for storing SPI data     FGPIOD_PCOR |= (1 << 0);                //Toggle CS/SS line low     while(!(SPI0_S & SPI_S_SPTEF_MASK))     {         __asm("NOP");     }                                       //Wait for SPI transmit empty flag to set     SPI0_D = spiWrite;                            //Write data to SPI     while(!(SPI0_S & SPI_S_SPRF_MASK))     {         __asm("NOP");     }                                       //Wait for receive flag to set     spiRead = SPI0_D;                       //Read the SPI data register     FGPIOD_PSOR |= (1 << 0);                //Toggle CS/SS line high     return spiRead; } Please note that the GPIO CS/SS toggling need not be in the function. It should work just as well if the GPIO CS/SS toggles occur before and after the function is call, just remove the FGPIO instructions from the function and place them outside. I hope this document proves useful to those of you designing multiple slave SPI buses around Kinetis L series parts.
記事全体を表示
For Remote Control means, that is needed two computers - Server Computer and User Computer, which will be in connection. There are two types of connection, which can be used - HTTP or DCOM. There are two different ways how to set up the remote control in Windows. I made the tutorial, which describes both types of Remote Control. Ok - so, let´s start! HTTP Settings On the Server Computer side: 1. Plug the board to the Server Computer 2. Go to Remote Communication Server 3. Set HTTP connection and choose the right COM Port according the plugged board If the plugged board is on e.g. COM23, it is possible to edit number of Port in Device Manager On the User PC side: 1. Open FreeMASTER,  go to Project -> Options 2. Choose Plug-in Module: FreeMASTER CommPlugin for Remote Server (HTTP) and type the IP address of the server, do not forget join to IP address :8080 3. And start communication by STOP button to successful connection DCOM Settings On the Server Computer side: 1. Plug board to the Server Computer 2. Launch DCOM in FreeMASTER Remote Server Choose COM according plugged board or edit COM according to step 2 - Server Computer in HTTP Connection (up). 3. Setting permissions for the user, User PC. Right click on Computer -> Manage. In Computer Management click to Distributed COM Users. In Distributed COM Users Properties add the user, User Computer. After that, set the permissions in Component Services. In cmd type dcomcnfg.exe In Component Services go to Computers -> My Computer -> DCOM Config -> MCB FreeMASTER Remote Server Application Right click on MCB FreeMASTER Remote Server Application and go to Properties. In Security Tab is possible to add the permissions. There are 3 types of permissions. First permission - Launch and Activation Permissions. There are 4 permission options. Local Launch and Remote Launch means, that user, User Computer can launch e.g. FM Remote Server Application. But for success communication is needed allowing Local Activation and Remote Activation. Second permission - Access Permissions. Click to Edit and Allow Local Access and Remote Access for the user. Do not forget that if there is a change of permissions, specifically allowing, it is necessary for User to log out and log in. On the User Computer side: 1. Open Freemaster, go to Project -> Options 2. Choose Plug-in Module: FreeMASTER CommPlugin for Remote Server (DCOM) and for filling Connect string is possible to use Configure. Definitely, type the IP address of the server and ;Port Name. 3. And start communication by STOP button in FreeMASTER to successful connection And now.. you can do anything 🙂
記事全体を表示
Here you will find the code and project files corresponding to the I2C-Accelerometer project. The accelerometer/magnetometer is connected to the I2C port, although bot the accelerometer and magnetometer are contained within a single package, they must be initialized individually. In this example the measurements from both devices (X,Y and Z axis) is performed and displayed at the serial terminal. In order to compile the project, the following library must be imported: FXOS8700Q.h Code: #include "mbed.h" #include "FXOS8700Q.h" //I2C lines for FXOS8700Q accelerometer/magnetometer FXOS8700Q_acc acc( PTE25, PTE24, FXOS8700CQ_SLAVE_ADDR1); FXOS8700Q_mag mag( PTE25, PTE24, FXOS8700CQ_SLAVE_ADDR1); //Temrinal enable Serial pc(USBTX, USBRX); MotionSensorDataUnits mag_data; MotionSensorDataUnits acc_data; int main() {     float faX, faY, faZ;     float fmX, fmY, fmZ;     acc.enable();     printf("\r\n\nFXOS8700Q Who Am I= %X\r\n", acc.whoAmI());     while (true)     {         acc.getAxis(acc_data);         mag.getAxis(mag_data);         printf("FXOS8700Q ACC: X=%1.4f Y=%1.4f Z=%1.4f  ", acc_data.x, acc_data.y, acc_data.z);         printf("    MAG: X=%4.1f Y=%4.1f Z=%4.1f\r\n", mag_data.x, mag_data.y, mag_data.z);         acc.getX(&faX);         acc.getY(&faY);         acc.getZ(&faZ);         mag.getX(&fmX);         mag.getY(&fmY);         mag.getZ(&fmZ);         printf("FXOS8700Q ACC: X=%1.4f Y=%1.4f Z=%1.4f  ", faX, faY, faZ);         printf("    MAG: X=%4.1f Y=%4.1f Z=%4.1f\r\n", fmX, fmY, fmZ);                 wait(1.0);     } }
記事全体を表示
   CodeWarrior v10.6 and KDS are integrated development tools which are based on Eclipse, these two IDEs provide easy way to build project when using the GUI, but some engineers still want to build their projects from command line to do automated builds. This document provides examples on how to do it! Build project in CodeWarrior from command line: For a CW v10.6 created project, CW provides the “Make” tool and can also generate the needed “MakeFile” to build this project out of eclipse GUI. The below are the steps: Create and new project “k22_makefile” in CW v10.6, you will see there are two build configurations: RAM & FLASH Launch “cmd prompt” in Windows and go to “eclipse” folder of CW installation Now, you can generate the makefile for configuration FLASH by executing the below command ecd.exe –generateMakefiles –project “C:\workspace_cmd\k22_makefile” –config FLASH Now, checking the “FLASH” subfolder in project location, you will see “makefile” is generated. 4.To use “make” tool convenient, we can define an environment variable pointing to {CW}\gnu\bin where “make” is located. See command as below: 5. Go to the configuration folder “FLASH” where the project’s makefiles are located and run the follow commands to build the project. %MCU_BIN%\make.exe PS: to get more information of make and ecd, please just run the below command: Ecd.exe –help Make.exe –help Build project in KDS from command line: Compare with CodeWarrior, it is much easier to build an application in command mode. KDS provides a command “eclipse.exe” with which you can build a project with only two steps. In this example, I have created an application with name “cmd_ke02”, and the workspace path is “C:\wks_kdscmd”. To build the application in cmd, please first launch command mode in Windows system and then go to {KDS}\eclipse. Then, you need import the application into current workspace in the below command: eclipsec.exe -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "C:\wks_kdscmd" -import "C:\wks_kdscmd\cmd_ke02" then, build the project with the below command: eclipsec.exe -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "C:\wks_kdscmd" -build "cmd_ke02" For more details of building project from command line in KDS, please refer: http://mcuoneclipse.com/2014/09/12/building-projects-with-eclipse-from-the-command-line/
記事全体を表示
Welcome to the FRDM-K64 mbed workshop, in this page you will find all the code examples we will review on this session. The program covers the following modules: GPIO Serial communication Interrupts PWM ADC I2C (Accelerometer) USB Ethernet Depending on how fast we advance during the session some of the modules might be skipped; however here you can find both the source code and binary files ready to be flashed into the FRDM-K64 development board. FRDM-K64Z120M The FRDM-K64 is fully compatible with the Arduino rapid prototyping system, the following image depicts the board's pinout, the green labels can be used directly into your mbed proyects, they have already been defined in the headers and libraries in order to make development easier. Sign up at mbed.org In order to create the projects covered on this session it is necessary to create an mbed user account, open the website and create a user account, if you have already signed up please log in. Mbed debugging application To enable the FRDM-K64 development board using the binary files generated by mbed it is necessary to update the board's firmware, follow the steps mentioned below in order to enable the board to be programmed: Press the board's reset button While pressing the reset button connect the board to your computer using the USB cable, it must be connected to the J26 USB connector. Once the unit has enumerated as "Bootloader", copy the 20140530_k20dx128_k64f_if_mbed.bin file into the unit Disconnect and reconnect the USB cable, the board must enumerate as "MBED" Serial communication driver To implement serial communication you need to install the serial driver in your computer, download the driver, once your board has enumerated as MBED execute the driver and wait for it to be finished, this might take a couple of minutes. Serial terminal In order to communicate with the board via serial port it is necessary to use a serial terminal, by default WIndows 7 and 8 do not have this application, XP does. If your OS does not feature a serial terminal, you can download the one at the bottom (Teraterm). ! Your board is now ready to be programmed using mbed!
記事全体を表示
Hi team ,      I would like to share an experiment that about the Fast IO - zero wait state access of KL series . Detail please refer to attached file . Best regards, David
記事全体を表示
This is a Processor Expert project created by CodeWarrior for MCUs v10.6 which implements the charge-discharge time of a RC circuit for measuring capacitance. The charge-discharge sequence is performed by TPM0 operating in PWM mode, while the time is measured by TPM1 operating in Input Capture mode. A 100K ohm series resistor is being used, and the result is expressed on nF. It is also using the LCDHTA component from Erich Styger for showing the measurements on a 16x2 LCD, connected to the FRDM-KL05Z through a proto shield. The project is attached, and the pictures shows the measurements of three different capacitors: 10nF, 47nF and 1uF.
記事全体を表示
Hi All Kinetis Lovers, Microcontroller programming is a passion for all we are following this Community, but sometimes, trying to understand the peripherals of a Microcontroller is not an easy task, especially if we are in our first approach to a new module or device. In this post you will find a document that explains in detail the DMA module for Kinetis devices and also some examples for CodeWarrior and Kinetis Design Studio using DMA and other peripherals. The Documentation found here is: Using DMA module in Kinetis devices (complete): Document that includes DMA module explanation: everything you need to know when using DMA and the necessary information to understand the code included (K20_DMA for CW or K20D72_DMA for KDS). Using DMA module in Kinetis devices (example): Document that includes the necessary information to understand the code included (K20_DMA for CW or K20D72_DMA for KDS). Attached are two folders named: DMA examples for CW: include the DMA example projects for CW DMA examples for KDS: include the DMA example projects for KDS. Each folder includes 5 examples that are: Please feel free to modify the examples; I hope this will be useful for you. Many thanks and credits to manuelrodriguez for his valuable help developing and editing this project. :smileyinfo:For the SPI examples it is necessary to make a bridge between MOSI and MISO pins (master loop mode is used for the example). For this the TWR Elevators were used.     In the attachments you can find some extra information when using SPI and DMA. Best Regards, Adrian Sanchez Cano Technical Support Engineer
記事全体を表示
You can put the code directory in the SDK_2.6.0_FRDM-K64F\boards\frdmk64f to use. 1、Introduction As is known to all, we use debugger to download the program or debug the device. FRDMK64 have the opsenSDA interface on the board, so wo do not need other’s debugger. But if we want to design a board without debugger but can download the program, we can use the bootloader. The bootloader is a small program designed to update the program with the interface such as UART,I2C,SPI and so on. This document will describe a simple bootloader based on the FRDMK64F.The board uses SD card to update the application. User can put the binary file into the card. When the card insert to the board ,the board will update the application automatically. The bootloader code and application code are all provided so that you can test it on your own board.   2、Bootloader’s implementation   The schematic for SD card is shown below. The board uses SDHC module to communicate with SD card.                                                  Figure 1.Schematic for SD card   We use the 2.6.0 version of FRDM-K64F’s SDK.You can download the SDK in our website. The link is “mcuxpresso.nxp.com”. The bootloader uses SDHC and fafts file system. So we should add files to support it.                   Figure 2.The support file   In main code, the program will wait until the card has inserted. Then it will find the file named “a000.bin” in sd card to update the application. If the file do not exist, the board will directly execute the application. If there is no application, the program will end. The following code shows how the program wait for inserting sd card. It will also check if the address has the application’s address.                      Figure 3.The code -- wait for inserting card   The following code shows how the program opens the binary file. If sd card doesn’t have the file, the program will go to the application. Figure 4.Open the binary file   If the program opens the file normally, the update will begin. It will erase 200k’s space from 0xa000. You can adjust it according to your project. Now I will explain update’s method in detail. Our data is written to the buffer called “rBUff”. The buffer size is 4K. Before write data to it, it is cleared.  Please note that when we erase or program the flash, we should disable all interrupts and when the operations finish we should enable the interrupts.  The file size will decide which way to write the data to flash.  1、If the size < 4k ,we just read the file’s data to buffer and judge if its size aligned with 8 byte. If not , we increase the size of “readSize” to read more data in our data buffer called “rBuffer”. The more data we read is just 0.    2、If the size > 4K, we use “remainSize” to record how much data is left. We read 4k each time until its size is smaller than 4k and then repeat step 1. When finish the operation at a  time, we should clear the buffer and increase the sector numer to prepare the next transmission. Figure 5.Write flash operation code   The way to clear the space is shown in the figure. It will initialize the flash and erase the given size from the given address.  “SectorNum” is used to show which sector to erase. Figure 6.Erase operation code   The following figure shows how to write the data to flash.              Figure 7.Program operation code    Before we go to the application, we should modify the configuration we did in the bootloader.     Close the systick, clear its value.     Set the VTOR to default value.     Our bootloader runs in PEE mode. So we should change it to FEI mode.     Disable the all pins. You should disable the global interrupt when run these codes. And don’t forget to enable the global interrupt. Figure 8.Deinitalization code   Then we can go to the application. Figure 9.Go to Application   3、Memory relocation The FRDMK64 has the 1M flash, from 0x00000000 to 0x00100000.As shown in figure 10,we use the 0xa000 as the application’s start address.            Figure 10.The memory map   Now, I will show you how to modify the link file for user application in different IDE. In IAR                                    Figure 11.IAR’s ICF In MDK Figure 12.MDK’s SCF   In MCUXpresso Figure 13.MCUXpresso’s flash configuration 4、Run the demo 1) Download the bootloader first. 2) Prepare a user application program. We use the “led blinky” as an example. 3) Modify the Link file. 4) Generate the binary file with your IDE, please name it as “a000.bin”. 5) Put it into the sd card like figure 5. Figure 14.SD card’s content        6) Insert the card. And power on. Wait for a moment, the application will execute automatically. 5、Reference 1) Kinetis MCU的bootloader解决方案 2) KEA128_can_bootloader
記事全体を表示
Explore the Features of MCU-Link Pro MCU-Link Pro is the latest ARM Cortex-M series core debugger tool from NXP. Some of its features are inherited from the past LPC-LINK2. But overall it was redesigned and introduced and many new features. These additional functions make the MCU-Link Pro a very powerful debugging tool. This article will explore these features and highlight interesting and useful ones. These functions mainly include the following aspects. SWD+SWO Measurement of current and power consumption MCU-Link pro is supported by new blhost LIBUSBSIO library for windows, Ubuntu Linux and MacOS A secondary chip LPC804 on the board   SWD+SWO MCU-Link Pro support SWD only. It doesn’t support JTAG. The main controller in the board is LPC55S69. There is level shifter circuit between the port and LPC55S69. It makes the board can debug the target board work at 1.2V to 5V. It has reference voltage trace circuit which is use to trace the target board voltage. It can trace the port automatically, needn’t any settings. The MCU-Link Pro also can supply 1.8V/3.3V to target board. The maximum current is 350mA. This is done by connecting J6 and selecting by J5. The maximum speed of SWO is 9.6Mbit/s. Same as <PC-Link, MCU-Link Pro support CMSIS-DAP and Jlink firmware. These firmware are kept updating. The latest firmware of CMSIS-DAP is 2.25. If the firmware version is old, there will be a message jump out telling customer to update it when connecting to computer. We can see that the new version gives two VCOM while the original version only have one. The new VCOM use J26-4 and J26-5. jingpan_0-1664529871686.png   Measurement of current and power consumption MCU-Link pro provides a very interesting real-time function of current and voltage measurement. It can capture a burst of samples of target current usage, the target supply voltage, the shield current, the analog input, the debug interface reference voltage, or target power consumption at up to 100ksps. This information is displayed in a graph and can also be exported for further analysis. The average value of the collected data can also be displayed. And based on the current and voltage data, the power consumption can also be calculated and displayed in the graph. The place where the red line is drawn in the figure below is the real-time voltage at the time point of the mouse. jingpan_1-1664529871909.png     What's more interesting is that the energy measurement function does not need to activate the debug to capture the data, it is offline and has a separate data channel. But it can also be linked to a session if such a debug session exists. This is very useful in debugging various low-power applications. Not only can you see the power consumption change under each step of the command, but you can also check the power change rule for a long period of time when the system is running. Since there is a separate data channel, you can even debug the program in KEIL and watch the current change in MCUXpresso. The MCU Link Pro has two current measurement configurations, each with a maximum measurable current. This is to achieve maximum measurement accuracy for a variety of different objectives. There are two automatically controlled ranges in each configuration to provide greater precision. The automatic switching from low current measurement to high current measurement is completely controlled by hardware. jingpan_2-1664529871937.png   Each time the MCU Link Pro is powered up, the measurement circuit calibrates itself. There is no need to disconnect/reconnect the MCU Link Pro before calibration due to transistors are used to isolate the sensing circuit from the target power supply to avoid contention and to ensure a known voltage is applied to the system during calibration. At high sample rates, the MCUXpresso IDE may not capture all data, so the sample rate may need to be adjusted using the configuration options in the energy measurement configuration settings in the tool. If the target current exceeds the maximum current in the selected range, the measurement will saturate and cut off and will therefore be inaccurate. Blhost and MCU-Link Pro The most noteworthy feature of MCU Link Pro is its USB to SPI and I2C bridge functions. This enables the computer to send I2C and SPI signals directly through USB. This powerful function is not ignored by blhost. The new version of blhost can support this function and adds a new command parameter '- L'. Specifically, '- L SPI' refers to the SPI interface and '- L I2C' refers to the I2C interface. The following figure shows the test results on frdm-k64f. It can be clearly seen in the figure that the SPI interface of MCU Link Pro can communicate with mcuboot firmware on k64 and download the encryption program to flash. jingpan_3-1664529872017.png     In addition to KINETIS, this function is most suitable for i.mxrt600 and I mxRT500。 These two chips have serial ISP mode. User can download the program to ram through SPI or I2C port, and then directly let it run. Many users have this usage. In the previous examples in SDK, a board of twr-kv46 or twr-k65 or frdm-kl25 was required to receive command and data from UART and translate them to SPI and I2C command. Since there is no direct interface on these boards, flying wires are required, which is very troublesome. Moreover, NXP only provides firmware for these three boards. If you want to use other chips or boards, you must also transplant firmware. It's also very troublesome. But with MCU Link Pro, it's all very easy and pleasant.   LIBUSBSIO library In order to better expand the use of bridge functions, NXP has provided libusbsio library. By calling this library, you can realize the USB to SPI \ I2C \ GPIO function in your own application. I also made the upper computer tools for writing kinetis ezport and flash according to the libusbsio library provided by NXP. I introduced this point in detail in my last article. Interested friends can read my article. It is not enough to provide libraries based on windows and Linux. NXP also provides a python library. This library is based on python3 and can be installed through the following command >pip install libusbsio Its usage is not described in detail in the libusbsio documentation. Here is a general introduction. The following is an initialization procedure of libusbsio. import logging import logging.config from libusbsio import * # enable basic console logging logging.basicConfig() # load DLL from default directory sio = LIBUSBSIO(loglevel=logging.DEBUG) # the main code # calling GetNumPorts is mandatory as it also scans for all connected USBSIO devices numports = sio.GetNumPorts() print("SIO ports = %d" % numports) if numports > 0 and sio.Open(0): print("LIB version = '%s'" % sio.GetVersion()) print("SPI ports = %d" % sio.GetNumSPIPorts()) print("Max data size = %d" % sio.GetMaxDataSize()) if(sio.GetNumSPIPorts() > 0): spi = sio.SPI_Open(1000000, portNum=0, dataSize=8, preDelay=100) if spi: data, ret = spi.Transfer(spi_ssel[0], spi_ssel[1], b"Hello World") sio.Close() else: print("No USBSIO device found") ​ Line 9 is to open an instance of libusbsio library; Line 14: get the number of usbsio ports of all USB bridges; Lines 18, 19 and 20 are the read version information, the number of SPI ports and the maximum size of SPI cache; Line 22: open an SPI interface; Line 24, start transmitting data. It can be seen from the above that the use process is relatively simple. And these commands are very similar to those of the C language library.   A secondary controller LPC804 on the board There is also an lpc804 on the MCU Link Pro board. This chip is confusing here. What is it for? Its UART, SPI and I2C ports are all connected for external use. But what's the use? One conceivable application is that the UART port is connected to the newly added vcom2, and then the SPI or I2C works in the slave mode. As a listener, it monitors the SPI or I2C bus to be debugged and displays it on the computer terminal. The LPC804 debug interface is the same as the debugging port of MCU Link Pro. Maybe the board itself is a development board, so that users can develop lpc804 programs? In addition, its UART-ISP port is connected to a UART port of LPC55S69. It seems that in the future, it can communicate with each other through the new version of CMSIS-DAP firmware. Let's look forward to new ways of playing in the future.
記事全体を表示
  CNN on FRDM_K64 1 Introduction Limited by resources, ordinary MCU is difficult to do some complex deep learning. However, although it is difficult, it can still be done. CNN, convolutional neural network, is a kind of deep learning algorithm, which can be used to solve the classification task. After the implementation of CNN, ordinary MCU can also be used as edge computing device. Next, we introduce how to run CNN on frdm-k64 to recognize handwritten numbers. The size of digital image is 28x28. 28x28 image as input for CNN will output a 1x10 matrix. There are few deep learning libraries written for MCU on the Internet. Even if there are, there will be various problems. NNoM framework is easy to transplant and apply, so we use it     2 Experiment 2.1 Required tools: frdm-k64, python 3.7, Pip, IAR, tcp232   2.2 Download the source code of deep learning framework, https://github.com/majianjia/nnom This is a pure C framework that does not rely on hardware structure. Transplantation is very convenient   2.3  we select the example ‘bubble’ to add the Inc, port and Src folders in NNoM to the project, as shown in the figure nxf56274_0-1611022952076.png          Figure 1 Open the file ‘port.h’ . The definitation of NNOM_LOG is changed to PRINTF (__ VA_ ARGS__ ), Open the ICF file, and change the heap size to 0x5000, define symbol__ size_ heap__ = 0x5000; Malloc, which is used in this library, allocates memory from here. If it is small, it can't run the network   2.4 From the download framework, go into ‘mnist-simple/mcu’, which has trained file ‘weights.h’, and randomly generated handwritten image file, ‘image.h’. Add these two files to the project   2.5 Add headfile to ‘bubble.c’        #include "nnom_port.h" #include "nnom.h" #include "weights.h" #include "image.h"   2.6 Delete the original code, add the following code   nnom_model_t *model; const char codeLib[] = "@B%8&WM#*oahkbdpqwmZO0QLCJUYXzcvunxrjft/\\|()1{}[]?-_+~<>i!lI;:,\"^`'.   "; /*******************************************************************************  * Code  ******************************************************************************/ void print_img(int8_t * buf) {     for(int y = 0; y < 28; y++)        {         for (int x = 0; x < 28; x++)               {             int index =  69 / 127.0 * (127 - buf[y*28+x]);                      if(index > 69) index =69;                      if(index < 0) index = 0;             PRINTF("%c",codeLib[index]);                      PRINTF("%c",codeLib[index]);         }         PRINTF("\r\n");     } }   // Do simple test using image in "image.h" with model created previously. void mnist(char num) {        uint32_t predic_label;        float prob;        int32_t index = num;        PRINTF("\nprediction start.. \r\n");               // copy data and do prediction        memcpy(nnom_input_data, (int8_t*)&img[index][0], 784);        nnom_predict(model, &predic_label, &prob);          //print original image to console        print_img((int8_t*)&img[index][0]);               PRINTF("\r\nTruth label: %d\n", label[index]);        PRINTF("\r\nPredicted label: %d\n", predic_label);        PRINTF("\r\nProbability: %d%%\n", (int)(prob*100)); }   int main(void) {     uint8_t ch;     /* Board pin, clock, debug console init */     BOARD_InitPins();     BOARD_BootClockRUN();     BOARD_InitDebugConsole();     /* Print a note to terminal */     model = nnom_model_create();        // dummy run        model_run(model);     PRINTF("\r\nwhich image to distinguish? 0-9 \r\n");     for(uint8_t i=0; i<10; i++)     {         print_img((int8_t*)&img[i][0]);     }     while(1)     {         PRINTF("\r\nwhich image to distinguish? 0-9 \r\n");         ch = GETCHAR();         if((ch >'9') || ch < '0')         {             continue;         }         PRINTF("\r\n");         mnist(ch-'0');     } }   An error will be reported when compiling ‘weights.h’, due to lack of few parameters. In layer [1], layer [4], layer [7], you need to add ‘division (1,1)’ after ‘stride (1,1)’. In this way, the compilation passes.   2.7 As a result, open the serial port software. At the beginning, the terminal will print out a variety of handwritten digital pictures, and then enter a number, The corresponded picture will be recognized. nxf56274_1-1611022952200.png                                                    Figure 2 When we input ‘8’, the recognition is the handwriting '9' nxf56274_2-1611022952340.png                        Figure 3   The ‘Truth label’ corresponds to IMG9_LABLE in ‘image.h’ and ‘Predicted label’ is the prediction results   3 training Through the above steps, we have realized a simple handwritten numeral recognition. Next, we will introduce ‘weights.h’. How to generate the weight model here? The image data here are all from MNIST digital set. How can we make a handwritten number for MCU to recognize?   3.1 Under ‘nnom-master\examples\mnist-simple’, there is a ‘mnist_ simple.py’. You need to run it to generate ‘weights.h’ and ‘image.h’. To run this, you need to install tensorflow, keras and so on. When you run it, you can use pip to install what is missing The network operation process is as shown in the figure nxf56274_3-1611022952397.png                               Figure 4 Conv2d-> convolution operation, Maxpool-> pooling. The meaning of convolution operation is to extract the features of the image. Pooling is a bit like compressing data, which can reduce the running space. 28x28 input and output a 1x10 matrix, representing the possibility of 0-9   3.2 We can use the ‘Paint’ program of WIN to adjust the canvas to 28x28, write numbers on it and save it in PNG format. I wrote a ‘4’   nxf56274_4-1611022952398.png   Figure 5   Change the code as following.   nnom_model_t *model; uint8_t temp[28*28]={0}; const char codeLib[] = "@B%8&WM#*oahkbdpqwmZO0QLCJUYXzcvunxrjft/\\|()1{}[]?-_+~<>i!lI;:,\"^`'.   "; /*******************************************************************************  * Code  ******************************************************************************/ void print_img(int8_t * buf) {     for(int y = 0; y < 28; y++)        {         for (int x = 0; x < 28; x++)               {             int index =  69 / 127.0 * (127 - buf[y*28+x]);                      if(index > 69) index =69;                      if(index < 0) index = 0;             PRINTF("%c",codeLib[index]);                      PRINTF("%c",codeLib[index]);         }         PRINTF("\r\n");     } }     void mnist_pic(uint8_t *temp) {        float prob;     uint32_t predic_label;        PRINTF("\nprediction start.. \r\n");          // copy data and do prediction        memcpy(nnom_input_data, (int8_t*)temp, 784);        nnom_predict(model, &predic_label, &prob);          //print original image to console        print_img((int8_t *)temp);        PRINTF("\r\nPredicted label: %d\n", predic_label);        PRINTF("\r\nProbability: %d%%\n", (int)(prob*100)); }   int main(void) {     /* Board pin, clock, debug console init */     BOARD_InitPins();     BOARD_BootClockRUN();     BOARD_InitDebugConsole();     /* Print a note to terminal */     model = nnom_model_create();        // dummy run        model_run(model);     while(1)     {         PRINTF("\r\n Send picture by serial\r\n");            DbgConsole_ReadLine(temp,784);         PRINTF("\r\n Got picture\r\n");           mnist_pic(temp);     } }   3.3 Then use pic2mnist.py(see the attachment), run this script with CMD and enter 'Python pic2mnist.py 1. PNG ', 1. PNG is the image to be parsed, and then ‘content.txt’ will be generated. The file contains the data of the picture. Send the data to the MCU through the serial port. Note that ‘Send as Hex’ should be checked. Similarly, the handwritten picture will be displayed first, and then the picture will be recognized. nxf56274_5-1611022952440.png                                                           Figure 6   We can see that '4' was identified
記事全体を表示
Making and Downloading Security Image for Kinetis Device   Introduction KINETIS devices have Flash base bootloader or ROM bootloader. They have same structure and same download tools. MCUBOOT shows supported device. The bootloader not only support plaintext image, but also encrypted image which is encrypted by AES. This can protect user’s application code from unauthorized using. Due to different internal Flash structure, security image making, key download and image download flow is a bit different to each Kinetis devices. This hands-on will introduce Flash base bootloader and ROM base bootloader security image making and downloading.   2 Security image to Flash bootloader Many NXP Kinetis device SDK have integrated bootloader. Take FRDM-K64F as example, the bootloader project is in SDK_2.8.0_FRDM-K64F\boards\frdmk64f\bootloader_examples\freedom_bootloader The bootloader support security format image by default. User can download security format image via UART and USB interface. In K64 bootloader, the key is stored in 0xb000. But the application code is start from 0xa000. That means each time the application is upgraded, key file need to be download again.   2.1 Generate key The elftosb tool can generate a key. But of course, you can take any string as key. jingpan_0-1609396818676.png     2.2 Image encryption Use the key to encrypt application image. Here is the bd file. options {  flags = 0x4; // 0x8 encrypted + signed, 0x4 encrypted  buildNumber = 0x1;  productVersion = "1.00.00";  componentVersion = "1.00.00";  keyCount = 1; }   sources {  inputFile = extern(0);  sbkey = extern(1); }   section (0) {  erase 0xa000..0xF6000; load inputFile > 0xa000; }   jingpan_1-1609396818771.png     2.3 Download key and image Connect FRDM-K64F openSDA usb port. Then download key and image. jingpan_2-1609396819004.png     2.4 Download key with KinetisFlashTool Use keyboard to input key is really annoying. There is a GUI tool named KinetisFlashTool which can download image same as blhost.exe. To download encrypted image by this tool, we can make a sb file to download key first. Here is the bd file.   sources { } section (0) {        erase 0xb000..0xc000;        load {{E0BAA2C8231283CAF1D327CEDB82AFF9}} > 0xb000; }   Using elftosb to generate the sb file. The elftosb command line is as below \>Elftosb -V -c program_key.bd -o program_key.sb   This sb file should be download at first, then download the encrypted application image. When customer want to download security image via USB MSC or HID, this is the only way to download key. There is a limitation in those bootloader which version is lower or equal to v2.7.0. MSC function and HID function can’t be enabled together. Otherwise bootloader will fail when copy encrypted sb file to MSC disk.   2.5 About the key But it is really strange that key file should always come with encrypted file. It is reasonable to keep the key in secure status, for example, an untouched place in flash. K64 has a program once field which is located in program flash IFR. This is a standalone space different from main space. It’s address is from 0x3C0 to 0x3FF. MCU core can read or write this area by special flash command. We can put the AES key here. Again, we can use sb file to download this key. sources { } section (0) {        load ifr 0xE0BAA2C8 > 0x3c0;        load ifr 0x231283CA > 0x3c1;        load ifr 0xF1D327CE > 0x3c2;        load ifr 0xDB82AFF9 > 0x3c3; } Then we should modify sbloader_init() in sbloader.c. The source code only read key form 0xb000. We should have it read key from IFR.   Security image to ROM bootloader Some Kinetis device has ROM bootloader. They are different with flash base bootloader. This document use FRDM-K32L2A as example.   3.1 Generate AES key and download the key The key can be set as 0x112233445566778899aabbccddeeff00. Besides sb file, it can also be programmed to IFR by blhost command. \>blhost -p COM9 – flash-program-once 0x30 4 11223344 msb \>blhost -p COM9 – flash-program-once 0x31 4 55667788 msb \>blhost -p COM9 – flash-program-once 0x32 4 99aabbcc msb \>blhost -p COM9 – flash-program-once 0x33 4 ddeeff00 msb If you do not write anything to IFR, the ROM bootloader will use all-zero key. Here I use all-zero key.   3.2 Encryption algorithm The ROM bootloader hasn’t encryption algorithm. Application should include algorithm code and assign the address to bootloader, or preprogram BCA table and MMCAU code into flash. You can find MMCAU code (mmcau_cm0p.bin) and BCA(BCA_mmcau_cm0p.bin) table in MCUBoot2.0.0 package. Before you program these code into flash, new address must be written into it. For example, we put MMCAU code into 0x7f800, then we should modify the BCA table as below jingpan_3-1609396819033.png     And then, according this new address, modify the MMCAU_function_info structure in mmcau_cm0p.bin. jingpan_4-1609396819123.png   After that, download BCA to 0x3c0 and mmcau_cm0p.bin to 0x7f800. jingpan_5-1609396819231.png   In order to avoid using manual operation in production, above steps can be integrate in a single sb file.   3.3 Encrypt the image and download The bd file in K64 example can be reused, just need to change the image address to 0x00. jingpan_6-1609396819344.png   Press the reset button, after 5 second, the led will blink.   References: Kinetis Bootloader v2.0.0 Reference Manual Kinetis Elftosb User's Guide Kinetis Bootloader QuadSPI User's Guide Kinetis blhost User's Guide
記事全体を表示
  This document describes the different source clocks and the main modules that manage which clock source is used to derive the system clocks that exists on the Kinetis devices. It’s important to know the different clock sources available on our devices, modifying the default clock configuration may have different purposes since increasing the processor performance, achieving specific baud rates for serial communications, power saving, or simply getting a known base reference for a clock timer. The hardware used for this document is the following: Kinetis:  FRDM-K64F Keep in mind that the described hardware and management clock modules in this document are a general overview of the different platforms and the devices listed above are used as a reference example, some terms and hardware modules functionality may vary between devices of the same platform. For more detailed information about the device hardware modules, please refer to your specific device Reference Manual. Kinetis platforms The Kinetis devices have a main module called Multipurpose Clock Generator (MCG) this module controls which clock source is used to derive the system clocks. A high-level description diagram is shown below: javier_chavezq_0-1599155712645.pngFigure 1. Multipurpose Clock Generator External clock sources can provide a frequency signal as the System oscillator module or the RTC oscillator module, also the MCG module has internal clock generators that the System integration module (SIM) manages, the SIM module provides module-specific clock gating to allow granular shutoff of modules. For more detailed information about the SIM module, refer to “Chapter 12. System Integration Module(SIM)” from the K64 Sub-Family Reference Manual.  The following clock diagram shows all the multiplexers, dividers, and clock gates that can be controlled by the MCG, however, we will focus on the external and internal clock sources and the MCG outputs. image004.png Figure 2. Oscillators,  MCG and SIM modules At ‘MCGOUTCLK’ line, the primary clocks for the system are generated, the circuitry provides fixed clock dividers for the Core clock, Bus clock, FlexBus clock, and the Flash Clock. This allows for trade-offs between performance and power dissipation. It’s important to know that the MCG has 9 states of operation shown in the following figure.   javier_chavezq_2-1599155713462.png  Figure 3. MCG operation states In the previous image, the arrows indicate the permitted MCG state transitions, for example, if the current MCG state is BLPI(Bypassed Low Power Internal) and the desired state is BLPE(Bypassed Low Power External) the shortest and allowed path to follow is first switch to FBI(FLL Bypassed Internal) then to FBE(FLL Bypassed External), and finally to the BLPE MCG state. These switching mode restrictions exist due to certain MCG configuration bits that must be changed to properly move from one mode to another. For example, in the K64 family, the MCG state after a power-on reset is FEI(FLL Engaged Internal) mode, the MCGOUTCLK is derived from the FLL clock that is controlled by the 32kHz Internal Reference Clock (IRC), the following table shows the output frequency values for this specific MCG state. Source Frequency MCGOUTCLK 20.97MHZ Core/System clocks 20.97MHz Bus clock 10.48MHz FlexBus clock 6.99MHz Flash clock 4.19MHz Table 1. K64 default MCG configuration after reset: FEI (FLL Engaged Internal) The following image shows the blocks used for the FEI state using Clocks Tool from MCUXpresso IDE. javier_chavezq_3-1599155713559.pngFigure 4. View of FEI state from Clock Tools For more detailed information, refer to “Chapter 25. Multipurpose Clock Generator (MCG)” from the K64 Sub-Family Reference Manual.  External Clock Sources     System oscillator The System Oscillator module is a crystal oscillator. The module, in conjunction with an external crystal or resonator, generates a reference clock for the MCU.  Supports 32 kHz crystals (Low Range mode) and supports 3–8 MHz, 8–32 MHz crystals and resonators (High Range mode) For more detailed information, refer to Chapter 26. Oscillator(OSC) at K64 Sub-Family Reference Manual.   RTC oscillator The RTC oscillator module, in conjunction with an external crystal, generates a reference clock source of 1Hz and 32.768KHz, supports 32 kHz crystals with very low power. For more detailed information, refer to Chapter 27. RTC Oscillator(OSC32K) at K64 Sub-Family Reference Manual.   Internal Clock Sources    IRC oscillators Internal clock driven by the Fast Internal Reference (FIR) @4MHz or the Slow Internal Reference (SIR) @32kHz.  IRC internal oscillator Internal 48 MHz oscillator that can be used as a reference to the MCG and also may clock some on-chip modules. PLL Phase-locked loop circuit that in conjunction with an external clock source can achieve higher and stable frequencies.   FLL Frequency-locked loop circuit that in conjunction with an internal/external clock source provides module-specific clock and achieves higher frequencies. Modifying MCG state from FEI to FBI state If the current system clock does not fit with our timing requirements we can modify it by changing the state of the MCG module, in this case, if the user requires a lower system clock frequency @32.7KHz(Slow IRC) or @4MHz(Fast IRC) instead @21MHz(FLL Engaged Internal ‘FEI’ default state) and a low power option of the MCG module, the FLL Bypass Internal (FBI) state is an option to reach these requirements. 1.1 Configure MCG mode The FBI state allows us to use the Fast IRC together with its frequency divider achieving frequencies between 31.25KHz to 4MHz, for this example the final core clock is @2MHz. Follow the next steps to change to the FBI state and select a 2MHz clock using the Clock-Tools tool from MCUXpresso IDE.        At the MCUXpresso QuickStart Panel select MCUXpresso Config Tools >> Open Clocks javier_chavezq_4-1599155713991.pngFigure 5. Open Config Tools        At the left top of the screen select the MCG mode to “FBI(FLL Bypassed Internal)” javier_chavezq_5-1599155714080.pngFigure 6. Selection of MCG Mode        Select the frequency divider block(FCRDIV) right-click on it and select “Edit settings of: FCRDIV” javier_chavezq_6-1599155714206.pngFigure 7. FCRDIV block        Modify the divider value from 1 to 2. javier_chavezq_7-1599155714287.pngFigure 8. FCRDIV divider value        Finally, the next image shows how the MCG state and the new yellow paths get modified. The Core and system clocks are @2MHz. javier_chavezq_8-1599155714633.pngFigure 9. FBI MCG state @2MHz 1.2 Export clock configuration to the project After you complete the clock configuration, the Clock Tool will update the source code in clock_config.c and clock_config.h, including all the clock functional groups that we created with the tool. In the previous example, we configured the MCG state to FBI mode, this is translated to the following instructions in source code: “CLOCK_SetInternalRefClkConfig();” and “CLOCK_SetFbiMode();” javier_chavezq_9-1599155715228.png Figure 10. Source code view of FBI MCG configuration Another way to change the MCG state is by directly modifying the internal MCG registers. The blocks shown in the following image need to be modified to switch from the default FEI state to the FBI state. javier_chavezq_10-1599155715513.pngFigure 11. Blocks in FEI state to modify at MCG registers Note. MCG registers can only be written in supervisor mode. The ARM core runs in privileged(supervisor mode) out of reset, it is controlled by [nPRIV] bit in CONTROL core register. For more detailed information visit the Cortex-M4 ARM Documentation Reference Manual.        Internal Reference Source Multiplexor (IREFS), selects the reference source clock for the FLL.  1 is written to C1[IREFS]. The slow internal reference is selected.        PLL Select  Multiplexor(PLLS) Controls whether the PLL or FLL output is selected. 0 is written to C6[PLLS] The FLL output is selected as the MCG source, the PLL is disabled.        Clock Source Select Multiplexor(CLKS), selects the clock source for the MCGOUTCLK  line. 01 is written to C1[CLKS].  The internal reference clock is selected at the CLKS multiplexor.        Fast Clock Internal Reference Divider(FCRDIV), selects the Fast Internal Reference Clock divider, the resulting frequency can be in the range of 31.25KHz to 4MHz. 001 is written to SC[FCRDIV]. The dividing factor is 2 since the desired frequency is @2MHz and the source clock is @4MHz.        Internal Reference Clock Select (IRCS). Selects between the fast or slow internal reference clock source.  x is written to C2[IRCS]. Write 0 for Slow IRC or 1 for Fast IRC.        Finally, to enable the low power when neither the PLL nor FLL are used, a register in C2[LP] is modified. x is written to C2[LP]. Enable, or Disable the PLL & FLL in all the bypass modes.     This is translated to the following instructions in source code in “CLOCK_SetInternalRefClkConfig();” and “CLOCK_SetFbiMode();” functions: javier_chavezq_11-1599155716412.png Figure 12. Source code view of Internal MCG Registers Note. C1, C2, C6, and SC registers are part of the internal MCG control registers.  References K64 Sub-Family Reference Manual Also visit LPC's System Clocks   
記事全体を表示
      In the practical KE KEA usage, a lot of customers meet the watchdog can’t reset problems. Some customers find when they want to enable the watchdog, but can’t really enable the watchdog by set the EN bit in register WDOG_CS1; Some customers find when in debug mode, the EN bit WDOG_S1 register always be clear, but from the reference manual, this bit should be set after reset, even they check their code, and make sure they didn’t disable the watchdog;  There also have some customers find when they use the KEXX_DRIVERS_V1.2.1_DEVD code, and set the timeout value register by themselves, but the watchdog can’t reset in the timeout value. Now according to these problems, this document will analyze it and give the recommendation to avoid these problems.      From the above problem description, we can get that there actually mainly 2 reasons caused these problems: 1, software configuration; 2, debugger usage 1.  Software configuration   1) Start code disable the watchdog In the KE KEA sample code, after reset, the chip will enter in the start code at first, the start code always disable the watchdog at first, if the watchdog is disabled, the watchdog can’t be enable just by set the EN bit in register WDOG_CS1, because bit EN in register WDOG_CS1 is the write-once bit after reset. It only can be modified when the UPDATE bit is set and with 128 bus clocks after performing the unlock write sequence. Now how to find the disable code in the start code? Take KEXX_DRIVERS_V1.2.1_DEVD sample code as an example IAR: from crt0.s, will find the watchdog disable code WDOG_DisableWDOGEnableUpdate();  in the start function. The above IAR start picture is for KE, but in the KEA start file, you can’t see the start function in the KEA sample code which download from the freescale web, just find the __iar_program_start in cstartup_M_KEA128.s after the reset happens, but where is the __iar_program_start function, it can’t be searched in the whole project. Actually __iar_program_start is the default program entry function, it include the following function: You can find it will enter __low_level_init function, the watchdog disable code is just in  __low_level_init function. MDK:  From startup_MK0XZ4.s will find the watchdog disable code in the SystemInit function. Codewarrior: From __arm_start.c file, will find the watchdog disable code in __init_hardware function. 2) Codewarrior script init_kinetis.tcl disable the watchdog      To the Codewarrior, just comment the disable watchdog code in the __arm_start.c file is not enough to check the watchdog enable after reset, because in the codewarrior connect script init_kinetis.tcl, there also have the watchdog disable code.      If you want to find the state of EN bit in register WDOG_S1 after reset, you must disable all these watchdog disable code.   3) Timeout register configuration incorrect From the header file MKE02Z2.h, we can find the time out register define like this:   union {                                          /* offset: 0x4 */     __IO uint16_t TOVAL;                             /**< WDOG_TOVAL register., offset: 0x4 */     struct {                                         /* offset: 0x4 */       __IO uint8_t TOVALH;                             /**< Watchdog Timeout Value Register: High, offset: 0x4 */       __IO uint8_t TOVALL;                             /**< Watchdog Timeout Value Register: Low, offset: 0x5 */     } TOVAL8B; This structure means that customer can define the watchdog timeout value by separated unit8 TOVALH, TOVALL or just defined it with unint16 TOVAL. But actually in the IAR project usage, take an example, use 1khz as the clock source for watchdog, then want to set the timeout value as 1s, it means the timeout value should be 1000=0x03e8, so one of the customers configure it like this:    You can find, we need the TOVALL= 0XE8, TOVALH=0X03, but from the test result, the register is TOVALL= 0X03, TOVALH=0Xe8, this will cause the timeout value is much larger than 1000, that is why customer can’t reset the mcu after 1s, because the register configuration is not correct. It is caused by the IAR int16 store endian mode, the default IAR endian mode is little endian mode. So in the practical usage, it is recommended to use the separated time out value definition. 2. debugger usage When in debug mode with IDE, some customers find even they comment all the watchdog disable code, they still can’t reset the MCU by the watchdog. After check the register WDOG_S1, bit EN is 0, it means the watchdog is disabled. But from the reference manual, we get that after reset, the EN bit should be 1. What caused this? After test, we find this actually caused by the debugger, the debugger hardware which you are using. Eg, in the same project which already comment all the watchdog disable code, SEGGER JLINK will still disable the watchdog, but the PE opensda or PE multilink won’t do this, the EN bit is enabled by default, the following is the test picture, take codewarrior as an example: 1) JLINK 2) PE Opensda or PE multilink    So, if you want to test the watchdog in debug mode, and want the EN is set after reset, you can choose PE debugger tool instead of JLINK, but this JLINK feature is just influence the debug mode, after you download the code to the chip flash, and after reset, the EN bit in WDOG_S1 will still be set. Wish this document will help you get out the problem of watchdog can’t be reset.
記事全体を表示