Kinetisマイクロコントローラ・ナレッジ・ベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Microcontrollers Knowledge Base

ディスカッション

ソート順:
OpenSDA/OpenSDAv2 is a serial and debug adapter that is built into several Freescale evaluation boards. It provides a bridge between your computer (or other USB host) and the embedded target processor, which can be used for debugging, flash programming, and serial communication, all over a simple USB cable.   The OpenSDA hardware consists of a circuit featuring a Freescale Kinetis K20 microcontroller (MCU) with an integrated USB controller. On the software side, it implements a mass storage device bootloader which offers a quick and easy way to load OpenSDA applications such as flash programmers, run-control debug interfaces, serial to USB converters, and more. Details on OpenSDA can be found in the OpenSDA User Guide.     The bootloader and app firmware that lay on top of the original OpenSDA circuit was proprietary.  But recently ARM decided to open source their CMSIS-DAP interface, and now a truly open debug platform could be created. This new open-sourced firmware solution is known as OpenSDAv2.   OpenSDAv2: OpenSDAv2 uses the exact same hardware circuit as the original OpenSDA solution, and out of the box it still provides a debugger, drag-and-drop flash programmer, and virtual serial port over a single USB cable.   The difference is the firmware implementation: OpenSDA: Programmed with the proprietary P&E Micro developed bootloader. P&E Micro is the default debug interface app. OpenSDAv2: Programmed with the open-sourced CMSIS-DAP/mbed bootloader. CMSIS-DAP is the default debug interface app.       Firmware Developer Kinetis K20 Based Hardware Circuit Default Debug Interface Drag-and-drop Target MCU Flash Programming Virtual Serial Port Source Code Available OpenSDA P&E Micro x P&E Micro .srec/.s19 x   OpenSDAv2 ARM/mbed.org x CMSIS-DAP .bin x x   The bootloader and app firmware used by OpenSDAv2 is developed by the community at mbed.org, and is known as “CMSIS-DAP Interface Firmware”. If you explore that site, you will find that this firmware was also ported to run on other hardware, but the combination of this mbed.org firmware with the Kinetis K20 MCU is known as OpenSDAv2.   It is important to understand however that it is possible to run a P&E Micro debug app on the CMSIS-DAP/mbed bootloader found on OpenSDAv2. Likewise it is possible to run a CMSIS-DAP debug app on the P&E Micro bootloader found on OpenSDA. The debug application used needs to be targeted towards a specific bootloader though, as a single binary cannot be used on both the OpenSDA and OpenSDAv2 bootloaders.   OpenSDAv2.1: During development of OpenSDAv2 features and bug fixes, it was found that the reserved bootloader space was too small. Thus a new version of OpenSDAv2 had to be created, which was named OpenSDAv2.1. The difference between the OpenSDAv2.0 and v2.1 is the address where the debug application starts: for OpenSDAv2.0 it expects the application at address 0x5000, while OpenSDAv2.1 expects the application to start at address 0x8000.   The only board with OpenSDAv2.0 is the FRDM-K64F. All other OpenSDAv2 boards (such as the just released FRDM-K22F) use OpenSDAv2.1.   Unfortunately this means that new OpenSDAv2 apps are needed. From a user perspective this mostly affects the JLink app since it was shared across all boards. Make sure you download the correct app for your board based on the OpenSDAv2 version.   OpenSDAv2 Apps: mbed CMSIS-DAP for FRDM-K64F mbed CMSIS-DAP for FRDM-K22F P&E Micro  (use the Firmware Apps link) Segger JLink (look at bottom of page for OpenSDAv2.0 or OpenSDAv2.1 app)   OpenSDAv2 Bootloader: The key difference between OpenSDA and OpenSDAv2 is the bootloader. Boards with OpenSDA use a proprietary bootloader developed by P&E Micro, and it cannot be erased or reprogrammed by an external debugger due to the security restrictions in the firmware. Boards with OpenSDAv2 use the open-source bootloader developed by mbed.org, and it can be erased and reprogrammed with an external debugger.   Apps need to be specifically created to work with either the P&E bootloader (Original OpenSDA) or the CMSIS-DAP/mbed bootloader (OpenSDAv2/OpenSDAv2.1) as the bootloader memory map is different.  Thus it’s important to know which type of bootloader is on your board to determine which version of an app to load.   You can determine the bootloader version by holding the reset button while plugging in a USB cable into the OpenSDA USB port. A BOOTLOADER drive will appear for both OpenSDA and OpenSDAv2.   The OpenSDAv2.0 bootloader (may also be called the CMSIS-DAP/mbed bootloader) developed by mbed.org will have the following files inside.  Viewing the HTML source of the bootload.htm file with Notepad will tell you the build version, date, and git hash commit. For the OpenSDAv2.1 bootloader, this file will be named mbed.htm instead.     The OpenSDAv1 bootloader developed by P&E Micro will have the following inside. Clicking on SDA_INFO.HTM will take you to the P&E website.       Using CMSIS-DAP: When you connect a Freedom board that has OpenSDAv2 (such as the FRDM-K64F) to your computer with a USB cable, it will begin running the default CMSIS_DAP/mbed application which has three main features.   1. Drag and Drop MSD Flash Programming You will see a new disk drive appear labeled “MBED”.   You can then drag-and-drop binary (.bin) files onto the virtual hard disk to program the internal flash of the target MCU.   2.Virtual Serial Port OpenSDAv2 will also enumerate as a virtual serial port, which you can use a terminal program , such as TeraTerm (shown below), to connect to. You may need to install the mbed Windows serial port driver first before the serial port will enumerate on Windows properly. It should work without a driver for MacOS and Linux.   3. Debugging The CMSIS-DAP app also allows you to debug the target MCU via the CMSIS-DAP interface. Select the CMSIS-DAP interface in your IDE of choice, and inside the CMSIS-DAP options select the Single Wire Debug (SWD) option:   Kinetis Design Studio (KDS): Note: OpenOCD with CMSIS-DAP for FRDM-K22F is not supported in KDS V1.1.0. You must use either the P&E app instructions or the JLink app instructions to use KDS with the FRDM-K22F at this time. This will be fixed over the next few weeks. OpenSDAv2 uses the OpenOCD debug interface which uses the CMSIS-DAP protocol. Make sure '-f kinetis.cfg' is specified as 'Other Options':   IAR     Keil:         Resources CMSIS-DAP Interface Firmware mbed.org FRDM-K64 Page FRDM-K64 User Guide OpenSDAv2 on MCU on Eclipse blog OpenSDA User Guide KDS Debugging   Appendix A: Building the CMSIS-DAP Debug Application The open source CMSIS-DAP Interface Firmware app is the default app used on boards with OpenSDAv2. It provides: Debugging via the CMSIS-DAP interface Drag-and-drop flash programming Virtual Serial Port providing USB-to-Serial convertor   While binaries of this app are provided for supported boards, some developers would like to build the CMSIS-DAP debug application themselves.   This debug application can be built for either the OpenSDAv2/mbed bootloader, or for the original OpenSDA bootloader developed by P&E Micro. If you are not sure which bootloader your board has, refer to the bootloader section in this document.   Building the CMSIS-DAP debug application requires Keil MDK. You will also need to have the “Legacy Support for Cortex-M Devices” software pack installed for Keil.   You will also need Python 2.x installed. Due to the python script used, Python 3.x will not work.   The code is found in the MBED git repository, so it can be downloaded using a git clone command: “git clone https://github.com/mbedmicro/CMSIS-DAP.git” Note that there is a Download Zip option, but you will run into a issue when trying to compile that version, so you must download it via git instead.   The source code can be seen below:   This repository contains the files for both the bootloader and the CMSIS-DAP debug interface application. We will concentrate on the interface application at the moment.   Open up Keil MDK, and open up the project file located at \CMSIS-DAP\interface\mdk\k20dx128\k20dx128_interface.uvproj In the project configuration drop-down box, you will notice there are a lot of options. Since different chips may have slightly different flash programming algorithms, there is a target for each specific evaluation board. In this case, we will be building for the FRDM-K64F board. Scroll down until you get to that selection:   Notice there are three options for the K64: k20dx128_k64f_if: Used for debugging the CMSIS-DAP application with Keil. Code starts at address 0x0000_0000 k20dx128_k64_if_openSDA_bootloader: Creates a binary to drag-and-drop on the P&E developed bootloader (Original OpenSDA) k20dx128_k64_if_mbed_bootloader: Creates a binary to drag-and-drop onto the CMSIS-DAP/mbed developed bootloader (OpenSDAv2)   Since the FRDM-K64F comes with the OpenSDAv2 bootloader, we will use the 3 rd option. If we were building the mbed app for another Freedom board which had the original OpenSDA bootloader, we would choose the 2 nd option instead.   Now click on the compile icon. You may get some errors If you get an error similar to the one shown below, make sure you have installed the Legacy pack for ARM as previously described earlier:           compiling RTX_Config.c...             ..\..\Common\src\RTX_Config.c(184): error:  #5: cannot open source input file "RTX_lib.c": No such file or directory            and           compiling usb_config.c...             ..\..\..\shared\USBStack\INC\usb_lib.c(18): error:  #5: cannot open source input file "..\..\RL\USB\INC\usb.h": No such file or directory   If you get an error regarding a missing version_git.h file, make sure that Python 2.x and git are in your path. A Python build script fetches that file. It's called from the User tab in the project options, under "Run User Programs Before Build/Rebuild". If there is a warning about “invalid syntax” when running the Python script, make sure your using Python 2.x. Python 3.x will not work with the build script.   Now recompile again, and it should successfully compile. If you look now in \CMSIS-DAP\interface\mdk\k20dx128 you will see a new k20dx128_k64f_if_mbed.bin file   If you compiled the project for the OpenSDA bootloader, there would be a new k20dx128_k64f_if_openSDA.S19 file instead.   Loading the CMSIS-DAP Debug Application: Now take the Freedom board, press and hold the reset button as you plug in the USB cable. Then, drag-and-drop the .bin file (for OpenSDAv2) or .S19 file (for OpenSDA) into the BOOTLOADER drive that enumerated.   Perform a power cycle, and you should see a drive called “MBED” come up and you can start using the CMSIS-DAP debug interface, as well as drag-and-drop programming and virtual serial port as described earlier in this document.   Appendix B: Building the CMSIS-DAP Bootloader All Freedom boards already come with a bootloader pre-flashed onto the K20.  But for those building their own boards that would like to use CMSIS-DAP, or those who would like to tinker with the bootloader, it possible to flash it to the Kinetis K20 device. Flashing the bootloader will require an external debugger, such as the Keil ULink programmer or Segger JLink.   Also note that the OpenSDA/PE Micro Bootloader cannot be erased! Due to the proprietary nature of the P&E firmware used by the original OpenSDA, it can only be programmed at the board manufacturer and JTAG is disabled. So these instructions are applicable for boards with OpenSDAv2 only.   First, open up the bootloader project which is located at \CMSIS-DAP\bootloader\mdk\k20dx128\k20dx128_bootloader.uvproj   There is only one target available because all OpenSDAv2 boards will use the same bootloader firmware as the hardware circuitry is the same.   Click on the compile icon and it should compile successfully. If you see errors about a missing version_git.h file, note that Python 2.x must be in the path to run a pre-build script which fetches that file.   Now connect a Keil ULink to J10 and then insert a USB cable to provide power to J26. Note that if you have the 20-pin connector, you’ll want to use the first 10 pins.   Then for Keil 5 you will need to change some debug options (CMSIS-DAP is built under Keil 4.x).   Right click on the bootloader project, and go to the Debug tab and next to ULINK Pro Cortex Debugger, click on Settings:   Then under “Cortex-M Target Driver Setup”, change the “Connect” drop down box to “under Reset” and “Reset” dropdown box to “HW RESET”. Hit OK to save the settings.     Then in Keil, click on Flash->Erase.   And then on Flash->Download.   If you get an “Invalid ROM Table” error when flashing the CMSIS-DAP bootloader, make sure you made the changes to the debugger settings listed above.   After some text scrolls by, you should see:   Now power cycle while holding down the reset button, and you should see the bootloader drive come up. You’ll then need to drag and drop the mbed application built earlier onto it. And that’s all there is to it!   The binaries for the bootloader and CMSIS-DAP debug app for the FRDM-K64F board created in writing this guide are attached. Original Attachment has been moved to: k20dx128_bootloader.axf.zip Original Attachment has been moved to: k20dx128_k64f_mbed.bin.zip
記事全体を表示
Hi All Kinetis Lovers, Microcontroller programming is a passion for all we are following this Community, but sometimes, trying to understand the peripherals of a Microcontroller is not an easy task, especially if we are in our first approach to a new module or device. In this post you will find a document that explains in detail the DMA module for Kinetis devices and also some examples for CodeWarrior and Kinetis Design Studio using DMA and other peripherals. The Documentation found here is: Using DMA module in Kinetis devices (complete): Document that includes DMA module explanation: everything you need to know when using DMA and the necessary information to understand the code included (K20_DMA for CW or K20D72_DMA for KDS). Using DMA module in Kinetis devices (example): Document that includes the necessary information to understand the code included (K20_DMA for CW or K20D72_DMA for KDS). Attached are two folders named: DMA examples for CW: include the DMA example projects for CW DMA examples for KDS: include the DMA example projects for KDS. Each folder includes 5 examples that are: Please feel free to modify the examples; I hope this will be useful for you. Many thanks and credits to manuelrodriguez for his valuable help developing and editing this project. :smileyinfo:For the SPI examples it is necessary to make a bridge between MOSI and MISO pins (master loop mode is used for the example). For this the TWR Elevators were used.     In the attachments you can find some extra information when using SPI and DMA. Best Regards, Adrian Sanchez Cano Technical Support Engineer
記事全体を表示
Hello Kinetis community. Attached there is a guide on how to modify an existing KDS project to be loaded using the KBOOT Flash Resident bootloader. Basically it explains 2 procedures: 1- Manipulating linker file to move application and vectors. 2- Adding data for the Bootloader Configuration Area (BCA). I am also including 3 adapted KDS v3.0.0 example projects ready to be used with KBOOT Flash Resident bootloader in a FRDM-K22F: - Baremetal project. - KSDK project. - KSDK project with Processor Expert support. The application simply toggles the red, green and blue LEDs sequentially. I hope you find the document and projects useful! Regards! Jorge Gonzalez
記事全体を表示
Hi community!! The following example uses a PIT to start an adc conversion, once the conversion has finished it issues a DMA request and the DMA controller stores the converted value in a buffer. The examples were implemented in both CodeWarrior 10.6 and KDS 1.1 for every board. The recommended test circuit is the following: Please feel free to modify the files, I hope this examples will be useful for you and will help you by decreasing your development time. Best Regards Manuel Rodríguez Technical Information Center Intern
記事全体を表示
Revise History: Version 23: NXP kinetis bootloader GUI upgrade from v1.0 to v1.1: added 04 extended linear address record  and 02 sector address record processing for hex format. This article describes how to do in-system reprogramming of Kinetis devices using standard communication media such as SCI. Most of the codes are written in C so that make it easy to migrate to other MCUs. The solution has been already adopted by customers. The pdf document is based on FRDM-KL26 demo board and Codewarrior 10.6.  The bootloader and user application source codes are provided. GUI and video show are also provided. Now the bootloader source code is ported to KDS3.0, Keil5.15 and IAR7.40 which are also enclosed in the SW package. Customer can make their own bootloader applications based on them. The application can be used to upgrade single target board and multi boards connected through networks such as RS485. The bootloader application checks the availability of the nodes between the input address range, and upgrades firmware nodes one by one automatically. ​ Key features of the bootloader: Able to update (or just verify) either single or multiple devices in a network. Application code and bootloader code are in separated projects, convenient for mass production and firmware upgrading. Bootloader code size is small, only around 2K, which reduces the requirement of on chip memory resources. Source code available, easy for reading and migrating. GUI supports S19,HEX and BIN format burning images. For more information, please see attached document and code. The attached demo code is for KL26 which is Cortex - M0+ core. For Cortex-M4 core demo, refer this url: https://community.freescale.com/docs/DOC-328365 User can also download the document and source code from Github: https://github.com/jenniezhjun/Kinetis-Bootloader.git Thanks for the great support from Chaohui Guo and his team. NOTE: The bootloader and GUI code are all open source, users can revise them based on your own requirement. Enjoy Bootloader programming 🙂
記事全体を表示
One of the new features that can be found on the FRDM-K82F is the FlexIO header. It’s be specifically designed to interface with the very cost-efficient OV7670 camera, and uses 8 FlexIO lines to read data from the camera. By using the FlexIO feature, it makes it easy to connect a camera to a Kinetis MCU. A demo is included with Kinetis SDK 1.3 which streams the video data from the camera to a host computer over USB. FlexIO: The FlexIO is a highly configurable module found on select Kinetis devices which provides a wide range of functionality including: • Emulation of a variety of serial/parallel communication protocols • Flexible 16-bit timers with support for a variety of trigger, reset, enable and disable conditions • Programmable logic blocks allowing the implementation of digital logic functions on-chip and configurable interaction of internal and external modules • Programmable state machine for offloading basic system control functions from CPU All with less overhead than software bit-banging, while allowing for more flexibility than dedicated IP. Running the Demo: First you’ll need to setup the hardware. An 18 pin header needs to be installed on the *back* of the board. The camera is oriented this way to allow for use of shields on the top, even if the camera is being used. This way the functionality could be extended with WiFi or LCD shields. After the header is soldered on, plug in the camera. It will look like the following when complete: Next we need to program the K82 device with the example firmware. The software can be found in the Kinetis SDK FRDM-K82F stand-alone release, in the C:\Freescale\KSDK_1.3.0_K82\examples\frdmk82f\demo_apps\usb\device\video\flexio_ov7670 folder. Open the project, compile, and program the example specific for your compiler like done for other examples. Make sure you also compile the USB Device library as well. After programming the K82, unplug the USB cable from J5 (OpenSDA) and plug it into J11 (K82 USB). The board will enumerate as a generic USB video device called “USB VIDEO DEMO”. You can then use this device with any video capture software, like Skype or Lync.  Here's a shot of the clock in my cube: The resolution is 160*120, the video image format is RGB565. You may need to manually adjust the focus by rotating the lens on the camera. The frame rate can also be sped up by modifying line 342 in usb_descriptor.c: 5fps: 0x80,0x84,0x1E,0x00, /* Default frame interval is 5fps */ 10fps:  0x40,0x42,0x0F,0x00, 15fps:  0x2A,0x2C,0x0A,0x00, 20fps:  0x20,0xA1,0x07,0x00, The 160*120 max resolution was determined by the amount internal SRAM of the device, as there is not external RAM on the FRDM-K82F board. More Information: One of many places to buy the OV7670 camera module​ OV7670 Reference Manual​ FlexIO Overview ​ FlexIO Training presented at FTF
記事全体を表示
For Remote Control means, that is needed two computers - Server Computer and User Computer, which will be in connection. There are two types of connection, which can be used - HTTP or DCOM. There are two different ways how to set up the remote control in Windows. I made the tutorial, which describes both types of Remote Control. Ok - so, let´s start! HTTP Settings On the Server Computer side: 1. Plug the board to the Server Computer 2. Go to Remote Communication Server 3. Set HTTP connection and choose the right COM Port according the plugged board If the plugged board is on e.g. COM23, it is possible to edit number of Port in Device Manager On the User PC side: 1. Open FreeMASTER,  go to Project -> Options 2. Choose Plug-in Module: FreeMASTER CommPlugin for Remote Server (HTTP) and type the IP address of the server, do not forget join to IP address :8080 3. And start communication by STOP button to successful connection DCOM Settings On the Server Computer side: 1. Plug board to the Server Computer 2. Launch DCOM in FreeMASTER Remote Server Choose COM according plugged board or edit COM according to step 2 - Server Computer in HTTP Connection (up). 3. Setting permissions for the user, User PC. Right click on Computer -> Manage. In Computer Management click to Distributed COM Users. In Distributed COM Users Properties add the user, User Computer. After that, set the permissions in Component Services. In cmd type dcomcnfg.exe In Component Services go to Computers -> My Computer -> DCOM Config -> MCB FreeMASTER Remote Server Application Right click on MCB FreeMASTER Remote Server Application and go to Properties. In Security Tab is possible to add the permissions. There are 3 types of permissions. First permission - Launch and Activation Permissions. There are 4 permission options. Local Launch and Remote Launch means, that user, User Computer can launch e.g. FM Remote Server Application. But for success communication is needed allowing Local Activation and Remote Activation. Second permission - Access Permissions. Click to Edit and Allow Local Access and Remote Access for the user. Do not forget that if there is a change of permissions, specifically allowing, it is necessary for User to log out and log in. On the User Computer side: 1. Open Freemaster, go to Project -> Options 2. Choose Plug-in Module: FreeMASTER CommPlugin for Remote Server (DCOM) and for filling Connect string is possible to use Configure. Definitely, type the IP address of the server and ;Port Name. 3. And start communication by STOP button in FreeMASTER to successful connection And now.. you can do anything 🙂
記事全体を表示
It has been reported that OpenSDA v2/2.1 bootloader could be corrupted when the board is plugged into a Windows 10 machine. An updated OpenSDA bootloader that fixes this issue is available at www.NXP.com/openSDA. There is also a blog article by Arm addressing this issue. To reprogram the bootloader on affected boards, you will require an external debugger, such as Segger JLink or Keil ULink programmer attached to the JTAG port connected to the K20 OpenSDA MCU. For your convenience, the binaries of the OpenSDA v2.2 bootloader is attached at the bottom of this post. If using a Segger JLink, download the latest JLink Software and Documentation pack and use the following JLink.exe commands to connect to the K20 OpenSDA MCU: Connect MK20DX128xxx5 S 4000 And then use the following commands to reflash the bootloader: erase loadbin <your Bootloader Binary> 0x00000000 Here is another post on how to recover bricked OpenSDA boards and to prevent it getting re-bricked. To check more information regarding OpenSDA on your boards, please go to www.nxp.com/opensda.
記事全体を表示
for M68HC08, HCS08, ColdFire and Kinetis MCUs by: Pavel Lajsner, Pavel Krenek, Petr Gargulak Freescale Czech System Center Roznov p.R., Czech Republic The developer's serial bootloader offers to user easiest possible way how to update existing firmware on most of Freescale microcontrollers in-circuit. In-circuit programming is not intended to replace any of debuging and developing tool but it serves only as simple option of embedded system reprograming via serial asynchronous port or USB. The developer’s serial bootloader supported microcotrollers includes 8-bit families HC08, HCS08 and 32-bit families ColdFire, Kinetis. New Kinetis families include support for K series and L series. This application note is for embedded-software developers interested in alternative reprogramming tools. Because of its ability to modify MCU memory in-circuit, the serial bootloader is a utility that may be useful in developing applications. The developer’s serial bootloader is a complementary utility for either demo purposes or applications originally developed using MMDS and requiring minor modifications to be done in-circuit. The serial bootloader offers a zero-cost solution to applications already equipped with a serial interface and SCI pins available on a connector. This document also describes other programming techniques: FLASH reprogramming using ROM routines Simple software SCI Software for USB (HC08JW, HCS08JM and MCF51JM MCUs) Use of the internal clock generator PLL clock programming EEPROM programming (AS/AZ HC08 families) CRC protection of serial protocol option NOTE: QUICK LINKS The Master applications user guides: Section 10, Master applications user guides. The description of Kinetis version of protocol including the changes in user application: Section 7, FC Protocol, Version 5, Kinetis. The quick start guide how to modify the user Kinetis application to be ready for AN2295 bootloader: Section 7.8, Quick guide: How to prepare the user Kinetis application for AN2295 bootloader. Full application note and  software attached.
記事全体を表示
The Real Time Clock (RTC) module is the right tool when we want to keep tracking the current time for our applications. For the Freedom Platform (KL25Z) the RTC module features include: 32-bit seconds counter with roll-over protection and 32-bit alarm 16-bit prescaler with compensation that can correct errors between 0.12 ppm and 3906 ppm. Register write protection. Lock register requires POR or software reset to enable write access. 1 Hz square wave output. This document describes how to implement the module configuration. Also, how to modify the hardware in order feed a 32 KHz frequency to RTC module (it is just a simple wire link).     Hardware. The RTC module needs a source clock of 32 KHz. This source is not wired on the board; hence we need to wire it. Do not be afraid of this, it is just a simple wire between PTC3 and PTC1 and the good news are that these pins are external.   PTC1 is configured as the RTC_CLKIN it means that this is the input of source clock.     PTC3 is configured as CLKOUT (several options of clock frequency can be selected in SIM_SOPT2[CLKOUTSEL] register). For this application we need to select the 32 Khz clock frequency.                         RTC configuration using Processor Expert. First of all we need to set the configurations above-mentioned in Component Inspector of CPU component. Enable RTC clock input and select PTC1 in Pin Name field. This selects PTC1 as RTC clock input. MCGIRCLK source as slow in Clock Source Settings > Clock Source Setting 0 > Internal reference clock > MCGIRCLK source. This selects the 32 KHz clock frequency. Set ERCLK32K Clock Source to RTC Clock Input in Clock Source Settings > Clock Source Setting 0 > External reference clock > ERCLK32K Clock Source. This sets the RTC_CLKIN as the 32 KHz input for RTC module. Select PTC3 as the CLKOUT pin and the CLKOUT pin output as MCGIRCLK in Internal peripherals > System Integration Module > CLKOUT pin control. With this procedure we have a frequency of 32 KHz on PTC3 and PTC1 configured as RTC clock-in source. The MCG mode configurations in this case is PEE mode: 96 MHz PLL clock, 48 MHz Core Clock and 24 MHz Bus clock.   For the RTC_LDD component the only important thing is to select the ERCKL32K as the Clock Source. The image below shows the RTC_LDD component configuration for this application.   After this you only need to Generate Processor Expert Code and write your application.  The code of this example application can be found in the attachments of the post. The application prints every second the current time.     RTC bare-metal configuration. For a non-PEx application we need to do the same configurations above. Enable the internal reference clock. MCGIRCLK is active.          MCG_C1 |= MCG_C1_IRCLKEN_MASK; Select the slow internal reference clock source.          MCG_C2 &= ~(MCG_C2_IRCS_MASK); Set PTC1 as RTC_CLKIN and select 32 KHz clock source for the RTC module.          PORTC_PCR1 |= (PORT_PCR_MUX(0x1));              SIM_SOPT1 |= SIM_SOPT1_OSC32KSEL(0b10); Set PTC3 as CLKOUT pin and selects the MCGIRCLK clock to output on the CLKOUT pin.     SIM_SOPT2 |= SIM_SOPT2_CLKOUTSEL(0b100);     PORTC_PCR3 |= (PORT_PCR_MUX(0x5));   And the RTC module configuration could be as follows (this is the basic configuration just with seconds interrupt): Enable software access and interrupts to the RTC module.     SIM_SCGC6 |= SIM_SCGC6_RTC_MASK; Clear all RTC registers.   RTC_CR = RTC_CR_SWR_MASK; RTC_CR &= ~RTC_CR_SWR_MASK;   if (RTC_SR & RTC_SR_TIF_MASK){      RTC_TSR = 0x00000000; } Set time compensation parameters. (These parameters can be different for each application) RTC_TCR = RTC_TCR_CIR(1) | RTC_TCR_TCR(0xFF); Enable time seconds interrupt for the module and enable its irq. enable_irq(INT_RTC_Seconds - 16); RTC_IER |= RTC_IER_TSIE_MASK; Enable time counter. RTC_SR |= RTC_SR_TCE_MASK; Write to Time Seconds Register. RTC_TSR = 0xFF;   After this configurations you can write your application, do not forget to add you Interrupt Service Routine to the vector table and implement an ISR code.   In the attachments you can find two zip files: PEx application and non-PEx application.   I hope this could be useful for you,   Adrián Sánchez Cano. Original Attachment has been moved to: FRDM-KL25Z-RTC-TEST.zip Original Attachment has been moved to: FRDM-KL25Z-PEx-RTC.zip
記事全体を表示
When you go with your laptop to a public place and you don't have a wi-fi connection available you can connect your cellphone in the USB port of your computer, turn on the USB tethering feature of your smartphone and you get full acess to the internet using your carrier data plan. The USB tethering uses the the RNDIS protocol and is easy to implement on a laptop.   But how to connect a Kinetis to the internet using a cellphone?   I'm sharing the the first version of the implementation I made of the RNDIS protocol.It's based in the KSDK 1.3 + MQX + LwIP and it can be used for reference in other projects. It's only a first release and I plan some additional implementation, bugfixes and support for other Kinetis boards in the near future but it already can be useful in some projects. Initially it only supports FRDM-K22F and FRDM-K64F but it can be implemented in any MCU with USB controller and enough FLASH. It's a low-cost and simple way to connect your MCU to the internet when you don't have a Ethernet cable available or an Wi-fi connection or a 4G module available in your board.   Introduction   This project implements the RNDIS protocol on the top of the USB Host Stack and in the bottom of the LwIP (TCP/IP stack). When a cellphone is connected to a freedom board, it acts as a USB device and the Freedom board acts as a host.   * Software implementation * Cellphone connected to a FRDM-K64F providing internet connection to the board   The user can design his own software in the top of the TCP/IP stack (LwIP) like if it's connected through an ethernet cable.   Demonstration   To run the demo you will need the KDS 1.3 (www.nxp.com/kds).   To load all the projects needed to your project you have to extract the .zip file and in KDS go to File -> Import, Project of Projects -> Existing Project Sets, and browse to the *.wsd file present in the folder:   USB_RNDIS\KSDK_1.3.0\examples\[your board]\demo_apps\lwip\usb_tethering_demo\usb_tethering_demo_mqx\kds   It will import all the needed project in to your workspaces so you will be able to build all the projects and flash it into your board.   With the application flashed, open a Serial terminal with 115200kbps, 8N1 for the CDC interface of OpenSDA.When the board starts, it will display:     Connect your cellphone in to the USB of the MCU. After connect the phone turn on the USB tethering feature and wait some seconds:   The Freedom Board will be connected to the internet. As an example, this demo connects to an HTTP server in the internet, download to MCU some data (Lastest news from an newspaper website) and displays it through the Serial connection.   You can modify this demo for your own application, using the TCP/IP and UDP/IP provided by the LwIP.   Typical Aplications   - Low-cost temporary internet connectivity to the MCU. - Remote updat (i.e.: bootloader through USB downloading the new firmware direct from the web) - Remote control - Remote diagnostics   Known Issues and Limitations: - This first version was only full implemented for FRDM-K22F and FRDM-K64F. I can implement for other boards through requests. - It was tested on Android Phones (Samsung Galaxy, Motorola G, Motorola X). I don't have a iPhone to test yet. - Some cellphones need additional current to detect that is attached to a host.A external power is needed in this situation.For FRDM-K64F I suggest to use the J27 footprint to provide 5V and short the diode D13. - Not all the RNDIS messages was implemented yet, only the most fundamental ones. - There's a flash size limitation due the size of the TCP/IP stacks ( that requires a considerably space of flash). It can adapted in the future for stacks with smaller footprint. - Only support KDS 3.0 at this time. And it only supports MQX at this time.   Let me  know if you have any question. Hope it can be useful!   1-      With the application flashed, open a Serial terminal with 115200kbps, 8N1 for the CDC interface of OpenSDA.When the board starts, it will display:
記事全体を表示
The following document contains a list of documents , questions and discussions that are relevant in the community based on the amount of views they are receiving each month. If you are having a problem, doubt or getting started in Kinetis processors or MCUXpresso, you should check the following links to see if your doubt have been already solved in the following documents and discussions. MCUXpresso MCUXpresso Supported Devices Table FAQ: MCUXpresso Software and Tools  Getting Started with MCUXpresso and FRDM-K64F  Generating a downloadable MCUXpresso SDK v.2 package  Quick Start Guide – Using MCUXpresso SDK with PINs&amp;CLOCKs Config Tools  Moving to MCUXpresso IDE from Kinetis Design Studio Kinetis Microcontrollers Guides and examples Using RTC module on FRDM-KL25Z  Baremetal code examples using FRDM-K64F Using IAR EWARM to program flash configuration field Understanding FlexIO  Kinetis K80 FAQ How To: Secure e-mail client (SMTP + SSL) with KSDK1.3 + WolfSSL for FRDM-K64F  Kinetis Bootloader to Update Multiple Devices in a Network - for Cortex-M0+  PIT- ADC- DMA Example for FRDM-KL25z, FRDM-K64F, TWR-K60D100 and TWR-K70  USB tethering host (RNDIS protocol) implementation for Kinetis - How to use your cellphone to provide internet connectivity for your Freedom Board using KSDK Write / read the internal flash Tracking down Hard Faults  How to create chain of pbuf's to be sent? Send data using UDP.  Kinetis Boot Loader for SREC UART, SD Card and USB-MSD loading  USB VID/PID numbers for small manufacturers and such like  Open SDA and FreeMaster OpenSDAv2  Freedom OpenSDA Firmware Issues Reported on Windows 10 Let´s start with FreeMASTER!  The Kinetis Design Studio IDE (KDS IDE) is no longer being actively developed and is not recommended for new designs. The MCUXpresso IDE has now replaced the Kinetis Design Studio IDE as the recommended software development toolchain for NXP’s Kinetis, LPC and i.MX RT Cortex-M based devices. However, this documents continue to receive considerable amount of views in 2019 which means it could be useful to some people. Kinetis Design Studio New Kinetis Design Studio v3.2.0 available Using Kinetis Design Studio v3.x with Kinetis SDK v2.0  GDB Debugging with Kinetis Design Studio  KDS Debug Configurations (OpenOCD, P&amp;E, Segger) How to use printf() to print string to Console and UART in KDS2.0  Kinetis Design Studio - enabling C++ in KSDK projects  Using MK20DX256xxx7 with KDS and KSDK  Kinetis SDK Kinetis SDK FAQ  Introducing Kinetis SDK v2  How to: install KSDK 2.0  Writing my first KSDK1.2 Application in KDS3.0 - Hello World and Toggle LED with GPIO Interrupt 
記事全体を表示
This is a Processor Expert project created by CodeWarrior for MCUs v10.6 which implements the charge-discharge time of a RC circuit for measuring capacitance. The charge-discharge sequence is performed by TPM0 operating in PWM mode, while the time is measured by TPM1 operating in Input Capture mode. A 100K ohm series resistor is being used, and the result is expressed on nF. It is also using the LCDHTA component from Erich Styger for showing the measurements on a 16x2 LCD, connected to the FRDM-KL05Z through a proto shield. The project is attached, and the pictures shows the measurements of three different capacitors: 10nF, 47nF and 1uF.
記事全体を表示
Latest version of the AN2295 universal bootloader includes support for IAR 7.6 IDE. - added support for Kinetis E MCUs - Kinetis K,L,M,E,W,V support
記事全体を表示
  This document describes the different source clocks and the main modules that manage which clock source is used to derive the system clocks that exists on the Kinetis devices. It’s important to know the different clock sources available on our devices, modifying the default clock configuration may have different purposes since increasing the processor performance, achieving specific baud rates for serial communications, power saving, or simply getting a known base reference for a clock timer. The hardware used for this document is the following: Kinetis:  FRDM-K64F Keep in mind that the described hardware and management clock modules in this document are a general overview of the different platforms and the devices listed above are used as a reference example, some terms and hardware modules functionality may vary between devices of the same platform. For more detailed information about the device hardware modules, please refer to your specific device Reference Manual. Kinetis platforms The Kinetis devices have a main module called Multipurpose Clock Generator (MCG) this module controls which clock source is used to derive the system clocks. A high-level description diagram is shown below: javier_chavezq_0-1599155712645.pngFigure 1. Multipurpose Clock Generator External clock sources can provide a frequency signal as the System oscillator module or the RTC oscillator module, also the MCG module has internal clock generators that the System integration module (SIM) manages, the SIM module provides module-specific clock gating to allow granular shutoff of modules. For more detailed information about the SIM module, refer to “Chapter 12. System Integration Module(SIM)” from the K64 Sub-Family Reference Manual.  The following clock diagram shows all the multiplexers, dividers, and clock gates that can be controlled by the MCG, however, we will focus on the external and internal clock sources and the MCG outputs. image004.png Figure 2. Oscillators,  MCG and SIM modules At ‘MCGOUTCLK’ line, the primary clocks for the system are generated, the circuitry provides fixed clock dividers for the Core clock, Bus clock, FlexBus clock, and the Flash Clock. This allows for trade-offs between performance and power dissipation. It’s important to know that the MCG has 9 states of operation shown in the following figure.   javier_chavezq_2-1599155713462.png  Figure 3. MCG operation states In the previous image, the arrows indicate the permitted MCG state transitions, for example, if the current MCG state is BLPI(Bypassed Low Power Internal) and the desired state is BLPE(Bypassed Low Power External) the shortest and allowed path to follow is first switch to FBI(FLL Bypassed Internal) then to FBE(FLL Bypassed External), and finally to the BLPE MCG state. These switching mode restrictions exist due to certain MCG configuration bits that must be changed to properly move from one mode to another. For example, in the K64 family, the MCG state after a power-on reset is FEI(FLL Engaged Internal) mode, the MCGOUTCLK is derived from the FLL clock that is controlled by the 32kHz Internal Reference Clock (IRC), the following table shows the output frequency values for this specific MCG state. Source Frequency MCGOUTCLK 20.97MHZ Core/System clocks 20.97MHz Bus clock 10.48MHz FlexBus clock 6.99MHz Flash clock 4.19MHz Table 1. K64 default MCG configuration after reset: FEI (FLL Engaged Internal) The following image shows the blocks used for the FEI state using Clocks Tool from MCUXpresso IDE. javier_chavezq_3-1599155713559.pngFigure 4. View of FEI state from Clock Tools For more detailed information, refer to “Chapter 25. Multipurpose Clock Generator (MCG)” from the K64 Sub-Family Reference Manual.  External Clock Sources     System oscillator The System Oscillator module is a crystal oscillator. The module, in conjunction with an external crystal or resonator, generates a reference clock for the MCU.  Supports 32 kHz crystals (Low Range mode) and supports 3–8 MHz, 8–32 MHz crystals and resonators (High Range mode) For more detailed information, refer to Chapter 26. Oscillator(OSC) at K64 Sub-Family Reference Manual.   RTC oscillator The RTC oscillator module, in conjunction with an external crystal, generates a reference clock source of 1Hz and 32.768KHz, supports 32 kHz crystals with very low power. For more detailed information, refer to Chapter 27. RTC Oscillator(OSC32K) at K64 Sub-Family Reference Manual.   Internal Clock Sources    IRC oscillators Internal clock driven by the Fast Internal Reference (FIR) @4MHz or the Slow Internal Reference (SIR) @32kHz.  IRC internal oscillator Internal 48 MHz oscillator that can be used as a reference to the MCG and also may clock some on-chip modules. PLL Phase-locked loop circuit that in conjunction with an external clock source can achieve higher and stable frequencies.   FLL Frequency-locked loop circuit that in conjunction with an internal/external clock source provides module-specific clock and achieves higher frequencies. Modifying MCG state from FEI to FBI state If the current system clock does not fit with our timing requirements we can modify it by changing the state of the MCG module, in this case, if the user requires a lower system clock frequency @32.7KHz(Slow IRC) or @4MHz(Fast IRC) instead @21MHz(FLL Engaged Internal ‘FEI’ default state) and a low power option of the MCG module, the FLL Bypass Internal (FBI) state is an option to reach these requirements. 1.1 Configure MCG mode The FBI state allows us to use the Fast IRC together with its frequency divider achieving frequencies between 31.25KHz to 4MHz, for this example the final core clock is @2MHz. Follow the next steps to change to the FBI state and select a 2MHz clock using the Clock-Tools tool from MCUXpresso IDE.        At the MCUXpresso QuickStart Panel select MCUXpresso Config Tools >> Open Clocks javier_chavezq_4-1599155713991.pngFigure 5. Open Config Tools        At the left top of the screen select the MCG mode to “FBI(FLL Bypassed Internal)” javier_chavezq_5-1599155714080.pngFigure 6. Selection of MCG Mode        Select the frequency divider block(FCRDIV) right-click on it and select “Edit settings of: FCRDIV” javier_chavezq_6-1599155714206.pngFigure 7. FCRDIV block        Modify the divider value from 1 to 2. javier_chavezq_7-1599155714287.pngFigure 8. FCRDIV divider value        Finally, the next image shows how the MCG state and the new yellow paths get modified. The Core and system clocks are @2MHz. javier_chavezq_8-1599155714633.pngFigure 9. FBI MCG state @2MHz 1.2 Export clock configuration to the project After you complete the clock configuration, the Clock Tool will update the source code in clock_config.c and clock_config.h, including all the clock functional groups that we created with the tool. In the previous example, we configured the MCG state to FBI mode, this is translated to the following instructions in source code: “CLOCK_SetInternalRefClkConfig();” and “CLOCK_SetFbiMode();” javier_chavezq_9-1599155715228.png Figure 10. Source code view of FBI MCG configuration Another way to change the MCG state is by directly modifying the internal MCG registers. The blocks shown in the following image need to be modified to switch from the default FEI state to the FBI state. javier_chavezq_10-1599155715513.pngFigure 11. Blocks in FEI state to modify at MCG registers Note. MCG registers can only be written in supervisor mode. The ARM core runs in privileged(supervisor mode) out of reset, it is controlled by [nPRIV] bit in CONTROL core register. For more detailed information visit the Cortex-M4 ARM Documentation Reference Manual.        Internal Reference Source Multiplexor (IREFS), selects the reference source clock for the FLL.  1 is written to C1[IREFS]. The slow internal reference is selected.        PLL Select  Multiplexor(PLLS) Controls whether the PLL or FLL output is selected. 0 is written to C6[PLLS] The FLL output is selected as the MCG source, the PLL is disabled.        Clock Source Select Multiplexor(CLKS), selects the clock source for the MCGOUTCLK  line. 01 is written to C1[CLKS].  The internal reference clock is selected at the CLKS multiplexor.        Fast Clock Internal Reference Divider(FCRDIV), selects the Fast Internal Reference Clock divider, the resulting frequency can be in the range of 31.25KHz to 4MHz. 001 is written to SC[FCRDIV]. The dividing factor is 2 since the desired frequency is @2MHz and the source clock is @4MHz.        Internal Reference Clock Select (IRCS). Selects between the fast or slow internal reference clock source.  x is written to C2[IRCS]. Write 0 for Slow IRC or 1 for Fast IRC.        Finally, to enable the low power when neither the PLL nor FLL are used, a register in C2[LP] is modified. x is written to C2[LP]. Enable, or Disable the PLL & FLL in all the bypass modes.     This is translated to the following instructions in source code in “CLOCK_SetInternalRefClkConfig();” and “CLOCK_SetFbiMode();” functions: javier_chavezq_11-1599155716412.png Figure 12. Source code view of Internal MCG Registers Note. C1, C2, C6, and SC registers are part of the internal MCG control registers.  References K64 Sub-Family Reference Manual Also visit LPC's System Clocks   
記事全体を表示
Hello all.   I would like to share an example project for FRDM-KL25Z board on which C90TFS Flash Driver was included to implement emulated EEPROM (Kinetis KL25 doesn’t have Flex Memory). It is based on the “NormalDemo” example project. A string of bytes is stored on the last page of the flash memory (address 0x1FC00-0x1FFFF), and then, it is overwritten with a different string.   The ZIP file also includes the “Standard Software Driver for C90TFS/FTFx Flash User’s Manual” document. For more information, please refer to Freescale website and search for “C90TFS” flash driver. Hope this will be useful for you. Best regards! /Carlos
記事全体を表示
The FRDM-KL25Z is an ultra-low-cost development platform enabled by Kinetis L Series KL1 and KL2 MCUs families built on ARM® Cortex™-M0+ processor. Features include easy access to MCU I/O, battery-ready, low-power operation, a standard-based form factor with expansion board options and a built-in debug interface for flash programming and run-control. The FRDM-KL25Z is supported by a range of Freescale and third-party development software. Features MKL25Z128VLK4 MCU – 48 MHz, 128 KB flash, 16 KB SRAM, USB OTG (FS), 80LQFP Capacitive touch “slider,” MMA8451Q accelerometer, tri-color LED Easy access to MCU I/O Sophisticated OpenSDA debug interface Mass storage device flash programming interface (default) – no tool installation required to evaluate demo apps P&E Multilink interface provides run-control debugging and compatibility with IDE tools Open-source data logging application provides an example for customer, partner and enthusiast development on the OpenSDA circuit Take a look at these application notes: USB DFU boot loader for MCUs Developer’s Serial Bootloader. Low Cost Universal Motor Drive Using Kinetis L family . Writing your First MQXLite Application Learn more...
記事全体を表示
Test Environment: FRDM-KL43Z Rev. A MCUXpresso IDE v10.2.0 MCUXpresso SDK for FRDM-KL43Z V2.4.1(2018-06-18) Create new project in MCUXpresso IDE select [New project...], there will pop the SDK Wizard panel, then select [frdmkl43z]: Then, click [Next] will enter into [Configure the project] panel, we can set the [Project name] and select [flexio_i2s] in [driver]: Click [Finish], the new project was created. In general, the project is based on [hello_world] project with board default console available. In [Project Explorer], we could find the <fsl_flexio_i2s.c> & <fsl_flexio_i2s.h> & <fsl_flexio.c> & <fsl_flexio.h> files in drivers folder: Edit the code The application note AN5397 detailed introduce how FlexIO emulate I2S bus communication. The MCUXpresso SDK <flexio_i2s> driver using the AN5397 showed second solution to use two timers and two shifters. Please check here to get more detailed info. The I2S signal was below, we need to use four FlexIO pins to provide: BCLK, Fss, TxData & RxData. In <pin_mux.c> file, it need to config pin function, we use PTD7 pin provide I2S BCLK clock; PTD6 pin as I2S Frame_sync pin; PTD5 pin as Tx data pin; PTD6 pin as Rx data pin; In <frdmkl43z_flexio_i2s_interrupt_tx.c>,  config flexio_i2s and config the audio frame format: Please check attached source code for the detailed project info. Test result From the actual measured I2S signal, it shows the 8 bytes was sent out:
記事全体を表示
In this document we are going to see how to use the attached code which implements the configuration of the FRDM-KL25 board as a USB HOST interfacing with a Numeric Keyboard and a 16x2 LCD. The project is compiled in the CodeWarrior IDE using Processor Expert and the Components to support the USB module of the USB Stack 4.1.1. How to add the Processor Expert USB components. The instructions to install the USB components to use them with Processor Expert are in the documentation of the USB Stack 4.1.1; here you can see the steps as well: Download the USB Stack 4.1.1 from the Freescale’s Website (USB Stack 4.1.1) Run the .exe file and install it in the default location. Open CodeWarrior and select Import Components in the Processor Expert button in menu bar. An Open windows will pop up, there you need to go to the path: <install folder>\Freescale USB Stack v4.1.1\ProcessorExpert\Components. To have the complete components and support for the USB module add each PEupd file repeating this step. Close CodeWarrior and open it again to ensure correct installation of the components. Check that the new components are available in the Components Library. About this Project. This project is based in the example code for Processor Expert in the USB Stack 4.1.1 USB_HID_MOUSE_HOST_MKL25Z128_PEx which implements the use of the FRDM-BOARD KL25 and a HID Mouse Device to interface with. In this project the HID Device is a Numeric Keyboard and the HOST Device (FRDM-KL25) is handling the data and printing them in a 16x2 LCD used in 8 bits mode (The LCDHTA component used here was created by Erich Styger; find the component an all the information about it here: http://mcuoneclipse.com/2012/12/22/hd44780-2x16-character-display-for-kinetis-and-freedom-board/ and say Thank you Erich: “Thank you Erich”). Here you can find a video of the implementation of this application: HID HOST WITH FRDM-KL25 The hardware components are: FRMD-KL25 Rev.E Adafruit Prototype Shield v.5 LCD JHD-162A Numeric USB Keyboard (Product Name: Numpad i110, Model No. GK-100010) USB _host Inside the project you can see there is a folder called USB_Host an it contains two important folders with source files: App_keyboard: Contains the specific function for the Keyboard configuration: in use, attached detached, callbacks and more; contain how to handle the data coming from the device. The function process_kdb_buffer is where the data is transmitted to the LCD and use it for the application. Classes: contain the necessary function to handle a hid as the device. Handle all the functions necessary for the USB protocol. Note: The usb_classes.c and usb_classes.h files are generated by processor expert. I attach these two files as well to have a reference how these files must look like. This is because sometimes during the code generation process Processor Expert erases part of the code. I hope this project is useful for you. Best Regards, Adrian.
記事全体を表示
This document shows the implementation of the infrared on the UART0 using the FRDM-KE02Z platform. The FRDM-KE02Z platform is a developing platform for rapid prototyping. The board has a MKE02Z64VQH2 MCU a Kinetis E series MCU which is the first 5-Volt MCU built on the ARM Cortex-M0+ core. You can check the evaluation board in the Freescale’s webpage (FRDM-KE02Z: Kinetis E Series Freedom Development Platform) The Freedom Board has a lot of great features and one of this is an IrDA transmitter and receiver on it. Check this out! One of the features of the MCU is that the UART0 module can implement Infrared functions just following some tricks (MCU-magic tricks). According to the Reference Manual (Document Number: MKE02Z64M20SF0RM) this tricks are:      UART0_TX modulation: UART0_TX output can be modulated by FTM0 channel 0 PWM output      UART0_RX Tag: UART0_RX input can be tagged to FTM0 channel 1 or filtered by ACMP0 module For this example we are going to use the ACMP0 module to implement the UART0_RX functionality. Note1: The Core is configured to run at the maximum frequency: 20 Mhz Note2: Refer to the reference manual document for more information about the registers. Configuring the FTM0. The next lines show the configuration of the FTM0; the module is configured with a Frequency of 38 KHz which is the ideal frequency for an infrared led. The FTM0_CH0 is in Edge_Aligned PWM mode (EPWM).           #define IR_FREQUENCY       38000 //hz      #define FTM0_CLOCK                BUS_CLK_HZ      #define FTM0_MOD_VALUE            FTM0_CLOCK/IR_FREQUENCY      #define FTM0_C0V_VALUE            FTM0_MOD_VALUE/2      void FTM0CH0_Init( void )      {        SIM_SCGC |= SIM_SCGC_FTM0_MASK;             // Init FTM0 to PWM output,frequency is 38khz        FTM0_MOD= FTM0_MOD_VALUE;        FTM0_C0SC = 0x28;        FTM0_C0V = FTM0_C0V_VALUE;        FTM0_SC = 0x08; // bus clock divide by 2      } With this we accomplish the UART0_TX modulation through a PWM on the FTM0_CH0. Configuring the ACMP0. The configuration of the ACMP0 is using a DAC and allowing the ACMP0 can be driven by an analog input.      void ACMP_Init ( void )      {        SIM_SCGC |= SIM_SCGC_ACMP0_MASK;        ACMP0_C1 |= ACMP_C1_DACEN_MASK |                   ACMP_C1_DACREF_MASK|                   ACMP_C1_DACVAL(21);    // enable DAC        ACMP0_C0 |= ACMP_C0_ACPSEL(0x03)|                            ACMP_C0_ACNSEL(0x01);        ACMP0_C2 |= ACMP_C2_ACIPE(0x02);  // enable ACMP1 connect to PIN        ACMP0_CS |= ACMP_CS_ACE_MASK;     // enable ACMP                } With this we have now implemented the UART0_RX.     IrDA initialization. Now the important thing is to initialize the UART0 to work together with these tricks and implement the irDA functions. Basically we initialize the UART0 like when we use normal serial communication (this is not the topic of this post, refer to the project to see the UART_init function) and we write to the most important registers:         SIM_SOPT |= SIM_SOPT_RXDFE_MASK; UART0_RX input signal is filtered by ACMP, then injected to UART0.      SIM_SOPT |= SIM_SOPT_TXDME_MASK; UART0_TX output is modulated by FTM0 channel 0 before mapped to pinout. The configuration is as follows:      void IrDA_Init( void )      { // initialize UART0, 2400 baudrate        UART_init(UART0_BASE_PTR,BUS_CLK_HZ/1000,2400);                  // clear RDRF flag        UART0_S1 |= UART_S1_RDRF_MASK;                  // initialize FTM0CH1 as 38k PWM output        FTM0CH0_Init();                      // enable ACMP        ACMP_Init(); SIM_SOPT |= SIM_SOPT_RXDFE_MASK;  //UART0_RX input signal is filtered by ACMP, then injected to UART0.        UART0_S2 &= ~UART_S2_RXINV_MASK;  //inverse data input SIM_SOPT |= SIM_SOPT_TXDME_MASK;  //UART0_TX output is modulated by FTM0 channel 0 before mapped to pinout.      } With the irDA initialization we got the infrared features on the UART0. Philosophy of the Example In the attachments of this post you can find the example which shows the use of these functions in a basic application; the project was compiled in CodeWarrior 10.6 and the philosophy is: I hope that the information presented on this document could be useful for you. Thank you! Best Regards!
記事全体を表示