The following document contains a list of documents , questions and discussions that are relevant in the community based on the amount of views they are receiving each month. If you are having a problem, doubt or getting started in Kinetis processors or MCUXpresso, you should check the following links to see if your doubt have been already solved in the following documents and discussions.
MCUXpresso
MCUXpresso Supported Devices Table
FAQ: MCUXpresso Software and Tools
Getting Started with MCUXpresso and FRDM-K64F
Generating a downloadable MCUXpresso SDK v.2 package
Quick Start Guide – Using MCUXpresso SDK with PINs&CLOCKs Config Tools
Moving to MCUXpresso IDE from Kinetis Design Studio
Kinetis Microcontrollers Guides and examples
Using RTC module on FRDM-KL25Z
Baremetal code examples using FRDM-K64F
Using IAR EWARM to program flash configuration field
Understanding FlexIO
Kinetis K80 FAQ
How To: Secure e-mail client (SMTP + SSL) with KSDK1.3 + WolfSSL for FRDM-K64F
Kinetis Bootloader to Update Multiple Devices in a Network - for Cortex-M0+
PIT- ADC- DMA Example for FRDM-KL25z, FRDM-K64F, TWR-K60D100 and TWR-K70
USB tethering host (RNDIS protocol) implementation for Kinetis - How to use your cellphone to provid...
Write / read the internal flash
Tracking down Hard Faults
How to create chain of pbuf's to be sent? Send data using UDP.
Kinetis Boot Loader for SREC UART, SD Card and USB-MSD loading
USB VID/PID numbers for small manufacturers and such like
Open SDA and FreeMaster
OpenSDAv2
Freedom OpenSDA Firmware Issues Reported on Windows 10
Let´s start with FreeMASTER!
The Kinetis Design Studio IDE (KDS IDE) is no longer being actively developed and is not recommended for new designs. The MCUXpresso IDE has now replaced the Kinetis Design Studio IDE as the recommended software development toolchain for NXP’s Kinetis, LPC and i.MX RT Cortex-M based devices. However, this documents continue to receive considerable amount of views in 2019 which means it could be useful to some people.
Kinetis Design Studio
New Kinetis Design Studio v3.2.0 available
Using Kinetis Design Studio v3.x with Kinetis SDK v2.0
GDB Debugging with Kinetis Design Studio
KDS Debug Configurations (OpenOCD, P&E, Segger)
How to use printf() to print string to Console and UART in KDS2.0
Kinetis Design Studio - enabling C++ in KSDK projects
Using MK20DX256xxx7 with KDS and KSDK
Kinetis SDK
Kinetis SDK FAQ
Introducing Kinetis SDK v2
How to: install KSDK 2.0
Writing my first KSDK1.2 Application in KDS3.0 - Hello World and Toggle LED with GPIO Interrupt