Let´s start with FreeMASTER!

Document created by Iva Susnova Employee on Apr 28, 2016Last modified by Diana Torres on Feb 28, 2017
Version 6Show Document
  • View in full screen mode

What is it FreeMASTER?

 

FreeMASTER is a tool with variety GUIs in one offered free. FreeMASTER is a user-friendly real-time debug monitor and data visualization tool

GUI can be easily extend by multimedia content (charts) and user-modified content (possible mix user´s data with default values)

offers access to target variables, symbols and data types

access over UART, CAN or USB with target-side driver and over BDM

possibility to direct control via variable modifications

addresses parsed from ELF file or provided by target (TSA)

scope graphs with real-time data in [ms] resolution

recorder visualization transitions close to 10[us] resolution

 

 

FreeMASTER features

Real Time Monitor

-Displaying variable values in various formats (Text, Real-Time waveforms, High-speed recorded data)

Control Panel

- Direct variable value settings and variable stimulation, scribtable in JScript or VBScript

Demonstration Platform

- Demostration embedded app by HTML pages, display simultaneous real-time data monitoring

Easy Project Deployment

- Entire project saved to a single file

 

FreeMASTER communication

There are two types of communication. It is possible to communicate via Direct RS232 or selected Plug-in Module.

In short:

SCI, UART
USB – CDC – Kinetis, ColdFire V2

CAN

JTAG (56F8xxx only)

BDM – Kinetis, PowerPC, ColdFire, HCS with Segger, P&E Micro, CMSIS-DAP…

 

 

FreeMASTER usage

Real-time debugging - FreeMASTER allows users to debug applications in true real-time through its ability to watch variables. Moreover, it allows debugging at the algorithm level, which helps to shorten the development phase

Diagnostic tool - FreeMASTER remote control capability allows it to be used as a diagnostic tool for debugging customer applications remotely across a network

Demonstrations - FreeMASTER is an outstanding tool for demonstrating algorithm or application execution and variable outputs.

Education - FreeMASTER may be used for educational purposes. Its application control features allow students to play with the application in demonstration mode, learning how to control program execution.

 

FreeMASTER description of the environment

 

The FreeMASTER window is divided into 4 parts - Project Tree, Detail View Pane, Commands and Variable Watch Grid.

Project Tree is the project, New Block is a root of the project, New Scope is similar to classical Oscilloscope. Scope periodically reads variable values and plots them in real-time. It is limited by the serial communication speed. The recorder is also monitoring and visualising variable values, but the change is much faster. The recorder is running on target board and variable values are sampled into memory buffer on the board and then these sampled data are downloaded from the board to FreeMASTER.

 

Detail View Area is dynamically changes depending on content which is selected in Project Tree. Detail View Tab can be control page, algorithm block description, scope, recorder or another HTML document whose URL is defined in the Scope or Recorder properties.

Commands window is list of commands to send, Variable Stimulus - is the list of defined variables for the defined time.

In Variable Watch Grid contains the list of watched variables.

 

Supported devices

supported_devices.png

FreeMASTER download and support

 

The installation package you can download from the Official website:

 

FreeMASTER Official website

www.nxp.com/freemaster

 

You can ask us on Community or you can create new SR according to https://community.freescale.com/docs/DOC-329745

 

More about FreeMASTER

 

FreeMASTER Official Website

https://www.nxp.com/freemaster

 

Using FreeMASTER

https://cache.freescale.com/files/microcontrollers/doc/reports_presentations/FREEMASTERPRESENT.pdf

 

FREEMASTER:  Remote Server Tutorial

https://community.freescale.com/docs/DOC-103293

 

Tutorial: FreeMASTER Visualization and Run-Time Debugging

https://mcuoneclipse.com/2013/08/24/tutorial-freemaster-visualization-and-run-time-debugging

 

Let´s continue with reading! Let´s start with KSDK!

6 people found this helpful

Attachments

    Outcomes