i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
i.MX95 Triple Display Patches for LF-6.6.52-2.2.0 BSP. iMX95 19x19 EVK. qiang_limpu_se_0-1739859470230.png     Patches files: 0001-iMX95-EVK-IT6263-LVDS-to-HDMI-bridge-chip-combine-it.patch Combine IT6263 with simple panel driver, no EDID is needed, 720P and 1080P display mode had been added as two examples.   0002-IT6263-Always-reported-connected-for-force-output.patch Let IT6263 always report cable connected to force output HDMI signals.   0003-iMX95-EVK-add-LVDS-clone-mode-based-on-IT6263.patch LVDS clone mode is supported on two LVDS ports, they output same content and same timing from one DPU display engine (1920*1080@60fps).   0004-iMX95-EVK-add-dual-LVDS-interleaver-mode-based-on-IT.patch LVDS interleave mode is supported on two LVDS ports, they output different content and same timing from one DPU display engine (3840*1080@60fps).   0005-iMX95-EVK-add-triple-display-support.patch Triple display is supported, 1 MIPI DSI + 2 LVDS.  imx95-19x19-evk-triple-display-lvds-clone.dtb: the two LVDS is in clone mode. imx95-19x19-evk-triple-display-lvds-interleaver.dtb: the two LVDS is in interleave mode.   For 1 MIPI DSI + 2 LVDS display clone mode: qiang_limpu_se_0-1739858854733.png For 1 MIPI DSI + 2 LVDS Interleave mode: qiang_limpu_se_2-1739859096402.png     Know issues:  Due to bridge numbers (3) and DPU engine/Pixel link/Pixel Interleaver number (2) is not aligned, during kernel boot up, there will be followed link error log, but there is no real function impact.   [    3.178741] imx95-ldb 4b0c0000.syscon:ldb@4: Failed to create device link (0x180) with 4b010000.syscon:bridge@8 ... [    4.209299] imx95-pixel-interleaver 4b0d0000.bridge: Failed to create device link (0x180) with 4b400000.display-controller [    4.220355] imx95-pixel-interleaver 4b0d0000.bridge: Failed to create device link (0x180) with 4b400000.display-controller ...     2025-8-19 update: Add the patch for L6.12.20_2.0.0 BSP. lf-6.12.20-2.0.0_triple_display_patches.zip   2026-9-7 update: Add patch for L6.18.37_2.1.0 BSP based on FRDM-IMX95.  
查看全文
  Purpose Under some situations, need to modify the binary image. Under some situations, no development environment. Under some situations, even no Linux. Only have windows. Board bring up need simple settings, such as simple/tiny rootfs.  Key Features Create small sdcard mirror image All operations are on binary files no need development environment(offline) Set the u-boot environment on binary image Windows OS support Snapshot:   Please download  create_sdcard_mirror_ext.zip.001.zip create_sdcard_mirror_ext.zip.002.zip create_sdcard_mirror_ext.zip.003.zip create_sdcard_mirror_ext.zip.004.zip create_sdcard_mirror_ext.zip.005.zip create_sdcard_mirror_ext.zip.006.zip extract each one to have below files  create_sdcard_mirror_ext.zip.001 create_sdcard_mirror_ext.zip.002 create_sdcard_mirror_ext.zip.003 create_sdcard_mirror_ext.zip.004 create_sdcard_mirror_ext.zip.005 create_sdcard_mirror_ext.zip.006 Put together and extract them.  
查看全文