i.MX95 Triple display Linux Patch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX95 Triple display Linux Patch

i.MX95 Triple display Linux Patch

i.MX95 Triple Display Patches for LF-6.6.52-2.2.0 BSP.
iMX95 19x19 EVK.
qiang_limpu_se_0-1739859470230.png

 

 
Patches files:
0001-iMX95-EVK-IT6263-LVDS-to-HDMI-bridge-chip-combine-it.patch
Combine IT6263 with simple panel driver, no EDID is needed, 720P and 1080P display mode had been added as two examples.
 
0002-IT6263-Always-reported-connected-for-force-output.patch
Let IT6263 always report cable connected to force output HDMI signals.
 
0003-iMX95-EVK-add-LVDS-clone-mode-based-on-IT6263.patch
LVDS clone mode is supported on two LVDS ports, they output same content and same timing from one DPU display engine (1920*1080@60fps).
 
0004-iMX95-EVK-add-dual-LVDS-interleaver-mode-based-on-IT.patch
LVDS interleave mode is supported on two LVDS ports, they output different content and same timing from one DPU display engine (3840*1080@60fps).
 
0005-iMX95-EVK-add-triple-display-support.patch
Triple display is supported, 1 MIPI DSI + 2 LVDS. 
imx95-19x19-evk-triple-display-lvds-clone.dtb: the two LVDS is in clone mode.
imx95-19x19-evk-triple-display-lvds-interleaver.dtb: the two LVDS is in interleave mode.
 
For 1 MIPI DSI + 2 LVDS display clone mode:
qiang_limpu_se_0-1739858854733.png

For 1 MIPI DSI + 2 LVDS Interleave mode:

qiang_limpu_se_2-1739859096402.png

 

 

Know issues: 
Due to bridge numbers (3) and DPU engine/Pixel link/Pixel Interleaver number (2) is not aligned, during kernel boot up, there will be followed link error log, but there is no real function impact.
 
[    3.178741] imx95-ldb 4b0c0000.syscon:ldb@4: Failed to create device link (0x180) with 4b010000.syscon:bridge@8
...
[    4.209299] imx95-pixel-interleaver 4b0d0000.bridge: Failed to create device link (0x180) with 4b400000.display-controller
[    4.220355] imx95-pixel-interleaver 4b0d0000.bridge: Failed to create device link (0x180) with 4b400000.display-controller
...
 
 
2025-8-19 update: Add the patch for L6.12.20_2.0.0 BSP.
lf-6.12.20-2.0.0_triple_display_patches.zip
 
2026-9-7 update: Add patch for L6.18.37_2.1.0 BSP based on FRDM-IMX95.
 
ラベル(2)
添付
コメント

Hello https://community.nxp.com/t5/user/viewprofilepage/user-id/4760,

do you know if the patch will be included in the standard BSP?

Is it availble an update patch for 6.12.34_2.1.0?

Pls. let me know if the DDR on the board is DDR5 or DDDR4.

 

BR
Stefano

 

Hi @StefanoGattazzo 

Do you  get any issue to try the patch on 6.12.34_2.1.0? I think it is close to 6.12.20.

Hi qiang_li-mpu_se,

I asked in advance before test.

 

BR

Stefano

評価なし
バージョン履歴
最終更新日:
1ヶ月前
更新者: