i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343344 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343372 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343273 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343518 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343528 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343521 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343715 
View full article
[中文翻译版] 见附件   原文链接: Add a new shared memory region on Android Auto P9.0.0_GA2.1.0 BSP 
View full article
[中文翻译版] 见附件   原文链接: eIQ Machine Learning Software for i.MX Linux 4.14.y 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343576 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343823 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343777 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343802 
View full article
[中文翻译版] 见附件   原文链接: Enable GmSSL which supports OSCCA Algorithm Toolbox on i.MX 
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343761 
View full article
i.MX8/8X/8XL在汽车中的应用 • 娱乐导航 • 虚拟仪表 • 电子座舱 • 360环视与ADAS • C-V2X Tbox
View full article
目录 1    硬件资源,文档及工具下载... 2 1.1    硬件资源... 2 1.2    内存配置测试相关的文档... 3 1.3    内存压力测试工具. 3 1.4    内存配置工具. 4 2    内存设计要求... 4 3    LPDDR4基础... 4 4    硬件连接... 6 5    i.MX8QXP/DXP+LPDDR4内存配置与测试步骤... 8 5.1    生成LPDDR4初始化脚本... 8 5.2    使用内存测试工具测试内存... 13 5.3    编译内存测试工具所用的SCFW镜像... 17 5.4    其它尺寸的LPDDR4配置... 18 6    i.MX8DX+DDR3L内存配置... 23 7    测试失败的DEBUG.. 26 8    内存参数应用到SCFW中... 30
View full article
目录 1 www.nxp.com公网资源 .............................................. 2 1.1 www.nxp.com Documentation ................................ 3 1.2 www.nxp.com Tools&Software ............................... 6 2 nxp 社区资源 ........................................................... 11 3 i.MX8M公网资源的其它资料 .................................... 13 4 i.MX8MNano公网资源的其它资料 ............................ 13 5 i.MX8MPlus公网资源的其它资料 ............................. 13
View full article
This doc show how to use i.MX8QXP Display Controller GammaCor unit to tune gamma. HW: i.MX8QXP MEK board, HDMI monitor SW: i.MX Linux 4.14.98_2.2.0 BSP release, patch in this doc 1.Introduce gamma The gamma, gamma correction, gamma encoding, gamma compression , these words all related one kind operation , see wiki page of it: The device used for image capture/print/display follow this power-law. For example the camera captured image , to view this image on display device as good as original captured image : gamma encoding when camera saved sensor data to image file,  and  gamma decoding when that image file display on your PC LCD monitor. That is : 2. i.MX8QXP Display Controller Gamma Correction Unit The Gamma Correction unit position is located between Frame Gen unit and TCon unit.   More detail see below contents from i.MX8QXP RM: So GammaCor unit could be used as adjust display gamma , or brightness or contrast. To used it, need follow the steps at RM 15.9.2.4.4.8.3.   Something need to note: You need program 33 sample point value into the register, these sample point value range is from 0 to 1023. Note, first write is start sample point value , then the other is delta value: current sample point minus previous sample point value. You can use GammaCor unit on any channel of R/G/B. If you use normalized function f(x), the following formula should be used to clut[i = 0..32] = round( f(i * 32 / 1023) * 1023) 3. i.MX8QXP Linux device driver patch and test code Apply attached  patch 8qxp_dpu_gammacor_4.14.98_2.2.0.diff on Linux kernel. In the kernel patch, function dpu_gammacor_update, I choose not calculate delta value between each sample pint , let user space application calculate delta value and passed to kernel. Apply 8qxp-dpu-gammacor-modetst.diff on libdrm-imx, to get test application which is based on modetest.  Test app will read one greyscale image file 720P.rgb, put it under same folder of test application , calculate sample point value by pow function  , and calling drmModeCrtcSetGamma to pass related value to kernel,  next loop will change sample point value, and will see that greyscale image will changed on HDMI monitor. After system boot up, run below cmd to check result of test application systemctl stop weston ./gamma_show_rgba.out -P 29@32:1280x720@AB24 Reference: a>https://www.nxp.com/webapp/Download?colCode=IMX8DQXPRM b>https://www.nxp.com/webapp/Download?colCode=L4.14.98_2.2.0_MX8QXP&appType=license c> https://source.codeaurora.org/external/imx/libdrm-imx/ d> https://en.wikipedia.org/wiki/Gamma_correction
View full article