i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
This section for all Freescale i.MX users ranging from customers to designers to help provide the best solution to the most frequently encountered questions related to Freescale i.MX products. Products Below are links to pages containing links to documentation related to that product. i.MX Family i.MX6 Multimedia Applications Processors i.MX53 Multimedia Applications Processors i.MX51 Multimedia Applications Processors i.MX35 Multimedia Applications Processors i.MX31 Multimedia Applications Processors i.MX28 Multimedia Applications Processors i.MX27 Multimedia Applications Processors i.MX25 Multimedia Applications Processors i.MX21 Multimedia Applications Processors Topics Below are links to pages containing links to documentation related to that topic. 19-iMX_Serial_Download_Protocol.py All Boards 2D/3D Graphics All Boards Accessing Registers All Boards Audio All Boards Bluetooth Dongle All Boards Compiling RedBoot All Boards Configuring RedBoot All Boards Creating App Video All Boards Deploy NFS All Boards DirectFB All Boards FlexCAN All Boards Hardware Software All Boards How To Convert RVICE CP15 To OpenOCD All Boards How To Understand JTAG BSDL All Boards I2C-tools All Boards Java All Boards JTAG All Boards LTIB All Boards LTIB Config Ubuntu All Boards LTIB Creating Uimage Uboot All Boards NFS on Fedora All Boards NFS on Slackware All Boards NFS on Ubuntu All Boards OpenEmbedded All Boards Pdfreader All Boards PMIC Registers All Boards Qtopia All Boards Qtopia on Ubuntu All Boards Qt v2 All Boards RedBoot All Boards Serial Console All Boards TCP All Boards Tethering All Boards TFTP All Boards TFTP Fedora All Boards TFTP on OpenSuse All Boards TFTP on Ubuntu All Boards Theora Encoder All Boards Transfer Serial RedBoot All Boards U-boot All Boards Updating RedBoot Through RedBoot All Boards Video All Boards Video Host All Boards VMWare All Boards Wi-Fi All Boards X11 Android Demonstration Platform Exercising the i.MX Serial Download Protocol with a Python Script Gstreamer GTK How to Enable Second Display Showing Different Things on JB4.2.2 SabreSD How to Measure Signal Frequency by Using the Camera Sensor Interface of an i.MX i.MX as a USB Playback/Capture Device on One OTG Port i.MX Bootlets (i.MX233 EVK) i.MX USB Loader i.MXS Development Kit InternalI2C Linux Kernel Mxuart patch New Release of the i.MX OTP Tools V1.3.3 NFS OpenEmbedded Redboot Running ATK on Linux Script to Flash a Linux System into a SD card U-Boot Yoctoproject
View full article
Support SSI Master function based on 0001_SSI_ASRC_P2P.patch
View full article
Configuring U-Boot LTIB Creating Uimage Uboot U-boot FW Printenv FW Env File Add New i.MX5x Board on LTIB i.MX25 PDK I.MX25 PDK U-boot SplashScreen I.MX25 PDK U-boot SDCard i.MX27 ADS Board Compiling U-Boot for i.MX27ADS Installing U-Boot on iMX27ADS i.MX31 ADS Board i.MX31ADS Compiling Uboot I.MX31ADS Installing Uboot i.MX31 PDK Board i.MX 31 PDK Board Screenshot I.MX31 PDK Board Flashing i.MX31 PDK Board DirectFB i.MX51 EVK Board i.MX51 EVK U-boot I.MX51EVK Install U-Boot i.MX51 EVK Compiling U-boot i.MX51 EVK Changing Env
View full article
Attached is the Kernel needed to construct the following image: i.MX 6Dual/6Quad Power Consumption Measurement Linux Image
View full article
Hi All, The i.MX6 Android R13.4-GA.03 patch release is now available on www.freescale.com ·         Files available # Name Description 1 IMX6_R13.4.03_ANDROID_PATCH This patch release is based on the i.MX 6 Android R13.4   release. The purpose of this patch release is correct the PFD workflow in   U-Boot, fix the miscalibration issue for the thermal sensor and corrects   ramp-up time of the internal LDOs
View full article
Summary of the Issue: We have had customers reporting failure to run MC and SC production parts at 1GHz or higher frequencies. The signature of the fail is that the system will hang once it tries to ramp from the boot frequency of 800MHz to 1GHz or higher. The root cause was tracked to the setting of the LDO_VOLT_CHANGE_EN fuse in production parts. The LDO_VOLT_CHANGE_EN fuse sets the LDO boot voltage to either 1.15V (indicated by a fuse setting of “1”) or 1.1V  (indicated by a fuse setting of “0”). In production parts the fuse is set to “1”, i.e. 1.15V, since this is the optimal setting based on characterization data. On pre-production units the LDO voltage was set to the lower setting of 1.1V (i.e. fuse set to “0”). The reason this is a problem with MC/SC parts is because the fuse is read by the ROM during boot and overwrites the LDO ramp rate bits in the PMU_MISC2 register based on the setting of the fuse. When the LDO_VOLT_CHANG_EN fuse is set to “1” then the LDO ramp up time to spec voltage is set (in PMU_MISC2) to 500uS instead of the 50uS assumed by the CPUFreq driver. This will cause the system to hang when transitioning from the boot frequency to a higher frequency/voltage point since the required voltage to support the higher frequency is not yet present. In real terms, customers who have production i.MX 6Quad/6Dual/6DualLite and 6 Solo parts have seen failures to ramp their products to 1GHz or higher frequencies. This is completely fixed by a software patch that corrects the LDO ramp setting in the PMU_MISC_2 register by setting it back to the fastest ramp time. Note that the LDO_VOLT_CHANGE_EN fuse is not in the reference manual since it is not a customer visible fuse. It is programmed and locked at final test. This is a mandatory fix for all customers. Affected Parts: i.MX 6Quad – all SC and MC parts, consumer and automotive. Industrial MC parts not yet shipping. i.MX 6Dual – all SC and MC parts, consumer and automotive. Industrial MC parts not yet shipping. i.MX 6DualLite – all MC parts consumer parts. Automotive and industrial MC parts not yet shipping. i.MX 6Solo – all MC consumer parts. Automotive and industrial MC parts not yet shipping. Patch Availability and Location: Patches exist for both Linux and Android. They are available on freescale.com. See below for more details. i.MX 6Quad – www.freescale.com/imx6q i.MX 6Dual – www.freescale.com/imx6d i.MX 6DualLite – www.freescale.com/imx6dl  i.MX 6Solo – www.freescale.com/imx6s Select the “Software and Tools” tab and then expand the section “Updates and Patches”.  The relevant patches are: Linux – L3.0.35_1.1.1_LDO_PATCH (i.MX 6Quad/6Dual) Linux – L3.0.35_3.0.3_LDO_PATCH (i.MX 6DualLite/6Solo) Android – IMX6_R13.4103_ANDROID_LDO_PATCH (i.MX 6Quad/6Dual/6DualLite/6Solo) Communication Roll-out: i.MX FAE’s: done (via maillist). Will post copy of this email to i.MX support space by end of day 1 st March. i.MX DFAE’s: 8 th March. Customer notification: 8 th March. i.MX community: 8 th March (to coincide with customer notification). We are also working on an engineering bulletin that describes the change for customers who are not using our provided Linux and Android BSP’s. Target date: TBD. But goal is to make this available on/around mid-March. Best regards, Amanda and Kyle This document was generated from the following discussion: i.MX 6 Series LDO Ramp Issue: Linux and Android Patches Now Available
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343113 
View full article
platform: imx8qxp c0 mek OS: yocto 4.19.35_1.1.0 hardware connection: imx8qxp lvds0 => dummy panel ,  lvds1 => it6263 => display   On imx8qxp there are one DPU(display process unit) and one ISI(image subsystem interface), ISI supports input from dpu.   dpu block diagram: note that only dsi0 and lvds0 can be used for loopback. and this patch only test the lvds0, since lvds support dummy panel.   Please see the readme in the attchment for how to enale this feature.   Note: for ISI loopback,  it needs output of 2x GPIO (4x for HDMI-TX or combo PHY) to pixel_link_receiver_address: For iMX8QM: o LVDS: pixel_link_receiver_address[1:0] = do_gpio_dr[7:6]  o MIPI-DSI: pixel_link_receiver_address[1:0] = do_gpio_dr[7:6] o HDMI-TX: odd_pixel_link_receiver_address[1:0] = do_gpio_dr[7:6],even_pixel_link_receiver_address[1:0] = do_gpio_dr[5:4]   For iMX8QXP: o Combo MIPI-DSI / LVDS: pixel_link0_receiver_address[1:0] = do_gpio_dr[7:6], pixel_link1_receiver_address[1:0] = do_gpio_dr[5:4]   
View full article
Since JB4.3, we have added a customer library in myandroid/devices/fsl/common/recovery to give a chance for customer to customize their UI menu in recovery.img Be sure you define the TARGET_RECOVERY_UI_LIB to be same as your defined in Android.mk in myandroid/devices/fsl/common/recovery, as we did in myandroid/devices/fsl/imx6/BoardConfigCommon.mk TARGET_RECOVERY_UI_LIB := librecovery_ui_imx Once you defined TARGET_RECOVERY_UI_LIB, myandroid/bootable/recovery will use the one to replace the default ui lib  as the source code myandroid/bootable/recovery/default_device.cpp. By default, we define below menu as below: const char* ITEMS[] = { "reboot system now",   "apply update from ADB",   "wipe data/factory reset",   "wipe cache partition",   NULL }; Below is an example to add a new menu as "apply update from SD Card": diff --git a/common/recovery/recovery_ui.cpp b/common/recovery/recovery_ui.cpp index ccf8ccd..9cbd91e 100644 --- a/common/recovery/recovery_ui.cpp +++ b/common/recovery/recovery_ui.cpp @@ -31,6 +31,7 @@ const char* HEADERS[] = { "Volume up/down to move highlight;", const char* ITEMS[] = { "reboot system now",   "apply update from ADB", + "apply update from SD Card",   "wipe data/factory reset",   "wipe cache partition",   NULL }; @@ -77,8 +78,9 @@ class ImxDevice : public Device { switch (menu_position) { case 0: return REBOOT; case 1: return APPLY_ADB_SIDELOAD; - case 2: return WIPE_DATA; - case 3: return WIPE_CACHE; + case 2: return APPLY_EXT; + case 3: return WIPE_DATA; + case 4: return WIPE_CACHE; default: return NO_ACTION; } } The handle on the menu is defined in function prompt_and_wait(Device* device, int status) in myandroid/bootable/recovery/recovery.cpp. Below is the buildin menu function in recovery.     enum BuiltinAction { NO_ACTION, REBOOT, APPLY_EXT, APPLY_CACHE,   APPLY_ADB_SIDELOAD, WIPE_DATA, WIPE_CACHE };
View full article
GTK+ is a highly usable, feature rich toolkit for creating graphical user interfaces which boasts cross platform compatibility and an easy to use API. GTK+ it is written in C, but has bindings to many other popular programming languages such as C++, Python and C# among others. GTK+ is licensed under the GNU LGPL 2.1 allowing development of both free and proprietary software with GTK+ without any license fees or royalties. [Source: gtk.org] As GTK+ is a graphical library, a program using GTK+ can be done in many languages like C, C++, Python, Perl, PHP, Ruby, and many others. Here a C example will be done. How to make a simple program with GTK An easier way to make a graphical interface (GUI) program using GTK+ is to use Glade as Graphical Editor. Glade3 Screenshot To install Glade on Ubuntu type: $sudo apt-get install glade-3 Old Glade versions used to generate C code. Currently version ONLY generates a .glade file that can be parsed in a .xml file which describes the hierachy of the widgets. Let's create, compile and test a sample program on host and after, cross-compile for iMX platform and check it running on a PDK i.MX31 Development kit. In order to develop on host PC, install libgtk2.0-dev typing: $sudo apt-get install libgtk2.0-dev
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-345322 
View full article
Download Linux kernel 2.6.29: $ wget -c http://www.kernel.org/pub/linux/kernel/v2.6/linux-2.6.29.tar.bz2 Extract this: $ tar jxvf linux-2.6.29.tar.bz2 Apply the patches: $ cd linux-2.6.29 Edit the file drivers/net/cs89x0.c adding: #include <mach/hardware.h> Export CROSS_COMPILE environmet: $ export PATH="$PATH:/opt/freescale/usr/local/gcc-4.1.2-glibc-2.5-nptl-3/arm-none-linux-gnueabi/bin/" $ export CROSS_COMPILE=arm-none-linux-gnueabi- Unselect all no essentials features: $ make ARCH=arm allnoconfig Start the configuration menu: $ make ARCH=arm menuconfig Change/Select the kernel options below. Select the MXC/iMX platform and iMX31ADS board: System Type ->             ARM system type -> (X) Freescale MXC/iMX-based             Freescale MXC Implementations  ->                            MXC/iMX Base Type -> (X) MX3-based                            MX3 Options  -> [*] Support MX31ADS platforms (NEW) Select ARM EABI standard to compile the kernel: Kernel Features  --->           [*] Use the ARM EABI to compile the kernel Add support to Linux Binary Format ELF: Userspace binary formats ->              [*] Kernel support for ELF binaries Add support to Network (TCP/IP): [*] Networking support  ->          Networking options  ->                          [*] Packet socket                          [*] Unix domain sockets                          [*] PF_KEY sockets                          [*] TCP/IP networking                                   [*] IP: kernel level autoconfiguration                                   [*]     IP: DHCP support Select network driver (CS89x0), serial driver and unselect VGA console: Device Drivers  ->                      [*] Network device support  --->                                      [*]   Ethernet (10 or 100Mbit)  --->                                             [*]   CS89x0 support                      Character devices  ->                              Serial drivers  --->                                       [*] IMX serial port support                                       [*]   Console on IMX serial port                      Graphics support  ->                             Console display driver support  --->                                        [ ] VGA text console Add support to NFS and support to use it as root file system: File systems  ->                            [*] Network File Systems (NEW)  ->                                        [*]   NFS client support                                        [*]     Root file system on NFS Compile the kernel: $ make ARCH=arm Copy the created zImage to tftp directory: $ cp arch/arm/boot/zImage /tftpboot/ Configure your RedBoot to boots with this kernel: load -r -b 0x100000 /tftpboot/zImage exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/nfs nfsroot=10.29.240.191:/tftpboot/rootfs ip=dhcp"
View full article
Dear All,       Our board is designed based on both EVK and HEG (Adeneo Embedded Home Energy Gateway), the ENET_FEC_RESET_B on EVK is replaced by LCD_D11 as it on HEG. We have re-config all pins based on i.mx28 BSP and successfully built by ltib. However, eth0 is not working due to "PHY is not found"! and we are still trying to figure it out.       The changes we apply on the BSP are(in mx28evk_pins.c): in static struct pin_desc mx28evk_fixed_pins[]:       the definition of LCD_D11 change to { .name = "LCD_D11", .id = PINID_LCD_D11, /* PHY reset pin*/ .fun = PIN_GPIO,      .voltage    = PAD_3_3V,      .strength = PAD_8MA,      .output     = 0, },      and replace all "PINID_ENET0_RX_CLK" in mx28evk_pins.c by "PINID_LCD_D11"      To prevent any possible interrupt, we also disable all LCD pins in both mx28_pins.h and mx28evk_pins.c since we don't have LCD.      Any comment/suggestion is highly appreciate! BR, TF
View full article
One chunk of the file system for the Linux Image i.MX 6Dual/6Quad Power Consumption Measurement Linux Image
View full article
The i.MX 6 D/Q L3.035_1.0.2 patch release is now available on the www.freescale.com ·         Files available # Name Description 1 L3.0.35_1.0.2_LDO_PATCH This patch release is based on the i.MX 6Dual/6Quad Linux   12.09.01 release. The purpose of this patch release is to manage the LDO and   PMIC ramp-up time correctly.
View full article
Computer On Module • Processor Freescale i.MX 6Quad, 1GHz • RAM 1GB DDR3 SDRAM 64-bit • ROM 4GB NAND Flash UP to 16GB • ROM 2M SPI Nor Flash ! • Power supply Single 5V • Size 40mm SO-DIMM • Temp.-Range          0 to + 95C (Consumer)         -20 to + 105C (Extended Consumer)         -40 to +105C (Industrial)         -40 to + 125C (Automotive) Key Features • 10/100Mbps Ethernet • One High Speed USB 2.0 ports • Full HD LCD controller, 24bpp • OpenGL ES 2.0 and OpenVG 1.1 hardware accelerators • Multi-format HD 1080p60 video decoder and 1080p30 encoder hardware engine • Two Camera Interfaces • NEON MPE coprocessor — SIMD Media Processing Architecture — dual, single-precision floating point execute pipeline • Unified 1MB L2 cache • Several interfaces: 5x UART, 2x SDIO, 1x SSI/AC97/I2S, 3x I2C, 2xCSPI • 3.3V I/O • 2x Controller Area Network (FlexCAN) • PCIe 2.0 (1-lane) OS Support     • Linux 3.0     • Android 4.2 Application:Media Tablet,Education Tablet PC,EBook,Automotive Infotainment,Aviation Infotainment,HMI,Portable Medical Instruments,IPTV,IP Phone,Smart Energy Systems,Intelligent industrial control systems For more information, please see Attachment We can provide a complete solution
View full article
i.MX Family Processor The i.MX family is designed for use in smartphones, wireless PDAs, gaming and many other mobile wireless applications, Freescale's i.MX Family of applications processors are a leading solution in today's smartphone environment. Based on ARM® core technology, the i.MX1, i. MXL, i.MX21, i.MX27 and i.MX31 are designed to offer low power consumption with real-world power performance and a high degree of integration to reduce your design time significantly. The i.MX Family supports a broad range of industry-leading platforms such as those based on the Microsoft® Window® CE operating systems, Palm® OS, Linux® OS, and Symbian™ operating systems. The i.MX portfolio is a leading solution in today's smartphone environment and is a central feature of Freescale's i.Smart smartphone reference design, providing power performance to our Innovative Convergence™ platforms. We are committed to continually expanding our Innovative Convergence platforms to support new technologies and new services as they emerge into the marketplace, such as advanced display technologies including smart panels; streaming video; multiple operating systems; and the far-reaching capabilities of the personal server.                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                              Processor CPU Speed FPU DMA Channels Embedded SRAM Flash Boot Video Acceleration 2D/3D Graphics i.MXS ARM920T 100MHz No 11 No NOR No No i.MXL ARM920T 200MHz No 11 No NOR DCT/iDCT Hardware Acceleration 2D/3D Graphics Through Software i.MX21S ARM926EJ-S 266MHz No 16 6KB NAND or NOR No No i.MX21 ARM926EJ-S 350MHz No 16 6KB NAND or NOR MPEG4 CIF 30 fps encoder and decoder 2D/3D Graphics with external accelerator i.MX27 ARM926EJ-S 400MHz No 16 45KB NAND or NOR H.264, MPEG-4, H.263 HW Enc/Dec; 24 fps VGA Full Duplex No i.MX31L ARM1136JF-S 532MHz Yes 32 16KB NAND or NOR MPEG4 VGA 30 fps Encode No i.MX31 ARM1136JF-S 532MHz Yes 32 16KB NAND or NOR MPEG4 VGA 30 fps Encode Integrated 2-D/3-D Processing Unit with OpenGL® Support i.MX35 ARM1136JF-S 532MHz Yes 32 128KB NAND, NOR, MMC/SD MPEG-4, H.264, ... Integrated 2D Processing Unit (Z160 @133MHz) with OpenVG® 1.1 Support i.MX51 ARM Cortex-A8 800MHz Yes 32 128kB NAND, NOR, MMC/SD MJPEG, MPEG-2, MPEG-4, H.263/264, VC-1, DivX, RV10 Integrated 2D (Z160 core @166MHz) and 3D (Z430 core @166MHz) Processing Unit with OpenVG® 1.1 and OpenGL ES® 2.0 / Direct3D Mobile Support i.MX53 ARM Cortex-A8 1GHz Yes 32 144kB NAND, NOR, MMC/SD MJPEG, MPEG-2, MPEG-4, H.263/264, VC-1, DivX, RV10 Integrated 2D and 3D (Z430 core @200MHz) Processing Unit with OpenVG® 1.1 and OpenGL ES® 2.0 / Direct3D Mobile Support For complete comparison click here. For more information about i.MX Family click here.
View full article
Question: To eliminate the need for pull-ups AND  pull-downs on the gpio boot override pins to save board space, does anyone know when in the boot rom that the GPIO pins are sampled and whether the internal Pull Downs are already enabled? Is this true for all the GPIO override pins? To just be able to provide an external Pull-up to specify boot options and NOT both pull-up and pull-down option. Can this be done? Answer: The pull-ups and pull-downs are active while POR_B is low (as defined in the datasheet). The pins are sampled on the 2 nd rising edge of RTC_XTALO before the rising edge of POR_B. As a caution, on-chip pull-up/downs are very weak and are primarily intended for controlling the pin (keeping it from logically wiggling) if the pin is not connected at all. If a pin is connected out to a trace, relaying on the on-chip PU/PD alone could be a little risky. Since the PU/PD is weak, it's possible to have noise coupled onto the pin. [Similar to Brett's comment above].
View full article
Question: The i.MX6 documentation gives several different values for the maximum frequency of the IPU’s HSP_CLK clock. What are the correct HSP_CLK maximum frequency values for the i.MX6 Dual/Quad and Solo/DualLite? Can HSP_CLK run at 270 MHz on both the DQ and SDL CPUs, but it’s not clear from the documentation if this is permitted. Maximum HSP_CLK frequencies listed in the reference manual (DQ😞 264 MHz (Table 9-2 (IPU IP Parametric Table), Table 9-5 (IPU Clock Sources)) 266 MHz (Table 18-3 (System Clock Frequency Values)) Maximum HSP_CLK frequencies listed in the reference manual (SDL😞 270 MHz (Table 9-2 (IPU IP Parametric Table), Table 9-5 (IPU Clock Sources), Table 18-3 (System Clock Frequency Values)) Answer: Referring to Figure 18-2, IPU1_HSP_CLK_ROOT may be selected to have 1 of 4 sources. These sources are highlighted in yellow on the northwest corner of the page and the previous paragraph states these are max values. Possible sources are 540, 528, 396, and 480 MHz. The 480 MHz is divided by 4 before the selector, so winds up being 120 MHz. Per the diagram, these are all divided by 2 for IPU1_HSP_CLK_ROOT. The result is 270, 264, 198, and 60 MHz choices. Therefore, the max for IPU1_HSP_CLK_ROOT is 270 MHz for DQ. MX6D/Q and MX6S/DL are different with respect to max HSP_CLK frequency. MX6D/Q = 264 MHz max MX6S/DL = 270 MHz max
View full article
Random Number Generator - RNGA Download rng-tools: http://downloads.sourceforge.net/sourceforge/gkernel/rng-tools-2.tar.gz This tool tests the link between a random number generator hardware and the kernel's PRNG (pseudo-random number generator). ./ltib -m shell LTIB> cd rpm/BUILD/ LTIB> cp ~/hwrandom/rng-tools-2.tar.gz . LTIB> tar zxvf rng-tools-2.tar.gz LTIB> cd rng-tools-2 LTIB> ./configure --host=arm-linux LTIB> make LTIB> sudo cp rngtest /tftpboot/ltib/home/ Restart your board and execute this command in the board's console: $ cat /dev/hwrng | /home/rngtest -c 1000
View full article