i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
Question: What is the correct path for the buffer generated by the GPU and sent to the display? When referring to Linux Manual Chapter 5 "Image Processing Unit (IPU) Drivers" and sect.37.5.68 "Current Buffer Register 0". i.MX6DQ Reference Manual (rev.1  4/2013) and further on text and associated with buffer events interrupts. A lot of printouts in the mxc_ipuv3_fb.c file have been added and in other files located in the drivers/video/mxc/ directory and still unable to capture the interrupt generated by the IPU. An open GL buffer (using the GLES and EGL) is generated with the frame buffer mechanism to a monitor connected to the HDMI output on the evaluation board. Direct it to /dev/fb0. The following functions are used to create EGL context fbGetDisplayByIndex(0) fbCreateWindow(…); Everything works and openGL on the monitor can be seen. To measure how long it takes for the data to be sent to the display/monitor after the buffer is ready in the GPU, can it be done in the IPU if where it is performed is known? Where is the exact location where the interrupt can be captured. The ltib on the Ubuntu 12.04 OS (the alsa-utils package was also installed using some patch)) is installed. Answer: GPU EGL swapbuffer is asyncronous. It means when you call swapbuffer it will not be displayed immediately. If will just flush the command buffer and when the GPU completes the frame, it will be displayed to the scree, To make sure the frame is complete, use glFinish after eglswapbuffer. Also please try with simple program rather using GPU driver to measure time to display on the screen. Swapbufferinterval will work when FB_MULTI_BUFFER = 2. By default it will be 1.
View full article
The i.MX53 family of processors represents Freescale's next generation of advanced multimedia and power-efficient implementation of the ARM Cortex™-A8 core with core processing speeds up to 1.2 GHz. It is optimized for both performance and power to meet the demands of high-end, advanced applications. Ideal for a broad range of applications in the consumer, automotive, medical and industrial markets, the i.MX53 includes an integrated display controller, full HD capability, enhanced graphics and connectivity features. i.MX Family Comparison Product Information on Freescale.com i.MX534 Multimedia Applications Processor i.MX535 Multimedia Applications Processor i.MX536 Multimedia Applications Processor i.MX537 Multimedia Applications Processor Evaluation/Development Boards and Systems i.MX53 Quick Start Board Android How to enable WIFI support for iMX53 QSB Android IMX53 QSB android recovery mode Linux I.MX53 QSB Board Get Started How to flash a 4GB SD Card with the image used in training Enabling Dual Display in UBUNTU with the iMX53 QSB @running_dual_display SABRE Platform for Tablets based on i.MX53 Linux i.MX53 ARD Dual LVDS Enabling Dual LVDS panels i.MX53 USB Eth NFS Using an USB/Eth adapter to boot NFS User Applications i.MX53 Qt LVDS display Touch on Qt with LVDS display Embedded Software and Tools Android OS for i.MX Applications Processors i.MX53 Current Software Updates and Releases Partners / 3rd-Party Development Tools Rainbow-G11D:  i.MX53 Development Kit (iWave Embedding Intelligence) STKa53:  Starterkit STKa53 (Technology in Quality) DS-5:  ARM Development Studio 5 (ARM) Additional Resources Board Bring-up and DDR Initialization Tools Building QT5 for i.MX53 Change AUDMUX src_port causes "imx_ssi_irq mxc_ssi SISR 8003a3 SIER 180100 fifo_errs=XXXX" ConnectCore® i.MX53 / Wi-i.MX53 by Digi International Develop a Simple OpenVG Application Under Linux: Tutorial Embedded i.MX5x Application Development Kit for Android -$199 HDMI Audio Setting How to Enable the souphttpsrc Plugin on i.MX53 i.MX53 ARD Dual LVDS Imx53-fastboot-example i.MX53 Memory Calibration Script (AN4466) i.MX53 QSB Android Recovery Mode I.MX53 QSB Board Get Started i.MX53 QSB Board Video IMX53 QSB enable WIFI android i.MX53 QSB Ubuntu Dual Display i.MX53 Quick Start Board IMX53 SABRE AI i.MX53 Start-R Lab Exercise - Prof. Massimo Violante Politecnico of Torino i.MX53 Start-R Lab Exercise - Developing a loadable kernel module to manage GPIOs in i.MX53QSB i.MX53 USB Eth NFS i.MX53 Qt LVDS Display NOVPEK i.MX53 by NovTech Running Dual Display on i.MX53QSB bin2txt.pyw (U-boot splash screen support)
View full article
The document to descript change the u-boot environment variables under the Linux rootfs.  Also provide a demo on i.MX6ull evk of sdcard mirror.  Linux fw_printenv fw_setenv to access U-Boot's environment variables.pdf  --- the document fw_printenv_fw_setenv_demo_iMX6ullevk_L4.14.98_2.0.0_ga.sdcard  --- demo sdcard mirror
View full article
Make boot SD Card for imx-android-r13.4-20121128 1. Extract imx-android-r13.4-20121128 2. Check mount device  @Disk Util     My case SD Card : /dev/sdb 3. Insert the uSD Card    Use 16GByte SD Card Cat10 4. Android/imx-android-r13.4-20121128$./device/boundary/mksdcard.sh /dev/sdb 5. Wait about 5 minutes. Finish!
View full article
Attached is a chunk of the filesystem for the Linux Image https://community.freescale.com/docs/DOC-93887
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-345148 
View full article
FAQ Question: I receive the following error message when compiling GTK2 using LTIB" Making all in demos make[2]: Entering directory `/home/ltib/rpm/BUILD/gtk+-2.14.3/demos' no --raw --build-list \         apple_red  ./apple-red.png \                 gnome_foot ./gnome-foot.png \         > test-inline-pixbufs.h \ || (rm -f test-inline-pixbufs.h && false) /bin/sh: no: command not found make[2]: *** [test-inline-pixbufs.h] Error 1 make[2]: Leaving directory `/home/ltib/rpm/BUILD/gtk+-2.14.3/demos' make[1]: *** [all-recursive] Error 1 make[1]: Leaving directory `/home/ltib/rpm/BUILD/gtk+-2.14.3' make: *** [all] Error 2 error: Bad exit status from /home/ltib/tmp/rpm-tmp.69212 (%build) Answer: Some packages on your host are missing, install the following packages: For deb distributions: sudo apt-get install libgtk2.0-dev or For Fedora distributions: sudo yum install gtk2-devel IMPORTANT: After install the package above, be sure to remove the installed GTK package on your ltib: On your LTIB directory: rm -rf rpm/BUILD/gtk+-2.14.3/ Question: I receive the following error message when booting through NFS: "Root-NFS: Server returned error -13 while mounting /tftpboot/ltib" Answer: Probabilty you remake your rootfs and forgot to restart NFS server. To solve this issue the command: "service nfs restart" Question: I am receiving "error: cannot open Name index using db3" when installing LTIB on new Ubuntu 9.10 Answer: Edit the file "ltib" and modify line 2428 to: $cf->{rpm}           = "rpm --force-debian"; Question: I receive the error message "Cannot create lockfile. Sorry." when I try to open minicom. Answer: This error message is generated because your user doesn't have permission to create a lock file in /var/lock. Change /var/lock permission: # chmod 777 /var/lock Question: I receive the error message "cannot open /dev/ttyS0: Permission denied" when I try to open minicom. Answer: This error message is generated because your user doesn't have permission to open /dev/ttyUSB0. Change /dev/ttyUSB0 permission: # chmod 777 /dev/ttyS0 Question: Compilation of e2fsprogs package or others packages with dependencies like Qtopia using LTIB in Debian derived linux system like Ubuntu makes an error like: make[1]: Leaving directory `/home/daiane/LTIB/L2.6.24_1.2.1_SDK_042008/rpm/BUILD/e2fsprogs-1.34/tests/progs' making all in po make[1]: Entering directory `/home/daiane/LTIB/L2.6.24_1.2.1_SDK_042008/rpm/BUILD/e2fsprogs-1.34/po' : --update cs.po e2fsprogs.pot rm -f cs.gmo && : -c --statistics -o cs.gmo cs.po mv: cannot stat `t-cs.gmo': No such file or directory make[1]: *** [cs.gmo] Error 1 make[1]: Leaving directory `/home/daiane/LTIB/L2.6.24_1.2.1_SDK_042008/rpm/BUILD/e2fsprogs-1.34/po' make: *** [all-progs-recursive] Error 1 error: Bad exit status from /home/daiane/LTIB/L2.6.24_1.2.1_SDK_042008/tmp/rpm-tmp.66904 (%build) Answer: This error is caused by lack of the new version of package gettext. Install the gettext. For Ubuntu, the command line is: sudo apt-get install gettext But LTIB just recognize the existence of this package if it was installed before the LTIB installation. So, reinstall the LTIB. Question Compiling LTIB I got this error message: checking for glib-genmarshal... no configure: error: Could not find a glib-genmarshal in your PATH error: Bad exit status from /home/alan/ltib/tmp/rpm-tmp.48168 (%build) Answer: This error happen when you don't have glib2.0-dev in your system. To Ubuntu execute: sudo apt-get install libglib2.0-dev Question: How to convert an ELF binary to raw ARM binary? Answer: arm-none-linux-gnueabi-objcopy -O binary test.elf test.bin Question: How to inform to kernel to print all message on screen? Answer: echo 8 > /proc/sys/kernel/printk Question: How to disassembly an ARM binary? Answer: arm-none-linux-gnueabi-objdump -b binary -m arm -D test.bin Question: RedBoot returns invalid parameter: RedBoot> load -r -b 0x100000 zImage Using default protocol (TFTP) Can't load 'zImage': invalid parameter Answer: Verify if your tftp server is running correctly. If so, then verify if RedBoot network is configured correctly. You can use ping command to verify if communication with computer is working. Insert non-formatted text here Configure RedBoot to not use script and configure network: RedBoot> ^C RedBoot> fc Run script at boot: false Use BOOTP for network configuration: true. Update RedBoot non-volatile configuration - continue (y/n)? y ... Read from 0x07ee0000-0x07eff000 at 0xa1fe0000: . ... Erase from 0xa1fe0000-0xa2000000: . ... Program from 0x07ee0000-0x07f00000 at 0xa1fe0000: . RedBoot> Reset the board and then load the image Question: How can I test GPIO using a very simple test? Answer: You can find a very simple test here
View full article
fw_env.config # Configuration file for fw_(printenv/saveenv) utility. # Up to two entries are valid, in this case the redundant # environment sector is assumed present. # Notice, that the "Number of sectors" is ignored on NOR.               # MTD device name Device offset Env. size Flash sector size Number of sectors #/dev/mtd1 0x0000 0x4000 0x4000 #/dev/mtd2 0x0000 0x4000 0x4000 # NAND example /dev/mtd0 0x80000 0x40000 0x20000 2
View full article
Trace the malloc and expose violate access to freed memory Introduction Libc has a malloc debug framework for difference debugger. Each debugger takes as a libraries, and override the default malloc/free/calloc/realloc/, hooked before calling the real functions. NOTE: This tip assume that you are working with an eng or userdebug build of the platform, not on a production device. Trace the low level malloc/free in bionic Bionic has a malloc debugger called leak debugger, which can record all the malloc/free in low level. And developers can use ddms on host to check each block of memory on heap by malloc. And ddms support convert caller function address to name conver. That makes easy for us to check which component, which function allocated for how many memories. You can turn on memory tracking with debug level 1: $ adb shell setprop libc.debug.malloc 1 $ adb shell stop $ adb shell start You need to restart the runtime so that zygote and all processes launched from it are restarted with the property set. Now all Dalvik processes have memory tracking turned on. You can look at these with DDMS, but first you need to turn on its native memory UI: Open ~/.android/ddms.cfg Add a line "native=true" Upon relaunching DDMS and selecting a process, you can switch to the new native allocation tab and populate it with a list of allocations. This is especially useful for debugging memory leaks. NOTE: to solve the module symbols, please export two env on HOST: $ export PATH=$PATH:<android src>/prebuilt/linux-x86/toolchain/arm-linux-androideabi-4.4.x/bin $ export ANDROID_PRODUCT_OUT=<android src>/out/target/product/<platform> Expose the memory access to freed area In this release he Electric Fence 2.2.0 has been ported to Android. it's also a memory debugger tool as above leak debugger. It helps you detect two common programming bugs: software that overruns the boundaries of a malloc() memory allocation, and software that touches a memory allocation that has been released by free(). It will dump the call stack and mmap of the process, if the malloc/free is not called with correct parameters. It will also make a segment fault, when applications want to access the address which is freed. The usage of efence is almost same as above, which we define it's debug level to 15: $ adb shell setprop libc.debug.malloc 15 After setting this property, you can run your applications, and if there's any memory leakage, logcat will show information. Example: Access the memory, which has been freed already: root@android:/data # setprop libc.debug.malloc 15 I/libc    ( 4136): setprop using MALLOC_DEBUG = 1 (leak checker) root@android:/data # ./memtest I/libc    ( 4138): ./memtest using MALLOC_DEBUG = 15 (efence) F/libc    ( 4138): Fatal signal 11 (SIGSEGV) at 0x4015bff4 (code=2) I/DEBUG  ( 3856): *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** *** I/DEBUG  ( 3856): Build fingerprint: 'freescale/sabresd_6dq/sabresd_6dq:4.0.4/R13.5-rc1/eng.b03824.20120711.11133 8:eng/test-keys' I/DEBUG  ( 3856): pid: 4138, tid: 4138  >>> ./memtest <<< I/DEBUG  ( 3856): signal 11 (SIGSEGV), code 2 (SEGV_ACCERR), fault addr 4015bff4 I/DEBUG  ( 3856):  r0 00000000  r1 00000002  r2 40151c6c  r3 00000000 I/DEBUG  ( 3856):  r4 4015bff4  r5 bec75a54  r6 00000001  r7 bec75a5c I/DEBUG  ( 3856):  r8 00000000  r9 00000000  10 00000000  fp 00000000 I/DEBUG  ( 3856):  ip 00000000  sp bec75a20  lr 40133f8f  pc 0000a554  cpsr 60000010 I/DEBUG  ( 3856):  d0  203f810033915fe5  d1  0000000000000000 I/DEBUG  ( 3856):  d2  0000000000000000  d3  0000000000000000 I/DEBUG  ( 3856):  d4  0000000000000000  d5  0000000000000000 I/DEBUG  ( 3856):  d6  0000000000000000  d7  204cb48d00000000 I/DEBUG  ( 3856):  d8  0000000000000000  d9  0000000000000000 I/DEBUG  ( 3856):  d10 0000000000000000  d11 0000000000000000 I/DEBUG  ( 3856):  d12 0000000000000000  d13 0000000000000000 I/DEBUG  ( 3856):  d14 0000000000000000  d15 0000000000000000 I/DEBUG  ( 3856):  d16 41c0265a46a47ae1  d17 3f50624dd2f1a9fc I/DEBUG  ( 3856):  d18 41c9c8aff2800000  d19 0000000000000000 I/DEBUG  ( 3856):  d20 0000000000000000  d21 0000000000000000 I/DEBUG  ( 3856):  d22 0000000000000000  d23 0000000000000000 I/DEBUG  ( 3856):  d24 0000000000000000  d25 0000000000000000 I/DEBUG  ( 3856):  d26 0000000000000000  d27 0000000000000000 I/DEBUG  ( 3856):  d28 0000000000000000  d29 0000000000000000 I/DEBUG  ( 3856):  d30 0000000000000000  d31 0000000000000000 I/DEBUG  ( 3856):  scr 00000010 I/DEBUG  ( 3856): I/DEBUG  ( 3856):          #00  pc 0000a554  /data/memtest I/DEBUG  ( 3856):          #01  pc 00016834  /system/lib/libc.so (__libc_init) I/DEBUG  ( 3856): I/DEBUG  ( 3856): code around pc: I/DEBUG  ( 3856): 0000a534 e3a0000a ebfff8d1 e3a01001 e1a00004  ................ I/DEBUG  ( 3856): 0000a544 e5c4100a ebfff8d9 e3560001 e3a03000  ..........V..0.. I/DEBUG  ( 3856): 0000a554 e5c43000 0a000064 e59f21f0 e2857004  .0..d....!...p.. I/DEBUG  ( 3856): 0000a564 e5954004 e08f1002 e1a00004 ebfff8c0  .@.............. I/DEBUG  ( 3856): 0000a574 e3500000 0a00003f e59fc1d4 e1a00004  ..P.?........... I/DEBUG  ( 3856): I/DEBUG  ( 3856): code around lr: I/DEBUG  ( 3856): 40133f6c 68200701 0001f020 454e1046 2e00d018  .. h ...F.NE.... I/DEBUG  ( 3856): 40133f7c 2102da01 1c81e000 43394338 f7eb4622  ...!....8C9C"F.. I/DEBUG  ( 3856): 40133f8c 4605ed56 d1ec2800 da062e00 0101f008  V..F.(.......... I/DEBUG  ( 3856): 40133f9c f06f4620 f7ea4200 4628e8d4 87f0e8bd  Fo..B....(F.... I/DEBUG  ( 3856): 40133fac eff0f7e9 6003234b 30fff04f bf00e7f6  ....K#.`O..0.... I/DEBUG  ( 3856): I/DEBUG  ( 3856): memory map around addr 4015bff4: I/DEBUG  ( 3856): 40150000-4015a000 I/DEBUG  ( 3856): 4015a000-4015d000 I/DEBUG  ( 3856): 4015d000-4015e000 I/DEBUG  ( 3856): I/DEBUG  ( 3856): stack: I/DEBUG  ( 3856):    bec759e0  00000000 I/DEBUG  ( 3856):    bec759e4  00000000 I/DEBUG  ( 3856):    bec759e8  00000000 I/DEBUG  ( 3856):    bec759ec  4012090f  /system/lib/libefence.so I/DEBUG  ( 3856):    bec759f0  4015a014 I/DEBUG  ( 3856):    bec759f4  00002000 I/DEBUG  ( 3856):    bec759f8  00000004 I/DEBUG  ( 3856):    bec759fc  40120df1  /system/lib/libefence.so I/DEBUG  ( 3856):    bec75a00  4015bff4 I/DEBUG  ( 3856):    bec75a04  bec75a54  [stack] I/DEBUG  ( 3856):    bec75a08  00000001 I/DEBUG  ( 3856):    bec75a0c  bec75a5c  [stack] I/DEBUG  ( 3856):    bec75a10  00000000 I/DEBUG  ( 3856):    bec75a14  400d9167  /system/lib/libc.so I/DEBUG  ( 3856):    bec75a18  df0027ad I/DEBUG  ( 3856):    bec75a1c  00000000 I/DEBUG  ( 3856): #00 bec75a20  00008924  /data/memtest I/DEBUG  ( 3856):    bec75a24  bec75a54  [stack] I/DEBUG  ( 3856):    bec75a28  00000001 I/DEBUG  ( 3856):    bec75a2c  bec75a5c  [stack] I/DEBUG  ( 3856):    bec75a30  00000000 I/DEBUG  ( 3856):    bec75a34  400d9837  /system/lib/libc.so I/DEBUG  ( 3856): #01 bec75a38  00000000 I/DEBUG  ( 3856):    bec75a3c  00000000 I/DEBUG  ( 3856):    bec75a40  00000000 I/DEBUG  ( 3856):    bec75a44  00000000 I/DEBUG  ( 3856):    bec75a48  00000000 I/DEBUG  ( 3856):    bec75a4c  b00046ef  /system/bin/linker I/DEBUG  ( 3856):    bec75a50  00000001 I/DEBUG  ( 3856):    bec75a54  bec75b79  [stack] I/DEBUG  ( 3856):    bec75a58  00000000 I/DEBUG  ( 3856):    bec75a5c  bec75b83  [stack] I/DEBUG  ( 3856):    bec75a60  bec75b8f  [stack] I/DEBUG  ( 3856):    bec75a64  bec75ba2  [stack] I/DEBUG  ( 3856):    bec75a68  bec75bc5  [stack] I/DEBUG  ( 3856):    bec75a6c  bec75bde  [stack] I/DEBUG  ( 3856):    bec75a70  bec75c08  [stack] I/DEBUG  ( 3856):    bec75a74  bec75c20  [stack] I/DEBUG  ( 3856):    bec75a78  bec75c57  [stack] I/DEBUG  ( 3856):    bec75a7c  bec75c61  [stack] I/BootReceiver( 3551): Copying /data/tombstones/tombstone_00 to DropBox (SYSTEM_TOMBSTONE) D/dalvikvm( 3551): GC_CONCURRENT freed 398K, 10% free 8805K/9735K, paused 3ms+5ms [2] + Segmentation fault  ./memtest
View full article
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343007 
View full article
Q: What is quality level of IBIS file? In chapter 8.6 in IMX6DQ6SDLHDG (Rev.0). It says the following about quality assurance. ===== All models (GPIO, DDR, LVDS, MLB) have passed the following checks: • IBISCHK without errors or unexplained warnings • Data for basic simulation checked • Data for timing analysis checked • Data for power analysis checked • Correlated against Spice simulations Validation reports can be provided upon demand. ==== A: In addition, please see http://www.vhdl.org/pub/ibis/quality_wip/checklist/Using_IQ_2.0_checklist.pdf. This document says about quality level. According to these information, the IBIS quality level is IQ4 (IQ3 + data for power  analysis checked) + "Correlated against Spice simulations". This document was generated from the following discussion: IBIS QUALITIY LEVEL
View full article
To fix LCD problem: Download DirectFB patches (click here). Copy patches and kernel spec to LTIB: tar zxvf DirectFB-patches-specs.tar.gz cd specs cp kernel-imx31_3stack-2.6.24-DirectFB-LCD-fix.patch /opt/freescale/pkgs/ cp kernel.spec.in ~/ltib-imx31pdk-r14/config/platform/imx/ Remove old kernel: ~/ltib-imx31pdk-r14$ rm -rf rpm/BUILD/linux* Issue LTIB to decompress kernel and apply patches: ~/ltib-imx31pdk-r14$ ./ltib -p kernel -m prep You will see at end: + echo Patch #1 (kernel-imx31_3stack-2.6.24-DirectFB-LCD-fix.patch): Patch #1 (kernel-imx31_3stack-2.6.24-DirectFB-LCD-fix.patch): + patch -p1 -s + exit 0 Build time for kernel: 21 seconds It means which kernel-imx31_3stack-2.6.24-DirectFB-LCD-fix.patch was applied correctly! Now compile your kernel: ~/ltib-imx31pdk-r14$ ./ltib -p kernel -m scbuild Install it on your rootfs: ~/ltib-imx31pdk-r14$ ./ltib -p kernel -m scdeploy To fix Touch-Screen Copy specs to LTIB: cd specs cp tslib.spec ~/ltib-imx31pdk-r14/dist/lfs-5.1/tslib/ cp DirectFB.spec ~/ltib-imx31pdk-r14/dist/lfs-5.1/DirectFB/ Remove old directories: ~/ltib-imx31pdk-r14$ rm -rf rpm/BUILD/tslib-1.0/ ~/ltib-imx31pdk-r14$ rm -rf rpm/BUILD/DirectFB-1.1.0/ Edit your pkg_map and change tslib order. DirectFB needs tslib, then this lib needs be compiled first: [alan@localhost ltib-imx31pdk-r14]$ vi config/userspace/pkg_map ... PKG_TSLIB                                      = tslib PKG_DIRECTFB                               = DirectFB PKG_DIRECTFB_EXAMPLES            = DirectFB-examples ... Now run: alan@armagedon:~/ltib-imx31pdk-r14$ ./ltib -c Then select DirectFB and tslib packages. To test Touch-Screen mx31# mknod /dev/input/tslib0 c 13 65 mx31# export TSLIB_TSDEVICE=/dev/input/tslib0 mx31# rm -f /etc/pointercal mx31# ts_calibrate mx31# df_window
View full article
How To Understand JTAG BSDL File This example explains how to understand the BSDL file in order to create an OpenOCD configure file. IR Len That information can be retrieved directly: attribute INSTRUCTION_LENGTH of imx_device: entity is 5; This means that IR Len is 5, then in OpenOCD config it will be informed this way: -irlen 5 IR Capture The IR Capture also can be retrieved directly: attribute INSTRUCTION_CAPTURE of imx_device : entity is "XXX01"; This means that IR Capture is 1, then in OpenOCD config it will be informed this way: -ircapture 0x1 IR Mask The IR Mask is based on IR Len size. Just create a binary number with "IR Len" bits 1. If the IR Len is 4 then the IR Mask will be 0xF (1111). Case the IR Len is 5 the IR Mask will be 0x1F (11111). In this BSDL example (IR Len = 5) the OpenOCD config needs to inform the IR Mask this way: -irmask 0x1f TAP ID attribute IDCODE_REGISTER  of imx_device : entity is     "0010"            & -- Version     "000110"          & -- Design Center Number     "0100000001"      & -- Sequence Number     "00000001110"      & -- Manufacturer Identity     "1";                -- IEEE 1149.1 Requirement This code can be converted directly to TAP ID: Binary: 0010-0001-1001-0000-0001-0000-0001-1101 Hexadecimal: 2-1-9-0-1-0-1-D Then in OpenOCD configure you will create: if { [info exists SDMATAPID ] } {   set _SDMATAPID $SDMATAPID } else {   set _SDMATAPID 0x2190101d } The final configure line will be: jtag newtap $_CHIPNAME smda -irlen 5 -ircapture 0x1 -irmask 0x1f -expected-id $_SDMATAPID
View full article
Application Note covering how to get the Silex SX-SDCAN working with the Sabre-SD i.MX6 Evaluation kit.
View full article
Introduction The SABRE Board for Smart Devices Based on the i.MX 6 Series is an evalutaion board featuring the i.MX6 Quad Core Cortex-A9 processor. Freescale ported the Linux Operating System (as of this writing version 3.0.35) and the Board Support Package (BSP) containing the Linux Kernel, build system called LTIB, GCC compiler tools, boot loader, u-boot, and root file system is available for download, install, and build. LTIB is a perl script and is the acroynm for Linux Target Image Builder. This document describes setting up a CentOS 6.3 64-bit host in a virtual machine for using the BSP and running the images on i.MX6Q-SDB evaluation board. References Description Reference CentOS 6.3 LiveCD installed in a virtual machine from virtual box. http://centos.org CentOS-6.3-x86_64-LiveCD.iso 9953ff1cc2ef31da89a0e1f993ee6335 Virtual Box - A Virtual Machine used for creating the CentOS host. Virtual Box installed on Windows 7 64-bit Pro, then create the VM. Allocated 20 GB Hard disk and 1 MB RAM. The steps for installations are found at the virtual box web site. http://www.virtualbox.org The BSP provides, a build system called ltib, GNU tools, U-Boot, Linux Kernel, and root file system: Download archive from http://freescale.com/sabresdb L3.0.35_12.09.01.0_GA_source.tar.gz 5ab4198278e92e03be74ca602227afad Document Conventions Bold lines are Linux commands and edits run on CentOS. The '$' indicates running the command as a regular user The '#' indicates running the command as root user. CentOS Host Setup For this example a virtual machine is used, however a dedicated PC running only CentOS linux could be used. 1. Add user login to sudo'ers file           Login as user root and run the visudo command          # visudo           Add the following line and save the file:           user     ALL=(ALL)     ALL 2. Update the system packages:           $ sudo yum udpate 3. Install package for "ltib" operations:           $ sudo yum install make gcc gcc-c++ kernel-devel bison libuuid-devel ncurses-devel zlib-devel lzo-devel intltool libtool tcl rpm-build perl-ExtUtils-MakeMaker ld-linux.so.2 zlib-1.2.3-27.el6.i686 4. Update sudo'ers file for supporting ltib rpm           $ sudo visudo           Add the following line and save the file:           user     ALL=NOPASSWD: /bin/rpm,/opt/freescale/ltib/usr/bin/rpm Install BSP The sources are in a tar gziped archive file which is downloaded from http://freescale.com/sabresdb, selecting the Software & Tools tab then expanding Run-time Software in the middle of the page. A free login is required for download which can be registered for by selecting the Login at the top right of the freescale.com page. Once downloaded, verify the md5 checksum (see references above for the value). $ mkdir ~/imx6 $ tar -zxf L3.0.35_12.09.01.01_GA_source.tar.gz -C ~/imx6 $ cd ~/imx6/*source $ ./install Read and accept the licensing information. Choose a directory to install too, for this example entered .. which is the parent directory. Build the i.MX6Q SDB $ cd ~/imx6/ltib $ ./ltib After some time (depends on how fast your host computer is) the menuing system is shown which allows you to select build configurations. The second screen selects the development platform which is imx6q for the SDB. For this example the Min profile is chosen which is the default. Use the arrow keys to move and the enter key to select. The space bar selects/deselects an entry. Use the right arrow key to move to <Exit> and press the enter key. The save dialog box is presented, save. The next menu is the iMX6x Base Boards which leaving all as default except for the U-boot board selection which is mx6q_sabresd for the SDB. Save and exit. Images When ltib completes, the images are found in <ltib>/rootfs/boot. Bootloader = u-boot.bin Linux Kernel = uImage File system = </ltib>/rootfs
View full article
How To Convert RealView CP15 Config To OpenOCD? # arm11 mcr <jtag_target> <coprocessor> <opcode 1> <CRn> <CRm> <opcode 2> <32bit value to write> Setting CP15 Control RealView: setreg @CP15_CONTROL=0x00050078 OpenOCD: arm11 mcr 1 15 0 1 0 0 0x00050078 Setting CP15 Peripheral Memory Remap RealView: setreg @CP15_PERIP_MEM_REMAP=0x40000015 OpenOCD: arm11 mcr 1 15 0 15 2 4 0x40000015
View full article
Attached is a chunk of the Filesystem needed to construct the Linux Image https://community.freescale.com/docs/DOC-93887
View full article
Splash Screen on U-boot for i.MX25 PDK Having a bitmap on the LCD a few seconds after boot is a requirement on several embedded systems, u-Boot supports this feature. However, currently, the code provided on Freescale's BSP only implements support for the LCD controller on Linux. This page provides instructions to add support for the LCDC on the u-boot. 1 - Install Freescale i.MX25 BSP, SDK 1.7 It is available on www.freescale.com. If needed follow the getting started section instructions. 2 - Update u-boot source After installing the BSP and running LTIB for the first time, it's time to update u-boot: - Download u-Boot patch and spec file. - Replace the file "u-boot.spec.in" located at <ltib_path>/config/platform/imx by the one downloaded - Copy the "u-boot-2009.08-1273860148.patch" downloaded to /opt/freescale/pkgs 3 - Extract and rebuild u-boot - To extract the source and aply the patch run: <Ltib_path>$ ./ltib -p u-boot -m prep - Now Build:     <Ltib_path>$ ./ltib -p u-boot -m scbuild    After completing this step an u-Boot binary (u-boot.bin) will be saved at <ltib_path>/rpm/BUILD/u-boot-2009.08 4 - Program the SD card Program a SD card with the new u-Boot binary and a bitmap image to be displayed. Insert the SD and run:      $sudo dd if=<ltib_path>/rpm/BUILD/u-boot-2009.08/u-boot.bin of=/dev/mmcblk0 bs=512 "/dev/mmcblk0" should replaced according to your host, use "dmesg" after inserting the SD to find out where is the SD on your host. Unmount it before issuing the dd command. $sudo dd if="your_image".bmp of=/dev/mmcblk0 bs=512 seek=608 Argument seek 608, skips the first 608 blocks of the SD (608x512) where the uboot is stored. If you need to relocate the image, update also the environment variable "splashimage_mmc_init_block", see step 6. 5 - Boot Boot the image from the SD. Personality Board settings:   12345678 SW22 -> 00000000 SW21 -> 11000000    Debug Board settings: SW5,6,7,8,9,10 -> OFF      12345678 SW4 -> 10000001 Turn on the board and stop at u-boot prompt: MX25 U-Boot > 6 - u-Boot environment variables Update u-Boot environment variables for the splash screen to work: The address in memory to load the splash screen from: MX25 U-Boot > setenv splashimage 0x80800000 The SD device on the board: MX25 U-Boot > setenv splashimage_mmc_dev 0 The block on the SD where the bitmap is stored, this must match the block on step 4. MX25 U-Boot > setenv splashimage_mmc_init_block 0x260  The amount in blocks to be read from the SD card, this depends on the bitmap size, i.e. for a 308278 bytes bitmap, 0x2B5 blocks are enough on a 512 bytes per block SD, (308278 / 512). MX25 U-Boot > setenv splashimage_mmc_blkcnt 0x2b5 The SD card block size in bytes: MX25 U-Boot > setenv splashimage_mmc_blksize 512 Save the environment variables: MX25 U-Boot > saveenv Now reboot the board and you should see the splash screen on the LCD. 7 - Booting Linux When Linux takes control of the board it initializes the LCD controller and Framebuffer again. To maintain the splash screen on the LCD you can replace the Linux Logo with the figure used for the splash screen, the side effect is a blink when Linux takes over the LCDC. To achieve this, create a new image in Gimp and save it as ".ppm". Copy it to Linux "logo" folder <ltib_path>/rpm/BUILD/linux-2.6.31/drivers/video/logo Run: $ ppmquant -mapfile clut_vga16.ppm "my_image.ppm" | pnmnoraw > logo_linux_vga16.ppm where: logo_linux_vga16.ppm is the current logo being used by Linux. Recompile the kernel and boot it.
View full article
Hello,   recently I'm running CTS test on MX6Q SabreSD to fix some of the issues my customer found, and found that "factory reset" is an important step during the test-environment setup but not mentioned in i.MX CTS test report.   "Factory reset" is need on official CTS page: Setting up CTS | Android Open Source Project     Without factory reset, the CTS test result in "android.core.tests.libcore.package.libcore" package looks like: There are total 8 failed items.     If we run "factory reset" before conduct the CTS test in in "android.core.tests.libcore.package.libcore" package, only 2 failed items found as below:   PS: and those 2 failed items can be waived, according to the test-house of CTS tests. PS1: the test reports of are also attached.       Please do run "factory reset" before CTS test, verified working on 4.2.2 and should also work on the version above according to the pages I found on Google when trying to fix this issue. Unfortunately "factory reset" is not documented in the environment setup process in i.MX CTS test report, you will need this if you are following the steps in i.MX CTS test report.   Best regards, Jim.
View full article
Hi All I make fsl-image-qt5 in yocto. make command: $ MACHINE=imx6slevk source fsl-setup-release.sh -b build -e fb $ bitbake fsl-image-qt5 However, I couldn't make meta-toolchin-qt5 in yocto. The error is as follows. > | WARNING: exit code 1 from a shell command. > | ERROR: Function failed: do_configure (log file is located at /opt/yocto_build/yocto_fsl-bsp-imx6slevk/fsl-release-bsp/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/qtdeclarative/5.3.2-r0/temp/log.do_configure.3411) > ERROR: Task 771 (/opt/yocto_build/yocto_fsl-bsp-imx6slevk/fsl-release-bsp/sources/meta-qt5/recipes-qt/qt5/qtdeclarative_5.3.2.bb, do_configure) failed with exit code '1' > NOTE: Tasks Summary: Attempted 1235 tasks of which 1234 didn't need to be rerun and 1 failed. > No currently running tasks (1234 of 3376) > > Summary: 1 task failed: >   /opt/yocto_build/yocto_fsl-bsp-imx6slevk/fsl-release-bsp/sources/meta-qt5/recipes-qt/qt5/qtdeclarative_5.3.2.bb, do_configure > Summary: There was 1 ERROR message shown, returning a non-zero exit code. How do you make toolchain include Qt5?
View full article