i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
This blog enables support of Qemu emulation for iMX8MM EVK.  Imagine not having the hardware but still you want to test the software. Qemu gives you exactly that. 1. Booting uboot, linux and user-space application even when you do not possess a real hardware. 2. Early firmware development when the silicon doesn’t yet exist. 3. Linux driver development, debugging and testing.
記事全体を表示
We are pleased to announce that Config Tools for i.MX 26.03 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) Version 26.03 System Manager Memory sector information for resources with memory configuration is added to the Resources overview. Support for memory sectors splitting. Memory configuration input for resources using MBC/MRC is improved. Support for macOS (aarch64 and x86_64) is added. Clocks Hierarchy for local configuration element settings is supported. TEE Multicore Interrupt Handling for Single Security Domain is supported. Option to filter only user-defined memory regions is added. Interrupts are now separated into groups based on the core.
記事全体を表示
This page serves as a hub to gather the links to all the currently available ISP supported camera lists for the i.MX Applications processors.  Camera Compatibility Guides Processor/Family Link to Guide i.MX 8M Plus i.MX 8M Plus ISP Camera Compatibility Guide i.MX 95 i.MX 95 ISP Camera Compatibility Guide   Additional Resources i.MX Camera Software Pack AN AN14376: i.MX Camera Software Pack | NXP Semiconductors
記事全体を表示
The purpose of this page is to provide supportive information for the selection of suitable camera modules that are supported by the i.MX95. The guide is attached in this page. This helps customers evaluate project feasibility and integration aspects when considering i.MX 95 SoCs for their products. It is strongly recommended to consult with NXP and the camera module vendor before finalizing the choice of the camera part number to ensure compatibility, availability, longevity, and pricing requirements.   NXP Supported Sensors: Sensor Vendor Image Sensor Max Resolution Camera Module OmniVision OS08A20 8MP IMX95-OS08A20 | NXP Semiconductors EXPI-OS08A20 OmniVision OX05B1S 5MP   OmniVision OX03C10 3MP   Onsemi AR0144 1MP AR0144   Partner Enabled Sensors: Partner Sensor Vendor Image Sensor Max Resolution ISP Tuning Camera Module Location FRAMOS Sony IMX662 2MP ✔ FSM:GO Munich, Germany/ Canada/USA Sony IMX678 8MP Sony IMX900 3.2MP Sony IMX676 12MP Onsemi Onsemi AR2020 19MP   Module available through Future Electronics   Entron OmniVision OS08A20 8MP ✔ EXPI-OS08A20 China Onsemi AR0820 8MP Order with Entron Onsemi AR0823 8MP Technexion Onsemi AR0144 1MP       Onsemi AR0145 1MP     Onsemi AR0234 2MP     Onsemi AR0235 2MP     Onsemi AR0236 2MP     Onsemi AR0521 5MP     Onsemi AR0522 5MP     Onsemi AR0544 5MP     Onsemi AR0821 8MP       Onsemi AR0822 8MP     Onsemi AR0830 8MP     Onsemi AR1335 13MP     PHYTEC Onsemi AR0144 1MP     Germany/ China/India/ USA Onsemi AR0234 2.3MP   Onsemi AR0521 5MP   E-consystems Sony IMX662 2.4MP     Riverside, CA, USA/India Sony IMX900 3.2MP    
記事全体を表示
Use Raspberry Pi Debug Probe with OpenOCD and i.MX93 FRDM   This document explains the integration process of the Raspberry Pi Debug Probe (Very low cost debugger) with the OpenOCD (On Chip Debugger) tool with the i.MX93 FRDM board.   Also, we will use GDB (GNU DeBugger) to interact with the OpenOCD.   1. Install and Configure OpenOCD   Update and install dependencies sudo apt update sudo apt install build-essential libtool automake pkg-config libusb-1.0-0-dev libhidapi-dev libftdi1-dev libjim-dev jimsh   Clone the OpenOCD repo git clone https://github.com/openocd-org/openocd.git cd openocd   Run ./bootstrap to create the configuration file git submodule update --init --recursive ./bootstrap ./configure --enable-cmsis-dap --enable-hidapi   Make OpenOCD make -j$(nproc) sudo make install   Download the configuration file for i.MX93 You can dowload the  imx93.cfg  in the Table 2. Software requirements on Ubuntu PC of the AN14367 Then, copy the downloaded file to the openocd/tcl/target/ as below: cp ../imx93_new-b42b7c4cac18508442d3df035cec1c6d.cfg tcl/target/imx93.cfg   2. Create UDEV rules   sudo nano /etc/udev/rules.d/99-openocd.rules Add the below in that file: ATTRS{idVendor}=="2e8a", ATTRS{idProduct}=="000c", MODE="660", GROUP="plugdev", TAG+="uaccess"   Reload rules sudo udevadm control --reload-rules && sudo udevadm trigger   3. Connecting the Hardware   To make the DAP works in the i.MX93 FRDM, we must rework the board removing the resistors R3017 and R3018:     Now, we need to connect the Raspberry Pi Debug Probe with the SWD (P14) of our i.MX93 FRDM board:       4. Running the Debug Session   In this moment, with the RP Debug Probe connected, we can Boot the i.MX93 FRDM board and run the below command to start the OpenOCD: $ openocd -s tcl -f interface/cmsis-dap.cfg -c "adapter speed 1000" -f target/imx93.cfg   tic-mpu@tic-mpu:~/Debug_test/openocd$ openocd -s tcl -f interface/cmsis-dap.cfg -c "adapter speed 1000" -f target/imx93.cfg Open On-Chip Debugger 0.12.0+dev-02429-ge4c49d860 (2026-03-21-23:05) Licensed under GNU GPL v2 For bug reports, read http://openocd.org/doc/doxygen/bugs.html adapter speed: 1000 kHz Warn : DEPRECATED: auto-selecting transport "swd". Use 'transport select swd' to suppress this message. Info : Listening on port 6666 for tcl connections Info : Listening on port 4444 for telnet connections Info : Using CMSIS-DAPv2 interface with VID:PID=0x2e8a:0x000c, serial=E6633861A33A1B2C Info : CMSIS-DAP: SWD supported Info : CMSIS-DAP: Atomic commands supported Info : CMSIS-DAP: Test domain timer supported Info : CMSIS-DAP: FW Version = 2.0.0 Info : CMSIS-DAP: Interface Initialised (SWD) Info : SWCLK/TCK = 0 SWDIO/TMS = 0 TDI = 0 TDO = 0 nTRST = 0 nRESET = 0 Info : CMSIS-DAP: Interface ready Info : clock speed 1000 kHz Info : SWD DPIDR 0x5ba02477 Info : imx93.a55.0: hardware has 6 breakpoints, 4 watchpoints Info : [imx93.a55.0] external reset detected Info : [imx93.a55.0] Examination succeed Info : [imx93.m33] Cortex-M33 r1p0 processor detected Info : [imx93.m33] target has 8 breakpoints, 4 watchpoints Info : [imx93.m33] Examination succeed Info : [imx93.ahb] Examination succeed Info : [imx93.a55.0] starting gdb server on 3333 Info : Listening on port 3333 for gdb connections Info : [imx93.m33] starting gdb server on 3334 Info : Listening on port 3334 for gdb connections Info : [imx93.ahb] gdb port disabled   From the Logs, we can see we have two ports: 3333 for Cortex A55 [imx93.a55.0] 3334 for Cortex M33 [imx93.m33]   Install gdb-multiarch   Now, we can install GDB: sudo apt install gdb-multiarch And start a Debug session: $ gdb-multiarch ~/linux-imx/vmlinux   $ gdb-multiarch ~/linux-development/linux-imx/vmlinux GNU gdb (Ubuntu 15.1-1ubuntu1~24.04.1) 15.1 Copyright (C) 2024 Free Software Foundation, Inc. License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html> This is free software: you are free to change and redistribute it. There is NO WARRANTY, to the extent permitted by law. Type "show copying" and "show warranty" for details. This GDB was configured as "x86_64-linux-gnu". Type "show configuration" for configuration details. For bug reporting instructions, please see: <https://www.gnu.org/software/gdb/bugs/>. Find the GDB manual and other documentation resources online at: <http://www.gnu.org/software/gdb/documentation/>. For help, type "help". Type "apropos word" to search for commands related to "word"... Reading symbols from /home/tic-mpu/linux-development/linux-imx/vmlinux... (gdb) target extended-remote localhost:3333 Remote debugging using localhost:3333 0x00000000fff118fc in ?? ()   A simple example of how to read a register with GDB: (gdb) x/xw 0x43810000 0x43810000: 0x02010001     Happy debugging!     Best regards, Salas. 
記事全体を表示
Tested in FRDM-i.MX91 Written in C LF-6.12.49
記事全体を表示
There are currently no additional test programs in I.MX Jailhouse program. This demo shares how to test RM67199 MIPI panel in Jailhouse inmate.   Please refer run.sh in attachments. modprobe jailhouse insmod jailhouse_clk.ko # adjust pixel clock for MIPI PANEL RMP67199 echo 129937500 > /sys/bus/platform/devices/jailhouse_clk/rate_pix export PATH=$PATH:/usr/share/jailhouse/tools/ jailhouse enable /root/imx8mm.cell jailhouse cell linux /root/imx8mm-inmate-demo.cell /root/Image.bin -d /root/imx8mm-evk-inmate.dtb -c "clk_ignore_unused console=ttymxc3,115200 earlycon=ec_imx6q,0x30890000,115200 root=/dev/mmcblk2p2 rootwait rw"  
記事全体を表示
There are currently no additional test programs in I.MX Jailhouse program. This demo shares how to test USB function in Jailhouse inmate. Inmate boot log: root@imx8mmevk:~# dmesg | grep usb [ 0.312280] usbcore: registered new interface driver usbfs [ 0.317206] usbcore: registered new interface driver hub [ 0.322279] usbcore: registered new device driver usb [ 0.911649] usbcore: registered new device driver r8152-cfgselector [ 0.917711] usbcore: registered new interface driver r8152 [ 0.994200] usbcore: registered new interface driver uas [ 0.999359] usbcore: registered new interface driver usb-storage [ 1.005192] usbcore: registered new interface driver usbserial_generic [ 1.011486] usbserial: USB Serial support registered for generic [ 1.017274] usbcore: registered new interface driver ftdi_sio [ 1.022813] usbserial: USB Serial support registered for FTDI USB Serial Device [ 1.029852] usbcore: registered new interface driver usb_serial_simple [ 1.036148] usbserial: USB Serial support registered for carelink [ 1.042016] usbserial: USB Serial support registered for flashloader [ 1.048144] usbserial: USB Serial support registered for funsoft [ 1.053931] usbserial: USB Serial support registered for google [ 1.059643] usbserial: USB Serial support registered for hp4x [ 1.065185] usbserial: USB Serial support registered for kaufmann [ 1.071051] usbserial: USB Serial support registered for libtransistor [ 1.077334] usbserial: USB Serial support registered for moto_modem [ 1.083371] usbserial: USB Serial support registered for motorola_tetra [ 1.089745] usbserial: USB Serial support registered for nokia [ 1.095368] usbserial: USB Serial support registered for novatel_gps [ 1.101486] usbserial: USB Serial support registered for siemens_mpi [ 1.107612] usbserial: USB Serial support registered for suunto [ 1.113316] usbserial: USB Serial support registered for vivopay [ 1.119111] usbserial: USB Serial support registered for zio [ 1.124578] usbcore: registered new interface driver usb_ehset_test [ 1.215499] usbcore: registered new interface driver usbhid [ 1.220879] usbhid: USB HID core driver [ 1.396384] usb_phy_generic usbphynop1: dummy supplies not allowed for exclusive requests [ 42.414253] usb 1-1: new high-speed USB device number 2 using ci_hdrc [ 42.577822] usb-storage 1-1:1.0: USB Mass Storage device detected [ 42.579492] scsi host0: usb-storage 1-1:1.0  
記事全体を表示
This tutorial describes the complete procedure for calibrating a touchscreen display using Weston, specifically validated with the DY1212W LVDS panel on the following NXP development platforms: i.MX93‑EVK FRDM‑i.MX95 FRDM‑i.MX8MP While the initial calibration performed by Weston works only temporarily, this guide will walk you through configuring the system so that the calibration becomes persistent across reboots. The steps below include performing the initial calibration, editing Weston’s configuration, creating a calibration helper script, and applying udev rules to store the calibration matrix automatically.   Temporary Touchscreen Calibration To begin, run the following command to perform an initial calibration of your touchscreen: weston-touch-calibrator LVDS-1   After running this command, your display should be correctly calibrated. However, this calibration is not persistent, and you will need to recalibrate after every reboot unless you complete the persistence steps below.   Making the Calibration Persistent Follow the steps below to ensure that calibration settings are preserved across system restarts. Step 1: Edit the Weston Configuration File Open the following file: /etc/xdg/weston/weston.ini Under the [libinput] section, add these lines: [libinput] touchscreen_calibrator=true + calibration_helper=/usr/bin/save-calibration.sh This enables the calibration helper script that will automatically save your settings. Step 2: Create the Calibration Helper Script Create a new script at: /usr/bin/save-calibration.sh   Insert the following content: #!/bin/bash # Store the transformation arguments for the resistive touchscreen as udev rule echo 'SUBSYSTEM=="input", KERNEL=="event[0-9]*", ENV{ID_INPUT_TOUCHSCREEN}=="1", ENV{LIBINPUT_CALIBRATION_MATRIX}="'$2' '$3' '$4' '$5' '$6' '$7'"' >> /etc/udev/rules.d/touchscreen.rules   Make the script executable: chmod 755 /usr/bin/save-calibration.sh   Step 3: Restart Weston and Recalibrate Restart the Weston service: systemctl restart weston   Run the calibration tool again to generate the persistent settings: weston-touch-calibrator LVDS-1 reboot   Conclusion After completing all of the steps above, your touchscreen calibration will now persist across reboots, ensuring a consistent user experience even after powering off the board. This configuration allows the system to automatically store and apply calibration data through a udev rule generated by your helper script. If you encounter any issues or require further assistance, feel free to reach out. Best regards, Chavira
記事全体を表示
this poring is based on the imx415 driver, the capture format is based on raw10, the bsp version is 6.6.52, the patches are attached Disclaimer: − “Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.”
記事全体を表示
i.MX 93 EVK LF-6.12.49 patches
記事全体を表示
SW : uboot-imx lf_v2025.04 HW : i.MX 8MP EVK board, Oscilloscope   1. Introduction This guide explains the concept of DDR clock spread spectrum on the i.MX 8MP EVK platform. Note that the official NXP BSP does not enable this feature by default. Additionally, this guide provides an example code patch and verification steps to enable the LPDDR4 clock spread spectrum feature on the NXP i.MX 8MP EVK board.   2. What is Spread Spectrum? Spread Spectrum (SS) is a technique used to reduce electromagnetic interference (EMI) by slightly modulating the clock frequency around its nominal value. Instead of operating at a fixed frequency (e.g., 800 MHz), the clock signal is varied within a small range (e.g., ±0.5%). This modulation spreads the energy of the clock signal over a wider frequency band, reducing the peak energy at any single frequency. In other words, SS does not change the average clock speed significantly, but it helps to distribute the spectral energy, making the system less likely to violate EMI regulations.   3. Why Enable Spread Spectrum on DRAM Clock? Enabling Spread Spectrum on the DRAM clock helps reduce electromagnetic interference (EMI) by slightly modulating the clock frequency, lowering peak emissions and making it easier to meet regulatory standards such as FCC and CE. This approach improves system reliability by minimizing interference with other components, offers a cost-effective alternative to hardware changes like shielding or PCB redesign, and is widely adopted in high-speed interfaces such as DDR, PCIe, and SATA to ensure compliance without additional hardware complexity.   4. Related registers CCM_ANALOG_DRAM_PLL_SSCG_CTRL                             Note :  PLL_MFREQ_CTL[19 : 12] : Value of modulation frequency control The larger the mfr value, the lower the MF value (the slower the modulation); the smaller the mfr value, the higher the MF value. MF : The frequency of spread spectrum modulation is the speed at which the triangular/sawtooth modulated wave travels back and forth once per second, measured in Hz (commonly in the tens of kHz range). The speed of the spread spectrum "jitter" is determined. Usually, around 20–50 kHz is chosen to make the energy "swipe evenly" within the bandwidth of the EMI test receiver, thereby reducing the peak radiation at a certain frequency point. PLL_MRAT_CTL[9 : 4] : Value of modulation rate control The larger mrr is, the larger MR is (the wider the range); similarly, MR is also directly proportional to mfr and inversely proportional to m. MR : Peak-to-peak percentage of spread spectrum (the percentage of the total range of the clock frequency swinging around the center value). For example, MR = 0.5% means that the frequency swings around the center value by a total of 0.5% (if it is center-spread spectrum, it is usually ±0.25%).The MR determines the depth (width) of the spread spectrum. The larger the MR, the wider the spectral energy distribution and the lower the peak value, but it comes at the cost of jitter/timing margin (timing should be carefully selected for DDR, SerDes, etc.). 5. About Uboot code patch. Please refer the attachment patch file. At high DRAM frequency, Enable SS may cause not stable problem. So, in this case, I will choose 2400Mbps data clock run the test. Firstly, we should make sure that our code include the 2400Mbps PLL setting. DRAM data speed is 2400Mbps, the DRAM clock is 1200MHz. So the DDRC PLL clock should set up with 600MHz. For example, refer the below code. static struct imx_int_pll_rate_table imx8mm_fracpll_tbl[] = {     PLL_1443X_RATE(1000000000U, 250, 3, 1, 0),     PLL_1443X_RATE(933000000U, 311, 4, 1, 0),     PLL_1443X_RATE(900000000U, 300, 2, 2, 0),     PLL_1443X_RATE(800000000U, 200, 3, 1, 0),     PLL_1443X_RATE(750000000U, 250, 2, 2, 0),     PLL_1443X_RATE(650000000U, 325, 3, 2, 0),     PLL_1443X_RATE(600000000U, 300, 3, 2, 0), // 2400Mbps     PLL_1443X_RATE(594000000U, 99, 1, 2, 0),     PLL_1443X_RATE(400000000U, 400, 3, 3, 0),     PLL_1443X_RATE(266000000U, 266, 3, 3, 0),     PLL_1443X_RATE(167000000U, 334, 3, 4, 0),     PLL_1443X_RATE(100000000U, 200, 3, 4, 0), }; PLL output calculator formula is : PLL_out = 24MHz*mdiv/pdiv/(2^sdiv) So, 2400MHz * 300 / 3 / 2^2 = 600MHz   6. Test result Non Enable SS Enable SS with 1% MR and Down spread Enable SS with 2% MR and Down spread Enable SS with 2% MR and Center spread  
記事全体を表示
Some customer need to run Zephyr on i.MX8QM CM4, but there is no support on Zephyr mainline(v4.3.0). This article will share the i.MX8QM CM4_0 porting based on Zephyr v4.3.0.  For i.MX8QXP CM4, please refer this link: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QXP-CM4-support-on-Zephyr-v4-3-0/ta-p/2296957   samples/hello_world/ samples/synchronization   Add pd_ignore_unused in bootargs before entering Linux. For the OpenAMP communication, need to refer this Zephyr application. https://github.com/nxp-real-time-edge-sw/heterogeneous-multicore/blob/main/apps/rpmsg_str_echo/zephyr/main.c
記事全体を表示
Some customer need to run Zephyr on i.MX8QXP CM4, but there is no support on Zephyr mainline(v4.3.0) This article will share the porting based on Zephyr v4.3.0. For i.MX8QM CM4, please refer this link: https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8QM-CM4-0-support-on-Zephyr-v4-3-0/ta-p/2296962   samples/hello_world/ samples/synchronization Add pd_ignore_unused in bootargs before entering Linux. For the OpenAMP communication, need to refer this Zephyr application. https://github.com/nxp-real-time-edge-sw/heterogeneous-multicore/blob/main/apps/rpmsg_str_echo/zephyr/main.c
記事全体を表示
Platform supported Kinara Ara2: imx95frdm imx8mpfrdm In this article, let's take imx8mpfrdm as example.   1. Create a Debian LSDK2512 release system for SD boot using the command below: $ ./flex-installer -i pf -d /dev/sdX $./flex-installer -b boot_IMX_arm64_lts_6.12.20.tar.zst -f firmware_imx8mpfrdm_sdboot.img -d /dev/sdX -m imx8mpfrdm -r rootfs_lsdk2512_debian_imx8mpevk.tar.zst note: if Debian base rootfs is used, please upgrade to full function Debian rootfs first. 2. Insert SD card on imx8mpfrdm and boot the system. Once the system has completed booting and you reach the kernel prompt: $ date -s "20260101 1100" // set date $ set proxy if needed 3. download rt-sdk-ara2.deb at: https://nxp1.sharepoint.com/:u:/r/teams/ext1081/Shared%20Documents/LF_v6.12.34/Debian%20Packages/r1.3/Package%201/rt-sdk-ara2.deb?csf=1&web=1&e=i4x1zD 4. Get the uiodma.ko kernel module for Debian from NXP. 5. Disable sleep when install package: $ systemctl mask sleep.target suspend.target hibernate.target hybrid-sleep.target 6. Prepare the packages ARA2 needed: $ apt update $ apt install --reinstall -y libc6-dev $ ln -sf /usr/include/aarch64-linux-gnu/sys /usr/include/sys $ apt install -y python3-dev build-essential $ e2fsck -f /dev/mmcblk1p2 7. install Ara2 package: $ dpkg -i rt-sdk-ara2.deb The tail of successful log as follows: ... [ 783.892116] Adding 2097148k swap on /swapfile. Priority:-2 extents:17 across:35913728k SS /swapfile none swap sw 0 0 Swap file of 2G configured and enabled successfully. Enable rt-sdk-ara2.service service... Created symlink '/etc/systemd/system/multi-user.target.wants/rt-sdk-ara2.service' → '/etc/systemd/system/rt-sdk-ara2.service'. rt-sdk-ara2.service has been enabled. To stop the service from starting automatically on boot run: systemctl disable rt-sdk-ara2.service Post-install script completed successfully. 8. overwrite the kernel module: $ cp /root/uiodma.ko /root/kinara/rt_sdk_r1.3/art/linux/drivers/uiodma_cache_management/uiodma.ko $ systemctl unmask sleep.target suspend.target hibernate.target hybrid-sleep.target // re-enable sleep 9. reboot the system: $ reboot You will see the log as bellow: ... [ 57.855988] bash[1492]: +----------+-----------------+ [ 57.856188] bash[1492]: | Product | Current Version | [ 57.856297] bash[1492]: +----------+-----------------+ [ 57.856397] bash[1492]: | firmware | 1.1.2.0 | [ 57.856501] bash[1492]: | proxy | 1.3.0.0 | [ 57.856593] bash[1492]: | sysapi | 1.1.61.0 | [ 57.856695] bash[1492]: +----------+-----------------+ [ 57.856788] bash[1492]: [I:20260109:09:02:44:636750] [DeviceManager] [kinara_main_1479][DeviceManager] [ 57.856894] bash[1492]: +------------+--------------------+ [ 57.857019] bash[1492]: | Product | Supported Versions | [ 57.857124] bash[1492]: +------------+--------------------+ [ 57.857227] bash[1492]: | client_lib | 1.0.0.0 | [ 57.857327] bash[1492]: | client_lib | 1.1.1.0 | [ 57.857419] bash[1492]: | client_lib | 1.1.2.0 | [ 57.857525] bash[1492]: | client_lib | 1.3.0.0 | [ 57.857642] bash[1492]: | cnn_model | 2.0.0.0 | [ 57.857741] bash[1492]: | cnn_model | 2.1.0.0 | [ 57.857833] bash[1492]: | firmware | 0.5.2.0 | [ 57.857931] bash[1492]: | firmware | 1.1.2.0 | [ 57.858030] bash[1492]: | llm_model | 3.0.0.0 | [ 57.858129] bash[1492]: | llm_model | 3.1.0.0 | [ 57.858222] bash[1492]: | pci_driver | 1.0.4.0 | [ 57.858322] bash[1492]: | pci_driver | 1.0.6.6 | [ 57.858421] bash[1492]: | proxy | 0.8.0.0 | [ 57.858533] bash[1492]: | proxy | 0.9.0.0 | [ 57.858633] bash[1492]: | proxy | 1.1.1.0 | [ 57.858732] bash[1492]: | proxy | 1.3.0.0 | [ 57.858823] bash[1492]: +------------+--------------------+ [ 57.858930] bash[1492]: 2026-01-09 09:02:44 - Proxy launched succesfully [ 58.752944] bash[1514]: 2026-01-09 09:02:45 - Hardware bringup is done (1 device(s) configured) and proxy is launched successfully in the background. [ 58.755142] bash[392]: Logs saved in: /root/kinara/rt_sdk_r1.3/saved_logs/rt-sdk-ara2_logs.txt Now, enjoy your AI journey.
記事全体を表示
We are pleased to announce that Config Tools for i.MX v25.12 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) DDR tool – Support for detecting multiple boards connected to the host system is added. – Automatic detection and selection of newly connected COM ports is implemented. – A Connection Test option to validate connectivity before running tests on the target is introduced. – i.MX 93 EVK LP4 configuration is added. – Training execution time information for i.MX 95 and i.MX 943 is included in logs. – Bus signal naming in the UI to align with i.MX pin naming conventions is consolidated. – CA bus values for i.MX943 with LPDDR4 are updated. – DRAM density calculation for i.MX 95 and i.MX 943 with LP4/4x is corrected. – Incorrect calculation of number of banks for i.MX 8M with DDR3L is fixed. – CS1_BNDs calculation for i.MX 91 is corrected. SerDes tool – i.MX 943 RFP support is added. System Manager – The ability to export user configuration in the CFG format is added. – Information about atomic resources to the Details view is added. – Generation and configuration of the config_fusa.h file is supported. – Resource and template assignment is improved. – Grayed-out resource assignments for unavailable configuration parameters in the Resources view are implemented. – Validation of configuration and user input is improved. – Problem decorators to the System and Boot view are added. – Design of the Boot and Details view is improved. – 5600 MT/s for i.MX 95 and i.MX 943 with LPDDR5 is enabled. – LP4/4x settings for DDR_SDRAM_ZQ_CNTL for i.MX 95 and i.MX 943 are updated. – Dual-rank configurations for i.MX 91 and i.MX 93 are updated. – LP4/4x configuration to support non-binary densities for i.MX 95 and i.MX 943 is updated. – Support for non-binary aligned LP4 density for i.MX 91 is added. – FRDM board support (LPDDR4X 15x15 at 4000 MT/s) for i.MX 95 is added. – Timing file discrepancies for i.MX 8MN with DDR3L are fixed. – Issue where changing PHY log level did not update generated code is fixed.
記事全体を表示
In some applications, we need to shift frequencies to avoid interference from certain frequencies, such as shifting to avoid Wi-Fi interference. The document is a guide for shifting DDR3 frequency.   The document uses the iMX8M Nano DDR3 as an example, but the process is the same for the iMX8M mini, iMX8M Plus, LPDDR4, etc. The main issue is resolving the DDR pll configuration. Before reading this article, we assume you are already familiar with using the DDR stress tool and DDR config rpa, or the DDR tool of the config tools.   pll_to_table_entry_rates.py can help you to find the settings. 
記事全体を表示
Hello everyone! In this document you'll find an example on how to build your Cortex-M33 code where some parts of the code runs from DDR, for this changes on ATF where the M33 core can visit DRAM in early stage. For this we will take advantage of RPROC framework, RPROC (Remote Processor Framework) is a Linux kernel and U-Boot subsystem that manages secondary, embedded processors (like Cortex-M cores), where we will use the A55 to load the M33 firmware. This will require changes on Linux device tree, ATF and M33 linker file. Requirements: Ubuntu 20.04 or later host PC i.MX93 QSB UUU Tool ARM GNU Toolchain (arm-gnu-toolchain-12.3.rel1-x86_64-aarch64-none-linux-gnu) SDK package (SDK_25_09_00_MCIMX93-QSB) Prebuild Linux Image (LF_v6.12.34-2.1.0_images_IMX93EVK) ### Clone imx-mkimage, it is better to download the same version of the sw we are working with ### $ git clone https://github.com/nxp-imx/imx-mkimage -b lf-6.12.34-2.1.0 ### Decompress the GNU toolchain into a path in local disk, in this test would be /opt/ ### $ sudo tar -xvJf arm-gnu-toolchain-12.3.rel1-x86_64-aarch64-none-linux-gnu.tar.xz -C /opt ### Clone and build Uboot ### $ git clone https://github.com/nxp-imx/uboot-imx -b lf-6.12.34-2.1.0 $ cd uboot-imx $ make -j $(nproc --all) clean $ make -j$(nproc --all) ARCH=arm CROSS_COMPILE=/opt/arm-gnu-toolchain-12.3.rel1-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- imx93_11x11_evk_defconfig $ make -j $(nproc --all) ARCH=arm CROSS_COMPILE=/opt/arm-gnu-toolchain-12.3.rel1-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- ### Download and extract ELE firmware ### $ cd .. $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-ele-imx-2.0.3-286c884.bin $ chmod +x firmware-ele-imx-2.0.3-286c884.bin $ ./firmware-ele-imx-2.0.3-286c884.bin --auto-accept ### Optional if using i.MX FW ### $ wget https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/firmware-imx-8.29-8741a3b.bin $ chmod +x firmware-imx-8.29-8741a3b.bin $ ./firmware-imx-8.29-8741a3b.bin --auto-accept ### Clone ATF ### $ git clone https://github.com/nxp-imx/imx-atf -b lf-6.12.34-2.1.0 $ cd imx-atf ### Modify ATF for the M33 to be able to access DDR ###   --- a/plat/imx/imx93/trdc_config.h +++ b/plat/imx/imx93/trdc_config.h struct trdc_mrc_config trdc_n_mrc[] = { { 0, 0, 0, 0x80000000, 0x80000000, 0, false }, /* MRC0 DRAM for S400 DID0 */ { 0, 1, 0, 0x80000000, 0x80000000, 0, false }, /* MRC0 DRAM for MTR DID1 */ - { 0, 2, 0, 0x80000000, 0x80000000, 0, true }, /* MRC0 DRAM for M33 DID2 */ + { 0, 2, 0, 0x80000000, 0x80000000, 1, true }, /* MRC0 DRAM for M33 DID2 */ { 0, 3, 0, 0x80000000, 0x80000000, 1, false }, /* MRC0 DRAM for A55 DID3 */ { 0, 5, 0, 0x80000000, 0x80000000, 0, false }, /* MRC0 DRAM for USDHC1 DID5 */ { 0, 6, 0, 0x80000000, 0x80000000, 0, false }, /* MRC0 DRAM for USDHC2 DID6 */ ### Build modified ATF ### $ make -j $(nproc --all) PLAT=imx93 bl31 CROSS_COMPILE=/opt/arm-gnu-toolchain-12.3.rel1-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- ### Modify linker file and build M33 code, in this example we are using hello world SDK example ### $ cd .. $ tar -xvzf SDK_25_09_00_MCIMX93-QSB.tar.gz $ cd SDK_25_09_00_MCIMX93-QSB/boards/mcimx93qsb/demo_apps/hello_world/armgcc --- a/boards/mcimx93autoevk/demo_apps/hello_world/armgcc/MIMX9352_cm33_ram.ld +++ b/boards/mcimx93autoevk/demo_apps/hello_world/armgcc/MIMX9352_cm33_ram.ld m_a55_suspend_ram (RW) : ORIGIN = 0x20002000, LENGTH = 0x00001000 m_data (RW) : ORIGIN = 0x20003000, LENGTH = 0x0001B000 m_rsc_tbl (RW) : ORIGIN = 0x2001E000, LENGTH = 0x00001000 + m_text_dram (RW) : ORIGIN = 0x8F000000, LENGTH = 0x00001000 + m_data_dram (RW) : ORIGIN = 0x8F001000, LENGTH = 0x00001000 } /* Define output sections */ . = ALIGN(4); } > m_text + .dram_text : + { + . = ALIGN(32); + *(.myDRAM) + . = ALIGN(32); + } > m_text_dram + .ARM.extab : { *(.ARM.extab* .gnu.linkonce.armextab.*) .ARM.attributes 0 : { *(.ARM.attributes) } ASSERT(__StackLimit >= __HeapLimit, "region m_data overflowed with stack and heap") + + .dram_data : + { + . = ALIGN(32); + *(.myDRAM_data) + . = ALIGN(32); + } > m_data_dram } a/boards/mcimx93autoevk/demo_apps/hello_world/hello_world.c +++ b/boards/mcimx93autoevk/demo_apps/hello_world/hello_world.c * Definitions ******************************************************************************/ +#define _RET_IP_ (unsigned long)__builtin_return_address(0) +#define _THIS_IP_ ({ __label__ __here; __here: (unsigned long)&&__here; }) /******************************************************************************* * Prototypes /******************************************************************************* * Variables ******************************************************************************/ - +const char myString[] __attribute__((section(".myDRAM_data"))) = "Hello, World!"; /******************************************************************************* * Code ******************************************************************************/ +__attribute__ ((section(".myDRAM"))) +void Dram_test(void) { + PRINTF("Dram_test!!\r\n"); + + PRINTF("%s!!\r\n", myString); + + PRINTF("function %p\n",_THIS_IP_); +} + /*! * @brief Main function */ BOARD_BootClockRUN(); BOARD_InitDebugConsole(); - PRINTF("hello world.\r\n"); + PRINTF("hello world from DRAM.\r\n"); while (1) { ch = GETCHAR(); PUTCHAR(ch); + if(ch == 'a'){ + Dram_test(); + } } } $ export ARMGCC_DIR=~/gcc-arm-none-eabi-10.3-2021.10 $ export PATH=$PATH:~/gcc-arm-none-eabi-10.3-2021.10 $ ./build_release.sh ### Copy the resulting binaries to imx-mkimage ### $ cp ~/imx-atf/build/imx93/release/bl31.bin ~/imx-mkimage/iMX93 $ cp ~/uboot-imx/u-boot.bin ~/imx-mkimage/iMX93 $ cp ~/uboot-imx/spl/u-boot-spl.bin ~/imx-mkimage/iMX93 ### Copy i.MX firmware ### $ cd .. $ cp firmware-imx-8.29-8741a3b/firmware/ddr/synopsys/lpddr4_dmem_* ~/imx-mkimage/iMX93 $ cp firmware-imx-8.29-8741a3b/firmware/ddr/synopsys/lpddr4_imem_* ~/imx-mkimage/iMX93 $ cpfirmware-ele-imx-2.0.3-286c884/mx93a1-ahab-container.img ~/imx-mkimage/iMX93 ### Build the flash.bin using mkimage $ cd imx-mkimage $ make SOC=iMX93 flash_singleboot ### Clone, modify and build device tree for Linux to be able to use RPROC to load M33 Firmware ### $ git clone https://github.com/nxp-imx/linux-imx -b lf-6.12.34-2.1.0 --- a/arch/arm64/boot/dts/freescale/imx93-9x9-qsb.dts +++ b/arch/arm64/boot/dts/freescale/imx93-9x9-qsb.dts no-map; }; + dram: dram@20480000 { + reg = <0 0x8f000000 0 0x20000>; + no-map; + }; + rsc_table: rsc-table@2021e000 { reg = <0 0x2021e000 0 0x1000>; no-map; <&mu1 1 1>, <&mu1 3 1>; - memory-region = <&vdevbuffer>, <&vdev0vring0>, <&vdev0vring1>, + memory-region = <&dram>, <&vdevbuffer>, <&vdev0vring0>, <&vdev0vring1>, <&vdev1vring0>, <&vdev1vring1>, <&rsc_table>; fsl,startup-delay-ms = <500>; status = "okay"; $ export ARCH=arm64 $ export CROSS_COMPILE=/opt/arm-gnu-toolchain-12.3.rel1-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- $ make imx_v8_defconfig $ make freescale/imx93-9x9-qsb.dtb Set SW for serial download on the QSB (0001), connect debug, download and power cables and turn on the QSB, for this test we will flash the demo image and just replace Linux device tree, flash.bin and M33 firmware into the QSB board. $ uuu -b sd_all flash.bin imx-image-full-imx93evk.wic Once it is done change SW to the respective bootmedia SD boot (0011) and boot the board and stop at uboot, to enter fastboot mode to load modified device tree and M33 firmware > fastboot 1 After this just run UUU tool on the host computer and fatload the files $ uuu -b fat_write imx93-9x9-qsb.dtb mmc 1:1 $ uuu -b fat_write hello_world.elf mmc 1:1 When the tool finish, stop fastboot mode by typing CTRL+C and then boot into Linux > boot Login with default password "root" and run the following commands to load M33 firmware $ root $ modprobe imx_rpmsg_tty $ cp /run/media/boot-mmcblk1p1/hello_world.elf /lib/firmware/ $ echo hello_world.elf > /sys/class/remoteproc/remoteproc0/firmware $ echo start >/sys/class/remoteproc/remoteproc0/state   Once done we can verify that the M33 firmware is running on DDR Hope everyone finds this useful! For any question regarding this document, please create a community thread and tag me if needed. Saludos/Regards, Aldo.
記事全体を表示
This article describes how to create a tiny rootfs based on BusyBox.   Test platform: i.MX 95 19x19 LPDDR5 EVK. The attached layer can be used with other platforms as well. Software: Linux BSP 6.12.34-2.1.0 Boot device: SD card   This article provides a custom meta-tiny-rootfs layer, to simplify the enablement. The layer: creates a custom distribution based on Poky, with no extra features creates a custom image based on BusyBox that only starts a terminal removes most of the machine features uses musl, instead of glibc   Using the default DISTRO=fsl-imx-wayland and core-image-minimal, the rootfs size is 800MB. Using the custom DISTRO=tiny-rootfs and core-image-tiny, the rootfs size reduces to 2.6MB.   How to? 1. Prepare the Yocto environment according to Section 3, 4, 5 in i.MX Yocto Project User's Guide. In the next commands, we'll assume the Yocto directory is imx-yocto-bsp, and the build directory is build. 2. Configure the build directory: cd ~/imx-yocto-bsp/ DISTRO=fsl-imx-wayland MACHINE=imx95-19x19-lpddr5-evk source ./imx-setup-release.sh -b build Note: The imx-setup-release.sh script accepts only Wayland distributions. We'll set the custom distro at the next step. 3. Set the custom distro. In the build directory, run: echo 'DISTRO = "tiny-rootfs"' >> conf/local.conf 4. Download the meta-tiny-rootfs archive, and extract it into the ~/imx-yocto-bsp/sources directory. cd ~/imx-yocto-bsp/sources tar -xvf meta-tiny-rootfs.tar.gz 5. Add the meta-tiny-rootfs layer to BBLAYERS: cd ~/imx-yocto-bsp/build bitbake-layers add-layer ../sources/meta-tiny-rootfs 6. Build the core-image-tiny image. bitbake core-image-tiny 7. Write the image on an SD card, and boot. You should be able to see a similar log: [ 6.183401] Run /sbin/init as init process init started: BusyBox v1.37.0 () starting pid 163, tty '': '/bin/mount -t proc proc /proc' starting pid 164, tty '': '/bin/mount -t sysfs sysfs /sys' starting pid 165, tty '': '/bin/mount -t devtmpfs devtmpfs /dev' mount: mounting devtmpfs on /dev failed: Resource busy starting pid 166, tty '': '/bin/mount -o remount,rw /' [ 6.246037] EXT4-fs (mmcblk1p2): re-mounted a5abac39-6c11-419f-97ef-86532e2616ad. starting pid 167, tty '': '/bin/mkdir -p /dev/pts' starting pid 168, tty '': '/bin/mount -t devpts devpts /dev/pts' starting pid 169, tty '': '/bin/mount -a' starting pid 170, tty '': '/sbin/swapon -a' starting pid 176, tty '': '/etc/init.d/rcS' starting pid 177, tty '/dev/ttyLP0': '/usr/sbin/ttyrun ttyLP0 /sbin/getty 115200 ttyLP0' Tiny Rootfs Operating System 1.0.0 imx95-19x19-lpddr5-evk /dev/ttyLP0 imx95-19x19-lpddr5-evk login:   How to add additional features?  If you want to add additional features to DISTRO_FEATURES, MACHINE_FEATURES, or IMAGE_FEATURES, please use the DISTRO_TINY_FEATURES, MACHINE_TINY_FEATURES and IMAGE_TINY_FEATURES variables. For example, to add bluetooth to MACHINE_FEATURES, add the following line in conf/local.conf. MACHINE_TINY_FEATURES = "bluetooth"   Note: If you need to add a package that requires the full libc (instead of musl), add the following in conf/local.conf: TCLIBC = "glibc"   These optimizations were inspired by this presentation: Honey, I shrunk the rootfs!
記事全体を表示
NETC presents itself as a multi-function PCIe Root Complex Integrated Endpoint (RCiEP) for easy software discovery of peripheral functions. As such, it contains multiple PCIe functions. PCIe RCiEP allows for easy software integration into OSes, which support PCIe but can be easily integrated as a simple platform device for RTOSes or bare metal implementations which do not support it. Configuration and control of ENETC(s) is implemented using a combination of registers and a command message interface implemented using descriptor rings in memory. Key goal of the DPDK is to provide a simple, complete framework for fast packet processing in data plane applications. Using the APIs provided as part of the framework, applications can leverage the capabilities of underlying network infrastructure. DPDK been prominent software in user space for networking applications pushes for eNetc driver to be written in user space. This document introduces overview of the NXP ENETC and how its driver is implemented and integrated into the DPDK. DPDK eNetc Driver support features Multi-queue supported, Packet type parsing, promisc, MAC exact filter table filtering, VLAN exact filter table filtering, Link status interrupt, Rx checksum offload, basic stats.
記事全体を表示