i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
Important: If you have any questions or would like to report any issues with the DDR tools or supporting documents please create a support ticket in the i.MX community. Please note that any private messages or direct emails are not monitored and will not receive a response.   These are the detailed programming aids for the registers associated with DRAM initialization (DDR3 and LPDDR2) of the MX6DQP (also known as Rev 2 or Dual/Quad Plus), and covers the Sabre_SD boards and DDR3 based Auto Infotainment board. The last work sheet tab in the tool formats the register settings for use with the ARM RealView debugger (.inc) and the DDR Stress Test. It can be manually converted, by the user, to the DS5 .ds format or to a DCD file format used by uboot or other. The programming aids were developed based on NXP development boards and can be customized by the user for their board design. This tool serves as an aid to assist with programming the DDR interface of the MX6DQP and is based on the DDR initialization scripts developed by the R&D team and no guarantees are made by this tool. The following are some general notes regarding this tool: • Refer to the "How To Use" tab in the tool as a starting point to use this tool. • This tool may be updated on an as-needed basis for bug fixes or future improvements.  There is no schedule for aforementioned maintenance. • The MX6DQP adds a new third party IP called the NoC. The programming for these registers are automatically updated in the tool given a set of user input MMDC parameters and should not be modified manually.
記事全体を表示
Here are two patchs: Patch 1: 0001-I.MX6-SSI_ASRC_P2P_Capture-for-SabreSD-board-Kernel-.patch Patch 2: 0001-I.MX6-SSI_ASRC_P2P-Capture-for-SebreSD-board.patch Patch 1 is based on patch 2.     memory <-- ASRC_Output FIFO | ASRC_Input FIFO <-- SSI_RX FIFO <-- Audio Codec                                              |           |     ASRC Out clk ASRCK1 <---|           |--->   ASRC In clk None                                              |           |     ASRC OutPut width            |           |       ASRC InPut width and data format     is set by arecord            <---|           |--->   is set by ASRC P2P parameter     parameter                          |           |                                             |           |     support 44100/48000          |           |       support 44100/48000     and S24_LE/S16_LE     <---|           |--->   and S24_LE/S16_LE    You can use:     arecord -Dhw:0,1 -c 2 -f S16_LE/S24_LE -r 44100/48000 XXX.wav     aplay XXX.wav     to test this patch.
記事全体を表示
NFS After LTIB installation, follow the instructions below to configure and build Linux Image and Root File System. TIP: Type: $./ltib --help to get more information on ltib In the folder where LTIB were installed, execute the file: $./ltib It should take some minutes to complete the installation. Configure the ltib to select the options and packages to be defined and installed in Linux Image and Root File System. $./ltib -c     or     $./ltib -m config The menu configuration should appear: To configure for use the system with NFS, go to: Target Image Generation -> Target Image -> NFS Only For basic compilation, exit LTIB. It will compile and add some pre-built packages to make the target file system.
記事全体を表示
    Attached is the SDHC DMA read supported patch, it is based on WCE600_MX51_ER_1104, it was verified on iMX51 EVK board. The SDHC DMA read can reduce the NK copy time, in this way it can speed up the WinCE boot.
記事全体を表示
Video Unit Test The BSP provides a package that allows testing of several i.MX 31 peripherals on the PDK. The name of this package is 'imx-test'.   The name of the package may vary according to SDK release, at the time of the writing SDK 1.4 was used, on SDK 1.2 the name of a similar package was 'mxc-misc'   For more information on the imx-test package refer to the SDK 1.4 manual, imx31_Linux_RM.pdf, chapter 49 - Unit Tests. This file is available on BSP tarball Testing To test the image sensor and the display on the PDK follow the steps below: Enable imx-test and util-linux packages: $ ./ltib -c Once "ltib" finishes boot the system. On the target board: $ modprobe mxc_v4l2_capture Check if /dev/video0 was created $ ll /dev/video* lrwxrwxrwx  1 root root            6 Jan 1 20:47 /dev/video -> video0 crw-rw----     1 root root    81,   0 Jan 1 20:47 /dev/video0 crw-rw----     1 root root    81, 16 Jan 1 20:46 /dev/video16 Now run the unit tests: $./mxc_v4l2_overlay.out -iw 640 -ih 480 -ow 480 -oh 640 -r 4 -fr 30 -t 10 - capture images with the sensor and display on the LCD $./mxc_v4l2_capture.out -w 640 -h 480 -r 0 -c 150 -fr 30 test3.yuv - capture images and save on /unit-tests/test3.yuv $./mxc_v4l2_output.out -iw 640 -ih 480 -ow 480 -oh 640 -d 4 -fr 60 test3.yuv - capture images and save on /unit-tests/test3.yuv   For usage syntax type: command -help. ./mxc_v4l2_output.out -help Source Code If you want to check the source code, on the host machine "ltib" install path type: $./ltib -m prep -p imx-tests Then, go to <ltib install path>/rpm/BUILD/imx-test-2.3.2/test/mxc_v4l2_test
記事全体を表示
MX6X_DDR3_调校_应用手册_V4_20150730.doc
記事全体を表示
Introduction i.MX25 PDK Board Get Started Bootloader i.MX25 PDK Board Flashing NAND i.MX25 PDK Board Flashing SD Card i.MX25 PDK Board Flashing SPI NOR I.MX25 PDK U-boot SDCard I.MX25 PDK U-boot SplashScreen I.MX25 PDK Using FEC
記事全体を表示
This steps are basically the same used to boot Linux mainline on i.MX 31 ADS, just replacing Network Driver cs89x0 by i.MX 27 internal FEC. Download Linux kernel 2.6.30: $ wget -c http://www.kernel.org/pub/linux/kernel/v2.6/linux-2.6.30.tar.bz2 Extract this: $ tar jxvf linux-2.6.30.tar.bz2 Export CROSS_COMPILE environmet: $ export PATH="$PATH:/opt/freescale/usr/local/gcc-4.1.2-glibc-2.5-nptl-3/arm-none-linux-gnueabi/bin/" $ export CROSS_COMPILE=arm-none-linux-gnueabi- Unselect all no essentials features: $ make ARCH=arm allnoconfig Start the configuration menu: $ make ARCH=arm menuconfig Change/Select the kernel options below. Select the MXC/iMX platform and iMX27ADS board: System Type ->             ARM system type -> (X) Freescale MXC/iMX-based             Freescale MXC Implementations  ->                            MXC/iMX Base Type -> (X) MX2-based                            MX2 Options  -> [*] Support MX27ADS platforms (NEW) Select ARM EABI standard to compile the kernel: Kernel Features  --->           [*] Use the ARM EABI to compile the kernel Add support to Linux Binary Format ELF: Userspace binary formats ->              [*] Kernel support for ELF binaries Add support to Network (TCP/IP): [*] Networking support  ->          Networking options  ->                           [*] Packet socket                           [*] Unix domain sockets                           [*] PF_KEY sockets                           [*] TCP/IP networking                                    [*] IP: kernel level autoconfiguration                                    [*]     IP: DHCP support Select network driver (FEC), serial driver and unselect VGA console: Device Drivers  ->                      [*] Network device support  --->                                       [*]   Ethernet (10 or 100Mbit)  --->                                              [*]   FEC ethernet controller (of ColdFire CPUs)                      Character devices  ->                              Serial drivers  --->                                       [*] IMX serial port support                                       [*]   Console on IMX serial port                      Graphics support  ->                              Console display driver support  --->                                         [ ] VGA text console Add support to NFS and support to use it as root file system: File systems  ->                           [*] Network File Systems (NEW)  ->                                    [*]   NFS client support                                    [*]     Root file system on NFS Compile the kernel: $ make ARCH=arm Copy the created zImage to tftp directory: $ cp arch/arm/boot/zImage /tftpboot/ Configure your RedBoot to boots with this kernel: load -r -b 0x100000 /tftpboot/zImage exec -b 0x100000 -l 0x200000 -c "noinitrd console=ttymxc0,115200 root=/dev/nfs nfsroot=10.29.240.191:/tftpboot/rootfs ip=dhcp" Change the default network device on RedBoot to internal FEC: Default network device: mxc_fec Connect the network cable on FEC connector (connector T3). Notes: We are using rootfs from LTIB then select to get parameters from DHCP: "Target System Configuration" Options  --->               [*] start networking                      Network setup  --->                            [*]   get network parameters using dhcp
記事全体を表示
Most i.MX8QXP/QM customers already work on L4.14.98 GA for their Auto product, like C-V2X TBOX, Car infortainment system. Some customers also want to adopt OP-TEE in their security design, but OP-TEE on i.MX8QXP/QM platform don't support HW cryptography accelerating which base on CAAM module. So I worked on the issue last week and fixed it. The package meta-optee-add-on_4.14.98_2.0.0_ga.tgz is Yocto layer which includes all patches for fixing the issue. Software environments as the belows: Linux kernel: imx_4.14.98_2.0.0_ga HW platform:  i.MX8QM/QXP MEK. How to build: 1, decompress meta-optee-add-on_4.14.98_2.0.0_ga.tgz and copy meta-optee-add-on to folder (Yocto 4.14.98_2.0.0_ga dir)/sources/ 2, Run DISTRO=fsl-imx-wayland MACHINE=imx8qxpmek source fsl-setup-release.sh -b build-optee and add BBLAYERS += " ${BSPDIR}/sources/meta-optee-add-on " into (Yocto 4.14.98_2.0.0_ga dir)/build-optee/conf/bblayers.conf  3, Run bitbake fsl-image-validation-imx. 4, You can run xtest or xtest -l 1 4007 on your MEK board to test optee crypto feature after completing build image. You can find it only take about one second comparing no CAAM accelerating when test "regression_4007.11 Generate RSA-2048 key".
記事全体を表示
This document provide an overall guide how to get started with i.MX6 development. There are several chapters: 1. how to get necessary docs from freescale website; 2. how to setup environment and build your own images;3. Hardware design consideration;4. How to get help. I hope the doc will bring you in i.MX world more easily, and hope you all have a fun in it.
記事全体を表示
This is the procedure and patch to set up Ubuntu 13.10 64bit Linux Host PC and building i.MX6x L3.0.35_4.1.0. It has been tested to build GNOME profile and with FSL Standard MM Codec for i.MX6Q SDB board. A) Basic Requirement: Set up the Linux Host PC using ubuntu-13.10-desktop-amd64.iso Make sure the previous LTIB installation and the /opt/freescale have been removed B) Installed the needed packages to the Linux Host PC $ sudo apt-get update $ sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev $ sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool $ sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool $ sudo apt-get install uuid-dev liblzo2-dev $ sudo apt-get install tcl dpkg $ sudo apt-get install asciidoc texlive-latex-base dblatex xutils-dev $ sudo apt-get install texlive texinfo $ sudo apt-get install lib32z1 lib32ncurses5 lib32bz2-1.0 $ sudo apt-get install libc6-dev-i386 $ sudo apt-get install u-boot-tools $ sudo apt-get install scrollkeeper $ sudo apt-get install gparted $ sudo apt-get install nfs-common nfs-kernel-server $ sudo apt-get install git-core git-doc git-email git-gui gitk $ sudo apt-get install meld atftpd $ sudo ln -s /usr/lib/x86_64-linux-gnu/librt.so   /usr/lib/librt.so C) Unpack and install the LTIB source package and assume done on the home directory: $ cd ~ $ tar -zxvf L3.0.35_4.1.0_130816_source. tar.gz $ ./L3.0.35_4.1.0_130816_source/install      After that, you will find ~/ltib directory created D) Apply the patch to make L3.0.35_4.1.0 could be installed and compiled on Ubuntu 13.10 64bit OS $ cd ~/ltib $ git apply 0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_13.10_64bit_OS.patch What the patch is doing: a) The patch modifies the following files:    dist/lfs-5.1/base_libs/base_libs.spec    dist/lfs-5.1/m4/m4.spec    dist/lfs-5.1/ncurses/ncurses.spec b) Add the following files to the pkgs directory:    pkgs/m4-1.4.16-1383761043.patch    pkgs/m4-1.4.16-1383761043.patch.md5 E) Then, it is ready to proceed the rest of the LTIB env setup process: $ cd ~/ltib $ ./ltib -m config $ ./ltib Reference: L3.0.35_4.1.0_130816_docs/doc/mx6/Setting_Up_LTIB_host.pdf https://community.freescale.com/message/332385#332385 https://community.freescale.com/thread/271675 https://community.freescale.com/message/360556#360556 m4 compilation issue: 1. https://github.com/hashdist/hashstack/commit/f6be2a58de62327d05e052d89c9aa931d4c926b3 2. https://github.com/hashdist/hashstack/issues/81 rpm-fs package failed to build issue: https://community.freescale.com/message/355771#355771 scrollkeeper is for the gnome-desktop compilation NOTE: When compiling gstreamer, this warning was pop up.  Just ignore it seems okay.
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343715 
記事全体を表示
The Compatibility Test Suite Verifier is a supplement to the Compatibility Test Suite. The main difference lies in that the verifier is developed for tests that cannot run on their own so they require user input in order to be tested. These tests would include the audio quality, the touchscreen, accelerometer, camera, etc. There is no “best verifier option”, one CTS complements the other. In this document we will focus on how to perform the Verifier test. Requirements: A PC with the Android SDK installed. Your “Device Under Test” (your development board) Optional >> A second android device with compatible Wifi and Bluetooth Setup Steps: Install de Android SDK on your PC Download the appropriate CTS Verifier APK. The list of APK’s can be found here: https://source.android.com/compatibility/downloads.html Make sure that your Device Under Test has its system date and time set correctly. Install the CTS Verifier APK on the Device Under Test* For more information regarding ADB commands, follow this link: https://community.freescale.com/docs/DOC-102514 Initialization: After the setup is done, you should see the application installed: You will see the list of available tests for manual verification: Video Link : 4502 For each test, you will see detailed instructions to run it, and a “pass” and “fail” buttons. Video Link : 4530 Once you run each test, you will have the posibility to choose the outcome. (in some cases, pass/fail outcome will be determined automatically). The list of tests (for CTS Verifier 5.1_r2) is: Camera: FOV Calibration, Formats, ITS, Intents, Orientation, Video. Car: Car Dock Test Clock: Alarms and Timers Test Device Administration: Policy serialization test, screen lock test. Features: Hardware/Software feature summary Hardware: USB Accessory Test Job Scheduler: Charging constraints, connectivity constraints, idle mode constraints. Location: Battery saving mode test, location mode off test Managed provisioning: BYOD managed provisioning, device owner provisioning Networking: Bluetooth test, Wi-Fi direct test Notifications: CA Cert notification, CA Cert notificacion on boot, notification attention management, notification listener, notificacion package priority Other: Data backup, screen pinning, widget framework Projection: Projection cube, projection multitouch, projection offscreen, projection scrolling, projection video playback, projection widget Security: Keyguard password verification, SUID file scanner. Sensors: Accelerometer mearument, CTS Sensor batching, CTS Sensor integration, CTS sensor test, CTS single sensor test, magnetic field measurement, sensor batching. Streaming: Streaming video quality verifier. Exporting test results: Tap the “save disk” icon. A pop-up will show the path of the report that was created. Video Link : 4531 With the board connected to the PC through USB, pull the report using ADB: To download all reports run : adb pull /mnt/sdcard/ctsVerifierReports/ .
記事全体を表示
All below changes are done based on imx_android-10.0_5.4.y. mek_8qm enable uSD 8987 wifi            1. hardware rework                no hardware rework required            2. patches The patch is attached as 0001-8qm-usd-8987-wifi.patch mek_8qm enable M.2 8987 wifi            1. hardware rework                no hardware rework required            2. patches The patch is attached as 0001-8qm-m2-8987-wifi.patch evk_8mq enable uSD 8987 wifi            1. hardware rework                no hardware rework required            2. patches diff --git a/imx8m/evk_8mq/BoardConfig.mk b/imx8m/evk_8mq/BoardConfig.mk index db7c4991..4d130cc0 100644 --- a/imx8m/evk_8mq/BoardConfig.mk +++ b/imx8m/evk_8mq/BoardConfig.mk @@ -136,7 +136,8 @@ ifeq ($(TARGET_USE_DYNAMIC_PARTITIONS),true) TARGET_BOARD_DTS_CONFIG ?= imx8mq:imx8mq-evk-no-product.dtb else # imx8mq with HDMI display - TARGET_BOARD_DTS_CONFIG ?= imx8mq:imx8mq-evk-pcie1-m2.dtb + TARGET_BOARD_DTS_CONFIG ?= imx8mq:imx8mq-evk-usd-wifi.dtb + # imx8mq with MIPI-HDMI display TARGET_BOARD_DTS_CONFIG += imx8mq-mipi:imx8mq-evk-lcdif-adv7535.dtb # imx8mq with HDMI and MIPI-HDMI display diff --git a/imx8m/evk_8mq/SharedBoardConfig.mk b/imx8m/evk_8mq/SharedBoardConfig.mk index 330ab1c5..a6654bad 100644 --- a/imx8m/evk_8mq/SharedBoardConfig.mk +++ b/imx8m/evk_8mq/SharedBoardConfig.mk @@ -7,10 +7,10 @@ PRODUCT_IMX_TRUSTY := true #Enable this to disable product partition build. #IMX_NO_PRODUCT_PARTITION := true -#NXP 8997 wifi driver module +# NXP 8987 wifi driver module BOARD_VENDOR_KERNEL_MODULES += \ - $(KERNEL_OUT)/drivers/net/wireless/marvell/mrvl8997/wlan_src/mlan.ko \ - $(KERNEL_OUT)/drivers/net/wireless/marvell/mrvl8997/wlan_src/pcie8xxx.ko + $(KERNEL_OUT)/drivers/net/wireless/nxp/mxm_wifiex/wlan_src/mlan.ko \ + $(KERNEL_OUT)/drivers/net/wireless/nxp/mxm_wifiex/wlan_src/moal.ko # mipi-panel touch driver module BOARD_VENDOR_KERNEL_MODULES += \ diff --git a/imx8m/evk_8mq/UbootKernelBoardConfig.mk b/imx8m/evk_8mq/UbootKernelBoardConfig.mk index 5aa1ce35..4c3378f0 100644 --- a/imx8m/evk_8mq/UbootKernelBoardConfig.mk +++ b/imx8m/evk_8mq/UbootKernelBoardConfig.mk @@ -14,7 +14,7 @@ endif TARGET_BOOTLOADER_CONFIG += imx8mq-evk-uuu:imx8mq_evk_android_uuu_defconfig TARGET_KERNEL_DEFCONFIG := imx_v8_android_defconfig -# TARGET_KERNEL_ADDITION_DEFCONF ?= android_addition_defconfig +TARGET_KERNEL_ADDITION_DEFCONF ?= android_addition_defconfig diff --git a/imx8m/evk_8mq/android_addition_defconfig b/imx8m/evk_8mq/android_addition_defconfig new file mode 100644 index 00000000..f51bd5ff --- /dev/null +++ b/imx8m/evk_8mq/android_addition_defconfig @@ -0,0 +1,2 @@ +CONFIG_WLAN_VENDOR_NXP=y +CONFIG_MXMWIFIEX=m diff --git a/imx8m/evk_8mq/early.init.cfg b/imx8m/evk_8mq/early.init.cfg index 9262d953..70097a1c 100644 --- a/imx8m/evk_8mq/early.init.cfg +++ b/imx8m/evk_8mq/early.init.cfg @@ -1,3 +1,3 @@ insmod vendor/lib/modules/mlan.ko -insmod vendor/lib/modules/pcie8xxx.ko sta_name=wlan uap_name=wlan wfd_name=p2p max_vir_bss=1 cfg80211_wext=0xf cal_data_cfg=none p2p_enh=1 fw_name=pcieuart8997_combo_v4.bin +insmod vendor/lib/modules/moal.ko sta_name=wlan uap_name=wlan wfd_name=p2p max_vir_bss=1 cfg80211_wext=0xf cal_data_cfg=none fw_name=sdiouart8987_combo_v0.bin insmod vendor/lib/modules/synaptics_dsx_i2c.ko diff --git a/imx8m/evk_8mq/evk_8mq.mk b/imx8m/evk_8mq/evk_8mq.mk index 7db1b212..210f8971 100644 --- a/imx8m/evk_8mq/evk_8mq.mk +++ b/imx8m/evk_8mq/evk_8mq.mk @@ -250,9 +250,9 @@ PRODUCT_PACKAGES += \ PRODUCT_PACKAGES += \ bt_vendor.conf -# NXP 8997 Wifi and Bluetooth Combo Firmware +# NXP 8987 Wifi and Bluetooth Combo Firmware PRODUCT_COPY_FILES += \ - vendor/nxp/imx-firmware/nxp/FwImage_8997/pcieuart8997_combo_v4.bin:vendor/firmware/pcieuart8997_combo_v4.bin + vendor/nxp/imx-firmware/nxp/FwImage_8987/sdiouart8987_combo_v0.bin:vendor/firmware/sdiouart8987_combo_v0.bin # Wifi regulatory PRODUCT_COPY_FILES += \ The patch is attached as 0001-8mq-usd-8987-wifi.patch evk_8mq enable M.2 8987 wifi            1. hardware rework                hardware rework required ( Be aware: after this rework, uSD is not working!)            2. patches diff --git a/imx8m/evk_8mq/BoardConfig.mk b/imx8m/evk_8mq/BoardConfig.mk index db7c4991..0cca9b8e 100644 --- a/imx8m/evk_8mq/BoardConfig.mk +++ b/imx8m/evk_8mq/BoardConfig.mk @@ -136,7 +136,8 @@ ifeq ($(TARGET_USE_DYNAMIC_PARTITIONS),true) TARGET_BOARD_DTS_CONFIG ?= imx8mq:imx8mq-evk-no-product.dtb else # imx8mq with HDMI display - TARGET_BOARD_DTS_CONFIG ?= imx8mq:imx8mq-evk-pcie1-m2.dtb + TARGET_BOARD_DTS_CONFIG ?= imx8mq:imx8mq-evk-usdhc2-m2.dtb + # imx8mq with MIPI-HDMI display TARGET_BOARD_DTS_CONFIG += imx8mq-mipi:imx8mq-evk-lcdif-adv7535.dtb # imx8mq with HDMI and MIPI-HDMI display diff --git a/imx8m/evk_8mq/SharedBoardConfig.mk b/imx8m/evk_8mq/SharedBoardConfig.mk index 330ab1c5..a6654bad 100644 --- a/imx8m/evk_8mq/SharedBoardConfig.mk +++ b/imx8m/evk_8mq/SharedBoardConfig.mk @@ -7,10 +7,10 @@ PRODUCT_IMX_TRUSTY := true #Enable this to disable product partition build. #IMX_NO_PRODUCT_PARTITION := true -#NXP 8997 wifi driver module +# NXP 8987 wifi driver module BOARD_VENDOR_KERNEL_MODULES += \ - $(KERNEL_OUT)/drivers/net/wireless/marvell/mrvl8997/wlan_src/mlan.ko \ - $(KERNEL_OUT)/drivers/net/wireless/marvell/mrvl8997/wlan_src/pcie8xxx.ko + $(KERNEL_OUT)/drivers/net/wireless/nxp/mxm_wifiex/wlan_src/mlan.ko \ + $(KERNEL_OUT)/drivers/net/wireless/nxp/mxm_wifiex/wlan_src/moal.ko # mipi-panel touch driver module BOARD_VENDOR_KERNEL_MODULES += \ diff --git a/imx8m/evk_8mq/UbootKernelBoardConfig.mk b/imx8m/evk_8mq/UbootKernelBoardConfig.mk index 5aa1ce35..4c3378f0 100644 --- a/imx8m/evk_8mq/UbootKernelBoardConfig.mk +++ b/imx8m/evk_8mq/UbootKernelBoardConfig.mk @@ -14,7 +14,7 @@ endif TARGET_BOOTLOADER_CONFIG += imx8mq-evk-uuu:imx8mq_evk_android_uuu_defconfig TARGET_KERNEL_DEFCONFIG := imx_v8_android_defconfig -# TARGET_KERNEL_ADDITION_DEFCONF ?= android_addition_defconfig +TARGET_KERNEL_ADDITION_DEFCONF ?= android_addition_defconfig # absolute path is used, not the same as relative path used in AOSP make diff --git a/imx8m/evk_8mq/android_addition_defconfig b/imx8m/evk_8mq/android_addition_defconfig new file mode 100644 index 00000000..f51bd5ff --- /dev/null +++ b/imx8m/evk_8mq/android_addition_defconfig @@ -0,0 +1,2 @@ +CONFIG_WLAN_VENDOR_NXP=y +CONFIG_MXMWIFIEX=m diff --git a/imx8m/evk_8mq/early.init.cfg b/imx8m/evk_8mq/early.init.cfg index 9262d953..70097a1c 100644 --- a/imx8m/evk_8mq/early.init.cfg +++ b/imx8m/evk_8mq/early.init.cfg @@ -1,3 +1,3 @@ insmod vendor/lib/modules/mlan.ko -insmod vendor/lib/modules/pcie8xxx.ko sta_name=wlan uap_name=wlan wfd_name=p2p max_vir_bss=1 cfg80211_wext=0xf cal_data_cfg=none p2p_enh=1 fw_name=pcieuart8997_combo_v4.bin +insmod vendor/lib/modules/moal.ko sta_name=wlan uap_name=wlan wfd_name=p2p max_vir_bss=1 cfg80211_wext=0xf cal_data_cfg=none fw_name=sdiouart8987_combo_v0.bin insmod vendor/lib/modules/synaptics_dsx_i2c.ko diff --git a/imx8m/evk_8mq/evk_8mq.mk b/imx8m/evk_8mq/evk_8mq.mk index 7db1b212..210f8971 100644 --- a/imx8m/evk_8mq/evk_8mq.mk +++ b/imx8m/evk_8mq/evk_8mq.mk @@ -250,9 +250,9 @@ PRODUCT_PACKAGES += \ PRODUCT_PACKAGES += \ bt_vendor.conf -# NXP 8997 Wifi and Bluetooth Combo Firmware +# NXP 8987 Wifi and Bluetooth Combo Firmware PRODUCT_COPY_FILES += \ - vendor/nxp/imx-firmware/nxp/FwImage_8997/pcieuart8997_combo_v4.bin:vendor/firmware/pcieuart8997_combo_v4.bin + vendor/nxp/imx-firmware/nxp/FwImage_8987/sdiouart8987_combo_v0.bin:vendor/firmware/sdiouart8987_combo_v0.bin The patch is attached as 0001-8mq-m2-8987-wifi.patch
記事全体を表示
This is a simple document  explaining the basics of creating a new layer within a Yocto BSP. We will be using the latest i.MX6 Linux BSP as reference, but the same logics apply to any Yocto Project BSP including the Community BSP. If you are new to Yocto it is recommended to go through the following very informative Training which is focused on the FSL Community BSP but covers the basics of Yocto step-by-step in a very clear and concise manner. Yocto Training - HOME Requirements - L4.1.15 BSP Release for the i.MX6 family of processors installed on the host. For more information on requirements for the Host please refer to the Yocto User’s Guide available as part of the Linux BSP Document Bundle (available on the link below) http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-processors/embedded-linux-for-i.mx-applications-processors:IMXLINUX?code=IMXLINUX -tree tool for the host, to see the directory format of the different layers. You may install it with the following command: sudo apt-get install tree - We will work with the bitbake environment so this needs to be initialized in our terminal. Introduction to layers in Yocto Layers in Yocto allow us to organize the long list of providers and to easily customize for our target hardware while reusing a lot of tools already available. It also makes it easy to distribute our customizable source code trough a unique layer. Once your environment is setup you can see the layers that compose the BSP using the command: bitbake-layers show-layers The layers that constitute out BSP will be displayed along with the path and priority of each. Layer Priority: Each layer has a priority, which is used by bitbake to decide which layer takes precedence if there are recipe files with the same name in multiple layers. A higher numeric value represents a higher priority. We can see that the poky and open embedded layers have a lower priority than those than the BSP and SDK layers as the later sit on top of the former. The general layout of a BSP is shown on the image below. If you would like to have a better look at the distinctive Layers that make up the Yocto BSP Release and the FSL Community Release please look at the Yocto Project Layers Mind Map available on the following link: YOCTO PROJECT LAYERS MIND MAP Adding an empty layer and a new recipe There are a couple of scripts available as part of the Open embedded tools that allows for easy creation of a new layer and recipe. Layers are basically a group of directories and meta data in configuration and recipe files (which contains metadata as text), so you may create these directories and meta data files by hand. However, it’s always easier to use the new layer script in order to create the required structure and then fill in with our customized configuration. cd <BSP_DIR>/sources ./poky/scripts/yocto-layer create <NEW_LAYER_NAME> We’ll name the new layer “new-layer” as shown below: ./poky/scripts/yocto-layer create new-layer We’ll be asked to enter le layer priority, we’ll keep the default 6 but you may want a higher priority depending on your application. You may opt for an example recipe to be created on your new layer.  We’ll leave this example recipe with the default settings. You may see the structure of the new layer by using the following command: tree -L 4 ./meta-new-layer Basic requirements of a layer - It is not a must but it’s strongly recommended to have the name of the layer start with “meta-“, the Poky new layer script uses this naming convention. - A README with information regarding what’s contained in the layer and any dependencies - A COPYING file with the copyright and use notice for the hardware in the new layer. - A conf folder which contains the layer’s configuration (.conf) files. Adding the layer to our BSP Once the layer has been created it’s necessary to add it to the list of Layers that make up the BSP so Bitbake can locate it and parse the metadata contained within it, in other words, you must make the build system aware of your new layer. In order to enable your layer you need to add the layer’s path to the BBLAYERS variable in the conf/bblayers.conf file which is found on the build directory. Please note that you will need to add your layer to each build directory in which you want to use it. We can add the following line to add our new layer. BBLAYERS += " ${BSPDIR}/sources/meta-new-layer " After doing so we’ll see that our layer is now listed when we run show-layers in bitbake-layers. bitbake-layers show-layers Adding a new recipe The new layer script also creates a basic recipe. It is recommended to look for recipes similar to what we need and use them as a template or starting point, as part of the benefits of Yocto is to be able to reuse a lot of open sourced code and resources. If there are many versions of the same recipe the default behavior is to use the recipe contained in the highest priority layer even if it’s not the higher version of the recipe. If you would want to force bitbake to use a certain version you may use the following variable on the local.conf file. PREFERRED_VERSION_recipename Main requirements of a recipe: SRC_URI which points to the location of the source code SRC_REV if applicable it would correspond to a particular commit or branch from the source code repository LICENSE a variable that defines the type of license to bitbake LIC_FILES_CHKSUM should point to a file within the source tree that corresponds to the md5 check-sum of the license file so it can be verified. Adding an append to a recipe You may also select the option to have the script create an append file. The append files allow us to change an existing recipe. The name of the file must be the same as the original recipe plus the append suffix (.bbappend) and should be located on the same path as the original recipe but in our own layer. The append file can be described as a piece of code or metadata that is added to the end of the original recipe. If there are more than one append files for a particular recipe all of them will be joined in reverse priority, that is, the highest priority layer’s bbappend will be added last. Appendix. Useful References FSL Community BSP Yocto Training - HOME Yocto Project Board Support Package Developer's Guide
記事全体を表示
What is HTML5 Video? HTML5 video is an element for the purpose of playing videos or movies in HTML5 specification. HTML5 video is intended by its creators to become the new standard way to show video on the web without plugins. Video will be shown inside the web page, like flash. HTML5 Video Web Page <video> element example <video src="movie.mp4" poster="movie.jpg" controls> </video> HTML5 video page source example <html>           <head>           </head>            <body>                      <video src="http://10.192.225.226/movie.mp4" width="640" height="480"  controls="true">                      </video>            </body> </html> HTML5 Video Rendering Path Performance Data in i.MX6Q with Android ICS With LVDS display, H264@1080p@20Mbps Can reach 30 fps With HDMI 1080p display, H264@1080p@10Mbps Can reach 25 fps HTML5 Video Website Some HTML5 Video website when accessing with android platform www.youtube.com www.iqiyi.com HTML5 reference document SPEC         http://dev.w3.org/html5/spec/single-page.html?utm_source=dlvr.it&utm_medium=feed Wikipedia page        http://en.wikipedia.org/wiki/HTML5
記事全体を表示
This example is useful  if you have your device connected to a host machine using a USB cable, and you want your host machine to be able to update your device using a protocol ready to go. Information you need prior to using this example Fastboot is a protocol used to update firmware in Android devices from a host over USB; Freescale implements fastboot as a uboot driver for the device and the implementation is available from patches applied to uboot source code; By default, fastboot is only enabled when building uboot to use with an Android BSP; To run fastboot at the device in default implementation you need to call it from uboot command line (using the debug serial port of the slave device, for example); The host fastboot application is available as source code from Google. You can build your own fastboot(.exe) binary (which is not in the scope of this howto), or you can find a binary ready for you to go searching the web; You are required to be familiar with Linux BSP and have i.MX53 BSP version 11.05 installed. With this information in mind, what do you get from this example? Patch for uboot to enable fastboot driver for iMX53 Quick Start Board with a new spec file; A command line application that set a flag in iMX53 to automatically start fastboot after a reset, either if it is a SOFT or a HARD reset. How to prepare the example Copy uboot patch file (attached) to /opt/freescale/pkgs; Replace your uboot spec file (u-boot.spec.in attached) in <bsp_root>/ltib/config/platform/imx/; Build a system image for iMX53 Quick Start Board with the packages you need; Build the command line application (setbootmode.c attached) using ltib shell; Prepare an SD card copy the command line application /usr/sbin in your SD card system partition. See attachment to this page. How to test the example Boot the Quick Start Board with the SD card you prepared; Login as root using a serial cable and a terminal application; Run setbootmode application as follows: $ setbootmode 1 Reboot the system: $ reboot After rebooting, the device will automatically run fastboot from uboot and will wait for a connection from the host machine. You can test the connection using a fastboot binary at the host machine (not provided here). Even if you HARD reset your hardware, your device will keep running fastboot at startup. If you want to go back to a regular boot operation, you need to cut power supply to your board. How does the magic happen? The setbootmode application sets the LSB in the Low Power General Register (LPGR) of the Secure Real Time Clock (SRTC) module to true. The patched version o uboot tests for this bit as a flag to run fastboot or not. The magic is that the LPGR is persistent, even during reset. Additional tips You can run setbootmode with no arguments to see its options; You need to set the boot mode to 0 after a successful update to avoid entering fastboot mode again after a new reboot; Partitioning of the device seen by fastboot is not implemented; Besides using setbootmode, you can read/set LPGR using either md.l / nm.l in uboot or devmem2 at command line: uboot-> md.l 0x53fa401c 1 - displays LPGR; uboot-> nm.l 0x53fa401c - presents a prompt for you to change LPGR; linux shell-> devmem2 0x53fa401c w - displays LPGR; linux shell-> devmem2 0x53fa401c w <value> - changes LPGR; devmem2 has issues that you need to fix so that you can use it to change LPGR: include "volatile" in all writing instruction; uncomment 'w' write instruction.
記事全体を表示
Documents Imx53-fastboot-example i.MX53 Multimedia Applications Processors I.MX53 QSB Board Get Started IMX53 QSB enable WIFI android I.MX53 QSB Ubuntu Dual Display i.MX53 Quick Start Board IMX53 SABRE AI i.MX53 Start-R Lab Exercise - Prof. Massimo Violante Politecnico of Torino i.MX53 Start-R Lab Exercise - Developing a loadable kernel module to manage GPIOs in i.MX53QSB ConnectCore® i.MX53 / Wi-i.MX53 by Digi International NOVPEK i.MX53 by NovTech
記事全体を表示
The i.MX 6 D/Q L3.035_1.0.3 patch release is now available on www.freescale.com ·         Files available # Name Description 1 L3.0.35_1.0.3_TEMP_PFD_PATCH This patch release is based on the i.MX 6Dual/6Quad Linux   12.09.01 release. The purpose of this patch release is update thermal sensor   calibration routine and correct the PFD workflow in U-Boot. More details in   the release notes.
記事全体を表示