i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
Audio transcoding # Transcode the input file into MP3 gst-launch filesrc location=media_file typefind=true ! beepdec ! mfw_mp3encoder ! matroskamux ! filesink location=output_audio_file.mk Audio transcoding + streaming # Transcode the input file into MP3 and stream it # On host, get the transcoded audio data gst-launch udpsrc port=8880 ! <CAPS_FROM_THE_TARGET> ! queue ! ffdec_mp3 ! alsasink # where <CAPS_FROM_THE_TARGET> can be something like 'audio/mpeg, mpegversion=(int)1, layer=(int)3, rate=(int)44100, channels=(int)2' # run the pipeline and check the caps gst-launch filesrc location=media_file typefind=true ! queue ! beepdec ! mfw_mp3encoder ! udpsink host=10.112.103.77 port=8880 -v Video Transcoding* # Transcode the input file into AVC (H-264) gst-launch filesrc location=media_file typefind=true ! aiurdemux name=demux ! queue ! vpudec ! vpuenc codec=avc ! matroskamux name=mux ! filesink location=output_media_file.mk Video Transcoding + scaling* # Transcode the input file into AVC (H264) and rescale video to 480p gst-launch filesrc location=media_file typefind=true ! aiurdemux name=demux ! queue ! vpudec ! mfw_ipucsc ! 'video/x-raw-yuv, width=(int)720, height=(int)480' ! vpuenc codec=avc ! matroskamux name=mux ! filesink location=output_media_file.mk Video transcoding + scaling + streaming* # NOTE: Run the pipelines in the presented order # On host, get the transcoded+scaled video data $ gst-launch udpsrc port=8888 ! <CAPS_FROM_THE_TARGET> ! queue ! ffdec_h264 ! xvimagesink # On target, run the pipeline and check the caps gst-launch filesrc location=media_file typefind=true ! aiurdemux name=demux ! queue ! vpudec ! mfw_ipucsc ! 'video/x-raw-yuv, width=(int)720, height=(int)480' ! vpuenc codec=avc ! udpsink host=$HOST_IP port=8888 -v * There is a limit for the number of pipelines which can be run simultaneously, for high resolution input files, at most two for 1080p and four for 720p.
記事全体を表示
You can power on/off i.MX31 PDK LEDs using U-Boot: u-boot> mw.b B6020000 FF Where B6020000 is the CPLD LED address and FF is the 8 bits hexadecimal value which will be displayed on LEDs.
記事全体を表示
Creating Deployment System          Configuring Bootloader       Running Linux     
記事全体を表示
The attached is the document and sample code for iMX5 system 80 interface LCD driver based on IPUV3. It is based on iMX51 2.6.31_09.12 BSP (SDK 1.7), tested on iMX53 3-Stack board. 1. Description This is Smartlcd driver for Freescale MX51 SDK1.7 release. (Kernel: 2.6.31_09.12.00/01)  2. File List -- Smartlcd_giantplus_4_IMX51_Linux_2.6.31_09.12.01.patch: SmartLCD panel support patch, and unit test code. -- Sample.config: the config file for reference. -- readme.txt: this file, please refer to it before use the package. -- SmartLCD Structure.pptx: the basic structure for smartlcd on IPUv3. 3. Requirement - MX51_3DS Green board(TO2.0) - No hardware rework needed, only need plug the giantplus GMA722A0 to J10. - MX51 SDK1.7 release package - L2.6.31_09.12.00_SDK_source.tar.gz                                - redboot_200952.zip 4. How to use 4.1 How to use demo -- Program default redboot.bin to board via ATKtools -- Copy attached zImage to tftp folder (assume /tftpboot) -- extract default rootfs to NFS folder (assume /nfsroot) -- COPY attached imx51_fb_test to ~/unit_test folder. -- Power on the board -- After redboot is boot up, use following command to boot up linux kernel    load -r -b 0x100000 zImage    exec -c "noinitrd console=ttymxc0 root=/dev/nfsroot rootfstype=nfsroot nfsroot=10.192.225.221:/nfsroot/rootfs rw ip=dhcp" -- Once the linux kernel launched, run following commands to test smartlcd panel.    cd /unit_tests    ./imx51_fb_test 4.2 How to use source code -- Current release code is based on L2.6.31_09.12.00_SDK_source.tar.gz. Extract the file to your working folder. -- Entering the working folder and type "./install", select a folder to install ltib. (such as .../ltib) -- Entering ltib folder and type "./ltib" to build Linux platform.  If you are not familiar with this setp, please refer to doc "i.MX_3Stack_SDK_UserGuide.pdf" for detail. -- Entering folder ".../ltib/rpm/BUILD/linux", copy "Smartlcd_giantplus_4_IMX51_Linux_2.6.31_09.12.01.patch" from release package to current folder    Run command "patch -p1 < Smartlcd_giantplus_4_IMX51_Linux_2.6.31_09.12.01.patch" -- When complete, run command "make ARCH=arm menuconfig", and you can refer to attached sample.config for detail.    * enable    Device Drivers ----> Graphics support ----> [*]   Asynchronous Panels                                            ----> [*] GiantPlus 240x320 Panel                                             * disable    Device Drivers ----> Graphics support ----> [ ]   Synchronous Panel Framebuffer                                         ----> Multimedia support    ----> [ ]   Video For Linux                                             -- Run command "make ARCH=arm" to build kernel.  4.3 How to do SMARTLCD driver test -- After Smartlcd_giantplus_4_IMX51_Linux_2.6.31_09.12.01.patch applied, there will be an folder "IMX51_TEST" under linux. -- Go to that folder, and run "make ARCH=arm", imx51_fb_test will be created. -- Copy imx51_fb_test to rootfs/unit_test. and run. 5. History N/A 6. Known Issue -- V4L2 not working yet.
記事全体を表示
Changing Freescale's BSP U-boot using LTIB This quick recipe demonstrates how to compile U-boot using Freescale BSP. 0. After installing i.MX51 BSP: 1. Extract u-boot source: ./ltib -m prep -p u-boot 2. (optional) If you wish to apply changes to the code, the source is located at: <ltib path>/rpm/BUILD/u-boot-2009.08 3. Compile u-boot for the i.MX51 EVK ./ltib -m scbuilb -p u-boot 4. Copy the compiled file to a SD card on your host machine, insert the SD card and: $ sudo dd if=rpm/BUILD/u-boot-2009.08/u-boot.bin of=/dev/mmcblk0 bs=512 /dev/mmcblk0 should replaced according to your host, use "dmesg" after inserting the SD to find out where is the SD on your host. Unmount it before issuing the dd command.   5. Insert the SD on the i.MX 51 EVK, set the switches for SD Card boot and power on the board.
記事全体を表示
Q: To minimize i.MX6DL power consumption at stop mode, but needs i.MX6DL to wake-up by USB resume signal from Host PC. Can LDO_2P5(VDDHIGH_CAP) be powered off at stop mode in order to resume i.MX6DL by a USB resume signal that Host PC sends to i.MX6DL USBOTG(us as device mode only)? In other words, can USB OTG detect resume signal from Host PC and generate wakeup interrupt during stop mode with following LDO condition? -          LDO_USB is enabled and powered by USB_OTG_VBUS. -          LDO_2P5 is disabled during stop mode. -          LDO_1P1 is enabled during stop mode. The system uses LPDDR2, hence LDO_2P5 can be powered off at stop mode(I know this is not allowed for DDR3 as DDR IO need 2P5 as pre-driver). Actually tested on SDP, the system can not be resumed without LDO_2P5 as DDR IO need 2P5 for DDR3. A: Please note that disabling the LDO_2P5 supply, you are also disabling the DRAM, as the DRAM pre-drivers are powered by this supply(!). SDCKE is pulled down on the board, and it ensures that the DRAM is in proper state during DSM without LDO_2P5 power. we recommend to keep LDO_2P5 on at any mode(include DSM mode). ldo_2p5 is also one of power for USB phy.   4.3.2.2 LDO_2P5 The LDO_2P5 module implements a programmable linear-regulator function from VDD_HIGH_IN. The LDO_2P5 supplies the SATA Phy, USB Phy, LVDS Phy,   Actually I have tested on SDP, but we cannot resume the system without LDO_2P5 as DDR IO need 2P5 for DDR3.
記事全体を表示
how to enable bt on imx6 sabreasd_dq
記事全体を表示
ro.hwui.disable_scissor_opt For Vivante GPU, the scissor should be enabled. The default value is enabled, So, keep the default value. ro.hwui.texture_cache_size ro.hwui.layer_cache_size ro.hwui.r_buffer_cache_size ro.hwui.path_cache_size ro.hwui.drop_shadow_cache_size These parameters depend on display resolution. The default value is calculated according to 720P resolution which near 1024x768 resolution on our platform. ro.hwui.text_small_cache_width ro.hwui.text_small_cache_height ro.hwui.text_large_cache_width ro.hwui.text_large_cache_height These variables depends on screen resolution, density(similar to ppi) and language used. On a larger resolution screen, there might be more characters painted on it. Better to have larger font cache size. On a larger density config, it tends to use larger fonts. If the language has more different characters (symbols), it may need larger texture size to cache the fonts. For example, English may only have 52 characters, but Chinese have more than 10K and each will occupy more memory cache than English character. If cache size is too small, performance may drop because the font renderer will flush existed cache and upload new ones. If cache size is too large, it just wastes memory. It's OK to flush existed cache sometimes. But it's better to have only one (or no) flush for rendering a single screen. The default value is optimum on out platform with 1024x768 display resolution. BTW, texture size limitation on current Vivante GPU are 8192 x 8192.
記事全体を表示
This is a HW design checklist for customer's reference. Please read and fill it in carefully before requesting a schematic review.
記事全体を表示
TFTP     TFTP service will be used to transfer the kernel image from host to target every time the system reboots. Select the Linux distribution: All Boards TFTP Fedora All Boards TFTP on OpenSuse All Boards TFTP on Ubuntu
記事全体を表示
This document describes the i.MX 8MM EVK mini-SAS connectors features on Linux and Android use cases, covering the supported daughter cards, the process to change Device Tree (DTS) files or Boot images, and enable these different display options on the board.
記事全体を表示
The i.MX21ADS board needs a flash programmer software called iMX21ADS_TOOLKIT or just HAB. This programmer evolved to current ATK. You can download iMX21ADS_TOOLKIT here.  
記事全体を表示
In order to create this Ogg Theora encoder example you need to add libogg, libvorbis and libtheora to your system. Download these libs from http://www.theora.org/downloads/ : libogg-1.1.3, libvorbis-1.2.0 and libtheora-1.0.tar.bz2 Copy them to /opt/ltib/pkgs Create the directories ltib/dist/lfs-5.1/libogg, ltib/dist/lfs-5.1/libvorbis, ltib/dist-5.1/lfs/libtheora. Copy these spec files to its respective directories: File:Libogg.gz File:Libvorbis.gz File:Libtheora.gz Execute this sequence to compile and install these libs: $ ./ltib -p libogg.spec -m prep $ ./ltib -p libogg.spec -m scbuild $ ./ltib -p libogg.spec -m scdeploy $ ./ltib -p libvorbis.spec -m prep $ ./ltib -p libvorbis.spec -m scbuild $ ./ltib -p libvorbis.spec -m scdeploy $ ./ltib -p libtheora.spec -m prep $ ./ltib -p libtheora.spec -m scbuild $ ./ltib -p libtheora.spec -m scdeploy Now download and compile yuv2theora.c encoder example: File:Yuv2theora.gz $ ./ltib -m shell LTIB> gcc yuv2theora.c -o yuv2theora `pkg-config --libs --cflags theora` In this example we used a video sample (YUV420) on CIF format: http://140.116.72.80/~jhlin5/ns2/yuv_to_avi/paris_cif.yuv Update: All these libraries were added on LTIB Savannah CVS, then you just need to use them and compile the above code.
記事全体を表示
Script which patches the ltib folder on Ubuntu 12.04. Steps: $ cp patch-ltib-ubuntu12.04.sh <your ltib folder> $ cd <your ltib folder> $ chmod +x patch-ltib-ubuntu12.04.sh $ ./patch-ltib-ubuntu12.04.sh
記事全体を表示
ERR005723           PCIe: PCIe does not support L2 Power Down   Description: When PCIe works as Root Complex, it can exit L2 mode only through reset. Since PCIe doesn't have a dedicated reset control bit, it cannot exit L2 mode.   Projected Impact: PCIe does not support L2 Power Down   Workarounds: The PCIe can be put in PDDQ mode to save on PCIe PHY power and wakeup only by the OOB (Out of Band) wakeup signal (since wakeup by a beacon from link partner is not supported) driven from the link partner (End Point). This signal could be used as a GPIO interrupt to exit this mode. The limitation of this workaround is that the link partner cannot be put into L2.   Proposed Solution:                 No fix scheduled   Linux BSP Status:                 No software workaround available   SW workaround used to fix ERR005723 in Linux BSP Why the original workarounds can’t be implemented in Linux BSP * PCIe controller doesn’t have the reset mechanism that can be used when re-insmod the PCIe driver without power down/up PCIe module. * During the PCie driver rmmod/insmod operations, the PCIe CLKs would be turned off/on. IC can’t guarantee that the PCIe PHY can work well and re-establish the PCIe link properly. One SIMPLE SW workaround for this errata imx: pcie: toggle bit18 of grp1 fix pcie can't exit L2 issue.   Set bit18 of gpr1 before enter into supend, and clean it after resume, can fix the following errata. Errata ERR005723_PCIe PCIe does not support L2 Power Down. About the details, please refer to the attached patch. "0001-imx-pcie-toggle-bit18-of-grp1-fix-pcie-can-t-exit-L2.patch"   The conception of the other SW workaround (System warm-reset) The procedures of the original suspend/resume. Suspend User suspend command echo mem > /sys/power/state All driver call suspend function SRPG,  ARM save all state to memory Enter Stop mode and Power down ARM   Resume:   GPC receive IRQ Wake up system Power on ARM domain. ROM code running Jump to SRPG point Recovery ARM status from memory Call all devices resume function.   Because PCIe only reset by system reset, we need change above follow. Resume:   GPC receive IRQ Wake up system Power on ARM domain. ROM code running Jump to SRPG point Warm Reset system, memory context will be kept. But all peripheral status lost. ROM code running Jump to SRPG point again. Recovery ARM status from memory Call all devices resume function. Resume function call init to initialize it.  And recover to the status saved before.   Impact: Can’t support usb remote wake up, which required 4ms responsive Longer latency, warm reset need some ms.  The recovery of the device status needs some more ms.   Risk:   Current BSP have not tested above follow Device driver have not supported this follow yet. Need additional work to enable \debug\test it.     Modules enabled in this workaround now: * UART * ENET * PCIe   Tests procedure. HW: one i.MX6Q SD boards, and one INTEL pciex1 1000M CT network card.   SW(The images used by me are attached):   * Apply the attached patches(kernel and uboot) to the kernel/uboot source codes, re-build, get the images. Kernel is based on imx_3.0.35_4.0 release, uboot , is based on imx_v2009.08 # build out SD/MMC and USB driver to make DRAM hibernate work     # build pcie in.   *procedure of the suspend/resume tests;     # unload ep's driver --> suspend/resume --> reload ep's driver.   NOTE: Please make sure that the command line contains “no_console_suspend” The command used to enable the console input wake up after login the consol: echo enabled > /sys/devices/platform/imx-uart.0/tty/ttymxc0/power/wakeup   Log when the INTEL CT 1G network card is used: -------------------------------log--------------------------------------------   PM: Syncing filesystems ... done.                                             start suspend Freezing user space processes ... (elapsed 0.01 seconds) done. Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done. add wake up source irq 101 add wake up source irq 99 add wake up source irq 103 add wake up source irq 51 add wake up source irq 58 PM: suspend of devices complete after 15.482 msecs PM: late suspend of devices complete after 0.823 msecs Disabling non-boot CPUs ... CPU1: shutdown CPU2: shutdown CPU3: shutdown IMX PCIe imx_pcie_pltfm_suspend entering. IMX PCIe imx_pcie_pltfm_suspend exit.          suspended     U-Boot 2009.08-00679-g6ec6783 (May 20 2013 - 14:50:20)     resume   CPU: Freescale i.MX6 family TO1.2 at 792 MHz src 0x92eac8 resume 0x92eac8 jump to resume IMX PCIe imx_pcie_pltfm_resume entering. IMX PCIe imx_pcie_pltfm_resume pcie start re-link. IMX PCIe port imx_pcie_pltfm_resume: re-link up. Enabling non-boot CPUs ... CPU1: Booted secondary processor Calibrating delay loop (skipped) already calibrated this CPU i.MXC CPU frequency driver CPU1 is up CPU2: Booted secondary processor Calibrating delay loop (skipped) already calibrated this CPU i.MXC CPU frequency driver CPU2 is up CPU3: Booted secondary processor Calibrating delay loop (skipped) already calibrated this CPU i.MXC CPU frequency driver CPU3 is up PM: early resume of devices complete after 0.974 msecs remove wake up source irq 58 imx-ipuv3 imx-ipuv3.0: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7) imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7) remove wake up source irq 51 remove wake up source irq 103 remove wake up source irq 101 remove wake up source irq 99 PM: resume of devices complete after 54.174 msecs Restarting tasks ... done. PHY: 1:01 - Link is Up - 100/Full                            resume is ok, reload ep’s driver num is 61 e1000e: Intel(R) PRO/1000 Network Driver - 1.3.10-k2 e1000e: Copyright(c) 1999 - 2011 Intel Corporation. e1000e 0000:01:00.0: Disabling ASPM L0s e1000e 0000:01:00.0: (unregistered net_device): Failed to initialize MSI-X interrupts.  Falling back to MSI interrupts. e1000e 0000:01:00.0: (unregistered net_device): Failed to initialize MSI interrupts.  Falling back to legacy interrupts. e1000e 0000:01:00.0: eth1: (PCI Express:2.5GT/s:Width x1) 00:1b:21:3a:18:8b e1000e 0000:01:00.0: eth1: Intel(R) PRO/1000 Network Connection e1000e 0000:01:00.0: eth1: MAC: 3, PHY: 8, PBA No: E42641-005 e1000e: eth1 NIC Link is Up 1000 Mbps Full Duplex, Flow Control: Rx/Tx PING 192.168.0.1 (192.168.0.1): 56 data bytes 64 bytes from 192.168.0.1: seq=0 ttl=64 time=3.126 ms 64 bytes from 192.168.0.1: seq=1 ttl=64 time=0.244 ms 64 bytes from 192.168.0.1: seq=2 ttl=64 time=0.232 ms 64 bytes from 192.168.0.1: seq=3 ttl=64 time=0.206 ms 64 bytes from 192.168.0.1: seq=4 ttl=64 time=0.222 ms 64 bytes from 192.168.0.1: seq=5 ttl=64 time=0.207 ms 64 bytes from 192.168.0.1: seq=6 ttl=64 time=0.250 ms 64 bytes from 192.168.0.1: seq=7 ttl=64 time=0.209 ms 64 bytes from 192.168.0.1: seq=8 ttl=64 time=0.154 ms 64 bytes from 192.168.0.1: seq=9 ttl=64 time=0.211 ms   --- 192.168.0.1 ping statistics --- 10 packets transmitted, 10 packets received, 0% packet loss round-trip min/avg/max = 0.154/0.506/3.126 ms PM: Syncing filesystems ... done.                                   ep’s functions are ok, re-do the suspend/resume tests Freezing user space processes ... (elapsed 0.01 seconds) done. -------------------------------end-------------------------------------------- Original Attachment has been moved to: 0001-imx-pcie-toggle-bit18-of-grp1-fix-pcie-can-t-exit-L2.patch.zip Original Attachment has been moved to: uboot_patch_image.zip Original Attachment has been moved to: kernel_patch_image.zip
記事全体を表示
Overview The purpose of this document is to provide the patches to fix display mess issue in TextView based on MX6 Android R13.4-GA and R13.4.1 ICS release. Please note these patches are only validated basically for dedicated issues. If you find any side effect with these patches, please add the comments into this document. Issue Description Software: R13.4-GA or R13.4.1 Android releases Hardware: i.MX6Dual/Quad SabreSD board or i.MX6DualLite SabreSD board. Test steps: Install testviewtest.apk Run this APK and key in the text, you will see the text display mess after key in more texts. You can also get the issue descriptions from https://community.freescale.com/thread/303194 Patches You can get the patches from attached textview_fix.zip. For R13.4-GA, please apply the following patches: kernel_imx, unzip Kernel/r13.4-ga/kernel-patch-r13.4-ga-gpu4.6.9p10.tar.gz and apply the patches. device/fsl-proprietary/gpu-viv: unzip gpu_lib/gpu-viv-lib-4.6.9p10-font-libGAL-crash-fix.tar.gz and replace lib folder. For R13.4.1, please apply the following patches: kernel_imx, Apply the patch Kernel/r13.4.1/0001-upgrade-gpu-4.6.9p10-kernel-driver_r13.4.1.patc device/fsl-proprietary/gpu-viv: unzip gpu_lib/gpu-viv-lib-4.6.9p10-font-libGAL-crash-fix.tar.gz and replace lib folder.
記事全体を表示
This document is a simple guide on one of the ways in which 3D models can be loaded and displayed using OpenGL.   Requirements - Blender (open source) or a similar program that allows to export 3D models in the .obj format. We’ll be using Blender to export the .obj file with the essential information to draw the 3D model, without information on textures, for example. https://www.blender.org/   - i.MX6 Linux BSP image with X11 support – For this document we’ll use the L3.10.31 BSP, which is compiled using Yocto 1.6.You may use a newer BSP. We’ll use the fsl-image-gui. You may use a Qt5 image with X11 from newer BSPs. - GCC Toolchain -You may either cross compile on a Host or compile on the same board by providing the necessary libraries and toolchain. On the L3.10.31 you need to manually add GCC to your baked image. In newer releases this may not necessary. For adding the GCC package to a Yocto image and compiling within the board itself please add the following line to the conf/local.conf file inside your build directory. IMAGE_INSTALL_append += " gcc libgcc" If you wish to cross compile from your host and then run on your board you first will need to extract the toolchain from the BSP, which can be done by following the instructions of the next document: https://community.nxp.com/docs/DOC-95122  - FreeGLUT – FreeGLUT is an open source alternative to the OpenGL Utility Toolkit (GLUT), a window system independent toolkit for writing OpenGL programs. It implements a simple windowing application programming interface (API) for OpenGL. This is not necessary for drawing the model on the window but foes allow for functions such as rotating it. You may install it on your host with the following command: $ sudo apt-get install freeglut3-dev For additional information and downloads of FreeGLUT please refer to the projects website: http://freeglut.sourceforge.net/   - i.MX6D/Q/DL/S/SX GPU Demo Framework SDK – We’ll use the GPU Test examples which are available at the following link. Source code for this document implementation is attached but for more examples of OpenGL ES please refer to this SDK. (Please note that you may need to login in order to download this file) https://www.nxp.com/webapp/Download?colCode=FSL_GPU_SDK_2.3&appType=license&location=null&fpsp=1&WT_TYPE=Software%20Development%20Kits&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=zip&WT_ASSET=Downloads&fileExt=.zip&Parent_nodeId=1337637154535695831062&Parent_pageType=product   - i.MX6Q Board – For this example we will be using the i.MX6Q SABRE Board, but you may run OpenGL ES on any i.MX6Q board provided that you provide the necessary packages to support OpenGL ES.   Brief introduction to OpenGL ES? OpenGL is a software interface to hardware accelerated graphics. The API of this interface consists of about 150 distinct commands that allow you to specify objects and perform operations on them in order to produce interactive three-dimensional applications. OpenGL ES is the OpenGL implementation for Embedded Systems. Somei.MX6 Processors like the i.MX6Q possess a Vivante GPU module that runs on OpenGL ES. When using OpenGL or OpenGL ES all 3D objects are descripted as a series of triangles. This is important to mention as it will make the instructions we will need for describing our model make more sense.   Step 1 - Exporting a model as .obj You may import a 3D model from other sources or make your own simple 3D model in blender. For this example we’ll make a simple 3D NXP logo and export it. Once you have your model ready, select the object in objet mode with a right click. Once selected select File > Export > Wavefront (.obj) You may now select where and with what name to export the object file. On the left panel you will have the export options. It’s important to leave all options unchecked except for: Write Normals Include UVs Triangulate Faces (You may change the scale of your model and it won’t negatively affect the process)     The .obj model may be opened with a text editor and we’ll see that it basically describes the object as a series of parameters that may include vertex data, free-form curve/surface attributes, elements, free-form curve/surface body statements, connectivity between free-form surfaces, grouping and display/render attribute information. For our example we’ll be using a simple file that just contains: - List of geometric vertices, with (x,y,z) coordinates v 0.292475 0.017345 -0.152653 - List of vertex normals in (x,y,z) form vn 0.0000 1.0000 -0.0000 - Polygonal face element f 3//1 113//1 4//1   Step 2- Converting .obj to OpenGL compatible information We’ll be using the following program that allows to convert from .obj format to a format compatible with OpenGL as the conversion from one format to the other is not part of the scope of this document. https://fr.jeffprod.com/obj-to-opengl.php This program does more than just changing the format on the file and do perform some operations to translate the parameters of the .obj file to the following OpenGL ES information: static GLfloat v_triangles[] static GLfloat vt_triangles[] static GLfloat vn_triangles[] We’ll be using these variables and also the number of triangles which for this example is 1440. This can be found at the end of the file on the following line which effectively draws the complete triangle array: glDrawArrays(GL_TRIANGLES, 0, 1440);   Step 3 – Loading the model arrays to the .C program. You will need to copy the three GLfloat arrays to your OpenGL ES .C code. (You may alternatively use an include to have it more neatly organized but this is outside the scope of this document) In our example we’ll copy them inside void render (). Inside this function we’ll find the Draw Array instruction in which we must specify the number of triangles in our array. You may just replace your model information AND also change the number of triangles, otherwise you will receive an error when running the program.   glDrawArrays(GL_TRIANGLES,0,1440); We are using a simple rotation using glRotate and incrementing the value of rotation with each flush of the screen.     glRotatef(rlogo, 2.0f, 1.0f, 1.0f); The variable rlogo gets increased each time the screen is drawn. Depending on your model you may need to change the view in order to be able to see your model. This example uses a very small model so we have a viewpoint just 1.25 units away from the screen (Z axis). Depending on your model you may need to be further away in order to see the model on the screen. glTranslatef(0.0f, 0.0f, -1.25f);    Step 4- Compiling the OpenGL example For this simple example we will be using the examples from the GPU  as base an add the information of the model we have just exported. We’ll use the two attached files for this: Makefile.x11 – A make file with the dependencies and attributes necessary to compile our C file. NXPlogo.c – C file with the information of the model and instructions on to draw it on the screen. You can compile using the following commands to first clean in case you built before and then compiling the code. make –f Makefile.x11 clean make Makefile.x11 Once the program has compiled you can run it from the command prompt by using: export DISPLAY=:0.0 ./NXPlogo The result will be as follows, where the 3D model is rotating,     Additional Resources 2D and 3D Graphics in NXP Devices http://www.nxp.com/files/training/doc/dwf/DWF13_AMF_CON_T1025.pdf   i.MX6D/Q/DL/S/SX GPU Demo Framework SDK – Which provides the source code for the demo in which this example was built upon and also contains good documentation for those interested in OpenGL ES. https://www.nxp.com/webapp/Download?colCode=FSL_GPU_SDK_2.3&appType=license&location=null&fpsp=1&WT_TYPE=Software%20Development%20Kits&WT_VENDOR=FREESCALE&WT_FILE_FORMAT=zip&WT_ASSET=Downloads&fileExt=.zip&Parent_nodeId=1337637154535695831062&Parent_pageType=product    OpenGL Redbook – Which is the most comprehensive book documenting and explaining the OpenGL API. http://www.opengl-redbook.com/
記事全体を表示
[中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-341473 
記事全体を表示
Overview i.MX28EVK Setup Build Yocto Project image Create a SDCARD from the Linux Host Boot i.MX28EVK Create file system on USB Create Mount Point and Mount the USB device Create 250 MB File Create Exports File Restart NFS Server Ubuntu Linux Host Setup Create Mount Directory Mount i.MX28EVK Exported Directory Access the NFS mounted directory Overview This document describes the steps for configuring a NFS Server running on an i.MX Application Processor - in this case the evaluation board i.MX28 EVK. Once the NFS server is running, an Ubuntu 12.04 Linux host is then configured to NFS mount the i.MX28EVK exported directory. The Ethernet interface is used for the connection transport. A block diagram of the connection setup is shown below: An Ethernet switch provided the Ethernet connection between the Linux Host and the i.MX28EVK. A thumb drive was connected to the USB port on the i.MX28EVK which was used for the exported directory. i.MX28EVK Setup Build Yocto Project image Use core-image-minimal and add packages to conf/local.conf to support NFS MACHINE=imx28evk source setup-environment mx28-evk echo "CORE_IMAGE_EXTRA_INSTALL += \"bash kernel-modules nfs-utils\" " >> conf/local.conf bitbake core-image-minimal When bitbake finishes the images are found in tmp/deploy/images/imx28evk Create a SDCARD from the Linux Host sudo dd if=/tmp/deploy/images/imx28evk/core-image-minimal-imx28evk.sdcard of=/dev/sdc bs=4M && sync Boot i.MX28EVK Insert the SDCARD into slot 0 on the bottom side of the i.MX28EVK and connect the serial console. Power-on and push the POWER button on the lower conner to turn on. The Login credentials are User Name: root      There is no password configured by default. Create file system on USB The USB drive had one partition which was formatted with vfat file system: mkfs.vfat /dev/sdb1 Create Mount Point and Mount the USB device mkdir /mnt/usb mount /dev/sdb1 /mnt/usb Create 250 MB File dd if=/dev/zero of=/mnt/usb/file1.txt bs=512K count=500 Create Exports File echo "/mnt/usb *(rw,sync,no_root_squash,no_subtree_check)" > /etc/exports Restart NFS Server /etc/init.d/nfsserver stop /etc/init.d/nfsserver start Ubuntu Linux Host Setup Create Mount Directory sudo mkdir /mnt/remote Mount i.MX28EVK Exported Directory sudo mount -t nfs 10.85.1.10:/mnt/usb /mnt/remote Access the NFS mounted directory ls /mnt/remote
記事全体を表示