i.MXプロセッサ ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Processors Knowledge Base

ディスカッション

ソート順:
As part of the patches attached with this blog, we will relay the pcie write transaction from Endpoint-A to Endpoint-B connected to iMX95FRDM PRO.   1.png Linux-imx used - lf-6.18.2-1.0.0 Attached are the following files:-   imx95-19x19-frdm-pro-pcie0-ep-dtbs - EP A shall use the dtb built with this dtbs imx95-19x19-frdm-pro-pcie1-ep-dtbs - EP B shall use the dtb built with this dtbs rc_pcie_dma_relay.c - driver used on RC to relay pcie write from EP-A to EP-B conf_pcie0.sh - script to be executed on Endpoints A and B to configure the EPF driver //To build the dtb and relay kernel driver 1. git clone  git clone https://github.com/nxp-imx/linux-imx.git git checkout origin/lf-6.18.y 2. Copy the dtbs to arch/arm64/boot/dts/freescale/ Copy rc_pcie_dma_relay.c to drivers/pci/   3. Make the following changes as per this diff   diff --git a/arch/arm64/boot/dts/freescale/Makefile b/arch/arm64/boot/dts/freescale/Makefile index aa3cfdf1aafc..56e3db653208 100644 --- a/arch/arm64/boot/dts/freescale/Makefile +++ b/arch/arm64/boot/dts/freescale/Makefile @@@ -1205,6 +1205,16 @@ dtb-$(CONFIG_ARCH_MXC) += imx95-15x15-frdm-8mic-reve.dt    dtb-$(CONFIG_ARCH_MXC) += imx95-19x19-frdm-pro.dtb imx95-19x19-frdm-pro-aud-hat.dtb   + +dtb-$(CONFIG_ARCH_MXC) += imx95-19x19-frdm-pro-pcie0-ep.dtb +dtb-$(CONFIG_ARCH_MXC) += imx95-19x19-frdm-pro-pcie1-ep.dtb + +imx95-19x19-frdm-pro-pcie0-ep-dtbs := imx95-19x19-frdm-pro.dtb \ +                      imx95-19x19-frdm-pro-pcie0-ep.dtbo + +imx95-19x19-frdm-pro-pcie1-ep-dtbs := imx95-19x19-frdm-pro.dtb \ +                      imx95-19x19-frdm-pro-pcie1-ep.dtbo +  imx95-19x19-frdm-pro-os08a20-isp-dtbs := imx95-19x19-frdm-pro.dtb \                                          imx95-19x19-frdm-pro-os08a20.dtbo  dtb-$(CONFIG_ARCH_MXC) += imx95-19x19-frdm-pro-os08a20-isp.dtb     4. Add the following to drivers/pci/Makefile +obj-m      += rc_pcie_dma_relay.o   5. Trigger the kernel build. You will obtain rc_pcie_dma_relay.ko, imx95-19x19-frdm-pro-pcie0-ep.dtb and imx95-19x19-frdm-pro-pcie1-ep.dtb. 6. We are only using pcie0 M.2 Key M slots of Endpoint A and Endpoint B so you only need to upload this dtb to both the endpoint boards - imx95-19x19-frdm-pro-pcie0-ep.dtb and boot linux with it after passing 'iommu.passthrough=1' at uboot mmcargs. This is to disable smmu for our tests. RC will boot with the default dtb - imx95-19x19-frdm-pro.dtb 7. Connect the Endpoint-A to RC's K1 via M.2 Key M to Key M cable. Similarly connect the other Endpoint-B to other RC's K2 M.2 slot via Key M to Key M cable. 8. Execute this script on both the endpoints - ./conf_pcie0.sh 2.png 9. Then reboot the RC iMX95 FRDM Pro and ensure that you see both the endpoints:-   3.png 0000:01:00.0 and 0001:01:00.0 are the enumerated endpoints. 4.png 5.png 10. Upload rc_pcie_dma_relay.ko to the RC board and insert it like this:-  insmod rc_pcie_dma_relay.ko src_phys=0x910100000 dst_phys=0xa10100000 relay_len=0x100000 chunk_len=0x10000 you will observe similar logs on dmesg:-   [ 4949.082087] rc_pcie_dma_relay: init src=0x910100000 dst=0xa10100000 len=1048576 chunk=65536 [ 4949.082150] rc_pcie_dma_relay src_before: [0]=0xdeadbeef [1]=0xdeadbeef [2]=0xdeadbeef [3]=0xdeadbeef [ 4949.082171] rc_pcie_dma_relay dst_before: [0]=0x00000000 [1]=0x00000000 [2]=0x00000000 [3]=0x00000000 [ 4949.125779] rc_pcie_dma_relay dst_zeroed: [0]=0x00000000 [1]=0x00000000 [2]=0x00000000 [3]=0x00000000 [ 4949.141380] rc_pcie_dma_relay src_after: [0]=0xdeadbeef [1]=0xdeadbeef [2]=0xdeadbeef [3]=0xdeadbeef [ 4949.141427] rc_pcie_dma_relay dst_after: [0]=0xdeadbeef [1]=0xdeadbeef [2]=0xdeadbeef [3]=0xdeadbeef [ 4954.272981] rc_pcie_dma_relay: verify OK for 1048576 bytes [ 4954.273000] rc_pcie_dma_relay: DMA relay verify PASSED   11. Finally, via devmem5 on RC, you can verify the data of EP-A transferred to EP-B  ./devmem5 r 0xa10100000 w  
記事全体を表示
Background: This article discusses the reboot mechanism on the i.MX8MP and i.MX93 platforms. It aims to help customers understand how the reboot command works. We will discuss two different kernel versions separately.   1. Linux version : LF_6.12.34_2.1.0 The executable file for the reboot command is as follows: When the ”reboot“ command is executed, the system enters the ”do_kernel_restart()“ function and executes the reboot mechanism by determining the priority of the registered functions. Since the ”reboot.c“ file does not print out the registered functions, a print function is added to the file to identify the function that is ultimately executed.   The print output is as follows: pengyong_zhang_0-1779943510533.png As shown in the figure above, in version 5.12, the reboot is performed via a reset executed by psci. Continuing to trace the ”psci_sys_reset()“ function, we can see that the system sends the function ID via the PSCI interface to initiate an SMC call, instructing the underlying firmware (ATF/EL3) to perform a system reboot (typically a cold reset). The value of PSCI_0_2_FN_SYSTEM_RESET is 0x80000009 pengyong_zhang_0-1779943988849.png   According to the Arm Power State Coordination Interface Platform Design Document, this ID represents a cold reset of the system. pengyong_zhang_1-1779944324615.png pengyong_zhang_2-1779944331293.png     2. Linux version : LF_6.18.2_1.0.0 Use the same debugging method to examine the reboot mechanism in version 6.18 As shown in the output below, in version 6.18, the system reset is triggered by the `sys_off_notify()` function. The final execution function is pca9450_i2c_restart_handler()   pengyong_zhang_0-1779944594004.png By examining the `pca9450_i2c_restart_handler()` function, we can see that the system writes a `SW_RST_COMMAND` value to the PMIC via I²C, where `SW_RST_COMMAND = 0x14`. pengyong_zhang_1-1779944599443.png According to the PMIC data sheet, 10b = Cold Reset; all voltage regulators are reset except LDO1/LDO2 pengyong_zhang_2-1779944606796.png   Summary: Regardless of the kernel version, the `reboot` command triggers a system cold reset. The triggering mechanism has been updated in versions 6.18 and later.
記事全体を表示
As part of this brief blog, we are enabling Asymmetric Multiprocessing (AMP) boot support for the Cortex-M7 core on the i.MX8MP SoC device model in Qemu. The M7 firmware can be loaded and started from Linux running on the Cortex-A53 cores via the remoteproc framework.
記事全体を表示
Customer requirement: Use NOR boot as a backup — boot from NOR, then mount kernel, DTB, and rootfs from NAND. Zhiming_Liu_0-1778118523038.png Test module: https://www.nxp.com/design/design-center/development-boards-and-designs/m2-nand-flash-daughter-card:M2-NAND-FLASH Zhiming_Liu_1-1778118550873.png   Test under L6.12.49 Uboot.   1. Why Does U-Boot Source Need Modification on i.MX95? i.MX93's boot ROM initializes the SD3_XXX and SD1_XXX PADs. On the i.MX93 EVK design, SD3_XXX is routed to the M.2 connector, and SD1_XXX is connected to eMMC. Zhiming_Liu_2-1778118572501.png   For i.MX95, the boot ROM only initializes the XSPI1_XXX PADs. The FlexSPI signals can be muxed out from SD3_XXX, but the boot ROM cannot boot from SD3_XXX. Zhiming_Liu_3-1778118590114.png   Due to these differences, the uboot.bin flashed into NOR must have the ability to read NAND. However, the default BSP always reads from NOR, so U-Boot must be modified to activate the M.2 NAND module. 2. Flashing NAND To flash NAND, a custom UUU script must be used. Using the built-in UUU spinand flashing script is not recommended — the built-in script assumes NAND is accessible in U-Boot, but the default imx-boot uses NOR. 2.1 UUU Script uuu_version 1.2.39 # Please replace below item with actual name # @_flash_fw.bin | boot loader firmware, for i.MX8QM/QX, it's different from _flash.bin, for all other platforms, it's same as _flash.bin # @_flash.bin | boot loader file burn to NAND # @_Image | linux kernel image, zImage for arm32, Image for arm64 # @_board.dtb | board dtb file # @_initramfs.cpio.zst.uboot | initramfs # @_tee | optee image # @_rootfs.tar.zst | rootfs # This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ SDP: boot -f .\imx-boot-imx95-19x19-lpddr5-evk-fspi.bin-flash_a55_flexspi # This command will be run when ROM support stream mode # i.MX8QXP, i.MX8QM, skip QSPI header SDPS: boot -f .\imx-boot-imx95-19x19-lpddr5-evk-fspi.bin-flash_a55_flexspi -skipfhdr # These commands will be run when use SPL and will be skipped if no spl # SDPU will be deprecated. please use SDPV instead of SDPU # { SDPU: delay 1000 SDPU: write -f .\imx-boot-imx95-19x19-lpddr5-evk-fspi.bin-flash_a55_flexspi -offset 0x10000 -skipfhdr SDPU: jump # } # These commands will be run when use SPL and will be skipped if no spl # if (SPL support SDPV) # { SDPV: delay 1000 SDPV: write -f .\imx-boot-imx95-19x19-lpddr5-evk-fspi.bin-flash_a55_flexspi -skipspl -skipfhdr SDPV: jump # } FB: ucmd setenv fastboot_buffer ${loadaddr} FB: download -f Image.bin FB: ucmd setenv fastboot_buffer ${fdt_addr} FB: download -f imx95-19x19-evk.dtb FB: ucmd setenv fastboot_buffer ${initrd_addr} FB: download -f fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.zst.u-boot FB: ucmd setenv bootargs ${bootargs} ${mtdparts} FB: ucmd setenv fdtfile imx95-19x19-evk.dtb #FB: ucmd setenv bootargs console=ttymxc3,115200 ${mtdparts} FB: acmd ${kboot} ${loadaddr} ${initrd_addr} ${fdt_addr} FBK: ucmd cat /proc/mtd FBK: ucmd rm -f /tmp/mtd.sh FBK: ucmd cat /proc/mtd | while read dev size erase name; do mtd=`echo $dev | sed 's/mtd//;s/://'`; name=`echo $name | tr -d '"'`; echo export $name=$mtd >> /tmp/mtd.sh; done # mapping name FBK: ucmd . /tmp/mtd.sh; [ -n "${bootloader}" ] && echo export nandboot=${bootloader} >> /tmp/mtd.sh FBK: ucmd . /tmp/mtd.sh; [ -n "${kernel}" ] && echo export nandkernel=${kernel} >> /tmp/mtd.sh FBK: ucmd . /tmp/mtd.sh; [ -n "${dtb}" ] && echo export nanddtb=${dtb} >> /tmp/mtd.sh FBK: ucmd . /tmp/mtd.sh; [ -n "${rootfs}" ] && echo export nandrootfs=${rootfs} >> /tmp/mtd.sh FBK: ucmd chmod 755 /tmp/mtd.sh FBK: ucmd cat /tmp/mtd.sh FBK: ucmd mount -t debugfs debugfs /sys/kernel/debug || true # write boot loader — this partition was set to read-only in DTS during testing, skip erase for now # FBK: ucmd . /tmp/mtd.sh; flash_erase /dev/mtd${nandboot} 0 0 # FBK: ucp imx-boot-imx95-19x19-lpddr5-evk-fspi.bin-flash_a55_flexspi t:/tmp/boot # FBK: ucmd . /tmp/mtd.sh; cd /tmp; soc=`cat /sys/devices/soc0/soc_id 2>/dev/null`; pad=""; case "$soc" in MX8Q*|MX8DXL*|MX8MN*|MX8MP*) ;; *) pad="-x" ;; esac; kobs-ng init $pad -v --chip_0_device_path=/dev/mtd${nandboot} /tmp/boot # burn kernel FBK: ucmd . /tmp/mtd.sh; flash_erase /dev/mtd${nandkernel} 0 0 FBK: acmd . /tmp/mtd.sh; nandwrite -p /dev/mtd${nandkernel} - FBK: ucp Image.bin t:- FBK: sync # burn dtb FBK: ucmd . /tmp/mtd.sh; flash_erase /dev/mtd${nanddtb} 0 0 FBK: ucp imx95-19x19-evk.dtb t:/tmp/dtb FBK: ucmd . /tmp/mtd.sh; nandwrite -p /dev/mtd${nanddtb} /tmp/dtb # burn uTee # FBK: ucmd . /tmp/mtd.sh; flash_erase /dev/mtd${nandtee} 0 0 # FBK: ucp _tee t:/tmp/tee # FBK: ucmd . /tmp/mtd.sh; nandwrite -p /dev/mtd${nandtee} /tmp/tee # burn rootfs FBK: ucmd . /tmp/mtd.sh; flash_erase /dev/mtd${nandrootfs} 0 0 FBK: ucmd ubidetach /dev/ubi_ctrl -m ${nandrootfs} || true FBK: ucmd . /tmp/mtd.sh; ubiattach /dev/ubi_ctrl -m ${nandrootfs} FBK: ucmd ubimkvol /dev/ubi0 -N nandrootfs -m FBK: ucmd mkdir -p /mnt/mtd FBK: ucmd mount -t ubifs ubi0:nandrootfs /mnt/mtd FBK: acmd export EXTRACT_UNSAFE_SYMLINKS=1; tar --zstd --warning=no-timestamp -x -C /mnt/mtd FBK: ucp core-image-base-imx95-19x19-lpddr5-evk.rootfs-20260429064745.tar.zst t:- FBK: sync FBK: ucmd umount /mnt/mtd FBK: done 2.2 Linux Patch diff --git a/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts b/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts index d21335d8af84..0db2cefbab01 100644 --- a/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts +++ b/arch/arm64/boot/dts/freescale/imx95-19x19-evk.dts @@ -388,17 +388,47 @@ &flexspi1 { pinctrl-0 = <&pinctrl_flexspi1>; status = "okay"; - mt35xu01gbba: flash@0 { - compatible = "jedec,spi-nor"; - reg = <0>; - pinctrl-names = "default"; - pinctrl-0 = <&pinctrl_flexspi1_reset>; - reset-gpios = <&gpio5 11 GPIO_ACTIVE_LOW>; + W25N02KWZEIR: flash@0 { + compatible = "spi-nand"; #address-cells = <1>; #size-cells = <1>; - spi-max-frequency = <200000000>; - spi-tx-bus-width = <8>; - spi-rx-bus-width = <8>; + reg = <0>; + spi-max-frequency = <104000000>; + spi-tx-bus-width = <4>; + spi-rx-bus-width = <4>; + + partitions { + compatible = "fixed-partitions"; + #address-cells = <1>; + #size-cells = <1>; + + partition@0 { + label = "bootloader"; + reg = <0x000000 0x800000>; // 8MB + // read-only;//if you hope imx-boot read only + }; + + partition@1 { + label = "config"; + reg = <0x800000 0x800000>; //8MB + }; + + partition@2 { + label = "kernel"; + reg = <0x1000000 0x2800000>; //40MB + }; + + partition@3 { + label = "dtb"; + reg = <0x3800000 0x20000>; //128K + }; + + partition@4 { + label = "rootfs"; + reg = <0x3820000 0xFFFFFFFF>; + linux,rootfs; + }; + }; }; }; @@ -887,17 +917,12 @@ IMX95_PAD_GPIO_IO27__CAN2_RX 0x39e pinctrl_flexspi1: flexspi1grp { fsl,pins = < - IMX95_PAD_XSPI1_SS0_B__FLEXSPI1_A_SS0_B 0x3fe - IMX95_PAD_XSPI1_SCLK__FLEXSPI1_A_SCLK 0x3fe - IMX95_PAD_XSPI1_DQS__FLEXSPI1_A_DQS 0x3fe - IMX95_PAD_XSPI1_DATA0__FLEXSPI1_A_DATA_BIT0 0x3fe - IMX95_PAD_XSPI1_DATA1__FLEXSPI1_A_DATA_BIT1 0x3fe - IMX95_PAD_XSPI1_DATA2__FLEXSPI1_A_DATA_BIT2 0x3fe - IMX95_PAD_XSPI1_DATA3__FLEXSPI1_A_DATA_BIT3 0x3fe - IMX95_PAD_XSPI1_DATA4__FLEXSPI1_A_DATA_BIT4 0x3fe - IMX95_PAD_XSPI1_DATA5__FLEXSPI1_A_DATA_BIT5 0x3fe - IMX95_PAD_XSPI1_DATA6__FLEXSPI1_A_DATA_BIT6 0x3fe - IMX95_PAD_XSPI1_DATA7__FLEXSPI1_A_DATA_BIT7 0x3fe + IMX95_PAD_SD3_CMD__FLEXSPI1_A_SS0_B 0x3fe + IMX95_PAD_SD3_CLK__FLEXSPI1_A_SCLK 0x3fe + IMX95_PAD_SD3_DATA0__FLEXSPI1_A_DATA_BIT0 0x3fe + IMX95_PAD_SD3_DATA1__FLEXSPI1_A_DATA_BIT1 0x3fe + IMX95_PAD_SD3_DATA2__FLEXSPI1_A_DATA_BIT2 0x3fe + IMX95_PAD_SD3_DATA3__FLEXSPI1_A_DATA_BIT3 0x3fe >; }; 2.3 Flashing Log 2:31-182BA9E87D9840BA>Start Cmd:SDPS: boot -f .\imx-boot-imx95-19x19-lpddr5-evk-fspi.bin-flash_a55_flexspi -skipfhdr 100%2:31-182BA9E87D9840BA>Okay (5.364s) New USB Device Attached at 2:31-182BA9E87D9840BA 2:31-182BA9E87D9840BA>Start Cmd:SDPV: delay 1000 2:31-182BA9E87D9840BA>Okay (1.009s) 2:31-182BA9E87D9840BA>Start Cmd:SDPV: write -f .\imx-boot-imx95-19x19-lpddr5-evk-fspi.bin-flash_a55_flexspi -skipspl -skipfhdr 100%2:31-182BA9E87D9840BA>Okay (3.165s) 2:31-182BA9E87D9840BA>Start Cmd:SDPV: jump 100%2:31-182BA9E87D9840BA>Okay (0.017s) New USB Device Attached at 2:31-182BA9E87D9840BA 2:31-182BA9E87D9840BA>Start Cmd:FB: ucmd setenv fastboot_buffer ${loadaddr} 2:31-182BA9E87D9840BA>Okay (0.014s) 2:31-182BA9E87D9840BA>Start Cmd:FB: download -f Image.bin 2:31-182BA9E87D9840BA>Okay (1.715s) 2:31-182BA9E87D9840BA>Start Cmd:FB: ucmd setenv fastboot_buffer ${fdt_addr} 2:31-182BA9E87D9840BA>Okay (0.011s) 2:31-182BA9E87D9840BA>Start Cmd:FB: download -f imx95-19x19-evk.dtb 2:31-182BA9E87D9840BA>Okay (0.026s) 2:31-182BA9E87D9840BA>Start Cmd:FB: ucmd setenv fastboot_buffer ${initrd_addr} 2:31-182BA9E87D9840BA>Okay (0.011s) 2:31-182BA9E87D9840BA>Start Cmd:FB: download -f fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.zst.u-boot 2:31-182BA9E87D9840BA>Okay (0.702s) 2:31-182BA9E87D9840BA>Start Cmd:FB: ucmd setenv bootargs ${bootargs} ${mtdparts} 2:31-182BA9E87D9840BA>Okay (0.011s) 2:31-182BA9E87D9840BA>Start Cmd:FB: ucmd setenv fdtfile imx95-19x19-evk.dtb 2:31-182BA9E87D9840BA>Okay (0.011s) 2:31-182BA9E87D9840BA>Start Cmd:FB: acmd ${kboot} ${loadaddr} ${initrd_addr} ${fdt_addr} 2:31-182BA9E87D9840BA>Okay (0.007s) New USB Device Attached at 2:31-0000000000000000 2:31-0000000000000000>Start Cmd:FBK: ucmd cat /proc/mtd dev: size erasesize name mtd0: 00800000 00020000 "bootloader" mtd1: 00800000 00020000 "config" mtd2: 02800000 00020000 "kernel" mtd3: 00020000 00020000 "dtb" mtd4: 0c7e0000 00020000 "rootfs" 2:31-0000000000000000>Okay (0.015s) 2:31-0000000000000000>Start Cmd:FBK: ucmd rm -f /tmp/mtd.sh 2:31-0000000000000000>Okay (0.007s) 2:31-0000000000000000>Start Cmd:FBK: ucmd cat /proc/mtd | while read dev size erase name; do mtd=`echo $dev | sed 's/mtd//;s/://'`; name=`echo $name | tr -d '"'`; echo export $name=$mtd >> /tmp/mtd.sh; done 2:31-0000000000000000>Okay (0.077s) 2:31-0000000000000000>Start Cmd:FBK: ucmd . /tmp/mtd.sh; [ -n "${bootloader}" ] && echo export nandboot=${bootloader} >> /tmp/mtd.sh 2:31-0000000000000000>Okay (0.006s) 2:31-0000000000000000>Start Cmd:FBK: ucmd . /tmp/mtd.sh; [ -n "${kernel}" ] && echo export nandkernel=${kernel} >> /tmp/mtd.sh 2:31-0000000000000000>Okay (0.008s) 2:31-0000000000000000>Start Cmd:FBK: ucmd . /tmp/mtd.sh; [ -n "${dtb}" ] && echo export nanddtb=${dtb} >> /tmp/mtd.sh 2:31-0000000000000000>Okay (0.006s) 2:31-0000000000000000>Start Cmd:FBK: ucmd . /tmp/mtd.sh; [ -n "${rootfs}" ] && echo export nandrootfs=${rootfs} >> /tmp/mtd.sh 2:31-0000000000000000>Okay (0.008s) 2:31-0000000000000000>Start Cmd:FBK: ucmd chmod 755 /tmp/mtd.sh 2:31-0000000000000000>Okay (0.007s) 2:31-0000000000000000>Start Cmd:FBK: ucmd cat /tmp/mtd.sh export name=dev export bootloader=0 export config=1 export kernel=2 export dtb=3 export rootfs=4 export nandboot=0 export nandkernel=2 export nanddtb=3 export nandrootfs=4 2:31-0000000000000000>Okay (0.007s) 2:31-0000000000000000>Start Cmd:FBK: ucmd mount -t debugfs debugfs /sys/kernel/debug || true 2:31-0000000000000000>Okay (0.01s) 2:31-0000000000000000>Start Cmd:FBK: ucmd . /tmp/mtd.sh; flash_erase /dev/mtd${nandkernel} 0 0 Erasing 40960 Kibyte @ 0 -- 100 % complete 2:31-0000000000000000>Okay (0.856s) 2:31-0000000000000000>Start Cmd:FBK: acmd . /tmp/mtd.sh; nandwrite -p /dev/mtd${nandkernel} - 2:31-0000000000000000>Okay (0.051s) 2:31-0000000000000000>Start Cmd:FBK: ucp Image.bin t:- 33%Writing data to block 0 at offset 0x0 Writing data to block 1 at offset 0x20000 Writing data to block 2 at offset 0x40000 Writing data to block 3 at offset 0x60000 Writing data to block 4 at offset 0x80000 Writing data to block 5 at offset 0xa0000 Writing data to block 6 at offset 0xc0000 Writing data to block 7 at offset 0xe0000 Writing data to block 8 at offset 0x100000 Writing data to block 9 at offset 0x120000 Writing data to block 10 at offset 0x140000 Writing data to block 11 at offset 0x160000 Writing data to block 12 at offset 0x180000 Writing data to block 13 at offset 0x1a0000 Writing data to block 14 at offset 0x1c0000 Writing data to block 15 at offset 0x1e0000 Writing data to block 16 at offset 0x200000 Writing data to block 17 at offset 0x220000 Writing data to block 18 at offset 0x240000 Writing data to block 19 at offset 0x260000 Writing data to block 20 at offset 0x280000 Writing data to block 21 at offset 0x2a0000 Writing data to block 22 at offset 0x2c0000 Writing data to block 23 at offset 0x2e0000 Writing data to block 24 at offset 0x300000 Writing data to block 25 at offset 0x320000 Writing data to block 26 at offset 0x340000 Writing data to block 27 at offset 0x360000 Writing data to block 28 at offset 0x380000 Writing data to block 29 at offset 0x3a0000 Writing data to block 30 at offset 0x3c0000 Writing data to block 31 at offset 0x3e0000 Writing data to block 32 at offset 0x400000 Writing data to block 33 at offset 0x420000 Writing data to block 34 at offset 0x440000 Writing data to block 35 at offset 0x460000 Writing data to block 36 at offset 0x480000 Writing data to block 37 at offset 0x4a0000 Writing data to block 38 at offset 0x4c0000 Writing data to block 39 at offset 0x4e0000 Writing data to block 40 at offset 0x500000 Writing data to block 41 at offset 0x520000 Writing data to block 42 at offset 0x540000 Writing data to block 43 at offset 0x560000 Writing data to block 44 at offset 0x580000 Writing data to block 45 at offset 0x5a0000 Writing data to block 46 at offset 0x5c0000 Writing data to block 47 at offset 0x5e0000 Writing data to block 48 at offset 0x600000 Writing data to block 49 at offset 0x620000 Writing data to block 50 at offset 0x640000 Writing data to block 51 at offset 0x660000 Writing data to block 52 at offset 0x680000 Writing data to block 53 at offset 0x6a0000 Writing data to block 54 at offset 0x6c0000 Writing data to block 55 at offset 0x6e0000 Writing data to block 56 at offset 0x700000 Writing data to block 57 at offset 0x720000 Writing data to block 58 at offset 0x740000 Writing data to block 59 at offset 0x760000 Writing data to block 60 at offset 0x780000 Writing data to block 61 at offset 0x7a0000 Writing data to block 62 at offset 0x7c0000 Writing data to block 63 at offset 0x7e0000 Writing data to block 64 at offset 0x800000 Writing data to block 65 at offset 0x820000 Writing data to block 66 at offset 0x840000 Writing data to block 67 at offset 0x860000 Writing data to block 68 at offset 0x880000 Writing data to block 69 at offset 0x8a0000 Writing data to block 70 at offset 0x8c0000 Writing data to block 71 at offset 0x8e0000 Writing data to block 72 at offset 0x900000 Writing data to block 73 at offset 0x920000 Writing data to block 74 at offset 0x940000 Writing data to block 75 at offset 0x960000 Writing data to block 76 at offset 0x980000 Writing data to block 77 at offset 0x9a0000 Writing data to block 78 at offset 0x9c0000 Writing data to block 79 at offset 0x9e0000 Writing data to block 80 at offset 0xa00000 Writing data to block 81 at offset 0xa20000 Writing data to block 82 at offset 0xa40000 Writing data to block 83 at offset 0xa60000 Writing data to block 84 at offset 0xa80000 Writing data to block 85 at offset 0xaa0000 Writing data to block 86 at offset 0xac0000 Writing data to block 87 at offset 0xae0000 Writing data to block 88 at offset 0xb00000 Writing data to block 89 at offset 0xb20000 Writing data to block 90 at offset 0xb40000 Writing data to block 91 at offset 0xb60000 Writing data to block 92 at offset 0xb80000 65%t offset 0xba0000k 93 a Writing data to block 94 at offset 0xbc0000 Writing data to block 95 at offset 0xbe0000 Writing data to block 96 at offset 0xc00000 Writing data to block 97 at offset 0xc20000 Writing data to block 98 at offset 0xc40000 Writing data to block 99 at offset 0xc60000 Writing data to block 100 at offset 0xc80000 Writing data to block 101 at offset 0xca0000 Writing data to block 102 at offset 0xcc0000 Writing data to block 103 at offset 0xce0000 Writing data to block 104 at offset 0xd00000 Writing data to block 105 at offset 0xd20000 Writing data to block 106 at offset 0xd40000 Writing data to block 107 at offset 0xd60000 Writing data to block 108 at offset 0xd80000 Writing data to block 109 at offset 0xda0000 Writing data to block 110 at offset 0xdc0000 Writing data to block 111 at offset 0xde0000 Writing data to block 112 at offset 0xe00000 Writing data to block 113 at offset 0xe20000 Writing data to block 114 at offset 0xe40000 Writing data to block 115 at offset 0xe60000 Writing data to block 116 at offset 0xe80000 Writing data to block 117 at offset 0xea0000 Writing data to block 118 at offset 0xec0000 Writing data to block 119 at offset 0xee0000 Writing data to block 120 at offset 0xf00000 Writing data to block 121 at offset 0xf20000 Writing data to block 122 at offset 0xf40000 Writing data to block 123 at offset 0xf60000 Writing data to block 124 at offset 0xf80000 Writing data to block 125 at offset 0xfa0000 Writing data to block 126 at offset 0xfc0000 Writing data to block 127 at offset 0xfe0000 Writing data to block 128 at offset 0x1000000 Writing data to block 129 at offset 0x1020000 Writing data to block 130 at offset 0x1040000 Writing data to block 131 at offset 0x1060000 Writing data to block 132 at offset 0x1080000 Writing data to block 133 at offset 0x10a0000 Writing data to block 134 at offset 0x10c0000 Writing data to block 135 at offset 0x10e0000 Writing data to block 136 at offset 0x1100000 Writing data to block 137 at offset 0x1120000 Writing data to block 138 at offset 0x1140000 Writing data to block 139 at offset 0x1160000 Writing data to block 140 at offset 0x1180000 Writing data to block 141 at offset 0x11a0000 Writing data to block 142 at offset 0x11c0000 Writing data to block 143 at offset 0x11e0000 Writing data to block 144 at offset 0x1200000 Writing data to block 145 at offset 0x1220000 Writing data to block 146 at offset 0x1240000 Writing data to block 147 at offset 0x1260000 Writing data to block 148 at offset 0x1280000 Writing data to block 149 at offset 0x12a0000 Writing data to block 150 at offset 0x12c0000 Writing data to block 151 at offset 0x12e0000 Writing data to block 152 at offset 0x1300000 Writing data to block 153 at offset 0x1320000 Writing data to block 154 at offset 0x1340000 Writing data to block 155 at offset 0x1360000 Writing data to block 156 at offset 0x1380000 Writing data to block 157 at offset 0x13a0000 Writing data to block 158 at offset 0x13c0000 Writing data to block 159 at offset 0x13e0000 Writing data to block 160 at offset 0x1400000 Writing data to block 161 at offset 0x1420000 Writing data to block 162 at offset 0x1440000 Writing data to block 163 at offset 0x1460000 Writing data to block 164 at offset 0x1480000 Writing data to block 165 at offset 0x14a0000 Writing data to block 166 at offset 0x14c0000 Writing data to block 167 at offset 0x14e0000 Writing data to block 168 at offset 0x1500000 Writing data to block 169 at offset 0x1520000 Writing data to block 170 at offset 0x1540000 Writing data to block 171 at offset 0x1560000 Writing data to block 172 at offset 0x1580000 Writing data to block 173 at offset 0x15a0000 Writing data to block 174 at offset 0x15c0000 Writing data to block 175 at offset 0x15e0000 Writing data to block 176 at offset 0x1600000 Writing data to block 177 at offset 0x1620000 Writing data to block 178 at offset 0x1640000 Writing data to block 179 at offset 0x1660000 Writing data to block 180 at offset 0x1680000 Writing data to block 181 at offset 0x16a0000 Writing data to block 182 at offset 0x16c0000 97%3 at offset 0x16e0000 Writing data to block 184 at offset 0x1700000 Writing data to block 185 at offset 0x1720000 Writing data to block 186 at offset 0x1740000 Writing data to block 187 at offset 0x1760000 Writing data to block 188 at offset 0x1780000 Writing data to block 189 at offset 0x17a0000 Writing data to block 190 at offset 0x17c0000 Writing data to block 191 at offset 0x17e0000 Writing data to block 192 at offset 0x1800000 Writing data to block 193 at offset 0x1820000 Writing data to block 194 at offset 0x1840000 Writing data to block 195 at offset 0x1860000 Writing data to block 196 at offset 0x1880000 Writing data to block 197 at offset 0x18a0000 Writing data to block 198 at offset 0x18c0000 Writing data to block 199 at offset 0x18e0000 Writing data to block 200 at offset 0x1900000 Writing data to block 201 at offset 0x1920000 Writing data to block 202 at offset 0x1940000 Writing data to block 203 at offset 0x1960000 Writing data to block 204 at offset 0x1980000 Writing data to block 205 at offset 0x19a0000 Writing data to block 206 at offset 0x19c0000 Writing data to block 207 at offset 0x19e0000 Writing data to block 208 at offset 0x1a00000 Writing data to block 209 at offset 0x1a20000 Writing data to block 210 at offset 0x1a40000 Writing data to block 211 at offset 0x1a60000 Writing data to block 212 at offset 0x1a80000 Writing data to block 213 at offset 0x1aa0000 Writing data to block 214 at offset 0x1ac0000 Writing data to block 215 at offset 0x1ae0000 Writing data to block 216 at offset 0x1b00000 Writing data to block 217 at offset 0x1b20000 Writing data to block 218 at offset 0x1b40000 Writing data to block 219 at offset 0x1b60000 Writing data to block 220 at offset 0x1b80000 Writing data to block 221 at offset 0x1ba0000 Writing data to block 222 at offset 0x1bc0000 Writing data to block 223 at offset 0x1be0000 Writing data to block 224 at offset 0x1c00000 Writing data to block 225 at offset 0x1c20000 Writing data to block 226 at offset 0x1c40000 Writing data to block 227 at offset 0x1c60000 Writing data to block 228 at offset 0x1c80000 Writing data to block 229 at offset 0x1ca0000 Writing data to block 230 at offset 0x1cc0000 Writing data to block 231 at offset 0x1ce0000 Writing data to block 232 at offset 0x1d00000 Writing data to block 233 at offset 0x1d20000 Writing data to block 234 at offset 0x1d40000 Writing data to block 235 at offset 0x1d60000 Writing data to block 236 at offset 0x1d80000 Writing data to block 237 at offset 0x1da0000 Writing data to block 238 at offset 0x1dc0000 Writing data to block 239 at offset 0x1de0000 Writing data to block 240 at offset 0x1e00000 Writing data to block 241 at offset 0x1e20000 Writing data to block 242 at offset 0x1e40000 Writing data to block 243 at offset 0x1e60000 Writing data to block 244 at offset 0x1e80000 Writing data to block 245 at offset 0x1ea0000 Writing data to block 246 at offset 0x1ec0000 Writing data to block 247 at offset 0x1ee0000 Writing data to block 248 at offset 0x1f00000 Writing data to block 249 at offset 0x1f20000 Writing data to block 250 at offset 0x1f40000 Writing data to block 251 at offset 0x1f60000 Writing data to block 252 at offset 0x1f80000 Writing data to block 253 at offset 0x1fa0000 Writing data to block 254 at offset 0x1fc0000 Writing data to block 255 at offset 0x1fe0000 Writing data to block 256 at offset 0x2000000 Writing data to block 257 at offset 0x2020000 Writing data to block 258 at offset 0x2040000 Writing data to block 259 at offset 0x2060000 Writing data to block 260 at offset 0x2080000 Writing data to block 261 at offset 0x20a0000 Writing data to block 262 at offset 0x20c0000 Writing data to block 263 at offset 0x20e0000 Writing data to block 264 at offset 0x2100000 Writing data to block 265 at offset 0x2120000 Writing data to block 266 at offset 0x2140000 Writing data to block 267 at offset 0x2160000 Writing data to block 268 at offset 0x2180000 Writing data to block 269 at offset 0x21a0000 Writing data to block 270 at offset 0x21c0000 Writing data to block 271 at offset 0x21e0000 100%2:31-0000000000000000>Okay (13.24s) 2:31-0000000000000000>Start Cmd:FBK: sync at offset 0x2200000 Writing data to block 273 at offset 0x2220000 Writing data to block 274 at offset 0x2240000 Writing data to block 275 at offset 0x2260000 Writing data to block 276 at offset 0x2280000 2:31-0000000000000000>Okay (0.038s) 2:31-0000000000000000>Start Cmd:FBK: ucmd . /tmp/mtd.sh; flash_erase /dev/mtd${nanddtb} 0 0 Erasing 128 Kibyte @ 0 -- 100 % complete 2:31-0000000000000000>Okay (0.015s) 2:31-0000000000000000>Start Cmd:FBK: ucp imx95-19x19-evk.dtb t:/tmp/dtb 100%2:31-0000000000000000>Okay (0.015s) 2:31-0000000000000000>Start Cmd:FBK: ucmd . /tmp/mtd.sh; nandwrite -p /dev/mtd${nanddtb} /tmp/dtb Writing data to block 0 at offset 0x0 2:31-0000000000000000>Okay (0.047s) 2:31-0000000000000000>Start Cmd:FBK: ucmd . /tmp/mtd.sh; flash_erase /dev/mtd${nandrootfs} 0 0 Erasing 204672 Kibyte @ 0 -- 100 % complete 2:31-0000000000000000>Okay (4.231s) 2:31-0000000000000000>Start Cmd:FBK: ucmd ubidetach /dev/ubi_ctrl -m ${nandrootfs} || true 2:31-0000000000000000>Okay (0.019s) 2:31-0000000000000000>Start Cmd:FBK: ucmd . /tmp/mtd.sh; ubiattach /dev/ubi_ctrl -m ${nandrootfs} UBI device number 0, total 1599 LEBs (203034624 bytes, 193.6 MiB), available 1555 LEBs (197447680 bytes, 188.3 MiB), LEB size 126976 bytes (124.0 KiB) 2:31-0000000000000000>Okay (0.384s) 2:31-0000000000000000>Start Cmd:FBK: ucmd ubimkvol /dev/ubi0 -N nandrootfs -m Set volume size to 197447680 Volume ID 0, size 1555 LEBs (197447680 bytes, 188.3 MiB), LEB size 126976 bytes (124.0 KiB), dynamic, name "nandrootfs", alignment 1 2:31-0000000000000000>Okay (0.051s) 2:31-0000000000000000>Start Cmd:FBK: ucmd mkdir -p /mnt/mtd 2:31-0000000000000000>Okay (0.008s) 2:31-0000000000000000>Start Cmd:FBK: ucmd mount -t ubifs ubi0:nandrootfs /mnt/mtd 2:31-0000000000000000>Okay (0.204s) 2:31-0000000000000000>Start Cmd:FBK: acmd export EXTRACT_UNSAFE_SYMLINKS=1; tar --zstd --warning=no-timestamp -x -C /mnt/mtd 2:31-0000000000000000>Okay (0.052s) 2:31-0000000000000000>Start Cmd:FBK: ucp core-image-base-imx95-19x19-lpddr5-evk.rootfs-20260429064745.tar.zst t:- 100%2:31-0000000000000000>Okay (192.3s) 2:31-0000000000000000>Start Cmd:FBK: sync   3. Flashing NOR The bootloader flashed to NOR must use the newly added imx95_19x19_evk_spinand_defconfig . Therefore, imx95-evk.inc must be modified to enable this. 3.1 UUU Script uuu_version 1.2.39 # @_flexspi.bin | bootloader # @_image [_flexspi.bin] | image burn to flexspi, default is the same as bootloader # This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ SDP: boot -f .\imx-boot-nor.bin-flash_a55_flexspi # This command will be run when ROM support stream mode # i.MX8QXP, i.MX8QM, skip QSPI header SDPS: boot -f .\imx-boot-nor.bin-flash_a55_flexspi -skipfhdr # These commands will be run when use SPL and will be skipped if no spl # SDPU will be deprecated. please use SDPV instead of SDPU # { SDPU: delay 1000 SDPU: write -f .\imx-boot-nor.bin-flash_a55_flexspi -offset 0x10000 -skipfhdr SDPU: jump # } # These commands will be run when use SPL and will be skipped if no spl # if (SPL support SDPV) # { SDPV: delay 1000 SDPV: write -f .\imx-boot-nor.bin-flash_a55_flexspi -skipspl -skipfhdr SDPV: jump # } #######################second################################# FB: ucmd setenv fastboot_buffer ${loadaddr} FB: download -f .\imx-boot-imx95-19x19-lpddr5-evk-fspi.bin-flash_a55_flexspi FB: ucmd if test ! -n "$fastboot_bytes"; then setenv fastboot_bytes $filesize; else true; fi # Check Image if include flexspi header FB: ucmd if qspihdr dump ${fastboot_buffer}; then setenv qspihdr_exist yes; else setenv qspihdr_exist no; fi; # Check Image size if larger than 16M, then use uboot command to write image FB: ucmd if itest ${fastboot_bytes} -gt 1000000; then setenv qspihdr_large yes; else setenv qspihdr_large no; fi; FB[-t 60000]: ucmd if test ${qspihdr_exist} = yes -a ${qspihdr_large} = no; then qspihdr init ${fastboot_buffer} ${fastboot_bytes} safe; else true; fi; #if uboot can't support qspihdr command, use uboot image to write qspi image, which require image include qspi flash header FB: ucmd if test ${qspihdr_exist} = no; then sf probe; else true; fi; FB[-t 40000]: ucmd if test ${qspihdr_exist} = no; then sf erase 0 +${fastboot_bytes}; else true; fi; FB[-t 20000]: ucmd if test ${qspihdr_exist} = no; then sf write ${fastboot_buffer} 0 ${fastboot_bytes}; else true; fi; # if Image is larger than 16M, use uboot command to write image FB: ucmd if test ${qspihdr_large} = yes; then sf probe; else true; fi; FB: write -f .\imx-boot-imx95-19x19-lpddr5-evk-fspi.bin-flash_a55_flexspi -format "if test ${qspihdr_large} = yes; then sf erase @off +@size; sf write ${fastboot_buffer} @off @size; else true; fi;" -blksz 1 -each 0x100000 FB: done   3.2 U-Boot Patches The functionality implemented is: in the SPL stage, activate NOR FLASH (this is the default code setting), so that uboot.bin can be read from NOR during the SPL stage; then upon entering U-Boot, override the pinctrl settings in the DTB so that the FlexSPI driver uses the NAND pins, and then bring up the NAND on the M.2 connector during U-Boot initialization. imx95_19x19_evk_spinand_defconfig is based on the FSPI defconfig with MTD NAND configuration enabled in U-Boot. diff --git a/arch/arm/dts/imx95-19x19-evk-u-boot.dtsi b/arch/arm/dts/imx95-19x19-evk-u-boot.dtsi index 3c0c2d7b0f2..0d8fb0c3978 100644 --- a/arch/arm/dts/imx95-19x19-evk-u-boot.dtsi +++ b/arch/arm/dts/imx95-19x19-evk-u-boot.dtsi @@ -182,3 +182,7 @@ assigned-clock-parents = <0>, <&scmi_clk IMX95_CLK_HSIOPLL_VCO>, <&scmi_clk IMX95_CLK_SYSPLL1_PFD1_DIV2>; }; + +#ifdef CONFIG_MTD_SPI_NAND +#include "imx95-19x19-evk-spinand.dtsi" +#endif \ No newline at end of file diff --git a/board/freescale/imx95_evk/imx95_evk.c b/board/freescale/imx95_evk/imx95_evk.c index 9790c610ac7..333e051c090 100644 --- a/board/freescale/imx95_evk/imx95_evk.c +++ b/board/freescale/imx95_evk/imx95_evk.c @@ -22,6 +22,8 @@ #include <i2c.h> #include <dm/uclass.h> #include <dm/uclass-internal.h> +#include <dm.h> +#include <dm/device.h> extern int board_fix_fdt_fuse(void *fdt); @@ -383,6 +385,25 @@ void netc_init(void) pci_init(); } +static void flexspi_nor_fixup(void) +{ + struct gpio_desc desc; + int ret; + + ret = dm_gpio_lookup_name("GPIO5_10", &desc); + if (ret) + return; + + ret = dm_gpio_request(&desc, "XSPI1_SS0_B"); + if (ret) + return; + + dm_gpio_set_dir_flags(&desc, GPIOD_IS_OUT); + dm_gpio_set_value(&desc, 1); + + printf("flexspi_nor_fixup\n"); +} + static void flexspi_nor_steup(void) { struct gpio_desc desc; @@ -453,6 +474,78 @@ void lvds_backlight_on(void) dm_i2c_write(dev, 0x8, &reg, 1); } +static int fdt_switch_flexspi_pinctrl_to_nand(void *fdt) +{ + int off; + const void *prop; + int len; + int ret; + const char *flexspi_path = "/soc/bus@42000000/spi@425e0000"; + + off = fdt_path_offset(fdt, flexspi_path); + if (off < 0) { + printf("FDT: failed to find flexspi node %s, err=%d\n", + flexspi_path, off); + return off; + } + + prop = fdt_getprop(fdt, off, "pinctrl-1", &len); + if (!prop || len <= 0) { + printf("FDT: no pinctrl-1 found under %s\n", flexspi_path); + return -FDT_ERR_NOTFOUND; + } + + ret = fdt_setprop(fdt, off, "pinctrl-0", prop, len); + if (ret < 0) { + printf("FDT: failed to overwrite pinctrl-0, err=%d\n", ret); + return ret; + } + + printf("FDT: switched %s pinctrl-0 <- pinctrl-1 (NAND)\n", + flexspi_path); + + return 0; +} + +static void delete_fdt_flash0(void *fdt) +{ + int i = 0; + int nodeoff, ret; + static const char * const spi_nodes[] = { + "/soc/bus@42000000/spi@425e0000/flash@0" + }; + + printf("delete_fdt_flash0\n"); + + for (i = 0; i < ARRAY_SIZE(spi_nodes); i++) { + nodeoff = fdt_path_offset(fdt, spi_nodes[i]); + if (nodeoff >= 0) { +delete_node: + ret = fdt_del_node(fdt, nodeoff); + if (ret == -FDT_ERR_NOSPACE) { + ret = fdt_increase_size(fdt, 512); + if (!ret) { + nodeoff = fdt_path_offset(fdt, spi_nodes[i]); + if (nodeoff >= 0) + goto delete_node; + } + } + + if (ret) + printf("failed to delete node %s, ret=%d\n", + spi_nodes[i], ret); + else + printf("deleted node %s\n", spi_nodes[i]); + } + } +} + +static void fdt_fixup_flexspi(void *fdt) +{ + delete_fdt_flash0(fdt); + fdt_switch_flexspi_pinctrl_to_nand(fdt); +} + int board_init(void) { int ret; @@ -475,17 +568,50 @@ int board_init(void) netc_init(); - flexspi_nor_steup(); + // avoid NAND erase affect NOR with same FLEXSPI1_A_SS0_B + flexspi_nor_fixup(); power_on_m7("mx95evkrpmsg"); + printf("board_init\n"); + lvds_backlight_on(); return 0; } +static void debug_probe_fspi_nand(void) +{ + struct udevice *bus; + struct udevice *child; + int ret; + + printf("debug_probe_fspi_nand: start\n"); + + ret = uclass_get_device_by_name(UCLASS_SPI, "spi@425e0000", &bus); + printf("get spi bus ret=%d, bus=%p\n", ret, bus); + if (ret) + return; + + ret = device_probe(bus); + printf("probe spi bus ret=%d\n", ret); + + child = NULL; + device_find_first_child(bus, &child); + while (child) { + printf("child name=%s\n", child->name); + ret = device_probe(child); + printf("probe child %s ret=%d\n", child->name, ret); + device_find_next_child(&child); + } + + printf("debug_probe_fspi_nand: done\n"); +} + int board_late_init(void) { + printf("board_late_init\n"); + debug_probe_fspi_nand(); if (IS_ENABLED(CONFIG_ENV_IS_IN_MMC)) board_late_mmc_env_init(); @@ -645,6 +771,8 @@ static int board_fix_19x19_evk(void *fdt) int ret; const char *netcfg = "mx95netc"; + fdt_fixup_flexspi(fdt); + ret = scmi_misc_cfginfo(&msel, cfgname); if (!ret) { debug("SM: %s\n", cfgname); diff --git a/drivers/spi/nxp_fspi.c b/drivers/spi/nxp_fspi.c index 078b97f6544..07fb96cbfcc 100644 --- a/drivers/spi/nxp_fspi.c +++ b/drivers/spi/nxp_fspi.c @@ -1177,6 +1177,7 @@ static int nxp_fspi_default_setup(struct nxp_fspi *f) static int nxp_fspi_probe(struct udevice *bus) { + printf("------------>nxp_fspi_probe\n"); struct nxp_fspi *f = dev_get_priv(bus); f->devtype_data = @@ -1241,6 +1242,7 @@ static int nxp_fspi_of_to_plat(struct udevice *bus) #if CONFIG_IS_ENABLED(CLK) int ret; #endif + printf("------------>nxp_fspi_of_to_plat\n"); fdt_addr_t iobase; fdt_addr_t iobase_size; diff --git a/dts/upstream/src/arm64/freescale/imx95-19x19-evk.dts b/dts/upstream/src/arm64/freescale/imx95-19x19-evk.dts index 6086cb7fa5a..10e9f76c5af 100644 --- a/dts/upstream/src/arm64/freescale/imx95-19x19-evk.dts +++ b/dts/upstream/src/arm64/freescale/imx95-19x19-evk.dts @@ -194,11 +194,12 @@ }; &flexspi1 { - pinctrl-names = "default"; + pinctrl-names = "default", "nand"; pinctrl-0 = <&pinctrl_flexspi1>; + pinctrl-1 = <&pinctrl_flexspi1_nand>; status = "okay"; - flash@0 { + flash0: flash@0 { compatible = "jedec,spi-nor"; reg = <0>; pinctrl-names = "default"; @@ -445,6 +446,18 @@ >; }; + pinctrl_flexspi1_nand: flexspi1nandgrp { + fsl,pins = < + IMX95_PAD_XSPI1_SS0_B__GPIO5_IO_BIT10 0x3fe + IMX95_PAD_SD3_CMD__FLEXSPI1_A_SS0_B 0x3fe + IMX95_PAD_SD3_CLK__FLEXSPI1_A_SCLK 0x3fe + IMX95_PAD_SD3_DATA0__FLEXSPI1_A_DATA_BIT0 0x3fe + IMX95_PAD_SD3_DATA1__FLEXSPI1_A_DATA_BIT1 0x3fe + IMX95_PAD_SD3_DATA2__FLEXSPI1_A_DATA_BIT2 0x3fe + IMX95_PAD_SD3_DATA3__FLEXSPI1_A_DATA_BIT3 0x3fe + >; + }; + pinctrl_flexspi1_reset: flexspi1-reset-grp { fsl,pins = < IMX95_PAD_XSPI1_SS1_B__GPIO5_IO_BIT11 0x3fe   3.3 imx95-evk.inc Content require conf/machine/include/imx-base.inc require conf/machine/include/arm/armv8-2a/tune-cortexa55.inc MACHINE_FEATURES += "pci wifi bluetooth optee" MACHINE_FEATURES:append:use-nxp-bsp = " nxpwifi-all-pcie nxpwifi-all-sdio jailhouse dpdk xen" KERNEL_DEVICETREE = " \ freescale/${KERNEL_DEVICETREE_BASENAME}.dtb \ " UBOOT_DTB_NAME = "${KERNEL_DEVICETREE_BASENAME}.dtb" IMX_DEFAULT_BOOTLOADER:use-nxp-bsp = "u-boot-imx" IMX_DEFAULT_BOOTLOADER:use-mainline-bsp = "u-boot-fslc" LOADADDR = "" UBOOT_SUFFIX = "bin" UBOOT_MAKE_TARGET = "" SPL_BINARY = "spl/u-boot-spl.bin" UBOOT_CONFIG ??= "sd" UBOOT_CONFIG[sd] = "${UBOOT_CONFIG_BASENAME}_defconfig,sdcard" UBOOT_CONFIG[sd-ecc] = "${UBOOT_CONFIG_BASENAME}_defconfig,sdcard" UBOOT_CONFIG[fspi] = "${UBOOT_CONFIG_BASENAME}_spinand_defconfig"///////////////////here UBOOT_CONFIG[spinand] = "${UBOOT_CONFIG_BASENAME}_spinand_defconfig"////////////////here ATF_PLATFORM = "imx95" OEI_CORE = "m33" OEI_SOC = "mx95" OEI_BOARD ?= "mx95lp5" DDR_TYPE ?= "lpddr5" IMXBOOT_VARIANTS = "alt jailhouse netc rpmsg sof" # Multiple system manager configs by IMXBOOT_VARIANT SYSTEM_MANAGER_CONFIG = \ "${@bb.utils.contains('IMXBOOT_VARIANT', 'alt', 'mx95alt', \ bb.utils.contains('IMXBOOT_VARIANT', 'jailhouse', 'mx95evkjailhouse', \ bb.utils.contains('IMXBOOT_VARIANT', 'netc', 'mx95netc', \ bb.utils.contains('IMXBOOT_VARIANT', 'rpmsg', 'mx95evkrpmsg', \ bb.utils.contains('IMXBOOT_VARIANT', 'sof', 'mx95evksof', \ 'mx95evk', d), d), d), d), d)}" # imx-boot (flash.bin) targets based on UBOOT_CONFIG and IMXBOOT_VARIANT IMXBOOT_TARGETS_SD = " \ ${@bb.utils.contains('IMXBOOT_VARIANT', 'alt', '${IMXBOOT_TARGETS_BASENAME}_alt', \ bb.utils.contains('IMXBOOT_VARIANT', 'jailhouse', '${IMXBOOT_TARGETS_BASENAME}_jailhouse', \ bb.utils.contains('IMXBOOT_VARIANT', 'netc', '${IMXBOOT_TARGETS_BASENAME}_netc', \ bb.utils.contains('IMXBOOT_VARIANT', 'rpmsg', '${IMXBOOT_TARGETS_BASENAME}_lpboot_sm_a55', \ bb.utils.contains('IMXBOOT_VARIANT', 'sof', '${IMXBOOT_TARGETS_BASENAME}_a55', \ '${IMXBOOT_TARGETS_BASENAME}_all ${IMXBOOT_TARGETS_BASENAME}_a55', d), d), d), d), d)} \ " IMXBOOT_TARGETS = " \ ${@bb.utils.contains('UBOOT_CONFIG', 'fspi', '${IMXBOOT_TARGETS_BASENAME}_a55_flexspi', \ bb.utils.contains('UBOOT_CONFIG', 'sd-ecc', '${IMXBOOT_TARGETS_BASENAME}_all', \ '${IMXBOOT_TARGETS_SD}', d), d)} \ " IMX_BOOT_SOC_TARGET = "iMX95" IMX_BOOT_SEEK = "32" # We have to disable SERIAL_CONSOLE due to auto-serial-console SERIAL_CONSOLES = "115200;ttyLP0" IMX_DEFAULT_BSP = "nxp"   4. NOR Boot Test After NOR boot, U-Boot activates the NAND on the M.2 connector, successfully reads the kernel and device tree from NAND. After entering the kernel, the rootfs is successfully mounted. U-Boot SPL 2025.04-g4ddbad60eff3-dirty (Mar 19 2026 - 03:13:58 +0000) SYS Boot reason: por, origin: -1, errid: -1 SYS shutdown reason: por, origin: -1, errid: -1 Normal Boot Trying to boot from SPI ------------>nxp_fspi_of_to_plat ------------>nxp_fspi_probe Boot stage: Primary Image set: 0, offset: 0x1000 Load image from QSPI 0xde400------------------------------->NOR BOOT NOTICE: BL31: v2.12.0(release):lf-6.12.49-2.2.0 NOTICE: BL31: Built : 10:35:59, Apr 21 2026 U-Boot 2025.04-g4ddbad60eff3-dirty (Mar 19 2026 - 03:13:58 +0000) CPU: i.MX9596 rev2.0 at 1800MHz CPU: Extended Industrial temperature grade (-40C to 125C) at 28C LM Boot reason: por, origin: -1, errid: -1 LM shutdown reason: por, origin: -1, errid: -1 Model: NXP i.MX95 19X19 board DRAM: delete_fdt_flash0 deleted node /soc/bus@42000000/spi@425e0000/flash@0 FDT: switched /soc/bus@42000000/spi@425e0000 pinctrl-0 <- pinctrl-1 (NAND) 15.8 GiB TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C6 0x50] PCIE-2: Link down PCIE-3: Link down cfg name not match mx95evkrpmsg:mx95evk, ignore board_init Core: 317 devices, 38 uclasses, devicetree: separate MMC: FSL_SDHC: 0, FSL_SDHC: 1 Loading Environment from nowhere... OK [*]-Video Link 0clk disp1pix already disabled adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c fail to probe panel device hdmi@3d probe video device failed, ret -19 [0] display-controller@4b400000, video [1] channel@0, video_bridge [2] bridge@8, video_bridge [3] dsi@4acf0000, video_bridge [4] hdmi@3d, panel clk disp1pix already disabled adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c fail to probe panel device hdmi@3d probe video device failed, ret -19 In: serial Out: serial Err: serial BuildInfo: - SM firmware Build 763, Commit de30901b, Apr 15 2026 01:18:07 - ELE firmware version 2.0.4-9ca4d997 board_late_init debug_probe_fspi_nand: start ------------>nxp_fspi_of_to_plat ------------>nxp_fspi_probe get spi bus ret=0, bus=00000000fd4a13d0 probe spi bus ret=0 child name=mt29f4g01abbfd12@0 probe child mt29f4g01abbfd12@0 ret=0----------------->SWITCH TO NAND debug_probe_fspi_nand: done UID: 182ba9e87d9840babd9d12161b48e82d Net: eth0: enetc-0 [PRIME], eth1: enetc-2 Fastboot: Normal Normal Boot Hit any key to stop autoboot: 0 u-boot=> setenv bootargs 'console=ttyLP0,115200 earlycon ubi.mtd=rootfs root=ubi0:nandrootfs rootfstype=ubifs rootwait rw' u-boot=> mtd read kernel ${loadaddr} 0 0x2800000 Reading 41943040 byte(s) (20480 page(s)) at offset 0x00000000 u-boot=> mtd read dtb ${fdt_addr} 0 0x20000 Reading 131072 byte(s) (64 page(s)) at offset 0x00000000 u-boot=> booti ${loadaddr} - ${fdt_addr} ------------------>read kernel, dtb in NAND ## Flattened Device Tree blob at 93000000 Booting using the fdt blob at 0x93000000 Working FDT set to 93000000 Loading Device Tree to 000000009ffe5000, end 000000009ffffeaf ... OK Working FDT set to 9ffe5000 clk disp1pix already disabled adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c fail to probe panel device hdmi@3d probe video device failed, ret -19 Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x412fd050] [ 0.000000] Linux version 6.18.2-1.0.0-gf49f45233f7b-dirty (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 15.2.0, GNU ld (GNU Binutils) 2.45.0.20250908) #1 SMP PREEMPT Tue Apr 28 08:20:17 UTC 2026 [ 0.000000] KASLR enabled [ 0.000000] Machine model: NXP i.MX95 19X19 board [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created CMA memory pool at 0x00000000c3000000, size 960 MiB [ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: 0x00000000c3000000..0x00000000feffffff (983040 KiB) map reusable linux,cma [ 0.000000] earlycon: lpuart32 at MMIO32 0x0000000044380000 (options '') ................... [ 2.416067] spi-nand spi1.0: Winbond SPI NAND was found. [ 2.428075] spi-nand spi1.0: 256 MiB, block size: 128 KiB, page size: 2048, OOB size: 128 [ 2.450050] 5 fixed-partitions partitions found on MTD device spi1.0 [ 2.450059] Creating 5 MTD partitions on "spi1.0": [ 2.463548] 0x000000000000-0x000000800000 : "bootloader" [ 2.529065] 0x000000800000-0x000001000000 : "config" [ 2.543539] 0x000001000000-0x000003800000 : "kernel" [ 2.580906] 0x000003800000-0x000003820000 : "dtb" [ 2.586513] 0x000003820000-0x00010381ffff : "rootfs" [ 2.591493] mtd: partition "rootfs" extends beyond the end of device "spi1.0" -- size truncated to 0xc7e0000 [ 2.748893] mtd: setting mtd4 (rootfs) as root device [ 4.909898] ubi0: attaching mtd4 [ 5.406361] ubi0: scanning is finished [ 5.454338] ubi0: attached mtd4 (name "rootfs", size 199 MiB) [ 5.460134] ubi0: PEB size: 131072 bytes (128 KiB), LEB size: 126976 bytes [ 5.467131] ubi0: min./max. I/O unit sizes: 2048/2048, sub-page size 2048 [ 5.473950] ubi0: VID header offset: 2048 (aligned 2048), data offset: 4096 [ 5.480935] ubi0: good PEBs: 1599, bad PEBs: 0, corrupted PEBs: 0 [ 5.487037] ubi0: user volume: 1, internal volumes: 1, max. volumes count: 128 [ 5.494255] ubi0: max/mean erase counter: 10/1, WL threshold: 4096, image sequence number: 2909496578 [ 5.503473] ubi0: available PEBs: 0, total reserved PEBs: 1599, PEBs reserved for bad PEB handling: 40 [ 5.512840] ubi0: background thread "ubi_bgt0d" started, PID 135 [ 5.594576] UBIFS (ubi0:0): Mounting in unauthenticated mode [ 5.600411] UBIFS (ubi0:0): background thread "ubifs_bgt0_0" started, PID 141 [ 5.617312] UBIFS (ubi0:0): recovery needed [ 5.801795] UBIFS (ubi0:0): recovery completed [ 5.806343] UBIFS (ubi0:0): UBIFS: mounted UBI device 0, volume 0, name "nandrootfs" [ 5.814101] UBIFS (ubi0:0): LEB size: 126976 bytes (124 KiB), min./max. I/O unit sizes: 2048 bytes/2048 bytes [ 5.824021] UBIFS (ubi0:0): FS size: 195923968 bytes (186 MiB, 1543 LEBs), max 1555 LEBs, journal size 9777152 bytes (9 MiB, 77 LEBs) [ 5.836024] UBIFS (ubi0:0): reserved for root: 4952683 bytes (4836 KiB) [ 5.842640] UBIFS (ubi0:0): media format: w5/r0 (latest is w5/r0), UUID 02E616B2-3C31-4F48-A886-9B4D26DB37C1, small LPT model [ 5.854616] VFS: Mounted root (ubifs filesystem) on device 0:23. [ 5.860973] devtmpfs: mounted [ 5.864349] Freeing unused kernel memory: 2112K [ 5.868991] Run /sbin/init as init process [ 5.874243] Run /etc/init as init process [ 5.879058] Run /bin/init as init process [ 5.884114] Run /bin/sh as init process  
記事全体を表示
The following table summarizes the assignment of the Low Power UARTs (LPUARTs) on the i.MX 943 EVK when running the NXP Linux BSP. LPUART instance Hardware interface FTDI channels/Pins Comment LPUART8 On-board FT4232H UART-USB adapter Channel A Used by Cortex-M33 Sync core (M33 core 1) N/A(BCU)/LPUART11/LPUART12 Channel B Used by the BCU tool, or used as serial port for Cortex-M70 (LPUART11), or Cortex-M71 (LPUART12) LPUART1 Channel C Used by Cortex-A55 (U-Boot/Linux) LPUART2 Channel D Used by Cortex-M33 (M33 core 0, System Manager) LPUART11 External UART pins (board connectors) M2_UART11_RXD M2_UART11_TXD Used by the Cortex-M70 (a UART to USB adapter is needed) LPUART12 M1_UART12_RXD M1_UART12_TXD Used by the Cortex-M71 (a UART to USB adapter is needed)   If USB DBG port is connected to a Linux host PC, the channels A..D of the FTDI will appear as /dev/ttyUSB0..3 in that order. 1. LPUART8 is used by the Cortex-M33 Sync core application. LPUART8 shares the pins with the JTAG interface, so to route these pins to the FTDI adapter, set: SW7[4] = 1 and SW7[3] = 0. 2. If the JTAG is needed, the M33 Sync core can use LPUART3 instead of LPUART8. In the MCUXSDK applications, the only required code change is to set BOARD_DEBUG_UART_INSTANCE to 3. Board pin connections for LPUART3: J51-18  - M1_PWM_CX (LPUART3_TX) ----- RX of USB-UART converter    ---- PC J44-10 - M1_LED_TP1   (LPUART3_RX) ----- TX of USB-UART converter    ---- PC J45-12 - GND                                        ----- GND of USB-UART converter ---- PC 3. The FTDI Channel B is multiplexed between two functionalities: for the Board Remote Control Utilities (BCU). In this case, set SW7[1] = 0. Do not open ttyUSB1 in a terminal while using the BCU tool. connection to LPUART11 (Cortex-M70) or LPUART12 (Cortex-M71). Set SW7[1] = 1. To select between the two UARTs, set: SW7[2] = 1 for LPUART11, or SW7[2] = 0 for LPUART12. To route the two UARTs towards the FTDI, an additional multiplexer needs to be configured through an IO expander pin (UART_M_FT_SEL in the figure below). elena_popa_1-1778437892999.png The following software changes are required: In the MCUXSDK application source code, call BOARD_SelectFTUART() in the BOARD_InitHardware() function in hardware_init.c. In the System Manager configuration file mx94evk.cfg, move the LPI2C6 and its pins (PIN_GPIO_IO28 and PIN_GPIO_IO29) to the the M7 core that will use the routed UART. LPI2C6 is needed to set UART_M_FT_SEL. In the Linux kernel device tree, disable the I2C6 peripheral. 4. LPUART1 is routed to the FTDI Channel C and is used by the A55 core (SPL, U-Boot, Linux). This path works by default. 5. LPUART2 is routed to the FTDI Channel D and is used by the M33 Core 0 (OEI, System Manager). 6. In the default configuration, LPUART11 (M70) and LPUART12 (M71) are routed to the M2 connectors. Board pin connections for LPUART11 (for Cortex-M70): J48-2 - M2_UART11_RXD   ---- TX of USB-UART adapter     ---- PC J48-4 - M2_UART11_TXD   ---- RX of USB-UART adapter     ---- PC GND                                     ---- GND of USB-UART adapter  ---- PC Board pin connections for LPUART12 (for Cortex-M71): J44-2 - M1_UART12_RXD   ---- TX of USB-UART adapter     ---- PC J44-4 - M1_UART12_TXD   ---- RX of USB-UART adapter     ---- PC GND                                     ---- GND of USB-UART adapter  ---- PC
記事全体を表示
This blog enables support of Qemu emulation for iMX8MM EVK.  Imagine not having the hardware but still you want to test the software. Qemu gives you exactly that. 1. Booting uboot, linux and user-space application even when you do not possess a real hardware. 2. Early firmware development when the silicon doesn’t yet exist. 3. Linux driver development, debugging and testing.
記事全体を表示
We are pleased to announce that Config Tools for i.MX 26.03 are now available. Downloads & links To download the installer for all platforms, please login to our download site via:  https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX Please refer to  Documentation  for installation and quick start guides. For further information about DDR config and validation, please go to this  blog post. Release Notes Full details on the release (features, known issues...) Version 26.03 System Manager Memory sector information for resources with memory configuration is added to the Resources overview. Support for memory sectors splitting. Memory configuration input for resources using MBC/MRC is improved. Support for macOS (aarch64 and x86_64) is added. Clocks Hierarchy for local configuration element settings is supported. TEE Multicore Interrupt Handling for Single Security Domain is supported. Option to filter only user-defined memory regions is added. Interrupts are now separated into groups based on the core.
記事全体を表示
This page serves as a hub to gather the links to all the currently available ISP supported camera lists for the i.MX Applications processors.  Camera Compatibility Guides Processor/Family Link to Guide i.MX 8M Plus i.MX 8M Plus ISP Camera Compatibility Guide i.MX 95 i.MX 95 ISP Camera Compatibility Guide   Additional Resources i.MX Camera Software Pack AN AN14376: i.MX Camera Software Pack | NXP Semiconductors
記事全体を表示
The purpose of this page is to provide supportive information for the selection of suitable camera modules that are supported by the i.MX95. The guide is attached in this page. This helps customers evaluate project feasibility and integration aspects when considering i.MX 95 SoCs for their products. It is strongly recommended to consult with NXP and the camera module vendor before finalizing the choice of the camera part number to ensure compatibility, availability, longevity, and pricing requirements.   NXP Supported Sensors: Sensor Vendor Image Sensor Max Resolution Camera Module OmniVision OS08A20 8MP IMX95-OS08A20 | NXP Semiconductors EXPI-OS08A20 OmniVision OX05B1S 5MP   OmniVision OX03C10 3MP   Onsemi AR0144 1MP AR0144   Partner Enabled Sensors: Partner Sensor Vendor Image Sensor Max Resolution ISP Tuning Camera Module Location FRAMOS Sony IMX662 2MP ✔ FSM:GO Munich, Germany/ Canada/USA Sony IMX678 8MP Sony IMX900 3.2MP Sony IMX676 12MP Onsemi Onsemi AR2020 19MP   Module available through Future Electronics   Entron OmniVision OS08A20 8MP ✔ EXPI-OS08A20 China Onsemi AR0820 8MP Order with Entron Onsemi AR0823 8MP Technexion Onsemi AR0144 1MP       Onsemi AR0145 1MP     Onsemi AR0234 2MP     Onsemi AR0235 2MP     Onsemi AR0236 2MP     Onsemi AR0521 5MP     Onsemi AR0522 5MP     Onsemi AR0544 5MP     Onsemi AR0821 8MP       Onsemi AR0822 8MP     Onsemi AR0830 8MP     Onsemi AR1335 13MP     PHYTEC Onsemi AR0144 1MP     Germany/ China/India/ USA Onsemi AR0234 2.3MP   Onsemi AR0521 5MP   E-consystems Sony IMX662 2.4MP     Riverside, CA, USA/India Sony IMX900 3.2MP    
記事全体を表示
Use Raspberry Pi Debug Probe with OpenOCD and i.MX93 FRDM   This document explains the integration process of the Raspberry Pi Debug Probe (Very low cost debugger) with the OpenOCD (On Chip Debugger) tool with the i.MX93 FRDM board.   Also, we will use GDB (GNU DeBugger) to interact with the OpenOCD.   1. Install and Configure OpenOCD   Update and install dependencies sudo apt update sudo apt install build-essential libtool automake pkg-config libusb-1.0-0-dev libhidapi-dev libftdi1-dev libjim-dev jimsh   Clone the OpenOCD repo git clone https://github.com/openocd-org/openocd.git cd openocd   Run ./bootstrap to create the configuration file git submodule update --init --recursive ./bootstrap ./configure --enable-cmsis-dap --enable-hidapi   Make OpenOCD make -j$(nproc) sudo make install   Download the configuration file for i.MX93 You can dowload the  imx93.cfg  in the Table 2. Software requirements on Ubuntu PC of the AN14367 Then, copy the downloaded file to the openocd/tcl/target/ as below: cp ../imx93_new-b42b7c4cac18508442d3df035cec1c6d.cfg tcl/target/imx93.cfg   2. Create UDEV rules   sudo nano /etc/udev/rules.d/99-openocd.rules Add the below in that file: ATTRS{idVendor}=="2e8a", ATTRS{idProduct}=="000c", MODE="660", GROUP="plugdev", TAG+="uaccess"   Reload rules sudo udevadm control --reload-rules && sudo udevadm trigger   3. Connecting the Hardware   To make the DAP works in the i.MX93 FRDM, we must rework the board removing the resistors R3017 and R3018:   frdm_r3017r3018_sch.png frdm_r3017r3018.png   Now, we need to connect the Raspberry Pi Debug Probe with the SWD (P14) of our i.MX93 FRDM board:   FRDM-IMX93.jpeg   rpdebug.jpeg   4. Running the Debug Session   In this moment, with the RP Debug Probe connected, we can Boot the i.MX93 FRDM board and run the below command to start the OpenOCD: $ openocd -s tcl -f interface/cmsis-dap.cfg -c "adapter speed 1000" -f target/imx93.cfg   tic-mpu@tic-mpu:~/Debug_test/openocd$ openocd -s tcl -f interface/cmsis-dap.cfg -c "adapter speed 1000" -f target/imx93.cfg Open On-Chip Debugger 0.12.0+dev-02429-ge4c49d860 (2026-03-21-23:05) Licensed under GNU GPL v2 For bug reports, read http://openocd.org/doc/doxygen/bugs.html adapter speed: 1000 kHz Warn : DEPRECATED: auto-selecting transport "swd". Use 'transport select swd' to suppress this message. Info : Listening on port 6666 for tcl connections Info : Listening on port 4444 for telnet connections Info : Using CMSIS-DAPv2 interface with VID:PID=0x2e8a:0x000c, serial=E6633861A33A1B2C Info : CMSIS-DAP: SWD supported Info : CMSIS-DAP: Atomic commands supported Info : CMSIS-DAP: Test domain timer supported Info : CMSIS-DAP: FW Version = 2.0.0 Info : CMSIS-DAP: Interface Initialised (SWD) Info : SWCLK/TCK = 0 SWDIO/TMS = 0 TDI = 0 TDO = 0 nTRST = 0 nRESET = 0 Info : CMSIS-DAP: Interface ready Info : clock speed 1000 kHz Info : SWD DPIDR 0x5ba02477 Info : imx93.a55.0: hardware has 6 breakpoints, 4 watchpoints Info : [imx93.a55.0] external reset detected Info : [imx93.a55.0] Examination succeed Info : [imx93.m33] Cortex-M33 r1p0 processor detected Info : [imx93.m33] target has 8 breakpoints, 4 watchpoints Info : [imx93.m33] Examination succeed Info : [imx93.ahb] Examination succeed Info : [imx93.a55.0] starting gdb server on 3333 Info : Listening on port 3333 for gdb connections Info : [imx93.m33] starting gdb server on 3334 Info : Listening on port 3334 for gdb connections Info : [imx93.ahb] gdb port disabled   From the Logs, we can see we have two ports: 3333 for Cortex A55 [imx93.a55.0] 3334 for Cortex M33 [imx93.m33]   Install gdb-multiarch   Now, we can install GDB: sudo apt install gdb-multiarch And start a Debug session: $ gdb-multiarch ~/linux-imx/vmlinux   $ gdb-multiarch ~/linux-development/linux-imx/vmlinux GNU gdb (Ubuntu 15.1-1ubuntu1~24.04.1) 15.1 Copyright (C) 2024 Free Software Foundation, Inc. License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html> This is free software: you are free to change and redistribute it. There is NO WARRANTY, to the extent permitted by law. Type "show copying" and "show warranty" for details. This GDB was configured as "x86_64-linux-gnu". Type "show configuration" for configuration details. For bug reporting instructions, please see: <https://www.gnu.org/software/gdb/bugs/>. Find the GDB manual and other documentation resources online at: <http://www.gnu.org/software/gdb/documentation/>. For help, type "help". Type "apropos word" to search for commands related to "word"... Reading symbols from /home/tic-mpu/linux-development/linux-imx/vmlinux... (gdb) target extended-remote localhost:3333 Remote debugging using localhost:3333 0x00000000fff118fc in ?? ()   A simple example of how to read a register with GDB: (gdb) x/xw 0x43810000 0x43810000: 0x02010001     Happy debugging!     Best regards, Salas. 
記事全体を表示
Tested in FRDM-i.MX91 Written in C LF-6.12.49
記事全体を表示
There are currently no additional test programs in I.MX Jailhouse program. This demo shares how to test RM67199 MIPI panel in Jailhouse inmate.   Please refer run.sh in attachments. modprobe jailhouse insmod jailhouse_clk.ko # adjust pixel clock for MIPI PANEL RMP67199 echo 129937500 > /sys/bus/platform/devices/jailhouse_clk/rate_pix export PATH=$PATH:/usr/share/jailhouse/tools/ jailhouse enable /root/imx8mm.cell jailhouse cell linux /root/imx8mm-inmate-demo.cell /root/Image.bin -d /root/imx8mm-evk-inmate.dtb -c "clk_ignore_unused console=ttymxc3,115200 earlycon=ec_imx6q,0x30890000,115200 root=/dev/mmcblk2p2 rootwait rw"  
記事全体を表示
There are currently no additional test programs in I.MX Jailhouse program. This demo shares how to test USB function in Jailhouse inmate. Inmate boot log: root@imx8mmevk:~# dmesg | grep usb [ 0.312280] usbcore: registered new interface driver usbfs [ 0.317206] usbcore: registered new interface driver hub [ 0.322279] usbcore: registered new device driver usb [ 0.911649] usbcore: registered new device driver r8152-cfgselector [ 0.917711] usbcore: registered new interface driver r8152 [ 0.994200] usbcore: registered new interface driver uas [ 0.999359] usbcore: registered new interface driver usb-storage [ 1.005192] usbcore: registered new interface driver usbserial_generic [ 1.011486] usbserial: USB Serial support registered for generic [ 1.017274] usbcore: registered new interface driver ftdi_sio [ 1.022813] usbserial: USB Serial support registered for FTDI USB Serial Device [ 1.029852] usbcore: registered new interface driver usb_serial_simple [ 1.036148] usbserial: USB Serial support registered for carelink [ 1.042016] usbserial: USB Serial support registered for flashloader [ 1.048144] usbserial: USB Serial support registered for funsoft [ 1.053931] usbserial: USB Serial support registered for google [ 1.059643] usbserial: USB Serial support registered for hp4x [ 1.065185] usbserial: USB Serial support registered for kaufmann [ 1.071051] usbserial: USB Serial support registered for libtransistor [ 1.077334] usbserial: USB Serial support registered for moto_modem [ 1.083371] usbserial: USB Serial support registered for motorola_tetra [ 1.089745] usbserial: USB Serial support registered for nokia [ 1.095368] usbserial: USB Serial support registered for novatel_gps [ 1.101486] usbserial: USB Serial support registered for siemens_mpi [ 1.107612] usbserial: USB Serial support registered for suunto [ 1.113316] usbserial: USB Serial support registered for vivopay [ 1.119111] usbserial: USB Serial support registered for zio [ 1.124578] usbcore: registered new interface driver usb_ehset_test [ 1.215499] usbcore: registered new interface driver usbhid [ 1.220879] usbhid: USB HID core driver [ 1.396384] usb_phy_generic usbphynop1: dummy supplies not allowed for exclusive requests [ 42.414253] usb 1-1: new high-speed USB device number 2 using ci_hdrc [ 42.577822] usb-storage 1-1:1.0: USB Mass Storage device detected [ 42.579492] scsi host0: usb-storage 1-1:1.0  
記事全体を表示
This tutorial describes the complete procedure for calibrating a touchscreen display using Weston, specifically validated with the DY1212W LVDS panel on the following NXP development platforms: i.MX93‑EVK FRDM‑i.MX95 FRDM‑i.MX8MP While the initial calibration performed by Weston works only temporarily, this guide will walk you through configuring the system so that the calibration becomes persistent across reboots. The steps below include performing the initial calibration, editing Weston’s configuration, creating a calibration helper script, and applying udev rules to store the calibration matrix automatically.   Temporary Touchscreen Calibration To begin, run the following command to perform an initial calibration of your touchscreen: weston-touch-calibrator LVDS-1   After running this command, your display should be correctly calibrated. However, this calibration is not persistent, and you will need to recalibrate after every reboot unless you complete the persistence steps below.   Making the Calibration Persistent Follow the steps below to ensure that calibration settings are preserved across system restarts. Step 1: Edit the Weston Configuration File Open the following file: /etc/xdg/weston/weston.ini Under the [libinput] section, add these lines: [libinput] touchscreen_calibrator=true + calibration_helper=/usr/bin/save-calibration.sh This enables the calibration helper script that will automatically save your settings. Step 2: Create the Calibration Helper Script Create a new script at: /usr/bin/save-calibration.sh   Insert the following content: #!/bin/bash # Store the transformation arguments for the resistive touchscreen as udev rule echo 'SUBSYSTEM=="input", KERNEL=="event[0-9]*", ENV{ID_INPUT_TOUCHSCREEN}=="1", ENV{LIBINPUT_CALIBRATION_MATRIX}="'$2' '$3' '$4' '$5' '$6' '$7'"' >> /etc/udev/rules.d/touchscreen.rules   Make the script executable: chmod 755 /usr/bin/save-calibration.sh   Step 3: Restart Weston and Recalibrate Restart the Weston service: systemctl restart weston   Run the calibration tool again to generate the persistent settings: weston-touch-calibrator LVDS-1 reboot   Conclusion After completing all of the steps above, your touchscreen calibration will now persist across reboots, ensuring a consistent user experience even after powering off the board. This configuration allows the system to automatically store and apply calibration data through a udev rule generated by your helper script. If you encounter any issues or require further assistance, feel free to reach out. Best regards, Chavira
記事全体を表示
this poring is based on the imx415 driver, the capture format is based on raw10, the bsp version is 6.6.52, the patches are attached Disclaimer: − “Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.”
記事全体を表示
   Memory Compatibility Guides   Processor/Family Link to Guide i.MX 8/8X/8XLite DDR3L & LPDDR4 i.MX 8M Quad/8M Mini/8M Nano/8M Plus DDR3L, DDR4, LPDDR4 i.MX 8ULP  LPDDR3, LPDDR4 & LPDDR4x i.MX 91 LPDDR4 - New i.MX 93 LPDDR4/LPDDR4x i.MX 95 LPDDR5/LPDDR4x - New Ara240 - DNPU LPDDR4 - New Other Processor Families Please contact NXP Support or Sales   Additional Resources i.MX Memory Fact Sheet DDR memory selection & enablement for i.MX platforms Smarter World Blog Building Resilient Embedded Systems: NXP’s Approach to DDR Memory Selection and Support DDR Configuration Tools DDR Configuration tool for i.MX  Developer Resources i.MX Developer Resources SW & Tools
記事全体を表示
i.MX 93 EVK LF-6.12.49 patches
記事全体を表示
Attached slides introduce the i.MX95 Power management with following topics: SoC Power Architecture Power Management with BSP Power on/off & Reboot Suspend Implementation Low Power Run
記事全体を表示
GUI Guider version:  1.9.x, 1.10.x LVGL version: v8.x.x , v9.x.x Host software requirements: Ubuntu 20.04, Ubuntu 22.04 or Debian 12 Target  software requirements:  BSP 6.6 or higher  Hardware requirements: FRDM i.MX 93 Development Board i.MX 93 Evaluation Kit FRDM i.MX 91 Development Board i.MX 91 Evaluation Kit i.MX95  Steps: 1. Export your project from the folder GUI-Guider-Projects to your Linux PC. Chavira_0-1769722552100.png 2. Build an image for iMX9 using The Yocto Project. Based on iMX Yocto Porject Users Guide set directories and download the repo a. Based on iMX Yocto Porject Users Guide set directories and download the repo $ mkdir imx-bsp-6.6 $ cd imx-bsp-6.6 $: repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-scarthgap -m imx-6.6.52-2.2.0.xml $ repo sync Use distro fsl-imx-xwayland and select machine imx93evk and use this commnad with a build folder name: $ MACHINE=imx93evk DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh - b bld-imx93evk b. Use bitbake command to start the build process. Also, add the -c populate_sdk to get the toolchain. $ bitbake imx-image-full -c populate_sdk  c. Install the Yocto toolchain located on <build-folder>/tmp/deploy/sdk/.  $ sudo sh ./fsl-imx-xwayland-glibc-x86_64-imx-image-full-armv8a-imx93evk-toolchain-6.6-scarthgap.sh d. Install ninja utility on the build host $ sudo apt update $ sudo apt upgrade -y $ sudo apt install ninja-build   3. Once your Yocto SDK has been generated and installed, you can build the required binaries using the script attached to this post.      a) Place the script           Copy the script into the same directory where your meta-gui-guider folder is located.      b) Run the script to build the Gui Guider binary           The script includes several options to rebuild, clean, or use a different toolchain in                case you are working with a Yocto SDK version other than the default one (6.6-scarthgap). Build Options Build the Gui Guider binary using the default Yocto SDK ./guider_1.9_project_builder.sh Build the Gui Guider binary using another Yocto SDK version ./guider_1.9_project_builder.sh -t <yocto_sdk_path>/sysroots/x86_64-pokysdk-linux/usr/share/cmake/armv8a-poky-linux-toolchain.cmake Prepare the source code before building ./guider_1.9_project_builder.sh -p Clean the previous build and recompile (Use -t if needed to specify a different toolchain) ./guider_1.9_project_builder.sh -c   4. The generated Gui Guider binary can be found at the following path: /meta-gui-guider/recipes-graphics/gui-guider/gui-guider/build/gui_guider Copy this binary to your board using either USB or SCP, and then execute it directly on the target device.   Using this method provides the flexibility to modify the source code before compilation. This is important because, by default, some configuration options are not available when using Gui Guider directly or when compiling inside Yocto. If you encounter any issues during this process, please open a new thread so we can assist you. Best regards, Chavira
記事全体を表示
This patch series enables the external 3.3 V and 5 V power rails used by the Raspberry Pi expansion connector on the i.MX93-QSB, i.MX93-FRDM, and i.MX91-FRDM boards. These regulators were already defined in the device tree but left disabled by default. By activating them, the RPI-compatible expansion header can properly power external modules, HATs, and add‑on boards. Changes by board: i.MX93-QSB Enables the 3.3 V and 5 V external supply lines used by the RPI connector.   i.MX93-FRDM Enables the 3.3 V and 5 V external supply lines used by the RPI connector.   i.MX91-FRDM Enables the 3.3 V and 5 V external supply lines used by the RPI connector.   Purpose: Provide proper power to the Raspberry Pi compatible expansion port. Improve hardware compatibility for users attaching external HATs or modules. Align all i.MX9 reference boards to use a consistent power‑tree configuration for the RPI connector.
記事全体を表示