i.MX Processors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX Processors Knowledge Base

Discussions

Sort by:
adv7180 is the 8 bits parallel CSI interface TVin to iMX8QXP validation board. Its weaving mode de-interlace can be supported on both iMX8QXP B0 and C0 chips, but blending mode de-interlace can only work on iMX8QXP C0 chips.   ISL79987 is the 4 virtual channel TVin chip which can input 4 CVBS cameras to iMX8QXP with MIPI CSI2 inteface, it can only work with iMX8QXP C0 chips. The iMX8QXP B0 chips have MIPI CSI2 virtual channel errata.   To test the capture to file: $ /unit_tests/V4L2/mx8_v4l2_cap_drm.out -cam 1 -num 300 -fmt YUYV -of   To test the preview on screen: $ killall weston $ /unit_tests/V4L2/mx8_v4l2_cap_drm.out -cam 1 -fmt RGBP -num 30000   Note: 1. For weaving mode de-interlace, when the ISI is doing de-interlace, it can't do CSC at the same time, so preview will get color issue, because the real output video is always YUYV format. 2. For blending mode de-interlace, it must use ISI0, so for ISL79987, only one camera can use blending mode, the other three cameras are still using weaving mode. The preview color is OK for such use case. 3. The patch is for L4.19.35 BSP.     2019-11-14 update: Add the test application "mx8_v4l2_cap_drm.tar.gz" to support YUYV render to display. Test command to render 4 weaving mode cameras:    ./mx8_v4l2_cap_drm.out -cam 0xF -fmt YUYV -num 30000     2020-04-29 update: Add "0006-isl7998x-fix-the-mipi_bps-overwrite-issue-from-set_f.patch", it fixed the issue that MIPI bps information in isl7998x_data->format.reserved[0] had been overwritten by isl7998x_set_fmt().   2021-06-11 update: Added the patches based on L5.4.70_2.3.0 GA BSP.
View full article
INTRODUCTION REQUIREMENTS CREATE A NEW PROJECT GPU EXAMPLE GSTREAMER EXAMPLE 1. INTRODUCTION:      The below steps show how to create different application examples using Elipse IDE. 2. REQUIREMENTS:      A fully working image and meta-toolchain generated in Yocto . You can follow the  next training: Yocto Training - HOME      Install and configure the Yocto Eclipse Plug-in. For more details about this requirement please refer to Setting up the Eclipse IDE for Yocto Application Development         To demonstrate the steps, L3.14.28  BSP, fsl-image-qt5 image and i.MX6Q SABRE-SDP board were used. 3. CREATE A NEW PROJECT      Follow the section Creating a Hello World Project of this document Setting up the Eclipse IDE for Yocto Application Development 4. GPU EXAMPLE           For this project we use the source code found in the fsl-gpu-sdk that can be downloaded from:      https://www.freescale.com/webapp/Download?colCode=IMX6_GPU_SDK&location=null&Parent_nodeId=1337637154535695831062&Parent…      Follow section 3 and create a new project named gputest.      From the IMX6_GPU_SDK choose one of the examples of GLES2.0 folder. In this case the 01_SimpleTriangle is chosen.      Copy the .c and .h files to the src directory of the gputest project. The Project Explorer window should look like this:              Add the needed files and libraries to compile and link in the Makefile.am file found in the ´src´ folder. The Makefile.am file should have the below content:          bin_PROGRAMS = gputest          gputest_SOURCES = gputest.c fsl_egl.c fslutil.c          AM_CFLAGS = @gputest_CFLAGS@          AM_LDFLAGS = @gputest_LIBS@ -lstdc++ -lm -lGLESv2 -lEGL -lX11 -ldl          CLEANFILES = *~ ​    Add the PATH to CFLAGS where the compiler will look for the headers at Project->Properties->Autotools->configure:           In this project there is no need to add extra PATHs for the headers. Apply the changes by clicking on Reconfigure Project. Build the project To test the file you can send the executable to the board with:           $ scp gputest root@<board_ip>:/home/root      $./gputest      You should get the next output in the display: 5. GSTREAMER EXAMPLE      For this project we use the source code found at Basic tutorial 1: Hello world! - GStreamer SDK documentation - GStreamer SDK documentation    Follow section 3 and create a new project named Gstreamer.    Copy the code of the basic tutorial to your Gstreamer.c file.    Add the needed files and libraries to compile and link in the Makefile.am file found in the ´src´ folder. The Makefile.am file should have the below content:                           bin_PROGRAMS = Gstreamer      Gstreamer_SOURCES = Gstreamer.c      AM_CFLAGS = @Gstreamer_CFLAGS@      AM_LDFLAGS = @Gstreamer_LIBS@ -lstdc++  -lVDK -lm -lGLESv2 -lGAL -lEGL  -ldl -lgstreamer-0.10 -lgobject-2.0 -lgmodule-2.0 -lgthread-2.0 -lrt -lxml2 -lglib-2.0      CLEANFILES = *~         ​    Add the PATH to CFLAGS where the compiler will look for the headers at Project->Properties->Autotools->configure:           For this example the next lines are added             -I${Sysroot}/usr/include/gstreamer-1.0        -I${Sysroot}/usr/include/glib-2.0        -I${Sysroot}/usr/include/libxml2        -I${Sysroot}/usr/lib/glib-2.0/include      Apply the changes by clicking on Reconfigure Project. Build the project To test the file you can send the executable to the board with:           $ scp Gstreamer root@<board_ip>:/home/root To execute the application on the board:      $./Gstreamer The board should have internet access and the application should play the video found at http://docs.gstreamer.com/media/sintel_trailer-480p.webm
View full article
    Xenomai is real-time framework, which can run seamlessly side-by-side Linux as a co-kernel system, or natively over mainline Linux kernels (with or without PREEMPT-RT patch). The dual kernel nicknamed Cobalt, is a significant rework of the Xenomai 2.x system. Cobalt implements the RTDM specification for interfacing with real-time device drivers. The native linux version, an enhanced implementation of the experimental Xenomai/SOLO work, is called Mercury. In this environment, only a standalone implementation of the RTDM specification in a kernel module is required, for interfacing the RTDM-compliant device drivers with the native kernel. You can get more detailed information from Home · Wiki · xenomai / xenomai · GitLab       I have ported xenomai 3.1 to i.MX Yocto 4.19.35-1.1.0, and currently support ARM64 and test on i.MX8MQ EVK board. I did over night test( 5 real-time threads + GPU SDK test case) and stress test by tool stress-ng on i.MX8MQ EVK board. It looks lile pretty good. Current version (20200730) also support i.MX8MM EVK.     You need git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git, and git checkout xenomai-4.19.35-1.1.0-20200818 (which inlcudes all patches and bb file) and add the following variable in conf/local.conf before build xenomai by command bitbake xenomai.  XENOMAI_KERNEL_MODE = "cobalt"  PREFERRED_VERSION_linux-imx = "4.19-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" PREFERRED_VERSION_linux-imx = "4.19-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" If XENOMAI_KERNEL_MODE = "cobalt", you can build dual kernel version. And If XENOMAI_KERNEL_MODE = "mercury", it is single kernel with PREEMPT-RT patch. The following is test result by the command (/usr/xenomai/demo/cyclictest -p 99 -t 5 -m -n -i 1000  -l 100000😞 //Over normal Linux kernel without GPU SDK test case T: 0 ( 4220) P:99 I:1000 C: 100000 Min: 7 Act: 10 Avg: 9 Max: 23 T: 1 ( 4221) P:99 I:1500 C: 66672 Min: 7 Act: 10 Avg: 10 Max: 20 T: 2 ( 4222) P:99 I:2000 C: 50001 Min: 7 Act: 12 Avg: 10 Max: 81 T: 3 ( 4223) P:99 I:2500 C: 39998 Min: 7 Act: 11 Avg: 10 Max: 29 T: 4 ( 4224) P:99 I:3000 C: 33330 Min: 7 Act: 13 Avg: 10 Max: 26 //Over normal Linux kernel with GPU SDK test case T: 0 ( 4177) P:99 I:1000 C: 100000 Min: 7 Act: 10 Avg: 11 Max: 51 T: 1 ( 4178) P:99 I:1500 C: 66673 Min: 7 Act: 12 Avg: 10 Max: 35 T: 2 ( 4179) P:99 I:2000 C: 50002 Min: 7 Act: 12 Avg: 11 Max: 38 T: 3 ( 4180) P:99 I:2500 C: 39999 Min: 7 Act: 12 Avg: 11 Max: 42 T: 4 ( 4181) P:99 I:3000 C: 33330 Min: 7 Act: 12 Avg: 11 Max: 36   //Cobalt with stress-ng --cpu 4 --io 2 --vm 1 --vm-bytes 512M --timeout 600s --metrics-brief T: 0 ( 4259) P:50 I:1000 C:3508590 Min:      0 Act:    0 Avg:    0 Max:      42 T: 1 ( 4260) P:50 I:1500 C:2338831 Min:      0 Act:    1 Avg:    0 Max:      36 T: 2 ( 4261) P:50 I:2000 C:1754123 Min:      0 Act:    1 Avg:    1 Max:      42 T: 3 ( 4262) P:50 I:2500 C:1403298 Min:      0 Act:    1 Avg:    1 Max:      45 T: 4 ( 4263) P:50 I:3000 C:1169415 Min:      0 Act:    1 Avg:    1 Max:      22   //Cobalt without GPU SDK test case T: 0 ( 4230) P:50 I:1000 C: 100000 Min: 0 Act: 0 Avg: 0 Max: 4 T: 1 ( 4231) P:50 I:1500 C:   66676 Min: 0 Act: 1 Avg: 0 Max: 4 T: 2 ( 4232) P:50 I:2000 C:   50007 Min: 0 Act: 1 Avg: 0 Max: 8 T: 3 ( 4233) P:50 I:2500 C:   40005 Min: 0 Act: 1 Avg: 0 Max: 3 T: 4 ( 4234) P:50 I:3000 C:   33338 Min: 0 Act: 1 Avg: 0 Max: 5 //Cobalt with GPU SDK test case T: 0 ( 4184) P:99 I:1000 C:37722968 Min: 0 Act: 1 Avg: 0 Max: 24 T: 1 ( 4185) P:99 I:1500 C:25148645 Min: 0 Act: 1 Avg: 0 Max: 33 T: 2 ( 4186) P:99 I:2000 C:18861483 Min: 0 Act: 1 Avg: 0 Max: 22 T: 3 ( 4187) P:99 I:2500 C:15089187 Min: 0 Act: 1 Avg: 0 Max: 23 T: 4 ( 4188) P:99 I:3000 C:12574322 Min: 0 Act: 1 Avg: 0 Max: 29 //Mercury without GPU SDK test case T: 0 ( 4287) P:99 I:1000 C:1000000 Min: 6 Act: 7 Avg: 7 Max: 20 T: 1 ( 4288) P:99 I:1500 C:  666667 Min: 6 Act: 9 Avg: 7 Max: 17 T: 2 ( 4289) P:99 I:2000 C:  499994 Min: 6 Act: 8 Avg: 7 Max: 24 T: 3 ( 4290) P:99 I:2500 C:  399991 Min: 6 Act: 9 Avg: 7 Max: 19 T: 4 ( 4291) P:99 I:3000 C:  333322 Min: 6 Act: 8 Avg: 7 Max: 21 //Mercury with GPU SDK test case T: 0 ( 4222) P:99 I:1000 C:1236790 Min: 6 Act: 7 Avg: 7 Max: 55 T: 1 ( 4223) P:99 I:1500 C:  824518 Min: 6 Act: 7 Avg: 7 Max: 44 T: 2 ( 4224) P:99 I:2000 C:  618382 Min: 6 Act: 8 Avg: 8 Max: 88 T: 3 ( 4225) P:99 I:2500 C:  494701 Min: 6 Act: 7 Avg: 8 Max: 49 T: 4 ( 4226) P:99 I:3000 C:  412247 Min: 6 Act: 7 Avg: 8 Max: 53 //////////////////////////////////////// Update for Yocto L5.4.47 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.4.47 2.2.0 and it supports i.MX8M series (8MQ,8MM,8MN and 8MP). You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git,  and git checkout xenomai-5.4.47-2.2.0. You need to add the following variable in conf/local.conf before build xenomai by command bitbake imx-image-multimedia.  XENOMAI_KERNEL_MODE = "cobalt"  PREFERRED_VERSION_linux-imx = "5-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" PREFERRED_VERSION_linux-imx = "5-${XENOMAI_KERNEL_MODE}" IMAGE_INSTALL_append += " xenomai" //////////////////////////////////////// Update for Yocto L5.4.70 2.3.0  /////////////////////////////////////////////////////////// New release  for Yocto release L5.4.70 2.3.0 and it supports i.MX8M series (8MQ,8MM,8MN and 8MP) and i.MX8QM/QXP. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.4.70-2.3.0. Updating: 1, Support i.MX8QM and i.MX8QXP 2, Fix altency's the issue which uses legacy API to get time   //////////////////////////////////////// update for Yocto L5.4.70 2.3.2  /////////////////////////////////////////////////////////// New release for Yocto release L5.4.70 2.3.2. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git, and git checkout xenomai-5.4.70-2.3.2. Updating: 1, Enable Xenomai RTDM driver in Linux Kernel 2, Currently CAN, UART, GPIO,  SPI and Ethernet (in debug for RTNet)  are added in Xenomai. 3, Add KERNEL_DEVICETREE += " freescale/imx8mp-rt-evk.dtb " in sources/meta-imx/meta-bsp/conf/machine/imx8mpevk.conf to enable relative device in Xenomai domain, for example rt-imx8mp-flexcan.   //////////////////////////////////////// Update for Yocto L5.4.70 2.3.4  /////////////////////////////////////////////////////////// New release for Yocto release L5.4.70 2.3.4. You need to git clone  https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.4.70-2.3.4. Updating: 1, Enable RTNet FEC driver 2, Currently CAN, UART, GPIO,  SPI and Ethernet ( FEC Controller)  are added in Xenomai. 3, Add KERNEL_DEVICETREE += " freescale/imx8mp-rt-evk.dtb " in sources/meta-imx/meta-bsp/conf/machine/imx8mpevk.conf and KERNEL_DEVICETREE += " freescale/imx8mm-rt-ddr4-evk.dtb " in sources/meta-imx/meta-bsp/conf/machine/imx8mmddr4evk.conf to enable rt_fec device in Xenomai domain. Verifying the network connection by RTnet Ping Between i.MX8M Mini EVK and i.MX8M Plus EVK a, Setup test environment 1, Connect ENET1 of  i.MX8M Plus EVK (used as a master) and  ENET of i.MX8M Mini EVK (used as a slave) of  to a switch or hub 2, Modify /usr/xenomai/etc/rtnet.conf in i.MX8M Plus EVK board as the following: @@ -16,7 +16,7 @@ MODULE_EXT=".ko" # RT-NIC driver -RT_DRIVER="rt_eepro100" +RT_DRIVER="rt_fec" RT_DRIVER_OPTIONS="" # PCI addresses of RT-NICs to claim (format: 0000:00:00.0) @@ -30,8 +30,8 @@ REBIND_RT_NICS="" # The TDMA_CONFIG file overrides these parameters for masters and backup # masters. Leave blank if you do not use IP addresses or if this station is # intended to retrieve its IP from the master based on its MAC address. -IPADDR="10.0.0.1" -NETMASK="" +IPADDR="192.168.100.101" +NETMASK="255.255.255.0" # Start realtime loopback device ("yes" or "no") RT_LOOPBACK="yes" @@ -65,7 +65,7 @@ TDMA_MODE="master" # Master parameters # Simple setup: List of TDMA slaves -TDMA_SLAVES="10.0.0.2 10.0.0.3 10.0.0.4" +TDMA_SLAVES="192.168.100.102" # Simple setup: Cycle time in microsecond TDMA_CYCLE="5000" 3, Modify /usr/xenomai/etc/rtnet.conf in i.MX8M Mini EVK board as the following: @@ -16,7 +16,7 @@ MODULE_EXT=".ko" # RT-NIC driver -RT_DRIVER="rt_eepro100" +RT_DRIVER="rt_fec" RT_DRIVER_OPTIONS="" # PCI addresses of RT-NICs to claim (format: 0000:00:00.0) @@ -30,8 +30,8 @@ REBIND_RT_NICS="" # The TDMA_CONFIG file overrides these parameters for masters and backup # masters. Leave blank if you do not use IP addresses or if this station is # intended to retrieve its IP from the master based on its MAC address. -IPADDR="10.0.0.1" -NETMASK="" +IPADDR="192.168.100.102" +NETMASK="255.255.255.0" # Start realtime loopback device ("yes" or "no") RT_LOOPBACK="yes" @@ -59,13 +59,13 @@ STAGE_2_CMDS="" # TDMA mode of the station ("master" or "slave") # Start backup masters in slave mode, it will then be switched to master # mode automatically during startup. -TDMA_MODE="master" +TDMA_MODE="slave" # Master parameters # Simple setup: List of TDMA slaves -TDMA_SLAVES="10.0.0.2 10.0.0.3 10.0.0.4" +TDMA_SLAVES="192.168.100.102" # Simple setup: Cycle time in microsecond TDMA_CYCLE="5000" 4, rename imx8mm-rt-ddr4-evk.dtb to imx8mm-ddr4-evk.dtb in /run/media/mmcblk1p1,  rename imx8mp-rt-evk.dtb to imx8mp-evk.dtb in /run/media/mmcblk1p1, and reboot board. 5, Run the below command on i.MX8M Mini EVK board. cd /usr/xenomai/sbin/ ./rtnet start & 5, Run the below command on i.MX8M Plus EVK board. cd /usr/xenomai/sbin/ ./rtnet start & When you see the log (rt_fec_main 30be0000.ethernet (unnamed net_device) (uninitialized): Link is Up - 100Mbps/Full - flow control rx/tx) and you can run command "./rtroute" to check route table if the slave IP (192.168.100.102) is in route.. b, Verify the network connection using the command below: ./rtping -s 1024 192.168.100.102 //////////////////////////////////////// Update for Yocto L5.10.52 2.1.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.10.52 2.1.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.10.52-2.1.0. Updating: 1, Upgrade Xenomai to v3.2 2, Enable Dovetail instead of ipipe. Copy xenomai-arm64 to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL_append += " xenomai" Notice: If XENOMAI_KERNEL_MODE = "cobalt", you can build dual kernel version. And If XENOMAI_KERNEL_MODE = "mercury", it is single kernel with PREEMPT-RT patch.  Latency testing of Xenomai3.2+Dovetail with isolating CPU 2,3 ( Xenomai 3.2 on 8MM DDR4 EVK with GPU test case (GLES2/S08_EnvironmentMappingRefraction_Wayland) + iperf3 + 2 ping 65000 size + stress-ng --cpu 2 --io 2 --vm 1 --vm-bytes 256M --metrics-brief )😞 The following is test result by the command (/usr/xenomai/demo/cyclictest -a 2,3 -p 50 -t 5 -m -n -i 1000) root@imx8mmddr4evk:~# /usr/xenomai/demo/cyclictest -a 2,3 -p 50 -t 5 -m -n -i 1000 # /dev/cpu_dma_latency set to 0us policy: fifo: loadavg: 5.96 6.04 6.03 7/155 1349 T: 0 ( 615) P:50 I:1000 C:63448632 Min: 0 Act: 0 Avg: 0 Max: 55 T: 1 ( 616) P:50 I:1500 C:42299087 Min: 0 Act: 0 Avg: 1 Max: 43 T: 2 ( 617) P:50 I:2000 C:31724315 Min: 0 Act: 0 Avg: 1 Max: 51 T: 3 ( 618) P:50 I:2500 C:25379452 Min: 0 Act: 0 Avg: 1 Max: 53 T: 4 ( 619) P:50 I:3000 C:21149543 Min: 0 Act: 0 Avg: 1 Max: 47 //////////////////////////////////////// Update for Yocto L5.10.72 2.2.2  /////////////////////////////////////////////////////////// New release for Yocto release L5.10.72 2.2.2. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.10.72-2.2.2. Updating: 1, Upgrade Xenomai to v3.2.1 Copy xenomai-arm64 to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL_append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL_append += " xenomai" //////////////////////////////////////// Update for Yocto L5.15.71 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L5.15.71 2.2.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git and git checkout xenomai-5.15.71-2.2.0. Updating: 1, Upgrade Xenomai to v3.2.2 Copy xenomai-arm64 to <Yocto folder>/sources/meta-imx/meta-bsp/recipes-kernel, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL:append += " xenomai"   //////////////////////////////////////// Update for Yocto L6.1.55 2.2.0  /////////////////////////////////////////////////////////// New release for Yocto release L6.1.55 2.2.0. You need to git clone https://gitee.com/zxd2021-imx/xenomai-arm64.git recipes-rtlinux-xenomai -b Linux-6.1.x Updating: 1, Upgrade Xenomai to v3.2.4 and support i.MX93 2, Enable EVL (aka Xenomai 4) for i.MX93 and legacy i.MX(6/7D/8X/8M) Copy recipes-rtlinux-xenomai to <Yocto folder>/sources/meta-imx/meta-bsp/, and add the following variable in conf/local.conf before build Image with xenomai enable by command bitbake imx-image-multimedia. XENOMAI_KERNEL_MODE = "cobalt" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "mercury" IMAGE_INSTALL:append += " xenomai" or XENOMAI_KERNEL_MODE = "evl" IMAGE_INSTALL:append += " libevl"  
View full article
GStreamer has a simple feature to enable tracing, allowing the developer to do basic debugging. These can be done in two ways: Adding the parameter --gst-debug=LIST to the pipeline (a pipeline is a executed gst-launch command) Prepending the environment variable GST_DEBUG=LIST' LIST is a a comma-separated argument, indicating the GStreamer elements to trace. For example, if one needs to trace the sink element      $ GST_DEBUG=*sink*:5 gst-launch playbin2 uri=file:///sample.avi or      $ gst-launch playbin2 uri=file:///sample.avi --gst-debug=*sink*:5 Both commands produces the same log. In case want to trace for than one element, so can simple add the <element>:5, for example      $ GST_DEBUG=mfw_v4lsink:5,vpudec:5 gst-launch playbin2 uri=file:///sample.avi The number 5 indicates the log category, where 5 is the highest (the most verbose log you can get) and 0 produces no output (5=LOG, 4=DEBUG, 3=INFO, 2=WARN, 1=ERROR). Log can be huge in each pipeline run. One way to filter it is using the grep command. Before grepping, one needs to redirect the standard error to the standard output (GStreamer log goes always to stderr), so      $ GST_DEBUG=mfw_v4lsink:5,vpudec:5 gst-launch playbin2 uri=file:///sample.avi 2>&1 | grep <filter string> In case the log needs to be shared, it is important to remove the 'color' of the log, again, one just needs to add the parameter --gst-debug-no-color or prepend the env variable GST_DEBUG_NO_COLOR=1 ----- More shell variables that GStreamer react, can be found here https://developer.gnome.org/gstreamer/0.10/gst-running.html
View full article
Here we show how to generate a minimal root filesystem fairly quickly with BusyBox, for the i.MX6 sabre sd platform. This document assumes you are able to boot a Linux kernel on your platform already. See this post for details on how to do it. This implies you already have a "working" Linux development environment with some ARM cross-compilers at hand (e.g. Debian + Emdebian). busybox is so small that we will go for a ramdisk as our main root filesystem. Get busybox sources We will use git to fetch busybox sources:   $ git clone git://git.busybox.net/busybox This should create a busybox directory with all the latest sources. Note that for more stability you might want to checkout a release instead of the latest version; to do so, list the available release tags with e.g. git tag -l, and git checkout <the-desired-tag>. Compile Assuming your cross compiler is called e.g. arm-linux-gnueabihf-gcc, you can compile by doing:   $ cd busybox   $ export ARCH=arm   $ export CROSS_COMPILE=arm-linux-gnueabihf-   $ make defconfig   $ sed -i.orig 's/^#.*CONFIG_STATIC.*/CONFIG_STATIC=y/' .config   $ make   $ make install This should create an _install folder hierarchy containing binaries and links. Note that we force the build of a static binary with the sed command. Configure the root filesystem We need to add some more configuration into the _install folder before we can call it a minimal filesystem. Create some folders We need to create some mountpoints and folders:   $ mkdir _install/dev   $ mkdir _install/proc   $ mkdir _install/sys   $ mkdir -p _install/etc/init.d Add some configuration files and scripts We need to prepare the main init configuration file, _install/etc/inittab, with this contents:   ::sysinit:/etc/init.d/rcS   ::askfirst:/bin/sh   ::ctrlaltdel:/sbin/reboot   ::shutdown:/sbin/swapoff -a   ::shutdown:/bin/umount -a -r   ::restart:/sbin/init This is very close to the default behavior busybox init has with no inittab file. It just suppresses some warnings about missing tty. We need to add some more configuration to mount a few filesystems at boot for convenience. This is done with an _install/etc/fstab file containing:   proc     /proc proc     defaults 0 0   sysfs    /sys  sysfs    defaults 0 0   devtmpfs /dev  devtmpfs defaults 0 0 We also need to actually trigger the mount in the _install/etc/init.d/rcS script, which is called from the inittab. It should contain:   #!/bin/sh   mount -a And we need to make it executable:   $ chmod +x _install/etc/init.d/rcS Generate the ramdisk contents Now that we have adapted the root filesystem contents, we can generate a busybox ramdisk image for u-boot with the following commands:   $ (cd _install ; find |cpio -o -H newc |gzip -c > ../initramfs.cpio.gz)   $ mkimage -A arm -T ramdisk -d initramfs.cpio.gz uInitrd This results in a uInitrd file, suitable for u-boot. Prepare a boot script The default u-boot commands are not sufficient to boot our system, so we need to edit a boot.txt file with the following contents:   run loaduimage   run loadfdt   setenv rdaddr 0x13000000   fatload mmc ${mmcdev}:$mmcpart $rdaddr uInitrd   setenv bootargs console=${console},${baudrate} rdinit=/sbin/init   bootm $loadaddr $rdaddr $fdt_addr Then we generate a boot.scr script, which can be loaded by u-boot with:   $ mkimage -A arm -T script -d boot.txt boot.scr Put on SD card Assuming you have prepared your SD card with u-boot and Linux as explained in this post, you have a single FAT partition on your card with your kernel and dtb. Our boot script and ramdisk image should be copied alongside:   $ mount /dev/<your-sd-card-first-partition> /mnt   $ cp uInitrd boot.scr /mnt/   $ umount /mnt Your SD card first partition is typically something in /dev/sd<X>1 or /dev/mmcblk<X>p1. Note that you need write permissions on the SD card for the command to succeed, so you might need to su - as root, or use sudo, or do achmod a+w as root on the SD card device node to grant permissions to users. Boot! Your SD card is ready for booting. Insert it in the SD card slot of your i.MX6 sabre sd platform, connect to the USB to UART port with a serial terminal set to 115200 baud, no parity, 8bit data and power up the platform. Your busybox system should boot to a prompt:   ...   Freeing unused kernel memory: 292K (806d5000 - 8071e000)   Please press Enter to activate this console. After pressing enter you should have a functional busybox shell on the target. Enjoy! See also... For a more featured root filesystem you might want to try a Debian filesystem in a second SD card partition, as explained in this post, or generate your filesystem with Buildroot. If you plan to compile busybox often, you might want to use a C compiler cache; see this post.
View full article
Dithering Implementation for Eink Display Panel by Daiyu Ko, Freescale Dithering a.          Dithering in digital image processing Dithering is a technique used in computer graphics to create the illusion of color depth in images with a limited color palette (color quantization). In a dithered image, colors not available in the palette are approximated by a diffusion of colored pixels from within the available palette. The human eye perceives the diffusion as a mixture of the colors within it (see color vision). Dithered images, particularly those with relatively few colors, can often be distinguished by a characteristic graininess, or speckled appearance. Figure 1. Original photo; note the smoothness in the detail http://en.wikipedia.org/wiki/File:Dithering_example_undithered_web_palette.png Figure 2.Original image using the web-safe color palette with no dithering applied. Note the large flat areas and loss of detail. http://en.wikipedia.org/wiki/File:Dithering_example_dithered_web_palette.png Figure 3.Original image using the web-safe color palette with Floyd–Steinberg dithering. Note that even though the same palette is used, the application of dithering gives a better representation of the original b.         Applications Display hardware, including early computer video adapters and many modern LCDs used in mobile phonesand inexpensive digital cameras, show a much smaller color range than more advanced displays. One common application of dithering is to more accurately display graphics containing a greater range of colors than the hardware is capable of showing. For example, dithering might be used in order to display a photographic image containing millions of colors on video hardware that is only capable of showing 256 colors at a time. The 256 available colors would be used to generate a dithered approximation of the original image. Without dithering, the colors in the original image might simply be "rounded off" to the closest available color, resulting in a new image that is a poor representation of the original. Dithering takes advantage of the human eye's tendency to "mix" two colors in close proximity to one another. For Eink panel, since it is grayscale image only, we can use the dithering algorism to reduce the grayscale level even to black/white only but still get better visual results. c.          Algorithm There are several algorithms designed to perform dithering. One of the earliest, and still one of the most popular, is the Floyd–Steinberg dithering algorithm, developed in 1975. One of the strengths of this algorithm is that it minimizes visual artifacts through an error-diffusion process; error-diffusion algorithms typically produce images that more closely represent the original than simpler dithering algorithms. (Original) Threshold Bayer   (ordered)                                     Example (Error-diffusion): Error-diffusion dithering is a feedback process that diffuses the quantization error to neighboring pixels. Floyd–Steinberg dithering only diffuses the error to neighboring pixels. This results in very fine-grained dithering. Jarvis, Judice, and Ninke dithering diffuses the error also to pixels one step further away. The dithering is coarser, but has fewer visual artifacts. It is slower than Floyd–Steinberg dithering because it distributes errors among 12 nearby pixels instead of 4 nearby pixels for Floyd–Steinberg. Stucki dithering is based on the above, but is slightly faster. Its output tends to be clean and sharp. Floyd–Steinberg Jarvis,   Judice & Ninke Stucki                         Error-diffusion dithering (continued): Sierra dithering is based on Jarvis dithering, but it's faster while giving similar results. Filter Lite is an algorithm by Sierra that is much simpler and faster than Floyd–Steinberg, while still yielding similar (according to Sierra, better) results. Atkinson dithering, developed by Apple programmer Bill Atkinson, resembles Jarvis dithering and Sierra dithering, but it's faster. Another difference is that it doesn't diffuse the entire quantization error, but only three quarters. It tends to preserve detail well, but very light and dark areas may appear blown out. Sierra Sierra   Lite Atkinson                              2.     Eink display panel characteristic a.       Low resolution Eink only has couple resolution modes for display      DU                  (1bit, Black/White)      GC4                (2bit, Gray scale)      GC16              (4bit, Gray scale)      A2                   (1bit, Black/White, fast update mode) b.      Slow update time For 800x600 panel size (per frame)      DU                  300ms                              GC4                450ms                              GC16              600ms                               A2                   125ms 3.       3.     Effect by doing dithering for Eink display panel a.       Low resolution with better visual quality By doing dithering to the original grayscale image, we can get better visual looking result. Even if the image becomes black and white image, with the dithering algorism, you will still get the feeling of grayscale image. b.      Faster update with Eink’s animation waveform Since the DU/A2 mode could update the Eink panel faster than grayscale mode, with dithering, we can get no only the better visual looking result, but also we can use DU/A2 fast update mode to show animation or even normal video files. 4.       4.     Our current dithering implementation a.       Choose a simple and effective algorism Considering Eink panel’s characteristics, we compared couple dithering algorism and decide to use Atkinson dithering algorism. It is simple and the result is better especially for Einkblack/white display case. b.      Made a lot of optimization so that it will not affect update time too much With the simplicity of the Atkinson dithering algorism, we can also put a lot of effort to do the optimization in order to reduce the dithering processing time and make it practical for actual use. c.       Current algorism performance and result Currently, with Atkinson dithering algorism, our processing time is about 70ms. 5.       5.     Availability a.       We implemented both Y8->Y1 and Y8->Y4 dithering with the same dithering algorism. b.      Implemented into our EPDC driver with i.MX6SL Linux 3.0.35 version release. c.       Also implemented in our Video for Eink demo 6.       6.     References a.       Part of dithering introduction from www.wikipedia.org
View full article
All, This document will help you to understand the " YOCTO PROJECT COMMUNITY LAYERS" and the "YOCTO PROJECT FREESCALE OFFICIAL RELEASE" differences and where the layer content is coming from.   Best Regards, Luis
View full article
1. Description     1) Support HDMI interlaced display mode, the followed format had been verified.         CEA format 5: 1920x1080i @60Hz         CEA format 6&7: 720(1440)x480i @60Hz         CEA format 20: 1920x1080i @50Hz         CEA format 21&22: 720(1440)x576i @50Hz     2) Support LCD interface for interlaced display mode, 1920x1080i @50Hz(CEA format 20)        had been verified. 2. File List -- 0001-IPUv3-support-interlaced-display-mode.patch    Patch to support interlaced display output for iMX6 ipuv3. -- 0002-iMX6-HDMI-support-interlaced-display-mode.patch    Patch to support interlaced display mode for iMX6 HDMI driver. -- 0003-iMX6-LCD-interface-supports-1920x1080i50-mode.patch    Patch to support interlaced display mode for iMX6 LCD interface driver.    -- readme.txt    this file, please refer to it before use the patches 3. Requirement - iMX6 SabreSD board. - L3.0.35_4.1.0_GA_iMX6DQ kernel. 4. How to use -- Copy the patch files to kernel folder.     $ cd ~/ltib/rpm/BUILD/linux-3.0.35/     $ git apply ./0001-IPUv3-support-interlaced-display-mode.patch     $ git apply ./0002-iMX6-HDMI-support-interlaced-display-mode.patch     $ git apply ./0003-iMX6-LCD-interface-supports-1920x1080i50-mode.patch -- Build the new kernel image:     $ cd ~/ltib/rpm/BUILD/linux-3.0.35     $ export CROSS_COMPILE=/opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-fsl-linux-gnueabi-     $ export ARCH=arm     $ make imx6_defconfig     $ make uImage -- Uboot parameters for video mode    Output 1080i50 display mode on HDMI:       "video=mxcfb0:dev=hdmi,1920x1080Mi@25,if=RGB24,bpp=32"    Output 1080i60 display mode on HDMI:       "video=mxcfb0:dev=hdmi,1920x1080Mi@30,if=RGB24,bpp=32"    Output 576i50 display mode on HDMI:       "video=mxcfb0:dev=hdmi,1440x576Mi@25,if=RGB24,bpp=32"    Output 480i60 display mode on HDMI:       "video=mxcfb0:dev=hdmi,1440x480Mi@30,if=RGB24,bpp=32"    Output 1080i50 display mode on LCD interface:       "video=mxcfb0:dev=lcd,LCD-1080I50,if=RGB565,bpp=32"       -- Switch HDMI interlaced mode    $ echo S:1920x1080i-50 > /sys/class/graphics/fb0/mode    $ echo S:1920x1080i-60 > /sys/class/graphics/fb0/mode    $ echo S:1440x480i-50 > /sys/class/graphics/fb0/mode    $ echo S:1440x576i-60 > /sys/class/graphics/fb0/mode 5. Know issue     1) When the interlaced display and another display work on same IPU,        blank and unblank the interlaced display will get the followed IPU        warning, but the display still works due to IPU can revover from the error.     imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_5 = 0x00800000     imx-ipuv3 imx-ipuv3.0: IPU Warning - IPU_INT_STAT_10 = 0x00080000 2015-05-13 update: Replace the fourth patch to make interlace display mode follow CEA-861-specification The patch "0004-IPU-fine-tuning-the-interlace-display-timing-for-CEA.patch" was fine tuned for CEA-861-D specification on interlaced mode display. Please use this patch to replace the old 0004 patch. 2016-05-20 Update: For 3.0.35 BSP, add patch 0005-IPU-update-interlaced-video-mode-parameters-to-align.patch      Align the interlaced video mode parameters to progressive mode. 0006-IPU-update-IDMAC-setting-for-interlaced-display-mode.patch      Udate the IDMAC setting for interlaced display mode, output odd field data from memory first, it aligns with IPU DI timing, odd field first. For 3.14.52 BSP, created the new patch L3.14.52_1.1.0_GA_HDMI_Interlaced_Mode_Patch_2016_05_20.zip.
View full article
INTRODUCTION REQUIREMENTS KERNEL DRIVER DEVICE NODE NFC LIBRARY TESTING NFC READER REFERENCES 1. INTRODUCTION This document is a step by step guide of the AN11697 PN7120 Linux Software Stack Integration Guidelines application note that can be downloaded from http://www.nxp.com/documents/application_note/AN11697.pdf . It explains how to add the PN7120 driver and NFC libraries to a Linux OS running in the i.MX6Q. 2. REQUIREMENTS The board used in this document is the Udoo Board thanks to the easy pin access. More information about this board can be found at Ultimate Single Board Mini PC for Android and Linux - UDOO A modified FSL L3.14.28 BSP. The modifications can be found in these 2 documents Basic Device Tree for the Udoo Board and  U-Boot Migration Example . If you have followed the previous documents, you already have a working yocto image and toolchain (meta-toolchain), if not you must follow this awesome training first Yocto Training - HOME . The OM5577/PN7120S demonstration kit. You can find more details of this board at http://www.nxp.com/documents/user_manual/UM10878.pdf 3. KERNEL DRIVER According to the AN11697.pdf we must follow the below steps: From the Linux source directory: $ cd drivers/misc $ git clone https://github.com/NXPNFCLinux/nxp-pn5xx.git Add the below line in the Makefile of the current directory obj-y += nxp-pn5xx/ Include the driver config in the drivers/misc/Kconfig file source "drivers/misc/nxp-pn5xx/Kconfig" Export the environment variables $ source source /opt/poky/1.7/environment-setup-cortexa9hf-vfp-neon-poky-linux-gnueabi $ export ARCH=arm $ export CROSS_COMPILE=$TARGET_PREFIX $ make imx_v7_defconfig Using menuconfig include the driver as module (<M>).  Compile the modules and install the .ko files into the target rootfs. $ make  modules You can send the .ko files with scp $ make  INSTALL_MOD_PATH=~/Desktop/modules modules_install $ cd ~/Desktop/modules $ sudo scp -r lib/modules/3.14.28+g91cf351/kernel root@<board_ip>:/lib/modules/3.14.28+g91cf351/ 4. DEVICE NODE The PN7120 interfaces with an MCU or MPU via I2C interface, therefore the device must be described into a i2c node. The signals used in the PN7120 are shown below: As you can see besides power, ground and I2C lines, an IRQ and Reset pins are needed. These pins must be configured as GPIO and one must generate an interrupt to the iMX6Q. The chosen connection is shown below: To achieve the above configuration, the device tree must be changed. The changes consist on adding a device node in the corresponding I2C bus, describing the PN7120. &i2c1 {         clock-frequency = <100000>;         pinctrl-names = "default";         pinctrl-0 = <&pinctrl_i2c1>;         status = "okay";         pn547: pn547@28 {                 compatible = "nxp,pn547";                 reg = <0x28>;                 clock-frequency = <400000>;                 interrupt-parent = <&gpio6>;                 interrupt-gpios = <&gpio6 2 0>;                 enable-gpios = <&gpio5 22 0>;         }; }; The pinctrl_i2c1 phandle contains the I2C pins configuration. Make sure that the PADs connected to the PN7120 are not used in other device node. &iomuxc {         imx6q-udoo {                       ...                 pinctrl_i2c1: i2c1grp {                         fsl,pins = <                         MX6QDL_PAD_GPIO_5__I2C3_SCL             0x4001b8b1                         MX6QDL_PAD_GPIO_6__I2C3_SDA             0x4001b8b1                         >;                 };         }; }; After this you can generate the dtb file and send it with scp make dtbs sudo scp arch/arm/boot/dts/imx6q-udoo.dtb root@<board_ip>:/run/media/mmcblk0p1/imx6q-udoo.dtb NOTE: Attached you can find the complete dts and dtsi files used in this document. 5. NFC LIBRARY     To work with the PN7120 in Linux the libnfc-nci stack is needed. You can find more details in http://www.nxp.com/documents/application_note/AN11697.pdf​ . This sections explains how to cross-compile the libray and install the required files in the target (The below steps must be performed in the host). Get the library $  git clone https://github.com/NXPNFCLinux/linux_libnfc-nci.git Generate the configuration script $ ./bootstrap Mount the target rootfs to /mnt in the host. $ sudo mount /dev/sdX2 /mnt Generate the Makefile $ ./configure --host=arm-none-linux --prefix=/opt/poky/1.7/sysroots/x86_64-pokysdk-linux/usr --sysconfdir=/mnt/etc Build and install the source code $ make $ make install After a succesful bulding the libraries and a application demo are built in .libs directory. Copy the libaries to /usr/lib directory of the target and nfcDemoApp to /usr/sbin $ cd linux_libnfc-nci/.libs $ sudo cp * /mnt/usr/lib/ 6. TESTING NFC READER     To test the application you have to follow the below steps on the target: Install the .ko file $ insmod /lib/modules/3.14.28+g91cf351/kernel/drivers/misc/nxp-pn5xx/pn5xx_i2c.ko Run the nfcDemoApp $  nfcDemoApp poll You should get a console output like the shown below when placing a NFC tag next to the NFC reader. 7. REFERENCES     Integrating NFC Controller library with KSDK http://www.nxp.com/documents/application_note/AN11697.pdf http://www.nxp.com/documents/user_manual/UM10878.pdf
View full article
In some cases, i.MX board connect to different module. It has very tiny changes, such as just one gpio different driver strength. We can build an entire new software to handle this requirement. Here we introduce another way, using u-boot to modify the device tree(dtb) at runtime.   Here is u-boot fdt command for  How to use gpio-hog demo https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-gpio-hog-demo/ta-p/1317709   run loadfdt fdt addr ${fdt_addr_r} fdt print /soc/bus/pinctrl/uart3grp fdt rm /soc/bus/pinctrl/uart3grp fdt print serial2 fdt set serial2 status disabled fdt print serial2 fdt print gpio4 fdt resize fdt mknode gpio4 gpio_hog_demo fdt set gpio4/gpio_hog_demo gpio-hog fdt set gpio4/gpio_hog_demo gpios <7 0> fdt set gpio4/gpio_hog_demo output-high fdt print gpio4 run mmcargs run loadimage booti ${loadaddr} - ${fdt_addr_r} root@imx8mmevk:~# cat /sys/kernel/debug/gpio gpiochip0: GPIOs 0-31, parent: platform/30200000.gpio, 30200000.gpio: gpio-5 ( |PCIe DIS ) out hi gpio-13 ( |ir-receiver ) in hi IRQ ACTIVE LOW gpio-15 ( |cd ) in hi IRQ ACTIVE LOW gpiochip1: GPIOs 32-63, parent: platform/30210000.gpio, 30210000.gpio: gpio-38 ( |? ) out hi gpio-42 ( |reset ) out lo ACTIVE LOW gpio-51 ( |regulator-usdhc2 ) out lo gpiochip2: GPIOs 64-95, parent: platform/30220000.gpio, 30220000.gpio: gpio-80 ( |status ) out hi gpiochip3: GPIOs 96-127, parent: platform/30230000.gpio, 30230000.gpio: gpio-117 ( |PCIe reset ) out hi gpiochip4: GPIOs 128-159, parent: platform/30240000.gpio, 30240000.gpio: gpio-135 ( |gpio_hog_demo ) out hi gpio-141 ( |spi1 CS0 ) out hi ACTIVE LOW gpio-149 ( |wlf,mute ) out hi ACTIVE LOW root@imx8mmevk:~# [ 33.758914] VSD_3V3: disabling dtc_utils-v1.6.1-win-x86_64.zip by msys2   
View full article
This document explains how to bring-up u-boot & Linux via JTAG This procedure has been tested on: i.MX6 Solo X Sabre SD i.MX6UL EVK Prerequistes: Get the latest BSP for your board. This procedure was tested with L4.1.15. Build the 'core-image-minimal' image to bring-up your board (Detailed steps here) Optional- Build a meta-toolchain for your device 1.- Set board to boot from Serial dowloader mode or set it to boot from the SD card and remove the sd card We basically want the board to stall in boot ROM to attach to the target. 2.- Connect JTAG probe and turn on the board The device should stall trying to establish a connection to download an image, this will allow us to attach to the target. 3.- Load Device Configuration Data In 'normal' boot sequence the boot ROM takes care of reading the DCD and configuring the device accordingly, but in this case we are skipping this sequence and we need to configure the device manually. The script used by Lauterbach to parse and configure the device is called dcd_interpreter.cmm and can be found here. Search for the package for your specific device. The DCD configuration for your board should be on your u-boot directory: yocto_build_dir/tmp/work/<your board>imx6ulevk/u-boot-imx/<u-boot_version>2016.03-r0/git under board/freescale/<name of your board>mx6ul_14x14_evk/imximage.cfg This file (imximage.cfg) contains all the data to bring up DRAM among other early configuration options. 4.- Load U-boot If an SREC file of U-boot is not present build it (meta-toolchain installed required) the SREC file contains all the information required by the probe to load it and makes this process easier. To build the SREC simply type: make <your board defconfig>mx6ul_14x14_evk_defconfig  (all supported boards are found under u-boot_dir/configs) make If you cannot build an SREC or do not want to, you can use the u-boot.imx (located under yocto_build_dir/tmp/deploy/images/<your board name>/) or u-boot.bin files but you will need to figure out the start address and load address for these files, this can be done by examining the IVT on u-boot.imx (here is a useful document explaining the structure of the IVT). Let U-boot run and you should see its output on the console I will try to boot from several sources but it will fail and show you the prompt. 5.- Create RAMDisk After building the core-image-minimal you will have all the required files under yocto_build_dir/tmp/deploy/images/<your board name>/ You will need: zImage.bin - zImage--<Linux Version>--<your board>.bin Device tree blob - zImage--<Linux Version>--<your board>.dtb Root file system - core-image-minimal-<your board>.rootfs.ext4 We need to create a RAMDisk out of the root file system we now have, these are the steps to do so: Compress current Root file system using gzip: gzip core-image-minimal-<your board>.rootfs.ext4 If you want to keep the original file use: gzip -c core-image-minimal-<your board>.rootfs.ext4 > core-image-minimal-<your board>.rootfs.ext4.gz Create RAMDisk using mkimage: mkimage -A arm -O linux -T ramdisk -C gzip -n core-image-minimal -d core-image-minimal-<your board>.rootfs.ext4.gz core-image-minimal-RAMDISK.rootfs.ext4.gz.u-boot Output: Image Name: core-image-minimal Created: Tue May 23 11:28:55 2017 Image Type: ARM Linux RAMDisk Image (gzip compressed) Data Size: 3017939 Bytes = 2947.21 kB = 2.88 MB Load Address: 00000000 Entry Point: 00000000 Here are some details on mkimage usage Usage: mkimage -l image -l ==> list image header information mkimage [-x] -A arch -O os -T type -C comp -a addr -e ep -n name -d data_file[:data_file...] image -A ==> set architecture to 'arch' -O ==> set operating system to 'os' -T ==> set image type to 'type' -C ==> set compression type 'comp' -a ==> set load address to 'addr' (hex) -e ==> set entry point to 'ep' (hex) -n ==> set image name to 'name' -d ==> use image data from 'datafile' -x ==> set XIP (execute in place) mkimage [-D dtc_options] [-f fit-image.its|-F] fit-image -D => set options for device tree compiler -f => input filename for FIT source Signing / verified boot not supported (CONFIG_FIT_SIGNATURE undefined) mkimage -V ==> print version information and exit 6.- Modify U-boot's environment variables Now we need to modify U-boot's bootargs as follows: setenv bootargs console=${console},${baudrate} root=/dev/ram rw We need to find out the addresses where u-boot will expect the zImage, the device tree and the initial RAMDisk, we can do it as follows: => printenv fdt_addr fdt_addr=0x83000000 => printenv initrd_addr initrd_addr=0x83800000 => printenv loadaddr loadaddr=0x80800000 Where: fdt_addr -> Device tree blob load address initrd_addr -> RAMDisk load address loadaddr -> zImage load address 7.- Load zImage, DTB and RAMDisk Now we know where to load our zImage, device tree blob and RAMDisk, on Lauterbach this can be achieved by running the following commands: Stop the target and execute: data.load.binary zImage.bin 0x80800000 data.load.binary Your_device.dtb 0x83000000 data.load.binary core-image-minimal-RAMDISK.rootfs.ext4.gz.u-boot 0x83800000 Let the device run again and deattach from the device in lauterbach this is achieved by: go SYStem.mode.NoDebug start the boot process on u-boot as follows: bootz ${loadaddr} ${initrd_addr} ${fdt_addr} You should now see the Linux kernel boot process on your terminal: After the kernel boots you should see its prompt on your terminal: Since we are running out of RAM there is no way for us to save u-boot's environment variables, but you can modify the source and compile u-boot with the new bootargs, by doing so you can create a Load script that loads all the binaries hits go and the boot process will continue automatically. One way to achieve this is to modify the configuration file under U-boot_dir/include/configs/<your board>.h find the mfgtool_args and modify accordingly. The images attached to this thread have been modified as mentioned.
View full article
NXP i.MX 8 series of application processors support running ArmV8a 64-bit and ArmV7a 32-bit user space programs.  A Hello World program that prints the size of a long int is cross-compiled as 32-bit and as 64-bit from an Ubuntu host and then each is copied to MCIMX8MQ-EVK and run. Resources: Ubuntu 18.04 LTS Host i.MX 8M Evaluation Kit|NXP  MCIMX8MQ-EVK Linux Binary Demo Files - i.MX 8MQuad EVK L4.9.88_2.0.0_GA release Source Code: Create a file with contents below using your favorite editor, example name hello-sizeInt.c. #include <stdio.h> int main (int argc, char **argv) { printf ("Hello World, size of long int: %zd\n", sizeof (long int)); return 0; }‍‍‍‍‍‍‍ Ubuntu host packages: $ sudo apt-get install -y gcc-arm-linux-gnueabihf $ sudo apt-get install -y gcc-aarch64-linux-gnu‍‍‍‍ Line 1 installs the ArmV7a cross-compile tools: arm-linux-gnueabihf-gcc is used to cross compile on Ubuntu host Line 2 install the ArmV8a cross-compile tools: aarch64-linux-gnu-gcc is used to cross compile on Ubuntu host Create Linux User Space Applications Build each application and use the static option to gcc to include run time libraries. Build ArmV7a 32-bit application: $ arm-linux-gnueabihf-gcc -static hello-sizeInt.c -o hello-armv7a‍-static‍‍ Build ArmV8a 64-bit application: $ aarch64-linux-gnu-gcc -static  hello-sizeInt.c -o hello-armv8a‍-static‍‍ Copy Hello applications from Ubuntu host and run on MCIMX8MQ-EVK Using a SDCARD written with images from L4.9.88_2.0.0 Linux release (see resources for image link), power on EVK with Ethernet connected to network and Serial Console port which was connected to a windows 10 PC. Launched a terminal client (TeraTerm) to access console port. Login credentials: root and no password needed. Since Ethernet was connected a DHCP IP address was acquired, 192.168.1.241 on the EVK.  On the Ubuntu host, secure copy the hello applications to EVK: $ scp hello-armv7a-static root@192.168.1.241:~/ hello-armv7a-static                           100%  389KB   4.0MB/s   00:00    $ scp hello-armv8a-static root@192.168.1.241:~/ hello-armv8a-static                           100%  605KB   4.7MB/s   00:00 ‍‍‍‍‍‍‍‍‍‍ Run: root@imx8mqevk:~# ./hello-armv8a-static Hello World, sizeof long int: 8 root@imx8mqevk:~# ./hello-armv7a-static Hello World, sizeof long int: 4‍‍‍‍‍‍‍‍
View full article
In this article, some experiments are done to verify the capability of i.MX6DQ on video playback under different VPU clocks. 1. Preparation Board: i.MX6DQ SD Bitstream: 1080p sunflower with 40Mbps, it is considered as the toughest H264 clip. The original clip is copied 20 times to generate a new raw video (repeat 20 times of sun-flower clip) and then encapsulate into a mp4 container. This is to remove and minimize the influence of startup workload of gstreamer compared to vpu unit test. Kernels: Generate different kernel with different VPU clock setting: 270MHz, 298MHz, 329MHz, 352MHz, 382MHz. test setting: 1080p content decoding and display with 1080p device. (no resize) 2. Test command for VPU unit test and Gstreamer The tiled format video playback is faster than NV12 format, so in below experiment, we choose tiled format during video playback. Unit test command: (we set the frame rate -a 70, higher than 1080p 60fps HDMI refresh rate)     /unit_tests/mxc_vpu_test.out -D "-i /media/65a78bbd-1608-4d49-bca8-4e009cafac5e/sunflower_2B_2ref_WP_40Mbps.264 -f 2 -y 1 -a 70" Gstreamer command: (free run to get the highest playback speed)     gst-launch filesrc location=/media/65a78bbd-1608-4d49-bca8-4e009cafac5e/sunflower_2B_2ref_WP_40Mbps.mp4 typefind=true ! aiurdemux ! vpudec framedrop=false ! queue max-size-buffers=3 ! mfw_v4lsink sync=false 3. Video playback framerate measurement During test, we enter command "echo performance > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor" to make sure the CPU always work at highest frequency, so that it can respond to any interrupt quickly. For each testing point with different VPU clock, we do 5 rounds of tests. The max and min values are removed, and the remaining 3 data are averaged to get the final playback framerate. #1 #2 #3 #4 #5 Min Max Avg Dec Playback Dec Playback Dec Playback Dec Playback Dec Playback Playback Playback Playback 270M unit test 57.8 57.3 57.81 57.04 57.78 57.3 57.87 56.15 57.91 55.4 55.4 57.3 56.83 GST 53.76 54.163 54.136 54.273 53.659 53.659 54.273 54.01967 298M unit test 60.97 58.37 60.98 58.55 60.97 57.8 60.94 58.07 60.98 58.65 57.8 58.65 58.33 GST 56.755 49.144 53.271 56.159 56.665 49.144 56.755 55.365 329M unit test 63.8 59.52 63.92 52.63 63.8 58.1 63.82 58.26 63.78 59.34 52.63 59.52 58.56667 GST 57.815 55.857 56.862 58.637 56.703 55.857 58.637 57.12667 352M unit test 65.79 59.63 65.78 59.68 65.78 59.65 66.16 49.21 65.93 57.67 49.21 59.68 58.98333 GST 58.668 59.103 56.419 58.08 58.312 56.419 59.103 58.35333 382M unit test 64.34 56.58 67.8 58.73 67.75 59.68 67.81 59.36 67.77 59.76 56.58 59.76 59.25667 GST 59.753 58.893 58.972 58.273 59.238 58.273 59.753 59.03433 Note: Dec column means the vpu decoding fps, while Playback column means overall playback fps. Some explanation: Why does the Gstreamer performance data still improve while unit test is more flat? On Gstreamer, there is a vpu wrapper which is used to make the vpu api more intuitive to be called. So at first, the overall GST playback performance is constrained by vpu (vpu dec 57.8 fps). And finally, as vpu decoding performance goes to higher than 60fps when vpu clock increases, the constraint becomes the display refresh rate 60fps. The video display overhead of Gstreamer is only about 1 fps, similar to unit test. Based on the test result, we can see that for 352MHz, the overall 1080p video playback on 1080p display can reach ~60fps. Or if time sharing by two pipelines with two displays, we can do 2 x 1080p @ 30fps video playback. However, this experiment is valid for 1080p video playback on 1080p display. If for interlaced clip and display with size not same as 1080p, the overall playback performance is limited by some postprocessing like de-interlacing and resize.
View full article
Freescale does not have a specific GStreamer element to do JPEG encoding, so the standard 'jpegenc' should be used. Image Capture With a web camera gst-launch v4l2src num-buffers=1 ! jpegenc ! filesink location=sample.jpeg With an embedded camera gst-launch mfw_v4lsrc num-buffers=1 !  jpegenc ! filesink location=sample.jpeg More pipelines on GStreamer i.MX6 Pipelines
View full article
There is no Freescale GStreamer element which does the JPEG decoding, so we must rely on a standard one, like 'jpegdec'. In case your Linux system was built using LTIB, in order to have the jpegdec element included on the gst-plugin-good, follow these steps: On the LTIB menuconfig, make sure the following packages are selected: gstreamer-plugins-good libjpeg libpng Remove the configure parameters '--disbale-libpng' and '--disable-jpeg' on the file './dist/lfs-5.1/gst-plugins-good/gst-plugins-good.spec' Rebuild and flash your board (or SD card) again. Image display VSALPHA=1 gst-launch filesrc location=sample.jpeg ! jpegdec ! imagefreeze ! mfw_isink Important: non 8 pixel aligned width and height is treated as not supported format in isink plugin.
View full article
  Test environment   i.MX8MP EVK LVDS0 LVDS-HDMI  bridge(it6263) Uboot2022, Uboot2023 Background   Some customers need show logo using LVDS panel. Current BSP doesn't support LVDS driver in Uboot. This patch provides i.MX8MPlus LVDS driver support in Uboot. If you want to connect it to LVDS panel , you need port your lvds panel driver like  simple-panel.c   Update [2022.9.19] Verify on L5.15.32_2.0.0  0001-L5.15.32-Add-i.MX8MP-LVDS-driver-in-uboot 'probe device is failed, ret -2, probe video device failed, ret -19' is caused by below code. It has been merged in attachment. // /* Only handle devices that have a valid ofnode */ // if (dev_has_ofnode(dev) && !(dev->driver->flags & DM_FLAG_IGNORE_DEFAULT_CLKS)) { // /* // * Process 'assigned-{clocks/clock-parents/clock-rates}' // * properties // */ // ret = clk_set_defaults(dev, CLK_DEFAULTS_PRE); // if (ret) // goto fail; // }   [2023.3.14] Verify on L5.15.71 0001-L5.15.71-Add-i.MX8MP-LVDS-support-in-uboot   [2023.9.12] For some panel with low DE, you need uncomment CTRL_INV_DE line and set this bit to 1. #include <linux/string.h> @@ -110,9 +111,8 @@ static void lcdifv3_set_mode(struct lcdifv3_priv *priv, writel(CTRL_INV_HS, (ulong)(priv->reg_base + LCDIFV3_CTRL_SET)); /* SEC MIPI DSI specific */ - writel(CTRL_INV_PXCK, (ulong)(priv->reg_base + LCDIFV3_CTRL_CLR)); - writel(CTRL_INV_DE, (ulong)(priv->reg_base + LCDIFV3_CTRL_CLR)); - + //writel(CTRL_INV_PXCK, (ulong)(priv->reg_base + LCDIFV3_CTRL_CLR)); + //writel(CTRL_INV_DE, (ulong)(priv->reg_base + LCDIFV3_CTRL_CLR)); }       [2024.5.15] If you are uing simple-panel.c, need use below patch to set display timing from panel to lcdif controller. diff --git a/drivers/video/simple_panel.c b/drivers/video/simple_panel.c index f9281d5e83..692c96dcaa 100644 --- a/drivers/video/simple_panel.c +++ b/drivers/video/simple_panel.c @@ -18,12 +18,27 @@ struct simple_panel_priv { struct gpio_desc enable; }; +/* define your panel timing here and + * copy it in simple_panel_get_display_timing */ +static const struct display_timing boe_ev121wxm_n10_1850_timing = { + .pixelclock.typ = 71143000, + .hactive.typ = 1280, + .hfront_porch.typ = 32, + .hback_porch.typ = 80, + .hsync_len.typ = 48, + .vactive.typ = 800, + .vfront_porch.typ = 6, + .vback_porch.typ = 14, + .vsync_len.typ = 3, +}; + @@ -100,10 +121,18 @@ static int simple_panel_probe(struct udevice *dev) return 0; } +static int simple_panel_get_display_timing(struct udevice *dev, + struct display_timing *timings) +{ + memcpy(timings, &boe_ev121wxm_n10_1850_timing, sizeof(*timings)); + + return 0; +} static const struct panel_ops simple_panel_ops = { .enable_backlight = simple_panel_enable_backlight, .set_backlight = simple_panel_set_backlight, + .get_display_timing = simple_panel_get_display_timing, }; static const struct udevice_id simple_panel_ids[] = { @@ -115,6 +144,7 @@ static const struct udevice_id simple_panel_ids[] = { { .compatible = "lg,lb070wv8" }, { .compatible = "sharp,lq123p1jx31" }, { .compatible = "boe,nv101wxmn51" }, + { .compatible = "boe,ev121wxm-n10-1850" }, { } };   [2024.7.23] Update patch for L6.6.23(Uboot2023)
View full article
I've done some research in Android boot optimization in the past months and have some getting. This page is for recording and sharing purpose only. It's target to provide some hints and directions for Android optimization. It's NOT a Freescale official document or patch release. The code/doc inside is only for reference. Background:      1. I've used SabreSD + Android KK 4.4.2 GA 1.0 as a reference platform.      2. I'm not doing some popular optimization way such as "hibernation", "suspend". I'm trying to "optimize" the boot process by re-arranging the boot process and make GUI related process run earlier and fine tune some boot code for running faster.      3. It's target to the Android IVI product. So, some features that will never be used in a IVI environment will be disabled or removed. Minor of them. I've come out with a patch package (latest is milestone 4 which is "_m4" in the version for short) and  a training document. I didn't find any confidential information from the patch or doc, so I'm open the sharing here. Updated on 2016/01/08 for new version (milestone m5): --------------------------------------------------------------------------------------- Change log against previous (milestone 4) version:      1. BSP base changed to Android KK 4.4.3 GA 2.0 which has a Linux kernel 3.10.53      2. Linux kernel and uboot optimization added. Kernel boot time (POR -> Android init entry) is less than 1.5s.      3. Some bug fixes.      4. Document updated accordingly. Total boot time tested on SabreSDP is about 8s.
View full article
Hardware connection: there are two board-to-board connectors on E-INK daughter card IMXEBOOKDC4, while there is only one on i.MX7D Sabre board, as the picture below. This might be a bit confusing to connect the two: Checked with internal, the original design was trying to wire both eLCDIF and EPDC bus out to one daughter card, add the flexibility to have different configurations on one display daughter card(LCD/EPD). On i.MX7D Sabre board, only one connector is available for EPDC bus. Here is how we connect i.MX7D Sabre and IMXEBOOKDC4: Software setup: here we use pre-build L3.14.38_6UL7D_Beta Linux as our boot-image, steps to setup/boot/test EPDC: 1. download and decompress BSP pre-build image package "L3.14.38_beta_images_MX6UL7D.tar.gz", you should be able to find the SD image in it -- "fsl-image-gui-x11-imx7dsabresd.sdcard" 2. program the SD image on your SD card(>800 MBytes) with command(I'm running this in Ubuntu): "dd if=fsl-image-gui-x11-imx7dsabresd.sdcard of=/dev/sdb;sync" 3. insert SD card to the slot(J6) on i.MX7D Sabre board, connect debug-UART and power-on the board 4. modify the u-boot environment variables as below:      a.) setenv fdt_file imx7d-sdb-epdc.dtb           (originally this is "fdt_file=imx7d-sdb.dtb")      b.) setenv mmcargs 'setenv bootargs console=${console},${baudrate} root=${mmcroot} epdc video=mxcepdcfb:E060SCM,bpp=16'           (originally this is "mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot}") 5. boot into Linux kernel, run unit-test: "/unit_tests/mxc_epdc_fb_test.out", should be able to have test patterns running on EPD.
View full article
The D-PHY PLL (in the red circle in the picture below) is the PLL that drives the MIPI Clock lane. It must be set in accordance with the video to be sent to the display.   Calculating the video bandwidth The video bandwidth is calculated with the following equation: Pixels per second = Horizontal res. x Vertical res. x Frame rate x Bits per pixel Taking as example the 1080p60 OLED display RM67191: Pixels per second = 1920 x 1080 x 60 x 24 Pixels per second = 2985984000 = 2,98Gpixels/sec Pixel clock calculation The Display pixel clock can be obtained on the display driver. In this example for RM67191, the pixel clock is 132Mpixel/sec, see file: panel-raydium-rm67191.c\panel\drm\gpu\drivers - linux-imx - i.MX Linux kernel  Line 530: .pixelclock = { 66000000, 132000000, 132000000 }, Or the number can be obtained with the following equation: pixel clock = (hactive + hfront_porch + hsync_len + hback_porch) x (vactive + vfront_porch + vsync_len + vback_porch) x frame rate pixel clock = (1080 + 20 + 2 +34) × (1920 + 10 + 2 + 4) x 60 pixel clock = 132000000 (rounded up) Bit clock calculation (clock lane) The mipi-dphy bit_clk is the output clock and is calculated on file sec-dsim.c (line 1283): sec-dsim.c\bridge\drm\gpu\drivers - linux-imx - i.MX Linux kernel  Bit clock can be calculated with the following equation: bit_clk = Pixel clock * Bits per pixel / Number of lanes In the case of 1980p60 (Raydium display), It is:   bit_clk = pixel clock * bits per pixel / number of lanes bit_clk = 132000000 * 24 / 4 bit_clk = 792000000 Other important timing parameters like 'p', 'm', 's' are obtained on the table in the following header file: sec_mipi_dphy_ln14lpp.h\imx\drm\gpu\drivers - linux-imx - i.MX Linux kernel 
View full article
It is based on 3.0.35 GA 4.1.0 BSP.   0001-Correct-mipi-camera-virtual-channel-setting-in-ipu_c.patch It is the updated IPU code for MIPI ID and SMFC setting in ipu_capture.c. These setting should not be combined with MIPI virtual channel value, they shoule be fixed with ID 0.   0002-Use-virtual-channel-3-for-ov5640-mipi-camera-on-iMX6.patch The sample code to modify ov5640_mipi camera to use virtual channel 3 on SabreSD board.   The followed command can be used to verify the mipi camera function after booted into Linux: $ gst-launch mfw_v4lsrc capture-mode=1 device=/dev/video1 ! mfw_v4lsink     2014-09-30 update: Added the patch for 3.10.17_GA1.0.0 BSP. "L3.10.17_1.0.0_mipi_camera_virtual_channel_3.zip"  
View full article