The purpose of this document is to provide supportive information for selection of suitable LPDDR4, DDR4 and DDR3L devices that are supported by i.MX 8M family of processors to aid project feasibility assessment capabilities of customers that are evaluating the SoCs for usage in their products.
It is strongly recommended to consult with NXP and the memory vendor the final choice of the memory part number to ensure that the device meets all the compatibility, availability, longevity and pricing requirements.
Please note that some of the LPDDR4 devices may not support operation at low speeds and in addition, DQ ODT may not be active, which can impact signal integrity at these speeds. If low speed operation is planned in the use case, please consult with the memory vendor the configuration aspects and possible customization of the memory device so correct functionality is ensured.
In all cases, it is strongly recommended to follow the DRAM layout guidelines outlined in the NXP Hardware Developer's Guides for the specific SoCs available on NXP.com
Memory devices with binary densities (e.g., 1 GB, 2 GB, 4 GB) are preferred because they simplify memory management by aligning with system addressing schemes and reducing software complexity.
For any questions related to specific DRAM part numbers please contact the respective DRAM vendor. For any questions regarding the i.MX SoC please contact your support representative or enter a support ticket.
LPDDR4 - maximum supported densities
Please note that the SoCs only support memory devices that support either the LPDDR4 mode or support both LPDDR4 and LPDDR4X modes. Memory devices that support only the LPDDR4X mode are not supported.
SoC
Max data bus width
Maximum density
Assumed memory organization
Notes
i.MX 8M Quad
32-bit
32Gb/4GB
dual rank, dual-channel device with 16-row addresses (R0-R15)
1, 2, 4
i.MX 8M Mini
32-bit
64Gb/8GB
dual rank, dual-channel device with 17-row addresses (R0-R16)
1, 2
i.MX 8M Nano
16-bit
32Gb/4GB
dual rank, single-channel device with 17-row addresses (R0-R16)
1, 2, 3, 12
i.MX 8M Plus
32-bit
64Gb/8GB
dual rank, dual-channel device with 17-row addresses (R0-R16)
1, 2
LPDDR4 - list of validated memories
Please note that the validation process is an ongoing effort - regular updates of the table are expected. Please contact NXP if a specific vendor or configuration is required.
SoC
Density
Validated part number
Vendor
Notes
i.MX 8M Quad
24Gb/3GB
MT53B768M32D4NQ-062 WT:B
Micron
15
32Gb/4GB
MT53D1024M32D4DT-046 AAT:D
Micron
14
4Gb/512MB
IS43LQ16256B-062BLI
ISSI
5, 14
8Gb/1GB
IS43LQ32256B-062BLI
ISSI
5, 14
i.MX 8M Mini
16Gb/2GB
MT53D512M32D2DS-053 WT:D
Micron
15
16Gb/2GB
M56Z16G32512A
ESMT
5, 14
32Gb/4GB
MT53E1G32D2FW-046 WT:A
Micron
5, 14
64Gb/8GB
MT53E2G32D4DT-046 AIT:A
Micron
5, 14
32Gb/4GB
B3221PM3BDGUI -U
Kingston
5
i.MX 8M Nano
16Gb / 2GB
C1612PC2WDGTKR-U
Kingston
15
16Gb / 2GB
D1611PM3BDGUI-U
Kingston
5,14
32Gb / 4GB
MT53E2G32D4DT-046 AIT:A
Micron
5, 13, 15
16Gb / 2GB
IMAG16L4KBB
Intelligent Memory (IM)
5,14
4Gb / 512MB
NT6AN256M16AV-J2
Nanya
5,14
4Gb / 512MB
W66CP6RBQAHJ
Winbond
5,14
8Gb / 1GB
IS43LQ16512A-053BLI
ISSI
5,14
8Gb / 1GB
MT53D512M32D2DS-053 WT:D
Micron
13, 15
i.MX 8M Plus
48Gb/6GB
MT53E1536M32D4DT-046 WT:A
Micron
15
64Gb/8GB
MT53E2G32D4DE-046 AUT:C
Micron
5, 14
32Gb/4GB
K4FBE3D4HB-KHCL
Samsung
5, 14
32Gb/4GB
D1611PM3BDGUI-U
Kingston
5, 14
64Gb/8GB
Q6422PM3BDGVK-U
Kingston
5, 14
8Gb/1GB
W66DP2RQQAHJ
Winbond
5, 14
32Gb/4GB
IS46LQ32K01S2A-046BLA2
ISSI
5, 14
32Gb/4GB
IS43LQ32K01S2A-046BLI
ISSI
5,14
LPDDR4 - list of incompatible devices
Given the limitations mentioned in this document, the following memory devices were identified as incompatible with the particular SoCs as detailed in the following table:
Memory vendor
Part Number
Density
Incompatible SoCs
Incompatibility reason
Samsung
K4FHE3S4HA-KU(H/F)CL
24Gb/3Gb
i.MX 8M Quad
The memory device requires 17th row address bit to function.
Samsung
K4UHE3S4AA-KU(H/F)CL
K4UJE3D4AA-KU(H/F)CL
24Gb/3Gb
48Gb/6GB
i.MX 8M Quad
i.MX 8M Mini
i.MX 8M Nano
i.MX 8M Plus
The memory device only supports the LPDDR4X mode.
Samsung
K4FCE3Q4HB-KU(H/F)CL
K4UCE3Q4AB-KU(H/F)CL
64Gb/8GB
i.MX 8M Quad
i.MX 8M Mini
i.MX 8M Nano
i.MX 8M Plus
A byte mode memory device.
The memory device only supports the LPDDR4X mode.
DDR4 - maximum supported densities
SoC
Max data bus width
Maximum density
Assumed memory organization
Notes
i.MX 8M Quad
32-bit
32Gb/4GB
x16, 16Gb device with 1 bank group address, 17-row addresses and 10 column addresses
1, 6
i.MX 8M Mini
32-bit
64Gb/8GB
x16, 16Gb device with 1 bank group address, 17-row addresses and 10 column addresses
1, 7
i.MX 8M Nano
16-bit
64Gb/8GB
x8, 16Gb device with 2 bank group addresses, 17-row addresses and 10 column addresses
1, 8
i.MX 8M Plus
32-bit
64Gb/8GB
x16, 16Gb device with 1 bank group address, 17-row addresses and 10 column addresses
1, 7
DDR4 - list of validated memories
Please note that the validation process is an ongoing effort - regular updates of the table are expected. Please contact NXP if a specific vendor or configuration is required.
SoC
Density
Vendor
Validated part number
Notes
i.MX 8M Quad
32Gb/4GB
Micron
4x MT40A512M16JY-083EAAT
15
i.MX 8M Mini
16Gb/2GB
Micron
2x MT40A512M16LY-075:E
15
i.MX 8M Nano
16Gb/2GB
Micron
1x MT40A1G16RC-062E:B
15
i.MX 8M Plus
64Gb/8GB
Micron
4x MT40A1G16RC-062E:B
15
16Gb/2GB
Nanya
NT5AD512M16C4-JRI
14
DDR3L - maximum supported densities
SoC
Max data bus width
Maximum density
Assumed memory organization
Notes
i.MX 8M Quad
32-bit
32Gb/4GB
x16, 8Gb device with 16-row addresses and 10 column addresses
1, 9
i.MX 8M Mini
32-bit
64Gb/8GB
x8, 8Gb device with 16-row addresses and 11 column addresses
1, 10
i.MX 8M Nano
16-bit
32Gb/4GB
x8, 8Gb device with 16-row addresses and 11 column addresses
1, 11
i.MX 8M Plus
i.MX 8M Plus does not support DDR3L
DDR3L - list of validated memories
Please note that the validation process is an ongoing effort - regular updates of the table are expected. Please contact NXP if a specific vendor or configuration is required.
SoC
Density
Vendor
Validated part number (vendor)
Notes
i.MX 8M Quad
16Gb/2GB
Micron
4x MT41K256M16TW-107 AAT
14
i.MX 8M Mini
16Gb/2GB
Micron
4x MT41K256M16TW-107 AAT
14
i.MX 8M Nano
8Gb/1GB
Micron
MT41K512M16VRN-107
15
Note 1:
The numbers are based purely on the IP vendor documentation for the DDR Controller and the DDR PHY, on the settings of the implementation parameters chosen for their integration into the SoC, and on the JEDEC standards JESD209-4/JESD209-4A (LPDDR4), JESD279-4/JESD279-4A (DDR4), and JESD79-3E/JESD79-3F/JESD79-3-1A (DDR3/DDR3L). Therefore, they are not backed by validation, unless said otherwise and there is no guarantee that an SoC with the specific density and/or desired internal organization is offered by the memory vendors. Should the customers choose to use the maximum density and assume it in the intended use case, they do it at their own risk.
Note 2:
Byte-mode LPDDR4 devices (x16 channel internally split between two dies, x8 each) of any density are not supported therefore, the numbers are applicable only to devices with x16 internal organization (referred to as "standard" in the JEDEC specification).
Note 3:
The memory vendors often do not offer so many variants of single-channel memory devices. As an alternative, a dual-channel device with only one channel connected may be used. For example:
A dual-rank, single-channel device with 16-row address bits has a density of 16Gb. If such a device is not available at the chosen supplier, a dual-rank, dual-channel device with 16-row address bits can be used instead. This device has a density of 32 Gb however since only one channel can be connected to the SoC, only half of the density is available (16 Gb).
Usage of more than one discrete memory chips to overcome market constraints is not supported since only point-to-point connections are assumed for LPDDR4.
Note 4:
Devices with 17-row addresses (R0-R16) are not supported by the DDR Controller
Note 5:
The memory part number did not undergo full JEDEC verification however, it passed all functional testing items.
Note 6:
The density can be achieved by connecting 2 single-rank discrete devices with one 16Gb die each. Since the SoC supports x8 devices and also has connectivity for a second rank, usage of more discrete devices is possible. However, this advantage cannot be used to get higher density since this SoC has only 32Gb/4GB of address space dedicated for the DDR. Two x16 16Gb devices giving 32Gb/4GB in total is, therefore, the optimal choice that balances the maximum density aspects, the signal integrity aspects (only two discrete devices used), and bandwidth aspects (full data bus width used).
Note 7:
The density can be achieved by connecting 4 single rank discrete devices with one 16Gb die each, 2 devices connected to each chip select. Since the SoC supports x8 devices, the usage of more discrete devices is possible. However, this advantage cannot be used to get higher density since this SoC has only 64Gb/8GB of address space dedicated for the DDR. Four x16 16Gb devices giving 64Gb/8GB in total is the optimal choice that balances the maximum density aspects, the signal integrity aspects (only four discrete devices used), and the bandwidth aspects (full data bus width used).
Note 8:
The density can be achieved by connecting 4 single rank discrete devices with one 16Gb die each, 2 devices connected to each chip select.
Note 9:
The density can be achieved by connecting 4 single rank discrete devices with one 8Gb die each, 2 devices connected to each chip select, or by connecting 2 dual rank discrete devices with two 8Gb dies each. Since the SoC supports x8 devices, the usage of more discrete devices is possible. However, this advantage cannot be used to get higher density since this SoC has only 32Gb/4GB of address space dedicated for the DDR. Four x16 8Gb devices giving 32Gb/4GB in total is, therefore, the optimal choice that balances the maximum density aspects, the signal integrity aspects (four discrete devices used), and bandwidth aspects (full data bus width used).
Note 10:
The density can be achieved by connecting 8 single rank discrete devices with one 8Gb die each, 4 devices connected to each chip select or by connecting 4 dual rank discrete devices with two 8Gb dies each. Note that the first option significantly exceeds the number of devices used on the validation board (4 discrete devices) therefore, it is not guaranteed that the i.MX would be able to drive the signals with margin to the required voltage levels due to increased loading on the traces. A significant effort would be required in terms of PCB layout and signal integrity analysis. Practically, it is not recommended to use more than 4 discrete DDR3L devices. This corresponds to the maximum density of 32Gb/4GB in the case of the single rank devices containing one 8Gb die or 64Gb/8GB in case of the dual-rank devices, each containing two 8Gb dies.
Note 11:
The density can be achieved by connecting 4 single rank discrete devices with one 8Gb die each, 2 devices connected to each chip select or by connecting 2 dual rank discrete devices with two 8Gb dies each.
Note 12:
For single-channel (x16) memory devices, the current maximum available density in the market is 16Gb/2GB (Q1 2022).
Note 13:
Only one channel of the device (and hence, half of its density) was utilized due to the reduced data bus width (x16) of the SoC.
Note 14:
Part is active. Reviewed Nov 2025
Note 15:
Part will either EoL or is not recommended for new designs by the respective vendor.
Additional Links
https://community.nxp.com/t5/iMX-and-Vybrid-Support/i-MX-8-8X-8XL-maximum-supported-LPDDR4-and-DDR3L-densities/ta-p/1152715
記事全体を表示