i.MX处理器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX Processors Knowledge Base

讨论

排序依据:
Android Power Debug and Optimization Introduction Android Power Management on i.MX Overview How to do power optimization for Android on i.MX How to check high power consumption on i.MX How to debug suspend/resume problems on i.MX Introduction This document describes i.MX Android power issues debug and power consumption optimization. Android Power Management on i.MX Overview What Power Manager introduced by Android • Early Suspend    It is allow drivers like LCD, keypad backlight, touch-screen, gsensor, to be notified when user-space writes to /sys/power/request_state to indicate that the user visible sleep state should change. These drivers will act as like Linux stand suspend() to let these devices entry in suspend for better battery life. •Late Resume    Late resume is matching with early suspend. It will resume the devices suspended during early suspend after the Stand Linux resume finished •Wake Locks     Wake locks are used by applications, services, kernel drivers to request CPU resources. A locked wakelock, depending on its type, prevents the system from entering suspend or other low-power states. It as a core member in android power management architecture from framework to kernel What introduced by i.MX to enhance the power framework BusFreq Support High bus, Low power audio bus and Low bus totally 3 system bus working points. Switching between these 3 bus mode according clock flags automatically. DDR running frequency will change according bus mode changing (highest 528/400MHz and lowest at 24MHz for MX6DQ/DL). CPUFreq The CPU frequency scaling device driver allows the clock speed of the CPUs to be changed on the fly. Once the CPU frequency is changed, the GP voltage will be changed to the voltage value. Enhance the default interactive governor for better performance on SDHC/GPU etc. System Power Profile Service and App (just for MX6DQ/DL) Support 3 profiles currently: Normal mode, Power Saving Mode and Performance Mode to get much better balance between performance and power consumption. Profiles can be customized according customers’ HW /MD design, including: CPU running max freq, trigger temperature, CPU running minimal freq, running cpu LDO bypass mode           i.MX6X has built-in LDO module, but also allows you to use external LDO suppliers. SW will provide the configuration using external LDO or internal LDO. How to do power optimization for Android on i.MX Suspend Mode All devices enter in suspend or low power Config GPIO PADs as High Z or input mode (depending on HW design,FSL provide Ref code) Cut off LDOs which no modules need (depending on HW design, FSL provide Ref code) DDR enter in self-refresh mode (FSL done) Config DDR IO Float pin to reduce the DDR IO consumption (FSL done) ARM core entry stop mode (WFI) (FSL done) All PLLs will cut off, just 32KHZ sleep clock living (FSL done) Notify the PMIC entry in standby to save some power (FSL done) User Idle Mode Optimization on device driver for WiFi, 3G, BT, screen brightness modules, etc., to save some power Let some device/GPIOs entry in suspend mode/low power mode Active power saving profile to reduce some system power loading. GPU 2D/3D auto entry in Stop/Standby mode if no activity needs update. (FSL done) Enable CPUFreq reduce ARM CORE power consumption (FSL done) Busfreq scanning to let system work at lower Freq to save power (FSL done) Audio/Video Playback Mode Optimization on device driver for WiFi, 3G, BT, screen brightness modules, etc., to save some power Let some device/GPIOs entry in suspend mode/low power mode Disable HW 3D acceleration for some Apps such as System UI, Music Player, etc., to save some power when System in IDLE or music playing mode. Enable CPUFreq and SOC WAIT mode, decrease CPU Freq/Voltage to save power for ARM CORE when no there is no task need cpu to handle(FSL done) Busfreq scanning will set bus work at low power audio bus mode to save some power (FSL done for audio case) DDR enter in self-refresh mode (FSL done for audio case) Reduce the screen brightness will save some power (for video case) VPU clock auto-gating to save power on SOC domain (for video case, FSL done) GPU 2D/3D auto-gating to save some power on SOC domain (FSL done) Try VDOA+IPU to bypass GPU in video playback(not comment for Android platform, pure Linux environment using this method, for it has some limitation such as the input/output size limit), this can save some power on DDR domain. How to check high power consumption on i.MX Idle Audio/Video Playback high power consumption Check the CPUFreq and  Bus_freq is enabled           cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor           cat /sys/devices/platform/imx_busfreq.0/enable Check whether the system bus working poing   For MX6Q:           cat /sys/kernel/debug/clock/osc_clk/pll2_528_bus_main_clk/periph_clk/mmdc_ch0_axi_clk/rate   For MX6DL/SL:           cat /sys/kernel/debug/clock/osc_clk/pll2_528_bus_main_clk/pll2_pfd_400M/periph_clk/mmdc_ch0_axi_clk/rate Check CPU Loading and Interrupt(cat /proc/interrupts) Check clock tree carefully to see which clocks arenot gated off  but no any modules need them.            powerdebug –d  -c SUSPEND MODE high power consumption Make sure all device entries are in suspend mode Make sure the system entry in DSM(measure the voltage &current of VDDARM_CAP, VDDSOC_CAP,DDR_1V5, VDD_HIGH…)      Some tips help to locate the problems Add debug message in device drivers which may lead high power consumption Enable PM debug in kernel Catch the waveform from these modules which may impact the high power consumption Remove devices from the board or do H/W rework to exclude some H/W problems How to debug suspend/resume problems on i.MX System could not entry in suspend mode Check below settings has been disabled: GPS has been disabled Don't connect USB cable to the board (adb will hold a wake lock) RIL will hold a wake lock if RIL failed to initialize (logcat -b radio) Setting->Application->Developer options->stay awake (stay awake not set) Check all wake locks which holed by kernel have been released          echo 15 > /sys/module/wakelock/parameters/debug_mask Check all user wake locks have been releaed          echo 15 > /sys/module/userwakelock/parameters/debug_mask System hang when resume or suspend Enable PM debug system to get more info about PM in kernel     make menuconfig  enable the PM debug sys [*] Power Management support                                                           [*]   Power Management Debug Support                                                           [*]     Verbose Power Management debugging Add no_console_suspend to the boot option for kernel         This makes the system print more useful info before entry in suspend Check the PMIC_STBY_REQ signal. Measure the VDDARM_IN Using Trace32 or ICE to locate the problem. Using RAMCONSOLE to dump the kernel log after reboot. Kernel resume back from suspend  but Android not    This is usually because of the wrong key layout file Use tool to get power key scan code        getevent  Correct the Keylayout         system/usr/keylayout/****.kl Correct the scandcode with your power key report value to Match the POWE key
查看全文
Description about VPU & IPU usage in Android R13.4 GA release for i.MX6DQ
查看全文
In this article, some experiments are done to verify the capability of i.MX6DQ on video playback under different VPU clocks. 1. Preparation Board: i.MX6DQ SD Bitstream: 1080p sunflower with 40Mbps, it is considered as the toughest H264 clip. The original clip is copied 20 times to generate a new raw video (repeat 20 times of sun-flower clip) and then encapsulate into a mp4 container. This is to remove and minimize the influence of startup workload of gstreamer compared to vpu unit test. Kernels: Generate different kernel with different VPU clock setting: 270MHz, 298MHz, 329MHz, 352MHz, 382MHz. test setting: 1080p content decoding and display with 1080p device. (no resize) 2. Test command for VPU unit test and Gstreamer The tiled format video playback is faster than NV12 format, so in below experiment, we choose tiled format during video playback. Unit test command: (we set the frame rate -a 70, higher than 1080p 60fps HDMI refresh rate)     /unit_tests/mxc_vpu_test.out -D "-i /media/65a78bbd-1608-4d49-bca8-4e009cafac5e/sunflower_2B_2ref_WP_40Mbps.264 -f 2 -y 1 -a 70" Gstreamer command: (free run to get the highest playback speed)     gst-launch filesrc location=/media/65a78bbd-1608-4d49-bca8-4e009cafac5e/sunflower_2B_2ref_WP_40Mbps.mp4 typefind=true ! aiurdemux ! vpudec framedrop=false ! queue max-size-buffers=3 ! mfw_v4lsink sync=false 3. Video playback framerate measurement During test, we enter command "echo performance > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor" to make sure the CPU always work at highest frequency, so that it can respond to any interrupt quickly. For each testing point with different VPU clock, we do 5 rounds of tests. The max and min values are removed, and the remaining 3 data are averaged to get the final playback framerate. #1 #2 #3 #4 #5 Min Max Avg Dec Playback Dec Playback Dec Playback Dec Playback Dec Playback Playback Playback Playback 270M unit test 57.8 57.3 57.81 57.04 57.78 57.3 57.87 56.15 57.91 55.4 55.4 57.3 56.83 GST 53.76 54.163 54.136 54.273 53.659 53.659 54.273 54.01967 298M unit test 60.97 58.37 60.98 58.55 60.97 57.8 60.94 58.07 60.98 58.65 57.8 58.65 58.33 GST 56.755 49.144 53.271 56.159 56.665 49.144 56.755 55.365 329M unit test 63.8 59.52 63.92 52.63 63.8 58.1 63.82 58.26 63.78 59.34 52.63 59.52 58.56667 GST 57.815 55.857 56.862 58.637 56.703 55.857 58.637 57.12667 352M unit test 65.79 59.63 65.78 59.68 65.78 59.65 66.16 49.21 65.93 57.67 49.21 59.68 58.98333 GST 58.668 59.103 56.419 58.08 58.312 56.419 59.103 58.35333 382M unit test 64.34 56.58 67.8 58.73 67.75 59.68 67.81 59.36 67.77 59.76 56.58 59.76 59.25667 GST 59.753 58.893 58.972 58.273 59.238 58.273 59.753 59.03433 Note: Dec column means the vpu decoding fps, while Playback column means overall playback fps. Some explanation: Why does the Gstreamer performance data still improve while unit test is more flat? On Gstreamer, there is a vpu wrapper which is used to make the vpu api more intuitive to be called. So at first, the overall GST playback performance is constrained by vpu (vpu dec 57.8 fps). And finally, as vpu decoding performance goes to higher than 60fps when vpu clock increases, the constraint becomes the display refresh rate 60fps. The video display overhead of Gstreamer is only about 1 fps, similar to unit test. Based on the test result, we can see that for 352MHz, the overall 1080p video playback on 1080p display can reach ~60fps. Or if time sharing by two pipelines with two displays, we can do 2 x 1080p @ 30fps video playback. However, this experiment is valid for 1080p video playback on 1080p display. If for interlaced clip and display with size not same as 1080p, the overall playback performance is limited by some postprocessing like de-interlacing and resize.
查看全文