Introduction
LVGL is a graphics library to run on devices using a limited amount of resources.
Previously, we have ran an LVGL demo from the LVGL repository, this contains a couple more demos which all of them are pieces of code included and lends us the opportunity to evaluate the library in a quick and easy way.
GUI projects are developed by customers through a lot more options than bare code, there are GUI tools that translate a graphic asset into LVGL code, in this demonstration we will use a tool that's widely used in MCU GUI development and translate the GUI created into LVGL code; SquareLine.
NOTE: refer to the appendix for precedent LVGL documents on i.MX series processors.
HW set-up
i.MX 93 EVK boot over eMMC/uSD to Linux Factory or Ubuntu.
Connect power and debug receptables.
Connect MX8_DSI_OLED1 to J701 (MIPI DSI) through MiniSAS cable.
SquareLine set-up
Download the latest version of SquareLine under the following link according to your host system.
JosephAtNXP_0-1732571954892.png
NOTE: This document is intended for demonstration of templates included within the tool, so it's recommended to download a free trial, for formal development please refer to the appendix of this document.
Unzip and execute the installer, this is the windows prompt.
JosephAtNXP_1-1732571954893.png
Demo download
After setting SquareLine up go to the example section, we will demonstrate the thermostat capabilities with the Thermostat Demo.
JosephAtNXP_2-1732571954894.png
We can directly export these UI files and they would be graphically ready to be build, click on Export -> Export UI Files and select your preferred destination to save these.
JosephAtNXP_3-1732571954894.png
LVGL setup. Option 1 Fresh Environment
Clone LVGL and LV_DRIVERS repositories, this is a .gitmodules file that points to the specific branches needed.
[submodule "lvgl"]
path = lvgl
url = https://github.com/lvgl/lvgl.git
branch = release/v8.3
[submodule "lv_drivers"]
path = lv_drivers
url = https://github.com/lvgl/lv_drivers.git
branch = release/v8.3
NOTE: If you are using other methods, you should point to these commits, lv_drivers @ 8cdabe8 and lvgl @ f2c1032.
Gather the necessary files described below from the LVGL Linux Port example found here.
Makefile
lv_conf.h
lv_drv_conf.h
main.c
mouse_cursor_icon.c
Patch the Makefile.
+ include $(LVGL_DIR)/thermostat/thermostat.mk
Patch the lv_drv_conf.h
# define EVDEV_NAME "/dev/input/event10" /*You can use the "evtest" Linux tool to get the list of devices and test them*/
+# define EVDEV_NAME "/dev/input/event<Number>"
NOTE: This changes according to the output of # evtest.
Patch lv_conf.h
-#define LV_FONT_MONTSERRAT_20 0
+#define LV_FONT_MONTSERRAT_20 1
Patch the main.c
- disp_drv.hor_res = 800;
- disp_drv.ver_res = 480;
+ disp_drv.hor_res = 1080;
+ disp_drv.ver_res = 1920;
…
- /*Create a Demo*/
- lv_demo_widgets();
+ /*Create a Squareline Demo*/
+ ui_init();
LVGL Setup. Option 2 with LVGL demos already running
Gather the necessary files described below from the LVGL Linux Port example found here.
Makefile
lv_conf.h
lv_drv_conf.h
main.c
mouse_cursor_icon.c
Patch the lv_drv_conf.h
# define EVDEV_NAME "/dev/input/event10" /*You can use the "evtest" Linux tool to get the list of devices and test them*/
+# define EVDEV_NAME "/dev/input/event<Number>"
NOTE: This changes according to the output of # evtest.
Patch the main.c
- disp_drv.hor_res = 800;
- disp_drv.ver_res = 480;
+ disp_drv.hor_res = 1080;
+ disp_drv.ver_res = 1920;
…
- /*Create a Demo*/
- lv_demo_widgets();
+ /*Create a Squareline Demo*/
+ ui_init();
Run the demo
Build the demo with the following command and copy the ./demo output to the i.MX 93 EVK RootFS.
# source /opt/path/to/your/toolchain
# make clean
# make
The demo can be ran with the following commands.
# systemctl stop weston # For LF
$ sudo service gdm3 stop # For Ubuntu
# ./demo JosephAtNXP_4-1732572830444.jpeg
Conclusion
SquareLine demos can run in prebuilt and basic builds of i.MX processors through FB, which can enable a quick set-up for GUI testing before moving to use a windowing stack without sacrificing any features.
Appendix
Document: How to run LGVL on iMX using framebuffer
Official page for pricing information
View full article