Wireless Connectivity Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wireless Connectivity Knowledge Base

Discussions

Sort by:
Sniffing is the process of capturing any information from the surrounding environment. In this process, addressing or any other information is ignored, and no interpretation is given to the received data. Freescale provides both means and hardware to create devices capable of performing this kind of operation. For example, a KW01 board can be easily turned into a Sub-GHz sniffer using Test Tool 12.2.0 which can be found at https://www.freescale.com/webapp/sps/download/license.jsp?colCode=TESTTOOL_SETUP&appType=file2&location=null&DOWNLOAD_ID=null After downloading and installing Test Tool 12.2.0 there are several easy steps to create your own sniffer for Sub-GHz bands. 1) How to download the sniffer image file onto KW01.      a) Connect KW01 to PC using the mini-usb cable      b) Connect the J-Link to the PC      c) Open Test Tool 12.2 and go to the Firmware Loaders tab      d) Select Kinetis Firmware Loader. A new tab will pop-up.      e) J-Link will appear under the J-Link devices tab.      f) Select the KW01Z128_Sniffer.srec file and press the upload button.     g) From the Development Board Option menu select KW01Z128.      h) Follow the on-screen instruction and unplug the board. Then plug it back in.      i) Close the Kinetis Firmware Loader tab and open the Protocol Analyzer Tab 2) How to use the Protocol Analyzer feature. Basics.     a) The Protocol Analyzer should automatically detect the KW01 sniffer. If not, close the tab, unplug the board, plug it back and re-open the tab. If this doesn’t work, try restarting Test Tool.     b) To start “sniffing” the desired channel, click the arrow down button from Devices: KW01 (COMx) Off and select the desired mode and channel.     c) The tab will change to ON meaning that KW01 will "sniff" on the specified channel. To select another channel, click the tab again and it will switch back to Off. Then select a new channel.      d) Regarding other configurations, please note that you can specify what decoding will be applied to the received data. Additional information: The sniffer image found in Test Tool is compiled for the 920-928MHz frequency band. Because of this, the present document will have attached to it two sniffer images, for the 863-870MHz and the 902-928MHz frequency bands. To upload a custom image perform the steps described at the beginning of this document, but instead of selecting a *.srec file from the list in Kinetis Firmware Loader click the Browse button and locate the file on disk. After selecting it, redo the steps for uploading an image file. A potential outcome: sometimes, if you load a different frequency band sniffer image, the Protocol Analyzer will display the previously used frequency band. To fix this, close Test Tool, re-open it and go to the Protocol Analyzer tab again. The new frequency band should be displayed. More information on this topic can be found in Test Tool User Guide (..\Freescale\Test Tool 12\Documentation\TTUG.pdf), under Chapter 5 (Protocol Analyzer, page 87).
View full article
This project is for Kinets L MCU Brazil challenge.Actually we don´t know if the project was registered. The goal of this project is to make Bluetooth communication between an android and  Freescale Freedom development kit FRDM-KL25Z. We will show the FRDM-KL25Z accelerometer status and the internal temperature sensor on android app. The android app requires version 4.x or above. Bluetooth module is connected to UART1.The embeddec code was created on CodeWarrior and exported to Keil MDK ARM.   http://youtu.be/-waEkfIuZCw
View full article
This article describes how to use the tcpdump tool to capture wireless network data packets. The test block diagram is as follows: weidong_sun_0-1620624281386.png For more detailed information, See attachment,please!   NXP CAS-TIC Wireless MCU team Weidong Sun
View full article
What is a BLE Beacon? A BLE Beacon is a hardware including a MCU, a BLE radio, an antenna and a power source. Things like Freescale Beacon, iBeacon, AltBeacon or Eddystone are software protocols with their own characteristics. How it works? A BLE Beacon is a non-connectable device that uses Bluetooth Low Energy (BLE or Bluetooth Smart) to broadcast packets that include identifying information and each packet receives the name of Advertising Packet. The packet structure and the information broadcasted by a Beacon depend on the protocol, but, the basic structure is conformed by: UUID. This is a unique identifier that allows identifying a beacon or a group of beacons from other ones. Major number. Used to identify a group of beacons that share a UUID. Minor number. Used to identify a specific beacon that share UUID and Major number. Example UUID Major Minor AAAAAAAA-AAAA-AAAA-AAAA-AAAAAAAAAAAA 1 1 These Beacons share the same UUID and Major number, and are differentiated by Minor number. AAAAAAAA-AAAA-AAAA-AAAA-AAAAAAAAAAAA 1 2 AAAAAAAA-AAAA-AAAA-AAAA-AAAAAAAAAAAA 2 1 This Beacon shares the same UUID as the previous ones, but has a different Major number, so it belongs to a different group. BBBBBBBB-BBBB-BBBB-BBBB-BBBBBBBBBBBB 1 1 This Beacon is completely different from the previous ones, since it doesn’t share the same UUID. These packets need to be translated or interpreted in order to provide the beacon a utility. There are applications that can interact with beacons, usually developed to be used with smartphones and/or tablets. These applications require being compliant with the protocol used by the beacon in order to be able to perform an action when a beacon is found. Use Cases Beacons can be used on different places to display different content or perform different actions, like: Restaurants, Coffee Shops, Bars Virtual Menu Detailed information Food source Suggested wine pairings Museums Contextual information. Analytics Venue check-in (entry tickets) Self-guided tours. Educational excursions Event Management and Trade Shows Frictionless Registration Improved Networking Sponsorship Navigation and Heat Mapping Content Delivery Auto Check-in Stadiums Seat finding and seat upgrading Knowing the crowded locations Promotions, offers and loyalty programs Sell Merchandise Future implementations Retail and Malls Shopping with digital treasure hunts Gather digital up-votes and down-votes from visitors Allow retailers to join forces when it comes to geo-targeted offers Use time-sensitive deal to entice new shoppers to walk in Help in navigation Engage your customers with a unified mall experience.
View full article
Introduction The FRDM-KW36 includes an RTC module with a 32 kHz crystal oscillator. This module generates a 32 kHz clock source for the MCU whilst running on very low power mode. This oscillator includes a set of programmable capacitors used as the C LOAD . Changing the value of these capacitors can modify the frequency the oscillator provides. This configurable capacitance ranges from 0 pF (capacitor bank disabled) to 30 pF in steps of 2 pF. These values are obtained by combining the enabled capacitors. The values available are 2 pF, 4 pF, 8 pF, and 16 pF. Any combination of these four can be done. It is recommended that these internal capacitors are disabled if the external capacitors are available (clearing SC2P, SC4P, SCS8, and SC16 bits in RTC Control Register SFR). To adjust the frequency provided by the oscillator, you must first be able to measure the frequency. Using a frequency counter would be ideal, as it provides a more precise measurement than an oscilloscope. You will also need to output the oscillator frequency. To output the oscillator frequency, using any of the Bluetooth demo applications as an example, you should do the following: Adjusting Frequency Example This example will make use of the Heart Rate Sensor demo (freertos version) from the Connectivity Software Stack and assumes that the developer has the knowledge of import or open projects from the SDK to IDE. Open or clone the Heart Rate Sensor project from your SDK. Find the board.c and board.h files in the board folder at the workspace.                                                                                Declare a void function on the board.h file as shown below. This function will be in order to mux the RTC clock out to the PTB3 and be able to measure the frequency.  /* Function to mux PTB3 to RTC_CLKOUT */ void BOARD_EnableRtcClkOut (void);‍‍ Develop the BOARD_EnableRtcClkOut function inside the board.c file as below. void BOARD_EnableRtcClkOut(void) { /* Enable PORTB clock gating */ CLOCK_EnableClock(kCLOCK_PortB); /* Mux the RTC_CLKOUT to PTB3 */ PORT_SetPinMux(PORTB, 3u, kPORT_MuxAlt7); /* Select the 32kHz reference for RTC_CLKOUT signal */ SIM->SOPT1 |= SIM_SOPT1_OSC32KOUT(1); } Call the BOARD_EnableRtcClkOut function in hardware_init function just after BOARD_BootClockRUN (board.c file). Find clock_config.c file in the board folder at the workspace. Add the following defines at the top of the file. #define RTC_OSC_CAP_LOAD_0 0x0U /*!< RTC oscillator, capacitance 0pF */ #define RTC_OSC_CAP_LOAD_2 0x2000U /*!< RTC oscillator, capacitance 2pF */ #define RTC_OSC_CAP_LOAD_4 0x1000U /*!< RTC oscillator, capacitance 4pF */ #define RTC_OSC_CAP_LOAD_6 0x3000U /*!< RTC oscillator, capacitance 6pF */ #define RTC_OSC_CAP_LOAD_8 0x800U /*!< RTC oscillator, capacitance 8pF */ #define RTC_OSC_CAP_LOAD_10 0x2800U /*!< RTC oscillator, capacitance 10pF */ #define RTC_OSC_CAP_LOAD_12 0x1800U /*!< RTC oscillator, capacitance 12pF */ #define RTC_OSC_CAP_LOAD_14 0x3800U /*!< RTC oscillator, capacitance 14pF */ #define RTC_OSC_CAP_LOAD_16 0x400U /*!< RTC oscillator, capacitance 16pF */ #define RTC_OSC_CAP_LOAD_18 0x2400U /*!< RTC oscillator, capacitance 18pF */ #define RTC_OSC_CAP_LOAD_20 0x1400U /*!< RTC oscillator, capacitance 20pF */ #define RTC_OSC_CAP_LOAD_22 0x3400U /*!< RTC oscillator, capacitance 22pF */ #define RTC_OSC_CAP_LOAD_24 0xC00U /*!< RTC oscillator, capacitance 24pF */ #define RTC_OSC_CAP_LOAD_26 0x2C00U /*!< RTC oscillator, capacitance 26pF */ #define RTC_OSC_CAP_LOAD_28 0x1C00U /*!< RTC oscillator, capacitance 28pF */ #define RTC_OSC_CAP_LOAD_30 0x3C00U /*!< RTC oscillator, capacitance 30pF */ Search the CLOCK_CONFIG_EnableRtcOsc call to a function inside the BOARD_BootClockRUN function (also in the clock_config.c file), and edit the argument by any of the defines above. Finally, disable the low power options and led support in the "preinclude.h" file located in the source folder of the project: #define cPWR_UsePowerDownMode 0 #define gLEDSupported_d 0 At this point, you can measure in PTB3 and play with the frequency adjust using your frequency counter. Each time that the board is programmed, you need to perform a POR to get the correct measure. The following table was obtained from an FRDM-KW36 board rev B and it can be used as a reference to adjust the frequency. Please note that the capacitance is not only composed of the enabled internal capacitance, but also the parasitic capacitances found in the package, bond wires, bond pad, and the PCB traces. So, while the reference measurements given below should be close to the actual value, you should also make measurements with your board, to ensure that the frequency is trimmed specifically to your board and layout.   Enabled Capacitors CLOAD Capacitance Definition Frequency - 0pF RTC_OSC_CAP_LOAD_0 (bank disabled) 32772.980Hz SC2P 2pF RTC_OSC_CAP_LOAD_2 32771.330Hz SC4P 4pF RTC_OSC_CAP_LOAD_4 32770.050Hz SC2P, SC4P 6pF RTC_OSC_CAP_LOAD_6 32769.122Hz SC8P 8pF RTC_OSC_CAP_LOAD_8 32768.289Hz SC2P, SC8P 10pF RTC_OSC_CAP_LOAD_10 32767.701Hz SC4P, SC8P 12pF RTC_OSC_CAP_LOAD_12 32767.182Hz SC2P, SC4P, SC8P 14pF RTC_OSC_CAP_LOAD_14 32766.766Hz SC16P 16pF RTC_OSC_CAP_LOAD_16 32766.338Hz SC2P, SC16P 18pF RTC_OSC_CAP_LOAD_18 32766.038Hz SC4P, SC16P 20pF RTC_OSC_CAP_LOAD_20 32765.762Hz SC2P, SC4P, SC16P 22pF RTC_OSC_CAP_LOAD_22 32765.532Hz SC8P, SC16P 24pF RTC_OSC_CAP_LOAD_24 32765.297Hz SC2P, SC8P, SC16P 26pF RTC_OSC_CAP_LOAD_26 32765.117Hz SC4P, SC8P, SC16P 28pF RTC_OSC_CAP_LOAD_28 32764.940Hz SC2P, SC4P, SC8P, SC16P 30pF RTC_OSC_CAP_LOAD_30 32764.764Hz
View full article
Hello,  Here are some helpful steps to follow when working with the NXP GitHub SDK. Step1: Ensure the necessary toolchains are installed:  https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/repo.html  Additional notes and links: VS code: https://code.visualstudio.com/ MCUXpresso plugin: https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-for-visual-studio-code:MCUXPRESSO-VSC Getting started with MCUXpresso for VS Code: https://www.nxp.com/design/design-center/training/TIP-GETTING-STARTED-WITH-MCUXPRESSO-FOR-VS-CODE   Step 2: Download and Install the SDK: GUI Method: - Open VS Code, navigate to Import Repository and select the Remote option as shown below: ovidiu_usturoi_0-1752492368597.png - Upon successful import, the repository will show up in the Imported Repositories window: ovidiu_usturoi_1-1752492786477.png    Command Line Method: - west commands: # Initialize west with the manifest repository west init -m https://github.com/nxp-mcuxpresso/mcuxsdk-manifests/ mcuxpresso-sdk # Update the west projects cd mcuxpresso-sdk west update More details:  https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/installation.html#get-mcuxpresso-sdk-repo  - import the local repository to VS code: Open VS Code, navigate to Import Repository and select the Local option and Browse.. to your local repo: ovidiu_usturoi_2-1752493440583.png   Step3: Run a Bluetooth LE Example Step3a: Run a Bluetooth LE Example using MCUXpresso for VS code - click Import Example from Repository from the QuickStart Panel - From the open dialog, select the MCUXpresso SDK, the Arm GNU toolchain, your target board, desired template, and application type, and proceed by clicking Import: ovidiu_usturoi_3-1752493896113.png   For the application type, you’ll typically see two options:  - Repository application  - Freestanding application. The key difference lies in where the project is imported. Repository applications are placed within the MCUXpresso SDK directory, while Freestanding applications can be imported to a custom location defined by the user. - Next, VS Code will prompt you to verify trust for the imported files—click Yes. Navigate to the PROJECTS view. - Identify your project, right click and select the Prestine Build icon to begin building: ovidiu_usturoi_5-1752495003978.png  - details of the build are into the terminal window: ovidiu_usturoi_6-1752495337012.png - using Debug button will allow you to download and debug the software: ovidiu_usturoi_7-1752495412398.png   (useful link: https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/run_a_demo_using_mcuxvsc.html ) Step3b: Run a Bluetooth LE Example using IAR Embedded Workbench for ARM: - use the west list_projects command to list the supported example for boards and the corresponding toolchain: Example to list Bluetooth examples:  west list_project -p .\examples\wireless_examples\bluetooth\ or if you know the platform or/and the project you can use: west list_project -b kw45b41zevk -p .\examples\wireless_examples\bluetooth\w_uart ovidiu_usturoi_8-1752497079546.png  west list_project -b frdmmcxw23 -p .\examples\wireless_examples\bluetooth\w_uart ovidiu_usturoi_9-1752497125122.png   Once you've confirmed that the project is available for the IAR toolchain, run the appropriate command to build it: west build -p always examples/wireless_examples/bluetooth/w_uart/freertos --toolchain iar --config debug -b kw45b41zevk The build folder will contain the generated output: ovidiu_usturoi_10-1752498250751.png   To work with IDE add  -t guiproject in the west command: west build -p always examples/wireless_examples/bluetooth/w_uart/freertos --toolchain iar --config debug -b kw45b41zevk -t guiproject --pristine --build-dir=build/w_uart_freertos_kw45   ovidiu_usturoi_11-1752498595529.png  The result of the build will indicate the path to the *.eww/*.ewp: ovidiu_usturoi_12-1752498651277.png   (additional details: https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/run_project.html )   Step4: Create a standalone example With the freestanding project approach, only the application code is included in the export folder. Other essential files remain linked to the repository. To generate a complete standalone project, the recommended method is using West by adding -t standalone_project option. Example of command for kw45b41zevk, IAR toolchain: west build -b kw45b41zevk ./examples/wireless_examples/bluetooth/w_uart/freertos -p always --toolchain iar --config debug -t standalone_project -d c:\work\w_uart_kw45 ovidiu_usturoi_13-1752499869665.png  The result of the build will indicate the path to the *.eww/*.ewp: ovidiu_usturoi_14-1752499888547.png   Example of command for kw45b41zevk, armgcc toolchain: west build -b kw45b41zevk ./examples/wireless_examples/bluetooth/w_uart/freertos -p always --toolchain armgcc --config debug -t standalone_project -d c:\work\w_uart_KW45_armgcc ovidiu_usturoi_0-1752500173467.png The result of the build will indicate the path to the project that need to be imported in VsCode: ovidiu_usturoi_1-1752500278581.png Regards, Ovidiu  
View full article
KW39_38_37 radio certification information 
View full article
In developing a Zigbee application, certain static configuration is required before the application is built. Configuring the network size, adding a new cluster, making the device discoverable and adding a new endpoint can be done by changing parameters in the following files: app_zps_cfg.h app_zcl_cfg.h app_zcl_global.c These files are responsible for setting up network parameters like device type and associated parameters, mainly related to the APS and NWK layers of the ZigBee PRO stack. Network Configuration The ZigBee device can be configured to be a coordinator, router and end device. The following section details the way in which the user can configure each device type. The app_zps_cfg header file lets the user configure the ZPS ZDO parameters of the node. The following macros are necessary for the corresponding device types: For coordinator in a ZigBee network #define ZPS_COORDINATOR #define ZPS_ZDO_DEVICE_TYPE                              ZPS_ZDO_DEVICE_COORD For router in a ZigBee network #define ZPS_ROUTER #define ZPS_ZDO_DEVICE_TYPE                              ZPS_ZDO_DEVICE_ROUTER For enddevice in a ZigBee network #define ZPS_ENDDEVICE #define ZPS_ZDO_DEVICE_TYPE                              ZPS_ZDO_DEVICE_ENDDEVICE Other ZPS ZDO configurations which are defined using macro are explained in comments inside the header file (app_zps_cfg.h). These macros provide the user with the ability to configure the device according to their network needs. The type of security for the ZigBee network can also be configured by the macro ZPS_ZDO_NWK_KEY_STATE. The user can change the security type to no network security (ZPS_ZDO_NO_NETWORK_KEY), pre-configured link key security (ZPS_ZDO_PRECONFIGURED_LINK_KEY), distributed link key security (ZPS_ZDO_DISTRIBUTED_LINK_KEY) or pre-configured installation code security (ZPS_ZDO_PRCONFIGURED_INSTALLATION_CODE). /* Specify No network Security */ #define ZPS_ZDO_NWK_KEY_STATE                               ZPS_ZDO_NO_NETWORK_KEY The application allows through this header file to configure ZPS APS AIB parameters, like extended PANID (ZPS_APS_AIB_INIT_USE_EXTENDED_PANID) or channel mask (ZPS_APS_AIB_INIT_CHANNEL_MASK). /* NWK EXTENDED PANID (EPID) that the device will use.*/ #define ZPS_APS_AIB_INIT_USE_EXTENDED_PANID                 0x0000000000000000ULL /*! CHANNEL MASK : Define all channels from 11 to 26*/ #define ZPS_APS_AIB_INIT_CHANNEL_MASK                       0x07fff800UL User can also configure the simple descriptor table size (AF_SIMPLE_DESCRIPTOR_TABLE_SIZE) as part of the ZPS AF Layer configuration parameters.The value depends on number of endpoints defined in application, one endpoint is always reserved for ZDO . So, for a device with one endpoint, the value would be 2 (1 ZDO + 1 application endpoint) #define AF_SIMPLE_DESCRIPTOR_TABLE_SIZE                     2 Among other ZPS network configuration parameters that can be changed by the user are scan duration (ZPS_SCAN_DURATION), default permit joining time (ZPS_DEFAULT_PERMIT_JOINING_TIME) and the maximum number of simultaneous key requests (ZPS_MAX_NUM_SIMULTANEOUS_REQUEST_KEY_REQS). Also, NIB values can be changed, like for example, the maximum number of routers in the network (ZPS_NWK_NIB_INIT_MAX_ROUTERS), the maximum number of children for a node (ZPS_NWK_NIB_INIT_MAX_CHILDREN), the maximum network depth (ZPS_NWK_NIB_INIT_MAX_DEPTH) or the network security level (ZPS_NWK_NIB_INIT_SECURITY_LEVEL). Different ZigBee network table sizes can be adjusted by the user from this header file. The important tables are mentioned below: The active neighbor table size (ZPS_NEIGHBOUR_TABLE_SIZE). The neighbor discovery table size, used to keep a list of the neighboring devices associated with the node (ZPS_NEIGHBOUR_DISCOVERY_TABLE_SIZE). The network address map table size, which represents the size of the address map that maps 64-bit IEEE addresses to 16-bit network (short) addresses (ZPS_ADDRESS_MAP_TABLE_SIZE). The network security material set size (ZPS_SECURITY_MATERIAL_SETS). The broadcast transaction table size, which stores the records of the broadcast messages received by the node (ZPS_BROADCAST_TRANSACTION_TABLE_SIZE). The route record table size (ZPS_ROUTE_RECORD_TABLE_SIZE) for the table that records each route, storing the destination network address, a count of the number of relay nodes to reach the destination and a list of the network addresses of the relay nodes. The route discovery table size (ZPS_ROUTE_DISCOVERY_TABLE_SIZE), used by the node to store temporary information used during route discovery. The MAC address table size (ZPS_MAC_ADDRESS_TABLE_SIZE). The binding table size (ZPS_BINDING_TABLE_SIZE). The group table size (ZPS_GROUP_TABLE_SIZE). The number of supported network keys, known also as the security material sets (ZPS_KEY_TABLE_SIZE). The child table size (ZPS_CHILD_TABLE_SIZE), that gives the size of the persisted sub-table of the active neighbor table. The stored entries are for the node’s parent and immediate children. The trust center device table size (ZPS_TRUST_CENTER_DEVICE_TABLE_SIZE). ZCL Configuration The app_zcl_cfg header file is used by the application to configure the ZigBee Cluster library. This file contains the definition for the application profile and cluster ids. The default application profiles are ZDP, HA, ZLO, GP. The ZDP (ZigBee Device Profile) id is identified by the following line: #define ZDP_PROFILE_ID             (0x0000) ZDP provides services for the following categories as cluster Ids: Device discovery services (for example, ZDP_DISCOVERY_CACHE_REQ_CLUSTER_ID) Service discovery services (for example, ZDP_IEEE_ADDR_REQ_CLUSTER_ID) Binding services (for example, ZDP_BIND_RSP_CLUSTER_ID) Management services (for example, ZDP_MGMT_NWK_DISC_REQ_CLUSTER_ID) The HA (Home Automation) profile id is identified by the following line: #define HA_PROFILE_ID             (0x0104) HA provides services for the following categories as cluster Ids: Generic devices (for example, HA_BASIC_CLUSTER_ID) Lighting devices (for example, HA_LEVELCONTROL_CLUSTER_ID) Intruder Alarm System (IAS) devices (for example, HA_IASZONE_CLUSTER_ID) The ZLO (ZigBee Lighting and Occupancy) profile is not an application profile but devices in this collection use the same application profile id as for the Home Automation application profile. This ensures backward compatibility with applications for devices based on the Home Automation 1.2 profile. ZigBee Green Power (GP) is an optional cluster with the aim of minimizing the power demands on a network node in order to support: Nodes that are completely self-powered through energy harvesting Battery-powered nodes that require ultra-long battery life The GP profile id is identified by the following line: #define GP_PROFILE_ID               (0xa1e0) The Zigbee GP cluster ID is defined as following: #define GP_GREENPOWER_CLUSTER_ID    (0x0021) Depending on the application, the app_zcl_cfg header file also contains the defines for the node endpoints. For example, the occupancy_sensor application contains the following endpoints: /* Node 'Coordinator' */ /* Endpoints */ #define COORDINATOR_ZDO_ENDPOINT    (0) #define COORDINATOR_COORD_ENDPOINT    (1) /* Node 'OccupancySensor' */ /* Endpoints */ #define OCCUPANCYSENSOR_ZDO_ENDPOINT    (0) #define OCCUPANCYSENSOR_SENSOR_ENDPOINT    (1)   /* Node 'LightSensor' */ /* Endpoints */ #define LIGHTSENSOR_ZDO_ENDPOINT    (0) #define LIGHTSENSOR_SENSOR_ENDPOINT    (1)   /* Node 'LightTemperatureOccupancySensor' */ /* Endpoints */ #define LIGHTTEMPERATUREOCCUPANCYSENSOR_ZDO_ENDPOINT    (0) #define LIGHTTEMPERATUREOCCUPANCYSENSOR_SENSOR_ENDPOINT    (1) The source file app_zcl_globals.c is used to declare the cluster lists for each endpoint. These act as simple descriptors for the node. Each endpoint has two cluster lists, containing uint16_t data. One is for input and one for output. The sizes of these two lists must be equal. For example, for endpoint 0, the declared lists will be the following: PRIVATE const uint16 s_au16Endpoint0InputClusterList[16]  =  { 0x0000, 0x0001, 0x0002, 0x0003, 0x0004, 0x0005, 0x0006 , 0x0007, \                                                               0x0008, 0x0010, 0x0011, 0x0012, 0x0012, 0x0013, 0x0014 , 0x0015}; PRIVATE const uint16 s_au16Endpoint0OutputClusterList[16] = { 0x0000, 0x0001, 0x0002, 0x0003, 0x0004, 0x0005, 0x0006 , 0x0007, \                                                              0x0008, 0x0010, 0x0011, 0x0012, 0x0012, 0x0013, 0x0014 , 0x0015}; The input list must also have a corresponding cluster APDU list, matching in size. For the endpoint 0 example, this will look like: PRIVATE const PDUM_thAPdu s_ahEndpoint0InputClusterAPdus[16] = { apduZDP, apduZDP, apduZDP, apduZDP, apduZDP, apduZDP, apduZDP, apduZDP,\                                                                  apduZDP, apduZDP, apduZDP, apduZDP, apduZDP, apduZDP, apduZDP, apduZDP}; Each output and input cluster list has a corresponding cluster discovery enabled flags list. As each bit inside the Cluster Disc Flag corresponds to cluster , for 16 clusters declared in Input and Output cluster list, one needs 2 bytes for Discoverable flag. In this example, the declaration is the following: PRIVATE uint8 s_au8Endpoint0InputClusterDiscFlags[2] = {0x1F, 0x08}; PRIVATE uint8 s_au8Endpoint0OutputClusterDiscFlags[2] = {0x08, 0x1B}; These parameters are registered in the node’s endpoints simple descriptor structure. The declared variable for the structure is s_asSimpleDescConts and its size depends on the number of endpoints available on the node. For example, for two endpoints, the declaration will be as below: PUBLIC zps_tsAplAfSimpleDescCont s_asSimpleDescConts[2] = {     {         {             0x0000,             0,             0,             0,             84,             84,             s_au16Endpoint0InputClusterList,             s_au16Endpoint0OutputClusterList,             s_au8Endpoint0InputClusterDiscFlags,             s_au8Endpoint0OutputClusterDiscFlags,         },         s_ahEndpoint0InputClusterAPdus,         1     },     {         {             0x0104,             0,             0,             1,             6,             4,             s_au16Endpoint1InputClusterList,             s_au16Endpoint1OutputClusterList,             s_au8Endpoint1InputClusterDiscFlags,             s_au8Endpoint1OutputClusterDiscFlags,         },         s_ahEndpoint1InputClusterAPdus,         1     }, }; The AF Context definition is as below: typedef struct _zps_tsAplAfSimpleDescCont {     ZPS_tsAplAfSimpleDescriptor sSimpleDesc;     const PDUM_thAPdu *phAPduInClusters;     bool_t bEnabled; } zps_tsAplAfSimpleDescCont; And the endpoint simple descriptor has the following structure definition: typedef struct {     uint16 u16ApplicationProfileId;     uint16 u16DeviceId;     uint8  u8DeviceVersion;     uint8  u8Endpoint;     uint8  u8InClusterCount;     uint8  u8OutClusterCount;     const uint16 *pu16InClusterList;     const uint16 *pu16OutClusterList;     uint8 *au8InDiscoveryEnabledFlags;     uint8 *au8OutDiscoveryEnabledFlags; } ZPS_tsAplAfSimpleDescriptor;
View full article
This post covers the below details. Introduction to Framework Serial Communication Interface (FSCI). BLE Server. Useful Commands to create a GATT database. Demonstrate the heart rate sensor profile using the FSCI black box application with Test Tool. Framework Serial Communication Interface The Framework Serial Communication Interface (FSCI) is a software module and a protocol that supports interfacing the Protocol Host Stack (i.e. BLE, Thread, and ZigBee) with a host or a PC tool (Test Tool for Connectivity Products) using a serial communication interface (e.g. UART, USB, SPI, and I2C). The below figure shows interaction between different layers. System Overview.PNG  Figure 1. System Overview The Host Processor (Application layer and control for Connectivity Stack) The Black Box application (APIs to interact with the Connectivity Stack) The below figure illustrates Interfacing between the host processor and black box application. Protocol stack separation.PNG  Figure 2. Protocol stack separation The Test Tool software for the connectivity products is an example of a host processor that can communicate with FSCI black boxes at various layers. The figure below shows FSCI based application structure. FSCI based Application Structure.PNG  Figure 3. FSCI based Application Structure The FSCI module executes in the context of the Serial Manager task. For more details regarding FSCI and Serial Manager module refer to the ‘Connectivity Framework Reference Manual.pdf’ document available inside SDK Documentation at location <SDK_Documentation\docs\wireless\Common>. The detailed description of the Bluetooth Low Energy Host Stack serial commands, communication packet structure, and usage of the Framework Serial Communication Interface is provided inside the ‘Bluetooth Low Energy Host Stack FSCI Reference Manual.pdf’ document available inside SDK Documentation at location <SDK_Documentation\docs\wireless\Bluetooth>. The detail about FSCI Host is described here. An example of FSCI based BLE temperature sensor application is described in AN12896. Bluetooth Low Energy Server Bluetooth Low Energy allows exchange of information using the Generic Attribute Profile (GATT), GATT defines below two roles: Server: Device that stores the information. Client: Device that request for information from the server. Going forward, this post describes how to implement a BLE Server using the FSCI black box application with Test Tool. The server device can implement the GATT Database using below two methods. Static database: MACROs are used to add services, characteristics, etc. Dynamic database: APIs are used to add services, characteristics, etc. It is useful when runtime database update is required. This is the approach used by FSCI for the management of GATT databases. The below figure shows an example of database hierarchy. GATT Database.png  Figure 4. GATT Database Service: It is a set of information. i.e., sensor location, sensor read value, etc. Bluetooth SIG has defined universally unique identifier (UUID) for various services and characteristics. This UUID will be useful to add services and characteristics to the database. Heart Rate, Battery Information, Device Information are examples of the service. Characteristic and value: It is the actual entity where information and its value are stored when the characteristic and value are added into the database. i.e., Device information service can have characteristics like manufacturer name, model string, Hardware version, etc. Descriptor: It is used to provide additional information regarding the characteristic and its value, e.g. format, scale, unit, etc. Client Characteristic Configuration Descriptor (CCCD): It is a descriptor used by the client device to enable or disable the notifications or indications. When the specific component is added using GATT_DB APIs, the stack will assign a handle to that component to index it in the database. Useful commands to create GATT database FSCI provides a set of commands for the management of the GATT Database. The most used ones are described below. Table 1 Some of the Basic GATT_DB Command Command Description No. of Handle assigned GATTDBDynamic-AddPrimaryServiceDeclaration.Request To add the primary service. 1 GATTDBDynamic-AddCharacteristicDeclarationAndValue.Request To add the characteristic and its value. It will be added as part of previously added service. 2 GATTDBDynamic-AddCharacteristicDescriptor.Request To add the descriptor for the previously added characteristic. 1 GATTDBDynamic-AddCccd.Request To add the CCCD for the previously added characteristic. 1 The attached Test Tool macro file demonstrates steps and setup required to implement a Heart Rate Sensor profile. The steps to execute it are described in the attached lab guide.
View full article
The KW40Z has support for a 32 MHz reference oscillator. This oscillator is used, among other things, as the clock for the RF operation. To properly adjust the frequency provided by this oscillator, there is a register that can be written, and this register (XTAL_TRIM) adjusts the capacitance provided by the internal capacitor bank to which the oscillator is connected. The KW40Z comes preprogramed with a default value (0x77) in the XTAL_TRIM register. However, since there is probably some variance when using different HW, the central frequency should be verified using a spectrum analyzer. Depending on the value measured, the XTAL_TRIM register can be modified to adjust the frequency. The Connectivity Test application provided here was modified, adding support to change the XTAL_TRIM register. In this case, the Agilent Technologies N9020A MXA Signal Analyzer was used, configured with the following parameters: FREQ (central frequency): 2405 MHz (test will be conducted on channel 11) SPAN (x-axis): 100 KHz AMPTD (amplitude, y-axis): 5 dBm   To perform the test, program the KW40Z device with the Connectivity Test application, using the provided .bin file, or using IAR and replacing the files in the project with the ones provided. To replace the files, unzip the provided .zip file in the KW40Z Connectivity Software folder and when asked, select to replace the existing files with the new ones. To measure and adjust the trimming, run the Connectivity Test application. Press ENTER to start the application. Press 1 to select the continuous tests mode. Press 4 to start a continuous unmodulated transmission. Once the test is running, you should be able to see the unmodulated signal in the spectrum analyzer. Use D and F to change the XTAL_TRIM value, thus changing the central frequency. Now, considering the test is being performed in channel 11, the central frequency should be centered exactly in 2.405 GHz, but on this board, for example, it is slightly above (2.4050259 GHz) by default. In order to fix this, you will need to adjust the value of the XTAL_TRIM register. As you change the XTAL_TRIM value, the central frequency changes too. Adjust the trim value until you find a value that moves the frequency to where it should be centered. For this particular board, a trimming value of 189 (0xBD) was used. Once you have found the trimming value that best adjusts the frequency, you can use it in other projects using the following function, included in the KW4xXcvrDrv.h file: XcvrSetXtalTrim(<YOUR 8 BIT XTAL_TRIM VALUE>)‍‍‍‍‍‍
View full article
Introduction The FRDM-KW36 includes an RSIM (Radio System Integration Module) module with an external 32 MHz crystal oscillator. This clock source reference is mainly intended to supply the Bluetooth LE Radio peripheral, but it can be used as the main clock source of the MCU as well. This oscillator includes a set of programmable capacitors to support crystals with different load capacitance needs. Changing the value of these capacitors can modify the frequency the oscillator provides, that way, the central frequency can be tuned to meet the wireless protocol standards. This configurable capacitance range is from C1: 5.7pF - C2: 7.1pF to C1: 22.6pF - C2: 28.2pF and it is configured through the BB_XTAL_TRIM field at the ANA_TRIM. The KW36 comes preprogrammed with a default load capacitance value. However, since there is variance in devices due to tolerances and parasite effects, the correct load capacitance should be checked by verifying that the optimal central frequency is attained.  You will need a spectrum analyzer to measure the central frequency. To find the most accurate value for the load capacitance, it is recommended to use the Connectivity Test demo application. Adjusting Frequency Example Program the KW36 Connectivity Test software on the device. This example can be found in wireless_examples -> genfsk -> conn_test folder from your SDK package. Baremetal and FreeRTOS versions are available. In case that FRDM-KW36 board is being used to perform the test, you should move the 10pF capacitor populated in C55 to C57, to direct the RF signal on the SMA connector. Connect the board to a serial terminal software. When you start the application, you will be greeted by the NXP logo screen:  Press the enter key to start the test. Then press "1" to select "Continuous tests": Finally, select "6" to start a continuous unmodulated RF test. At this point, you should be able to measure the signal in the spectrum analyzer. You can change the RF channel from 0 to 127 ("q" Ch+ and "w" Ch- keys), which represents the bandwidth from 2.360GHz to 2.487GHz, stepping of 1MHz between two consecutive channels. To demonstrate the trimming procedure, this document will make use of channel 42 (2.402GHz) which corresponds to the Bluetooth LE channel 37. In this case, with the default capacitance value, our oscillator is not exactly placed at the center of the 2.402GHz, instead, it is slightly deflected to 2.40200155 GHz, as depicted in the following figure: The capacitance can be adjusted with the "d" XtalTrim+ and "f" XtalTrim- keys. Increasing the capacitance bank means a lower frequency. In our case, we need to increase the capacitance to decrease the frequency. The nearest frequency of 2.402 GHz was 2.40199940 GHz  Once the appropriate XTAL trim value has been found, it can be programmed as default in any Bluetooth LE example, changing the mXtalTrimDefault constant located in the board.c file: static const uint8_t mXtalTrimDefault‍ = 0x36;‍‍‍
View full article
Hi RF High Power Model Kit 2020 Rev2.1 Installation Questions URL: nxp.com/products/rf/rf-high-power-models/models-for-ads-keysight-advanced-design-system:RF_HIGH_POWER_MODELS_KEYSIGHT file name: RF-POWER-ADS2020v2p1-DK.zip I installed it but the library does not contain anything as shown below. Please help with this. Thank you!
View full article
Hello community, This time I bring to you a document which explains how easy is to add a new endpoint and a new cluster to a ZigBee device in the BeeStack in BeeKit. This document is based in the MC1323x MCUs but the procedure applies to the Kinetis devices. Before to start you need to install the BeeKit Wireless Connectivity Toolkit​. If you are interested about what an endpoint is, the document ZigBee Endpoints Reserved could be useful for you. I hope you find this guide useful. Enjoy this guide, enjoy ZigBee! Any feedback is welcome. Best regards, Earl Orlando Ramírez-Sánchez Technical Support Engineer NXP Semiconductors
View full article
Where can I find the KW20-30-40 radio certification documents?     FRDM-KW40 platforms have passed the CE RED & FCC radio certification (BLE & 15.4).  Find below for information the certification documents and test reports.  For further information on the FRDM board and the product please refer to the corresponding KW40 Product Summary page and FRDM-KW40.
View full article
从 MKW36Z512VHT4 到 MKW36A512VFT4 的软件移植指南 URL:https://community.nxp.com/docs/DOC-345487 由 Edgar Eduardo Lomeli Gonzalez 于 2020-09-14 创建的文档 引言 这篇文章将指导您如何从 MKW36Z512VHT4 移植到 MKW36A512VFT4 MCU。本示例将使用 “信标(beacon)” SDK 示例程序。 SDK 的下载和安装 1- 前往 MCUXpresso 网页:MCUXpresso 网页 2- 使用您的注册帐户登录。 3- 搜索“ KW36A”设备。单击建议的处理器型号,然后单击“Build MCUXpresso SDK”。 hansonhe_0-1627031632957.png 4- 点击后将显示另一页面。在“Toolchain / IDE”框中选择“All toolchains”,并提供名称以标 识软件包。然后点击“Download SDK”。 hansonhe_1-1627031664007.png   5- 接受许可协议。等待几分钟直到系统将软件包放入您的配置文件中。 单击“下载 SDK 存 档”(Download SDK Archive),下载 SDK,如下图所示。 hansonhe_2-1627031690301.png   6- 如果使用了 MCUXpresso IDE,请在“ Installed SDK’s”视图中拖放 KW36A SDK 压缩文件 夹来安装软件包。 hansonhe_3-1627031717790.png 至此,您已经下载并安装了 KW36A 芯片的 SDK 软件包。 MCUXpresso IDE 中的软件迁移 1- 在 MCUXpresso 工作区上导入“信标(beacon)”示例。单击“Import SDK examples(s)…” 选项,将出现一个新窗口。然后选择“ MKW36Z512xxx4”,单击 FRDM-KW36 图像。点击 “Next >”按钮。   hansonhe_4-1627031767212.png 2- 搜索信标例程并选择您的项目版本(裸机的 bm 或带 freertos 操作系统)。 hansonhe_5-1627031788721.png 3- 转到 Project/Properties。展开 C / C ++ Build / MCU 设置,然后选择 MKW36A512xxx4 MCU。单击“Apply and Close”按钮以保存配置。 hansonhe_6-1627031819475.png 4- 将 MKW36Z 文件夹重命名为 MKW36A,单击鼠标右键并选择“重命名”。这些是以下内容: framework/DCDC/Interface -> MKW36Z framework/DCDC/Source -> MKW36Z framework/LowPower/Interface -> MKW36Z framework/LowPower/Source -> MKW36Z framework/XCVR -> MKW36Z4 hansonhe_7-1627031852314.png 5- 在 MCUXpresso IDE 中打开“Project/Properties”窗口。 转到 C / C ++ Build / Settings,然 后在 Tool Settings 窗口中选择 MCU C Compiler / Includes 文件夹。在创建之前,根据 MKW35 文件夹,编辑与 MKW36 MCU 相关的所有路径。结果类似如下所示: ../framework/LowPower/Interface/MKW36A ../framework/LowPower/Source/MKW36A ../framework/DCDC/Interface/MKW36A ../framework/XCVR/MKW36A4 hansonhe_8-1627031890271.png  6- 在工具设置中选择 MCU Assembler/General 文件夹。 编辑与 MKW36 MCU 相关的路径。 结果类似如下所示: ../framework/LowPower/Interface/MKW36A ../framework/LowPower/Source/MKW36A ../framework/DCDC/Interface/MKW36A ../framework/XCVR/MKW36A4 hansonhe_9-1627031914674.png 7- 转到 Project/Properties。展开 MCU CCompiler/Preprocessor 窗口。编辑 “ CPU_MKW36Z512VHT4”和“ CPU_MKW36Z512VHT4_cm0plus”符号,分别将其重命名为 “ CPU_MKW36A512VFT4”和“ CPU_MKW36A512VFT4_cm0plus”。保存更改。 hansonhe_10-1627031936791.png 8- 转到工作区。删除位于 CMSIS 文件夹中的“ fsl_device_registers,MKW36Z4, MKW36Z4_features,system_MKW36Z4.h 和 system_MKW36Z4.c”文件。然后解压缩 MKW35Z SDK 软件包并在以下路径中搜索“ fsl_device_registers,MKW36A4,MKW36A4_features, system_MKW36A4.h 和 system_MKW36A4.c”文件到该文件夹中: <SDK_folder_root>/devices/MKW36A4/fsl_device_registers.h <SDK_folder_root>/devices/MKW36A4/MKW36A4.h <SDK_folder_root>/devices/MKW36A4/MKW36A4_features.h <SDK_folder_root>/devices/MKW36A4/system_MKW36A4.h <SDK_folder_root>/devices/MKW36A4/system_MKW36A4.c hansonhe_11-1627031958794.png 9- 通过位于路径<SDK_folder_root> /devices/MKW36A4/mcuxpresso/startup_mkw36a4.c 中的“ startup_mkw36a4.c”覆盖“ startup_mkw36z4.c”(位于启动文件夹中)。 您只需拖放 启动文件夹,然后删除较旧的文件夹即可。 hansonhe_12-1627031982968.png 10- 在 CMSIS 文件夹中打开“ fsl_device_registers.h”文件。在以下代码(文件的第 18 行)中 添加“ defined(CPU_MKW36A512VFT4)”: hansonhe_13-1627032027413.png 11- 在 bluetooth->host->config 文件夹中打开“ ble_config.h”文件。在以下代码中添加 “ defined(CPU_MKW36A512VFT4)”(文件的第 146 行): hansonhe_14-1627032054277.png hansonhe_15-1627032064628.png 12- 在 source-> common 文件夹中打开“ ble_controller_task.c”文件。在以下代码(文件的 第 272 行)中添加“ defined(CPU_MKW36A512VFT4)”: hansonhe_16-1627032085185.png 13-生成项目。 至此,该项目已经在 MCUXpresso IDE 环境中移植完成。 IAR Embedded Workbench IDE 中的软件移植 1- 打开位于以下路径的信标项目: 2- 在工作区中选择项目,然后按 Alt + F7 打开项目选项。 hansonhe_17-1627032109838.png 3- 在 General Options/Target”窗口中,单击器件名称旁边的图标,再选择合适的器件 NXP / KinetisKW / KW3x / NXP MKW36A512xxx4,然后单击“确定”按钮。 hansonhe_18-1627032130130.png 4- 在以下路径中创建一个名为 MKW36A 的新文件夹: <SDK_root>/middleware/wireless/framework_5.4.6/DCDC/Interface <SDK_root>/middleware/wireless/framework_5.4.6/DCDC/Source <SDK_root>/middleware/wireless/framework_5.4.6/LowPower/Interface <SDK_root>/middleware/wireless/framework_5.4.6/LowPower/Source <SDK_root>/middleware/wireless/framework_5.4.6/XCVR hansonhe_19-1627032149132.png  5- 复制位于上述路径的 MKW36Z 文件夹内的所有文件,然后粘贴到 MKW36A 文件夹中。 hansonhe_20-1627032171998.png  6- .在工作区中选择信标项目,然后按 Alt + F7 打开项目选项窗口。 在“ C/C++ Compiler/Preprocessor”窗口中,将所有路径里的 MKW36Z 文件夹重命名为 MKW36A 文件 夹。在已定义的符号文本框中,将 CPU_MKW36Z512VHT4 宏重命名为 CPU_MKW36A512VFT4。结果如下图所示:单击确定按钮。 hansonhe_21-1627032201469.png hansonhe_22-1627032213887.png 7- 展开启动文件夹,选择所有文件,单击鼠标右键,然后选择“Remove”选项。在文件夹上 单击鼠标右键,然后选择““Add/Add files”。添加位于以下路径的 startup_MKW36A4.s: <SDK_root>/devices/MKW36A4/iar/startup_MKW36A4.s 另外,将 system_MKW36A4.c 和 system_MKW36A4.h 添加到启动文件夹中。 这两个文件都 位于如下的路径中: hansonhe_23-1627032237365.png 8- 在 bluetooth->host->config 文件夹中打开“ ble_config.h”文件。在以下代码中添加 “ defined(CPU_MKW36A512VFT4)”: hansonhe_24-1627032258644.png 9- 在 source-> common 文件夹中打开“ ble_controller_task.c”文件。在以下代码中添加 “ defined(CPU_MKW36A512VFT4)”: hansonhe_25-1627032278866.png 10-生成项目。 至此,该项目已经在 IAR Embedded Workbench IDE 环境中移植完成。          
View full article
简介: 当 OTAP 客户端(接收软件更新的设备,通常为 Bluetooth LE 外围设备)从 OTAP 服务器 (发送软件更新的设备,通常为 Bluetooth LE Central)请求软件更新时,您可能希望保留一 些数据,例如绑定信息,系统振荡器的匹配值或您的应用程序的 FlexNVM 非易失数据。 本 文档指导您在执行 OTAP 更新时, 如何保留您感兴趣的闪存数据内容。 本文档适用于熟悉 OTAP 定制 Bluetooth LE 服务的开发人员,有关更多基础信息,您可以阅读以下文章: 使用 OTAP 客户端软件对 KW36 设备进行重新编程。 OTAP 标头和子元素 OTAP 协议为软件更新实现了一种格式,该格式由标题和定义数量的子元素组成。 OTAP 标 头描述了有关软件更新的一般信息,并且其定义的格式如下图所示。 有关标题字段的更多 信息,请转至 SDK 中的<SDK_2.2.X_FRDM-KW36_Download_Path> \ docs \ wireless \ Bluetooth 中的《 Bluetooth Low Energy Application Developer's Guide》文档的 11.4.1 Bluetooth Low Energy OTAP 标头一章。 daweiyou_0-1627095941659.png   每个子元素都包含用于特定目的的信息。 您可以为您的应用程序实现专有字段(有关子元 素字段的更多信息, 请转至 SDK 中的<SDK_2.2.X_FRDM-KW36_Download_Path> \ docs \ wireless \ Bluetooth 中的《 Bluetooth Low Energy Application Developer's Guide》文档的 11.4.1 Bluetooth Low Energy OTAP 标头一章。 OTAP 包含以下子元素: 镜像文件子元素 值字段长度(字节) 描述 升级镜像 变化 该子元素包含实际的二进制可执行镜像,该镜像将被复制到 OTAP 客户端设备的闪存中。 该子元素的最 大大小取决于目标硬件。 扇区位图 32 该子元素包含目标设备闪存的扇区位图,该位图告诉引导加载程序哪些扇区应被覆盖,哪些扇区保持完 整。 该字段的格式是每个字节的最低有效位在前,最低有效字节和位代表闪存的最低存储部分。 镜像文件CRC 2 是在镜像文件的所有元素(此字段本身除外)上计算的 16 位 CRC。 该元素必须是通过空中发送的镜像文件中的最后一个子元素。   OTAP 扇区位图子元素 KW36 闪存分为: 一个 256 KB 程序闪存( P-Flash)阵列, 最小单元为 2 KB 扇区,闪存地址范围为 0x0000_0000 至 0x0003_FFFF。 一个 256 KB FlexNVM 阵列, 最小单元为 2 KB 扇区,闪存地址范围为 0x1000_0000 至 0x1003_FFFF, 同时它也会被映射到地址范围为 0x0004_0000 至 0x0007_FFFF 的空间。 位图子元素的长度为 256 位,就 KW36 闪存而言,每个位代表 2KB 扇区,覆盖从 0x0- 0x0007_FFFF 的地址范围(P-Flash 到 FlexNVM 映射地址范围),其中 1 表示该扇区应 被擦 除, 0 表示应保留该扇区。 OTAP 引导加载程序使用位图字段来获取在使用软件更新对 KW36 进行编程之前应擦除的地址范围,因此必须在发送软件更新之前对其进行配置,以使包含您 的数据的内存的地址范围保持不变。仅擦除将被软件更新覆盖的地址范围。 例如:假设开发人员想要保留 0x7D800-0x7FFFF 之间的地址范围和 0x0-0x1FFF 之间的地址 范围,并且必须擦除剩余的存储器。 0x7D800-0x7FFFF 之间的地址范围对应于前 5 个闪存 扇区, 0x0-0x1FFF 之间的地址范围是最低的 4 个扇区。 因此,这意味着应将 256 和 252 之间的位(256、 255、 254、 253 和 252)以及 4 和 1 之间 的位(4、 3、 2 和 1)设置为 0,这样本示例的 OTAP 位图为 : 0x07FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF0 使用 NXP 测试工具配置 OTAP 位图以保护地址范围 在恩智浦网站上下载并安装用于连接产品的测试工具 daweiyou_1-1627097016284.png   在 PC 上打开 NXP Test Tool 12 软件。 转到“ OTA 更新-> OTAP 蓝牙 LE”,然后单击“浏 览...”按钮加载用于软件更新的映像文件(NXP 测试工具仅接受.bin 和.srec 文件)。 您 可以配置 OTAP 位图,选择“覆盖扇区位图”复选框,并通过新的位图值更改默认值。 配 置位图后,选择“保存...”。 daweiyou_0-1627098005611.png   然后,将显示一个窗口,用于选择保存.bleota 文件的目的地,保存文件可以自行取名。 您可以将此文件与 Android 和 iOS 的 IoT Toolbox App 一起使用,以使用 OTAP 更新软 件。 这个新的.bleota 文件包含位图,该位图告诉 OTAP 引导加载程序哪些扇区将被擦 除,哪些扇区将被保留。 daweiyou_1-1627098038245.png    
View full article
The FRDM-KW40Z includes an RTC module with a 32 kHz crystal oscillator. This module generates a 32 kHz clock source for the MCU whilst running on very low power mode. This oscillator includes a set of programmable capacitors used as the C LOAD . Changing the value of these capacitors can modify the frequency the oscillator provides. This configurable capacitance ranges from 1 pF (which is effectively two 2 pF capacitors in series) all the way to 15 pF (30 pF capacitors in series). These values are obtained by combining the enabled capacitors. The values available are 2 pF, 4 pF, 8 pF and 16 pF. Any combination between these four can be done. It is recommended that these internal capacitors are disabled if the external capacitors are available. Figure 1. External capacitors for the 32 kHz crystal To adjust the frequency provided by the oscillator, you must first be able to measure the frequency. Using a frequency counter would be ideal, as it provides a more precise measurement than an oscilloscope. You will also need to output the oscillator frequency. To output the oscillator frequency, using any of the Bluetooth demo applications as an example, you should do the following: 1. Since the RTC module is going to be used to output the oscillator frequency, the RTC_CLKOUT will be the output signal. The output pin for RTC_CLKOUT is PTB3. To configure PTB3 as the oscillator output use the function configure_rtc_pins(RTC instance). Port B clock must be enabled first. Figure 2. PTB3 pin mux   /* hardware_init.c */     /* enable clock for PORTs */   CLOCK_SYS_EnablePortClock(PORTA_IDX);   CLOCK_SYS_EnablePortClock(PORTB_IDX);   CLOCK_SYS_EnablePortClock(PORTC_IDX);   /* RTC CLKOUT */   configure_rtc_pins(0);     //This function changes the pin mux to select RTC_CLKOUT. It is included in the pin_mux.c file. 2.  Modify the System Options Register 1 (SIM_SOPT1) to select the clock source and to allow the selected clock source to be output in PTB3. The field you should change is OSC32KOUT. To select the clock source to be output on PTB3, use the function CLOCK_HAL_SetExternalRefClock32kSrc(). Remember to include the fsl_sim_hal.h file. Figure 3. SIM_SOPT1 register fields /* hardware_init.c */ /* RTC CLKOUT */ configure_rtc_pins(0); SIM_Type *simBase = g_simBase[0];     SIM_SOPT1 = SIM_SOPT1_OSC32KOUT(kClockRtcoutSrc32kHz);                // This field in register SIM_SOPT1 allows a clock source to be output to PTB3 CLOCK_HAL_SetExternalRefClock32kSrc(simBase, kClockEr32kSrcOsc0);     // This function chooses the clock source for the RTC 3.  Make sure the oscillator is enabled. The RTC external clock configurations can be found in the board.h file. This is also where the internal capacitors are enabled. /* board.h */ /* RTC external clock configuration. */ #define RTC_XTAL_FREQ                32768U #define RTC_SC2P_ENABLE_CONFIG       false      // 2 pF capacitors enable #define RTC_SC4P_ENABLE_CONFIG       false      // 4 pF capacitors enable #define RTC_SC8P_ENABLE_CONFIG       false      // 8 pF capacitors enable #define RTC_SC16P_ENABLE_CONFIG      false      // 16 pF capacitors enable #define RTC_OSC_ENABLE_CONFIG        true       // Oscillator enable 4.  You should now be able to measure the oscillator frequency through the PTB3 pin. Measurements should be done with a frequency counter, as change in the output can be very subtle, and an oscilloscope might not be able to pick it up. Remember that these capacitors give you the option to use the 32 kHz oscillator when you do not have the external capacitors. They are not supposed to be used when the external capacitors are being used. Now, to change the internal capacitance, you can simply change the macros contained in the board.h file (step 4). It is important that the oscillator is disabled before making any changes to the enabled capacitors. The fsl_clock_manager.c file already contains the function CLOCK_SYS_RtcOscInit() that configures the oscillator with the values established in the previously mentioned macros, however, the oscillator is not disabled before attempting to change the capacitors (and therefore, no changes are made). To fix this, you can use the RTC_HAL_SetOscillatorCmd() function to disable the oscillator before making changes with the capacitors. /* fsl_clock_manager.c */     // Disable the oscillator in case any changes are made to the capacitors RTC_HAL_SetOscillatorCmd(RTC, false);     // If the oscillator is not enabled and should be enabled. if ((!RTC_HAL_IsOscillatorEnabled(RTC)) && (config->enableOsc)) {     /* Enable the desired capacitors */     RTC_HAL_SetOsc2pfLoadCmd(RTC, config->enableCapacitor2p);     RTC_HAL_SetOsc4pfLoadCmd(RTC, config->enableCapacitor4p);     RTC_HAL_SetOsc8pfLoadCmd(RTC, config->enableCapacitor8p);     RTC_HAL_SetOsc16pfLoadCmd(RTC, config->enableCapacitor16p);         /* Re-enable the oscillator */     RTC_HAL_SetOscillatorCmd(RTC, config->enableOsc); } The fsl_clock_manager.c file can be found in: <KW40Z_connSw_install_dir>\KSDK_1.3.0\platform\system\src\clock Some reference measurements with different values for the internal capacitance: With external capacitors (internal capacitors disabled) Board Revision C LOAD Measured Frequency KW40Z – rev. C C46 & C47 32,769.03 Hz KW40Z – rev. B C46 & C47 32,769.27 Hz With internal capacitors (external capacitors removed) Enabled Capacitors C LOAD Measured Frequency SC2P 1 pF 32,773.21 Hz SC4P 2 pF 32,772.06 Hz SC2P, SC4P 3 pF 32,771.2 Hz SC4P, SC8P 6 pF 32,769.39 Hz SC2P, SC4P, SC8P 7 pF 32,769 Hz SC16P 8 pF 32,768.6 Hz SC2P, SC16P 9 pF 32,768.31 Hz SC4P, SC16P 10 pF 32,768.05 Hz SC2P, SC4P, SC16P 11 pF 32,767.83 Hz SC4P, SC8P, SC16P 14 pF 32,767.27 Hz SC2P, SC4P, SC8P, SC16P 15 pF 32,767.11 Hz Please note that the capacitance is not only composed of the enabled internal capacitance, but also the parasitic capacitances found in the package, bond wires, bond pad and the PCB traces. So, while the reference measurements given before should be close to the actual value, you should also make measurements with your board, to ensure that the frequency is trimmed specifically to your board and layout.
View full article
This document describes the Persistent Data Manager (PDM) module which handles the storage of stack context data and application data in Non-Volatile Memory (NVM). For the KW41Z devices, this memory is internal Flash and this document will therefore refer to Flash. Tip: In this document, a cold start refers to either a first-time start or a re-start without memory (RAM) held. A warm start refers to a re-start with memory held (for example following sleep with memory held). 1.    Overview If the data needed for the operation of a network node is stored only in on-chip RAM, this data is maintained in memory only while the node is powered and will be lost during an interruption to the power supply (e.g. power failure or battery replacement). This data includes context data for the network stack and application data. In order for the node to recover from a power interruption with continuity of service, provision must be made for storing essential operational data in Non-Volatile Memory (NVM), such as Flash. This data can then be recovered during a re-boot following power loss, allowing the node to resume its role in the network. The storage and recovery of operational data in KW41Z Flash can be handled using the Persistent Data Manager (PDM) module, as described in the rest of this document, which covers the following topics: Initializing the PDM module - see Section 2 Managing data in Flash - see Section 3 PDM features like record searching by record ID – see Section 4 The PDM can be used with ZigBee PRO and IEEE802.15.4 wireless networking protocols. 2.    Initializing the PDM and Building a File System Using the Kinetis NVM framework requires that the user must register the necessary data sets for NVM writing. This is done by calling function NVM_RegisterDataSet(). This function registers the given data set to be written in the NVM_TABLE section from Flash. The PDM module must be initialized by the application following a cold or warm start, irrespective of the PDM functionality used (e.g. context data storage or counter implementation). PDM initialization is performed using the function PDM_eInitialise(). This function requires the following information to be specified: The number of Flash sectors to be used by PDM (a zero value means use all segments) Once the PDM_eInitialise() function has been called, the PDM module builds a file system in RAM containing information about the sectors that it manages in Flash. The PDM reads the header data from each Flash sector and builds the file system. Application records are grouped and initialized in function InitAplRecords(), while network stack records are grouped and initialized in function InitNwkRecords(). For ZigBee PRO, the PDM is used in its most general form, as described above. 3.    Managing Data in Flash This section describes use of the PDM module to persist data in Flash in order to provide continuity of service when the KW41Z device resumes operation after a cold start or a warm start without memory held. Data is stored in Flash in terms of ‘records’. A record occupies at least one Flash sector but may be larger than a sector and occupy multiple sectors. Any number of records of different lengths can be created, provided that they do not exceed the Flash capacity. The records are created automatically for stack context data and by the application (as indicated in Section 3.1) for application data. Each record is identified by a unique 16-bit value which is assigned when the record is created - for application data, this identifier is user-defined. The stack context data which is stored in Flash includes the following: Application layer data: AIB members, such as the EPID and ZDO state Group Address table Binding table Application key-pair descriptor Trust Centre device table Network layer data: NIB members, such as PAN ID and radio channel Neighbor table Network keys Address Map table On performing a KW41Z cold start or warm start without RAM held, the PDM must be initialized in the application as described in Section 2. If this is the first ever cold start, there will be no stack context data or application data preserved in the Flash. If it is a cold or warm start following previous use (such as after a reset), there should be stack context data and application data preserved in the Flash. On start-up, the PDM builds a file system in RAM and scans the Flash for valid data. If any data is found, it is incorporated in the file system. Saving and recovering application data in Flash are described in the subsections below. 3.1   Saving Data to Flash       Application data and stack context data are saved from RAM to Flash as described below.       Note: During a data save, if the Flash needs to be defragmented and purged, this will be performed automatically resulting in all records being re-saved.     Application data           You should save application data to Flash when important changes have been made to the data in RAM. Application data in RAM can be saved to an individual record           in Flash using the function PDM_eSaveRecordData(). A buffer of data in RAM is saved to a single record in Flash (a record may span multiple Flash sectors).          The records are created when calling PDM_eInitialise(). These records are traced by a unique 16-bit identifier assigned by the application - this identifier is subsequently          used to reference the record. The value used must not clash with those used by the NXP libraries - the ZigBee PRO stack libraries use values above 0x8000.          Subsequently, in performing a re-save to the same record (specified by its 16-bit identifier), the original Flash sectors associated with the record will be overwritten but          only the sector(s) containing data changes will be altered (if no data has changed, no write will be performed). This method of only making incremental saves improves          the occupancy level of the size-restricted Flash.     Stack Context Data          The NXP ZigBee PRO stack automatically saves its own context data from RAM to Flash when certain data items change. This data will not be encrypted. 3.2   Recovering Data from Flash       Application data and stack context data are loaded from the Flash to RAM as described below.     Application Data             During a cold start or a warm start without memory held, once the PDM module has been initialized (see Section 2.2), PDM_eReadDataFromRecord() must be called             for each record of application data in Flash that needs to be copied to RAM.     Stack Context Data             The function PDM_eReadDataFromRecord(), described above, is not used for records of stack context data. Loading this data from the Flash to RAM is handled             automatically by the stack (provided that the PDM has been initialized). 3.3   Deleting Data in Flash         All records (application data and stack context data) in the Flash can be deleted using the function PDM_vDeleteAllDataRecords().          Caution: You are not recommended to delete records of ZigBee PRO stack context data by calling PDM_vDeleteAllDataRecords() before a rejoin of the same secured          network. If these records are deleted, data sent by the node after the rejoin will be rejected by the destination node since the frame counter has been reset on the source          node. For more information and advice, refer to the “Application Design Notes” appendix in the ZigBee 3.0 Stack User Guide. 4.    PDM Features PDM offers a function that can be used to search for a specific record by using the 16-bit record ID. This function is called PDM_GetNVMTableEntry() and the required parameters are the record ID and an output pointer for the found entry. Another available PDM feature is providing a mechanism to safely write the data to NVM. This is done by calling the function PDM_vCompletePendingOperations(), which calls the appropriate NVM function that is used to complete all writings to NVM before any other operation. As an example, user can use this function to make sure that the data is written to the NVM before a reset.
View full article
MIFARE DESFire EV1 supports the APDU message structure according to ISO/IEC 7816-4 for an optional wrapping of the native MIFARE DESFire EV1 APDU format and for the additionally implemented 7816-4 commands from a practical point of view.
View full article