Technology Days - Training Material

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

Discussions

Sort by:
This talk will review the driver, receiver, and common PCB characteristics and show how simulation with IBIS models are used to weigh the trade-offs for the DDR bus design. We will also review the high-speed signal channel and its characteristics and illustrate how the TX and RX circuits in general are used to offset signal losses, and discuss key characteristics of the channels that are needed to allow these TX and RX circuits to work effectively, such as minimizing return loss.
View full article
This session shows how to optimize FreeRTOS™ applications using the MCUXpresso SDK and IDE, including tools as Segger SystemView and Percepio Tracealizer. The  session covers optimizing the RTOS with configuration settings, inspecting stack and run-time using NXP Kernel Awareness, streaming real time data using Segger RTT and SystemView and up to analyzing and optimizing system performance with RTOS and application trace.
View full article
The PF81 and PF82 PMIC family is designed for high-performance processing applications such as infotainment, telematics, clusters, vehicle networking, ADAS, vision and sensor fusion. It is ideal for i.MX 8, i.MX 8X, S32V, and Networking processors in Automotive, Industrial, and Consumer applications. In this session we will offer a detailed overview of the family, its features and advantages of scalability and functional safety
View full article
Creating Graphics on the i.MX RT1060 lab material. The i.MX RT series supports product designs that include advanced multimedia for GUI and enhanced human machine interface (HMI) experience. Its features include advanced 2D graphics acceleration engine, LCD display controllers, camera sensor interfaces, and audio interfaces for high-performance, multi-channel audio streaming. Join this session to learn how to develop graphics on i.MX RT. The attendees in this class will leave with an i.MX RT1060 board on behalf of Digi-Key.  
View full article
Learn from our experiences with thousands of Layerscape customers. We'll share tips and tricks we have learned through designing the NXP LS1012A, LS1043A and LS1046A products, as well as through assisting early adopters. These products are suited for cost and power conscious applications where high core performance and high integration is required. We will also review various tools services and support offered by NXP.
View full article
Hands-on getting started with S32K. Participants will work with bare metal application code, working with an S32K144 development kit and S32 Design Studio. Short presentations followed by hands-on labs. Learn coding secrets for S32K and Arm® Cortex-M!
View full article
This session will take a concentrated look at NXP's Automotive NFC chipset solutions supporting an evolving market where smart phones and wearables used for interacting with the vehicle. From authentication for smart phone car entry to car start to Bluetooth pairing, NFC can enable intuitive functionality encompassing the vehicle.
View full article
GUI Guider is a user-friendly GUI development tool from NXP that enables the rapid development of high quality displays with the open-source LVGL graphics library, and the i.MX RT1170 MCU is a great choice for graphics applications. Learn more about the i.MX RT1170 MCU and see how LVGL and GUI Guider make it easy to design your next embedded GUI. Presenters: Shelby Unger, MCU Ecosystem Product Marketer, NXP Justin Mortimer, Director Mass Market Industrial Edge Processing, NXP
View full article
Introducing the new KE1xZ 5V robust MCUs with Touch and CAN. This class will provide an overview of the new KE1xZ MCUs and give details on the highlighted features of TSI and CAN. A touch demo presentation will also help the attendees understand the TSI measurement and innovate new touch applications.
View full article
SE050: The New Generation of NXP’s Plug & Trust Solutions to Secure Your IoT Services
View full article
This hands-on session explores the MCUXpresso SDK APIs and how to use the SDK to develop your application. Several of the included SDK examples will be utilized.
View full article
This class will show how advanced MPUs and MCUs are made for PMICs and peripheral components.
View full article
This session will introduce the Sensor Toolbox, the complete ecosystem for product development with the NXP sensors. The key focal points would be introducing the IoT Sensing SDK (ISSDK) application development framework, Freedom Sensor Toolbox-Community Edition (STB-CE) and a wide range of the new sensor boards. The highlight of the training would be showcasing multiple STB-CE out of box sensor demonstrations and the steps to get started with IoT Sensing SDK (ISSDK) sensor application development.
View full article
Get immersed in enriched user interfaces with audio, video, voice and vision. Sense how the i.MX 8M portfolio delivers performance, versatility and connectivity to applications as media streaming, voice assistance, edge computing, machine learning/vision and Industrial IoT.
View full article
The presenter gives a detailed introduction of the NXP BLE solutions for Automotive. This session includes the description of the latest standard defined by the BT-SIG, and a clear presentation of the NXP silicon roadmap. The speaker also walks the audience through the development tools required to successfully implement a BLE communication system, with a  specific attention given to applications such as car access and tire pressure monitoring. The attendees leave this session with a call for action that helps them select the right device and quickly move into their own development environment.
View full article
Join this session to understand all the security features integrated in the recently launched LPC5500 MCU Family and learn how to implement these features to design a low-power system with robust security.
View full article
Overview of the i.MX RT family, where to find the related tools, getting started, and where to go for support.
View full article
MCU Alexa Voice, software and tools installation. Learn how to debug and develop code on the MCU all throughout to cloud enablement.
View full article
Whether you are looking for an easy and cost-efficient parametrization solution or want to use a smartphone for ad-hoc diagnosis of a device - Near-field-communication (NFC) makes this possible now. Or you might want to communicate with a fully sealed, batteryless device? Learn in this session about many new use cases, in which NFC simplifies handling, saves cost or enables features which were not possible before in industrial or healthcare applications. With iOS11 now opened up for NFC reading there are more possibilities than you would have imagined!
View full article