テクノロジーデイズ - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

ディスカッション

ソート順:
Security is fast becoming a hot topic in the automotive world, as a foundational element in building connected, and increasingly autonomous vehicles. From secure boot support to higher level functionality enabling leaner & cheaper SW upgrades and protecting OEM IP, you will find out in this session what will the i.MX 8 QM/QX offer as basis to build your secure solutions around it.
記事全体を表示
Products today need to support a wide array of wireless technologies. This session will address the challenges of supporting multiple IoT protocols (BLE® and 802.15.4) on a single device while coexisting with Wi-Fi from another device, all in the same product.
記事全体を表示
An overview of NXP ARM® microcontrollers.
記事全体を表示
Learn more about NFC's co-inventor product proposal and use cases.
記事全体を表示
Using our product demonstration and reference design, this class will teach you how to build your own cloud connected end node with our latest power-efficient LPC54018 flashless MCU. We will use Amazon Web Services (AWS).
記事全体を表示
EUF-NET-T1751 - Layerscape Management Complex firmware is built to enable DPAA2 customers with resource, state and flow management. It is designed specifically for resource allocation and tracking, resource recovery in fault scenarios, and abstraction, virtualization and management of network functions. These networking functions include network interfaces, switches and aggregators, accelerator interfaces, and more. It's also designed specifically for supporting key attributes for objects management like direct access by different software contexts, dynamic discovery of objects, hot plug/unplug and security and isolation between software contexts.
記事全体を表示
An introduction to NXP vCPE solution.
記事全体を表示
Overview of improving RF performance in connectivity.  
記事全体を表示
Automakers and their Tier 1s are bring revolutionary capabilities to the car with new convenience and safety features such as automated driving, Car-to-Car communication, Over-the-Air Updates (OTA) and heads-up displays (HUD). The modern car now demands authentication, identification and separation of critical software components to run in routinely insecure environments for the operational lifespan of the vehicle. By starting with a trusted run-time software foundation as the essential building block, they are designing future scalable platforms on NXP’s i.MX 8 and next-gen S32 processor families for ADAS, automated driving, consolidated integrated cockpit, C2C/V2X, Linux /Android infotainment and safety-critical instrument clusters with GPU accelerated OpenGL graphics.
記事全体を表示
This session introduces our safety power management portfolio. Learn how to develop applications for automotive infotainment and connectivity.
記事全体を表示
Controller area network (CAN) is used to create robust and flexible networks in applications such as industrial automation, motor control, and many others. To take full advantage of CAN, a higher-level protocol like CANopen FD is needed. Join this session to learn how EmSA’s CANopen FD stacks in the MCUXpresso SDK can be combined with other middleware components to create custom applications. We will discuss the steps taken to create an application where acceleration data from an LPC55S16 EVK is transferred to and visualized on an i.MX RT1064 EVK. Presenters: Olaf Pfeiffer, President, EmSA Shelby Unger, MCU Ecosystem Product Marketer, NXP
記事全体を表示
Motion sensor overview and introduction of sensor related application and NXP reference design plus success story for industry IoT and medical market.
記事全体を表示
An update to NXP QorIQ networking ARM 64-bit product and solution.
記事全体を表示
Learn more about the main Wireless protocols and the NXP value proposition for each of them.
記事全体を表示
EUF-HMB-T2472 - Are You Ready for the Next Generation of NFC?  Introduction to NXP Semiconductors  MCU Product Update and Roadmap  NXP Processors for Environmental Contracts and Security  Processor Overview  QorIQ and Layerscape Processor Solutions  Secure Wireless Connectivity Solutions  Sensors Overview
記事全体を表示