テクノロジーデイズ - トレーニング教材

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

ディスカッション

ソート順:
Security is fast becoming a hot topic in the automotive world, as a foundational element in building connected, and increasingly autonomous vehicles. From secure boot support to higher level functionality enabling leaner & cheaper SW upgrades and protecting OEM IP, you will find out in this session what will the i.MX 8 QM/QX offer as basis to build your secure solutions around it.
記事全体を表示
Advanced Graphics Application on i.MX-RT Crossover MCU: Hardware Implementation and TouchGFX Support  Discover New i.MX RT - Security Features_Paris  i.MX-RT: The Disruptive Crossover MCU 
記事全体を表示
Advanced Graphics Application on i.MX-RT Crossover MCU: Hardware Implementation and TouchGFX Support i.MX-RT: The Disruptive Crossover MCU  Security Features on i.MX-RT
記事全体を表示
Secure Connected & Automated Vehicles ETAS: AUTOSAR Toolchain Overview General Overview of the i.MX 8 Family  Getting Ethernet on the Road  Green Hills Software: Trusted Software Foundation for Safe and Secure Automotive Systems on i.MX 8 and S32  i.MX 8QM/QX Security Capabilities  Lauterbach: Debug & Trace for New NXP i.MX 8 and S32 Automotive Processors  Leveraging i.MX 8 Hardware for Automotive Functional Safety Case Study of SafeAssure Display and Rear View Camera 
記事全体を表示
Ethernet is becoming the leading technology for high bandwidth applications such as ADAS and infotainment systems. In this presentation, we will discuss the main use-cases of Automotive Ethernet in the vehicle, review the trends and new upcoming standards such as AVB and TSN and finally discuss what solutions are available from NXP to enable customers to get today.
記事全体を表示
Automakers and their Tier 1s are bring revolutionary capabilities to the car with new convenience and safety features such as automated driving, Car-to-Car communication, Over-the-Air Updates (OTA) and heads-up displays (HUD). The modern car now demands authentication, identification and separation of critical software components to run in routinely insecure environments for the operational lifespan of the vehicle. By starting with a trusted run-time software foundation as the essential building block, they are designing future scalable platforms on NXP’s i.MX 8 and next-gen S32 processor families for ADAS, automated driving, consolidated integrated cockpit, C2C/V2X, Linux /Android infotainment and safety-critical instrument clusters with GPU accelerated OpenGL graphics.
記事全体を表示
This training will take a user from “out of box” to a functioning IoT system including edge devices, gateway/border router, smart phone app and cloud connectivity, then run the system through its paces to highlight a subset of common IoT capabilities. The training will leverage the NXP Modular IoT Framework using a currently shipping, fully documented, Integrated Development Experience for the exercises. Southbound connectivity between gateway and the edge devices will be Thread and ZigBee®. Device commissioning will be via NFC and BLE. Northbound connectivity from gateway to cloud will be Wi-Fi. Cloud support will be via a major cloud provider. Note: Users will be able to use their own Android or iPhone with a recent OS version.
記事全体を表示
The low-power LS1012A is a diverse processor that can be used in many applications, including, IOT, gateways, board management controllers, chassis management and consumer applications. With a 64-bit ARMv8 processor, dual 2.5G MAC, 10 by 10mm package and 1W power, LS1012A may be just the processor you've been looking for. Join this session to explore how others have used LS1012A, and learn more about the tools, software and development platform that make this processor easy to use.
記事全体を表示
Learn how NXP's CodeWarrior Development Tools for ARMv8 architecture can boost your productivity and speed your time to market. The vast array of ARM development tool options can make it a challenge to assemble a tool chain and use it productively. NXP offers a complete integrated development environment based on open source tools and advanced capabilities made possible with NXP specific extensions. CodeWarrior combines the power and versatility of open source GNU tools like gcc and gdb with the GUI usability improvements provided by the development tools based on Eclipse. When basics are completed, CodeWarrior further extends the features portfolio with bare-metal debugging capabilities and a simplified user experience with Linux kernel and u-boot awareness capabilities.
記事全体を表示
Learn from our experiences with thousands of Layerscape customers. We'll share tips and tricks we have learned through designing the NXP LS1012A, LS1043A and LS1046A products, as well as through assisting early adopters. These products are suited for cost and power conscious applications where high core performance and high integration is required. We will also review various tools services and support offered by NXP.
記事全体を表示
In-vehicle wireless charging solutions portfolio overview, automotive grade hardware and software offerings, market success stories, technical description of charging deliver and control, foreign object detection, NFC and AUTOSAR integration, and special considerations for in-vehicle operation.
記事全体を表示
Join this session to learn how to take advantage of the innovative features of LPC84x MCU family, the first of three LPC800 releases planned for 2017. Through product feature training and demonstrations, we will show how these low-power, ARM® Cortex®-M0+ based MCUs offer 8-bit simplicity for today’s entry-level 32-bit microcontroller market. We expect that you will leave this session with the right training and evaluation boards to get started immediately in your own embedded development.
記事全体を表示
Enabling Design, Technologies & Solutions Hands-On Workshop: MCUXpresso Software and Tools  Hands-On Workshop: MCUXpresso Software and Tools_Lab Guide.pdf  Hands-On Workshop: Using MCUXpresso SDK  Introduction to the Next-Generation USB Type-C Connector and NXP’s End-to-End Solution  Irvine: Boost Your Productivity with CodeWarrior® Development Tools for ARM®v8 Architecture  Irvine: LPC800 MCUs Technical Overview: NXP®’s Fastest Growing Portfolio for the Broad, 8-bit Alternative Market  Irvine: Overview of the I3C Interface, Successor of the Well-Known I2C Interface  NXP’s Next-Generation Layerscape Linux® SDK  Payment, Banking & Retail Hands-On Workshop: Solution Card Reader Training: The Purpose and Value of a Solution  Hands-On Workshop: Solution Card Reader Training: The Purpose and Value of a Solution_Lab Guide 1  Hands-On Workshop: Solution Card Reader Training: The Purpose and Value of a Solution_Lab Guide 2  Secure Connected & Automated Vehicles i.MX 8 and 8X Applications Processor Overview  Introduction to Wireless Charging Solutions  Smart Buildings & Consumer Goods Google™ Home and NXP®: Android Things, Google Assistant and Chromecast™ Built-in  Identification and Authentication of Consumables and Accessories via NFC  i.MX 8M Processor Overview and the Road Ahead  Irvine: Modular IoT Framework  Irvine: NFC in Consumer Electronics and Home Appliances  Low-Power i.MX Applications Processors Overview  Secure Authentication for Anti-Counterfeit Applications  Voice Control Solutions: Creating Amazon® Alexa® Devices with i.MX  Smart Networks & Computing How Far Can You Go with NXP's Flexible Layerscape Portfolio?  Learn from Our Experience! Hints, Tips and Tricks to Speed your QorIQ® LS1012A, LS1043A and LS1046A Design Cycle using NXP Support  NXP RF Solutions for IoT to Deliver Reliable, High-Performance Wireless Connections What Can You Build with a 1W 64-bit ARM®v8 SoC? 
記事全体を表示