Technology Days - Training Material

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

Discussions

Sort by:
Whether you are looking for an easy and cost-efficient parametrization solution or want to use a smartphone for ad-hoc diagnosis of a device - Near-field-communication (NFC) makes this possible now. Or you might want to communicate with a fully sealed, batteryless device? Learn in this session about many new use cases, in which NFC simplifies handling, saves cost or enables features which were not possible before in industrial or healthcare applications. With iOS11 now opened up for NFC reading there are more possibilities than you would have imagined!
View full article
This talk will review the driver, receiver, and common PCB characteristics and show how simulation with IBIS models are used to weigh the trade-offs for the DDR bus design. We will also review the high-speed signal channel and its characteristics and illustrate how the TX and RX circuits in general are used to offset signal losses, and discuss key characteristics of the channels that are needed to allow these TX and RX circuits to work effectively, such as minimizing return loss.
View full article
The session will introduce an upcoming xEV traction motor power inverter platform system-play solution featuring a new MCU, new IGBT gate driver, and new safe SBC bound together with system enablement software and ASIL-D compliant safety support. A fully functional traction motor reference design being designed by partner Vepco will also be introduced based on a Power IGBT Module from Fuji Electric. The session will describe the platform’s components, software structure, value proposition, enablement support and go-to-market approach to help enhance understanding of the application and NXP solution as well as how to sell the system platform.
View full article
Learn more about the innovative new industry standard USB Type-C connector offering seamless connectivity of data, video, power and security over a single connector. Usage spans multiple applications from computing and mobile to peripherals and accessories. You will learn about the compelling applications and NXP’s leadership in AC-DC, TC-PC PHY, high-speed switching signal integrity, authentication and power switches product portfolio offering differentiated end-to end Type-C solutions.
View full article
The presenter gives a detailed introduction of the NXP BLE solutions for Automotive. This session includes the description of the latest standard defined by the BT-SIG, and a clear presentation of the NXP silicon roadmap. The speaker also walks the audience through the development tools required to successfully implement a BLE communication system, with a  specific attention given to applications such as car access and tire pressure monitoring. The attendees leave this session with a call for action that helps them select the right device and quickly move into their own development environment.
View full article
Overview of an open battery management system reference design planned for PX4 enabled drones and Hovergames.com. Alternative use cases, unique features, and collaborative development challenges. Plans for battery health and open SW platform.
View full article
Introducing the new KE1xZ 5V robust MCUs with Touch and CAN. This class will provide an overview of the new KE1xZ MCUs and give details on the highlighted features of TSI and CAN. A touch demo presentation will also help the attendees understand the TSI measurement and innovate new touch applications.
View full article
Whether you are looking for an easy and cost-efficient parametrization solution or want to use a smartphone for ad-hoc diagnosis of a device - Near-field-communication (NFC) makes this possible now. Or you might want to communicate with a fully sealed, batteryless device? Learn in this session about many new use cases, in which NFC simplifies handling, saves cost or enables features which were not possible before in industrial or healthcare applications. With iPhones now also enabled for NFC reading there are more possibilities than you would have imagined!
View full article
This session will provide an overview of the NXP wireless charging solutions portfolio with integrated NFC communication in wireless charging transmitters. Attendees will receive a clear understanding about NXP’s state of the art transmit and receive reference designs available for automotive, consumer, appliance and infrastructure markets.
View full article
As memory interface data rates increase, so does the need for ensuring proper margins have been designed into the system’s usage of that interface. One way Micron has studied the system’s usage of the memory interface is through Timing & Signal Analysis (TSA). A TSA attaches physical hardware to the memory device to observe a subset of the memory interface as operated by the system. Another approach to memory interface is Virtual TSA (vTSA). This method uses the memory controller’s training algorithms to provide margin information without the use of physical test hardware. This method allows characterization of the entire memory interface. This session will compare and contrast the two different methods, and will ultimately demonstrate the value of integrating vTSA tools on the system platform. We intend to reference actual results from the latest i.MX 8 QXP board.
View full article
MCUupdate_public version.pdf Next generation of NFC_Tech Days Lyon & Strasbourg_May 2016-02.pdf  NXP - i.MX Latest NPI Introduction_non NDA .pdf Sensors_Multimarkets_may16.pdf Thread tech days.pdf USB_TypeC_Portfolio Presentation (Tech Days Lyon & Strasboug - May 2016)....pdf
View full article
Join this session to understand all the security features integrated in the recently launched LPC5500 MCU Family and learn how to implement these features to design a low-power system with robust security.
View full article
Motion sensor overview and introduction of sensor related application and NXP reference design plus success story for industry IoT and medical market.
View full article
Learn more about In-Vehicle networking, safety and power management as well as drivers and energy solutions from NXP.
View full article
Overview of Kinetis new products, KE+, security with K8x & KL8x. 
View full article
Learn more about NFC's co-inventor product proposal and use cases.
View full article
EUF-DES-T1741 - Scalable Multicore QorIQ Layerscape Processors Based on 64-bit Software Environment for Enterprise, Home and Industrial Applications
View full article
Discover NXP’s Layerscape multicore 64-bit ARM®-based solutions and learn how this scalable family leverages line-rate networking and production grade software to accelerate your time-to-market in industrial, networking and consumer applications.
View full article
This training will take a user from “out of box” to a functioning IoT system including edge devices, gateway/border router, smart phone app and cloud connectivity, then run the system through its paces to highlight a subset of common IoT capabilities. The training will leverage the NXP Modular IoT Framework using a currently shipping, fully documented, Integrated Development Experience for the exercises. Southbound connectivity between gateway and the edge devices will be Thread and ZigBee®. Device commissioning will be via NFC and BLE. Northbound connectivity from gateway to cloud will be Wi-Fi. Cloud support will be via a major cloud provider. Note: Users will be able to use their own Android or iPhone with a recent OS version.
View full article
Enabling Design, Technologies & Solutions Hands-On Workshop: MCUXpresso Software and Tools  Hands-On Workshop: MCUXpresso Software and Tools_Lab Guide.pdf  Hands-On Workshop: Using MCUXpresso SDK  Introduction to the Next-Generation USB Type-C Connector and NXP’s End-to-End Solution  Irvine: Boost Your Productivity with CodeWarrior® Development Tools for ARM®v8 Architecture  Irvine: LPC800 MCUs Technical Overview: NXP®’s Fastest Growing Portfolio for the Broad, 8-bit Alternative Market  Irvine: Overview of the I3C Interface, Successor of the Well-Known I2C Interface  NXP’s Next-Generation Layerscape Linux® SDK  Payment, Banking & Retail Hands-On Workshop: Solution Card Reader Training: The Purpose and Value of a Solution  Hands-On Workshop: Solution Card Reader Training: The Purpose and Value of a Solution_Lab Guide 1  Hands-On Workshop: Solution Card Reader Training: The Purpose and Value of a Solution_Lab Guide 2  Secure Connected & Automated Vehicles i.MX 8 and 8X Applications Processor Overview  Introduction to Wireless Charging Solutions  Smart Buildings & Consumer Goods Google™ Home and NXP®: Android Things, Google Assistant and Chromecast™ Built-in  Identification and Authentication of Consumables and Accessories via NFC  i.MX 8M Processor Overview and the Road Ahead  Irvine: Modular IoT Framework  Irvine: NFC in Consumer Electronics and Home Appliances  Low-Power i.MX Applications Processors Overview  Secure Authentication for Anti-Counterfeit Applications  Voice Control Solutions: Creating Amazon® Alexa® Devices with i.MX  Smart Networks & Computing How Far Can You Go with NXP's Flexible Layerscape Portfolio?  Learn from Our Experience! Hints, Tips and Tricks to Speed your QorIQ® LS1012A, LS1043A and LS1046A Design Cycle using NXP Support  NXP RF Solutions for IoT to Deliver Reliable, High-Performance Wireless Connections What Can You Build with a 1W 64-bit ARM®v8 SoC? 
View full article