技术日 - 培训资料

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

讨论

排序依据:
Learn about NXP's S32V family for vision processing, with a special focus product architectures and software (enablement and application level). You will also see real application use case examples using APEXCV Libraries and EVB.
查看全文
AWS Greengrass - Labs 3-4
查看全文
Emerging Connected and Automated Vehicles (CAVs) require far more compute horsepower, more memory bandwidth, and more high speed IO connectivity than the vehicles in show rooms today. Digital Networking processors are the highest performance processors in NXP, and they aren't just for networking! These devices are also used in safety critical applications like avionics, industrial automation and smart grid. Come learn more about where DN Layerscape processors fit in CAVs!
查看全文
Automakers and their Tier 1s are bring revolutionary capabilities to the car with new convenience and safety features such as automated driving, Car-to-Car communication, Over-the-Air Updates (OTA) and heads-up displays (HUD). The modern car now demands authentication, identification and separation of critical software components to run in routinely insecure environments for the operational lifespan of the vehicle. By starting with a trusted run-time software foundation as the essential building block, they are designing future scalable platforms on NXP’s i.MX 8 and next-gen S32 processor families for ADAS, automated driving, consolidated integrated cockpit, C2C/V2X, Linux /Android infotainment and safety-critical instrument clusters with GPU accelerated OpenGL graphics.
查看全文
This session will take a concentrated look at NXP's Automotive NFC chipset solutions supporting an evolving market where smart phones and wearables used for interacting with the vehicle. From authentication for smart phone car entry to car start to Bluetooth pairing, NFC can enable intuitive functionality encompassing the vehicle.
查看全文
An introduction to NXP vCPE solution.
查看全文
This session introduces new low cost S32V system-on-module (SOM) board from MicroSys for vision processing. Class also walks through complete hardware and software ecosystem with hands-on approach. These boards include support with QNX, LDW demo and many other demos.
查看全文
Come learn about the components required for IoT Gateways. Gateways must support low power wireless protocols to end nodes, such as Bluetooth®, ZigBee®, Thread, or LoRa and then support a WAN connection through LTE, Wi-Fi or Ethernet.  Any IoT design today must be designed for security from the ground up, see how these demands shape hardware and software decisions.
查看全文
Introduction to RCI for NXP's RF products, Lizard, MantraCS, MantraF. System integration and development made easy using the RCI firmware together with the Configuration Development Kit (CDK).
查看全文
Edge computing puts cloud-computing software infrastructure on embedded-class processing platforms to reduce latency and uplink bandwidth consumption. Ranging from 1-core to 16-core devices, integrating important I/O features and integrating a hardware root of trust, the Layerscape family is ideal for edge-computing platforms. Complementary software like EdgeScale increases these platforms ease of use and accelerates customers' time to market. This session provides an overview of running Edge compute applications on Layerscape family of processors. It covers the concept of Edge computing and why it is needed, and goes on to elaborate the various use-cases where it can be used. It explains how customers can use the Layerscape SDK to run container based Edge compute applications, and leverage popular Edge Compute frameworks from AWS, Azure, Alibaba amongst others.
查看全文
This class will provide an overview of the i.MX RT series, key peripheral, including a demo using the i.MX RT EVK.
查看全文
Design, Software & Services EUF-DES-T2474 - Interface Solutions  Insight & Innovation EUF-INS-T2477 - Sensor Update  Secure Connected & Automated Vehicles Advanced Analog Products for Automotive and Industrial Markets  EUF-AUT-T2475 - Analog Products  Secure Mobile, Healthcare & Wearables EUF-MHW-T2470 - Wireless Solutions  Smart Home & Buildings EUF-HMB-T2472 - Are You Ready for the Next Generation of NFC?  Smart Networks EUF-NET-T2471 - Layerscape Update 
查看全文
Business Line Smart Antenna Solution delivers a broad range of RF products for many different applications ranging from mobile phones to wireless infrastructure. All these applications require high performance RF products to deliver reliable, high data rate connections. This training will show how our RF products can be successfully used in IoT applications to improve the RF connection: range extension by using LNAs in the receive chain or by adding a PA at the transmit side. Our wide product portfolio ensures that  the different needs of IoT (frequency range, power consumption and performance gain) can be met.
查看全文
Join this session to learn how to leverage and get started with NXP’s power optimized LPC546xx MCU family, which now scales up in performance to 220 MHz. With rich peripheral integration, which includes 21 communication interfaces, including HS USB, dual CAN FD, graphics controller, to package option scalability, these microcontrollers address the various needs of today’s embedded IoT applications. Leave the session with the knowledge and skills to get up and running with the LPC546xx MCU family, which includes our comprehensive ecosystem of software and tools.
查看全文
Expect your platform to boot in less than one second...do your customer's demand it? Even if that is not fast enough for some cases...we will discuss what can be done to improve the booting performance. Learn from the experts on how to architect and optimize the boot process from boot ROM, boot loader through to OS and applications.
查看全文
VortiQa-IVAS-T1747 - VortiQa IVAS (Intelligent Virtulization Acceleration Software) is an accelerated NFVI (Network Functions Virtualization Infrastructure)
查看全文
Building on its 10+ year of industry-leading innovation, an exciting future is in store for the LPC portfolio. Join this session to learn more about the renewed LPC roadmap and take a closer look into the power advantages offered with by the latest family introduced – the LPC546xx MCU family.
查看全文