Sensors Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sensors Knowledge Base

Labels

Discussions

Sort by:
Hi Everyone, In this document I would like to present a very simple example code I created for the PCT2075. This I2C digital temperature sensor offers a resolution of 0.125°C with an accuracy of ±1°C over -25°C to 100°C range. It operates with a single supply from 2.7V to 5.5V and has three address pins, allowing up to 27 devices to operate on a single I2C bus without address collisions. The device also includes an open-drain output (OS) which becomes active when the temperature exceeds the programmed limits. NXP offers the PCT2075DP Arduino Shield and GUI for easy evaluation of this temperature sensor. However, I have decided to pair this demo board with the LPC55S06-EVK and create a simple example code in the MCUXpresso IDE using Config tools (Pins, Clocks and Peripherals). The connection is very straightforward. The PCT2075DP-ARD daughter board is inserted to J9, J10, J12 and J13 connectors located on LPC55S06-EVK development board. Both SDA pin (J1-5) and SCL (J1-6) lines are connected through the on-board 5.6K pull-up resistors to the FlexComm1 SDA (PIO0_13, J13_9) and SCL (PIO0_14, J13_11) pins on the LPC55S06-EVK board. The VCC pin (J6-4) is connected to the 3.3V supply voltage and the GND pin to common ground. The address select pins A0, A1 and A2 are connected to GND using jumpers between pins 2 and 3 of J7, J8 and J9, resulting in a 7-bit I2C slave address of 0x48. I created a new project in MCUXpresso IDE v11.3.0 based on SDK_2.8.2_LPCXpresso55S06 using the New project wizard:   It was not necessary to make any changes to the project and I named it LPC55S06 PCT2075 Temp reading using I2C in the wizard:   Let’s start with the Pins Config tool...:   ...to configure PIO0_13 and PIO0_14 for their I2C functions (I2C_SDA and I2C_SCL, respectively). Simply search for each pad in the Pins view:   In the diagram above, I already have PIO0_13 routed for I2C function (it is showing green). However, you may want to check the checkbox in the first column to mark the pin for routing. A dialog pops up, offering you all the possible pin multiplex functions for the pad. Scroll down through the list and select FlexComm1’s SDA function:   When you put a checkmark (“tick”) in the FC1_CTS_SDA row, the Pins Config tool routes the pad and you will see a new entry (in yellow) in the Routed Details view at the bottom of the perspective:   Follow the same procedure to route PIO0_14 for function FC1_SCL. That is already done in the screen-grab above, so I am ready to move to the Peripherals Config tool.  Use the Peripherals icon to switch to the Peripherals perspective:   The Peripherals Config tool identifies that I have set up the pads/pins for FlexComm1 to be used as I2C. But I have not yet set up the I2C peripheral, and so the tool reports a Warning:   There is a very simple fix, proposed by the tool. Select the FLEXCOMM1 warning line, and right-click to bring up a context menu:   Selecting “Initialize FLEXCOMM1 peripheral” opens a dialog where I can select the desired function for FlexComm1… in this case I want I2C configuration. So I select I2C and click [OK]:   The Peripherals Config tool displays the Flexcomm Interface I2C configuration screen. This shows all of the ‘top level’ settings for the I2C module. I configured it as follows:   As the PCT2075 does not have a data ready interrupt, I use the MicroTick (UTICK0) timer to read the Temp register periodically at a fixed rate of about 10Hz since the temp-to-digital conversion is executed every 100 ms. The UTICK0 is configured in the Peripherals Config tool as follows:   I am ready to move to the final, Clocks Config tool:   I chose to use the BOARD_BootClockFRO12M() functional group:   Then I enabled the clock to FlexComm1, since this is the FlexComm module that I use for I2C. I used the fro_12m as the clock source for FlexComm1 I2C:   Finally I enabled the fro_1m and attached the fro_1m to the UTICK timer:   All the configuration is now complete. I can click “Update Code” at the top of the screen to generate all of the necessary configuration code, accept the changes, and return to the C/C++ Develop perspective. In the UTICK0_Callback function, the Temp register is read and then the real temperature in °C is calculated as shown below. For more information on how to convert the raw values from the Temp register to real values in °C, please refer to the PCT2075 data sheet (Chapter 7.4.3).   This screenshot shows the two bytes read of the Temp register (0x00).    The calculated temperature can be watched either in the "Global Variables" window on the top right of the Debug perspective...:   ...or in the Console window:   Attached you can find the complete project developed in the MCUXpresso IDE v11.3.0. If there are any questions regarding this simple application, please feel free to ask below.   Regards, Tomas
View full article
As we develop videos on Sensor subjects for posting to QUMU and YouTube, these guidelines are a quick reminder of some important production points to remember. These lessons are relevent for any video content we develop.
View full article
The FRDM33772BSPIEVB serves as a 6-channel and FRDM33771BSPIVB as a 14 channel battery cell controller with a passive cell balancing. A FRDM-KL25Z evaluation board is used for communication with FRDM3377xBSPIEVB and a computer through SPI interface. The kit together with BATT-6EMULATOR 6-cell battery emulator  for the FRDM33772BSPIEVB and BATT-14EMULATOR 14-cell battery emulator for FRDM33771BSPIVB or a battery pack BATT-14AAAPACK for either of them is dedicated to support customer development and evaluation. For a status reading and settings an MC3377x EvalGUI is used. Figure 1. FRDM33771SPI evaluation board Figure 2. BATT-14AAAPACK battery pack Figure 3. BATT-14EMULATOR to supply MC33771 EVBs MC3377x EvalGUI The Graphic User Interface MC3377x EvalGUI is intended to use for evaluation of MC3377x cell controllers. Figure 4. MC3377x Evaluation GUI version 4.02 Hardware setup The GUI supports two types of BMS architectures. Central, only one cluster and distributed, up to 15 clusters. For the central BMS architecture an MC33771 EVB or MC33772 EVB must be stacked on top of an FRDM-KL25Z board. One of the battery emulators or the battery pack is connected through a 34-pin cells connector. For the distributed BMS architecture a MC33664 evaluation board stacked on top of a FRDM-KL25Z is used. The MC3377x evaluation boards are connected to the MC33664 EVB through a twisted pair TPL bus. Connection to a computer is made through OpenSDA port on FRDM-KL25Z and USB on the computer side. Figure 5. FRDM-33771SPIEVB stacked on top of FRDM-KL25Z and BATT-14AAAPACK connected as central BMS architecture After hardware setup is done start the MC3377x EvalGUI and follow instructions for Initial Configuration in MC33771/772 Evaluation GUI Documentation. For access click info->Open docu in MC33771/772 Evaluation GUI. Figure 6. Access to MC33771/772 Evaluation GUI document When the initial configuration is done, voltage reading of every battery cell and overall voltage of all connected batteries in series is enabled. However current measurement is disabled by default. Figure 7. Battery cells measurement with current measurement disabled Enablement of current measurement is done in Cluster view by setting a Bit9 (IMeasEn) in in SYS_CFG1 register to logic 1. The field changes from dark green to  light green and the current measurement is enabled. Figure 8. Enablement of the current measurement Figure 9. Current measurement enabled Current in the GUI is displayed in mV and for the current consumption has to be calculated. Because shunt resistor is Rshunt=100mΩ and measured voltage 1.243mV, thus for this case the current consumption is I=Ushunt/Rshunt = 12.43mA. The shunt resistor has to be chosen so the voltage doesn’t exceed +/-150mV. The voltage is sensed on SENSE_P and SENSE_N pins of the MC3377x controller. Figure 10. Shunt resistor R1 on the BATT-14AAAPACK It’s also possible to use a resistor in the battery pack as a load. The resistor is not populated. Recommended value is 1kΩ, 3W , SMT 2512. The resistor can be connected and disconnected with SW3 switch. Figure 11. Recommended load resistor R7 and toggle switch SW3
View full article
Hi Everyone,   In this document I would like to present a very simple bare-metal example code I created for the LM75A. This I 2 C digital temperature sensor offers an improved resolution of 0.125°C with an accuracy of ±2°C from –25°C to 100°C and ±3°C over –55°C to 125°C. It operates with a single supply from 2.8V to 5.5V and has three address pins, allowing up to eight LM75A devices to operate on a single I 2 C bus without address collisions. The device also includes an open-drain output (OS) which becomes active when the temperature exceeds the programmed limits.   NXP offers the OM13257 temperature sensor daughter card for easy evaluation of most NXP’s temperature sensors including the LM75ADP in a small 8-pin TSSOP8 package. The daughter card is shipped with no temperature sensors soldered to the board, so the LM75ADP needs to be purchased and soldered separately. The daughter board is designed to connect directly to the OM13320 Fm+ Development kit, but I have decided to pair it with one of the most popular Freedom development boards – FRDM-KL25Z.   The wiring is very straightforward as shown on the picture below. Both SCL (JP4-2) and SDA (JP3-2) lines are connected through the on-board 10K pull-up resistors to the I2C1 module (PTE1 and PTE0 pins) on the KL25Z128 MCU. The Vcc pin (JP2-2) is connected to the 3.3V supply voltage and the GND pin to common ground. The address select pins A2, A1 and A0 are connected to GND using jumpers between pins 1 and 2 of JP12, JP11 and JP10, resulting in a 7-bit I 2 C slave address of 0x48.       The LM75A does not have a data ready interrupt, so the PIT (Periodic Interrupt Timer) module is used to read the Temp register periodically at a fixed rate of about 10Hz since the temp-to-digital conversion is executed every 100 ms. The MCU is configured as follows.   /************* MCU initialization function ******/   void MCU_Init(void) {   //I2C1 module initialization SIM_SCGC4 |= SIM_SCGC4_I2C1_MASK; // Turn on clock to I2C1 module  SIM_SCGC5 |= SIM_SCGC5_PORTE_MASK; // Turn on clock to Port E module  PORTE_PCR1 |= PORT_PCR_MUX(6); // PTE1 pin is I2C1 SCL line PORTE_PCR0 |= PORT_PCR_MUX(6); // PTE0 pin is I2C1 SDA line I2C1_F  |= I2C_F_ICR(0x14); // SDA hold time = 2.125us, SCL start hold time = 4.25us, SCL stop hold time = 5.125us   I2C1_C1 |= I2C_C1_IICEN_MASK; // Enable I2C1 module     //PIT initialization    SIM_SCGC6 |= SIM_SCGC6_PIT_MASK; // Turn on clock to to the PIT module   PIT_LDVAL0 = 1048000; // Timeout period = 100 ms   PIT_MCR = PIT_MCR_FRZ_MASK; // Enable clock for PIT, freeze PIT in debug mode PIT_TCTRL0 = PIT_TCTRL_TIE_MASK | // Enable PIT interrupt   PIT_TCTRL_TEN_MASK; // and PIT     //Enable PIT interrupt on NVIC NVIC_ICPR |= 1 << ((INT_PIT - 16) % 32); NVIC_ISER |= 1 << ((INT_PIT - 16) % 32); }       In the PIT ISR, the Temp register is read and then the real temperature in °C is calculated as shown below. For more information on how to convert the raw values from the Temp register to real values in °C, please refer to the LM75A data sheet (chapter 7.4.3).   /******** Interrupt handler for PIT ************/   void PIT_IRQHandler() {   PIT_TFLG0 |= PIT_TFLG_TIF_MASK; // Clear the PIT interrupt flag I2C_ReadMultiRegisters(LM75A_I2C_ADDRESS, TEMP_REG, 2, TemperatureData); // Read LM75A Temperature register (MSB + LSB)    Temperature_11_bit = ((short) (TemperatureData[0]<<8 | TemperatureData[1])) >> 5; // Compute 11-bit temperature output value   Temperature = ((float) Temperature_11_bit) * 0.125; // Compute temperature in °C }       The screenshot below shows the two bytes read of the Temp register. It also illustrates how the OS output is activated in interrupt mode by crossing the Tos threshold value stored in the Tos register. The threshold value was set to 26°C, which corresponds to 16-bit value of 0x1A00 read out of the Temp register.       The calculated temperature can be watched in the "Variables" window on the top right of the Debug perspective or in the FreeMASTER application. To open and run the FreeMASTER project, install the FreeMASTER 2.0 application and FreeMASTER Communication Driver. You can try touching your finger to the sensor to see the temperature rise.         Attached you can find the complete source code written in the CW for MCU's v10.6 including the FreeMASTER project.   If there are any questions regarding this simple application, please feel free to ask below. Your feedback or suggestions are also welcome.   Regards, Tomas Original Attachment has been moved to: FreeMASTER---FRDM-KL25Z-LM75A-Temperature-reading-using-I2C.rar Original Attachment has been moved to: FRDM-KL25Z-LM75A-Temperature-reading-using-I2C.rar
View full article
This document provides answers for some of the common questions received by the Technical Support team about some inquiries with the usage of the CRTOUCH GUI.
View full article
clicktaleID