S32K ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K Knowledge Base

ラベル

ディスカッション

ソート順:
****************************************************************************************************  Detailed Description:  The current RTD RTM 2.0.0 does not support overflow notification  if EMIOS ICU is used in the Edge Detect mode.  Workaround is to use another channel in ECU mode  clocked by the same counter bus as the ICU channel.  Emios_0 input clock: 48MHz CORE_CLK  MCL EMIOS_0_Ch_23 (BUS_A)  Global clock devider: 48  MCB prescaler: 1  MCB clock: 1MHz  MCB tick: 1us  MCB period: 65_535 ticks  Both OCU (Emios_0_Ch0) and ICU (Emios_0_ch3) use the same BUS_A counter clock.  GPIO generated PWM period: ~0.5s  That's 500_000 ticks  ICU routed to PTB0  GPIO PWM to PTB1  -----------------------------------------------------------------------------------------------  Test HW: S32K3X4EVB-Q172  MCU: S32K344  Debugger: S32DS 3.4, PEMicro Multilink rev.C  Target: internal_FLASH ****************************************************************************************************
記事全体を表示
************************************************************************************************************************** * Detailed Description: * * Connect PTC24 (PWM) to PTC25 (IC) * * PWM signal generated by EMIOS_1_ch0 (in OPWFMB mode) is measured by EMIOS_1_ch_1 (IPWM mode). * * EMIOS_1 global global clock (core clock = 48MHz) prescaled in EMIOS_Mcl driver (/48) = 1MHz. * * BUS_A generated by EMIOS_1_ch_23 * Tick = 10us (1MHz global clock prescaled by 10 = 100kHz) * * PWM (OPWFMB), EMIOS_1_ch_0, PTC24 * Tick = 10us (1MHz global clock prescaled by 10 = 100kHz) * * IC (IPWM), EMIOS_1_ch_1, PTC25 * Clocked by BUS_A * Tick = 10us * * ------------------------------------------------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K344 * Debugger: S32DS 3.4, PEMicro Multilink rev.C * Target: internal_FLASH **************************************************************************************************************************
記事全体を表示
Hi,    Firstly, you should get the flash block size of your S32K3xx. Table in RM could be the reference. OliverTian_0-1641979572873.png    Secondly, you should know that there are super sector and sector in S32K3xx.   Sector                    Subdivision of the Flash Block that is independently erasable. Sector Size is always 8 KB. Super sector          Subdivision of the flash block that includes a group of sectors. Super Sector Size is always 64 KB, and consists of 8 sectors.    Thirdly, based on the information of PFCBLKx_SSPELOCK in RM, you can calculate the numbers of super sector and sector in each flash block.   OliverTian_2-1641979572947.png For example in S32K312, it has 2MB flash totally and each block is 1MB. So, in each 1MB, its first 768KB is with super sector granularity. The numbers of super sector is 768/64=12; the followed sector number is 256/8=32. Cheers! Oliver
記事全体を表示
******************************************************************************** * Detailed Description: * * FlexIO module is configured for UART RX and TX function. * Timer 0 and Shifter 0 is used for UART TX function. * Timer 1 and Shifter 1 is used for UART RX function. * Timer 2 is used for idle detection. * Baud rate = 115200 * HW connection: PTA0 - TX, PTA1 - RX, PTA7 is used to signalize idle detection. * Connect PTA0 and PTA1 to create external loopback for this test. * ------------------------------------------------------------------------------ * Test HW: S32K144EVB * MCU: FS32K144HAMLL 0N57U * Fsys: 80MHz * Debugger: Lauterbach Trace32 * Target: internal_FLASH ********************************************************************************
記事全体を表示
Some customers inquire about the FreeMASTER JumpStart Project mentioned in the Get Started with the S32K1xxEVB. So here to talk about the problems you may encounter and how to solve them. FreeMASTER JumpStart project download.png Where to download FreeMASTER JumpStart Project Customers may not find where to download FreeMASTER JumpStart Project at the moment. It should be downloaded from the Embedded Software under Design Resources of the development board. But the download link of S32K142EVB \ S32K144EVB \ S32K146EVB is missing. Design Resources Embedded Software.pngWe can search the keywords “* JumpStart” at www.nxp.com download embedded application software and PC host application software that you need. Search JumpStart.png Which version of S32 Design Studio should be used The readme file will tell us which version of S32 Design Studio the project was created. For example: the readme in the S32K144_EVB_JumpStart_Firmware package shows that the project for S32K14x EVB JumpStart SW was created in S32 Design Studio for ARM v2.0. created in S32 Design Studio for ARM v2.0.png Which version of SDK should be used You may get the Validation of S32K144_EVB_JumpStart_Firmware Kinetis SDK project when import the project : The project S32K144_EVB_JumpStart_Firmware was created for Kinetis SDK SDK_S32K14x_08 which is not installed in this product (repository SDK_S32K14x_08 not found).  S32K144_EVB_JumpStart_Firmware SDK_S32K14x_08.pngThe chapter Version Tracking of S32SDK_for_S32K1xx_RTM_3.0.3_ReleaseNotes shows that the SDK_S32K14x_08 means EAR 0.8.5. Version Tracking S32SDK_for_S32K1xx_RTM_3.0.3_ReleaseNotes.pngBy default only S32 SDK EAR 0.8.4 is installed in S32DS for ARM 2.0, so we need to update the S32 Design Studio for Arm® v2.0 Update 2 – S32 SDK 0.8.5 EAR & MQX by refer S32 Design Studio for Arm v2.0 - Update 2 available S32DS_ARM_v2.0_UP2_K14x_SDK_085_MQX_170928.png Incorrect UART baud rate setting The baud rate selected for LPUART in Processor Expert is 600 by default, which does not match the description in the readme file. 600 is not in the FreeMASTER serial port baud rate support list, so let us reconfigure the baud rate to 115200 and then click Generate Processor Expert Code. select Baudrate 115200.png Generate Processor Expert Code.pngWhen connect S32K144EVB with FreeMASTER by UART, you can see that the Baud rate 300 is not in the support list. This is the reason why using the default configuration of S32K144_EVB_JumpStart_Firmware is not able to connect with FreeMASTER. Probing UART Ports.png      
記事全体を表示
Some customers inquire how to use FreeMASTER with S32K3. But there is no exists example projects which demonstrate usage of the FreeMASTER serial communication driver in S32K3 Real Time Drivers at the moment. So this article will introduce how to use FreeMaster SDKs in S32K3 RTD 0.9.0. Download S32DS \ S32K3 Development Package \ RTD (SDK) \ FreeMASTER Driver Login your account on NXP website, and download the S32K3 Standard software from TOOLS &SOFTWARE of S32K3 webpage. If you have already installed the S32DS3.4 \ S32K3 Development Package 3.4.0 \ RTD 0.9.0, then you can skip the following part and start directly from 4.Install FreeMASTER Driver 3.0 for S32K3 S32K3 Standard Software.png Download S32DS S32K3 Development Package RTD FreeMASTER Driver.png Install S32K3 Development Package 3.4.0 After install the S32 Design Studio v3.4, we should install S32K3 Development Package 3.4.0(SW32K3_S32DS_3.4.0_D2012.zip): go to menu "Help" -> "Install New Software" and click on "Add..." button Add Repository.png Here we uncheck S32 Design Studio S32K3 SDK (RTD S32K3 0.8.1), because we will install the newer version S32K3 RTD 0.9.0 later. Install New Software SW32K3_S32DS_3.4.0_D2012.png Install S32K3 Real Time Drivers Version 0.9.0 S32K3 Real Time Drivers Version 0.9.0 can be installed by refer the Offline Package Installation Setup of S32DS Extensions & Updates: Explanation and How To Use. Offline Package Installation Setup S32K3 Real Time Drivers Version 0.9.0.png S32K3 RTD AUROSAR 4.4 Version 0.9.0 selected.png Install FreeMASTER Driver 3.0 for S32K3 Offline Package Installation Setup FreeMASTER Driver 3.0 for S32K3.png FreeMASTER Driver 3.0 for S32K3 selected RTD090.png Attach FreeMASTER_S32K3 to S32K344_UART_Printf_Sample_090_34 The reason for choosing the S32K344_UART_Printf_Sample_090_34 project to demonstrate the combination of FreeMaster SDKs is that the project has already configured the LPUART of the S32K3X4EVB-Q257 development board. S32K3_EVB defined symbols.png Attach FreeMASTER_S32K3.png Select LPUART peripheral as host communication Through the description in the Requirements and Release Description chapter of FreeMASTER Driver Release Notes(FMSTRS32K3RN), we can see that currently only UART interface is supported. The S32K3 FreeMASTER 3.0 version 1.0.0 only support NXP GCC 6.3 or 9.2 for ARM at the moment, but the latest S32K3 Real Time Drivers Version 1.0.0 is based on NXP GCC 10.2.0. This is the reason why RTD 0.9.0 is selected in this article.  Requirements and Release Description FMSTRS32K3RN.png The README.txt also shows that: Current package provides FreeMASTER Communication Driver support for S32K344 over LPUART module README include_freemaster.png  LPUART13 is selected in this project for S32K3X4EVB-Q257, so we need to define the base address for FreeMASTER: #define FMSTR_LPUART_BASE           0x404A0000 define FMSTR_LPUART_BASE.pngModify the main function according to the README.txt: main.png Connect FreeMASTER3.1 to S32K3X4EVB-Q257 board Here we can see that the FreeMASTER3.1 is connected to S32K3X4EVB-Q257 board. connected.png  
記事全体を表示
******************************************************************************** * Detailed Description: * * Example shows possible setting for PWM duty cycle update using DMA. * FTM0 ch0 is set to Edge aligned mode with 20KHz period. * Initialization trigger is routed back to HW trigger 1 using TRGMUX, so this HW * trigger can be used for CnV synchronization. * DMA on FTM0 ch0 is enabled (on ch0 CHF flag) and DMA ch0 configured to update C0V * from duty cycle variable. * NOte CHF is not set for 0% and 100% duty cycle, thus no DMA trigger is generated. * * Green LED is dimming as duty is changing. * * ------------------------------------------------------------------------------ * Test HW: S32K118EVB-Q64 * MCU: PS32K118LAMLH 0N97V * Compiler: S32DS.ARM.2.2 * SDK release: S32SDK_S32K1xx_RTM_3.0.3 * Debugger: Lauterbach, OpenSDA * Target: internal_FLASH * ******************************************************************************** Revision History: 1.0 Sep-16-2021 Petr Stancik Initial Version *******************************************************************************/
記事全体を表示
The purpose of this demo application is to show you the usage of the FlexCAN module configured to use Flexible Data Rate using the S32 SDK API. - In the first part, the application will setup the board clocks, pins and other system functions such as SBC if the board uses this module as a CAN transceiver. - Then it will configure the FlexCAN module features such as FD, Bitrate and Message buffers - The application will wait for frames to be received on the configured message buffer or for an event raised by pressing one of the two buttons which will trigger a frame send to the recipient. - Pressing SW3 button of board 1 shall trigger a CAN transfer that results in toggling the RED led on board 2. - Pressing SW2 button of board 1 shall trigger a CAN transfer that results in toggling the GREEN led on board 2. - This demo application requires two boards, one configured as master and the other one configured as slave (see MASTER/SLAVE defines in application code) or single board connected with CAN tool. - Both the event and error callbacks are installed, callback_test variable indicates event entering bit0 .. RX complete bit1 .. TX complete bit2 .. ERR INT flag set bit3 .. BOFF INT flag set - to enter bus off simply short CANH with GND and send message using either SW1 or SW2, FlexCAN enters bus off (error event) and blue LED is ON. Also TX MB is aborted. Remove short connection and send message again normally, blue LED is off.   ------------------------------------------------------------------------------ * Test HW: S32K144EVB-Q100 * MCU: FS32K1441 0N57U * Compiler: S32DS.ARM.2.2 * SDK release: S32SDK_S32K1xx_RTM_3.0.3 * Debugger: Lauterbach, OpenSDA * Target: internal_FLASH  
記事全体を表示
Due to K3 hasn't been mass-produced yet, this content is moved to S32K3 Internal forum: https://community.nxp.com/t5/S32K3-Internal-Community/S32K3-Low-power-lab/ta-p/1280219 Any question, pls contact [email protected].
記事全体を表示
******************************************************************************** * File: main.c * Owner: David Tosenovjan * Version: 0.0 * Date: Mar-12-2021 * Classification: General Business Information ******************************************************************************** * Detailed Description: * Example code configures the whole 4kB FlexRAM area for SRAM use. * By default or after mass erase, S32K1 device has only address range * 0x1400_0000-0x1400_0DFF (3.5kB) accessible for SRAM use. * To enable remaining 0.5kB it is needed to perform Program Partition Command * (with the setting shown in the example), but only once with the blank new * device (or previously mass erased). It sets up address range * 0x1400_0000-0x1400_0FFF for SRAM use. * ------------------------------------------------------------------------------ * Test HW: S32K146EVB-Q144 * MCU: PS32K146UAVLQ 0N73V QAC1735D * Fsys: default * Debugger: Lauterbach Trace32, OpenSDA * Target: Debug_RAM * Terminal: none * EVB connection: default ********************************************************************************
記事全体を表示
********************************************************************************  Detailed Description:  Example shows FlexCAN 0 usage in RUN/VLPR modes using SDK.  CAN bitrate is set to 250bit/s.  MCU enters VLPR mode by pressing SW3 button. CAN std message is sent with data VLPRmode"  MCU exits VLPR to RUN mode when one of following happens:  - CAN std message with RX_MSG_ID is received and MCU is in VLPR  - SW2 button is pressed (PTC12 interrupt). CAN std message is sent with data "RUN mode"  Blue LED is dimming and the rate is different for each power mode due to different  system clock (48Mhz vs 4MHz)  ------------------------------------------------------------------------------  Test HW: S32K116EVB-Q48  MCU: PS32K116LAM 0N96V  Compiler: S32DS.ARM.2.2  SDK release: S32SDK_S32K1xx_RTM_3.0.3  Debugger: Lauterbach, OpenSDA  Target: internal_FLASH ********************************************************************************
記事全体を表示
Hello everyone, SEGGER's Real Time Transfer (RTT) is the new technology for interactive user I/O in embedded applications. It combines the advantages of SWO and semihosting at very high performance. Bi-directional communication with the target application Very high transfer speed without affecting real-time behavior Uses debug channel for communication No additional hardware or pin on target required Supported by any J-Link model Supported by ARM Cortex-M0/M0+/M1/M3/M4/M7/M23/M33 and Renesas RX100/200/600 Complete implementation code providing functionality and freedom Here, I'd like to share you the SEGGER RTT porting project on S32K144 as attached. SW requirements: S32DS for ARM v2.2 IDE + S32K1xx SDK RTM 3.0 HW requirements: S32K144-EVB  + J-LINK debugger   For SEGGER RTT, you can refer to: About Real-Time Transfer: https://www.segger.com/products/debug-probes/j-link/technology/about-real-time-transfer/   RTT SEGGER Wiki: https://wiki.segger.com/RTT#SEGGER_RTT_TerminalOut.28.29;   Using Segger Real Time Terminal (RTT) with Eclipse: https://mcuoneclipse.com/2015/07/07/using-segger-real-time-terminal-rtt-with-eclipse/   Hope this project can help you, and enjoy the RTT! Best regard, Enwei Hu.
記事全体を表示
Audio Video Bridging(AVB) is a protocol for the transport of audio and video streams over Ethernet-based networks, which makes it possible to deliver high volumes of data in real-time to multiple destinations with very low latency. This reference design board demonstrates the usage for AVB over S32K148. Alternatively, it can be an S32K148 evaluation board of 100pin version besides S32K148EVB-Q144 and S32K148EVB-Q176. Below shows the board layout, diagram, and main features. AVB RDB V2 picture.jpg Figure 1. S32K148AVB-RDB Layout   S32K148AVB-RDB Diagram(Rev B) Figure 2. S32K148AVB-RDB Diagram S32K148AVB-RDB Features Figure 3. S32K148AVB-RDB Features In terms of the software, we provide several examples to show the AVB/TSN usages and other applications. The avb_listener_talker project is the main example which implements most features and demonstrates by connecting 2 AVB boards by Ethernet cable.   AVB examples.jpg Figure 4. S32K148AVB-RDB Code Examples Below software stack and middleware are implemented. ✓ RTOS: FreeRTOS ✓ Peripherial Driver: SDK RTM 3.0 (Work with Processer Expert) ✓ AVB Stream: RTM 1.0 ✓ AVB AudioIf: RTM 1.0 ✓ gPTP Stack Version: 1.3.4 ✓ Lwip Stack Version: 2.1.2 •Note: Even though we did a lot of tests, it’s still the customer’s responsibility to ensure the total quality by themselves when it’s integrated into a real application project, all the sample codes and user guide documentation are just reference for the customer. •Note: We do not have an FCC or CE certificate for this board.   Now we have 50 pcs boards available in Chongqing, China. For applying for the board, please contact NXP sales or GPIS marketing.  Since the AVB stack is not free of use, for accessing the code please contact NXP sales or GPIS marketing. For technical discussion, please contact [email protected] or [email protected].  
記事全体を表示
******************************************************************************************************** Detailed Description: LPUART1 echoes RX signal at 115200 bps When an 's' char is received, the MCU enters VLPS. A falling edge of the RX signal brings the MCU from VLPS via LPUART RXEDGIF interrupt. BUS_CLK can be monitored at CLKOUT PTD14. In VLPS, BUS_CLK is gated off. -------------------------------------------------------------------------------------------------------------------------- Test HW: S32K144EVB-Q100 MCU: S32K 0N57U Debugger: S32DS_ARM_2.2, OpenSDA Target: internal_FLASH ******************************************************************************************************** danielmartynek_0-1605283306283.png danielmartynek_2-1605283434147.png    
記事全体を表示
Hi,      The draft time gap, from power-on to clock output of S32K14x, is as below. Snipaste_2020-11-09_14-10-24_Reset vs CLKOUT.jpg Snipaste_2020-11-09_14-09-54.jpg    You can take a reference. Cheers! Oliver
記事全体を表示
NXP S32K1xx serial MCU is widely used in automotive body control and many general-purpose automotive applications, while to target some applications with special requirements such as requiring more peripherals instance than the portfolio can offer (e.g. 6x CAN-FD, 6x LIN or 4 I2C) like mid-end BCM or DCU, an on-board dual/multi MCU sync solution is proposed as an alternate solution to extend the S32K1xx MCU peripherals/memory resource and CPU process capability. The eRPC (Embedded Remote Procedure Call) is a Remote Procedure Call (RPC) system created by NXP(https://github.com/EmbeddedRPC/erpc/). An RPC is a mechanism used to invoke a software routine on a remote system using a sample local function call. eRPC software architecture Figure 1. eRPC software architecture In this project, we ported the eRPC protocol to S32K1xx platform, tested and figured out its performance. An out-of-box software package with detailed user guide (this document) is provided to simplify and accelerate users’ assessment of eRPC on S32K1xx. Two S32K144EVB boards are connected to demonstrate the usage of the eRPC protocol. One works as the client, another as the server. The client board starts an eRPC request and the server board responds to the request and executes the service. eRPC task workflow on S32K144-EVB.png Figure 2. eRPC task workflow on S32K144-EVB There are three types of MCU extensions are demonstrated in the project: MCU IO extension: Set LED; MCU peripheral extension: CAN and LIN message forwarding, LED luminance regulator; CPU process capability extension: Matrix multiply and addition math operation. Please find the attached sample projects and user guide for more details. Table of Contents in User Guide.png Figure 3. Table of Contents in User Guide •Note: Even though we did a lot of tests for the solution with the sample projects on S32K144-EVB, it’s still customer’s responsibility to ensure the total quality by themselves when it’s integrated in a real application project, all the sample codes and user guide documentation are just reference for customer. If you have any questions about this solution, please post here and we can have an open discussion. Best Regard, Enwei Hu(胡恩伟) GPIS System Apps Engineer.  
記事全体を表示
Often we need to implement a SENT receiver in order to read the information sent by some sensors. It is useful to have the possibility of transmitting different message patterns in order to test your implementation. With this project you can transmit via a computer terminal a group of messages (up to 64). The project runs on a S32K144 EVB board, the output signal goes through J206 pin.
記事全体を表示
******************************************************************************** Detailed Description: This example shows SRAM ECC injection. By default, a double-bit ECC error is injected on read access of a location in SRAM_U region. This can be changed with the SRAM_U and DOUBLE_BIT macros. The errors can be detected by both the ERM and MCM modules and the corresponding interrupts can be called. Although only ERM is needed, for demonstration purposes, the MCM interrupt is enabled as well with a lower priority than the ERM interrupts. The ERM interrupts that are called first disable the injection mechanism so that subsequent errors can not be detected during a stack read access. The default S32 Design Studio start_up file copies the vector table to the SRAM_L region. To be able to inject ECC errors in this SRAM region and call the interrupts, the copying is disabled by __flash_vector_table__ symbol  declared in the start_up.h file and defined in the S32K144_64_flash linker file. -------------------------------------------------------------------------------------------- Test HW: S32K144EVB-Q100 MCU: S32K144 0N57U Debugger: S32DSR1 Target: internal_FLASH ********************************************************************************
記事全体を表示
Hi,     I would like to share with you the follow solution for S32K14x which could be attached while couldn't be re-programmed and stopped at RAM initializing.     If you met the issue as title, please check the SIM_CHIPCTL's value in IDE with attach function. Maybe you can find that the value is 0x0, which is not as default value after reset which is 0x0030_0000.     If you check the meaning on SIM_CHIPCTL, you can find that SRAMU and SRAML are retained across resets.  To solute the issue, you should add 'WRITE_LONG=00300000/40048004/ ;' in front of it the algorithm (it's better after reset) of freescale_s32k144f512m15_pflash_dflash_eeprom.arp which is at  'C:\NXP\S32DS_ARM_v20\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_3.3.3.201712132114\win32\gdi\P&E\supportFiles_ARM\NXP\S32K1xx' After that, you can download your project as normal. Cheers! Oliver
記事全体を表示
An example implementation of SENT protocol receiver with S32K118 evaluation board. The input is expected in J106, TICK duration is 2,75us. CRC is calculated and check, the decoded output is printed into terminal via UART (ASCII)
記事全体を表示