SEGGER Real Time Transfer (RTT) porting on S32K144(S32DS for ARM v2.2 + S32K1xx SDK RTM 3.0)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SEGGER Real Time Transfer (RTT) porting on S32K144(S32DS for ARM v2.2 + S32K1xx SDK RTM 3.0)

SEGGER Real Time Transfer (RTT) porting on S32K144(S32DS for ARM v2.2 + S32K1xx SDK RTM 3.0)

Hello everyone,

SEGGER's Real Time Transfer (RTT) is the new technology for interactive user I/O in embedded applications. It combines the advantages of SWO and semihosting at very high performance.

  • Bi-directional communication with the target application
  • Very high transfer speed without affecting real-time behavior
  • Uses debug channel for communication
  • No additional hardware or pin on target required
  • Supported by any J-Link model
  • Supported by ARM Cortex-M0/M0+/M1/M3/M4/M7/M23/M33 and Renesas RX100/200/600
  • Complete implementation code providing functionality and freedom

Here, I'd like to share you the SEGGER RTT porting project on S32K144 as attached.

SW requirements: S32DS for ARM v2.2 IDE + S32K1xx SDK RTM 3.0

HW requirements: S32K144-EVB  + J-LINK debugger

 

For SEGGER RTT, you can refer to:

About Real-Time Transfer:
 
RTT SEGGER Wiki
 
Using Segger Real Time Terminal (RTT) with Eclipse

 

Hope this project can help you, and enjoy the RTT!

Best regard,

Enwei Hu.

附件
无评分
版本历史
最后更新:
‎11-18-2020 07:56 AM
更新人: