S32K ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K Knowledge Base

ラベル

ディスカッション

ソート順:
Where can I get s32k14x data sheet or reference manual???
記事全体を表示
******************************************************************************** * Detailed Description: * * This example shows how to use the back-to-back mode of the PDB to trigger * sequence of ADC channels conversion. 4 PDB channel pre-triggers/triggers are * generated upon single PDB SW trigger. The first trigger is started by the PDB, * no delay is used. Next 3 triggers start after corresponding acknowledgment is * received from ADC. * * DMA is configured to read the ADC result registers. * Within DMA major interrupt the new conversion scan is started via PDB SW request. * * Converted data is used to change color of the EVB led based on Trimmer position. * * ------------------------------------------------------------------------------ * Test HW:         FRDM-S32K144 * MCU:             PS32K144HFVLL 0N77P * Fsys:            160MHz * Debugger:        S32DS * Target:          internal_FLASH * ********************************************************************************
記事全体を表示
******************************************************************************** * Detailed Description: * * This example shows how to init DMA for simple memory to memory copy. * Eight 16-bit values are copied upon SW start. * * ------------------------------------------------------------------------------ * Test HW:         FRDM-S32K144 * MCU:             PS32K144HFVLL 0N77P * Fsys:            default * Debugger:        S32DS * Target:          internal_FLASH * ******************************************************************************** Original Attachment has been moved to: Example-S32K144-DMA-RAM2RAM-test-v1_0-S32DS.zip
記事全体を表示
******************************************************************************** * Detailed Description: * This simple example shows how to force function to RAM memory in S32 Design * Studio and how to perform flash functions (Erase flash sector and Program * phrase command in this case). * * ------------------------------------------------------------------------------ * Test HW:         FRDM-S32K144 * MCU:             PS32K144HFVLL 0N77P * Fsys:            default * Debugger:        Lauterbach Trace32 * Target:          internal_FLASH * ********************************************************************************
記事全体を表示
This article provides a software package with additional example projects for wakeup use case using RTD 4.0.0 & 5.0.0. All the wakeup example projects mentioned in this page are developed based on RTD, with LLD or HLD.
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the  LPSPI IP Driver for the S32K3xx MCU.  The example uses LPSPI2 for transmit & receive Twelve bytes using the DMA. MOSI MISO connected on Hardware in loopback.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************    
記事全体を表示