Measure the running time of one function on S32K

cancel
Showing results for 
Search instead for 
Did you mean: 

Measure the running time of one function on S32K

100% helpful (1/1)

Measure the running time of one function on S32K

Hi, 

      ARM Cortex-M have a DWT (Data Watchpoint and Trace) unit implemented, and it has a nice feature in that unit which counts the execution cycles. The DWT is usually implemented on most Cortex-M3, M4 and M7 devices, including e.g. the NXP S32K14x. 

    Attachment is the sample project on S32K142 to measure the running time of a function.

    Password of extraction is nxp.

    Enjoy the measuring!

 

Cheers!

Oliver

BTW, Measure the running time of one function on PowerPC could also be gotten through the link.

Attachments
Version history
Revision #:
1 of 1
Last update:
‎05-17-2020 08:58 PM
Updated by: