S32K ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K Knowledge Base

ラベル

ディスカッション

ソート順:
This article has been moved to a new location: https://community.nxp.com/t5/S32M-Knowledge-Base/S32M2xx-Motor-control-use-cases/ta-p/2039790
記事全体を表示
What is S32K1‘s IDLE feature: IDLE is set when the LPUART receive line becomes idle for a full character time after a period of activity.When CTRL[ILT] is cleared, the receiver starts counting idle bit times after the start bit. Why write this demo? Because the RTM driver does not support Lpuart's IDLE detect. What needs to be modified? -1.add "UART_EVENT_DMA_IDLE = 0x04U" to “callbacks.h”   -2 add "LPUART_DRV_RxIdleCallback" to ".lpuart_driver.c"   -3 Define “LPUART_DRV_RxIdleCallback” function   static void LPUART_DRV_RxIdleCallback(uint32_t instance) { DEV_ASSERT(instance < LPUART_INSTANCE_COUNT); LPUART_Type *base = s_lpuartBase[instance]; lpuart_state_t * lpuartState = (lpuart_state_t *)s_lpuartStatePtr[instance]; LPUART_ClearStatusFlag(base,LPUART_IDLE_LINE_DETECT); if(lpuartState->transferType == LPUART_USING_DMA) { lpuartState->rxSize = EDMA_DRV_GetRemainingMajorIterationsCount(lpuartState->rxDMAChannel); LPUART_DRV_StopRxDma(instance); lpuartState->rxCallback(lpuartState,UART_EVENT_DMA_IDLE,NULL);/*UART_EVENT_DMA_IDLE : 0x04*/ } }     -4 add below code to "LPUART_DRV_IRQHandler" and be sure these code must  be put before "LPUART_DRV_ErrIrqHandler(instance)" /* Handle idle line interrupt */ if (LPUART_GetIntMode(base, LPUART_INT_IDLE_LINE)) { if (LPUART_GetStatusFlag(base, LPUART_IDLE_LINE_DETECT)) { LPUART_DRV_RxIdleCallback(instance); } }   -5 configure IDLE releated register in main function. LPUART1->CTRL |= LPUART_CTRL_ILT(1); LPUART1->CTRL |= LPUART_CTRL_IDLECFG(7); LPUART1->CTRL |= LPUART_CTRL_ILIE(1);   Test environment: Hardware is base on S32K144EVB-Q100 Software is S32 Design Studio for Arm V 2.2 + RTM 3.0.X Demo Description:           The baud rate of the serial port is set to 19200, and the function implemented is to send back the received data using DMA methods .      
記事全体を表示
 ------------------------------------------------------------------------------ * Test HW: S32K3 T-BOX * MCU: S32K324 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** S32K3 T-BOX : SJA1110 Firmware update using SPI HAP : S32DS-3.5 : RTD-3.0.0 :-- https://community.nxp.com/t5/S32K-Knowledge-Base/S32K3-T-BOX-SJA1110-Firmware-update-using-SPI-HAP-S32DS-3-5-RTD/ta-p/1939324
記事全体を表示
 ------------------------------------------------------------------------------ * Test HW: S32K3 T-BOX * MCU: S32K324 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ********************************************************************************  The purpose of this demo application is to present a usage of the  SPI-HAP of S32K3xx MCU to download firmware to SJA1110. SPI using Interrupt working code :-- S32K324_SPI_DMA_SJA1110_Load_firmware__Working__SPI__Interrupt.zip SPI using DMA working code :-- S32K324_SPI_DMA_SJA1110_Load_firmware__SPI_DMA_not_working.zip Firmware image of the SJA1110 is stored inside the S32K3 flash memory.. See the linker file of S32K3, we specify the location where the firmware image is present. This this firmware attached to be loaded to SJA1110, any one of the firmware can be selected and renamed to flash_image.bin  :-- 1>  flash_image.bin  --> Green LED blink on SJA1110 2> flash_image_RED.bin  --> Green LED blink on SJA1110 If you use your proprietary SJA1110 binary firmware, then this example to work, you have to change this MACO, in SJA1110_APP.h file  :-- You can get the size of the SJA1110 image from the MAP file of the attached project. Check for this __sja1110_BIN_SIZE, Symbol in MAP file :--   Switch connection to S32K3 SPI pins :--   LED connected to these pins of SJA1110, on T-BOX hardware :---  
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the  POWER & WKUP IP Driver for the S32K3xx MCU. In current example :-- SW-6 = PTB-19 -----> PRESS to enter the STANDBY mode. SW-5 = PTB-26 = WKUP[41] --> PRESS to exit the STANDBY mode. RTC --> Wakeup source-1 The example uses PIT-0 timer, to generate the periodic interrupt. T ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************   Make following settings, SIRC enabled in Standby mode :--    
記事全体を表示
******************************************************************************** * Detailed Description: * CM7_0 starts CM7_2 using Power_Ip or directly in MC_ME (macro USE_RTD_POWER_IP). * Disconnect the debugger and power-cycle the MCU. * * ------------------------------------------------------------------------------ * Test HW: S32K3x8EVB-Q289 * MCU: S32K358 * Debugger: S32DS_ARM_3.5, S32K3_RTD_4_0_0_P24_D2405 * Target: internal_FLASH ******************************************************************************** Any support, information, and technology (“Materials”) provided by NXP are provided AS IS, without any warranty express or implied, and NXP disclaims all direct and indirect liability and damages in connection with the Material to the maximum extent permitted by the applicable law. NXP accepts no liability for any assistance with applications or product design. Materials may only be used in connection with NXP products. Any feedback provided to NXP regarding the Materials may be used by NXP without restriction.
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the  POWER & WKUP IP Driver for the S32K3xx MCU. In current example :-- SW-5 = PTB-26  -----> PRESS to enter the STANDBY mode. SW-6 = PTB-19 = WKUP[38] --> PRESS to exit the STANDBY mode. CAN-0-RX = PTA-6 = WKUP[15] --> send CAN message to exit the STANDBY mode The example uses PIT-0 timer, to generate the periodic interrupt. The example uses FLEXCAN-0 for transmit & receive using following Message buffer :-- #define RX_MB_IDX_0 10U #define RX_MB_IDX 11U #define TX_MB_IDX 12U BAUDRATE : 500 KBPS  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 * MCU: S32K324 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** CAN BUS :--   Push Buttons :---         Wake-up source, SW-6 GPIO:--   Wake-up source, CAN-0-RX :-- According to the IOMUX table in RM, for example, PTA6 can be used as WKPU15 and CAN0_RX. It means that the WKPU15 input doesn't require specific MSCR configuration. So if its input buffer is enabled and the corresponding WKPU input channel is enabled/configured in the WKPU, it should be able to act as wake-up input.   Standby entry :--   STandby clock :--   Enter Standby mode :--   ********* If you use external BJT on your board to generate 1.5 volts *******************     I tested on Our T172 EVB, with NPN external Ballast transistor is selected to supply the V15_MCU domain. I am able to wake up from standby mode. If we select 2-3 in J31 then NPN external Ballast transistor is selected to supply the V15_MCU domain & wakeup is ok on T172 EVB You have to make following settings in code :--      
記事全体を表示
******************************************************************************** * Detailed Description: * The example updates th UART TX buffer for continuous transfer. * ---------------------------------------------------------------------- * Test HW: S32K344EVB-Q172 * MCU: S32K344, RTD 4.0.0 P24 * Debugger: S32DS_ARM_3.5 * Target: internal_FLASH ********************************************************************************
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the  POWER & WKUP IP Driver for the S32K3xx MCU. In current example :-- SW-5 = PTB-26  -----> PRESS to enter the STANDBY mode. SW-6 = PTB-19 = WKUP[38] --> PRESS to exit the STANDBY mode. The example uses PIT-0 timer, to generate the periodic interrupt.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 * MCU: S32K324 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Push Buttons :---     Wake-up source, SW-6 GPIO:--     ********* If you use external BJT on your board to generate 1.5 volts *******************   I tested on Our T172 EVB, with NPN external Ballast transistor is selected to supply the V15_MCU domain. I am able to wake up from standby mode. If we select 2-3 in J31 then NPN external Ballast transistor is selected to supply the V15_MCU domain & wakeup is ok on T172 EVB You have to make following settings in code :--      
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the  POWER & WKUP IP Driver for the S32K3xx MCU. In current example :-- SW-6 = PTB-19 -----> PRESS to enter the STANDBY mode. SW-5 = PTB-26 = WKUP[41] --> PRESS to exit the STANDBY mode. CAN-0-RX = PTA-6 = WKUP[15] --> send CAN message to exit the STANDBY mode. The example uses PIT-0 timer, to generate the periodic interrupt. The example uses FLEXCAN-0 for transmit & receive using following Message buffer :-- #define RX_MB_IDX_0 10U #define RX_MB_IDX 11U #define TX_MB_IDX 12U BAUDRATE : 500 KBPS  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************     Push button :--   Wake-up source, CAN-0-RX :-- According to the IOMUX table in RM, for example, PTA6 can be used as WKPU15 and CAN0_RX. It means that the WKPU15 input doesn't require specific MSCR configuration. So if its input buffer is enabled and the corresponding WKPU input channel is enabled/configured in the WKPU, it should be able to act as wake-up input. Wake-up source, SW-5 GPIO:-- Standby entry :--   STandby clock :-- Enter Standby mode :--  
記事全体を表示
 ------------------------------------------------------------------------------ * MCU: S32K310 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Example MCAL S32K310 MEM_InFls DS3.5 RTD300 :-- Example MCAL S32K310 MEM_InFls DS3.5 RTD300 - NXP Community
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the MEM_InFls MCAL Driver for the S32K3x1 MCU.  The example uses MEM_InFls driver to write 128 bytes to FLASH memory address  0x47_A000   starting of FLS_CODE_ARRAY_0_BLOCK_0_S61.  ------------------------------------------------------------------------------ * MCU: S32K310 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Flash end address = 0x480000 Size of each block = 8192 = 0x2000 Start Address of 63 block = 0x480000 - 0x2000 = 0x47E000 = 4710400 Start Address of 62 block = 0x480000 - 0x4000 = 0x47C000 = 4702208 Start Address of 61 block = 0x480000 - 0x6000 = 0x47A000 = 4694016   Ram location where FLASH writing erase code is placed :-- I placed the code at 0x256 byte below the MAX address of the RAM size 16*1024 = 16384 = 0x4000 End of RAM = 0x20400000 + 0x4000 = 0x20404000  0x20404000 - 0x256 = 0x20403DAA 0x20403DAA = 541081002   Size of RAM need to save the flashing routine, as per the MAP & linker file :-- 0x00407b80 - 0x00407b54 = 0x2C = 44 byte  S32K3 FLASH Memory Terminology :--        
記事全体を表示
------------------------------------------------------------------------------ * Test HW: S32K31XEVB-Q100 * MCU: S32K311 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** S32K31XEVB-Q100 :-- S32K31XEVB-Q100 Evaluation Board for Automotive General Purpose | NXP Semiconductors Example MCAL S32K311 MEM_InFls DS3.5 RTD300 :-- Example MCAL S32K311 MEM_InFls DS3.5 RTD300 - NXP Community
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the MEM_InFls MCAL Driver for the S32K3x1 MCU.  The example uses MEM_InFls driver to write 128 bytes to FLASH memory address  0x48_0000 .  ------------------------------------------------------------------------------ * Test HW: S32K31XEVB-Q100 * MCU: S32K311 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************     Results :--     Ram location where FLASH writing erase code is placed :-- I placed the code at 256 byte below the MAX address of the RAM size 0x20407DAA = 541097386             Size of RAM need to save the flashing routine, as per the MAP & linker file :-- 0x00406ff0 - 0x00406f78 = 120 bytes                S32K3 FLASH Memory Terminology :--        
記事全体を表示
------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 * MCU: S32K344 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** Example S32K344 UART Transmit & Receive Using DMA DS3.5 RTD300 :-- Example S32K344 UART Transmit & Receive Using DMA DS3.5 RTD300 - NXP Community Example S32K344 UART Transmit & Receive Using Interrupt DS3.5 RTD300 :-- Example S32K344 UART Transmit & Receive Using Interrupt DS3.5 RTD300 - NXP Community
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the  UART IP Driver for the S32K3xx MCU.  The example uses LPUART6 for transmit & receive five bytes using the Interrupt.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 * MCU: S32K344 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************         Putty output :--  
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the  UART IP Driver for the S32K3xx MCU.  The example uses LPUART6 for transmit & receive five bytes using the DMA.  ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-T172 * MCU: S32K344 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************     Putty output :--  
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the FEE MCAL Driver for the S32K3xx MCU. This example read & write 4 byte FEE BLock. I have renamed the FEE block using a MACRO as FOUR_BYTE_EEPROM_FEE_VARIABLE. The example uses MEM_InFls driver to write 128 bytes to FLASH memory address  0x52_0000 .  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************    
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the FEE MCAL Driver for the S32K3xx MCU. This example read & write 4 byte FEE BLock. I have renamed the FEE block using a MACRO as FOUR_BYTE_EEPROM_FEE_VARIABLE.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Driver configuration :--   Three FEE blocks are created. Each FEE block can be considered as EEPROM variables    How customer can use FEE block as EEPROM variable. Max size of FEE block :--     You can declare a MACRO for the Variable of EEPROM :-- FOUR_BYTE_EEPROM_FEE_VARIABLE How to Read and write the FEE variables :--  
記事全体を表示
*******************************************************************************  The purpose of this demo application is to present a usage of the MEM_InFls MCAL Driver for the S32K3xx MCU.  The example uses MEM_InFls driver to write 128 bytes to FLASH memory address  0x50_0000 .  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Results :-- Ram location where FLASH writing erase code is placed :-- I placed the code at 256 byte below the MAX address of the RAM size 0x20417DAA = 541162922     Size of RAM need to save the flashing routine, as per the MAP & linker file :-- 0x00407e64 - 0x00407e38 = 44 bytes      S32K3 FLASH Memory Terminology :--    
記事全体を表示