Example S32K344 PIT TRGMUX ADC DS3.5 RTD300

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example S32K344 PIT TRGMUX ADC DS3.5 RTD300

Example S32K344 PIT TRGMUX ADC DS3.5 RTD300

*******************************************************************************

 The purpose of this demo application is to present a usage of 
 configure TRGMUX to select triggers for staring Normal/Injected chain conversion.

Select PIT0_Ch0 as the hardware trigger source of ADC1_Ch34 & Ch48 via TRGMUX and two LEDs to show the trigger Sequence.

ADC1_Ch34 is connected to board's potentiometer,Ch38 is bandgap channel.

 ------------------------------------------------------------------------------
* Test HW: S32K3X4EVB-Q257
* MCU: S32K344
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: OpenSDA
* Target: internal_FLASH
********************************************************************************

Attachments
Comments

Thanks for sharing. Is there any example with MCAL drivers?

No ratings
Version history
Last update:
‎11-21-2023 07:28 PM
Updated by: