S32 Design Studio知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Design Studio Knowledge Base

讨论

排序依据:
When a new application project is created using the New Project Wizard, it is possible to select the debugger to be used. This results in the associated debugger configurations being created within the new project. But what if support for multiple debuggers is required or it is desired to switch to a different debugger? There are easy ways to resolve this. One is as simple as creating a new debug configuration. Another method is by creating new application project, selecting the new debugger to be supported. Then either repurposing the associated debug configuration or duplicating then modifying the debug configuration to support instead the previously existing project. This minimizes the effort by benefiting from the automation of the New Project Wizard.   Detailed below are the steps to add a new debug configuration.  Create A New S32 Debugger Configuration Load the existing project. For this demonstration, the SDK project ‘hello_world_s32v234’ will be used. Select the project so it appears highlighted in blue. mikedoidge_2-1618502998085.png Notice that the other project, ‘New_App_Project’, is bold text. This is because the main.c file open in the editor window to the right is the currently selected source file and is from this project. This has no effect on the process detailed in this document. Check that the existing project has been build and the executable is present. If the executable is not present, then an error will be displayed within the Debug Configurations menu and the executable file will need to be selected in a later additional step after it has been created. Open the Debug Configurations menu. Run -> Debug Configurations mikedoidge_3-1618503057621.png   Now select the Debugger Group for which you wish to create the new configuration. In this case, we will select ‘S32 Debugger’. mikedoidge_4-1618503102530.png Next, click ‘New Launch Configuration’ mikedoidge_5-1618503240330.png Now a new Debug Configuration has been created for your project and for the S32 Debugger. Most of the fields are already completed for you. Select the Debugger tab to see the source of the error message. mikedoidge_6-1618503272212.png The error message indicates ‘Specify Device and Core’. So click on ‘Select device and core’. mikedoidge_7-1618503322900.png Now expand the lists until the Device and Core are visible. Select the correct core for your project. In the demonstration example, the correct Device and Core are ‘S32V234’ and ‘M4’, respectively. Click OK, when done. mikedoidge_8-1618504433139.png If you have a debug probe connected, it may have been detected. If not, the Debug Probe Connection section will need to be completed. Now select the ‘Common’ tab to setup the storage location for this new Debug Configuration. mikedoidge_9-1618504500358.png Select ‘Shared file’ and then ‘Browse…’ mikedoidge_10-1618504532843.png Expand the lists until ‘Project_Settings/Debugger’ is open. Select ‘Debugger’, then click OK. mikedoidge_11-1618504568372.png Now the basic debug configuration settings are complete. It is now ready to be used and the Debug button could be clicked to start debug. Otherwise, you may have more customizations to make, such as for Attach Mode. Repurpose S32 Debugger Configuration From A New Project Create new project New -> S32DS Application Project mikedoidge_12-1618504622748.png New Project Wizard, processor and toolchain page Enter a project name Select the device and core to match the existing project If necessary, select the toolchain to match the existing project Click Next image.png New Project Wizard, cores and parameters page Select the number of cores to match the existing project Select the debugger, S32 Debugger If necessary, select other parameters to match the existing project Click Finish DanielBarbu_0-1719827180985.png   Open existing project which does not already have the S32 Debugger debug configurations (for this demonstration, we will use the hello_world_s32v234 example project from the S32 SDK) Copy debug configurations and modify settings to adapt to existing project Run -> Debug Configurations... image.png Debug Configurations window Within the S32 Debugger grouping, select the debug configuration for the new project which corresponds to the build configuration and core of the existing project Change the name of the debug configuration. Change the portion of the name containing the project name to match the name of the existing project. image.png Main tab Project field Click Browse... Select existing project image.png C/C++ Application Click Search Project... Select the Elf file image.png Common tab Save as field Click Browse... Select {existing_project_name}\Project_Settings\Debugger image.png Debugger tab, Debug Probe Connection Setup connection parameters image.png Click Apply Repeat as needed for all core/build config options The existing project now has the S32 Debugger configurations and is ready for debug with the S32 Debug Probe.
查看全文
This document details the steps to program external EEPROM with the 32 reset configuration bits in support of the 'Boot from serial RCON' method detailed in the S32G Reference Manual. The Python scripts used for this task are designed and tested to work on the S32G-VNP-EVB with S32G2xx Rev2 and the Atmel AT24C01C it contains.(Serial EEPROM is not implemented on NXP VNP-RDB board)   The RCON can be set by the following: Fuses (internal to the device) Parallel (GPIO pins/DIP Switches on EVB) Serial (EEPROM connected via I2C) The Serial option can be programmed using a debug probe connected via JTAG. This enables the RCON to be controlled remotely, assuming the debug probe is setup to allow remote connections.    Preparation Install S32 Design Studio IDE  Install the Development Package for the device you are debugging. This is important as the S32 Debugger provides access to the EEPROM programming capabilities via I2C of the S32 Debug Probe.  Connect the S32 Debug Probe to the S32G-VNP-EVB and the host PC containing S32 Design Studio installation. Set BOOTMOD pins to boot from RCON Set BOOT_CFG[8]=1 on the S32G-VNP-EVB, for serial RCON mode VNP-EVB shown here with switch BOOT_CFG[8] = 0 See the EVB documentation and device reference manual for more details. Procedure   Open cmd window to the S32 Debugger folder where the device-specific scripts are located. C:\NXP\S32DS.3.4\S32DS\tools\S32Debugger\Debugger\scripts\s32g2xx Set Python path so correct version is used (if not already set in env vars) set PYTHONPATH=C:\NXP\S32DS.3.4\S32DS\build_tools\msys32\mingw32\lib\python2.7;C:\NXP\S32DS.3.4\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages Edit the python script to adjust the value to be programmed to RCON, s32g2xx_i2c_RCON.py. Note: The listed examples show only the minimum values required to configure each of the external memory types. Additional settings may be required for your specific application. Adjust the RCON_DATA for the configuration you wish to program.  Do not adjust RCON_ADDR. Adjust the S32DBG_IP for the IP address of your S32 Debug Probe.  Adjust the INTERACTIVE_MODE  Set True, if desired to be prompted to enter RCON_DATA Set False, if desired to have script automatically enter RCON_DATA, based on the value set within the file. Adjust _SOC_NAME as appropriate for the specific S32G2xx device you are using. The valid options are defined in s32g2xx_context.py. Enter the command to start GDB, passing in the RCON Python script: Windows OS: C:\NXP\S32DS.3.4\S32DS\build_tools\gcc_b1620\gcc-6.3-arm32-eabi\bin\arm-none-eabi-gdb-py.exe -x s32g2xx_i2c_RCON.py OR C:\NXP\S32DS.3.4\S32DS\build_tools\gcc_v9.2\gcc-9.2-arm32-eabi\bin\arm-none-eabi-gdb-py.exe -x s32g2xx_i2c_RCON.py Linux OS: arm-none-eabi-gdb-py -x .\s32g274a_i2c_RCON.py If everything worked properly, then the value you programmed will be displayed to the screen. To exit GDB, enter 'quit'.
查看全文
Bare-metal project migration from an older version of S32DS into a newer one is typically pretty straightforward. Despite of that the migration into S32DS Power v1.2+ requires more attention due the fact it includes a new version of GCC compiler + GCC binutils (see the GCC release notes - here). This version of GCC is now fully EABI VLE compliant  (in contrast to previous versions of S32DS Power  v1.0 and v1.1) and it has several consequences for the project migration object code/libraries are not backward compatible - if you have an object code/library built by a previous version of S32DS Power v1.x you have to rebuild it in new S32DS v1.2+ compiler. default compiler setup has changed - bitfield access is not volatile anymore. This may have a impact on a peripheral registers access via standard header file bitfield structures. Such access may require a specific load/store instruction e.g. "stw" but if compiler is allowed to optimize the access (e.g. use "stb" instead of "stw") an exception may occur. Therefore it is recommended to add  -fstrict-volatile-bitfields  flag into your project GCC compiler settings: linker script file (*.ld) requires some additional linker sections - Linker script file in S32DS Power v1.2+ must contain the sections below: •  KEEP for .init and .fini sections • .ctors and .dtors sections • .preinit array .init array and .fini array sections If the linker script file is not updated and the linker warnings are ignored you may experience an exception at the runtime - typically when __init routine is executed. Missing .init section causes that an invalid instructions is fetched and causes the core IVOR exception. There is an easy way how to automatically fix the linker script file issue directly in IDE. If you import and build an older project in S32DS Power v1.2 the linker issues these linker script related warnings: Right click on the warning and select Quick Fix: Select "Add missed section in linker script"  + "Select All" and press "Finish". Repeat these steps until all the linker script warnings disappears. If you don't use IDE project you have to add the sections below into your linker script manually: .text_vle : { INPUT_SECTION_FLAGS (SHF_PPC_VLE) *(.text.startup) *(.text) *(.text.*) KEEP (*(.init)) KEEP (*(.fini)) . = ALIGN(16); } > m_text /* that will force pick VLE .text sections */ .ctors : { __CTOR_LIST__ = .; /* gcc uses crtbegin.o to find the start of the constructors, so we make sure it is first. Because this is a wildcard, it doesn't matter if the user does not actually link against crtbegin.o; the linker won't look for a file to match a wildcard. The wildcard also means that it doesn't matter which directory crtbegin.o is in. */ KEEP (*crtbegin.o(.ctors)) KEEP (*crtbegin?.o(.ctors)) /* We don't want to include the .ctor section from from the crtend.o file until after the sorted ctors. The .ctor section from the crtend file contains the end of ctors marker and it must be last */ KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .ctors)) KEEP (*(SORT(.ctors.*))) KEEP (*(.ctors)) __CTOR_END__ = .; } > m_text .dtors : { __DTOR_LIST__ = .; KEEP (*crtbegin.o(.dtors)) KEEP (*crtbegin?.o(.dtors)) KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .dtors)) KEEP (*(SORT(.dtors.*))) KEEP (*(.dtors)) __DTOR_END__ = .; } > m_text .preinit_array : { PROVIDE_HIDDEN (__preinit_array_start = .); KEEP (*(.preinit_array*)) PROVIDE_HIDDEN (__preinit_array_end = .); } > m_text .init_array : { PROVIDE_HIDDEN (__init_array_start = .); KEEP (*(SORT(.init_array.*))) KEEP (*(.init_array*)) PROVIDE_HIDDEN (__init_array_end = .); } > m_text .fini_array : { PROVIDE_HIDDEN (__fini_array_start = .); KEEP (*(SORT(.fini_array.*))) KEEP (*(.fini_array*)) PROVIDE_HIDDEN (__fini_array_end = .); } > m_text‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ This may help you to avoid time consuming debugging to figure out the root cause of the core exception. 
查看全文
Product Release Announcement Analog & Automotive Embedded Systems S32 Design Studio 3.6.2 Irina_Costachescu_0-1765791524153.png   The Analog & Automotive Embedded Systems (AAES) - Software Development Tools Engineering Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio 3.6.2 with support for: AMCU AP RAS S32K3 Family S32G Family S32R41 Family S32K1 Family S32ZE Family S32R45 Family S32M2 Family       Major Features for S32 Design Studio 3.6.2 Installer S32 Design Studio 3.6.2 is delivered with all public NPI's in a single 3GB installer to improve first time user experience. Additional packages for alpha customers are available based on Flexera entitlement and can be installed on top of S32 Design Studio 3.6.2 using Extension and Updates. Irina_Costachescu_0-1765808449510.png     Platform IDE and UI   Enhanced debugging efficiency by at least 20%. It applies to the entire debug session initialization pipeline and was measured from the moment Debug is pressed until the main() is reached. Live view mechanism was introduced in Memory Spaces and Global Variables views when target is running in non-stop mode. Users can observe real-time changes to memory addresses and variables, improving visibility into the runtime behavior. A configurable refresh rate allows tunning the update frequency based on performance needs. animation-ezgif.com-optimize.gif A new entry named assigned core was added in the Task List (FreeRTOS) view, it targets SMP cases. freertos_new.png Expressions with global scope can now be added straight from the Global Variables panel, without needing to switch to a separate view. new_var_global_var.png Added option to export registers description during data export from the Watch Registers view.  export_regs.png Find & Paste functions were enabled in Memory Management Unit (MMU) view. Added support for Enable auto build in S32 Debugger configuration. Enabled support for Additional Images in S32 Debugger configuration, for cases when additional source objects are loaded in the Flash memory. Enabled Advanced Settings to set the CCS IP and Port for S32 Debugger Flash Programmer debug configurations.   3 rd Party Solutions  Update of 3rd Party Debug support: Segger J-Link v8.28 PEmicro v6.0.2 TASKING v9.21.333   Major Features for NPIs S32K3 Family Merged  S32K389 into S32K3xx development pack to be available for all customers with S32DS 3.6.2 installer file. Enabled Wind River Diab 7.0.6 and IAR 8.50.10 compilers for S32K389. Enabled PEmicro v6.0.2 and IAR 8.50.10 debuggers for S32K389. Extended IAR and Segger debugging support for S32K36x, S32K37x, S32K39x, S32K341, S32K342 and S32K322 derivatives. Enhanced S32Flash programmer over JTAG to detect the presence of the HSE FW and adapt the flash operations considering HSE FW reserved flash addresses. gdb.jpg   This release is available for download on: S32 Design Studio 3.6.2 can be found on:  nxp.com  Flexera catalogue S32 Design Studio for S32 Platform v.3.6  Automotive Software Package Manager   Target Audience: S32 Design Studio 3.6.2 and bundled NPIs releases are targeted for public audience.   The Installation Procedure for Packages: Download S32 Design Studio v3.6.2, available on nxp.com, in Flexera catalogue S32 Design Studio for S32 Platform v.3.6, and in Automotive Software Package Manager. If you have any local admin restrictions(ex. Admin by Request) the installer will request elevation, alternatively you can use “Run as Administrator” to run the installer. Download any additional packages if it’s required. Start S32 Design Studio v3.6.2 and install the desired package. Go to  Help > S32DS Extensions and Updates. For additional packages, in the S32DS Extensions and Updates dialog box, click Add Update Sites. Navigate to the directory with the downloaded ZIP file. Choose it and click Open, then click OK. You will get back to S32DS Extensions and Updates and can use this dialog to select desired packages.​​   Technical Support: Please use the public community for general questions: https://community.nxp.com/community/s32/s32ds For internal packages please use INTERNAL S32DS NXP Community space:https://community.nxp.com/groups/internals32ds Irina_Costachescu_2-1765793361328.png  
查看全文
The FreeMASTER serial communication driver is a piece of code that enables an embedded application to communicate with the FreeMASTER PC application. Please note: The FreeMASTER_S32xx does not support all Toolchains and not all versions of supported Toolchains. The available SDKs will vary depending upon the toolchain which is selected. It is independent of the S32/MPC SDKs. In most cases, it is not integrated with the S32/MPC SDKs, although this could change in the future. When creating a new S32DS Application Project, you may have noticed the FreeMASTER_S32xx SDK option in the Select SDK menu. To add the FreeMASTER SDK to your project, simply add it in the New Project Wizard (as pictured above) or add it later through the project properties menu, SDKs: Select the desired SDK from the list, then click 'Attach/Detach...' Click in the column for each build configuration for which you wish to have the SDK attached. You can remove SDKs by clicking the '+', making it disappear. It should also be noted that there exists example projects which demonstrate usage of the FreeMASTER serial communication driver, though these do not use the FreeMASTER SDK, the driver was added manually. When working in your project, you can use the SDK Explorer to drag and drop macros and function calls into your code. To add the SDK Explorer to your perspective, there are at least 2 methods: 1) Menu method a) Window -> Show View -> Other... OR Alt + Shift + Q, Q b) Filter on 'SDK' c) Select 'SDK Explorer' d) Click OK 2) Quick Access method a) Type 'SDK' b) Select 'SDK Explorer' To access the macros and function calls from the SDK Explorer: 1) Go to the Project Explorer and select your project to make it active. 2) Go to SDK Explorer and all of the SDKs you included in the project will be listed. 3) For the SDK you wish to access, expand the folders and files until you can see the function you wish to add. You can set some filters to hide unwanted content. 4) Simply drag and drop the macro/function call into your source file. The #include statement for the associated header file will be automatically added near the top of your source file. Happy FreeMASTER serial communicating!
查看全文
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM v2.0 Update 2          What is new? S32 SDK 0.8.5 EAR (S32K142, S32K144, S32K146, S32K148) - see attached release notes for more details   MXQ 4.2 for MAC47D54H - see attached MQX release notes for more details. Installation instructions The update is available for online (via Eclipse Updater) or offline (direct download link) installation   online installation: go to menu "Help" -> "Install New Software..." dialog select predefined NXP S32 Design Studio update repository  "S32 Design Studio for ARM v2.0 - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2_0/com.freescale.s32arm.updatesite" select all available items and click "Next" button.   offline installation:  go to S32 Design Studio product page -> Downloads section or use the direct download link to download the Update archive file. Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded Update archive file you downloaded in the previous step: Select all available items and click "Next" button. This will starts the update installation.
查看全文
Product Release Announcement Analog & Automotive Embedded Systems S32 Design Studio 3.6.5 Irina_Costachescu_0-1765531594525.png   The Analog & Automotive Embedded Systems (AAES) - Software Development Tools Engineering Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio 3.6.5 with support for: AMCU AP RAS APN S32K3 Family S32G Family S32R41 Family S32J Family S32K1 Family S32ZE Family S32R45 Family   S32M2 Family S32N Family S32R47 Family       SAF8xxx Family     Major Features for S32 Design Studio 3.6.5 Installer S32 Design Studio 3.6.5 is delivered with all public NPI's in a single 2.63GB installer to improve first time user experience. Additional packages for alpha customers are available based on Flexera entitlement and can be installed on top of S32 Design Studio 3.6.5 using Extension and Updates. Irina_Costachescu_1-1765531866020.png   Installer will require admin rights only when the user chooses to install components which need elevation (Visual Studio Redistributable or debugger drivers). If a user chooses a custom installation only with S32DS IDE and its components (no drivers) the installation will finish without admin rights. Irina_Costachescu_2-1765531914107.png   Platform IDE and UI Integrated Cody, the open-source Eclipse plugin from Sourcegraph, into S32 Design Studio. This plugin is installed by default, allowing users with a valid Cody license to log in directly within S32DS and access Generative AI features. Note: Users must agree to the Sourcegraph Terms of Service before using Cody. Irina_Costachescu_2-1765456346536.gif Enabled integration with the NXP Application Code Hub, allowing users to browse available examples and import them directly from the hub page into S32 Design Studio. Note: the application examples will be published soon on the Application Code Hub URL. Irina_Costachescu_3-1765456346537.png Note: This image is taken from internal sources. The illustrated examples are currently under development and will be available soon. Extended the Quick Fix mechanism for the missing NPI and Real Time Drivers packages. Basically, an error message displays in the Problems view whenever the IDE identifies a missing package (build tool, NPI, RTD) associated with the current project. The Quick Fix automatically installs the missing package if it is available in the configured Update Sites. Note: not all scenarios are covered, there may be cases where the tool cannot determine if a package is missing. Irina_Costachescu_4-1765456345392.png A new Recent tab has been added in S32DS Extensions and Updates to display the latest installed packages, providing a clear history of user actions related to package installations. In addition, the default sorting was changed in All tab to bring greater visibility to NXP packages. Irina_Costachescu_5-1765456346540.png Added support for drag-and-drop of S32 Design Studio p2 update sites / installable packages into the S32DS Extensions & Updates window. Users can now simply drag the ZIP file into the window, and the package will be automatically inserted and selected, requiring only a click on Next to complete the installation. Irina_Costachescu_6-1765456348052.gif Significant improvements to Secure Debugging:  Added a dedicated Debug Card view that allows users to generate debug card binaries based on custom input. Implemented Challenge & Response functionality for Linux environment.  Enabled Secure Registry Key view for managing secure registry keys on Linux.  UI is aligned to the secure debugging functionality latest changes introduced by HSE2. Irina_Costachescu_0-1765808827917.png Extended the S32 Debugger OS awareness support with FreeRTOS. OS threads are now visible in S32 Design Studio and user will be able to individually debug them. Extended the command line support to display OS threads and objects. Irina_Costachescu_8-1765456347125.png Enable debug in low power mode with S32 Debugger for S32K3xx devices:  The debug session will recover after core exits low power or standby mode, allowing the user to continue application debugging. Debugging from the first instruction after low power exit is now possible by using this configuration command when starting the debug session: monitor template config :ccs:S32K3XX:SoC#0 6 1 Expanded the S32Trace debug-info parser to fully support DWARF-5, adding compatibility with projects using GCC 11.4 and newer.   Major Features for NPIs S32N Family S32Flash Programmer improvements for erase and verify write operations on S32N5. S32G2/G3, S32J100, and SAF8xxx Families S32J100 development package is now public and delivered inside S32DS installer. Enabled debugging support for S32G2 devices on VDK R10. S32Flash Programmer enhancements for erase and verify write operations. Various bug fixes and improvements for arm cores and accelerators. Irina_Costachescu_3-1765532135684.png   This release is available for download on: S32 Design Studio 3.6.5 can be found on  nxp.com  Flexera catalogue S32 Design Studio for S32 Platform v.3.6   Target Audience: S32 Design Studio 3.6.5 and bundled NPIs releases are targeted for public audience.   The Installation Procedure for Packages: Download S32 Design Studio v3.6.5, available on nxp.com and in Flexera catalogue S32 Design Studio for S32 Platform v.3.6. If you have any local admin restrictions(ex. Admin by Request) the installer will request elevation, alternatively you can use “Run as Administrator” to run the installer. Download any additional packages if it’s required. Start S32 Design Studio v3.6.5 and install the desired package. Go to  Help > S32DS Extensions and Updates. For additional packages, in the S32DS Extensions and Updates dialog box, drag the ZIP file into the window, and the package will be automatically inserted and selected, requiring only a click on Next to complete the installation, or click Add Update Sites. Navigate to the directory with the downloaded ZIP file. Choose it and click Open, then click OK. You will get back to S32DS Extensions and Updates and can use this dialog to select desired packages.​​   Technical Support: Please use the public community for general questions: https://community.nxp.com/community/s32/s32ds For internal packages please use INTERNAL S32DS NXP Community space:https://community.nxp.com/groups/internals32ds   Irina_Costachescu_10-1765457452129.png
查看全文
Purpose This document holds information about how the Design Studio and S32Debugger probe can be used to debug Zephyr OS (Operating System) applications running on NXP’ S32 family processors.    Scope    This document is addressed to the software developer or tester (referred below as user) looking to debug or verify its software using the S32Debugger probe.    The document assumes the user has basic knowledge about Zephyr OS and he can rebuild the image with debug configuration.    The information about the building of the Zephyr application using NXP’s Zephyr distribution is not in the scope of this document. This is part of the user manual delivered with the Zephyr NXP release.    Hardware support    This support is available for Cortex-A53 and Cortex-R52 cores only.    It has been confirmed on S32R41, S32R45 and S32Z/E SoCs (System on Chip).    Software support    This feature is available starting with Design Studio 3.5.3.    It is confirmed with Zephyr OS versions 2.7.2 (S32R41), 3.2.0 (S32Z/E), 3.3.0 (S32R41).    Background    Zephyr is a lightweight RTOS (Real Time Operating System) that supplies support for multiple architectures (aarch64, arm, riscv, x86).    The thread awareness support stands for the capability of the debugger to supply low-level information about OS threads (referred below as standard support) or system-level OS information (referred below as extended support).      Standard support    Design Studio can supply low-level information about Zephyr threads:    Name    State    CPU registers - including FPU (Floating Point Unit)    Call stack    Priority    User options    Core number    Prerequisites    S32Debugger automatically detects the Zephyr OS image using the specific debug symbols.    The Zephyr application image should include the following configuration options:    CONFIG_DEBUG_THREAD_INFO    Mandatory    If this choice is not set, the debugger is not able to parse the kernel internal data.    In debug view, the user will see one thread only and no extra information about this.                                         Debug window    The Zephyr threads are listed in the Debug window when the CPU is stopped.    DanielBarbu_0-1724062892992.png   This is an example about how to follow thread entry can be read:    DanielBarbu_1-1724063689089.png   The Thread with index #15 and thread ID 868402064 (TCB (Thread Control Block) address in decimal format) is running on the CPU core 0 and it is in the Stopped state.    It has running priority 15, the user options 0x01 and its name is “idle 00”.    This is suspended in a breakpoint set in function arch_cpu_idle();    Thread states    The thread states names reported by debugger are accordingly with the output of the kernel function k_thread_state_str() excluding Stopped, that is the active Zephyr thread suspended by debugger.    Thread’s state values:    Stopped    Dummy    Pending    Prestart    Dead    Suspended    Aborting    Queued      CPU registers    The CPU registers of the thread selected in the Debug window can be read from the Registers window. This window is updated automatically when other thread is selected.    Known limitations    The warning message “ccs: Invalid parameter” is printed twice into the Design Studio IDE console (for S32Z/E only).    These can be ignored because the functionality is not affected.    DanielBarbu_2-1724066921031.png   Breakpoint per thread is not supported    Write thread registers is not supported (excluding the thread in state Stopped)    Performance may be affected by high number of Zephyr threads    FPU registers read support requires patch of Zephyr OS to save the offset in the table for ARM64 build. This is the snippet code that must be added in the initialization of _kernel_thread_info_offsets  into file thread_info.c😞    #elif defined(CONFIG_FPU) && defined(CONFIG_FPU_SHARING) && defined(CONFIG_ARM64)     [THREAD_INFO_OFFSET_T_PREEMPT_FLOAT] = offsetof(struct _thread_arch,                          saved_fp_context),        [THREAD_INFO_OFFSET_T_COOP_FLOAT] = THREAD_INFO_UNIMPLEMENTED,        Extended support    Design Studio can supply system-level information about Zephyr OS resources like:    Timer    Semaphore    Mutex    Stack    Message queue    Mailboxes    Pipes    Queues    Threads    This implementation is not CPU architecture specific like standard support.    Prerequisites    The Zephyr application image should include the following configuration options:      CONFIG_DEBUG_THREAD_INFO    Mandatory    If this choice is not set, the debugger is not able to parse kernel internal data and to supply information about resource owners or waiting lists.    CONFIG_TRACING    CONFIG_TRACING_OBJECT_TRACKING    CONFIG_TRACING_NONE    Mandatory    Enable the kernel object tracking. If this is not set, the debugger can show system information about Threads only. Note: This configuration is working on Zephyr version 3.0.0 or higher.    CONFIG_INIT_STACKS    Optional    Enable the fill of stack with a marker that can be used by debugger to report the peak stack usage.    This information might be useful for stack size tunning.    CONFIG_THREAD_STACK_INFO    Recommended    The debugger supplies information about the stack (address, size or usage).        GDB (GNU Debugger)    This support is available through extended GDB commands.    Command name    Description    thread-aware-list-supported-os    List the supported OS types and the detected OS    thread-aware-list-supported-objs    List the supported kernel objects by the detected or specified OS. This is based on types used by the current image only.    thread-aware-read-objs    Read the specified or all objects supported by current image.        These commands can be configured to supply the output in JSON (JavaScript Object Notation) or table format.    Use the help command to get more information about these thread awareness commands.    DanielBarbu_3-1724067731467.png   Figure 2 GDB - Get Thread, Mutex & Semaphore info    Common attributes    Most of the object's attributes are type specific with 2 exceptions:    Attribute name    Description    Format               S32Debugger Zephyr Thread Awareness                                                                       User Manual v1.3                                                                        address    Object data address                     integer                                 name    ELF Symbol name                          string                                    Thread attributes    Attribute name    Description    Format    user_options    User options    integer    state    Thread state – see Thread states    string    prio    Thread priority    integer    stack_addr        integer    stack_delta        integer    stack_size        integer    stack_usage_max    Largest stack usage    float    stack_usage    Current stack usage    float    MemSlab attributes    Attribute name    Description    Format    num_blocks        integer    block_size        integer    buffer        integer    free_list        integer    num_used        integer    locked    Locked by this thread (name)    string    waiting    Threads (name) waiting for this object    string list    Queue attributes    Attribute name    Description    Format    locked    Locked by this thread (name)    string      waiting    Threads (name) waiting for this object    string list    Pipe attributes    Attribute name    Description    Format    buffer        integer    size        integer    bytes_used        integer    read_index        integer    write_index        integer    flags        integer    locked    Locked by this thread (name)    string    waiting_tx    Threads (name) waiting for this object on write    string list    waiting_rx    Threads (name) waiting for this object on read    string list    MBox attributes    Attribute name    Description    Format    locked    Locked by this thread (name)    string    waiting_tx    Threads (name) waiting for this object on write    string list    waiting_rx    Threads (name) waiting for this object on read    string list    Attribute name    Description    Format    timeout        integer      period        integer    MsgQ Attribute name    Description    Format    attributes    Attribute name    Description    Format    msg_size        integer    max_msgs        integer    buffer_start        integer    buffer_end        integer    read_ptr        integer    write_ptr        integer    used_msgs        integer    flags        integer    locked    Locked by this thread (name)    string    waiting    Threads (name) waiting for this object    string list    Stack attributes    Attribute name    Description    Format    base        integer    next        integer    top        integer    flags        integer    locked    Locked by this thread (name)    string    waiting    Threads (name) waiting for this object on write    string list    Timer attributes    status        integer    waiting    Threads (name) waiting for this object on write    string list    Mutex attributes      owner    Own by this thread (name)    string    lock_count        integer    owner_orig_prio        integer    waiting    Threads (name) waiting for this object on write    string list    Semaphore attributes    Attribute name    Description    Format    limit        integer    count        integer    waiting    Threads (name) waiting for this object on write    string list        DS (Design Studio)    The DS version 3.5.3 or higher offers the possibility to display the Thread information only into a dedicated view.    The extended support is still available in DS by running the extended GDB commands directly from the Debugger Console window.      DanielBarbu_4-1724067870467.jpeg       Figure 3 DS - Execute thread awareness GDB commands    Thread view    This window can be accessed from the menu RTOS/Zephyr RTOS/Threads.    DanielBarbu_5-1724067870470.jpeg         DanielBarbu_6-1724067870508.jpeg       Figure 4 DS IDE - Thread view    Some information can be missing from the view depending on the build configuration used. For example, in the above figure, the Peak stack usage is not available because the CONFIG_INIT_STACKS is not set.    Note the Thread’s field names into DS IDE Thread view can be different than GDB Thread attributes.    Stack    The thread view holds more information about the stack.    The Stack usage stands for the current stack usage, and it is based on SP (Stack Pointer) register while the Peak stack usage stands for the maximum usage of the stack.    Known limitations    Performance may be affected by number of OS resources    Limited configurations tested       
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 11          What is new? S32 SDK for Power Architecture RTM 3.0.0 supporting  S32R274, S32R372, MPC574x-B-C-G, MPC574x-P, MPC574x-R and MPC577x-B-E-C (see the S32 SDK release notes) Integrated Radar SDK RTM 1.2.1 (see the Radar SDK release notes) This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6, Update 7, Update 8, Update 9, Update 10  ). Installation instructions The update is available for online installation (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
查看全文
This document shows, how to set optimization level for whole project and how to edit single files with different optimization level. As soon as the project is created, it has set optimization level to 0 by default. This means, compiler do neither size optimization nor speed optimization. Optimization level can be set for every project according to the project requirements. 1) Optimization level set Right click the project and select project properties. Click C/C++ Build ->Settings->Standard S32DS C Compiler ->Optimization. You can see, optimization level is none -O0. Click the arrow on the right side of the list and choose the required optimization level. There are five options you can choose. Details description of the options are included in S32DS reference manual. Chosen optimization is used for all files in the project. 2) Change optimization level for single file in the project If you want to change optimization level for single file and do no affect another files, select required file, right click on it and select properties. As you can see, there are limited possibilities to set the file itself. Select required optimization level, click apply and close the window. Now, selected file has different options than the rest of the project. Hope it helps. Martin
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture v2.1 Update 10          What is new? Service Pack for S32R264 This is a cumulative update - it includes all the content of previous updates (Update 1,Update 2, Update 7, Update 8 ) Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Go to Preferences' link And add a new site "Add..." repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select the 'S32 Design Studio for Power Architecture Device Package' and 'Update with S32 SDK 3.0.2 for Power Architecture' packages and click "Install/Update" button.   This will start the update installation process.
查看全文
There are three methods to run the configuration tool; from S32DS, from Terminal and JTAG, and from command line. S32DS Method 1) Make sure EVB is powered and connected to PC via PEMicro (Universal Multilink) or Lauterbach 2) Launch S32DS for Vision 3) File -> New -> S32V DDR Configuration Project 4) Enter a name for the project, for example 'DDR_Config_test'. Click Next 5) Expand 'S32V' and select 'S32V_234' 6) Click Finish to generate the project with default settings OR if you wish, to view or adjust more project settings, click Next. For this demonstration, we click Next. a. Select which DDR controller to which the settings will be applied. For this demonstration, we leave it at default (1st DDR Controller) b. There is an option to import settings from a file c. Board setting allows you to select from a list of predefined configurations, one for each of the NXP S32V234 evaluation boards i. S32V234_EVB is for LPDDR2 (SCH28899 and SCH28292(old board)) ii. X_TR_DVAL_625 is for DDR3 (SCH28662(old board)) iii. S32V234_NXP_EVB is for SCH29288 (S32V234-EVB2) iv. Custom allows for more options to be selected. See user manual for more detail d. For this demonstration, we select S32V234_EVB e. Click Finish 7) It will take a couple minutes to generate the project. You will get a prompt to pen the S32V DDR Configuration perspective. Click Yes. 😎 Now the project is generated and you can see it listed in the Project Explorer 9) Notice the Components and Component Inspector views of the S32V DDR Configuration perspective. 10) Select the component 'MMDC_0:Init_MMDC from the Components view 11) In the Component Inspector window you can see all of the configuration settings. You can modify the settings here. Changes made to some of the high-level settings may also cause changes to some of the low-level settings. There are some consistency checks that are run automatically after settings are changed which will trigger an error message in the case of an invalid configuration. a. For an example of high-level settings affecting low-level settings, try changing the 'Memory type' from LPDDR2 to DDR3. You can see the Burst Length, Column Address Width, and Row Address Width have changed. b. For an example of a consistency check on an invalid configuration, try changing the CAS Read Latency value (MDCFG0) from 8 to 12 (valid range as displayed with mouse hover tooltip shows 3-11), you will see the error appear. Change back to 8 and error is gone. 12) Open Configuration Registers view. Window -> Show View -> Other -> Processor Expert -> Configuration Registers. This shows how the settings will appear in the memory map. As you change the settings, the values will update here and the affected rows will be highlighted. Try it by changing Column Address Width in MDCTL of the Component Selector window. Likewise, you can try changing the value manually in the Configuration Registers view and see the setting in the Component Selector window update as well. *Hint: enter the name of the view in the search bar to find it quicker 13) Once all changes to the settings are complete, code can be generated. Press the 'Generate Processor Expert Code' button in the Components view. The generated .c and .h file will appear in the 'Generated_Code' folder of the Configuration project. These can be copied into your application project. OR 14) Back in the Component Inspector view, there are tabs for Import and Export settings. The Import settings tab will allow you to import existing settings files, as was also shown in the new project wizard. From the Export settings tab, you can generate a settings file for storage or sharing. The settings files for MMDC_0 and MMDC_1 for each of the supported NXP EVBs are included and can be located in 'C:\NXP\S32DS_Vision_v2.0\eclipse\ProcessorExpert\Optimization\resources\S32V\Boards' and then select the folder for the specific board. The CodeWarrior Register Text format is recommended for these files. 15) Now select the 'Validation' tab (some views, such as Configuration Registers, can be minimized for better view). Here we can execute a validation of the configuration settings we've made. Now is a good time to double check the hardware connections. 16) Select the connection method (either PEMicro or Lauterbach, depending on your setup). We will use System: S32V234; PEMICRO 17) Press 'Connect to Target' 18) Check a box for one of the scenarios. For example, select 'Read Delay Calibration' 19) Select the 'Choose Tests' tab 20) You can select tests from a list. To see the script behind the test, simply double-click on the name. For faster operation, ELF file versions are also provided. 21) Select the tests you wish to execute and press 'Start Validation'. For example select 'Write-Read-Compare-Elf', 'Walking Ones Elf', and 'Walking Zeros Elf'. 22) These tests will try different values and to determine which will work and which will not. After the test is finished, the best values are chosen and written back to the project configuration settings. To see the values change, go to the Properties tab and find 'PHY Read delay-lines Configuration' or restore the 'Configuration Registers' view and see the values changed. 23) For each test, you can see the errors which occurred in the 'Summary' tab, Test results section. There is also Updated configuration registers section which shows the register and the new value which was written to it. For more details on the errors, there is a Log tab which displays the log for each test which was run. Finally there is a Scripts tab which shows the script for each test containing the test settings. Each test box is colored to reflect the result of the test. Clicking on different ones causes the display below to change and show the results for that test. 24) The Write Delay Calibration test scenario is very similar to the Read Delay Calibration test scenario, but instead, the Write delay-lines Configuration will be updated. 25) The Operational DDR Tests run the same tests, but no value in the configuration is changed. You can set it to run for many repetitions to test for stability. Terminal window Method (JTAG) This checks what settings are already uploaded in MMDC module 1) Make sure EVB is powered and connected to PC via PEMicro (Universal Multilink) or Lauterbach (to load test application) AND serial communications via USB cable(for terminal access). 2) In S32DS, create a simple project a. File->New->S32DS Application Project b. Enter name 'test' c. Select S32V234 Cortex-A53 d. Next e. Uncheck boxes for cores 2-4 f. Finish 3) Setup debug configuration a. Run->Debug Configurations… b. Select test_A53_1_PNE c. Change C/C++ Application to C:\NXP\S32DS_Vision_v2.0\utils\ddr_stresstool\ddr-test-uboot-jtag-s32v234.elf d. Select Debugger tab e. Click Advanced Options f. Check box for Enable initialization script g. Browse to find C:\NXP\S32DS_Vision_v2.0\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_3.1.3.201709051622\win32\gdi\P&E\supportFiles_ARM\NXP\S32Vxxx\S32V234M100_DDR.mac h. OK 4) Click Debug. You will see error message indicating the source file could not be found. This is expected. 5) Open terminal (such as PuTTY.exe) and connect a serial line using the USB port you have connected to the EVB, speed set to 115200, 8 data bits, 1 stop bit, and no parity or flow control. 6) Click Resume in S32DS Debugger. 7) In terminal window, you will see the test script has started. 😎 Select the MMDC channel (for example, enter 1 for MMDC1) 9) Select the DDR density (for example, enter 6 for 32MB) 10) Enter 'y' to accept the DDR Calibration 11) Enter 'y' to accept the DDR frequency of 533MHz 12) Wait and watch while the test completes. 13) When the test completes, the results are shown. You will have to manually update your settings from the information displayed. 14) Next you will have the option to run the DDR Stress Test.
查看全文
The list of S32 Design Studio examples has been moved here: https://community.nxp.com/docs/DOC-341380  S32K144 EXAMPLE: S32K_printf_implementation - S32DS  EXAMPLE: S32k144 UART printf/scanf under FreeRTOS - S32DS  EXAMPLE: S32K SDK  - Function call on configurable period using LPIT timer.  EXAMPLE: FlexNVM used as code/data flash  EXAMPLE: S32K144 EEEPROM usage  EXAMPLE: S32K144 EEEPROM usage - No SDK  EXAMPLE: S32K144 .noinit section usage  For more examples and how to's: S32K1xx document & example list
查看全文
This short video demonstrates how you can get the RTD version 5.0.0 from your NXP User Account and then install it on top of S32 Design Studio 3.6.0 Afterwords, a simple IO example is shown to exercise the Headers and Source Code configuration & generation & build
查看全文
The S32 Debugger included within the S32 Design Studio for S32 Platform IDE provides the ability to access the flash programming and debugging of the S32 Debug Probe via GDB command line. This document provides only the necessary commands specific to launching a debug session on NXP devices. It does not cover general GDB command line operations, these are covered in detail in the GNU communities and other public websites which are not associated with NXP. Preparation Setup the software tools Install S32 Design Studio for S32 Platform Install the Development Package for the device you are debugging. In this case, the S32R41 development package. This package is important as the S32 Debugger support component contains the device-specific Python scripts required for initialization of the cores. s32r41.PNG Setup the hardware Confirm the setup of the S32R41 evaluation board. Connect the power supply cable Setup the S32 Debug Probe. Refer to the S32 Debug Probe User Manual for installation instructions. Connect the S32 Debug Probe to the evaluation board via JTAG cable. Connect the S32 Debug Probe to the host PC via USB OR via Ethernet (via LAN or directly connected, and configured for static IP address) and power supply connected to USB port. Launch S32 Design Studio for S32 Platform Create new or open existing project and check that it successfully builds. If creating a new project, be sure the S32 Debugger is selected in the New Project Wizard DanielBarbu_0-1718791409475.png   Procedure As separate debug threads need to be started for each core to be debugged, and the method for launching a debug thread differs depending upon whether it is a primary core or secondary core and if the executable image will be loaded or if the executable is already running and the debugger just needs to be attached. These scenarios will be covered by the following 3 sections: Primary Core Load Image and Run: The application image will be loaded directly to memory by the debugger and then initialized and started. The primary core will launch any secondary cores used by the application. Secondary Cores: The primary core has launched a secondary core, it is now running and the debugger will connect through the attach method. Primary Core Image Already In Memory and Running: The primary core has already been initialized and launched by other means, such as via a Linux OS on the target, so the debugger will connect through the attach method without initializing or loading the image to memory. Please proceed with the section which applies to the core for which you are starting a debug thread. Primary Core Load Image and Run Prepare the initialization script for the core(s) to be debugged. Open the core initialization Python script: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\scripts\s32r41\s32r41_generic_bareboard_all_cores.py Uncomment the following lines: # _JTAG_SPEED = 16000 # _GDB_SERVER_PORT = 45000# _RESET_TYPE = "default" # _PROBE_IP = "s32dbg" # _CORE_NAME = 'M7_0' # _RESET_DELAY = 1 # _REMOTE_TIMEOUT = 110 # _IS_LOGGING_ENABLED = False # _SOC_NAME = "S32R41" This file is used by the S32 Debugger within the S32 Design Studio IDE where the settings are provided from the GUI, so these lines are commented out in order to allow the GUI settings to have control. The commented lines are provided so the script could more easily be run by the command line method. Update the IP address line (_PROBE_IP) to match the IP address of the S32 Debug Probe which is connected to your PC. See the user guide for the S32 Debug Probe for details on how to obtain the IP address. Update the core name (_CORE_NAME), if necessary. See s32r41_context.py for complete list of supported cores. Save the file with a new name to preserve the original. For example, s32r41_gen_bb_all_c_my_probe.py. This ensures the S32 Debugger will still function correctly. Launch GTA server. From command prompt or Windows File Explorer run the command: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\Server\gta\gta.exe Should see a window appear like this: Ensure Environment Variable for Python is set. From command prompt, run the command: set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages Start GDB. In a command window, run the command: Windows OS: {S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32) OR {S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64) Linux OS: arm-none-eabi-gdb-py A (gdb) prompt should now be displayed in the command window: From (gdb) prompt, enter the following commands(in this order): source {S32DS Install Path}\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32r41\\s32r41_gen_bb_all_c_my_probe.py This specifies the script for initialization. py board_init() This initializes the board. It should only be called for the initial core. In a multicore debugging workflow, the debugger launch for additional cores would omit this step. py core_init() This initializes the core specified in the initialization script in step 1. Now standard GDB commands may be used. For example, you may wish to load an ELF file: file {S32DS Workspace Path}\\New_S32R_Project_M7_0\\Debug_RAM\\New_S32R_Project_M7_0.elf load Secondary Cores After completing the launch of debug for the primary core, it is possible to perform multicore debug by launching GDB debugging on the secondary cores. Some additional steps will need to be performed from within the primary core GDB session, enter the following commands: set *0x34100000 = 0x34200000 set *0x34100004 = 0x34100025 set *0x34100024 = 0xFFFEF7FF b main c These lines prepare the environment for launching debugging on secondary cores. This will allow for multicore debugging in the case of separate ELF files for each core. These can be found in the Run Commands field of the Startup tab on the Debug Configuration for the primary core within S32 Design Studio IDE, of any multicore project created from the New Application Project Wizard. Note: If there is just one ELF file for all cores, then these 'set *0x... = 0x...' commands should be skipped. In general, it will be correct to set the break-point at main, as shown, but this might need to be changed depending on when the secondary cores are started within the project. Prepare the initialization script for the secondary core to be debugged. Open the core initialization Python script: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\scripts\s32r41\s32r41_attach.py This is a different script than the one used for the primary core. It is designed to launch a debug session on a core which is already initialized and running. Edit the script for the secondary core to be debugged. Since this script is setup for the primary core, some adjustments need to be made to setup for a secondary core Uncomment the following lines: # _JTAG_SPEED = 16000 # _GDB_SERVER_PORT = 45000 # _RESET_TYPE = "default" # _PROBE_IP = "s32dbg" # _CORE_NAME = 'M7_0' # _RESET_DELAY = 1 # _REMOTE_TIMEOUT = 110 # _IS_LOGGING_ENABLED = False # _SOC_NAME = "S32R41" Make the following changes to the lines: _JTAG_SPEED = 16000 ->  None _GDB_SERVER_PORT = 45000 _RESET_TYPE = "default" _PROBE_IP = "s32dbg" -> None _CORE_NAME = 'M7_0' -> 'M7_1' (this should be set to match the name of the core to be debugged, see s32r41_context.py for complete list) _RESET_DELAY = 1 _REMOTE_TIMEOUT = 110 _IS_LOGGING_ENABLED = False -> ‘True’ _SOC_NAME = "S32R41" Save the file with a new name to preserve the original. For example, s32r41_attach_my_probe_core1.py. This ensures the S32 Debugger will still function correctly. The existing GTA server is used, so do not launch a new one. Open an new command window and follow similar steps as done for the primary core. Setup the Python environment variable, if not done globally set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages Start GDB Windows OS: {S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32) OR {S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64) Linux OS: arm-none-eabi-gdb-py A (gdb) prompt should now be displayed in the command window: From (gdb) prompt, enter the following commands (in this order): source {S32DS Install Path}\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32r41\\s32r41_attach_my_probe_core1.py This specifies the script for initialization. We will not execute the py board_init() as this was already done for the primary core. py core_init() This initializes the core specified in the initialization script in step 2. Now standard GDB commands may be used. For example, you may wish to load an ELF file: file {S32DS Workspace Path}\\S32R_Multicore\\S32R_Multicore_M7_1\ \Debug_RAM\\S32R_Multicore_M7_1.elf load Primary Core Image Already in Memory and Running The core is running and does not need to be initialized. Prepare the initialization script for the core to be debugged. Open the core initialization Python script: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\scripts\s32r41\s32r41_attach.py This is a different script than the one used for the primary core. It is designed to launch a debug session on a core which is already initialized and running. Edit the script for the secondary core to be debugged. Since this script is setup for the primary core, some adjustments need to be made to setup for a secondary core Uncomment the following lines: # _JTAG_SPEED = 16000 # _GDB_SERVER_PORT = 45000 # _RESET_TYPE = "default" # _PROBE_IP = "s32dbg" # _CORE_NAME = 'M7_0' # _RESET_DELAY = 1 # _REMOTE_TIMEOUT = 110 # _IS_LOGGING_ENABLED = False # _SOC_NAME = "S32R41" Make the following changes to the lines: _JTAG_SPEED = 16000 _GDB_SERVER_PORT = 45000 _RESET_TYPE = "default" _PROBE_IP = "s32dbg" -> (enter the IP address of your probe) _CORE_NAME = 'M7_0' (this should be set to match the name of the core to be debugged, see s32r41_context.py for complete list) _RESET_DELAY = 1 _REMOTE_TIMEOUT = 110 _IS_LOGGING_ENABLED = False -> ‘True’ _SOC_NAME = "S32R41" Save the file with a new name to preserve the original. For example, s32r41_attach_my_probe_core0.py. This ensures the S32 Debugger will still function correctly. Launch GTA server. From command prompt or Windows File Explorer run the command: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\Server\gta\gta.exe Should see a window appear like this: Ensure Environment Variable for Python is set. From command prompt, run the command: set PYTHONPATH={S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7;{S32DS Install Path}\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages Start GDB. In a command window, run the command: Windows OS: {S32DS Install Path}\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe (for arm32) OR {S32DS Install Path}\S32DS\tools\gdb-arm\arm64-eabi\bin\aarch64-none-elf-gdb-py.exe (for arm64) Linux OS: arm-none-eabi-gdb-py A (gdb) prompt should now be displayed in the command window: From (gdb) prompt, enter the following commands(in this order): source {S32DS Install Path}\\S32DS\\tools\\S32Debugger\\Debugger\\scripts\\s32r41\\s32r41_attach_my_probe_core0.py This specifies the script for debugger initialization. Do not execute the py board_init() as this will initialize the board, and reset the currently executing application, which is not desired for this case. py core_init() This initializes the debugger connection to the core specified in the initialization script in step 1. Now standard GDB commands may be used. For example, you may wish to load an ELF file: file {S32DS Workspace Path}\\ New_S32R41_Project\\New_S32R41_Project_M7_0\\Debug_RAM\\New_S32R41_Project_M7_0.elf load After completing the launch of debug for the primary core, it is possible to perform multicore debug by launching GDB debugging on the secondary cores. See section ‘Secondary Cores’ for each additional core to be debugged.
查看全文
The list of S32 Design Studio examples has been moved here: https://community.nxp.com/docs/DOC-329623  MPC5644A Example MPC5644A BookE PinToggle - S32DS Power 2017.R1 MPC5744P Example MPC5744P PinToggleStationery S32DS_1.0  Example MPC5744P LINFlex UART with DMA S32DS_1.0  Example MPC5744P ETimerCountMode S32DS_1.0  MPC5777M Example MPC5777M PinToggleStationery S32DS_1.0 Processor Expert RAppID Suite for MPC5777M and S32 Design Studio Integration Multicore Example  MPC5775K Example MPC5775K PinToggleStationery S32DS_1.0  Example MPC5775K-DMA_Transfer S32DS_1.0  Example MPC5775K UART_with_DMA S32DS_1.0  Example MPC5775K-UART_with_Interrupts S32DS_1.0  Example MPC5775K FlexCAN_with_interrupts_v1.1 S32DS_1.1  Example MPC5775K Semaphores S32DS_1.0  Example MPC5775K eTimer_PWM S32DS_1.0  Example MPC5775K ADC_example S32DS_1.0  Example MPC5775K IIC Communication with RTC PCA8565TS/1 S32DS_1.0  Example MPC5775K DSPI_with_interrupts S32DS_1.0  MPC5748G Example MPC5748G-FlexCAN_with_interrupts S32DS_1.0  Example MPC5748G PretendedNetworkingCAN S32DS_1.0  MPC5746R Example MPC5746R FlexCAN_with_interrupts S32DS Example MPC5746R PinToggleStationery - S32DS Power 2017.R1 S32R274 Example S32R274 FlexCAN_with_Interrupts S32DS_1.1  Example S32R274 Watchdog_example S32DS_1.1  Example S32R274 multi-core shared memory - S32DS Power v1.2  MPC5777C Example MPC5777C Single ELF multi-core Pin Toggling - S32DS Power v1.2
查看全文
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Vision 2018.R1          Austin, Texas, USA November 23, 2018 The Automotive Microcontrollers and Processors’ Embedded Tools Team at NXP Semiconductors, is pleased to announce the release of the S32 Design Studio for Vision  2018.R1. The S32 Design Studio enablement simplifies and accelerates the deployment of ADAS vision and neural network solutions in automotive, transportation and industrial applications. Here are some of its major features: Release Content S32 Debugger ISP Graph Tool APEX2 Graph Tool NXP GCC Compiler 6.3 NXP Compiler for APU Vision SDK 1.2.0 Complete S32 Design Studio for Vision 2018.R1 release notes are available here. Installation To download the installer please visit the S32 Design Studio product page downloads section or click the direct here. The installer requires the Activation ID to be entered. You should receive a notification email including the Activation ID after the download of the installation package starts. For more information about the product installation see S32DS Vision Installation Manual.   Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space. https://community.nxp.com/community/s32/s32ds  
查看全文
This document shows the step-by-step process to create a simple project which recreates the included example 'hello_world_s32v234'. The purpose of this demo is to provide the user with an example application for S32V234 platform, using S32 SDK. The demo toggles two LEDs (PTA8 and PTA9). This HW used in this demo is the SBC-S32V234 EVB, connected to a PC through NXP's S32 Debug Probe or P&E Micro's debug probe. Setup S32 Design Studio 3.1 or later installed AND S32V2xx development package installed SBC-S32V234 EVB connected to power AND switched ON Either S32 Debug Probe OR P&E Micro debug probe connected to the SBC-S32V234 EVB through JTAG connection. S32 Debug Probe connected to PC via either USB cable OR Ethernet cable (also requires power via included power supply and connected to USB port). For more information on HW setup, see HOWTO: Start Debug on an ISP Application Project with S32 Debugger and S32 Debug Probe . P&E Micro debug probe connected to PC via USB cable Procedure Create a new application project for M4 core File -> New -> S32DS Application Project Enter project name, select processor S32V234 Cortex-M4, click Next. Click '...' to select the SDK Select S32V234 SDK v1.0.0 (or later version) Notice the box is now checked for S32 Configuration Tool. The S32 Configuration Tool is dependent upon the S32 SDK. Select either S32 Debugger (default) or PE Micro GDB server. Click Finish The new project appears in the Project Explorer, notice the S32V234_M4.mex file is there as well. This .mex file contains all of the configuration data for the S32 Configuration Tool for this project. After clicking on the project name, the toolbar icon for the S32 Configuration Tool is now active. Click the S32 Configuration Tool button or double-click on the .mex file to open the S32 Configuration Tool perspectives. Notice the new perspective buttons in the toolbar: Go to Pins tool perspective, this is the default perspective that opens when the S32 Configuration Tool is launched. Notice there are errors at the lower right. There is a dependency upon the PINS driver from the S32 SDK. This driver is not mandatory, and while there are some rare cases where the drivers would not be needed, in most cases the user should choose to include them.                                                                                                                            To resolve the error, right-click on the error message to bring up the context menu and then select the option Add SDK component 'PINS' into the project '<project_name>'. After selecting the context menu option, you are presented with a confirmation window to review the list of files which will be added to the project. In this case, the option did not result in any new files, so there is nothing to review. You can check a box to avoid seeing this confirmation window in the future. Click Yes to confirm the changes. Select the Peripheral Signals tab at the upper left of the Pins perspective Check box for SIUL2 In the popup window Peripheral SIUL2, scroll to find gpio, 8 >> [A11] PA8 and gpio, 9 >> [B11] PA9. Check the box next to each. For each pin that is selected, an additional popup menu appears. Set both pins as Output. Then click OK and then Done. Set Identifiers for each as follows Pin Identifier PTA8/A11 LED1 PTA9/B11 LED2 Go to Peripherals tool Select Peripherals tab at upper left, check box to enable MC_ME Click OK. Now the driver is installed. Go to Clocks tool Change the following settings. They are not Run Mode specific. Hovering the mouse pointer over the object in the diagram will produce a tooltip window with information about the object including the name, current setting, output value, etc. Change prescaler ENETPLL_PHI0 (.pll2Config/.phi0Divider) from 2 to 8 Change the setting by first clicking on the prescaler box in the diagram, then clicking on the value in the 'Details' panel to the right. This brings up a list of available values. Select the desired value from the list. Once successfully changed, the values will be highlighted. Alternatively, a double-click on the value inside the prescaler box will bring up a drop list of the values and the selection can be made. Change prescaler VIDEOPLL_PHI0 (.pll4Config/.phi0Divider) from 4 to 2 Change mux AUX0_MUX (CGM0_AUX0_MUX) from FIRC to DDRPLL_DFS1 Change mux AUX8_MUX (CGM0_AUX8_MUX) from FIRC to DDRPLL_PHI0 To locate the next two, it is necessary to scroll down on the Clocks Diagram: Change mux CGM0_AUX7_MUX (MC_CGM_0_AUX7_MUX) from FIRC_CLK to ENETPLL_PHI0 Change mux CGM2_AUX2_MUX (MC_CGM_2_AUX2_MUX) from FIRC_CLK to ENETPLL_PHI0 Click Update Code Click OK Switch to C/C++ perspective Insert pins init using the configuration from 'board\pin_mux.c' If not already open, double-click on the following files from Project Explorer: 'board\pin_mux.c' 'src\main.c' Use the SDK Explorer Go to Quick Access field and enter 'sdk' Select 'SDK Explorer' If needed, drag the new SDK Explorer tab to the pane you prefer. In general, for this tool, a taller tab window works better. Select the project name in the Project Explorer tab and then expand the list under the SDK until you can see the list of CLOCK_DRV function defines. Drag and drop the function 'CLOCK_DRV_Init()' into main() of 'main.c', after the comment '/* Write your code here */'. Now locate the PINS_DRV function defines. . Drag and drop the following functions into the main() function of 'main.c', after the function call CLOCK_DRV_Init(): PINS_DRV_Init() PINS_DRV_ClearPins() The function calls are not in the format we need so let's modify them: Drag and dropped from SDK Explorer Change to this for our application status_t = CLOCK_DRV_Init(const clock_user_config_t*); CLOCK_DRV_Init(&clock_InitConfig0); status_t = PINS_DRV_Init(uint32_t, const pin_settings_config_t[]); PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr); PINS_DRV_ClearPins(GPIO_Type* const, pins_channel_type_t); PINS_DRV_ClearPins(LED1_PORT, ((1<<LED1_PIN)|(1<<LED2_PIN))); clock_InitConfig0 is defined in 'board/clock_config.c' NUM_OF_CONFIGURED_PINS, LED1_PORT, LED1_PIN, LED2_PORT, LED2_PIN are defined in 'board/pin_mux.h' g_pin_mux_InitConfig_Arr is defined in 'board/pin_mux.h' LED1_PORT == LED2_PORT Replace the contents of the FOR loop to toggle the pins (PINS_DRV_TogglePins() comes from SDK Explorer) Original New for(;;) {      if(exit_code != 0)      {           break;      } } for (;;) {      /* Insert a small delay to make the blinking visible */      delay(720000);      /* Toggle output value LED1 & LED2 */      PINS_DRV_TogglePins(LED1_PORT, (1 << LED1_PIN)|(1 << LED2_PIN)); } Insert delay function code in main.c delay() void delay(volatile int cycles) {      /* Delay function - do nothing for a number of cycles */      while(cycles--); } Now main.c should look as follows Build the project Now we have the ELF file We are ready to run on the hardware. Open the Debug Configurations Select the debug configuration within the debugger grouping for the debugger that was chosen in the new project wizard (step 1f), and for build type Debug_TCM S32 Debugger/S32 Debug Probe Select the Debugger tab. Some setup is required to configure how we are connected to the S32 Debug Probe There are two options: Ethernet USB   If connecting the Probe via Ethernet, please refer to the Quick Start Guide or S32 Debug Probe User Guide provided with the S32 Debug Probe for instructions on how to connect it and determine the Hostname or IP address.     If connecting the Probe via USB, then the COM port will appear in the Port selection setting. If you have more than one S32 Debug Probe connected, you will need to determine which COM port is the correct one, otherwise, only the COM port for your S32 Debug Probe will appear.   PEMicro GDB Server When debug probe setup is done, then click Debug to run the code. Agree to launch the debug perspective Now the debugger starts and you can see it has stopped on the default breakpoint at the first line in main(). From here you can Resume, Step, set a breakpoint, set watch variables and monitor registers. If you Resume, then you will see the LEDs on the EVB blinking. You can set a breakpoint on the PINS_DRV_TogglePins() and use Resume to see the LEDs come on and off.
查看全文
Example shows how can be expanded default 512kB flash memory by 64 kB using FlexNVM as a program/data flash. In FlexNVM are stored two ASCII images and function PrintImage. FlexNVM is divided into 32kB data section and 32kB code section in the linker file. Output is printed on terminal. As a output device you can use putty or any other serial terminal. Terminal settings: 9600, 8N1 - no flow control. In debugger settings you have to Enable partitioning device with code 0F0C. This value is written into FCCOB4 and FCCOB5 registers before flashing. Putty settings: Test HW: S32K144EVB, MCU: S32K144 Debugger: OpenSDA Target: internal_FLASH (debug mode and release mode)
查看全文
* Brief Periodical function call by LPIT timer ******************************************************************************** * Detailed Description: * Application performs function call on configurable period. Period in ms is * taken from potentiometer connected to ADC. * * * * ------------------------------------------------------------------------------ * Test HW: S32K144EVB, * MCU: S32K144 * * Debugger: PeMicro USB-ML-PPCNEXUS * * Target: internal_FLASH (debug mode, debug_ram and release mode) *
查看全文