S32 Design Studio 3.6.5 Release Announcement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio 3.6.5 Release Announcement

S32 Design Studio 3.6.5 Release Announcement

Product Release Announcement

Analog & Automotive Embedded Systems

S32 Design Studio 3.6.5

Irina_Costachescu_0-1765531594525.png

 

The Analog & Automotive Embedded Systems (AAES) - Software Development Tools Engineering Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio 3.6.5 with support for:

AMCU AP RAS APN
S32K3 Family S32G Family S32R41 Family S32J Family
S32K1 Family S32ZE Family S32R45 Family  
S32M2 Family S32N Family S32R47 Family  
    SAF8xxx Family  

 

Major Features for S32 Design Studio 3.6.5

Installer

  • S32 Design Studio 3.6.5 is delivered with all public NPI's in a single 2.63GB installer to improve first time user experience. Additional packages for alpha customers are available based on Flexera entitlement and can be installed on top of S32 Design Studio 3.6.5 using Extension and Updates.
Irina_Costachescu_1-1765531866020.png
 
  • Installer will require admin rights only when the user chooses to install components which need elevation (Visual Studio Redistributable or debugger drivers). If a user chooses a custom installation only with S32DS IDE and its components (no drivers) the installation will finish without admin rights.

Irina_Costachescu_2-1765531914107.png

 

Platform IDE and UI

  • Integrated Cody, the open-source Eclipse plugin from Sourcegraph, into S32 Design Studio. This plugin is installed by default, allowing users with a valid Cody license to log in directly within S32DS and access Generative AI features. Note: Users must agree to the Sourcegraph Terms of Service before using Cody.

Irina_Costachescu_2-1765456346536.gif

  • Enabled integration with the NXP Application Code Hub, allowing users to browse available examples and import them directly from the hub page into S32 Design Studio. Note: the application examples will be published soon on the Application Code Hub URL.

Irina_Costachescu_3-1765456346537.png

Note: This image is taken from internal sources. The illustrated examples are currently under development and will be available soon.

  • Extended the Quick Fix mechanism for the missing NPI and Real Time Drivers packages. Basically, an error message displays in the Problems view whenever the IDE identifies a missing package (build tool, NPI, RTD) associated with the current project. The Quick Fix automatically installs the missing package if it is available in the configured Update Sites. Note: not all scenarios are covered, there may be cases where the tool cannot determine if a package is missing.

Irina_Costachescu_4-1765456345392.png

  • A new Recent tab has been added in S32DS Extensions and Updates to display the latest installed packages, providing a clear history of user actions related to package installations. In addition, the default sorting was changed in All tab to bring greater visibility to NXP packages.

Irina_Costachescu_5-1765456346540.png

  • Added support for drag-and-drop of S32 Design Studio p2 update sites / installable packages into the S32DS Extensions & Updates window. Users can now simply drag the ZIP file into the window, and the package will be automatically inserted and selected, requiring only a click on Next to complete the installation.

Irina_Costachescu_6-1765456348052.gif

  • Significant improvements to Secure Debugging: 
    • Added a dedicated Debug Card view that allows users to generate debug card binaries based on custom input.
    • Implemented Challenge & Response functionality for Linux environment. 
    • Enabled Secure Registry Key view for managing secure registry keys on Linux. 
    • UI is aligned to the secure debugging functionality latest changes introduced by HSE2.

Irina_Costachescu_0-1765808827917.png

  • Extended the S32 Debugger OS awareness support with FreeRTOS.
    • OS threads are now visible in S32 Design Studio and user will be able to individually debug them.
    • Extended the command line support to display OS threads and objects.

Irina_Costachescu_8-1765456347125.png

  • Enable debug in low power mode with S32 Debugger for S32K3xx devices: 
    • The debug session will recover after core exits low power or standby mode, allowing the user to continue application debugging.
    • Debugging from the first instruction after low power exit is now possible by using this configuration command when starting the debug session: monitor template config :ccs:S32K3XX:SoC#0 6 1
  • Expanded the S32Trace debug-info parser to fully support DWARF-5, adding compatibility with projects using GCC 11.4 and newer.

 

Major Features for NPIs

S32N Family

  • S32Flash Programmer improvements for erase and verify write operations on S32N5.

S32G2/G3, S32J100, and SAF8xxx Families

  • S32J100 development package is now public and delivered inside S32DS installer.
  • Enabled debugging support for S32G2 devices on VDK R10.
  • S32Flash Programmer enhancements for erase and verify write operations.
  • Various bug fixes and improvements for arm cores and accelerators.

Irina_Costachescu_3-1765532135684.png

 

This release is available for download on:

 

Target Audience:

  • S32 Design Studio 3.6.5 and bundled NPIs releases are targeted for public audience.

 

The Installation Procedure for Packages:

  • Download S32 Design Studio v3.6.5, available on nxp.com and in Flexera catalogue S32 Design Studio for S32 Platform v.3.6.
  • If you have any local admin restrictions(ex. Admin by Request) the installer will request elevation, alternatively you can use “Run as Administrator” to run the installer.
  • Download any additional packages if it’s required.
  • Start S32 Design Studio v3.6.5 and install the desired package.
  • Go to  Help > S32DS Extensions and Updates.
  • For additional packages, in the S32DS Extensions and Updates dialog box, drag the ZIP file into the window, and the package will be automatically inserted and selected, requiring only a click on Next to complete the installation, or click Add Update Sites.
  • Navigate to the directory with the downloaded ZIP file. Choose it and click Open, then click OK.
  • You will get back to S32DS Extensions and Updates and can use this dialog to select desired packages.​​

 

Technical Support:

 

Irina_Costachescu_10-1765457452129.png

Attachments
No ratings
Version history
Last update:
‎12-16-2025 01:27 AM
Updated by: