S32 Design Studio 3.6.2 Release Announcement

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio 3.6.2 Release Announcement

S32 Design Studio 3.6.2 Release Announcement

Product Release Announcement

Analog & Automotive Embedded Systems

S32 Design Studio 3.6.2

Irina_Costachescu_0-1765791524153.png

 

The Analog & Automotive Embedded Systems (AAES) - Software Development Tools Engineering Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio 3.6.2 with support for:

AMCU AP RAS
S32K3 Family S32G Family S32R41 Family
S32K1 Family S32ZE Family S32R45 Family
S32M2 Family    

 

Major Features for S32 Design Studio 3.6.2

Installer

  • S32 Design Studio 3.6.2 is delivered with all public NPI's in a single 3GB installer to improve first time user experience. Additional packages for alpha customers are available based on Flexera entitlement and can be installed on top of S32 Design Studio 3.6.2 using Extension and Updates.
Irina_Costachescu_0-1765808449510.png
 
 
Platform IDE and UI
 
  • Enhanced debugging efficiency by at least 20%. It applies to the entire debug session initialization pipeline and was measured from the moment Debug is pressed until the main() is reached.
  • Live view mechanism was introduced in Memory Spaces and Global Variables views when target is running in non-stop mode. Users can observe real-time changes to memory addresses and variables, improving visibility into the runtime behavior. A configurable refresh rate allows tunning the update frequency based on performance needs.

animation-ezgif.com-optimize.gif

  • A new entry named assigned core was added in the Task List (FreeRTOS) view, it targets SMP cases.

freertos_new.png

  • Expressions with global scope can now be added straight from the Global Variables panel, without needing to switch to a separate view.

new_var_global_var.png

  • Added option to export registers description during data export from the Watch Registers view. 

export_regs.png

  • Find & Paste functions were enabled in Memory Management Unit (MMU) view.
  • Added support for Enable auto build in S32 Debugger configuration.
  • Enabled support for Additional Images in S32 Debugger configuration, for cases when additional source objects are loaded in the Flash memory.
  • Enabled Advanced Settings to set the CCS IP and Port for S32 Debugger Flash Programmer debug configurations.

 

3rd Party Solutions 

  • Update of 3rd Party Debug support:
    • Segger J-Link v8.28
    • PEmicro v6.0.2
    • TASKING v9.21.333

 

Major Features for NPIs

S32K3 Family

  • Merged  S32K389 into S32K3xx development pack to be available for all customers with S32DS 3.6.2 installer file.
  • Enabled Wind River Diab 7.0.6 and IAR 8.50.10 compilers for S32K389.
  • Enabled PEmicro v6.0.2 and IAR 8.50.10 debuggers for S32K389.
  • Extended IAR and Segger debugging support for S32K36x, S32K37x, S32K39x, S32K341, S32K342 and S32K322 derivatives.
  • Enhanced S32Flash programmer over JTAG to detect the presence of the HSE FW and adapt the flash operations considering HSE FW reserved flash addresses.

gdb.jpg

 

This release is available for download on:

 

Target Audience:

  • S32 Design Studio 3.6.2 and bundled NPIs releases are targeted for public audience.

 

The Installation Procedure for Packages:

  • Download S32 Design Studio v3.6.2, available on nxp.com, in Flexera catalogue S32 Design Studio for S32 Platform v.3.6, and in Automotive Software Package Manager.
  • If you have any local admin restrictions(ex. Admin by Request) the installer will request elevation, alternatively you can use “Run as Administrator” to run the installer.
  • Download any additional packages if it’s required.
  • Start S32 Design Studio v3.6.2 and install the desired package.
  • Go to  Help > S32DS Extensions and Updates.
  • For additional packages, in the S32DS Extensions and Updates dialog box, click Add Update Sites.
  • Navigate to the directory with the downloaded ZIP file. Choose it and click Open, then click OK.
  • You will get back to S32DS Extensions and Updates and can use this dialog to select desired packages.​​

 

Technical Support:

Irina_Costachescu_2-1765793361328.png

 

Attachments
No ratings
Version history
Last update:
‎12-16-2025 01:27 AM
Updated by: