S32 Design Studio Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio Knowledge Base

Discussions

Sort by:
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM v2.0, Update 1             What is new? This update/service pack adds bareboard support for NXP S32K146 device into the S32 Design Studio for ARM v2.0   Installation instructions The update is available for online (Eclipse Updater) or offline (direct download link) installation.   online installation: go to menu "Help" -> "Install New Software..." dialog select predefined NXP S32 Design Studio update repository S32 Design Studio for ARM v2.0 - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2_0/com.freescale.s32arm.updatesite select all available items and click "Next" button   offline installation: go to S32 Design Studio product page -> Downloads section or use the direct download link to download the "S32 Design Studio for Power v1.2 - Update 2" file.   Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded Update 2 archive file: Select all available items and click "Next" button. This will starts the update installation.
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 3          What is new? S32 SDK for Power Architecture 0.8.3 EAR for S32Rx7x. This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2 ). Installation instructions The update is available for online (via S32DS Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use  direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Updates 5 and 6          What is new? S32 SDK for Power Architecture 1.0.0 RTM supporting MPC574xx.  Service Pack supporting MPC5775 B/E This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4 ). Installation instructions The update is available for online (via S32DS Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use  direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
View full article
This application shows how to  build and debug BOOKE based project. It contains BOOKE startup/ISR code and it is compiled to generate non-VLE BOOKE code. Note: Before running this project please make sure your startup script is configuring MMU to use BOOKE instructions. The script is typically located here: "c:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.3.201803261737\win32\gdi\P&E\s32e200_mpc564xa.mac" The plugin version folder may differ. The updated script is part of attached ZIP archive.
View full article
This document details the steps to program external EEPROM with the 32 reset configuration bits in support of the 'Boot from serial RCON' method detailed in the S32R Reference Manual. The Python scripts used for this task are designed and tested to work on the S32R45 EVB and the Atmel AT24C01C it contains.   The RCON can be set by the following: Fuses (internal to the device) Parallel (GPIO pins/DIP Switches on S32R45 EVB) Serial (EEPROM connected via I2C) The Serial option can be programmed using a debug probe connected via JTAG. This enables the RCON to be controlled remotely, assuming the debug probe is setup to allow remote connections.  Preparation Install S32 Design Studio IDE  Install the Development Package for the device you are debugging. This is important as the S32 Debugger support within it contains the device-specific Python scripts required for initialization of the cores.  Connect the S32 Debug Probe to the S32R45 EVB and the host PC containing S32 Design Studio installation. Set BMODE pins to Boot from RCON Set BOOT_CFG[8]=1 on the S32R EVB, for serial RCON mode See the EVB documentation and device reference manual for more details on BOOT_CFG settings, etc.   Procedure  Open cmd window to the S32 Debugger folder where the device-specific scripts are located. C:\NXP\S32DS.3.4\S32DS\tools\S32Debugger\Debugger\scripts\s32r45 Set Python path so correct version is used (if not already set in env vars) set PYTHONPATH=C:\NXP\S32DS.3.4\S32DS\build_tools\msys32\mingw32\lib\python2.7;C:\NXP\S32DS.3.4\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages Edit the python script to adjust the value to be programmed to RCON, s32r45_i2c_RCON.py. Note: The listed examples show only the minimum values required to configure each of the external memory types. Additional settings may be required for your specific application.       Adjust the RCON_DATA for the configuration you wish to program.  Do not adjust RCON_ADDR. Adjust the S32DBG_IP for the IP address of your S32 Debug Probe.  Adjust the INTERACTIVE_MODE Set True, if desired to be prompted in the command window to enter RCON_DATA Set False, if desired to have script automatically enter RCON_DATA, based on the value set within the file. Enter the command to start GDB, passing in the RCON Python script: Windows OS: C:\NXP\S32DS.3.4\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe -x s32r45_i2c_RCON.py Linux OS: arm-none-eabi-gdb-py -x .\s32r45_i2c_RCON.py   You may need to press enter a couple of times. If everything worked properly, then the value you programmed will be displayed to the screen. To exit GDB, enter 'quit'. Before performing boot from serial RCON, remember to set BOOT_CFG[8] = 1. See the EVB documentation and device reference manual for more details.
View full article
This example performs basic initialization, sets PLL to maximum allowed frequency 200MHz, sets clock for peripherals, GPIO pins, PIT timer and interrupt controller. After initialization it blinks LED2 in the main loop using timeout counter variable. PIT timer generates periodical interrupts and toggles LED1 with 1s period. Test HW: MPC5746R-252BGA, MPC57xxMB Motherboard MCU:  PPC5746R 1N83M Fsys: PLL0 266MHz       Z4 Core 200MHz Debugger: PeMicro USB-ML-PPCNEXUS IDE/Compiler: S32DS for Power 2017.R1 / GCC Target: internal_FLASH - debug, release              internal_SRAM - debug_ram EVB connection:   Default EVB jumper setup   Connect LED1 to P14.3 on motherboard   Connect LED2 to P14.4 on motherboard
View full article
So you've just installed the S32DS for Vision and are using it for the first time and would like to see how it works. Here is a quick and simple project to get you started.   1. Launch S32DS for Vision 2. Select 'S32DS Application Project' 3. Enter a name for the project 4. Select the 'A53 Linux' processor option 5. Click Next 6. Click Finish 7. Change to C/C++ perspective, click on 'Switch to C/C++ Development' 8. Build the project for Debug 9. Project is now built, ELF file is read to be loaded to EVB for execution. However, if we have not prepared the EVB, we must first complete HOWTO: Setup S32V234 EVB for debugging with S32DS for Vision and Linux BSP. 10. Once the EVB is properly prepared, we must complete HOWTO: Setup A Remote Linux Connection in S32DS for Vision. 11. With the project debug configuration and remote linux connection selected, select the debug dropdown menu and click Debug Configurations 12. Make sure the Debug_Remote_Linux debug configuration is selected and the connection setup in step 10 is selected (points to the IP address of your EVB). Click Debug 13. The first time you connect to a new IP address (i.e. the first time you debug after booting the board), you will receive a warning message, Click Yes and proceed. 14. The executable file is copied to Linux file system and gdbserver starts. 15. The Debug perspective is opened. You can now step through the code*     *Only debugging of the A53 code is supported by Linux GDB. For multicore debugging, including ISP and APEX2, additional debugger and probe(S32 Debugger with S32 Debug Probe, Lauterbach, etc) will be required.
View full article
Users can now get the AMMCLib for S32K3 in S32DS 3.4 if they manually add the following URL to the list of “Available S32DS Software Sites”: http://www.nxp.com/lgfiles/updates/Eclipse/AMMCLIB/S32DS_3.5 (the URL will be auto-added with the upcoming S32DS 3.5 release). From within S32 Design Studio for S32 Platform 3.4, launch S32DS Extensions and Updates menu (Help -> S32DS Extensions and Updates), then select 'Add Update Sites'. Please note that the S32K3XXMCLUG.pdf User’s Guide incorrectly indicates that the library is available as a standalone SDK, which is incorrect. AMMCLib for S32K3 is part of the “PlatformSDK” system which means that users must use the RTD for S32K3 in their S32DS project to gain access to AMMCLib:   Then they must activate the „S32 Configuration Tool“ (CT):   Within the CT, they must click on the „Peripherals“, then „Libraries“, and select „AMMCLib“ from the list:   Then they must click on „Update code“, to update the paths in the project:    
View full article
S32DS contains many example projects from which you can learn how S32DS can be used with the help of the Vision SDK to develop vision applications. The example projects contain generated and hand-written code, which utilize the Vision SDK to demonstrate a workflow using S32DS. In this document, the procedure for creating a project from one of the provided ISP examples through to execution on the EVB is detailed. This project was run using S32DS version 3.2 and VSDK version 1.5.0.   1) Launch S32DS 2) Select 'File -> New -> S32DS Project from Example' 3) Select 'isp_h264dec_single_stream' project    In this particular project, the ISP graph diagram is included. If you wish to view it, go to the Project Explorer panel and expand 'isp_h264dec_single_stream_graph'. Then double click on 'ISP data flow : h264dec_single_stream'. The ISP graph diagram will appear in the editor panel. 4) If not in the C/C++ Perspective, switch over by clicking on the icon showed below (Hovering over the correct icon should display 'C/C++'). The current perspective is displayed on the top bar. 5) Select isp_h264dec_single_stream: A53 in the Project Explorer panel 6) Build project for A53  7) Start a debug session using method as described in HOWTO Create A53 Linux Project in S32DS for Vision, beginning at step 9. 😎 Click Resume  The program takes the input H264 encoded image img_1280x960.h264 located in the /home/root/vsdk/data/common folder on the Linux BSP and outputs it on the display The output image should look like below.
View full article
S32DS contains many example projects from which you can learn how S32 can be used with the help of the Vision SDK to develop vision applications. The example projects contain generated and hand-written code, which utilize the Vision SDK to demonstrate a workflow using S32DS. In this document, the procedure for creating a project from one of the provided APEX2 examples through to execution on the EVB is detailed. This tutorial was made with S32DS Version 3.2 and VSDK Version 1.5.0. 1) Launch S32DS 2) Select 'File -> New -> S32DS Project from Example' 3) Select apex2_rotate_180 project 4) Click Finish 5) If not in the C/C++ Perspective, switch over by clicking on the icon showed below (Hovering over the correct icon should display 'C/C++'). The current perspective is displayed on the top bar. 6) Select apex2_rotate_180: A53 in the Project Explorer panel. Build the project using build config 'TEST_A53'. 7) Start a debug session using method as described in HOWTO: Create A53 Linux Project in S32DS for Vision, beginning at step 9. 😎 Click Resume  The program takes the input image  in_grey_256x256.png located in the /home/root/vsdk/data/common folder on the Linux BSP and rotates it 180 degrees The output image out.png is located inside the /home/root/vsdk folder 9) To see the output, access the device from the remote systems view. If this has not been set up, complete the steps described in HOWTO: Access Linux BSP file system on S32V234-EVB from S32DS for Vision.  10) Open both the input and output files from the remote systems view to verify that the program ran correctly.
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio 3.2  Update 191226          What is new? Vision Extension Package for S32V234 1.1.0 with VSDK 1.5.0 integrated.(VSDK Release Notes) This is a cumulative update (includes previous updates: Update 191219) Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link)  online installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button   offline installation:   go to S32 Design Studio product page -> Downloads section or use direct link to download the update archive zip file Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates" Add a new "Add.." S32DS Software Site and browse to select the downloaded update archive .zip file you downloaded in the previous step         Select from available items and click "Install/Update" button. This will start the update installation process.
View full article
The S32 Debugger included within the S32 Design Studio for S32 Platform IDE provides the capability to access the flash programming capabilities of the S32 Debug Probe via the S32 Debugger.   Note: currently only QSPI flashing is supported.   Preparation Install S32 Design Studio IDE  Install the Development Package for the device you are debugging. In this case, the S32R4xx development package. This package is important as the S32 Debugger support component contains the device-specific Python scripts required for initialization of the cores.   Open the application project from which the flash image will be generated. Follow the steps in HOWTO: Generate S-Record/Intel HEX/Binary file , selecting the 'Raw Binary' option. Build the project, generating the binary executable. This will be our application binary input to the IVT Tool. The IVT Tool must be used to generate the BLOB image which can be programmed to flash memory device and loaded to the RAM by the BootROM. Follow the steps in HOWTO: Use IVT Tool To Create A BLOB Image S32R45. The resulting BLOB image file is what can be flashed to the device.   Procedure Open Debug Configuration menu Select 'S32 Debugger Flash Programmer', then right-click and select New. Enter an name for the new configuration and click Add... to add the file to be flashed. Click Browse... to select the project from the workspace where the application binary is located Select the project and click OK By default, the ELF file is found. Click Search in project to select the binary file. Select the .bin file and click OK Now we must enter the base address. Typically, this could be 0, but you may have other requirements. Click OK. Now we are ready to configure the debugger connection settings. Click on the Debugger tab. Starting from the top and working our way down, click on Select device. Select the device and click OK The correct Initialization script will automatically be set. Set the Debug Probe Connection settings to match your setup. When done, click Apply To start the flashing, click Debug Flashing progress will be displayed. When complete, the Debug perspective will show at terminated thread.   Happy flashing with GDB! Note, to debug this application since it will be subsequently started by the BootROM: use 's32r45_attach.py' in the Initialization script field on the debugger tab of the Debug Configurations menu Make the following adjustments on the Startup tab within the Debug Configurations menu: Uncheck "Load image" Check “Set program counter at:” and enter the value “Reset_Handler”
View full article
The NXP device S32R41 has accelerators that can be programmed. The S32 Debugger included within the S32 Design Studio for S32 Platform IDE with the S32 Debug Probe provides the ability to debug these accelerators. The accelerator covered in this document: Signal Processing Toolbox (SPT).   Section map: Preparation             Setup the software tools             Setup the hardware Procedure             Create A New Debug Configuration                                Start A Debug Session                         Multi-Core Preparation Setup the software tools Install S32 Design Studio for S32 Platform Install the S32R41 development package and the Radar extension package for S32R41. Both of these are required for the SPT3.5 accelerator. Setup the hardware Confirm the setup of the S32R41 evaluation board. Connect the power supply cable Setup the S32 Debug Probe. Refer to the S32 Debug Probe User Guide for installation instructions. Connect the S32 Debug Probe to the evaluation board via JTAG cable. Connect the S32 Debug Probe to the host PC via USB cable OR via Ethernet cable (via LAN or directly connected and configured for static IP address) and power supply connected to USB port. Launch S32 Design Studio for S32 Platform Open existing project or create a new project and check that it successfully builds. If creating a new project, be sure the S32 Debugger is selected in the New Project Wizard.   Procedure The procedure for starting a debug session and accessing the associated accelerator-specific registers is detailed here. Debugging SPT is only conducted through the multi-core method. The SPT executable is included within A53 executable, the A53 application loads the SPT executable to the SPT core and both A53 and SPT core are available for debugging. The debug connection is made to the two cores through the Baremetal/Bareboard method. The debugger connects to both the A53 and SPT cores using the probe over JTAG. Before a debug session can be started a debug configuration must exist.   Create A New Debug Configuration If the New Project Wizard was used to create the project using the S32DS Application Project option, then there was an opportunity to select the desired debugger from within the wizard. If the desired debugger option was selected at this time, then the needed configuration already exists and will only require adjustments to the hardware connection settings.   If the New Project Wizard was not used to create the project OR the currently desired debugger was not the one selected at the time of project creation, a new debug configuration must be created. With the existing project selected in Project Explorer, open the Debug Configurations Menu: Run -> Debug Configurations Having the existing project selected in the Project Explorer view will make the creation of a new launch configuration easier as many settings will be imported from the selected project. To select a project, click on it so it becomes highlighted. Next, select the debugger for which the new debug configuration will be created. To create the new configuration, either click on the ‘New launch configuration’ button from the toolbar at the top and to the left, or right-click on the ‘S32 Debugger’ and select ‘New Configuration’ from the menu. Once the configuration is created it will be displayed and any errors with the configuration will be shown. If the project was selected in the Project Explorer, then the Name of the debug configuration will contain the project’s name and the Project and C/C++ Application fields may be populated as well. The C/C++ Application field will only be populated if the build output executable exists. Confirm these values are correct before moving on. If the C/C++ Application field is empty, just click ‘Browse..’ button (The ‘Search Project…’ button is setup to identify standard executable file types, not the SPT’s ‘aspt’ file type) and navigate to the folder containing the build output <project name>.aspt. If you like, the tool already knows the project directory path, so you could shorten the path to start with from the ‘Debug’ folder, as shown here. There is an error showing that the Device core ID is not specified on the Debugger tab. Switch to the Debugger tab and click on the button ‘Select device and core’. From the Select Target Device and Core window, expand the listing until all cores are listed. Notice that all supported cores on the S32R41 are listed. Select the SPT35 core and click OK. Now that the device and core are selected, the attach script is selected automatically. The attach script will allow to start debugging on a core that is already initialized. This is correct for the SPT core as it is always launched in multicore scenario. Refer to the document 'README.txt' located in the same folder as these script files for details on all of the provided scripts. Confirm the setting of the ‘Initial core’ checkbox. This box should be checked within the debug configuration that establishes the first connection to the target device via S32 Debug Probe. When this box is checked, the Debug Probe Connection interface and GDB Server settings become available. The probe connection only needs to be configured once and only one GDB Server needs to be running for each debug session. When debugging the SPT3.5 core, the A53 core will always launch first, so this box should be checked for the A53 debug configuration and should not be checked for the SPT debug configuration. Check that the GDB Client section has the correct path to the SPT GDB executable. It should point to the variable ‘S32DS_R41_GDB_SPT_PATH’. Startup tab check the following settings Load image is NOT checked for multicore debugging. Basically, if it is loaded by A53 core (SPT executable is contained within A53 ELF file), then it does not need to be loaded. Load symbols is NOT checked. The SPT source file is assembly code, so there are no symbols to load. Set breakpoint at main and Resume are NOT checked for multicore debugging. After saving the new configuration with the ‘Apply’ button, SPT debugging can be performed. Start A Debug Session For convenience, the S32DS Application Project wizard was used to create a new project for demonstrating multi-core A53/SPT debugging. The SPT core does not support standalone debugging. For instructions on loading this example project to your workspace, see ‘HOWTO: S32 Design Studio - Create New Application Project’, selecting instead the Processor option Family S32R41 -> S32R41xxx Cortex-A53 SPT3 from the wizard menu. A53 / SPT Multi-Core For multi-core debugging, the A53 core is running an executable which also contains the SPT code. The A53 code will make a call into the SPT to load the SPT code to memory and to start the SPT execution. So the A53 must be started first. The EVB settings are irrelevant as the debugger will take control of the target via the JTAG connection. Before beginning the debug sessions, be sure each project is built clean. Start A53 debug. From the menu at the top, select Run -> Debug Configurations… In the Debug Configurations menu, from the configuration list, look for the ‘S32 Debugger’ group and select the A53 Debug_RAM configuration for the project to be debugged. In the case of our example, the ‘New_S32R41_SPT_Project_A53_Debug_RAM_S32Debug’ configuration. On the Debugger tab, check that the Debug Probe Connection settings match with the current hardware connection configuration for the S32 Debug Probe. Use the ‘Test connection’ button to confirm. Click Debug to start debugging on the A53 core. The debugger will launch and execute until the first executable line in main(). See Debugger tab in Debug Configurations menu to adjust this setting. Once the A53 debug session is running, advance the program counter to a line after the desired SPT kernel is loaded to memory but before the SPT kernel is launched. In the example here, this would be in ‘main.c’, line 57, where ‘StartSptProgram()’ function is called. This can be done by setting a breakpoint on the line and clicking Resume.  After the breakpoint is reached, the SPT debug session can be started. Return to the Debug Configurations menu, select the SPT debug configuration. In the case of this example, ‘New_S32R41_SPT_Project_SPT35_Debug_S32Debug’, and click Debug. Wait for the SPT debug session to launch and stop in the disassembly. Use the Step Over command one time in the A53 debug thread to complete the SPT launch. Select the SPT debug thread to change the context of the Disassembly, Registers and etc.views. Notice the SPT code is not loaded yet. Enable Instruction Stepping Mode and step one time. Notice the SPT code is now loaded. Now you can step through the assembly code, access registers, etc.
View full article
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 4          What is new? Radar SDK RTM 1.0.0. This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3). Installation instructions The update is available for online (via S32DS Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use  direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
View full article
Example contains modified startup code to be able run in BookE only mode. For GNU gcc and as you need to add -mno-vle parameter in project properties:  For debugging with PE Micro you need to use modified Initialization script in Advanced options: Please note that there is no STD C BookE only library available:
View full article
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power v1.2, Update 1 1            What is new? The S32 Software Development Kit (S32 SDK v0.8.0 EAR) which is an extensive suite of peripheral drivers, RTOS, stacks and middleware designed to simplify and accelerate application development on NXP Power MPC5748G and MPC5746C microcontrollers. Release notes are available here: http://www.nxp.com/docs/en/release-note/C55_SDK_EAR_0.8.0-RN.pdf  Installation instructions The update is available for online (Eclipse Updater) or offline (direct download link) installation.   online installation: go to menu "Help" -> "Install New Software..." dialog select predefined NXP S32 Design Studio update repository http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_1_2/com.freescale.s32power.updatesite  select all available items and click "Next" button offline installation: go to S32 Design Studio product page -> Downloads section or use the direct download link to download the "S32 Design Studio for Power v1.2 - Update 1" file.   Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded Update 1 archive file: Select all available items and click "Next" button.
View full article
On some versions of Windows 10, there is an issue which could impact your ability to open documents from the Getting Started page in S32 Design Studio. While we have resolved this issue in some of the newer releases, not all editions of S32 Design Studio have been updated since this issue was discovered. Also, you may required to use an older release. The problem occurs when a document linked within the Getting Started window of S32 Design Studio. The S32 Design Studio is configured to use the Windows default web browser to open the files. For some Windows 10 installations, Microsoft Edge is the default browser and it is unable to correctly open the requested file. The typical error message is as shown below: To resolve the issue, it is necessary to change the default browser within your Windows preferences. Here are some steps to do that: 1) Click on 'Settings' from the Windows Start Menu 2) Type 'browser' in the search bar, then select 'Choose a default web browser' 3) Click on the currently selected Web browser to bring up the selection menu and select 'Internet Explorer' or 'Google Chrome' 4) Relaunch S32 Design Studio and try again to open the document from the link in Getting Started page.
View full article
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio v3.4 Vision Extension Package for S32V23x 1.3.0          What is new? Integrated VSDK 1.7.0   Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button offline installation:   go to S32 Design Studio for S32 Platform product page -> Downloads section or use direct link to download the update archive zip file        Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Add Update Sites' link Select the downloaded update archive zip file you downloaded in the previous step       Select the 'Vision extension package for S32V23x' package and click "Install/Update" button.   This will start the update installation process.
View full article