S32 Design Studio知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Design Studio Knowledge Base

讨论

排序依据:
In embedded systems development, attention to memory utilization is universal. In S32 Design Studio, this information can easily be provided at the end of a successful build by invoking a linker option. Right-click on the project name in the Project Explorer panel and select 'Properties' from the menu. Navigate to the C/C++ Build -> Settings ->Standard S32DS C Linker -> Miscellaneous menu. From the Other options section, click Add. image.png In the 'Enter Value' pop-up menu, enter: -print-memory-usage image.png Click OK, then Apply and Close. Now build the project and see the memory usage information displayed in the Console window. image.png
查看全文
Migrating an SDK project for S32K1xx devices between SDK v4.0.1 and v4.0.2 is not as simple as attach and detaching the SDKs. It is complicated by the fact that SDK v4.0.1 is supported by only S32DS v3.3 and SDK v4.0.2 is supported by only S32DS v3.4. So this means both SDKs will not be present at the same time in one version of S32DS. In addition, the method for attaching the SDKs changed between SDK v4.0.1 and v4.0.2. In v4.0.1, the SDKs were added to the S32DS project via a link. In v4.0.2, the SDK files are added to the S32DS project by copying the actual files into the project. To overcome this, it is necessary to perform some manual operations. The steps required are detailed in this document, along with the necessary steps to adapt the .mex file containing the S32 Configuration Tools settings. Due to differences in projects based on the method of creation, there are 3 scenarios to be covered here which are assumed to be the most common: Project was created by 'New Project from Example' wizard and one of the SDK example projects was selected. Project was created by 'New Application Project' wizard and the SDK was selected for attachment within the wizard. Project was existing one and SDK was attached using the SDK management tool. Due to enough similarities between the projects, the last two will be covered as one scenario, under the heading 'New Application Project'. The first one will be covered under the heading 'New Project from Example'. Prerequisites Install S32 Design Studio IDE 3.4 Install the S32K1xx development package and S32SDK S32K1XX RTM 4.0.2 package image.png Procedure New Project from Example For this demonstration, the S32K1xx SDK v4.0.1 example project 'flexio_i2s_master_s32k144' will be used. Open or create the project within S32DS 3.3 image.png Expand project directory in Project Explorer and look for .mex file image.png If no .mex file is present, then right click on project name and select 'S32 Configuration Tool -> Open Pins' (could select any tool within S32 Configuration Tool). Even though the .mex file contains the settings for S32 Configuration Tools, the same settings are also preserved in YAML code placed into the headers of each of the .c files generated by the S32 Configuration Tools into the 'board' folder in the project. By opening the S32 Configuration Tools, it detects there is no .mex file and scans the generated files for the YAML code. If YAML code is found, then a new .mex file is produced and placed in the project. image.png The perspective is changed to the Pins Tool, nothing more needs to be done, .mex file has been created from the YAML code. If no YAML code had been found, then the user would be presented with a menu to select target device and SDK. Switch back to C/C++ perspective to confirm. image.png image.png Open S32DS 3.4 and import the project. It is important to note that separate workspaces should be used for S32DS 3.3 and S32DS 3.4. The project should be imported into the S32DS 3.4 workspace so the checkbox 'Copy projects into workspace' should be ticked. image.png image.png image.png Right-click on Project -> Properties -> C/C++ Build -> Settings -> Standard S32DS C Compiler -> Includes, then delete all paths which contain 'S32_SDK_PATH' image.png image.png Repeat for Standard S32DS Assembler -> General image.png Apply and Close image.png The files in the SDK folder were included in the project as links and not actual files, and since the SDK 4.0.1 is not installed to S32DS 3.4, the links point to non-existing files. This means the Attach function in the SDK manager will not be able to replace them with the corresponding files from SDK 4.0.2 because it doesn't know how to replace files which don't exist. From Project Explorer, delete folder ' SDK' from the project. image.png Now the project is ready to use the SDK manager to detach the old SDK and attach the new SDK. In Project Explorer, right-click on Project -> SDKs. image.png When the SDK manager launches, it scans the project for any attached SDKs. In the case of this example, an SDK is detected as attached, but since it does not match any installed SDKs, a message appears asking to detach SDK 4.0.1. Since this is a desired action, click OK. image.png With SDK 4.0.1 already detached, select SDK 4.0.2, click 'Attach/Detach...' image.png Click 'Select All' to attach the SDK to all build configurations. This sets up the include paths, and linker paths for the SDK for each build configuration. If desired, the build configurations could be selected individually. Click OK to complete the selections. image.png To apply the changes and exit the SDK manager, click 'Apply and Close'. image.png The SDK Manager detects that some of the files from the new SDK are replacing existing files in the project. By default, all conflicting files are set to replace the existing file. If desired, individual files can be deselected. Please note, with the checkbox for 'Backup project files' ticked, any files replaced will be preserved in a backup folder for future recovery, comparison, etc. In general, it may be wise to allow the file to be replaced and later merge with the customizations in the backup folder. For this example, no modifications were made, so default settings are kept. Click OK to complete the process. image.png The new SDK is attached and the new SDK folder can be identified. image.png The .mex file contains the settings for the S32 Configuration Tools, however, it is still set for the SDK 4.0.1. It must be manually updated so the S32 Configuration Tools can be used to generate the new code for the 'board' folder. Right-click on .mex file and select 'Open With -> Text Editor'. image.png All that is required is to modify the mcu_data section containing the SDK name: 's32sdk_s32k1xx_rtm_401' -> 's32sdk_s32k1xx_rtm_402' image.png image.png Now save the change. image.png Next, the files in the 'board' folder must be regenerated from the S32 Configuration Tools to reflect the new SDK. Right-click on the .mex file and select 'Open With -> S32 Configuration Tools'. image.png A warning message appears indicating that it has detected the mex file was created in an older version of the tool and that once the mex file is saved in the current tool, it may no longer open in an older version of the tool. This is expected. Click OK. image.png Notice the error symbol. Mouse-over to see the details. It is an error with Peripherals tool. Select Peripherals tool. image.png The issue is with edma_config_1, because it is highlighted red. Click on it to see the interface. The interface changed from the previous version to allow for multiple configurations where previously it supported only one. To resolve the error a new configuration must be added to the list. Click on the '+' as shown to add the new configuration. This particular error will only appear for projects which include the EDMA module. image.png The Problem Indicator is now green, this means there are no warnings or errors. It is now time to generate the code, click 'Update Code' image.png A menu appears identifying new and/or updated files. If desired, selecting 'change' on a row will open a comparison tool showing the changes between the existing and the new versions of the associated file. Click OK to proceed. image.png Switch to C/C++ perspective image.png Errors on project are now gone. If the project successfully built before the conversion, then build again to confirm everything was converted properly. image.png image.png   New Application Project For this demonstration, a new project will be created in S32DS 3.3 using the New Application Project wizard and the S32K1xx SDK 4.0.1 will be selected during project creation. Import the project into S32DS 3.4 image.png image.png image.png Use the SDK Manager to detach the old SDK and then attach the new SDK. In Project Explorer, right-click on Project -> SDKs. image.png When the SDK manager launches, it scans the project for any attached SDKs. In the case of this example, an SDK is detected as attached, but since it does not match any installed SDKs, a message appears asking to detach SDK 4.0.1. Since this is a desired action, click OK image.png With SDK 4.0.1 already detached, select SDK 4.0.2, click 'Attach/Detach...' image.png Click 'Select All' to attach the SDK to all build configurations. This sets up the include paths, and linker paths for the SDK for each build configuration. If desired, the build configurations could be selected individually. Click OK to complete the selections. image.png To apply the changes and exit the SDK manager, click 'Apply and Close'. image.png The SDK Manager detects that some of the files from the new SDK are replacing existing files in the project. By default, all conflicting files are set to replace the existing file. If desired, individual files can be deselected. Please note, with the checkbox for 'Backup project files' ticked, any files replaced will be preserved in a backup folder for future recovery, comparison, etc. In general, it may be wise to allow the file to be replaced and later merge with the customizations in the backup folder. For this example, no modifications were made, so default settings are kept. Click OK to complete the process. image.png The .mex file contains the settings for the S32 Configuration Tools, however, it is still set for the SDK 4.0.1. It must be manually updated so the S32 Configuration Tools can be used to generate the new code for the 'board' folder. Right-click on .mex file and select 'Open With -> Text Editor'. image.png All that is required is to modify the mcu_data section containing the SDK name: 's32sdk_s32k1xx_rtm_401' -> 's32sdk_s32k1xx_rtm_402' image.png image.png Now save the change. image.png Next, the files in the 'board' folder must be regenerated from the S32 Configuration Tools to reflect the new SDK. Right-click on the .mex file and select 'Open With -> S32 Configuration Tools'. image.png A warning message appears indicating that it has detected the mex file was created in an older version of the tool and that once the mex file is saved in the current tool, it may no longer open in an older version of the tool. This is expected. Click OK. image.png Check for any errors or warnings by looking for the yield sign. It will change color based on the conditions: Green = No Problems, Yellow = Warnings, Red = Errors. Mouse-over the icon for more information on the location of the error. Aside from resolving warnings and errors, there should be no changes required as the settings have been preserved from the original project. In this example, there are no warnings or errors, so it is possible to proceed with updating the generated files. Click 'Update Code' image.png A menu appears identifying new and/or updated files. If desired, selecting 'change' on a row will open a comparison tool showing the changes between the existing and the new versions of the associated file. Click OK to proceed. image.png Change back to C/C++ perspective. Errors on project are now gone. If the project successfully built before the conversion, then build again to confirm everything was converted properly. image.png
查看全文
      Product Release Announcement Automotive Processing S32 Design Studio v3.4 Update 1 for S32G2 mikedoidge_0-1624918289889.png         Austin, Texas, USA Apr 30, 2021 The Automotive Processing' Software Development Tools Engineering Team at NXP Semiconductors is pleased to announce the release of the  S32 Design Studio v3.4 Update 1 for S32G2 Here are some of major features:​ S32 Configuration Tool framework 1.4 with the Pin, Clock, Peripheral, DCD, IVT, DDR and QuadSPI Configuration tools (SDK/RTD packages required to get support for particular device)  Updates S32 Debugger  Updated S32 Flash Tool Update is available for online install on update site and for download on flexera  S32G2 support: (SW32G2_S32DS_3.4.1_D2104.zip) updated version of header files in accordance with RM Rev 3 Update is available for online install on update site and for download on flexera. Note that Update 1 (S32DS Platform Package version 3.4.1 and S32DS Platform Tools package version 3.4.1) is required for the S32G2 support package. It is included into archive for download. Installation instructions The update is available for online (via Eclipse Updater) or offline installation   online installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button image.png   offline installation:   go to S32 Design Studio product download page: S32 Design Studio for S32 Platform -> Downloads, click 'Download' button next to S32 Design Studio 3.4 -- Windows/Linux image.png from the Product Information page, select S32 Design Studio 3.4 Update 1, support for S32G2 family image.png then select 'SW32G2_S32DS_3.4.1_D2104.zip' to download the update archive zip file image.png Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates" image.png Add the downloaded archive as a software site. Click "Add Software Site" and browse to select the archive file downloaded in the prior step        image.png Select from available items and click "Install/Update" button. mikedoidge_1-1624999657510.png This will start the update installation process.   Technical Support please use public community for questions https://community.nxp.com/community/s32/s32ds   mikedoidge_1-1624918522979.png
查看全文
S32DS ARM2.2 K144xx fPic Example description. Provided example demonstrate possibility of creation Position Independent Code using  standard  S32DS ARM 2.2 tools.  Example code blink RGB LED using svc interrupt handler. Output  picExample.bin should be loaded via restore gdb command only into existing K144 RAM area(0x1fff8000 – 20007000 for EVB board), then pc set to startup value.(see picExample_Debug_RAM_PNE_fpic  Debug configuration). Note: restore gdb command needs absolute path to *.bin file. Example is based on standard K144 application. Changes: -fPIC option should be set(Project->Properties->C/C++ Build ->Settings->Standard S32DS Compiler->Miscalenous->Position Independent Code). Create flash image checkbox should bes set.( Project->Properties->Cross Settings -> Create flash image). Flash Image output file format  should be set to Raw binary(Project->Properties->C/C++ Build ->Settings->Standard S32DS Create Flash Image ) Add -nostdlib linker option(Project->Properties->C/C++ Build ->Settings->Standard S32DS Linker->General ->No startup or default libs). Existing S was modified(stack pointer was corrected, bl instead of blx for function calls was used. Standard linker script was modified(see example) Interrupts vector table was moved to data area. Due to this vector addresses are corrected on startup by FixGot routine(see SystemInit()c) Common RAM area was declared starting from 0. __got_start and __got_end were declared in Global Offset Table   For an in-depth analysis and step-by-step guide on the topic of implementing position-independent code, please see the following blog at mcuoneclipse.com: Position-Independent Code With GCC for arm Cortex M 
查看全文
Hi,     With S32DS and multilink, you can try the follow steps to dump flash or RAM data into file.  1. Attach    (https://community.nxp.com/t5/S32-Design-Studio/How-attach-to-running-program/m-p/1030375) 2. Export the data which you need    (https://community.nxp.com/t5/S32-Design-Studio/S32DS-how-to-properly-dump-RAM-in-debug-session/m-p/649974#M1089) Cheers! Oliver
查看全文
This document details the steps to program external EEPROM with the 32 reset configuration bits in support of the 'Boot from serial RCON' method detailed in the S32R Reference Manual. The Python scripts used for this task are designed and tested to work on the S32R45 EVB and the Atmel AT24C01C it contains.   The RCON can be set by the following: Fuses (internal to the device) Parallel (GPIO pins/DIP Switches on S32R45 EVB) Serial (EEPROM connected via I2C) The Serial option can be programmed using a debug probe connected via JTAG. This enables the RCON to be controlled remotely, assuming the debug probe is setup to allow remote connections.  Preparation Install S32 Design Studio IDE  Install the Development Package for the device you are debugging. This is important as the S32 Debugger support within it contains the device-specific Python scripts required for initialization of the cores.  Connect the S32 Debug Probe to the S32R45 EVB and the host PC containing S32 Design Studio installation. Set BMODE pins to Boot from RCON Set BOOT_CFG[8]=1 on the S32R EVB, for serial RCON mode See the EVB documentation and device reference manual for more details on BOOT_CFG settings, etc.   Procedure  Open cmd window to the S32 Debugger folder where the device-specific scripts are located. C:\NXP\S32DS.3.4\S32DS\tools\S32Debugger\Debugger\scripts\s32r45 Set Python path so correct version is used (if not already set in env vars) set PYTHONPATH=C:\NXP\S32DS.3.4\S32DS\build_tools\msys32\mingw32\lib\python2.7;C:\NXP\S32DS.3.4\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages Edit the python script to adjust the value to be programmed to RCON, s32r45_i2c_RCON.py. Note: The listed examples show only the minimum values required to configure each of the external memory types. Additional settings may be required for your specific application.       Adjust the RCON_DATA for the configuration you wish to program.  Do not adjust RCON_ADDR. Adjust the S32DBG_IP for the IP address of your S32 Debug Probe.  Adjust the INTERACTIVE_MODE Set True, if desired to be prompted in the command window to enter RCON_DATA Set False, if desired to have script automatically enter RCON_DATA, based on the value set within the file. Enter the command to start GDB, passing in the RCON Python script: Windows OS: C:\NXP\S32DS.3.4\S32DS\tools\gdb-arm\arm32-eabi\bin\arm-none-eabi-gdb-py.exe -x s32r45_i2c_RCON.py Linux OS: arm-none-eabi-gdb-py -x .\s32r45_i2c_RCON.py   You may need to press enter a couple of times. If everything worked properly, then the value you programmed will be displayed to the screen. To exit GDB, enter 'quit'. Before performing boot from serial RCON, remember to set BOOT_CFG[8] = 1. See the EVB documentation and device reference manual for more details.
查看全文
The S32 Flash Tool is provided with support for a few QuadSPI flash memory devices which are typically the devices provided as part of the standard NXP EVB for each of the support NXP Automotive Processors. This will work for most users, but some may select a device for which support is not included with the tool. The FlashSDK was created to provide an easy method for adding support for additional QuadSPI flash memory devices to the S32 Flash Tool. First, a brief explanation of how the S32 Flash Tool works. The S32 Flash Tool programs external flash devices such as QuadSPI, SD, MMC, and eMMC. For each external flash device, there is a flash device-specific flash algorithm file. This flash algorithm file is downloaded by S32 Flash Tool to the target device SRAM, where it will be executed by the target device BootROM. The S32 Flash Tool then sends commands to the flash algorithm along with the image to be programmed to external flash. The flash algorithm will perform the programming of the image to the external flash device. The Flash SDK provides the capability to produce new flash algorithm files, which could then be uploaded to the target device by the S32 Flash Tool and then used to program images to the associated external flash device. The FlashSDK is provided in the form of a S32 Design Studio for S32 Platform v3.x project. This example project, as provided, will build and output a binary file similar to the MX25UM51245G.bin, MX25UW51245G.bin files included in the S32 Flash Tool. The project is designed to build for the Arm M7 core. It is located within the S32 Flash Tool installation directory and inside the folder 'FlashSDK_Ext'. For example, since the S32 Flash Tool is included within the S32 Design Studio 3.x, if the default installation settings were used, this could be found at the path: C:\NXP\S32DS.3.x\S32DS\tools\S32FlashTool\FlashSDK_Ext There is some limited documentation included with the FlashSDK, it can be found by navigating to the '...\FlashSDK_Ext\doc\html' directory and then open 'index.html' with your web browser. In this document, an example process for using the FlashSDK to produce a new binary file will be detailed. Prerequisites Install S32 Design Studio Locate or prepare an image file to be programmed to flash memory Setup hardware to Serial Boot mode Procedure Launch the S32 Design Studio Import the FlashSDK project, using copy to workspace option to preserve the original project. File -> Import image.png Select 'Existing Projects from Workspace' image.png Click 'Browse', locate and then select the 'FlashSDK_Ext' folder, check the box for 'Copy projects into the workspace' image.png Open source files. The files in the project which should be modified for a new flash device are: ...\FlashSDK\Algo\Generic\qSPI_Algorithm.c and qSPI_chip_commands.h Locate the files within the Project Explorer and double click them to open them in the editor. image.png Edit source files. The header file 'qSPI_chip_commands.h' contains many #defines for the flash memory chip which should be adjusted to your new device. Please refer to the reference manual provided by the flash device manufacturer for details on the correct values. As you can see, it is currently setup for the MX25UM51245G device from Macronix. image.png Build the project. The project is setup for 2 build types for you, Debug and Release. The Release build type is more efficient and will run faster, and the Debug build type will allow you to run the debugger in attach mode to investigate issues with the changes you've made. image.png Test new binary on the target and flash memory device. Follow the usual steps to use the S32 Flash Tool.
查看全文
This instruction details the steps to create an image vector table, then subsequently generate a blob image which can be written to external flash on the S32R45 EVB. For this, the 'hello_world_s32r45' example project from the S32R45 SDK installed to S32 Design Studio IDE. This instruction shows the process for QSPI, however, SD, MMC, and eMMC are also supported.   The Image Vector Table (IVT) image is a set of pointers to other images which are required by the BootROM. It typically contains the following images, though not all are required to create a valid IVT image: DCD Self-Test DCD HSE Application Bootloader   The IVT Tool enables configuration and generation of the IVT image as specified in the BootROM reference manual.   Prerequisites Before using the IVT Tool, it will be useful to have already generated the binary image from your application project, it will be an input to the IVT. It may also be necessary to include a DCD image, for example, to initialize the SRAM. For application bootloader image, follow the steps in HOWTO: Generate S-Record/Intel HEX/Binary file, selecting 'Raw binary' option. For DCD image, follow the steps in HOWTO: Use DCD Tool To Create A Device Configuration Data Image .     Procedure With desired project open in project explorer (C/C++ perspective), switch to IVT perspective. Click on 'Open IVT'. In the Boot Configuration section, check that the correct Boot Target is selected. For the demonstration here, M7_0 is the correct selection. Check the 'Interface selection' section. If your intended boot device is SD, MMC or eMMC, then change the setting from QuadSPI Serial Flash. If your intended boot device is QuadSPI AND you do not have a QuadSPI parameter file to specify, then uncheck the box for 'Configure QuadSPI parameters'. QuadSPI parameters change some flash registers' settings away from the default setting and are generally required for larger memory sizes (for ex. applications over 1 MB in size, for some supported devices). From the Image Table section, depending on your configuration, turn off all unused images. For the demonstration here, the following will be changed to Reserved: Self-Test DCD, Self-Test DCD (backup), DCD (backup), Application bootloader (backup). The following images will remain enabled: DCD, Application bootloader. In DCD section of the Image Table, click 'Browse File' and select the DCD binary file. Ignore the red shading on the Start address and Size in bytes fields for now. Now the red shading should be resolved. This is appearing because when the DCD section was enabled, it added a block to the Memory Layout map. But the other blocks in the map are unchanged resulting in overlaps. To resolve this, click on the ‘Align’ button from within the Automatic Align section.. After the Memory Map has been aligned, a confirmation message will be displayed and the red shading will disappear. In Application bootloader section, again use  'Browse File' and select the application binary. When the application boot image is loaded, the tool processes the file to check if it contains the header for the application bootloader image. If the header is not found, it means that the file is only the raw code (the bin generated by S32 Design Studio) and it will be necessary to provide the values for RAM start & entry addresses (code length is automatically calculated), as noted with the expanded view and red shading. To set the RAM start pointer and entry pointer addresses, from to the C/C++ perspective: From Project Explorer on the C/C++ perspective, open the linker file (hello_world_s32r45\Project_Settings\Linker_Files\S32R45_common_ram.ld) and locate the RAM start address and enter it in both the RAM start pointer AND RAM entry pointer fields in the IVT Tool. Since the application binary file which was loaded is just a raw binary file, it is necessary to generate the full application bootloader image. The Export Image function takes the values entered for the RAM start & entry pointers and Code length, then generates the Application bootloader header. This header is added to the raw binary file producing a new image, the full application bootloader image file. Within the Application bootloader section, click 'Export Image' and enter a meaningful name for the image file. In addition to being a necessary source component of the IVT image, this file can more easily be shared or re-used to as an input to other IVT images. After the file has been generated, you will notice that the address settings section has collapsed. This is because it has replaced the file you originally selected with the newly generated one and the tool has recognized that the file contains the required header information. Click 'Export Blob Image' to generate the blob image file. This is what will be flashed to the target. Now that the Blob Image is generated, the 'Flash Image' button could be used to program the image to the target over serial connection, use the S32 Flash Tool, or over the JTAG connection using the Flash Programmer within the S32 Debugger (QSPI only).
查看全文
On reset, all module registers have default values. These settings are typically not ideal for achieving optimal system performance. Also, some peripherals must be configured before they can be used. DCD is the configuration information contained in the DCD image that BootROM uses to configure peripherals on the device. BootROM determines the location of the DCD table from the associated pointer in the IVT.   The main functionality of the DCD Tool is to generate the Device Configuration Data (DCD) image using the format and constraints as specified in the Boot ROM reference manual.   In the steps below, an example process for creating the DCD binary for initializing SRAM is shown. To initialize the SRAM, a logic '1' must be written to the INITREQ bit within the PRAMCR register of the SRAMC and SRAMC_1 peripherals.   Procedure With a project open in project explorer (C/C++ perspective), switch to DCD perspective. Click on the arrow next to the 'Open S32 Configuration' button and select 'Open DCD'. Check that correct project is selected  In DCD Commands panel, select Command Type 'Write', then click 'Set' Click 'Add Register', then set the following settings. Can start typing the names to filter the list for faster setting selection.   For Peripheral setting, select 'SRAMC'. You can search for it by typing the name. Register setting, select 'PRAMCR'. The list is short, so it is not necessary to type the name. In Bitfields, select 'INITREQ' Now click on the highlighted bit to set it. Again using 'New Command' box, repeat settings of steps 3 & 4, however, this time select Peripheral 'SRAMC_1'. If everything was done correctly, in the DCD Binary panel to the right, should appear as shown. If so, click 'Export'. The generated DCD file will be displayed. By default, C format is selected. Select Binary format and click OK. Select a location to save the file (such as the project folder in the workspace directory) and give it a meaningful name. Click Save. You are done! DCD image file is created in binary format and ready to be imported to IVT Tool.  
查看全文
Trace functionality is supported in the S32 Debugger for A53 cores on the S32R, RAM-target builds. With Trace, you can record some execution data on an application project and then review it to determine the actions and data surrounding an event of interest.   This document outlines the method to begin using Trace on the S32R45 device. We start by creating a project on which to execute the trace, however, you may start at step 2, if you are starting with an existing project. Please note, you will need to have debug configurations for the S32 Debugger setup for each core which you intend to capture trace. If you do not already have such configurations, you may copy them from another project and adapt them to the new project as shown in HOWTO: Add a new debugger configuration to an existing project.   Create a new application project, selecting the 'S32R45 Cortex-A53' processor and 'S32 Debugger' options.  There should now be 4 new application projects in your workspace. One for each A53 core. The first core of the S32R45, A53_0_0, is also a possible boot core, so this project will have build configurations for RAM and FLASH. The other A53 cores (0_1, 1_0, 1_1) will not. Build all projects for Debug_RAM and check that they build clean before proceeding. Open 'Debug Configurations...' and select the 'Debug_RAM' configuration for the first core (A53_0_0_Debug_RAM_S32Debug). Select the 'Debugger' tab. Enter the Debug Probe Connection settings as appropriate for your hardware setup. Click Apply. Now select the Launch Group configuration for 'Debug_RAM'. It is important to use the launch group to start the debug for each core, not just because it makes it easier, but also because it is necessary to allow for some delay after the first A53 core is started before bringing the other A53 cores from reset to debug state. Press Debug Once the code is loaded to the target and the debugger has started each core and executed to the first line within main(), then it is ready to perform any of the standard debug functions including Trace. Trace does not start automatically, it must be turned on before it will start logging data. To do this, it is necessary to add the view 'Trace Commander'. It can be found by either Window -> Show View -> Other, then search for 'Trace Commander' or enter 'Trace Commander' in the Quick Access field of the toolbar and select Trace Commander from the list. The Trace Commander view will show in the panel with the Console, Problems, etc. Double-click on the tab to enlarge it. Click on the configure button to change settings. Click on the Advanced Trace Generators configuration button For each core to be logged, set the associated ELF file. Select the core, click Add, then '...', and select the elf file for that core. Select Data Streams. Now it is possible to change how the data is captured. Since the buffers have finite memory, they can be set to collect data until full, or to overwrite. If set to One buffer, the data will be collected until the buffer is full, then data collection stops. It is useful to gather data when starting logging from a breakpoint to gather data during execution of a specific section of code. If set to Overwrite, the data collection continues and starts overwriting itself once the buffer is full. This is useful when trying to gather data prior to a breakpoint triggered by a condition.  To turn on the Trace logging, click on the 'Close this trace stream' button. The Trace is now enabled. To collect trace data, the cores must be executing. First double-click the Trace Commander tab to return to the normal Debug Perspective view. Then, one by one, select the main() thread on each core and press Resume to start them all. If collecting from a breakpoint, start the code first with Trace disabled, wait for the breakpoint to be reached, then enable the Trace. Allow the cores to run for a period of time to gather the data, then press Suspend on each one until they are all suspended. Look to the Trace Commander tab to see that the data icon is no longer shaded and click on it to upload the trace data. A new tab, Analysis Results, has appeared. Double-click this tab to see it better. Click on the arrow next to ETF 0 to show the data collected in the trace buffer. Notice there are 5 separate views on the captured data: Trace (raw data), Timeline, Code Coverage, Performance, and Call Tree. Trace - this is the fully decoded trace data log Timeline - displays the functions that are executed in the application and the number of cycles each function takes, separate tabs for each core Code Coverage - displays the summarized data of a function in a tabular form, separate tabs for each core Performance - displays the function performance data in the upper summary table and the call pair data for the selected function and it's calling function Call Tree - shows the call tree for identification of the depth of stack utilization See the S32DS Software Analysis Documentation for more details on settings, ways to store the logged data, etc.
查看全文
Trace functionality is supported in the S32 Debugger for A53 cores on the S32V, RAM-target builds. With Trace, you can record some execution data on an application project and then review it to determine the actions and data surrounding an event of interest.   This document outlines the method to begin using Trace on the S32V234 device. We start by creating a project on which to execute the trace, however, you may start at step 2, if you are starting with an existing project. Please note, you will need to have debug configurations for the S32 Debugger setup for each core which you intend to capture trace. If you do not already have such configurations, you may copy them from another project and adapt them to the new project as shown in HOWTO: Add a new debugger configuration to an existing project.   Create a new application project, selecting the 'S32V234 Cortex-A53' processor and 'S32 Debugger' options.  image.png image.png There should now be 4 new application projects in your workspace. One for each A53 core. The first core of the S32V234, A53_0_0, is also a possible boot core, so this project will have build configurations for RAM and FLASH. The other A53 cores (0_1, 1_0, 1_1) will not. Build all projects for Debug_RAM and check that they build clean before proceeding. Open 'Debug Configurations...' and select the 'Debug_RAM' configuration for the first core (A53_0_0_Debug_RAM_S32Debug). Select the 'Debugger' tab. Enter the Debug Probe Connection settings as appropriate for your hardware setup. image.png Now select the Launch Group configuration for 'Debug_RAM'. It is important to use the launch group to start the debug for each core, not just because it makes it easier, but also because it is necessary to allow for some delay after the first A53 core is started before bringing the other A53 cores from reset to debug state. Press Debug Once the code is loaded to the target and the debugger has started each core and executed to the first line within main(), then it is ready to perform any of the standard debug functions including Trace. Trace does not start automatically, it must be turned on before it will start logging data. To do this, it is necessary to add the view 'Trace Commander'. It can be found by either Window -> Show View -> Other, then search for 'Trace Commander' or enter 'Trace Commander' in the Quick Access field of the toolbar and select Trace Commander from the list. The Trace Commander view will show in the panel with the Console, Problems, etc. Double-click on the tab to enlarge it. image.png Click on the configure button to change settings. image.png Click on the Advanced Trace Generators configuration button For each core to be logged, set the associated ELF file. Select the core, click Add, then '...', and select the elf file for that core. image.png Select Data Streams. Now it is possible to change how the data is captured. Since the buffers have finite memory, they can be set to collect data until full, or to overwrite. If set to One buffer, the data will be collected until the buffer is full, then data collection stops. It is useful to gather data when starting logging from a breakpoint to gather data during execution of a specific section of code. If set to Overwrite, the data collection continues and starts overwriting itself once the buffer is full. This is useful when trying to gather data prior to a breakpoint triggered by a condition.  image.png To turn on the Trace logging, click on the 'Close this trace stream' button. image.png The Trace is now enabled. To collect trace data, the cores must be executing. First double-click the Trace Commander tab to return to the normal Debug Perspective view. Then, one by one, select the main() thread on each core and press Resume to start them all. If collecting from a breakpoint, start the code first with Trace disabled, wait for the breakpoint to be reached, then enable the Trace. image.png Allow the cores to run for a period of time to gather the data, then press Suspend on each one until they are all suspended. image.png Look to the Trace Commander tab to see that the data icon is no longer shaded and click on it to upload the trace data. image.png A new tab, Analysis Results, has appeared. Double-click this tab to see it better. Click on the arrow next to ETF 0 to show the data collected in the trace buffer. image.png Notice there are 5 separate views on the captured data: Trace (raw data), Timeline, Code Coverage, Performance, and Call Tree. Trace - this is the fully decoded trace data log image.png Timeline - displays the functions that are executed in the application and the number of cycles each function takes, separate tabs for each core Code Coverage - displays the summarized data of a function in a tabular form, separate tabs for each core Performance - displays the function performance data in the upper summary table and the call pair data for the selected function and it's calling function Call Tree - shows the call tree for identification of the depth of stack utilization See the S32DS Software Analysis Documentation for more details on settings, ways to store the logged data, etc.
查看全文
Hi: I just wonder whether I can use S32 debug probe for S32K3 EVB in S32DS 3.4? I couldn't locate script and algorism for S32K3xx. Thanks.
查看全文
This document details the steps to program external EEPROM with the 32 reset configuration bits in support of the 'Boot from serial RCON' method detailed in the S32G Reference Manual. The Python scripts used for this task are designed and tested to work on the S32G-VNP-EVB with S32G2xx Rev2 and the Atmel AT24C01C it contains.(Serial EEPROM is not implemented on NXP VNP-RDB board)   The RCON can be set by the following: Fuses (internal to the device) Parallel (GPIO pins/DIP Switches on EVB) Serial (EEPROM connected via I2C) The Serial option can be programmed using a debug probe connected via JTAG. This enables the RCON to be controlled remotely, assuming the debug probe is setup to allow remote connections.    Preparation Install S32 Design Studio IDE  Install the Development Package for the device you are debugging. This is important as the S32 Debugger provides access to the EEPROM programming capabilities via I2C of the S32 Debug Probe.  Connect the S32 Debug Probe to the S32G-VNP-EVB and the host PC containing S32 Design Studio installation. Set BOOTMOD pins to boot from RCON Set BOOT_CFG[8]=1 on the S32G-VNP-EVB, for serial RCON mode VNP-EVB shown here with switch BOOT_CFG[8] = 0 See the EVB documentation and device reference manual for more details. Procedure   Open cmd window to the S32 Debugger folder where the device-specific scripts are located. C:\NXP\S32DS.3.4\S32DS\tools\S32Debugger\Debugger\scripts\s32g2xx Set Python path so correct version is used (if not already set in env vars) set PYTHONPATH=C:\NXP\S32DS.3.4\S32DS\build_tools\msys32\mingw32\lib\python2.7;C:\NXP\S32DS.3.4\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages Edit the python script to adjust the value to be programmed to RCON, s32g2xx_i2c_RCON.py. Note: The listed examples show only the minimum values required to configure each of the external memory types. Additional settings may be required for your specific application. Adjust the RCON_DATA for the configuration you wish to program.  Do not adjust RCON_ADDR. Adjust the S32DBG_IP for the IP address of your S32 Debug Probe.  Adjust the INTERACTIVE_MODE  Set True, if desired to be prompted to enter RCON_DATA Set False, if desired to have script automatically enter RCON_DATA, based on the value set within the file. Adjust _SOC_NAME as appropriate for the specific S32G2xx device you are using. The valid options are defined in s32g2xx_context.py. Enter the command to start GDB, passing in the RCON Python script: Windows OS: C:\NXP\S32DS.3.4\S32DS\build_tools\gcc_b1620\gcc-6.3-arm32-eabi\bin\arm-none-eabi-gdb-py.exe -x s32g2xx_i2c_RCON.py OR C:\NXP\S32DS.3.4\S32DS\build_tools\gcc_v9.2\gcc-9.2-arm32-eabi\bin\arm-none-eabi-gdb-py.exe -x s32g2xx_i2c_RCON.py Linux OS: arm-none-eabi-gdb-py -x .\s32g274a_i2c_RCON.py If everything worked properly, then the value you programmed will be displayed to the screen. To exit GDB, enter 'quit'.
查看全文
NXP devices can be secured either with password or challenge and response authentication scheme. The S32 Debugger included within the S32 Design Studio for S32 Platform IDE with the S32 Debug Probe provides the ability to debug a secured device. This document provides only the necessary commands specific to launching a debug session on secured NXP devices.. Once the device is unsecured, it will remain so until a power-on-reset or destructive reset occurs. Preparation Setup the software tools Install S32 Design Studio for S32 Platform Install the Development Package for the device you are debugging. In this case, the S32R4xx development package. This package is important as it contains the S32 Debugger support component Setup the hardware Confirm the setup of the S32R45 evaluation board. Connect the power supply cable Setup the S32 Debug Probe. Refer to the S32 Debug Probe User Manual for installation instructions. Connect the S32 Debug Probe to the evaluation board via JTAG cable. Connect the S32 Debug Probe to the host PC via USB cable OR via Ethernet cable (via LAN or directly connected and configured for static IP address) and power supply connected to USB port. Launch S32 Design Studio for S32 Platform Open existing project or create a new project and check that it successfully builds. If creating a new project, be sure the S32 Debugger is selected in the New Project Wizard. Procedure Before starting a secure debug session, first confirm that the device is indeed secure. Once one core is unlocked, all cores are unlocked and will remain so until a power-on-reset or destructive reset occurs. After confirming the device is secured, then select the procedure which applies to the lifecycle of the SoC to be debugged.   Check the state of the SoC Open a command window from the installation directory containing the GTA server: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\Server\gta\ Execute the following command: gta.exe -t s32dbg This will invoke a utility that launces a new GTA server instance and then communicates with the target via the S32 Debug Probe and will request a set of properties of the SoC. These properties are available to be read regardless of security state. The GTA server will close once the information is returned. As is shown above, the Debug state is ‘Locked’. This means it is secured and the secure debug steps outlined within this document must be used. There is no way to determine the security enabled on the SoC, so this should be known by the user in order to select the correct authentication scheme. Proceed from here using the method (Password or Challenge & Response) which applies for your SoC security configuration. Password From S32DS, open the Debug Configurations menu, select the configuration for the project you wish to debug, select the ‘Debugger’ tab and scroll down until the ‘Secure debugging’ section is visible. Check the box for ‘Enable secure debugging’ and then select the Debugging type ‘Password’. Click Debug. When the debug session initialization reaches the stage where the password must be entered to unsecure the SoC, the following menu will appear. Enter the password. This is a 16-byte value entered as a hexadecimal without the leading ‘0x’. If you choose to check the box for ‘Store keyword in secure storage’, the value entered will be stored within the Eclipse secure storage and will remain available for the duration of the current S32DS instance. This saves the user from having to enter the password again, should the security state of the SoC becomes once again secured. Now the debug session initialization will complete and debug activities may be executed as with any SoC which is not secured. After terminating the debug session, the GTA utility can be used again to see the new state of the SoC. This utility cannot be executed while the debug session is running. It launches a new instance of the GTA server, which would be blocked by the already running debug session. Challenge & Response For the Challenge & Response security scheme, the included Volkano Browser must be used. From the S32DS menu bar, select Window -> Show View -> Other -> ‘Volkano Browser’. The Volkano Browser will now appear in the current perspective. Since there is no current key stored in the Volkano local storage, a new key must be registered. Click on ‘Register Key’ to register a new key. This will bring up the Volkano command dialog. Now enter the ADKP value (Application Debug Key/Password) which is correct for the SoC to be debugged. The Volkano utility uses the same functionality as the command-line GTA utility shown earlier to check the state of the SoC. This will read the UID from the Soc. Click Connect to the SoC and load the UID (Device Unique ID). The UID is associated with the ADKP when it is registered within the Volkano local storage for easier access in the future. Click OK to complete the registration of the new key. Now the key is registered, the debug session can be setup and started. Open the Debug Configurations menu, select the configuration for the project you wish to debug, select the ‘Debugger’ tab and scroll down until the ‘Secure debugging’ section is visible. Check the box for ‘Enable secure debugging’ and then select the Debugging type ‘Challenge & Response’. Click Debug. Now the debug session initialization will complete and debug activities may be executed as with any SoC which is not secured. During debug session initialization, the key that was registered will be used to unsecure the SoC. After terminating the debug session, the GTA utility used earlier can be used again to see the new state of the SoC. This utility cannot be executed while the debug session is running. It launches a new instance of the GTA server, which would be blocked by the already running debug session. Troubleshooting There are some messages displayed when things go wrong that can help to identify the cause of the issue. Due to the sensitive nature of the Secure Debug, the error indications detailed below are inherently general and are provided as a guide for interpreting them to determine the likely cause. Debug session started when SoC is still secured There is an error message reported in the S32 Debugger Console to indicate the SoC is still secure. To see this message the GDB Server log must be enabled in Debug Configurations -> Debugger tab, GDB Server section: When this error is incurred, first indication is popup error message for Error code 102: Next, the following text will be displayed in the S32 Debugger console window: If needed, select this view from the menu: In addition, if GDB Traces log is enabled, the following error message can be found in the gdb traces console view: Enable the GDB Traces log in Window->Preferences, then search on GDB: To select the view from console: Incorrect Challenge/Response Or Password If the SoC is setup for Challenge & Response security scheme, but Password security scheme is selected in Debug Configuration, or Challenge & Response is correctly selected but the wrong ADKP value is provided, below are the expected error messages. The result is same if the SoC is setup for Password and either Challenge & Response or wrong password is used. First error message is Error code 601: Next, the gdb traces console displays the following error: There is no error displayed in the S32 Debugger console.
查看全文
NXP devices can be secured either with password or challenge and response authentication scheme. The S32 Debugger included within the S32 Design Studio for S32 Platform IDE with the S32 Debug Probe provides the ability to debug a secured device. This document provides only the necessary commands specific to launching a debug session on secured NXP devices.. Once the device is unsecured, it will remain so until a power-on-reset or destructive reset occurs. Preparation Setup the software tools Install S32 Design Studio for S32 Platform Install the Development Package for the device you are debugging. In this case, the S32G2xx development package. This package is important as it contains the S32 Debugger support component Setup the hardware Confirm the setup of the S32G274A evaluation board. Connect the power supply cable Setup the S32 Debug Probe. Refer to the S32 Debug Probe User Manual for installation instructions. Connect the S32 Debug Probe to the evaluation board via JTAG cable. Connect the S32 Debug Probe to the host PC via USB cable OR via Ethernet cable (via LAN or directly connected and configured for static IP address) and power supply connected to USB port. Launch S32 Design Studio for S32 Platform Open existing project or create a new project and check that it successfully builds. If creating a new project, be sure the S32 Debugger is selected in the New Project Wizard.     Procedure Before starting a secure debug session, first confirm that the device is indeed secure. Once one core is unlocked, all cores are unlocked and will remain so until a power-on-reset or destructive reset occurs. After confirming the device is secured, then select the procedure which applies to the lifecycle of the SoC to be debugged.   Check the state of the SoC Open a command window from the installation directory containing the GTA server: {S32DS Install Path}\S32DS\tools\S32Debugger\Debugger\Server\gta\ Execute the following command: gta.exe -t s32dbg This will invoke a utility that launces a new GTA server instance and then communicates with the target via the S32 Debug Probe and will request a set of properties of the SoC. These properties are available to be read regardless of security state. The GTA server will close once the information is returned. As is shown above, the Debug state is ‘Locked’. This means it is secured and the secure debug steps outlined within this document must be used. There is no way to determine the security enabled on the SoC, so this should be known by the user in order to select the correct authentication scheme. Proceed from here using the method (Password or Challenge & Response) which applies for your SoC security configuration. Password From S32DS, open the Debug Configurations menu, select the configuration for the project you wish to debug, select the ‘Debugger’ tab and scroll down until the ‘Secure debugging’ section is visible. Check the box for ‘Enable secure debugging’ and then select the Debugging type ‘Password’. Click Debug. When the debug session initialization reaches the stage where the password must be entered to unsecure the SoC, the following menu will appear. Enter the password. This is a 16-byte value entered as a hexadecimal without the leading ‘0x’. If you choose to check the box for ‘Store keyword in secure storage’, the value entered will be stored within the Eclipse secure storage and will remain available for the duration of the current S32DS instance. This saves the user from having to enter the password again, should the security state of the SoC becomes once again secured. Now the debug session initialization will complete and debug activities may be executed as with any SoC which is not secured. After terminating the debug session, the GTA utility can be used again to see the new state of the SoC. This utility cannot be executed while the debug session is running. It launches a new instance of the GTA server, which would be blocked by the already running debug session. Challenge & Response For the Challenge & Response security scheme, the included Volkano Browser must be used. From the S32DS menu bar, select Window -> Show View -> Other -> ‘Volkano Browser’. The Volkano Browser will now appear in the current perspective. Since there is no current key stored in the Volkano local storage, a new key must be registered. Click on ‘Register Key’ to register a new key. This will bring up the Volkano command dialog. Now enter the ADKP value (Application Debug Key/Password) which is correct for the SoC to be debugged. The Volkano utility uses the same functionality as the command-line GTA utility shown earlier to check the state of the SoC. This will read the UID from the Soc. Click Connect to the SoC and load the UID (Device Unique ID). The UID is associated with the ADKP when it is registered within the Volkano local storage for easier access in the future. Click OK to complete the registration of the new key. Now the key is registered, the debug session can be setup and started. Open the Debug Configurations menu, select the configuration for the project you wish to debug, select the ‘Debugger’ tab and scroll down until the ‘Secure debugging’ section is visible. Check the box for ‘Enable secure debugging’ and then select the Debugging type ‘Challenge & Response’. Click Debug. Now the debug session initialization will complete and debug activities may be executed as with any SoC which is not secured. During debug session initialization, the key that was registered will be used to unsecure the SoC. After terminating the debug session, the GTA utility used earlier can be used again to see the new state of the SoC. This utility cannot be executed while the debug session is running. It launches a new instance of the GTA server, which would be blocked by the already running debug session. Troubleshooting There are some messages displayed when things go wrong that can help to identify the cause of the issue. Due to the sensitive nature of the Secure Debug, the error indications detailed below are inherently general and are provided as a guide for interpreting them to determine the likely cause. Debug session started when SoC is still secured There is an error message reported in the S32 Debugger Console to indicate the SoC is still secure. To see this message the GDB Server log must be enabled in Debug Configurations -> Debugger tab, GDB Server section: When this error is incurred, first indication is popup error message for Error code 102: Next, the following text will be displayed in the S32 Debugger console window: If needed, select this view from the menu: In addition, if GDB Traces log is enabled, the following error message can be found in the gdb traces console view: Enable the GDB Traces log in Window->Preferences, then search on GDB: To select the view from console: Incorrect Challenge/Response Or Password If the SoC is setup for Challenge & Response security scheme, but Password security scheme is selected in Debug Configuration, or Challenge & Response is correctly selected but the wrong ADKP value is provided, below are the expected error messages. The result is same if the SoC is setup for Password and either Challenge & Response or wrong password is used. First error message is Error code 601: Next, the gdb traces console displays the following error: There is no error displayed in the S32 Debugger console.
查看全文
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio v3.4 Vision Extension Package for S32V23x 1.3.0          What is new? Integrated VSDK 1.7.0   Installation instructions The update is available for online installation (via S32DS Extensions and Updates) or offline installation (direct download link)  installation:  go to menu "Help" -> "S32DS Extensions and Updates" dialog  select from available items and click "Install/Update" button image.png offline installation:   go to S32 Design Studio for S32 Platform product page -> Downloads section or use direct link to download the update archive zip file        image.png Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates", then click 'Add Update Sites' link image.png Select the downloaded update archive zip file you downloaded in the previous step       image.png Select the 'Vision extension package for S32V23x' package and click "Install/Update" button.   image.png This will start the update installation process.
查看全文
**************************************************************************************** IDE: S32 Design Studio Version 3.4 Workspace: C:\Projects\S32DS_3_4 Project name: S32K314_00_blank_00 Project location: C:\Projects\S32DS_3_4\S32K314_00_blank_00 **************************************************************************************** 1. After you finish the edit on your codes, please close S32DS 2. Input the command(as below) at your clean_and_build_s32k3_commandLine.bat clean_build.png 3. Run command prompt with Administrator right. 4. Run clean_and_build_s32k3_commandLine.bat at command prompt   You will get the *.elf under the folder of C:\Projects\S32DS_3_4\S32K314_00_blank_00\Debug_FLASH Cheers! Oliver
查看全文
Installation & Activation HOWTO: Install Lauterbach TRACE32 debugger plug-in into S32 Design Studio HOWTO: Install IAR Eclipse plug-in into S32 Design Studio for ARM  HOWTO: Activate S32 Design Studio     Getting Started HOWTO: Create a New Project in S32 Design Studio for ARM  HOWTO: Create S32DS Project from Example 'Hello World' for S32K144 (w/o SDK)    Build tools & Standard libraries  HOWTO: Build a Project and Setup a Debug Configuration for debugging in S32 Design Studio  HOWTO: Add a static library file into S32 Design Studio GCC project HOWTO: Place custom data into flash memory  HOWTO: Link a binary file(s) into the application project using GNU build tools HOWTO: Execute a library function from RAM memory using GNU build tools  NEW!   Debug  & Flash Programming HOWTO: download separate elf/srec/hex file to microcontroller using S32 Design Studio  HOWTO: Update OpenSDA Firmware on EVB Using GDB Server Monitor Commands from Eclipse GDB Console  HOWTO: Debug multiple elf files in S32 Design Studio with GDB  HOWTO: Reset MCU in S32 Design Studio debugger (Pemicro/OpenSDA interface) Debugging the Startup Code with Eclipse and GDB | MCU on Eclipse   https://community.nxp.com/docs/DOC-345344  HOWTO: Program multiple memory types in single debug session NEW!   S32 SDK & Other SDKs HOWTO: Create FreeRTOS project in S32 Design Studio How to change package on S32DS Processor Expert  HOWTO: Create the Blinking LED example project using S32K144 SDK  HOWTO: Show FreeRTOS Threads in Eclipse Debug View with Segger J-link and NXP S32 Design Studio  Tutorial: FreeRTOS 10.0.1 with NXP S32 Design Studio 2018.R1  Using custom FreeRTOS with S32K SDK and OSIF for ARM | MCU on Eclipse  Implementing FreeRTOS Performance Counters on ARM Cortex-M | MCU on Eclipse  HOWTO: Change the CPU Derivative in an SDK-Based Application Project  HOWTO: Working with AMMCLib SDKs  HOWTO: Working with FreeMASTER SDKs  HOWTO: Add custom SDK into existing project   HOWTO: Use SDK based example code as standalone (usable for GIT, SVN...)  NEW!   General Usage HOWTO: S32 Design Studio Command Line Interface  HOWTO: Add user example into S32DS HOWTO: Generate S-Record/Intel HEX/Binary file  HOWTO: Update S32 Design Studio  HOWTO: Set project optimization level  HOWTO: Export S32DS Project to IAR EW (S32K14x/S32K11x)  NEW!   Troubleshooting Troubleshooting: PEmicro Debug Connection: Target Communication Speed  Troubleshooting: Indexer errors on header file  S32 Design Studio Offline activation issue hot fix  Troubleshooting: Installer rolls back immediately following activation code entry  Troubleshooting: Activation fails with error message FNP ERROR 0 
查看全文
Project created by S32 Design Studio (S32DS) new project wizard typically contains the debugger configurations to load  and debug the project into the code memory (Flash/RAM). However there might be situations that require also to load a content/data (e.g. calibration values) into a special on-chip memory (such as shadow flash, data flash, utest flash...) or an external memory (QSPI). This document describes how to program multiple memory types (using different programming algorithms) just by single click on the debug button. The decription applies to PEMICRO probes (Multilink Universal, Multilink FX or OpenSDA) anyway a similar approach might be applicable for other vendor probes. The process can be splitted into two steps: 1. create a separate debugger configurations to program a specific memory modules(QSPI,  data flash,..) 2. associate the program and debug configurations into the single launch group  - this alows to execute multiple actions by invoking the single debug launch . Let's demonstrate this on MPC5744P and program code and data flash memory using S32DS for Power v2.1 (similar approach can be applied also to other architectures/versions of S32DS). •  Create a new empty project for MPC5744P. Such a project typically contains Debug/Debug_RAM debugger configuration. First we will add a dummy code  (see below) that creates a record to be stored into the data flash memory (different to code flash memory block). • The project linker file (MPC57xx_flash.ld) should have the data flash memory block and a linker section associated with data flash (.dflash) defined: MEMORY { dflash : org = 0x00800000, len = 0x1F /* not entire dflash - just for test*/ flash_rchw : org = 0x00FA0000, len = 0x4 cpu0_reset_vec : org = 0x00FA0004, len = 0x4 m_text : org = 0x1000000, len = 2048K m_data : org = 0x40000000, len = 384K local_dmem : org = 0x50800000, len = 64K } SECTIONS { .dflash : { KEEP(*(.dflash)) } > dflash … •Add a test code into main.c that results in creating a dummy data record in data flash memory (0x0800000) __attribute__((section(".dflash"))) volatile char dflash_data[]="DTEST String"; // place the string into .dflash segment int main(void) { volatile int counter = 0; volatile char test_str[10]; test_str[0] = dflash_data[0]; // use DFLASH data (to avoid deadstripping) /* Loop forever */ for(;;) { counter++; } } Now if you build the project you can see the data that belong to dflash and code flash in the .map or srec file. If you debug the project using the default debug configuration data flash (DFLASH) memory is not programmed. To program DFLASH you should create another debug configuration simply by duplicating the existing one and changing the programming algorithm to dflash one: nxp_mpc5744p_1x32x20k_dflash.pcp. Note: There are many flash programming algorithms available in PEMICRO eclipse plugin folder typically located here (version of plugin may vary): "C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.2.202005132054\win32\gdi\P&E\" S32DS: Duplicate Debug Configuration S32DS: Load parameters S32DS: Choose alternative programming algorithmNow the new debug configuration (MPC5744P_code_dflash_Debug_DFLASH) is able to program data flash memory. The final step is to create a launch group configuration and associate it with all the programming/debugging configurations that should be executed once debug is started. S32DS_Debug_Data_Flash_Launch.png Add the debug configuration used just for programming purpose as flash type and code debug configuration as debug type. In order to avoid interference between programming of various memories select post launch action -> "Wait until terminated" S32DS_Debug_Data_Flash_Launch2.png S32DS_Debug_Data_Flash_Launch3.png S32DS_Debug_Data_Flash_Launch4.pngFinally as soon as the debug session is established by launching the launch group created above - all the memories are programmed and you can debug the code. S32DS_Debug_Data_Flash_Final.png Note: There is an information about executed flash configurations in the debug context view. Since the programming has alredy finished the thread is terminated and could be cleared by double cross icon. Enjoy single click programming&debugging in S32 Design Studio!
查看全文