S32DS_3.4 _ Command Line compiling

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS_3.4 _ Command Line compiling

S32DS_3.4 _ Command Line compiling

****************************************************************************************

IDE: S32 Design Studio Version 3.4

Workspace: C:\Projects\S32DS_3_4

Project name: S32K314_00_blank_00

Project location: C:\Projects\S32DS_3_4\S32K314_00_blank_00

****************************************************************************************

1. After you finish the edit on your codes, please close S32DS

2. Input the command(as below) at your clean_and_build_s32k3_commandLine.bat

clean_build.png

3. Run command prompt with Administrator right.

4. Run clean_and_build_s32k3_commandLine.bat at command prompt

 

You will get the *.elf under the folder of C:\Projects\S32DS_3_4\S32K314_00_blank_00\Debug_FLASH


Cheers!

Oliver

Comments

Hi, 

   If you use RTD to generate your project,  then, you need add all the libraries with option -I, like 

   '-I C:\NXP\S32DS_3_4\S32DS\software\SW32K344_RTD_x_x_xx_xxxx\include'

   '-I C:\NXP\S32DS_3_4\S32DS\software\SW32K344_RTD_x_x_xx_xxxx\header'

  Otherwise, error will be happened. 

  Hope you will be successful!

Cheers!

Oliver

 

Dear Team, 

I am getting the error when I am trying to call the eclipse command 

shrey2415_0-1667987465173.png

Do you know if I am missing anything ? 

Hi, 

   You should use "eclipsec.exe".

   

Oliver

Hey @OliverTian 
Thanks 

Dear @OliverTian, I am getting following error while trying to build from command line. 

please support me to resolve, Thanks in advance

prakashkaruppannan_0-1722591546837.png

 

100% helpful (1/1)
Version history
Last update:
‎02-25-2021 09:02 PM
Updated by: