S32DS for ARM - list of HOWTOs

cancel
Showing results for 
Search instead for 
Did you mean: 

S32DS for ARM - list of HOWTOs

No ratings

S32DS for ARM - list of HOWTOs

Installation & Activation

HOWTO: Install Lauterbach TRACE32 debugger plug-in into S32 Design Studio

HOWTO: Install IAR Eclipse plug-in into S32 Design Studio for ARM 

HOWTO: Activate S32 Design Studio  

 

Getting Started

HOWTO: Create a New Project in S32 Design Studio for ARM 

HOWTO: Create S32DS Project from Example 'Hello World' for S32K144 (w/o SDK) 

 

Build tools & Standard libraries 

HOWTO: Build a Project and Setup a Debug Configuration for debugging in S32 Design Studio 

HOWTO: Add a static library file into S32 Design Studio GCC project

HOWTO: Place custom data into flash memory 

HOWTO: Link a binary file(s) into the application project using GNU build tools

HOWTO: Execute a library function from RAM memory using GNU build tools  NEW!

 

Debug  & Flash Programming

HOWTO: download separate elf/srec/hex file to microcontroller using S32 Design Studio 

HOWTO: Update OpenSDA Firmware on EVB

Using GDB Server Monitor Commands from Eclipse GDB Console 

HOWTO: Debug multiple elf files in S32 Design Studio with GDB 

HOWTO: Reset MCU in S32 Design Studio debugger (Pemicro/OpenSDA interface)

Debugging the Startup Code with Eclipse and GDB | MCU on Eclipse  

https://community.nxp.com/docs/DOC-345344 

HOWTO: Program multiple memory types in single debug session NEW!

 

S32 SDK & Other SDKs

HOWTO: Create FreeRTOS project in S32 Design Studio

How to change package on S32DS Processor Expert 

HOWTO: Create the Blinking LED example project using S32K144 SDK 

HOWTO: Show FreeRTOS Threads in Eclipse Debug View with Segger J-link and NXP S32 Design Studio 

Tutorial: FreeRTOS 10.0.1 with NXP S32 Design Studio 2018.R1 

Using custom FreeRTOS with S32K SDK and OSIF for ARM | MCU on Eclipse 

Implementing FreeRTOS Performance Counters on ARM Cortex-M | MCU on Eclipse 

HOWTO: Change the CPU Derivative in an SDK-Based Application Project 

HOWTO: Working with AMMCLib SDKs 

HOWTO: Working with FreeMASTER SDKs 

HOWTO: Add custom SDK into existing project  

HOWTO: Use SDK based example code as standalone (usable for GIT, SVN...)  NEW!

 

General Usage

HOWTO: S32 Design Studio Command Line Interface 

HOWTO: Add user example into S32DS

HOWTO: Generate S-Record/Intel HEX/Binary file 

HOWTO: Update S32 Design Studio 

HOWTO: Set project optimization level 

HOWTO: Export S32DS Project to IAR EW (S32K14x/S32K11x)  NEW!

 

Troubleshooting

Troubleshooting: PEmicro Debug Connection: Target Communication Speed 

Troubleshooting: Indexer errors on header file 

S32 Design Studio Offline activation issue hot fix 

Troubleshooting: Installer rolls back immediately following activation code entry 

Troubleshooting: Activation fails with error message FNP ERROR 0 

Tags (2)
Version history
Last update:
‎01-05-2021 05:38 AM
Updated by: